index d4ebf47d8d96c2221adf91276ca89a68dd92e9d7..f08961779ab8010505cecf91cd485cdfabe1857c 100644 (file)
--- a/RELEASE
+++ b/RELEASE
-GStreamer: Release notes for GStreamer 0.8.6 "Narc"
+Release notes for GStreamer 0.10.35 "Nuclear Fission"
-The GStreamer team is happy to announce a new release
-in the 0.8.x stable series of the GStreamer streaming-media framework.
+The GStreamer team is proud to announce a new release
+in the 0.10.x stable series of the
+core of the GStreamer streaming media framework.
-The 0.8.x series is a stable series aimed at end users.
-It is not API or ABI compatible with the stable 0.6.x series.
-It is, however, parallel installable with the 0.6.x series.
+
+The 0.10.x series is a stable series targeted at end users.
+It is not API or ABI compatible with the stable 0.8.x series.
+It is, however, parallel installable with the 0.8.x series.
+
+
+The 0.10.x series has been reworked for threadsafety. It also features
+various feature additions and enhancements.
+
+
+This module, gstreamer, only contains core functionality.
+For actual media playback, you will need other modules.
+
+gst-plugins-base
+contains a basic set of well-supported plug-ins
+gst-plugins-good
+contains a set of well-supported plug-ins under our preferred license
+gst-plugins-ugly
+contains a set of well-supported plug-ins, but might pose problems for
+ distributors
+gst-plugins-bad
+contains a set of less supported plug-ins that haven't passed the
+ rigorous quality testing we expect
-This module only contains core functionality. For actual media playback,
-you will need other modules. GStreamer Plugins contains a huge set of
-additional plugins. GStreamer FFmpeg contains a plugin based on the popular
-FFmpeg decoding library. These modules need not have the same source version
-as the core, as long as they are in the 0.8.x series.
+
Features of this release
- * Parallel installability with 0.6.x series
- * Internationalization
- * spider, queue fixes
- * fakesrc and identity now have a datarate property
- * dataprotocol threadsafety fix
+ * work around GLib atomic ops API change
+ * some minor win32/mingw fixes
+ * don't use G_CONST_RETURN in public headers
Bugs fixed in this release
-
- * 136962 : crc error when decoding flac with typefind and threads
- * 150001 : [PATCH] Mem leaks in gstpad.c, gstxml.c and gstelement.c
- * 150262 : gstreamer.spec file needs correction to work with rpmbuil...
- * 150626 : bug trying to play a theora web stream
- * 153657 : make typefind prevent unneeded discont element
- * 153881 : [PATCH] in-code C declarations
-
-API changed in this release
-
-- API additions:
-
-* The "fakesrc" element now has a datarate property.
-* The "identity" element now has a datarate property.
+ * 652211 : Use const instead G_CONST_RETURN
Download
Developers
-CVS is hosted on cvs.freedesktop.org.
-All code is in CVS and can be checked out from there.
+GStreamer is stored in Git, hosted at git.freedesktop.org, and can be cloned from there.
Interested developers of the core library, plug-ins, and applications should
subscribe to the gstreamer-devel list. If there is sufficient interest we
will create more lists as necessary.
Applications
-Applications already ported to use GStreamer 0.8.x include the GNOME
-desktop components like gnome-media and nautilus-media, as well as other
-GNOME applications including sound-juicer, totem and RhythmBox.
+Applications ported to GStreamer 0.10 include Totem, RhythmBox, Sound-Juicer,
+Gnome Media, Flumotion, Amarok, Jamboree, Pitivi, Istanbul, AnnoAmp, Elisa, and others.
+Let us know if you want to be added to this list.
Contributors to this release
- * Benjamin Otte
* David Schleef
- * Luca Ognibene
- * Ronald Bultje
- * Steve Lhomme
- * Thomas Vander Stichele
- * Wim Taymans
-
+ * Javier Jardón
+ * Руслан Ижбулатов
+
\ No newline at end of file