index faa5f4ca09c6504d5d713356005b130aebaa96dd..f08961779ab8010505cecf91cd485cdfabe1857c 100644 (file)
--- a/RELEASE
+++ b/RELEASE
-GStreamer: Release notes for GStreamer 0.10.1 "Nollaig chridheil"
+Release notes for GStreamer 0.10.35 "Nuclear Fission"
The 0.10.x series has been reworked for threadsafety. It also features
-various feature additions and enchancements.
+various feature additions and enhancements.
This module, gstreamer, only contains core functionality.
+
Features of this release
- * Parallel installability with 0.8.x series
- * Threadsafe design and API
- * element factory leak fixes
- * tests cleanup
- * BaseSrc seeking in other format than BYTES
- * collectpad fixes
+ * work around GLib atomic ops API change
+ * some minor win32/mingw fixes
+ * don't use G_CONST_RETURN in public headers
Bugs fixed in this release
-
- * 322441 : getcontext() in common/m4/gst-mcsc.m4 uses incorrect stac...
- * 323041 : [BASESRC] basesrc does not handle a seek to non-bytes for...
- * 323870 : [tools] gst-feedback needs updating for 0.9/0.10
- * 323882 : gst-launch manpage needs updates
- * 323905 : use return val of g_list_append
-
-API changed in this release
-
-- API additions:
-
-* GST_TYPE_STATIC_CAPS
-* GST_TYPE_STATIC_PAD_TEMPLATE
-* GstNetTimeProvider::active
-* gst_base_src_set_format
+ * 652211 : Use const instead G_CONST_RETURN
Download
Developers
-CVS is hosted on cvs.freedesktop.org.
-All code is in CVS and can be checked out from there.
+GStreamer is stored in Git, hosted at git.freedesktop.org, and can be cloned from there.
Interested developers of the core library, plug-ins, and applications should
subscribe to the gstreamer-devel list. If there is sufficient interest we
will create more lists as necessary.
Applications
-At this point, ports of existing applications to 0.10 are still experimental.
-Totem HEAD has a configure option to build the 0.10 backend.
-A patch for Rhythmbox is maintained at
-
-http://bugzilla.gnome.org/show_bug.cgi?id=309609.
-Jamboree builds against GStreamer 0.10.
-Flumotion has been ported to 0.10 as well.
+Applications ported to GStreamer 0.10 include Totem, RhythmBox, Sound-Juicer,
+Gnome Media, Flumotion, Amarok, Jamboree, Pitivi, Istanbul, AnnoAmp, Elisa, and others.
+Let us know if you want to be added to this list.
Contributors to this release
- * Andy Wingo
* David Schleef
- * Edward Hervey
- * Jan Schmidt
- * Julien MOUTTE
- * Michael Smith
- * Stefan Kost
- * Thomas Vander Stichele
- * Tim-Philipp Müller
- * Wim Taymans
+ * Javier Jardón
+ * Руслан Ижбулатов
\ No newline at end of file