]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/gstreamer0-10.git/blobdiff - configure.ac
Bump git version after unplanned 0.10.35 release
[glsdk/gstreamer0-10.git] / configure.ac
index 6f30757747d390829e4767100d15ed421c86eb50..0a03ccdd9dd7cd2dbe2a98d702fca61e82c73df8 100644 (file)
@@ -1,15 +1,15 @@
-AC_PREREQ(2.52)
+AC_PREREQ(2.60)
 
 dnl initialize autoconf
 dnl when going to/from release please set the nano (fourth number) right !
 dnl releases only do Wall, git and prerelease does Werror too
-AC_INIT(GStreamer, 0.10.25.1,
+AC_INIT(GStreamer, 0.10.35.1,
     http://bugzilla.gnome.org/enter_bug.cgi?product=GStreamer,
     gstreamer)
 AG_GST_INIT
 
 dnl initialize automake (we require GNU make)
-AM_INIT_AUTOMAKE([-Wno-portability])
+AM_INIT_AUTOMAKE([-Wno-portability 1.10])
 
 dnl define PACKAGE_VERSION_* variables
 AS_VERSION
@@ -29,6 +29,11 @@ AM_MAINTAINER_MODE
 dnl sets host_* variables
 AC_CANONICAL_HOST
 
+dnl use pretty build output with automake >= 1.11
+m4_ifdef([AM_SILENT_RULES],[AM_SILENT_RULES([yes])],
+  [AM_DEFAULT_VERBOSITY=1
+   AC_SUBST(AM_DEFAULT_VERBOSITY)])
+
 dnl our libraries and install dirs use major.minor as a version
 GST_MAJORMINOR=$PACKAGE_VERSION_MAJOR.$PACKAGE_VERSION_MINOR
 dnl we override it here for release candidates for a new series
@@ -43,7 +48,7 @@ dnl - interfaces added/removed/changed -> increment CURRENT, REVISION = 0
 dnl - interfaces added -> increment AGE
 dnl - interfaces removed -> AGE = 0
 dnl sets GST_LT_LDFLAGS
-AS_LIBTOOL(GST, 22, 0, 22)
+AS_LIBTOOL(GST, 29, 0, 29)
 
 dnl FIXME: this macro doesn't actually work;
 dnl the generated libtool script has no support for the listed tags.
@@ -59,7 +64,7 @@ dnl allow for different autotools
 AS_AUTOTOOLS_ALTERNATE
 
 dnl Add parameters for aclocal (keep in sync with Makefile.am)
-AC_SUBST(ACLOCAL_AMFLAGS, "-I common/m4 -I .")
+AC_SUBST(ACLOCAL_AMFLAGS, "-I m4 -I common/m4")
 
 dnl set up gettext
 dnl the version check needs to stay here because autopoint greps for it
@@ -125,6 +130,12 @@ AG_GST_ARG_WITH_PKG_CONFIG_PATH
 AG_GST_ARG_WITH_PACKAGE_NAME
 AG_GST_ARG_WITH_PACKAGE_ORIGIN
 
+AG_GST_PKG_CONFIG_PATH
+
+AG_GST_SET_PACKAGE_RELEASE_DATETIME_WITH_NANO([$PACKAGE_VERSION_NANO],
+  ["${srcdir}/gstreamer.doap"],
+  [$PACKAGE_VERSION_MAJOR.$PACKAGE_VERSION_MINOR.$PACKAGE_VERSION_MICRO])
+
 dnl building of tests
 AC_ARG_ENABLE(tests,
   AC_HELP_STRING([--disable-tests], [disable building test apps]),
@@ -197,43 +208,7 @@ fi
 AC_SUBST(GST_HAVE_UNALIGNED_ACCESS_DEFINE)
 
 dnl check for platform specific settings
-case $host_os in
-     rhapsody*)
-       AC_DEFINE_UNQUOTED(GST_EXTRA_MODULE_SUFFIX, [".dylib"], [Extra platform specific plugin suffix])
-        ;;
-     darwin*)
-       AC_DEFINE_UNQUOTED(GST_EXTRA_MODULE_SUFFIX, [".dylib"], [Extra platform specific plugin suffix])
-        AC_DEFINE_UNQUOTED(HAVE_OSX, 1, [Defined if compiling for OSX])
-       ;;
-     cygwin*)
-       AC_DEFINE_UNQUOTED(GST_HAVE_UNSAFE_FORK, 1, [Defined when registry scanning through fork is unsafe])
-       ;;
-     mingw* | msvc* | mks*)
-        dnl HAVE_WIN32 currently means "disable POSIXisms".
-        AC_DEFINE_UNQUOTED(HAVE_WIN32, 1, [Defined if compiling for Windows])
-
-        dnl define __MSVCRT_VERSION__ version if not set already by the
-        dnl compiler (ie. mostly for mingw). This is needed for things like
-        dnl __stat64 to be available. If set by the compiler, ensure it's
-        dnl new enough - we need at least WinXP SP2.
-        AC_TRY_COMPILE([ ], [ return __MSVCRT_VERSION__; ], [
-            AC_TRY_COMPILE([ ], [
-              #if __MSVCRT_VERSION__ < 0x0601
-              #error "MSVCRT too old"
-              #endif
-            ], [
-              AC_MSG_NOTICE([MSVCRT version looks ok])
-            ], [
-              AC_MSG_ERROR([MSVCRT version too old, need at least WinXP SP2])
-            ])
-        ], [
-          AC_MSG_NOTICE([Setting MSVCRT version to 0x0601])
-          AC_DEFINE_UNQUOTED(__MSVCRT_VERSION__, 0x0601, [We need at least WinXP SP2 for __stat64])
-        ])
-        ;;
-     *)
-       ;;
-esac
+AG_GST_PLATFORM
 
 dnl * software *
 
@@ -245,6 +220,7 @@ dnl *** checks for programs ***
 
 dnl find a compiler
 AC_PROG_CC
+AC_PROG_CC_STDC
 
 dnl check if the compiler supports '-c' and '-o' options
 AM_PROG_CC_C_O
@@ -252,6 +228,16 @@ AM_PROG_CC_C_O
 dnl find an assembler
 AM_PROG_AS
 
+dnl determine if c++ is available on this system
+AC_PROG_CXX
+dnl CXX may be set to some default even if no c++ compiler is available
+dnl (thanks autotools!), so just try to compile some c++ code to make sure
+AC_LANG_PUSH([C++])
+AC_TRY_COMPILE([ class Foo { int bar; };], , working_cxx=yes, working_cxx=no)
+AC_LANG_POP([C++])
+AC_MSG_NOTICE([working c++ compiler found: $working_cxx])
+AM_CONDITIONAL(HAVE_CXX, test "x$working_cxx" = "xyes")
+
 dnl Perl is used in building documentation and in the version checks
 AC_PATH_PROG(PERL_PATH, perl, no)
 if test x$PERL_PATH = xno; then
@@ -312,6 +298,9 @@ dnl check for pthreads
 AC_CHECK_HEADERS([pthread.h], HAVE_PTHREAD_H=yes)
 AM_CONDITIONAL(HAVE_PTHREAD_H, test "x$HAVE_PTHREAD_H" = "xyes")
 
+dnl check for sys/prctl for setting thread name on Linux
+AC_CHECK_HEADERS([sys/prctl.h], HAVE_SYS_PRCTL_H=yes)
+
 dnl Check for valgrind.h
 dnl separate from HAVE_VALGRIND because you can have the program, but not
 dnl the dev package
@@ -326,18 +315,20 @@ if test "x$HAVE_WINSOCK2_H" = "xyes"; then
 fi
 
 dnl check for GMP/GSL, used by the gst_util_uint64_scale unit test only
-AG_GST_CHECK_LIBHEADER(GMP, gmp,
-                        __gmpz_init_set_d, ,
-                        gmp.h,
-                        GMP_LIBS="-lgmp"
-                        AC_SUBST(GMP_LIBS)
-                       AC_DEFINE(HAVE_GMP, [1],[Have GMP library]))
-AG_GST_CHECK_LIBHEADER(GSL, gsl,
-                        gsl_rng_uniform_int, -lgslcblas,
-                        gsl/gsl_rng.h,
-                        GSL_LIBS="-lgsl -lgslcblas"
-                        AC_SUBST(GSL_LIBS)
-                       AC_DEFINE(HAVE_GSL, [1],[Have GSL library]))
+if test "x$BUILD_TESTS" = "xyes"; then
+  AG_GST_CHECK_LIBHEADER(GMP, gmp,
+                         __gmpz_init_set_d, ,
+                         gmp.h,
+                         GMP_LIBS="-lgmp"
+                         AC_SUBST(GMP_LIBS)
+                         AC_DEFINE(HAVE_GMP, [1],[Have GMP library]))
+  AG_GST_CHECK_LIBHEADER(GSL, gsl,
+                         gsl_rng_uniform_int, -lgslcblas,
+                         gsl/gsl_rng.h,
+                         GSL_LIBS="-lgsl -lgslcblas"
+                         AC_SUBST(GSL_LIBS)
+                         AC_DEFINE(HAVE_GSL, [1],[Have GSL library]))
+fi
 
 dnl *** checks for types/defines ***
 
@@ -346,11 +337,14 @@ dnl *** checks for structures ***
 dnl *** checks for compiler characteristics ***
 
 dnl check if the compiler supports __uint128_t (gcc)
+dnl Actually check for 128-bit division, since that's what we use
+dnl uint128_t for.
 AC_CACHE_CHECK(for __uint128_t, gst_cv_uint128_t,
-    AC_TRY_COMPILE([ ], [
-      __uint128_t u = 0;
-
-      return 0;
+    AC_TRY_LINK([ ], [
+      static __uint128_t v1 = 100;
+      static __uint128_t v2 = 10;
+      static __uint128_t u;
+      u = v1 / v2;
     ], [
       gst_cv_uint128_t=yes
     ], [
@@ -361,23 +355,26 @@ if test x$gst_cv_uint128_t = xyes; then
   AC_DEFINE(HAVE_UINT128_T, 1, [Have __uint128_t type])
 fi
 
-OPT_CFLAGS=
-dnl Check for some compiler flags that optimize our code.
-if test "x$GCC" = xyes; then
-  AS_COMPILER_FLAG(-fno-common, OPT_CFLAGS="$OPT_CFLAGS -fno-common")
-fi
+dnl *** checking for tm_gmtoff ***
+AC_MSG_CHECKING([for tm_gmtoff])
+AC_RUN_IFELSE([AC_LANG_SOURCE([[
+       #include <time.h>
+       int main(void) {
+         struct tm t;
+         t.tm_gmtoff = 0;
+         exit(0);
+       }]])],
+  [have_tm_gmtoff=yes
+   AC_DEFINE(HAVE_TM_GMTOFF,1,[Have tm_gmtoff field in struct tm])],
+  [have_tm_gmtoff=no],
+  [have_tm_gmtoff="no (cross compiling)"])
+AC_MSG_RESULT($have_tm_gmtoff)
 
-dnl FIXME: decide what kind of flag this is, maybe it's not an optimization
-dnl flag
-dnl check if we should use -Wa,-mregnames on PowerPC, so we can use
-dnl symbolic register names in inline asm
-if test x$HAVE_CPU_PPC = xyes ; then
-  AS_COMPILER_FLAG(["-Wa,-mregnames"],
-    [OPT_CFLAGS="$OPT_CFLAGS -Wa,-mregnames"])
-fi
 
 dnl *** checks for library functions ***
 
+AC_CHECK_FUNCS([gmtime_r])
+AC_CHECK_FUNCS([localtime_r])
 AC_CHECK_FUNCS([sigaction])
 
 dnl check for fseeko()
@@ -393,10 +390,44 @@ AC_CHECK_FUNCS([poll])
 AC_CHECK_FUNCS([ppoll])
 AC_CHECK_FUNCS([pselect])
 
+dnl ****************************************
+dnl *** GLib POLL* compatibility defines ***
+dnl ****************************************
+
+AC_MSG_CHECKING([for broken poll])
+AC_RUN_IFELSE([AC_LANG_SOURCE([[
+       #include <stdlib.h>
+       #include <fcntl.h>
+       #include <poll.h>
+       #ifdef HAVE_SYS_POLL_H
+       #include <sys/poll.h>
+       #endif
+       int main(void) {
+         struct pollfd fds[1];
+         int fd;
+         fd = open("/dev/null", 1);
+         fds[0].fd = fd;
+         fds[0].events = POLLIN;
+         fds[0].revents = 0;
+         if (poll(fds, 1, 0) < 0 || (fds[0].revents & POLLNVAL) != 0) {
+               exit(1);  /* Does not work for devices -- fail */
+         }
+         exit(0);
+       }]])],
+  [broken_poll=no],
+  [broken_poll=yes
+   AC_DEFINE(BROKEN_POLL,1,[poll doesn't work on devices])],
+  [broken_poll="no (cross compiling)"])
+AC_MSG_RESULT($broken_poll)
+
 dnl check for mmap()
 AC_FUNC_MMAP
 AM_CONDITIONAL(HAVE_MMAP, test "x$ac_cv_func_mmap_fixed_mapped" = "xyes")
 
+dnl check for posix_memalign(), getpagesize()
+AC_CHECK_FUNCS([posix_memalign])
+AC_CHECK_FUNCS([getpagesize])
+
 dnl Check for POSIX timers
 AC_CHECK_FUNCS(clock_gettime, [], [
   AC_CHECK_LIB(rt, clock_gettime, [
@@ -415,7 +446,6 @@ AC_CACHE_CHECK(for posix timers, gst_cv_posix_timers,
 #if !defined(_POSIX_TIMERS) || _POSIX_TIMERS < 0 || !defined(CLOCK_REALTIME)
 #error Either _POSIX_TIMERS or CLOCK_REALTIME not defined
 #endif
-      return 0;
     ], [
       gst_cv_posix_timers=yes
     ], [
@@ -442,7 +472,6 @@ AC_CACHE_CHECK(for monotonic clock, gst_cv_monotonic_clock,
 #if !defined(_POSIX_MONOTONIC_CLOCK) || _POSIX_MONOTONIC_CLOCK < 0 || !defined(CLOCK_MONOTONIC)
 #error Either _POSIX_MONOTONIC_CLOCK or CLOCK_MONOTONIC not defined
 #endif
-      return 0;
     ], [
       gst_cv_monotonic_clock=yes
     ], [
@@ -506,7 +535,7 @@ LIBS="$save_libs"
 dnl *** checks for dependency libraries ***
 
 dnl GLib
-GLIB_REQ=2.16
+GLIB_REQ=2.24
 
 AG_GST_GLIB_CHECK([$GLIB_REQ])
 
@@ -553,6 +582,40 @@ dnl bit of a misnomer, but keep the conditional named like this so we don't
 dnl have to change too much elsewhere
 AM_CONDITIONAL(HAVE_CHECK, test "x$BUILD_CHECK" = "xyes")
 
+dnl configure the desired buffer alignment
+AC_ARG_WITH([buffer-alignment],
+  AS_HELP_STRING([--with-buffer-alignment],[8,N,malloc,pagesize (default is 32)]),
+  [
+    if test "x$withval" = "xyes"
+    then
+      AC_DEFINE(BUFFER_ALIGNMENT, 32, [Buffer alignment to use])
+    else
+      case "${withval}" in
+        malloc) AC_DEFINE(BUFFER_ALIGNMENT_MALLOC, 1, [Buffer alignment by malloc default]) ;;
+        pagesize)  AC_DEFINE(BUFFER_ALIGNMENT_PAGESIZE, 1, [Buffer alignment by pagesize]) ;;
+        *)   AC_DEFINE_UNQUOTED(BUFFER_ALIGNMENT, ${withval}, [Buffer alignment to use]) ;;
+      esac
+    fi
+  ], [
+    AC_DEFINE(BUFFER_ALIGNMENT_MALLOC, 1, [Buffer alignment by malloc default]) 
+  ]
+)
+
+dnl Check for -Bsymbolic-functions linker flag used to avoid
+dnl intra-library PLT jumps, if available.
+AC_ARG_ENABLE(Bsymbolic,
+              [AC_HELP_STRING([--disable-Bsymbolic],
+                              [avoid linking with -Bsymbolic])],,
+              [SAVED_LDFLAGS="${LDFLAGS}"
+               AC_MSG_CHECKING([for -Bsymbolic-functions linker flag])
+               LDFLAGS=-Wl,-Bsymbolic-functions
+               AC_TRY_LINK([], [int main (void) { return 0; }],
+                           AC_MSG_RESULT(yes)
+                           enable_Bsymbolic=yes,
+                           AC_MSG_RESULT(no)
+                           enable_Bsymbolic=no)
+               LDFLAGS="${SAVED_LDFLAGS}"])
+
 
 dnl *** set variables based on configure arguments
 
@@ -575,7 +638,7 @@ GST_PKG_DEPS="glib-2.0, gobject-2.0, gmodule-no-export-2.0, gthread-2.0"
 AC_SUBST(GST_PKG_DEPS)
 
 dnl define an ERROR_CFLAGS Makefile variable
-AG_GST_SET_ERROR_CFLAGS($GST_GIT)
+AG_GST_SET_ERROR_CFLAGS($GST_GIT, [-Wmissing-declarations -Wmissing-prototypes -Wredundant-decls -Wundef -Wwrite-strings -Wformat-nonliteral -Wformat-security -Wold-style-definition -Winit-self -Wmissing-include-dirs -Waddress -Waggregate-return -Wno-multichar -Wnested-externs])
 
 dnl define correct level for debugging messages
 AG_GST_SET_LEVEL_DEFAULT($GST_GIT)
@@ -610,8 +673,10 @@ AC_SUBST(DEPRECATED_CFLAGS)
 
 dnl every flag in GST_OPTION_CFLAGS can be overridden at make time via e.g.
 dnl make DEPRECATED_CFLAGS=''
-GST_OPTION_CFLAGS="\$(ERROR_CFLAGS) \$(DEBUG_CFLAGS) \$(PROFILE_CFLAGS) \$(GCOV_CFLAGS) \$(OPT_CFLAGS) \$(DEPRECATED_CFLAGS)"
+GST_OPTION_CFLAGS="\$(WARNING_CFLAGS) \$(DEBUG_CFLAGS) \$(PROFILE_CFLAGS) \$(GCOV_CFLAGS) \$(OPT_CFLAGS) \$(DEPRECATED_CFLAGS)"
+GST_OPTION_CXXFLAGS="\$(WARNING_CXXFLAGS) \$(ERROR_CXXFLAGS) \$(DEBUG_CFLAGS) \$(PROFILE_CFLAGS) \$(GCOV_CFLAGS) \$(OPT_CFLAGS) \$(DEPRECATED_CFLAGS)"
 AC_SUBST(GST_OPTION_CFLAGS)
+AC_SUBST(GST_OPTION_CXXFLAGS)
 
 dnl GST_ALL_*
 dnl vars common to for all internal objects (core libs, elements, applications)
@@ -621,7 +686,8 @@ dnl - src and build dirs need to be added because every piece that gets built
 dnl   will need the GStreamer source and generated headers
 dnl LIBS: XML doesn't need to be added because we don't explicitly use symbols
 dnl       from LibXML except for in the core library
-GST_ALL_CFLAGS="-I\$(top_srcdir)/libs -I\$(top_srcdir) -I\$(top_builddir)/libs -I\$(top_builddir) $GLIB_CFLAGS $XML_CFLAGS \$(GST_OPTION_CFLAGS)"
+GST_ALL_CXXFLAGS="-I\$(top_srcdir)/libs -I\$(top_srcdir) -I\$(top_builddir)/libs -I\$(top_builddir) $GLIB_CFLAGS $GLIB_EXTRA_CFLAGS $XML_CFLAGS \$(GST_OPTION_CXXFLAGS) \$(ERROR_CXXFLAGS)"
+GST_ALL_CFLAGS="-I\$(top_srcdir)/libs -I\$(top_srcdir) -I\$(top_builddir)/libs -I\$(top_builddir) $GLIB_CFLAGS $GLIB_EXTRA_CFLAGS $XML_CFLAGS \$(GST_OPTION_CFLAGS) \$(ERROR_CFLAGS)"
 
 dnl FIXME: check if LTLIBINTL is needed everywhere
 dnl I presume it is given that it contains the symbols that _() stuff maps to
@@ -630,8 +696,12 @@ GST_ALL_LIBS="$GLIB_LIBS $LTLIBINTL \$(GCOV_LIBS)"
 dnl LDFLAGS really should only contain flags, not libs - they get added before
 dnl whatevertarget_LIBS and -L flags here affect the rest of the linking
 GST_ALL_LDFLAGS="-no-undefined"
+if test "x${enable_Bsymbolic}" = "xyes"; then
+  GST_ALL_LDFLAGS="$GST_ALL_LDFLAGS -Wl,-Bsymbolic-functions"
+fi
 
 AC_SUBST(GST_ALL_CFLAGS)
+AC_SUBST(GST_ALL_CXXFLAGS)
 AC_SUBST(GST_ALL_LIBS)
 AC_SUBST(GST_ALL_LDFLAGS)
 
@@ -645,31 +715,29 @@ dnl GST_OBJ_*
 dnl default vars for all internal objects built on libgstreamer
 dnl includes GST_ALL_*
 GST_OBJ_CFLAGS="\$(GST_ALL_CFLAGS)"
+GST_OBJ_CXXFLAGS="\$(GST_ALL_CXXFLAGS)"
 GST_OBJ_LIBS="\$(top_builddir)/gst/libgstreamer-$GST_MAJORMINOR.la \$(GST_ALL_LIBS)"
 AC_SUBST(GST_OBJ_CFLAGS)
+AC_SUBST(GST_OBJ_CXXFLAGS)
 AC_SUBST(GST_OBJ_LIBS)
 
 dnl GST_PLUGIN_LDFLAGS
 dnl LDFLAGS for plugins; includes GST_ALL_LDFLAGS
-GST_PLUGIN_LDFLAGS="-module -avoid-version -export-symbols-regex '^[_]*gst_plugin_desc\$\$' $GST_ALL_LDFLAGS"
+GST_PLUGIN_LDFLAGS="-module -avoid-version -export-symbols-regex '^[_]*gst_plugin_desc.*' $GST_ALL_LDFLAGS"
 AC_SUBST(GST_PLUGIN_LDFLAGS, "$GST_PLUGIN_LDFLAGS")
 
 dnl plugin scanner locations
-AS_AC_EXPAND(GST_PLUGIN_SCANNER_INSTALLED,${libexecdir}/plugin-scanner)
+AS_AC_EXPAND(GST_PLUGIN_SCANNER_INSTALLED,${libexecdir}/gstreamer-$GST_MAJORMINOR/gst-plugin-scanner)
 AC_DEFINE_UNQUOTED(GST_PLUGIN_SCANNER_INSTALLED,
-    "$GST_PLUGIN_SCANNER_INSTALLED", [location of the installed plugin-scanner])
+    "$GST_PLUGIN_SCANNER_INSTALLED", [location of the installed gst-plugin-scanner])
+AC_SUBST(GST_PLUGIN_SCANNER_INSTALLED)
 
-SHAVE_INIT([common],[enable])
-
-dnl things for our internal libcheck
-if test "x$BUILD_CHECK" = "xyes"; then
-  AG_GST_CHECK_CHECKS()
-fi
+dnl things for our internal libcheck (must be called even if building
+dnl libcheck is disabled because it defines conditionals)
+AG_GST_CHECK_CHECKS()
 
 AC_CONFIG_FILES(
 Makefile
-common/shave
-common/shave-libtool
 gst/Makefile
 gst/gstconfig.h
 gst/gstversion.h
@@ -703,7 +771,6 @@ tests/examples/metadata/Makefile
 tests/examples/queue/Makefile
 tests/examples/streams/Makefile
 tests/examples/typefind/Makefile
-tests/examples/xml/Makefile
 tools/Makefile
 common/Makefile
 common/m4/Makefile
@@ -719,6 +786,7 @@ docs/pwg/Makefile
 docs/slides/Makefile
 docs/xsl/Makefile
 docs/version.entities
+m4/Makefile
 pkgconfig/Makefile
 stamp.h
 pkgconfig/gstreamer.pc
@@ -748,6 +816,7 @@ sed \
     -e 's/.* GST_MAJORMINOR$/#define GST_MAJORMINOR "'$GST_MAJORMINOR'"/' \
     -e "s,.* GST_PACKAGE_NAME$,#define GST_PACKAGE_NAME \"${GST_PACKAGE_NAME}\"," \
     -e 's/.* GST_PACKAGE_ORIGIN$/#define GST_PACKAGE_ORIGIN "Unknown package origin"/' \
+    -e "s,.* GST_PACKAGE_RELEASE_DATETIME$,#define GST_PACKAGE_RELEASE_DATETIME \"${GST_PACKAGE_RELEASE_DATETIME}\"," \
     -e 's/.* HAVE_CPU_I386$/#define HAVE_CPU_I386 1/' \
     -e 's/.* HAVE_FGETPOS$/#define HAVE_FGETPOS 1/' \
     -e 's/.* HAVE_FSETPOS$/#define HAVE_FSETPOS 1/' \
@@ -760,6 +829,7 @@ sed \
     -e 's/.* HAVE_WIN32$/#define HAVE_WIN32 1/' \
     -e 's/.* HAVE_WINSOCK2_H$/#define HAVE_WINSOCK2_H 1/' \
     -e 's/.* HOST_CPU$/#define HOST_CPU "i686"/' \
+    -e 's/.* BUFFER_ALIGNMENT_MALLOC/#define BUFFER_ALIGNMENT_MALLOC 1/' \
     -e 's/.* LIBDIR$/#ifdef _DEBUG\n#  define LIBDIR PREFIX "\\\\debug\\\\lib"\n#else\n#  define LIBDIR PREFIX "\\\\lib"\n#endif/' \
     -e 's/.* LOCALEDIR$/#define LOCALEDIR PREFIX "\\\\share\\\\locale"/' \
     -e 's/.* PACKAGE$/#define PACKAGE "gstreamer"/' \
@@ -769,6 +839,7 @@ sed \
     -e 's/.* PACKAGE_TARNAME$/#define PACKAGE_TARNAME "'$PACKAGE_TARNAME'"/' \
     -e 's/.* PACKAGE_VERSION$/#define PACKAGE_VERSION "'$PACKAGE_VERSION'"/' \
     -e 's/.* PLUGINDIR$/#ifdef _DEBUG\n#  define PLUGINDIR PREFIX "\\\\debug\\\\lib\\\\gstreamer-0.10"\n#else\n#  define PLUGINDIR PREFIX "\\\\lib\\\\gstreamer-0.10"\n#endif/' \
+    -e 's/.* GST_PLUGIN_SCANNER_INSTALLED$/#define GST_PLUGIN_SCANNER_INSTALLED LIBDIR "\\\\gst-plugin-scanner"/' \
     -e 's/.* VERSION$/#define VERSION "'$VERSION'"/' \
     config.h.in >win32/common/config.h-new
 
@@ -791,7 +862,7 @@ Configuration
        Version                    : ${VERSION}
        Source code location       : ${srcdir}
        Prefix                     : ${prefix}
-       Compiler                   : ${SHAVE_SAVED_CC}
+       Compiler                   : ${CC}
        Package name               : ${GST_PACKAGE_NAME}
        Package origin             : ${GST_PACKAGE_ORIGIN}