diff --git a/configure.ac b/configure.ac
index 98acf8422545aea2fd04234cb64bbeee02a2e0c0..93dc7ed0f5dbb4aa72f480bcd282c81365abf2f1 100644 (file)
--- a/configure.ac
+++ b/configure.ac
-AC_PREREQ(2.52)
+AC_PREREQ(2.60)
dnl initialize autoconf
dnl when going to/from release please set the nano (fourth number) right !
dnl releases only do Wall, git and prerelease does Werror too
-AC_INIT(GStreamer, 0.10.24.1,
+AC_INIT(GStreamer, 0.10.32,
http://bugzilla.gnome.org/enter_bug.cgi?product=GStreamer,
gstreamer)
AG_GST_INIT
dnl initialize automake (we require GNU make)
-AM_INIT_AUTOMAKE([-Wno-portability])
+AM_INIT_AUTOMAKE([-Wno-portability 1.10])
dnl define PACKAGE_VERSION_* variables
AS_VERSION
dnl sets host_* variables
AC_CANONICAL_HOST
+dnl use pretty build output with automake >= 1.11
+m4_ifdef([AM_SILENT_RULES],[AM_SILENT_RULES([yes])],
+ [AM_DEFAULT_VERBOSITY=1
+ AC_SUBST(AM_DEFAULT_VERBOSITY)])
+
dnl our libraries and install dirs use major.minor as a version
GST_MAJORMINOR=$PACKAGE_VERSION_MAJOR.$PACKAGE_VERSION_MINOR
dnl we override it here for release candidates for a new series
dnl - interfaces added -> increment AGE
dnl - interfaces removed -> AGE = 0
dnl sets GST_LT_LDFLAGS
-AS_LIBTOOL(GST, 21, 0, 21)
+AS_LIBTOOL(GST, 28, 0, 28)
dnl FIXME: this macro doesn't actually work;
dnl the generated libtool script has no support for the listed tags.
AS_AUTOTOOLS_ALTERNATE
dnl Add parameters for aclocal (keep in sync with Makefile.am)
-AC_SUBST(ACLOCAL_AMFLAGS, "-I common/m4 -I .")
+AC_SUBST(ACLOCAL_AMFLAGS, "-I m4 -I common/m4")
dnl set up gettext
dnl the version check needs to stay here because autopoint greps for it
AG_GST_ARG_WITH_PACKAGE_NAME
AG_GST_ARG_WITH_PACKAGE_ORIGIN
+AG_GST_PKG_CONFIG_PATH
+
+AG_GST_SET_PACKAGE_RELEASE_DATETIME_WITH_NANO([$PACKAGE_VERSION_NANO],
+ ["${srcdir}/gstreamer.doap"],
+ [$PACKAGE_VERSION_MAJOR.$PACKAGE_VERSION_MINOR.$PACKAGE_VERSION_MICRO])
+
dnl building of tests
AC_ARG_ENABLE(tests,
AC_HELP_STRING([--disable-tests], [disable building test apps]),
AC_SUBST(GST_HAVE_UNALIGNED_ACCESS_DEFINE)
dnl check for platform specific settings
-case $host_os in
- rhapsody*)
- AC_DEFINE_UNQUOTED(GST_EXTRA_MODULE_SUFFIX, [".dylib"], [Extra platform specific plugin suffix])
- ;;
- darwin*)
- AC_DEFINE_UNQUOTED(GST_EXTRA_MODULE_SUFFIX, [".dylib"], [Extra platform specific plugin suffix])
- AC_DEFINE_UNQUOTED(GST_HAVE_UNSAFE_FORK, 1, [Defined when registry scanning through fork is unsafe])
- AC_DEFINE_UNQUOTED(HAVE_OSX, 1, [Defined if compiling for OSX])
- ;;
- cygwin*)
- AC_DEFINE_UNQUOTED(GST_HAVE_UNSAFE_FORK, 1, [Defined when registry scanning through fork is unsafe])
- ;;
- mingw* | msvc* | mks*)
- dnl HAVE_WIN32 currently means "disable POSIXisms".
- AC_DEFINE_UNQUOTED(HAVE_WIN32, 1, [Defined if compiling for Windows])
-
- dnl define __MSVCRT_VERSION__ version if not set already by the
- dnl compiler (ie. mostly for mingw). This is needed for things like
- dnl __stat64 to be available. If set by the compiler, ensure it's
- dnl new enough - we need at least WinXP SP2.
- AC_TRY_COMPILE([ ], [ return __MSVCRT_VERSION__; ], [
- AC_TRY_COMPILE([ ], [
- #if __MSVCRT_VERSION__ < 0x0601
- #error "MSVCRT too old"
- #endif
- ], [
- AC_MSG_NOTICE([MSVCRT version looks ok])
- ], [
- AC_MSG_ERROR([MSVCRT version too old, need at least WinXP SP2])
- ])
- ], [
- AC_MSG_NOTICE([Setting MSVCRT version to 0x0601])
- AC_DEFINE_UNQUOTED(__MSVCRT_VERSION__, 0x0601, [We need at least WinXP SP2 for __stat64])
- ])
- ;;
- *)
- ;;
-esac
+AG_GST_PLATFORM
dnl * software *
dnl find a compiler
AC_PROG_CC
+AC_PROG_CC_STDC
dnl check if the compiler supports '-c' and '-o' options
AM_PROG_CC_C_O
dnl find an assembler
AM_PROG_AS
+dnl determine if c++ is available on this system
+AC_PROG_CXX
+dnl CXX may be set to some default even if no c++ compiler is available
+dnl (thanks autotools!), so just try to compile some c++ code to make sure
+AC_LANG_PUSH([C++])
+AC_TRY_COMPILE([ class Foo { int bar; };], , working_cxx=yes, working_cxx=no)
+AC_LANG_POP([C++])
+AC_MSG_NOTICE([working c++ compiler found: $working_cxx])
+AM_CONDITIONAL(HAVE_CXX, test "x$working_cxx" = "xyes")
+
dnl Perl is used in building documentation and in the version checks
AC_PATH_PROG(PERL_PATH, perl, no)
if test x$PERL_PATH = xno; then
AC_CHECK_HEADERS([pthread.h], HAVE_PTHREAD_H=yes)
AM_CONDITIONAL(HAVE_PTHREAD_H, test "x$HAVE_PTHREAD_H" = "xyes")
+dnl check for sys/prctl for setting thread name on Linux
+AC_CHECK_HEADERS([sys/prctl.h], HAVE_SYS_PRCTL_H=yes)
+
dnl Check for valgrind.h
dnl separate from HAVE_VALGRIND because you can have the program, but not
dnl the dev package
fi
dnl check for GMP/GSL, used by the gst_util_uint64_scale unit test only
-AG_GST_CHECK_LIBHEADER(GMP, gmp,
- __gmpz_init_set_d, ,
- gmp.h,
- GMP_LIBS="-lgmp"
- AC_SUBST(GMP_LIBS)
- AC_DEFINE(HAVE_GMP, [1],[Have GMP library]))
-AG_GST_CHECK_LIBHEADER(GSL, gsl,
- gsl_rng_uniform_int, -lgslcblas,
- gsl/gsl_rng.h,
- GSL_LIBS="-lgsl -lgslcblas"
- AC_SUBST(GSL_LIBS)
- AC_DEFINE(HAVE_GSL, [1],[Have GSL library]))
+if test "x$BUILD_TESTS" = "xyes"; then
+ AG_GST_CHECK_LIBHEADER(GMP, gmp,
+ __gmpz_init_set_d, ,
+ gmp.h,
+ GMP_LIBS="-lgmp"
+ AC_SUBST(GMP_LIBS)
+ AC_DEFINE(HAVE_GMP, [1],[Have GMP library]))
+ AG_GST_CHECK_LIBHEADER(GSL, gsl,
+ gsl_rng_uniform_int, -lgslcblas,
+ gsl/gsl_rng.h,
+ GSL_LIBS="-lgsl -lgslcblas"
+ AC_SUBST(GSL_LIBS)
+ AC_DEFINE(HAVE_GSL, [1],[Have GSL library]))
+fi
dnl *** checks for types/defines ***
dnl *** checks for compiler characteristics ***
-OPT_CFLAGS=
-dnl Check for some compiler flags that optimize our code.
-if test "x$GCC" = xyes; then
- AS_COMPILER_FLAG(-fno-common, OPT_CFLAGS="$OPT_CFLAGS -fno-common")
+dnl check if the compiler supports __uint128_t (gcc)
+dnl Actually check for 128-bit division, since that's what we use
+dnl uint128_t for.
+AC_CACHE_CHECK(for __uint128_t, gst_cv_uint128_t,
+ AC_TRY_LINK([ ], [
+ static __uint128_t v1 = 100;
+ static __uint128_t v2 = 10;
+ static __uint128_t u;
+ u = v1 / v2;
+ ], [
+ gst_cv_uint128_t=yes
+ ], [
+ gst_cv_uint128_t=no
+ ])
+)
+if test x$gst_cv_uint128_t = xyes; then
+ AC_DEFINE(HAVE_UINT128_T, 1, [Have __uint128_t type])
fi
-dnl FIXME: decide what kind of flag this is, maybe it's not an optimization
-dnl flag
-dnl check if we should use -Wa,-mregnames on PowerPC, so we can use
-dnl symbolic register names in inline asm
-if test x$HAVE_CPU_PPC = xyes ; then
- AS_COMPILER_FLAG(["-Wa,-mregnames"],
- [OPT_CFLAGS="$OPT_CFLAGS -Wa,-mregnames"])
-fi
+dnl *** checking for tm_gmtoff ***
+AC_MSG_CHECKING([for tm_gmtoff])
+AC_RUN_IFELSE([AC_LANG_SOURCE([[
+ #include <time.h>
+ int main(void) {
+ struct tm t;
+ t.tm_gmtoff = 0;
+ exit(0);
+ }]])],
+ [have_tm_gmtoff=yes
+ AC_DEFINE(HAVE_TM_GMTOFF,1,[Have tm_gmtoff field in struct tm])],
+ [have_tm_gmtoff=no],
+ [have_tm_gmtoff="no (cross compiling)"])
+AC_MSG_RESULT($have_tm_gmtoff)
+
dnl *** checks for library functions ***
+AC_CHECK_FUNCS([gmtime_r])
+AC_CHECK_FUNCS([localtime_r])
AC_CHECK_FUNCS([sigaction])
-dnl we use fork in the registry code
-AC_CHECK_FUNCS([fork])
-
dnl check for fseeko()
AC_FUNC_FSEEKO
dnl check for ftello()
AC_CHECK_FUNCS([ppoll])
AC_CHECK_FUNCS([pselect])
+dnl ****************************************
+dnl *** GLib POLL* compatibility defines ***
+dnl ****************************************
+
+AC_MSG_CHECKING([for broken poll])
+AC_RUN_IFELSE([AC_LANG_SOURCE([[
+ #include <stdlib.h>
+ #include <fcntl.h>
+ #include <poll.h>
+ #ifdef HAVE_SYS_POLL_H
+ #include <sys/poll.h>
+ #endif
+ int main(void) {
+ struct pollfd fds[1];
+ int fd;
+ fd = open("/dev/null", 1);
+ fds[0].fd = fd;
+ fds[0].events = POLLIN;
+ fds[0].revents = 0;
+ if (poll(fds, 1, 0) < 0 || (fds[0].revents & POLLNVAL) != 0) {
+ exit(1); /* Does not work for devices -- fail */
+ }
+ exit(0);
+ }]])],
+ [broken_poll=no],
+ [broken_poll=yes
+ AC_DEFINE(BROKEN_POLL,1,[poll doesn't work on devices])],
+ [broken_poll="no (cross compiling)"])
+AC_MSG_RESULT($broken_poll)
+
dnl check for mmap()
AC_FUNC_MMAP
AM_CONDITIONAL(HAVE_MMAP, test "x$ac_cv_func_mmap_fixed_mapped" = "xyes")
+dnl check for posix_memalign(), getpagesize()
+AC_CHECK_FUNCS([posix_memalign])
+AC_CHECK_FUNCS([getpagesize])
+
dnl Check for POSIX timers
AC_CHECK_FUNCS(clock_gettime, [], [
AC_CHECK_LIB(rt, clock_gettime, [
#if !defined(_POSIX_TIMERS) || _POSIX_TIMERS < 0 || !defined(CLOCK_REALTIME)
#error Either _POSIX_TIMERS or CLOCK_REALTIME not defined
#endif
- return 0;
], [
gst_cv_posix_timers=yes
], [
#if !defined(_POSIX_MONOTONIC_CLOCK) || _POSIX_MONOTONIC_CLOCK < 0 || !defined(CLOCK_MONOTONIC)
#error Either _POSIX_MONOTONIC_CLOCK or CLOCK_MONOTONIC not defined
#endif
- return 0;
], [
gst_cv_monotonic_clock=yes
], [
dnl *** checks for dependency libraries ***
dnl GLib
-GLIB_REQ=2.16
+GLIB_REQ=2.22
AG_GST_GLIB_CHECK([$GLIB_REQ])
dnl have to change too much elsewhere
AM_CONDITIONAL(HAVE_CHECK, test "x$BUILD_CHECK" = "xyes")
+dnl configure the desired buffer alignment
+AC_ARG_WITH([buffer-alignment],
+ AS_HELP_STRING([--with-buffer-alignment],[8,N,malloc,pagesize (default is 32)]),
+ [
+ if test "x$withval" = "xyes"
+ then
+ AC_DEFINE(BUFFER_ALIGNMENT, 32, [Buffer alignment to use])
+ else
+ case "${withval}" in
+ malloc) AC_DEFINE(BUFFER_ALIGNMENT_MALLOC, 1, [Buffer alignment by malloc default]) ;;
+ pagesize) AC_DEFINE(BUFFER_ALIGNMENT_PAGESIZE, 1, [Buffer alignment by pagesize]) ;;
+ *) AC_DEFINE_UNQUOTED(BUFFER_ALIGNMENT, ${withval}, [Buffer alignment to use]) ;;
+ esac
+ fi
+ ], [
+ AC_DEFINE(BUFFER_ALIGNMENT_MALLOC, 1, [Buffer alignment by malloc default])
+ ]
+)
+
+dnl Check for -Bsymbolic-functions linker flag used to avoid
+dnl intra-library PLT jumps, if available.
+AC_ARG_ENABLE(Bsymbolic,
+ [AC_HELP_STRING([--disable-Bsymbolic],
+ [avoid linking with -Bsymbolic])],,
+ [SAVED_LDFLAGS="${LDFLAGS}"
+ AC_MSG_CHECKING([for -Bsymbolic-functions linker flag])
+ LDFLAGS=-Wl,-Bsymbolic-functions
+ AC_TRY_LINK([], [int main (void) { return 0; }],
+ AC_MSG_RESULT(yes)
+ enable_Bsymbolic=yes,
+ AC_MSG_RESULT(no)
+ enable_Bsymbolic=no)
+ LDFLAGS="${SAVED_LDFLAGS}"])
+
dnl *** set variables based on configure arguments
AC_SUBST(GST_PKG_DEPS)
dnl define an ERROR_CFLAGS Makefile variable
-AG_GST_SET_ERROR_CFLAGS($GST_GIT)
+AG_GST_SET_ERROR_CFLAGS($GST_GIT, [-Wmissing-declarations -Wmissing-prototypes -Wredundant-decls -Wundef -Wwrite-strings -Wformat-nonliteral -Wformat-security -Wold-style-definition -Winit-self -Wmissing-include-dirs -Waddress -Waggregate-return -Wno-multichar -Wnested-externs])
dnl define correct level for debugging messages
AG_GST_SET_LEVEL_DEFAULT($GST_GIT)
dnl every flag in GST_OPTION_CFLAGS can be overridden at make time via e.g.
dnl make DEPRECATED_CFLAGS=''
-GST_OPTION_CFLAGS="\$(ERROR_CFLAGS) \$(DEBUG_CFLAGS) \$(PROFILE_CFLAGS) \$(GCOV_CFLAGS) \$(OPT_CFLAGS) \$(DEPRECATED_CFLAGS)"
+GST_OPTION_CFLAGS="\$(WARNING_CFLAGS) \$(DEBUG_CFLAGS) \$(PROFILE_CFLAGS) \$(GCOV_CFLAGS) \$(OPT_CFLAGS) \$(DEPRECATED_CFLAGS)"
+GST_OPTION_CXXFLAGS="\$(WARNING_CXXFLAGS) \$(ERROR_CXXFLAGS) \$(DEBUG_CFLAGS) \$(PROFILE_CFLAGS) \$(GCOV_CFLAGS) \$(OPT_CFLAGS) \$(DEPRECATED_CFLAGS)"
AC_SUBST(GST_OPTION_CFLAGS)
+AC_SUBST(GST_OPTION_CXXFLAGS)
dnl GST_ALL_*
dnl vars common to for all internal objects (core libs, elements, applications)
dnl will need the GStreamer source and generated headers
dnl LIBS: XML doesn't need to be added because we don't explicitly use symbols
dnl from LibXML except for in the core library
-GST_ALL_CFLAGS="-I\$(top_srcdir)/libs -I\$(top_srcdir) -I\$(top_builddir) $GLIB_CFLAGS $XML_CFLAGS \$(GST_OPTION_CFLAGS)"
+GST_ALL_CXXFLAGS="-I\$(top_srcdir)/libs -I\$(top_srcdir) -I\$(top_builddir)/libs -I\$(top_builddir) $GLIB_CFLAGS $GLIB_EXTRA_CFLAGS $XML_CFLAGS \$(GST_OPTION_CXXFLAGS) \$(ERROR_CXXFLAGS)"
+GST_ALL_CFLAGS="-I\$(top_srcdir)/libs -I\$(top_srcdir) -I\$(top_builddir)/libs -I\$(top_builddir) $GLIB_CFLAGS $GLIB_EXTRA_CFLAGS $XML_CFLAGS \$(GST_OPTION_CFLAGS) \$(ERROR_CFLAGS)"
dnl FIXME: check if LTLIBINTL is needed everywhere
dnl I presume it is given that it contains the symbols that _() stuff maps to
dnl LDFLAGS really should only contain flags, not libs - they get added before
dnl whatevertarget_LIBS and -L flags here affect the rest of the linking
GST_ALL_LDFLAGS="-no-undefined"
+if test "x${enable_Bsymbolic}" = "xyes"; then
+ GST_ALL_LDFLAGS="$GST_ALL_LDFLAGS -Wl,-Bsymbolic-functions"
+fi
AC_SUBST(GST_ALL_CFLAGS)
+AC_SUBST(GST_ALL_CXXFLAGS)
AC_SUBST(GST_ALL_LIBS)
AC_SUBST(GST_ALL_LDFLAGS)
dnl default vars for all internal objects built on libgstreamer
dnl includes GST_ALL_*
GST_OBJ_CFLAGS="\$(GST_ALL_CFLAGS)"
+GST_OBJ_CXXFLAGS="\$(GST_ALL_CXXFLAGS)"
GST_OBJ_LIBS="\$(top_builddir)/gst/libgstreamer-$GST_MAJORMINOR.la \$(GST_ALL_LIBS)"
AC_SUBST(GST_OBJ_CFLAGS)
+AC_SUBST(GST_OBJ_CXXFLAGS)
AC_SUBST(GST_OBJ_LIBS)
dnl GST_PLUGIN_LDFLAGS
GST_PLUGIN_LDFLAGS="-module -avoid-version -export-symbols-regex '^[_]*gst_plugin_desc\$\$' $GST_ALL_LDFLAGS"
AC_SUBST(GST_PLUGIN_LDFLAGS, "$GST_PLUGIN_LDFLAGS")
-SHAVE_INIT([common],[enable])
+dnl plugin scanner locations
+AS_AC_EXPAND(GST_PLUGIN_SCANNER_INSTALLED,${libexecdir}/gstreamer-$GST_MAJORMINOR/gst-plugin-scanner)
+AC_DEFINE_UNQUOTED(GST_PLUGIN_SCANNER_INSTALLED,
+ "$GST_PLUGIN_SCANNER_INSTALLED", [location of the installed gst-plugin-scanner])
+AC_SUBST(GST_PLUGIN_SCANNER_INSTALLED)
-dnl things for our internal libcheck
-if test "x$BUILD_CHECK" = "xyes"; then
- AG_GST_CHECK_CHECKS()
-fi
+dnl things for our internal libcheck (must be called even if building
+dnl libcheck is disabled because it defines conditionals)
+AG_GST_CHECK_CHECKS()
AC_CONFIG_FILES(
Makefile
-common/shave
-common/shave-libtool
gst/Makefile
gst/gstconfig.h
gst/gstversion.h
libs/gst/check/libcheck/check.h
libs/gst/controller/Makefile
libs/gst/dataprotocol/Makefile
+libs/gst/helpers/Makefile
libs/gst/net/Makefile
plugins/Makefile
plugins/indexers/Makefile
tests/examples/queue/Makefile
tests/examples/streams/Makefile
tests/examples/typefind/Makefile
-tests/examples/xml/Makefile
tools/Makefile
common/Makefile
common/m4/Makefile
docs/slides/Makefile
docs/xsl/Makefile
docs/version.entities
+m4/Makefile
pkgconfig/Makefile
stamp.h
pkgconfig/gstreamer.pc
-e 's/.* GST_MAJORMINOR$/#define GST_MAJORMINOR "'$GST_MAJORMINOR'"/' \
-e "s,.* GST_PACKAGE_NAME$,#define GST_PACKAGE_NAME \"${GST_PACKAGE_NAME}\"," \
-e 's/.* GST_PACKAGE_ORIGIN$/#define GST_PACKAGE_ORIGIN "Unknown package origin"/' \
+ -e "s,.* GST_PACKAGE_RELEASE_DATETIME$,#define GST_PACKAGE_RELEASE_DATETIME \"${GST_PACKAGE_RELEASE_DATETIME}\"," \
-e 's/.* HAVE_CPU_I386$/#define HAVE_CPU_I386 1/' \
-e 's/.* HAVE_FGETPOS$/#define HAVE_FGETPOS 1/' \
-e 's/.* HAVE_FSETPOS$/#define HAVE_FSETPOS 1/' \
-e 's/.* HAVE_WIN32$/#define HAVE_WIN32 1/' \
-e 's/.* HAVE_WINSOCK2_H$/#define HAVE_WINSOCK2_H 1/' \
-e 's/.* HOST_CPU$/#define HOST_CPU "i686"/' \
+ -e 's/.* BUFFER_ALIGNMENT_MALLOC/#define BUFFER_ALIGNMENT_MALLOC 1/' \
-e 's/.* LIBDIR$/#ifdef _DEBUG\n# define LIBDIR PREFIX "\\\\debug\\\\lib"\n#else\n# define LIBDIR PREFIX "\\\\lib"\n#endif/' \
-e 's/.* LOCALEDIR$/#define LOCALEDIR PREFIX "\\\\share\\\\locale"/' \
-e 's/.* PACKAGE$/#define PACKAGE "gstreamer"/' \
-e 's/.* PACKAGE_TARNAME$/#define PACKAGE_TARNAME "'$PACKAGE_TARNAME'"/' \
-e 's/.* PACKAGE_VERSION$/#define PACKAGE_VERSION "'$PACKAGE_VERSION'"/' \
-e 's/.* PLUGINDIR$/#ifdef _DEBUG\n# define PLUGINDIR PREFIX "\\\\debug\\\\lib\\\\gstreamer-0.10"\n#else\n# define PLUGINDIR PREFIX "\\\\lib\\\\gstreamer-0.10"\n#endif/' \
+ -e 's/.* GST_PLUGIN_SCANNER_INSTALLED$/#define GST_PLUGIN_SCANNER_INSTALLED LIBDIR "\\\\gst-plugin-scanner"/' \
-e 's/.* VERSION$/#define VERSION "'$VERSION'"/' \
config.h.in >win32/common/config.h-new
Version : ${VERSION}
Source code location : ${srcdir}
Prefix : ${prefix}
- Compiler : ${SHAVE_SAVED_CC}
+ Compiler : ${CC}
Package name : ${GST_PACKAGE_NAME}
Package origin : ${GST_PACKAGE_ORIGIN}