diff --git a/docs/random/autoplug2 b/docs/random/autoplug2
index 1c727973b9b1a49b325cfe97e611787fc2393c87..22df0ca7d6bfe1d3fd77538c22259e43a300b91f 100644 (file)
--- a/docs/random/autoplug2
+++ b/docs/random/autoplug2
We will create a little pipeline to detect the media type by connecting
a disksrc element to a typefind element. The typefind element will
-repeadedly call all registered typefind functions with the buffer it
+repeatedly call all registered typefind functions with the buffer it
receives on its sink pad. when a typefind function returns a non NULL
GstCaps*, that caps is set to the sink pad of the typefind element and
a signal is emitted to notify the app.
Note that for the audio connection the element list "mpeg1parse, mp3parse,
mpg123" would also connect the srccaps to the audiosink caps. Since the
-"mpeg1parse, mad" list is shorter, it it always prefered by the autoplugger.
+"mpeg1parse, mad" list is shorter, it it always preferred by the autoplugger.
We now have two lists of elementfactories.