index c4df59970fbe624b566a1d97a261901da7489b09..b3122b10c86ec51abc3d2f65bbf855e41f3f4150 100644 (file)
The element can also return a NULL pointer if it has run out of
options for the caps structure. When this happens, both pads are set
-the the NULL caps again and the pad connnection is broken.
+the NULL caps again and the pad connnection is broken.
The negotiation process is stopped after a fixed number of tries,
when the counter has reached some limit. This limit is typically