diff --git a/gst/gstelement.c b/gst/gstelement.c
index 17c0c61bb243a1dc232a74ca9bc254a8aea686ef..afa25b9d3717cbe247c5606cf9bbd57e73886cc7 100644 (file)
--- a/gst/gstelement.c
+++ b/gst/gstelement.c
* An existing pad of an element can be retrieved by name with
* gst_element_get_static_pad(). A new dynamic pad can be created using
* gst_element_request_pad() with a #GstPadTemplate or
- * gst_element_get_request_pad() with the template name such as "src_%d".
+ * gst_element_get_request_pad() with the template name such as "src_\%d".
* An iterator of all pads can be retrieved with gst_element_iterate_pads().
*
* Elements can be linked through their pads.
static void
gst_element_class_init (GstElementClass * klass)
{
- GObjectClass *gobject_class;
- GstObjectClass *gstobject_class;
-
- gobject_class = (GObjectClass *) klass;
- gstobject_class = (GstObjectClass *) klass;
+ GObjectClass *gobject_class = (GObjectClass *) klass;
+#if !defined(GST_DISABLE_LOADSAVE) && !defined(GST_REMOVE_DEPRECATED)
+ GstObjectClass *gstobject_class = (GstObjectClass *) klass;
+#endif
parent_class = g_type_class_peek_parent (klass);
* @element: a #GstElement to find a request pad of.
* @name: the name of the request #GstPad to retrieve.
*
- * Retrieves a pad from the element by name (e.g. "src_%d"). This version only
+ * Retrieves a pad from the element by name (e.g. "src_\%d"). This version only
* retrieves request pads. The pad should be released with
* gst_element_release_request_pad().
*
klass->numpadtemplates++;
}
+/**
+ * gst_element_class_add_static_pad_template:
+ * @klass: the #GstElementClass to add the pad template to.
+ * @templ: (transfer none): a #GstStaticPadTemplate describing the pad
+ * to add to the element class.
+ *
+ * Adds a padtemplate to an element class. This is mainly used in the _base_init
+ * functions of classes.
+ *
+ * Since: 0.10.36
+ */
+void
+gst_element_class_add_static_pad_template (GstElementClass * klass,
+ GstStaticPadTemplate * templ)
+{
+ GstPadTemplate *pt;
+
+ g_return_if_fail (GST_IS_ELEMENT_CLASS (klass));
+
+ pt = gst_static_pad_template_get (templ);
+ gst_element_class_add_pad_template (klass, pt);
+ gst_object_unref (pt);
+}
+
static void
gst_element_class_add_meta_data (GstElementClass * klass,
const gchar * key, const gchar * value)
if (ret == GST_STATE_CHANGE_FAILURE)
goto done;
- /* we got no_preroll, report immediatly */
+ /* we got no_preroll, report immediately */
if (ret == GST_STATE_CHANGE_NO_PREROLL)
goto done;