diff --git a/gst/gstelement.h b/gst/gstelement.h
index 20798e5738b760b3d32313cfed1ab21df7e25c0e..5c3286fb406a720d6fd17528d0c5605cd500ac96 100644 (file)
--- a/gst/gstelement.h
+++ b/gst/gstelement.h
/* gstmessage.h needs State */
/**
* GstState:
- * @GST_STATE_VOID_PENDING : no pending state.
- * @GST_STATE_NULL : the NULL state or initial state of an element
- * @GST_STATE_READY : the element is ready to go to PAUSED
- * @GST_STATE_PAUSED : the element is PAUSED
- * @GST_STATE_PLAYING : the element is PLAYING
- *
- * The posible states an element can be in.
+ * @GST_STATE_VOID_PENDING: no pending state.
+ * @GST_STATE_NULL : the NULL state or initial state of an element.
+ * @GST_STATE_READY : the element is ready to go to PAUSED.
+ * @GST_STATE_PAUSED : the element is PAUSED, it is ready to accept and
+ * process data. Sink elements however only accept one
+ * buffer and then block.
+ * @GST_STATE_PLAYING : the element is PLAYING, the #GstClock is running and
+ * the data is flowing.
+ *
+ * The possible states an element can be in. States can be changed using
+ * gst_element_set_state() and checked using gst_element_get_state().
*/
typedef enum {
GST_STATE_VOID_PENDING = 0,
G_BEGIN_DECLS
-#define GST_TYPE_ELEMENT (gst_element_get_type ())
-#define GST_IS_ELEMENT(obj) (G_TYPE_CHECK_INSTANCE_TYPE ((obj), GST_TYPE_ELEMENT))
-#define GST_IS_ELEMENT_CLASS(klass) (G_TYPE_CHECK_CLASS_TYPE ((klass), GST_TYPE_ELEMENT))
-#define GST_ELEMENT_GET_CLASS(obj) (G_TYPE_INSTANCE_GET_CLASS ((obj), GST_TYPE_ELEMENT, GstElementClass))
-#define GST_ELEMENT(obj) (G_TYPE_CHECK_INSTANCE_CAST ((obj), GST_TYPE_ELEMENT, GstElement))
-#define GST_ELEMENT_CLASS(klass) (G_TYPE_CHECK_CLASS_CAST ((klass), GST_TYPE_ELEMENT, GstElementClass))
-#define GST_ELEMENT_CAST(obj) ((GstElement*)(obj))
+#define GST_TYPE_ELEMENT (gst_element_get_type ())
+#define GST_IS_ELEMENT(obj) (G_TYPE_CHECK_INSTANCE_TYPE ((obj), GST_TYPE_ELEMENT))
+#define GST_IS_ELEMENT_CLASS(klass) (G_TYPE_CHECK_CLASS_TYPE ((klass), GST_TYPE_ELEMENT))
+#define GST_ELEMENT_GET_CLASS(obj) (G_TYPE_INSTANCE_GET_CLASS ((obj), GST_TYPE_ELEMENT, GstElementClass))
+#define GST_ELEMENT(obj) (G_TYPE_CHECK_INSTANCE_CAST ((obj), GST_TYPE_ELEMENT, GstElement))
+#define GST_ELEMENT_CLASS(klass) (G_TYPE_CHECK_CLASS_CAST ((klass), GST_TYPE_ELEMENT, GstElementClass))
+#define GST_ELEMENT_CAST(obj) ((GstElement*)(obj))
/**
* GstStateChangeReturn:
* @GST_STATE_CHANGE_FAILURE : the state change failed
* @GST_STATE_CHANGE_SUCCESS : the state change succeeded
* @GST_STATE_CHANGE_ASYNC : the state change will happen asynchronously
- * @GST_STATE_CHANGE_NO_PREROLL: the state change cannot be prerolled
+ * @GST_STATE_CHANGE_NO_PREROLL: the state change succeeded but the element
+ * cannot produce data in %GST_STATE_PAUSED.
+ * This typically happens with live sources.
*
- * the possible return values from a state change function.
+ * The possible return values from a state change function such as
+ * gst_element_set_state(). Only @GST_STATE_CHANGE_FAILURE is a real failure.
*/
typedef enum {
GST_STATE_CHANGE_FAILURE = 0,
*
* This macro returns the current #GstState of the element.
*/
-#define GST_STATE(elem) (GST_ELEMENT_CAST(elem)->current_state)
+#define GST_STATE(elem) (GST_ELEMENT_CAST(elem)->current_state)
/**
* GST_STATE_NEXT:
*
* This macro returns the next #GstState of the element.
*/
-#define GST_STATE_NEXT(elem) (GST_ELEMENT_CAST(elem)->next_state)
+#define GST_STATE_NEXT(elem) (GST_ELEMENT_CAST(elem)->next_state)
/**
* GST_STATE_PENDING:
*
* This macro returns the currently pending #GstState of the element.
*/
-#define GST_STATE_PENDING(elem) (GST_ELEMENT_CAST(elem)->pending_state)
+#define GST_STATE_PENDING(elem) (GST_ELEMENT_CAST(elem)->pending_state)
+
+/**
+ * GST_STATE_TARGET:
+ * @elem: a #GstElement to return the target state for.
+ *
+ * This macro returns the target #GstState of the element.
+ *
+ * Since: 0.10.13
+ */
+#define GST_STATE_TARGET(elem) (GST_ELEMENT_CAST(elem)->abidata.ABI.target_state)
/**
* GST_STATE_RETURN:
*
* This macro returns the last #GstStateChangeReturn value.
*/
-#define GST_STATE_RETURN(elem) (GST_ELEMENT_CAST(elem)->last_return)
+#define GST_STATE_RETURN(elem) (GST_ELEMENT_CAST(elem)->last_return)
-#define __GST_SIGN(val) ((val) < 0 ? -1 : ((val) > 0 ? 1 : 0))
+#define __GST_SIGN(val) ((val) < 0 ? -1 : ((val) > 0 ? 1 : 0))
/**
* GST_STATE_GET_NEXT:
* @cur: A starting #GstState
* Given a current state @cur and a target state @pending, calculate the next (intermediate)
* #GstState.
*/
-#define GST_STATE_GET_NEXT(cur,pending) ((cur) + __GST_SIGN ((gint)(pending) - (gint)(cur)))
+#define GST_STATE_GET_NEXT(cur,pending) ((GstState)((cur) + __GST_SIGN ((gint)(pending) - (gint)(cur))))
/**
* GST_STATE_TRANSITION:
* @cur: A current state
* Given a current state @cur and a next state @next, calculate the associated
* #GstStateChange transition.
*/
-#define GST_STATE_TRANSITION(cur,next) (((cur)<<3)|(next))
+#define GST_STATE_TRANSITION(cur,next) ((GstStateChange)(((cur)<<3)|(next)))
/**
* GST_STATE_TRANSITION_CURRENT:
* @trans: A #GstStateChange
*
* Given a state transition @trans, extract the current #GstState.
*/
-#define GST_STATE_TRANSITION_CURRENT(trans) ((trans)>>3)
+#define GST_STATE_TRANSITION_CURRENT(trans) ((GstState)((trans)>>3))
/**
* GST_STATE_TRANSITION_NEXT:
* @trans: A #GstStateChange
*
* Given a state transition @trans, extract the next #GstState.
*/
-#define GST_STATE_TRANSITION_NEXT(trans) ((trans)&0x7)
+#define GST_STATE_TRANSITION_NEXT(trans) ((GstState)((trans)&0x7))
/**
* GstStateChange:
- * @GST_STATE_CHANGE_NULL_TO_READY : state change from NULL to READY
- * @GST_STATE_CHANGE_READY_TO_PAUSED : state change from READY to PAUSED
- * @GST_STATE_CHANGE_PAUSED_TO_PLAYING: state change from PAUSED to PLAYING
- * @GST_STATE_CHANGE_PLAYING_TO_PAUSED: state change from PLAYING to PAUSED
- * @GST_STATE_CHANGE_PAUSED_TO_READY : state change from PAUSED to READY
- * @GST_STATE_CHANGE_READY_TO_NULL : state change from READY to NULL
- *
- * The different (interesting) state changes that are passed to the
- * state change functions of elements.
+ * @GST_STATE_CHANGE_NULL_TO_READY : state change from NULL to READY.
+ * <itemizedlist>
+ * <listitem><para>
+ * The element must check if the resources it needs are available. Device
+ * sinks and -sources typically try to probe the device to constrain their
+ * caps.
+ * </para></listitem>
+ * <listitem><para>
+ * The element opens the device (in case feature need to be probed).
+ * </para></listitem>
+ * </itemizedlist>
+ * @GST_STATE_CHANGE_READY_TO_PAUSED : state change from READY to PAUSED.
+ * <itemizedlist>
+ * <listitem><para>
+ * The element pads are activated in order to receive data in PAUSED.
+ * Streaming threads are started.
+ * </para></listitem>
+ * <listitem><para>
+ * Some elements might need to return %GST_STATE_CHANGE_ASYNC and complete
+ * the state change when they have enough information. It is a requirement
+ * for sinks to return %GST_STATE_CHANGE_ASYNC and complete the state change
+ * when they receive the first buffer or %GST_EVENT_EOS (preroll).
+ * Sinks also block the dataflow when in PAUSED.
+ * </para></listitem>
+ * <listitem><para>
+ * A pipeline resets the running_time to 0.
+ * </para></listitem>
+ * <listitem><para>
+ * Live sources return %GST_STATE_CHANGE_NO_PREROLL and don't generate data.
+ * </para></listitem>
+ * </itemizedlist>
+ * @GST_STATE_CHANGE_PAUSED_TO_PLAYING: state change from PAUSED to PLAYING.
+ * <itemizedlist>
+ * <listitem><para>
+ * Most elements ignore this state change.
+ * </para></listitem>
+ * <listitem><para>
+ * The pipeline selects a #GstClock and distributes this to all the children
+ * before setting them to PLAYING. This means that it is only alowed to
+ * synchronize on the #GstClock in the PLAYING state.
+ * </para></listitem>
+ * <listitem><para>
+ * The pipeline uses the #GstClock and the running_time to calculate the
+ * base_time. The base_time is distributed to all children when performing
+ * the state change.
+ * </para></listitem>
+ * <listitem><para>
+ * Sink elements stop blocking on the preroll buffer or event and start
+ * rendering the data.
+ * </para></listitem>
+ * <listitem><para>
+ * Sinks can post %GST_MESSAGE_EOS in the PLAYING state. It is not allowed
+ * to post %GST_MESSAGE_EOS when not in the PLAYING state.
+ * </para></listitem>
+ * <listitem><para>
+ * While streaming in PAUSED or PLAYING elements can create and remove
+ * sometimes pads.
+ * </para></listitem>
+ * <listitem><para>
+ * Live sources start generating data and return %GST_STATE_CHANGE_SUCCESS.
+ * </para></listitem>
+ * </itemizedlist>
+ * @GST_STATE_CHANGE_PLAYING_TO_PAUSED: state change from PLAYING to PAUSED.
+ * <itemizedlist>
+ * <listitem><para>
+ * Most elements ignore this state change.
+ * </para></listitem>
+ * <listitem><para>
+ * The pipeline calculates the running_time based on the last selected
+ * #GstClock and the base_time. It stores this information to continue
+ * playback when going back to the PLAYING state.
+ * </para></listitem>
+ * <listitem><para>
+ * Sinks unblock any #GstClock wait calls.
+ * </para></listitem>
+ * <listitem><para>
+ * When a sink does not have a pending buffer to play, it returns
+ * %GST_STATE_CHANGE_ASYNC from this state change and completes the state
+ * change when it receives a new buffer or an %GST_EVENT_EOS.
+ * </para></listitem>
+ * <listitem><para>
+ * Any queued %GST_MESSAGE_EOS items are removed since they will be reposted
+ * when going back to the PLAYING state. The EOS messages are queued in
+ * #GstBin containers.
+ * </para></listitem>
+ * <listitem><para>
+ * Live sources stop generating data and return %GST_STATE_CHANGE_NO_PREROLL.
+ * </para></listitem>
+ * </itemizedlist>
+ * @GST_STATE_CHANGE_PAUSED_TO_READY : state change from PAUSED to READY.
+ * <itemizedlist>
+ * <listitem><para>
+ * Sinks unblock any waits in the preroll.
+ * </para></listitem>
+ * <listitem><para>
+ * Elements unblock any waits on devices
+ * </para></listitem>
+ * <listitem><para>
+ * Chain or get_range functions return %GST_FLOW_WRONG_STATE.
+ * </para></listitem>
+ * <listitem><para>
+ * The element pads are deactivated so that streaming becomes impossible and
+ * all streaming threads are stopped.
+ * </para></listitem>
+ * <listitem><para>
+ * The sink forgets all negotiated formats
+ * </para></listitem>
+ * <listitem><para>
+ * Elements remove all sometimes pads
+ * </para></listitem>
+ * </itemizedlist>
+ * @GST_STATE_CHANGE_READY_TO_NULL : state change from READY to NULL.
+ * <itemizedlist>
+ * <listitem><para>
+ * Elements close devices
+ * </para></listitem>
+ * <listitem><para>
+ * Elements reset any internal state.
+ * </para></listitem>
+ * </itemizedlist>
+ *
+ * These are the different state changes an element goes through.
+ * %GST_STATE_NULL ⇒ %GST_STATE_PLAYING is called an upwards state change
+ * and %GST_STATE_PLAYING ⇒ %GST_STATE_NULL a downwards state change.
*/
typedef enum /*< flags=0 >*/
{
- GST_STATE_CHANGE_NULL_TO_READY = (GST_STATE_NULL<<3) | GST_STATE_READY,
- GST_STATE_CHANGE_READY_TO_PAUSED = (GST_STATE_READY<<3) | GST_STATE_PAUSED,
- GST_STATE_CHANGE_PAUSED_TO_PLAYING = (GST_STATE_PAUSED<<3) | GST_STATE_PLAYING,
- GST_STATE_CHANGE_PLAYING_TO_PAUSED = (GST_STATE_PLAYING<<3) | GST_STATE_PAUSED,
- GST_STATE_CHANGE_PAUSED_TO_READY = (GST_STATE_PAUSED<<3) | GST_STATE_READY,
- GST_STATE_CHANGE_READY_TO_NULL = (GST_STATE_READY<<3) | GST_STATE_NULL
+ GST_STATE_CHANGE_NULL_TO_READY = (GST_STATE_NULL<<3) | GST_STATE_READY,
+ GST_STATE_CHANGE_READY_TO_PAUSED = (GST_STATE_READY<<3) | GST_STATE_PAUSED,
+ GST_STATE_CHANGE_PAUSED_TO_PLAYING = (GST_STATE_PAUSED<<3) | GST_STATE_PLAYING,
+ GST_STATE_CHANGE_PLAYING_TO_PAUSED = (GST_STATE_PLAYING<<3) | GST_STATE_PAUSED,
+ GST_STATE_CHANGE_PAUSED_TO_READY = (GST_STATE_PAUSED<<3) | GST_STATE_READY,
+ GST_STATE_CHANGE_READY_TO_NULL = (GST_STATE_READY<<3) | GST_STATE_NULL
} GstStateChange;
/**
* @GST_ELEMENT_IS_SINK: the element is a sink
* @GST_ELEMENT_UNPARENTING: Child is being removed from the parent bin.
* gst_bin_remove() on a child already being removed immediately returns FALSE
+ * @GST_ELEMENT_IS_SOURCE: the element is a source. Since 0.10.31
* @GST_ELEMENT_FLAG_LAST: offset to define more flags
*
* The standard flags that an element may have.
GST_ELEMENT_LOCKED_STATE = (GST_OBJECT_FLAG_LAST << 0),
GST_ELEMENT_IS_SINK = (GST_OBJECT_FLAG_LAST << 1),
GST_ELEMENT_UNPARENTING = (GST_OBJECT_FLAG_LAST << 2),
+ GST_ELEMENT_IS_SOURCE = (GST_OBJECT_FLAG_LAST << 3),
/* padding */
GST_ELEMENT_FLAG_LAST = (GST_OBJECT_FLAG_LAST << 16)
} GstElementFlags;
* Gets the name of this element. Use only in core as this is not
* ABI-compatible. Others use gst_element_get_name()
*/
-#define GST_ELEMENT_NAME(elem) (GST_OBJECT_NAME(elem))
+#define GST_ELEMENT_NAME(elem) (GST_OBJECT_NAME(elem))
/**
* GST_ELEMENT_PARENT:
*
* Get the parent object of this element.
*/
-#define GST_ELEMENT_PARENT(elem) (GST_ELEMENT_CAST(GST_OBJECT_PARENT(elem)))
+#define GST_ELEMENT_PARENT(elem) (GST_ELEMENT_CAST(GST_OBJECT_PARENT(elem)))
/**
* GST_ELEMENT_BUS:
*
* Get the message bus of this element.
*/
-#define GST_ELEMENT_BUS(elem) (GST_ELEMENT_CAST(elem)->bus)
+#define GST_ELEMENT_BUS(elem) (GST_ELEMENT_CAST(elem)->bus)
/**
* GST_ELEMENT_CLOCK:
*
* Get the clock of this element
*/
-#define GST_ELEMENT_CLOCK(elem) (GST_ELEMENT_CAST(elem)->clock)
+#define GST_ELEMENT_CLOCK(elem) (GST_ELEMENT_CAST(elem)->clock)
/**
* GST_ELEMENT_PADS:
*
* Get the pads of this elements.
*/
-#define GST_ELEMENT_PADS(elem) (GST_ELEMENT_CAST(elem)->pads)
+#define GST_ELEMENT_PADS(elem) (GST_ELEMENT_CAST(elem)->pads)
+
+/**
+ * GST_ELEMENT_START_TIME:
+ * @elem: a #GstElement to return the start time for.
+ *
+ * This macro returns the start_time of the @elem. The start_time is the
+ * running_time of the pipeline when the element went to PAUSED.
+ *
+ * Since: 0.10.24
+ */
+#define GST_ELEMENT_START_TIME(elem) (GST_ELEMENT_CAST(elem)->abidata.ABI.start_time)
/**
* GST_ELEMENT_ERROR:
- * @el: the element that throws the error
- * @domain: like CORE, LIBRARY, RESOURCE or STREAM (see #GstGError)
- * @code: error code defined for that domain (see #GstGError)
+ * @el: the element that generates the error
+ * @domain: like CORE, LIBRARY, RESOURCE or STREAM (see #gstreamer-GstGError)
+ * @code: error code defined for that domain (see #gstreamer-GstGError)
* @text: the message to display (format string and args enclosed in
parentheses)
* @debug: debugging information for the message (format string and args
enclosed in parentheses)
*
* Utility function that elements can use in case they encountered a fatal
- * data processing error. The pipeline will throw an error signal and the
+ * data processing error. The pipeline will post an error message and the
* application will be requested to stop further media processing.
*/
-#define GST_ELEMENT_ERROR(el, domain, code, text, debug) \
-G_STMT_START { \
- gchar *__txt = _gst_element_error_printf text; \
- gchar *__dbg = _gst_element_error_printf debug; \
- if (__txt) \
- GST_WARNING_OBJECT (el, "error: %s", __txt); \
- if (__dbg) \
- GST_WARNING_OBJECT (el, "error: %s", __dbg); \
- gst_element_message_full (GST_ELEMENT(el), GST_MESSAGE_ERROR, \
- GST_ ## domain ## _ERROR, GST_ ## domain ## _ERROR_ ## code, \
- __txt, __dbg, __FILE__, GST_FUNCTION, __LINE__); \
+#define GST_ELEMENT_ERROR(el, domain, code, text, debug) \
+G_STMT_START { \
+ gchar *__txt = _gst_element_error_printf text; \
+ gchar *__dbg = _gst_element_error_printf debug; \
+ if (__txt) \
+ GST_WARNING_OBJECT (el, "error: %s", __txt); \
+ if (__dbg) \
+ GST_WARNING_OBJECT (el, "error: %s", __dbg); \
+ gst_element_message_full (GST_ELEMENT(el), GST_MESSAGE_ERROR, \
+ GST_ ## domain ## _ERROR, GST_ ## domain ## _ERROR_ ## code, \
+ __txt, __dbg, __FILE__, GST_FUNCTION, __LINE__); \
} G_STMT_END
/**
* GST_ELEMENT_WARNING:
- * @el: the element that throws the error
- * @domain: like CORE, LIBRARY, RESOURCE or STREAM (see #GstGError)
- * @code: error code defined for that domain (see #GstGError)
+ * @el: the element that generates the warning
+ * @domain: like CORE, LIBRARY, RESOURCE or STREAM (see #gstreamer-GstGError)
+ * @code: error code defined for that domain (see #gstreamer-GstGError)
* @text: the message to display (format string and args enclosed in
parentheses)
* @debug: debugging information for the message (format string and args
enclosed in parentheses)
*
* Utility function that elements can use in case they encountered a non-fatal
- * data processing problem. The pipeline will throw a warning signal and the
+ * data processing problem. The pipeline will post a warning message and the
* application will be informed.
*/
-#define GST_ELEMENT_WARNING(el, domain, code, text, debug) \
-G_STMT_START { \
- gchar *__txt = _gst_element_error_printf text; \
- gchar *__dbg = _gst_element_error_printf debug; \
- if (__txt) \
- GST_WARNING_OBJECT (el, "warning: %s", __txt); \
- if (__dbg) \
- GST_WARNING_OBJECT (el, "warning: %s", __dbg); \
- gst_element_message_full (GST_ELEMENT(el), GST_MESSAGE_WARNING, \
- GST_ ## domain ## _ERROR, GST_ ## domain ## _ERROR_ ## code, \
- __txt, __dbg, __FILE__, GST_FUNCTION, __LINE__); \
+#define GST_ELEMENT_WARNING(el, domain, code, text, debug) \
+G_STMT_START { \
+ gchar *__txt = _gst_element_error_printf text; \
+ gchar *__dbg = _gst_element_error_printf debug; \
+ if (__txt) \
+ GST_WARNING_OBJECT (el, "warning: %s", __txt); \
+ if (__dbg) \
+ GST_WARNING_OBJECT (el, "warning: %s", __dbg); \
+ gst_element_message_full (GST_ELEMENT(el), GST_MESSAGE_WARNING, \
+ GST_ ## domain ## _ERROR, GST_ ## domain ## _ERROR_ ## code, \
+ __txt, __dbg, __FILE__, GST_FUNCTION, __LINE__); \
+} G_STMT_END
+
+/**
+ * GST_ELEMENT_INFO:
+ * @el: the element that generates the information
+ * @domain: like CORE, LIBRARY, RESOURCE or STREAM (see #gstreamer-GstGError)
+ * @code: error code defined for that domain (see #gstreamer-GstGError)
+ * @text: the message to display (format string and args enclosed in
+ parentheses)
+ * @debug: debugging information for the message (format string and args
+ enclosed in parentheses)
+ *
+ * Utility function that elements can use in case they want to inform
+ * the application of something noteworthy that is not an error.
+ * The pipeline will post a info message and the
+ * application will be informed.
+ *
+ * Since: 0.10.12
+ */
+#define GST_ELEMENT_INFO(el, domain, code, text, debug) \
+G_STMT_START { \
+ gchar *__txt = _gst_element_error_printf text; \
+ gchar *__dbg = _gst_element_error_printf debug; \
+ if (__txt) \
+ GST_INFO_OBJECT (el, "info: %s", __txt); \
+ if (__dbg) \
+ GST_INFO_OBJECT (el, "info: %s", __dbg); \
+ gst_element_message_full (GST_ELEMENT(el), GST_MESSAGE_INFO, \
+ GST_ ## domain ## _ERROR, GST_ ## domain ## _ERROR_ ## code, \
+ __txt, __dbg, __FILE__, GST_FUNCTION, __LINE__); \
} G_STMT_END
/* the state change mutexes and conds */
#define GST_STATE_UNLOCK_FULL(elem) g_static_rec_mutex_unlock_full(GST_STATE_GET_LOCK(elem))
#define GST_STATE_LOCK_FULL(elem,t) g_static_rec_mutex_lock_full(GST_STATE_GET_LOCK(elem), t)
#define GST_STATE_WAIT(elem) g_cond_wait (GST_STATE_GET_COND (elem), \
- GST_OBJECT_GET_LOCK (elem))
+ GST_OBJECT_GET_LOCK (elem))
#define GST_STATE_TIMED_WAIT(elem, timeval) g_cond_timed_wait (GST_STATE_GET_COND (elem), \
- GST_OBJECT_GET_LOCK (elem), timeval)
+ GST_OBJECT_GET_LOCK (elem), timeval)
#define GST_STATE_SIGNAL(elem) g_cond_signal (GST_STATE_GET_COND (elem));
#define GST_STATE_BROADCAST(elem) g_cond_broadcast (GST_STATE_GET_COND (elem));
* @last_return: the last return value of an element state change
* @bus: the bus of the element. This bus is provided to the element by the
* parent element or the application. A #GstPipeline has a bus of its own.
- * @clock: the clock of the element. This clock is usually provided by to the
+ * @clock: the clock of the element. This clock is usually provided to the
* element by the toplevel #GstPipeline.
* @base_time: the time of the clock right before the element is set to
* PLAYING. Subtracting @base_time from the current clock time in the PLAYING
- * state will yield the stream time.
+ * state will yield the running_time against the clock.
* @numpads: number of pads of the element, includes both source and sink pads.
* @pads: list of pads
* @numsrcpads: number of source pads of the element.
*/
struct _GstElement
{
- GstObject object;
+ GstObject object;
/*< public >*/ /* with LOCK */
GStaticRecMutex *state_lock;
/* element state */
GCond *state_cond;
- guint32 state_cookie;
+ guint32 state_cookie;
GstState current_state;
GstState next_state;
GstState pending_state;
GstStateChangeReturn last_return;
- GstBus *bus;
+ GstBus *bus;
/* allocated clock */
- GstClock *clock;
- GstClockTimeDiff base_time; /* NULL/READY: 0 - PAUSED: current time - PLAYING: difference to clock */
+ GstClock *clock;
+ GstClockTimeDiff base_time; /* NULL/READY: 0 - PAUSED: current time - PLAYING: difference to clock */
/* element pads, these lists can only be iterated while holding
* the LOCK or checking the cookie after each LOCK. */
guint32 pads_cookie;
/*< private >*/
- gpointer _gst_reserved[GST_PADDING];
+ union {
+ struct {
+ /* state set by application */
+ GstState target_state;
+ /* running time of the last PAUSED state */
+ GstClockTime start_time;
+ } ABI;
+ /* adding + 0 to mark ABI change to be undone later */
+ gpointer _gst_reserved[GST_PADDING + 0];
+ } abidata;
};
/**
* @send_event: send a #GstEvent to the element
* @get_query_types: get the supported #GstQueryType of this element
* @query: perform a #GstQuery on the element
+ * @request_new_pad_full: called when a new pad is requested. Since: 0.10.32.
+ * @state_changed: called immediately after a new state was set. Since: 0.10.36.
*
* GStreamer element class. Override the vmethods to implement the element
* functionality.
/*< public >*/
/* the element details */
- GstElementDetails details;
+ /* FIXME-0.11: deprecate this in favour of meta_data */
+ GstElementDetails details;
/* factory that the element was created from */
- GstElementFactory *elementfactory;
+ GstElementFactory *elementfactory;
/* templates for our pads */
GList *padtemplates;
/*< private >*/
/* signal callbacks */
- void (*pad_added) (GstElement *element, GstPad *pad);
- void (*pad_removed) (GstElement *element, GstPad *pad);
- void (*no_more_pads) (GstElement *element);
+ void (*pad_added) (GstElement *element, GstPad *pad);
+ void (*pad_removed) (GstElement *element, GstPad *pad);
+ void (*no_more_pads) (GstElement *element);
/*< public >*/
/* virtual methods for subclasses */
/* request/release pads */
- GstPad* (*request_new_pad) (GstElement *element, GstPadTemplate *templ, const gchar* name);
- void (*release_pad) (GstElement *element, GstPad *pad);
+ GstPad* (*request_new_pad) (GstElement *element, GstPadTemplate *templ, const gchar* name);
+ void (*release_pad) (GstElement *element, GstPad *pad);
/* state changes */
- GstStateChangeReturn (*get_state) (GstElement * element, GstState * state,
- GstState * pending, GstClockTime timeout);
- GstStateChangeReturn (*set_state) (GstElement *element, GstState state);
- GstStateChangeReturn (*change_state) (GstElement *element, GstStateChange transition);
+ GstStateChangeReturn (*get_state) (GstElement * element, GstState * state,
+ GstState * pending, GstClockTime timeout);
+ GstStateChangeReturn (*set_state) (GstElement *element, GstState state);
+ GstStateChangeReturn (*change_state) (GstElement *element, GstStateChange transition);
/* bus */
- void (*set_bus) (GstElement * element, GstBus * bus);
+ void (*set_bus) (GstElement * element, GstBus * bus);
/* set/get clocks */
- GstClock* (*provide_clock) (GstElement *element);
- gboolean (*set_clock) (GstElement *element, GstClock *clock);
+ GstClock* (*provide_clock) (GstElement *element);
+ gboolean (*set_clock) (GstElement *element, GstClock *clock);
/* index */
- GstIndex* (*get_index) (GstElement *element);
- void (*set_index) (GstElement *element, GstIndex *index);
+ GstIndex* (*get_index) (GstElement *element);
+ void (*set_index) (GstElement *element, GstIndex *index);
/* query functions */
- gboolean (*send_event) (GstElement *element, GstEvent *event);
+ gboolean (*send_event) (GstElement *element, GstEvent *event);
- const GstQueryType* (*get_query_types) (GstElement *element);
- gboolean (*query) (GstElement *element, GstQuery *query);
+ const GstQueryType* (*get_query_types) (GstElement *element);
+ gboolean (*query) (GstElement *element, GstQuery *query);
/*< private >*/
- gpointer _gst_reserved[GST_PADDING];
+ /* FIXME-0.11: move up and replace details */
+ gpointer meta_data;
+
+ /*< public >*/
+ /* Virtual method for subclasses (additions) */
+ /* FIXME-0.11 Make this the default behaviour */
+ GstPad* (*request_new_pad_full) (GstElement *element, GstPadTemplate *templ,
+ const gchar* name, const GstCaps *caps);
+
+ void (*state_changed) (GstElement *element, GstState oldstate,
+ GstState newstate, GstState pending);
+
+ /*< private >*/
+ gpointer _gst_reserved[GST_PADDING-3];
};
/* element class pad templates */
-void gst_element_class_add_pad_template (GstElementClass *klass, GstPadTemplate *templ);
-GstPadTemplate* gst_element_class_get_pad_template (GstElementClass *element_class, const gchar *name);
+void gst_element_class_add_pad_template (GstElementClass *klass, GstPadTemplate *templ);
+void gst_element_class_add_static_pad_template (GstElementClass *klass, GstStaticPadTemplate *templ);
+GstPadTemplate* gst_element_class_get_pad_template (GstElementClass *element_class, const gchar *name);
GList* gst_element_class_get_pad_template_list (GstElementClass *element_class);
-void gst_element_class_set_details (GstElementClass *klass,
- const GstElementDetails *details);
+
+/* element class meta data */
+void gst_element_class_set_documentation_uri (GstElementClass * klass, const gchar *uri);
+void gst_element_class_set_icon_name (GstElementClass * klass, const gchar *name);
+#ifndef GST_DISABLE_DEPRECATED
+void gst_element_class_set_details (GstElementClass *klass, const GstElementDetails *details);
+#endif
+void gst_element_class_set_details_simple (GstElementClass *klass,
+ const gchar *longname,
+ const gchar *classification,
+ const gchar *description,
+ const gchar *author);
/* element instance */
-GType gst_element_get_type (void);
+GType gst_element_get_type (void);
/* basic name and parentage stuff from GstObject */
/**
* gst_element_get_name:
- * @elem: a #GstElement to set the name of.
+ * @elem: a #GstElement to get the name of @elem.
+ *
+ * Returns a copy of the name of @elem.
+ * Caller should g_free() the return value after usage.
+ * For a nameless element, this returns NULL, which you can safely g_free()
+ * as well.
+ *
+ * Returns: (transfer full): the name of @elem. g_free() after usage. MT safe.
*
- * Gets the name of the element.
*/
-#define gst_element_get_name(elem) gst_object_get_name(GST_OBJECT_CAST(elem))
+#define gst_element_get_name(elem) gst_object_get_name(GST_OBJECT_CAST(elem))
/**
* gst_element_set_name:
*
* Sets the name of the element, getting rid of the old name if there was one.
*/
-#define gst_element_set_name(elem,name) gst_object_set_name(GST_OBJECT_CAST(elem),name)
+#define gst_element_set_name(elem,name) gst_object_set_name(GST_OBJECT_CAST(elem),name)
/**
* gst_element_get_parent:
* @elem: a #GstElement to get the parent of.
*
- * Gets the parent of an element.
+ * Get the parent of an element.
+ *
+ * Returns: (transfer full): the parent of an element.
*/
-#define gst_element_get_parent(elem) gst_object_get_parent(GST_OBJECT_CAST(elem))
+#define gst_element_get_parent(elem) gst_object_get_parent(GST_OBJECT_CAST(elem))
/**
* gst_element_set_parent:
*
* Sets the parent of an element.
*/
-#define gst_element_set_parent(elem,parent) gst_object_set_parent(GST_OBJECT_CAST(elem),parent)
+#define gst_element_set_parent(elem,parent) gst_object_set_parent(GST_OBJECT_CAST(elem),parent)
/* clocking */
-gboolean gst_element_requires_clock (GstElement *element);
-gboolean gst_element_provides_clock (GstElement *element);
-GstClock* gst_element_provide_clock (GstElement *element);
-GstClock* gst_element_get_clock (GstElement *element);
-gboolean gst_element_set_clock (GstElement *element, GstClock *clock);
-void gst_element_set_base_time (GstElement *element, GstClockTime time);
-GstClockTime gst_element_get_base_time (GstElement *element);
+gboolean gst_element_requires_clock (GstElement *element);
+gboolean gst_element_provides_clock (GstElement *element);
+GstClock* gst_element_provide_clock (GstElement *element);
+GstClock* gst_element_get_clock (GstElement *element);
+gboolean gst_element_set_clock (GstElement *element, GstClock *clock);
+void gst_element_set_base_time (GstElement *element, GstClockTime time);
+GstClockTime gst_element_get_base_time (GstElement *element);
+void gst_element_set_start_time (GstElement *element, GstClockTime time);
+GstClockTime gst_element_get_start_time (GstElement *element);
/* indexes */
-gboolean gst_element_is_indexable (GstElement *element);
-void gst_element_set_index (GstElement *element, GstIndex *index);
-GstIndex* gst_element_get_index (GstElement *element);
+gboolean gst_element_is_indexable (GstElement *element);
+void gst_element_set_index (GstElement *element, GstIndex *index);
+GstIndex* gst_element_get_index (GstElement *element);
/* bus */
-void gst_element_set_bus (GstElement * element, GstBus * bus);
-GstBus * gst_element_get_bus (GstElement * element);
+void gst_element_set_bus (GstElement * element, GstBus * bus);
+GstBus * gst_element_get_bus (GstElement * element);
/* pad management */
-gboolean gst_element_add_pad (GstElement *element, GstPad *pad);
-gboolean gst_element_remove_pad (GstElement *element, GstPad *pad);
-void gst_element_no_more_pads (GstElement *element);
-
-GstPad* gst_element_get_pad (GstElement *element, const gchar *name);
-GstPad* gst_element_get_static_pad (GstElement *element, const gchar *name);
-GstPad* gst_element_get_request_pad (GstElement *element, const gchar *name);
-void gst_element_release_request_pad (GstElement *element, GstPad *pad);
-
-GstIterator * gst_element_iterate_pads (GstElement * element);
-GstIterator * gst_element_iterate_src_pads (GstElement * element);
-GstIterator * gst_element_iterate_sink_pads (GstElement * element);
+gboolean gst_element_add_pad (GstElement *element, GstPad *pad);
+gboolean gst_element_remove_pad (GstElement *element, GstPad *pad);
+void gst_element_no_more_pads (GstElement *element);
+
+#ifndef GST_DISABLE_DEPRECATED
+GstPad* gst_element_get_pad (GstElement *element, const gchar *name);
+#endif /* GST_DISABLE_DEPRECATED */
+GstPad* gst_element_get_static_pad (GstElement *element, const gchar *name);
+GstPad* gst_element_get_request_pad (GstElement *element, const gchar *name);
+GstPad* gst_element_request_pad (GstElement *element,
+ GstPadTemplate *templ,
+ const gchar * name, const GstCaps *caps);
+void gst_element_release_request_pad (GstElement *element, GstPad *pad);
+
+GstIterator * gst_element_iterate_pads (GstElement * element);
+GstIterator * gst_element_iterate_src_pads (GstElement * element);
+GstIterator * gst_element_iterate_sink_pads (GstElement * element);
/* event/query/format stuff */
-gboolean gst_element_send_event (GstElement *element, GstEvent *event);
-gboolean gst_element_seek (GstElement *element, gdouble rate,
- GstFormat format, GstSeekFlags flags,
- GstSeekType cur_type, gint64 cur,
- GstSeekType stop_type, gint64 stop);
-G_CONST_RETURN GstQueryType*
- gst_element_get_query_types (GstElement *element);
-gboolean gst_element_query (GstElement *element, GstQuery *query);
+gboolean gst_element_send_event (GstElement *element, GstEvent *event);
+gboolean gst_element_seek (GstElement *element, gdouble rate,
+ GstFormat format, GstSeekFlags flags,
+ GstSeekType cur_type, gint64 cur,
+ GstSeekType stop_type, gint64 stop);
+const GstQueryType* gst_element_get_query_types (GstElement *element);
+gboolean gst_element_query (GstElement *element, GstQuery *query);
/* messages */
-gboolean gst_element_post_message (GstElement * element, GstMessage * message);
+gboolean gst_element_post_message (GstElement * element, GstMessage * message);
/* error handling */
-gchar * _gst_element_error_printf (const gchar *format, ...);
-void gst_element_message_full (GstElement * element, GstMessageType type,
- GQuark domain, gint code, gchar * text,
- gchar * debug, const gchar * file,
- const gchar * function, gint line);
+/* gcc versions < 3.3 warn about NULL being passed as format to printf */
+#if (defined(GST_USING_PRINTF_EXTENSION) || !defined(__GNUC__) || (__GNUC__ < 3) || (__GNUC__ == 3 && __GNUC_MINOR__ < 3))
+gchar * _gst_element_error_printf (const gchar *format, ...);
+#else
+gchar * _gst_element_error_printf (const gchar *format, ...) G_GNUC_PRINTF (1, 2);
+#endif
+void gst_element_message_full (GstElement * element, GstMessageType type,
+ GQuark domain, gint code, gchar * text,
+ gchar * debug, const gchar * file,
+ const gchar * function, gint line);
/* state management */
-gboolean gst_element_is_locked_state (GstElement *element);
-gboolean gst_element_set_locked_state (GstElement *element, gboolean locked_state);
-gboolean gst_element_sync_state_with_parent (GstElement *element);
-
-GstStateChangeReturn gst_element_get_state (GstElement * element,
- GstState * state,
- GstState * pending,
- GstClockTime timeout);
-GstStateChangeReturn gst_element_set_state (GstElement *element, GstState state);
-
-void gst_element_abort_state (GstElement * element);
-GstStateChangeReturn gst_element_continue_state (GstElement * element,
+gboolean gst_element_is_locked_state (GstElement *element);
+gboolean gst_element_set_locked_state (GstElement *element, gboolean locked_state);
+gboolean gst_element_sync_state_with_parent (GstElement *element);
+
+GstStateChangeReturn gst_element_get_state (GstElement * element,
+ GstState * state,
+ GstState * pending,
+ GstClockTime timeout);
+GstStateChangeReturn gst_element_set_state (GstElement *element, GstState state);
+
+void gst_element_abort_state (GstElement * element);
+GstStateChangeReturn gst_element_change_state (GstElement * element,
+ GstStateChange transition);
+GstStateChangeReturn gst_element_continue_state (GstElement * element,
GstStateChangeReturn ret);
-void gst_element_lost_state (GstElement * element);
+void gst_element_lost_state (GstElement * element);
+void gst_element_lost_state_full (GstElement * element, gboolean new_base_time);
/* factory management */
-GstElementFactory* gst_element_get_factory (GstElement *element);
+GstElementFactory* gst_element_get_factory (GstElement *element);
G_END_DECLS