]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/gstreamer0-10.git/blobdiff - gst/gstinfo.h
Changes to make it possible to LD_PRELOAD libttif
[glsdk/gstreamer0-10.git] / gst / gstinfo.h
index 28df24f0bc3fa7bd35b81f681cfbffc1cc36da37..3abdb2dd42512de0733a3ca29224fa11169f9762 100644 (file)
 
 #include <glib.h>
 #include <glib-object.h>
-#include <gst/gstatomic.h>
-#include <gst/gstlog.h>
 #include <gst/gstconfig.h>
 
 G_BEGIN_DECLS
 
-/*
- * GStreamer's debugging subsystem is an easy way to get information about what
- * the application is doing.
- * It is not meant for programming errors. Use GLibs methods (g_warning and so
- * on for that.
+/**
+ * GstDebugLevel:
+ * @GST_LEVEL_NONE: No debugging level specified or desired. Used to deactivate
+ *  debugging output.
+ * @GST_LEVEL_ERROR: Error messages are to be used only when an error occured
+ *  that stops the application from keeping working correctly.
+ *  An examples is gst_element_error, which outputs a message with this priority.
+ *  It does not mean that the application is terminating as with g_errror.
+ * @GST_LEVEL_WARNING: Warning messages are to inform about abnormal behaviour
+ *  that could lead to problems or weird behaviour later on. An example of this
+ *  would be clocking issues ("your computer is pretty slow") or broken input
+ *  data ("Can't synchronize to stream.")
+ * @GST_LEVEL_INFO: Informational messages should be used to keep the developer
+ *  updated about what is happening.
+ *  Examples where this should be used are when a typefind function has
+ *  successfully determined the type of the stream or when an mp3 plugin detects
+ *  the format to be used. ("This file has mono sound.")
+ * @GST_LEVEL_DEBUG: Debugging messages should be used when something common
+ *  happens that is not the expected default behavior, or something that's
+ *  useful to know but doesn't happen all the time (ie. per loop iteration or
+ *  buffer processed or event handled).
+ *  An example would be notifications about state changes or receiving/sending
+ *  of events.
+ * @GST_LEVEL_LOG: Log messages are messages that are very common but might be
+ *  useful to know. As a rule of thumb a pipeline that is iterating as expected
+ *  should never output anything else but LOG messages. Use this log level to
+ *  log recurring information in chain functions and loop functions, for
+ *  example.
+ * @GST_LEVEL_FIXME: Fixme messages are messages that indicate that something
+ *  in the executed code path is not fully implemented or handled yet. Note
+ *  that this does not replace proper error handling in any way, the purpose
+ *  of this message is to make it easier to spot incomplete/unfinished pieces
+ *  of code when reading the debug log. (Since: 0.10.23)
+ * @GST_LEVEL_TRACE: Tracing-related messages (Since: 0.10.30)
+ *  Examples for this are referencing/dereferencing of objects.
+ * @GST_LEVEL_MEMDUMP: memory dump messages are used to log (small) chunks of
+ *  data as memory dumps in the log. They will be displayed as hexdump with
+ *  ASCII characters. (Since: 0.10.23)
+ * @GST_LEVEL_COUNT: The number of defined debugging levels.
+ *
+ * The level defines the importance of a debugging message. The more important a
+ * message is, the greater the probability that the debugging system outputs it.
  */
-
-/* log levels */
 typedef enum {
   GST_LEVEL_NONE = 0,
   GST_LEVEL_ERROR,
@@ -47,16 +80,30 @@ typedef enum {
   GST_LEVEL_INFO,
   GST_LEVEL_DEBUG,
   GST_LEVEL_LOG,
+  GST_LEVEL_FIXME = 6,
+  GST_LEVEL_TRACE = 7,
+  /* add more */
+  GST_LEVEL_MEMDUMP = 9,
   /* add more */
   GST_LEVEL_COUNT
 } GstDebugLevel;
 
-/* we can now override this to be more general in maintainer builds or cvs checkouts */
+/**
+ * GST_LEVEL_DEFAULT:
+ *
+ * Defines the default debugging level to be used with GStreamer. It is normally
+ * set to #GST_LEVEL_NONE so nothing get printed.
+ * As it can be configured at compile time, developer builds may chose to
+ * override that though.
+ * You can use this as an argument to gst_debug_set_default_threshold() to
+ * reset the debugging output to default behaviour.
+ */
 #ifndef GST_LEVEL_DEFAULT
 #define GST_LEVEL_DEFAULT GST_LEVEL_NONE
 #endif
 
-/* defines for format (colors etc) - don't change them around, it uses terminal layout 
+/* defines for format (colors etc)
+ * don't change them around, it uses terminal layout
  * Terminal color strings:
  * 00=none 01=bold 04=underscore 05=blink 07=reverse 08=concealed
  * Text color codes:
@@ -64,6 +111,30 @@ typedef enum {
  * Background color codes:
  * 40=black 41=red 42=green 43=yellow 44=blue 45=magenta 46=cyan 47=white
  */
+/**
+ * GstDebugColorFlags:
+ * @GST_DEBUG_FG_BLACK: Use black as foreground color.
+ * @GST_DEBUG_FG_RED: Use red as foreground color.
+ * @GST_DEBUG_FG_GREEN: Use green as foreground color.
+ * @GST_DEBUG_FG_YELLOW: Use yellow as foreground color.
+ * @GST_DEBUG_FG_BLUE: Use blue as foreground color.
+ * @GST_DEBUG_FG_MAGENTA: Use magenta as foreground color.
+ * @GST_DEBUG_FG_CYAN: Use cyan as foreground color.
+ * @GST_DEBUG_FG_WHITE: Use white as foreground color.
+ * @GST_DEBUG_BG_BLACK: Use black as background color.
+ * @GST_DEBUG_BG_RED: Use red as background color.
+ * @GST_DEBUG_BG_GREEN: Use green as background color.
+ * @GST_DEBUG_BG_YELLOW: Use yellow as background color.
+ * @GST_DEBUG_BG_BLUE: Use blue as background color.
+ * @GST_DEBUG_BG_MAGENTA: Use magenta as background color.
+ * @GST_DEBUG_BG_CYAN: Use cyan as background color.
+ * @GST_DEBUG_BG_WHITE: Use white as background color.
+ * @GST_DEBUG_BOLD: Make the output bold.
+ * @GST_DEBUG_UNDERLINE: Underline the output.
+ *
+ * These are some terminal style flags you can use when creating your
+ * debugging categories to make them stand out in debugging output.
+ */
 typedef enum {
   /* colors */
   GST_DEBUG_FG_BLACK           = 0x0000,
@@ -93,32 +164,67 @@ typedef enum {
 #define GST_DEBUG_FORMAT_MASK  (0xFF00)
 
 typedef struct _GstDebugCategory GstDebugCategory;
+/**
+ * GstDebugCategory:
+ *
+ * This is the struct that describes the categories. Once initialized with
+ * #GST_DEBUG_CATEGORY_INIT, its values can't be changed anymore.
+ */
 struct _GstDebugCategory {
   /*< private >*/
-  GstAtomicInt *       threshold;
+  gint                  threshold;
   guint                        color;          /* see defines above */
 
   const gchar *                name;
   const gchar *                description;
+
+  void *ext;                /**< for use by LD_PRELOADED trace extension */
 };
 
 /********** some convenience macros for debugging **********/
 
-/* This is needed in printf's if a char* might be NULL. Solaris crashes then */
+/**
+ * GST_STR_NULL:
+ * @str: The string to check.
+ *
+ * Macro to use when a string must not be NULL, but may be NULL. If the string
+ * is NULL, "(NULL)" is printed instead.
+ * In GStreamer printf string arguments may not be NULL, because on some
+ * platforms (ie Solaris) the libc crashes in that case. This includes debugging
+ * strings.
+ */
 #define GST_STR_NULL(str) ((str) ? (str) : "(NULL)")
 
-/* easier debugging for pad names */
+/* FIXME, not MT safe */
+/**
+ * GST_DEBUG_PAD_NAME:
+ * @pad: The pad to debug.
+ *
+ * Evaluates to 2 strings, that describe the pad. Often used in debugging
+ * statements.
+ */
 #define GST_DEBUG_PAD_NAME(pad) \
-  (GST_OBJECT_PARENT(pad) != NULL) ? \
+  (pad != NULL) ?  \
+  ((GST_OBJECT_PARENT(pad) != NULL) ? \
   GST_STR_NULL (GST_OBJECT_NAME (GST_OBJECT_PARENT(pad))) : \
-  "''", GST_OBJECT_NAME (pad)
-
-/* You might want to define GST_FUNCTION in apps' configure script */
+  "''" ) : "''", \
+  (pad != NULL) ? GST_STR_NULL (GST_OBJECT_NAME (pad)) : "''"
 
+/**
+ * GST_FUNCTION:
+ *
+ * This macro should evaluate to the name of the current function and be should
+ * be defined when configuring your project, as it is compiler dependant. If it
+ * is not defined, some default value is used. It is used to provide debugging
+ * output with the function name of the message.
+ *
+ * Note that this is different from G_STRFUNC as we do not want the full
+ * function signature in C++ code.
+ */
 #ifndef GST_FUNCTION
-#if defined (__GNUC__)
-#  define GST_FUNCTION     ((const char*) (__PRETTY_FUNCTION__))
-#elif defined (G_HAVE_ISO_VARARGS)
+#if defined (__GNUC__) || (defined (_MSC_VER) && _MSC_VER >= 1300)
+#  define GST_FUNCTION     ((const char*) (__FUNCTION__))
+#elif defined (__STDC__) && defined (__STDC_VERSION__) && __STDC_VERSION__ >= 199901L
 #  define GST_FUNCTION     ((const char*) (__func__))
 #else
 #  define GST_FUNCTION     ((const char*) ("???"))
@@ -127,80 +233,193 @@ struct _GstDebugCategory {
 
 
 typedef struct _GstDebugMessage GstDebugMessage;
-typedef void (*GstLogFunction) (GstDebugCategory *     category,
-                                GstDebugLevel          level,
-                                const gchar *          file,
-                                const gchar *          function,
-                                gint                   line,
-                                GObject *              object,
-                                GstDebugMessage *      message,
-                                gpointer               data);
-
-/* Disable this subsystem if no varargs macro can be found. 
-   Use a trick so the core builds the functions nonetheless if it wasn't
-   explicitly disabled. */
-#if !defined(G_HAVE_ISO_VARARGS) && !defined(G_HAVE_GNUC_VARARGS)
-#define __GST_DISABLE_GST_DEBUG
-#endif
-#ifdef GST_DISABLE_GST_DEBUG
-#ifndef __GST_DISABLE_GST_DEBUG
-#define __GST_DISABLE_GST_DEBUG
-#endif
+
+/**
+ * GstLogFunction:
+ * @category: a #GstDebugCategory
+ * @level: a #GstDebugLevel
+ * @file: file name
+ * @function: function name
+ * @line: line number
+ * @object: a #GObject
+ * @message: the message
+ * @data: user data for the log function
+ *
+ * Function prototype for a logging function that can be registered with
+ * gst_debug_add_log_function().
+ * Use G_GNUC_NO_INSTRUMENT on that function.
+ */
+typedef void (*GstLogFunction)  (GstDebugCategory * category,
+                                 GstDebugLevel      level,
+                                 const gchar      * file,
+                                 const gchar      * function,
+                                 gint               line,
+                                 GObject          * object,
+                                 GstDebugMessage  * message,
+                                 gpointer           data);
+
+
+/* FIXME 0.11: move this into private headers */
+void            _gst_debug_init (void);
+
+typedef struct {
+       const gchar *file;
+       const gchar *function;
+       const gint   line;
+} GstDebugTraceLocation;
+
+#define GST_DEBUG_TRACE_LOCATION() \
+       { __FILE__, GST_FUNCTION, __LINE__ }
+
+#ifdef GST_USING_PRINTF_EXTENSION
+
+/* not using G_GNUC_PRINTF, since gcc will choke on GST_PTR_FORMAT being %P */
+void               gst_debug_log            (GstDebugCategory * category,
+                                          GstDebugLevel      level,
+                                          const gchar      * file,
+                                          const gchar      * function,
+                                          gint               line,
+                                          GObject          * object,
+                                          const gchar      * format,
+                                          ...) G_GNUC_NO_INSTRUMENT;
+
+void               gst_debug_log2           (GstDebugCategory * category,
+                                          GstDebugLevel      level,
+                                          const GstDebugTraceLocation *location,
+                                          GObject          * object,
+                                          const gchar      * format,
+                                          ...) G_GNUC_NO_INSTRUMENT;
+
+#else /* GST_USING_PRINTF_EXTENSION */
+
+void               gst_debug_log            (GstDebugCategory * category,
+                                          GstDebugLevel      level,
+                                          const gchar      * file,
+                                          const gchar      * function,
+                                          gint               line,
+                                          GObject          * object,
+                                          const gchar      * format,
+                                          ...) G_GNUC_PRINTF (7, 8) G_GNUC_NO_INSTRUMENT;
+
+void               gst_debug_log2           (GstDebugCategory * category,
+                                          GstDebugLevel      level,
+                                          const GstDebugTraceLocation *location,
+                                          GObject          * object,
+                                          const gchar      * format,
+                                          ...) G_GNUC_PRINTF (5, 6) G_GNUC_NO_INSTRUMENT;
+
+#endif /* GST_USING_PRINTF_EXTENSION */
+
+void            gst_debug_log_valist     (GstDebugCategory * category,
+                                          GstDebugLevel      level,
+                                          const gchar      * file,
+                                          const gchar      * function,
+                                          gint               line,
+                                          GObject          * object,
+                                          const gchar      * format,
+                                          va_list            args) G_GNUC_NO_INSTRUMENT;
+
+/* do not use this function, use the GST_DEBUG_CATEGORY_INIT macro */
+GstDebugCategory *_gst_debug_category_new (const gchar * name,
+                                           guint         color,
+                                           const gchar * description);
+/* do not use this function, use the GST_DEBUG_CATEGORY_GET macro */
+GstDebugCategory *_gst_debug_get_category (const gchar *name);
+
+
+/* do not use this function, use the GST_CAT_MEMDUMP_* macros */
+void _gst_debug_dump_mem (GstDebugCategory * cat, const gchar * file,
+    const gchar * func, gint line, GObject * obj, const gchar * msg,
+    const guint8 * data, guint length);
+
+/* we define this to avoid a compiler warning regarding a cast from a function
+ * pointer to a void pointer
+ * (see https://bugzilla.gnome.org/show_bug.cgi?id=309253)
+ */
+typedef        void (* GstDebugFuncPtr)        (void);
+
+/* do no use these functions, use the GST_DEBUG*_FUNCPTR macros */
+void   _gst_debug_register_funcptr     (GstDebugFuncPtr        func,
+                                        const gchar *          ptrname);
+const gchar *
+       _gst_debug_nameof_funcptr       (GstDebugFuncPtr        func) G_GNUC_NO_INSTRUMENT;
+
+
+void            gst_debug_log_valist2    (GstDebugCategory * category,
+                                          GstDebugLevel      level,
+                                          const GstDebugTraceLocation *location,
+                                          GObject          * object,
+                                          const gchar      * format,
+                                          va_list            args) G_GNUC_NO_INSTRUMENT;
+
+const gchar   * gst_debug_message_get    (GstDebugMessage  * message);
+
+gchar *         gst_debug_print_object (gpointer ptr);
+
+#ifdef HAVE_PRINTF_EXTENSION
+gchar *         gst_debug_print_segment (gpointer ptr);
 #endif
 
-#ifndef __GST_DISABLE_GST_DEBUG
-
-void           _gst_debug_init                 (void);
-
-/* note we can't use G_GNUC_PRINTF (7, 8) because gcc chokes on %P, which
- * we use for GST_PTR_FORMAT. */
-void           gst_debug_log                   (GstDebugCategory *     category,
-                                                GstDebugLevel          level,
-                                                const gchar *          file,
-                                                const gchar *          function,
-                                                gint                   line,
-                                                GObject *              object,
-                                                const gchar *          format,
-                                                ...) G_GNUC_NO_INSTRUMENT;
-void           gst_debug_log_valist            (GstDebugCategory *     category,
-                                                GstDebugLevel          level,
-                                                const gchar *          file,
-                                                const gchar *          function,
-                                                gint                   line,
-                                                GObject *              object,
-                                                const gchar *          format,
-                                                va_list                args) G_GNUC_NO_INSTRUMENT;
-
-const gchar *  gst_debug_message_get           (GstDebugMessage *      message);
-
-void           gst_debug_log_default           (GstDebugCategory *     category,
-                                                GstDebugLevel          level,
-                                                const gchar *          file,
-                                                const gchar *          function,
-                                                gint                   line,
-                                                GObject *              object,
-                                                GstDebugMessage *      message,
-                                                gpointer               unused) G_GNUC_NO_INSTRUMENT;
-
-G_CONST_RETURN gchar *
-               gst_debug_level_get_name        (GstDebugLevel          level);
-
-void           gst_debug_add_log_function      (GstLogFunction         func,
-                                                gpointer data);
-guint          gst_debug_remove_log_function   (GstLogFunction         func);
-guint          gst_debug_remove_log_function_by_data (gpointer         data);
-
-void           gst_debug_set_active            (gboolean active);
-gboolean       gst_debug_is_active             (void);
-
-void           gst_debug_set_colored           (gboolean colored);
-gboolean       gst_debug_is_colored            (void);
-
-void           gst_debug_set_default_threshold (GstDebugLevel          level);
-GstDebugLevel  gst_debug_get_default_threshold (void);
-void           gst_debug_set_threshold_for_name (const gchar *         name,
-                                                GstDebugLevel          level);
-void           gst_debug_unset_threshold_for_name (const gchar *       name);
+void            gst_debug_log_default    (GstDebugCategory * category,
+                                          GstDebugLevel      level,
+                                          const gchar      * file,
+                                          const gchar      * function,
+                                          gint               line,
+                                          GObject          * object,
+                                          GstDebugMessage  * message,
+                                          gpointer           unused) G_GNUC_NO_INSTRUMENT;
+
+const gchar *   gst_debug_level_get_name (GstDebugLevel level);
+
+void            gst_debug_add_log_function            (GstLogFunction func,
+                                                       gpointer       data);
+
+guint           gst_debug_remove_log_function         (GstLogFunction func);
+guint           gst_debug_remove_log_function_by_data (gpointer       data);
+
+void            gst_debug_set_active  (gboolean active);
+gboolean        gst_debug_is_active   (void);
+
+void            gst_debug_set_colored (gboolean colored);
+gboolean        gst_debug_is_colored  (void);
+
+void            gst_debug_set_default_threshold      (GstDebugLevel level);
+GstDebugLevel   gst_debug_get_default_threshold      (void);
+void            gst_debug_set_threshold_for_name     (const gchar * name,
+                                                      GstDebugLevel level);
+void            gst_debug_unset_threshold_for_name   (const gchar * name);
+
+
+void            gst_debug_category_free              (GstDebugCategory *       category);
+void               gst_debug_category_set_threshold     (GstDebugCategory *    category,
+                                                      GstDebugLevel            level);
+void            gst_debug_category_reset_threshold   (GstDebugCategory *       category);
+GstDebugLevel   gst_debug_category_get_threshold     (GstDebugCategory *       category);
+const gchar *   gst_debug_category_get_name          (GstDebugCategory *       category);
+guint           gst_debug_category_get_color         (GstDebugCategory *       category);
+const gchar *   gst_debug_category_get_description   (GstDebugCategory *       category);
+GSList *        gst_debug_get_all_categories   (void);
+
+
+gchar * gst_debug_construct_term_color (guint colorinfo);
+gint    gst_debug_construct_win_color  (guint colorinfo);
+
+
+#ifndef GST_DISABLE_GST_DEBUG
+
+#define gst_debug_add_log_function(func,data) \
+G_STMT_START{                                 \
+  if (func == gst_debug_log_default) {        \
+    gst_debug_add_log_function(NULL,data);    \
+  } else {                                    \
+    gst_debug_add_log_function(func,data);    \
+  }                                           \
+}G_STMT_END
+
+#define gst_debug_remove_log_function(func)   \
+    (func == gst_debug_log_default) ?         \
+        gst_debug_remove_log_function(NULL) : \
+        gst_debug_remove_log_function(func)
 
 /**
  * GST_DEBUG_CATEGORY:
@@ -218,6 +437,7 @@ void                gst_debug_unset_threshold_for_name (const gchar *       name);
  * This macro expands to nothing if debugging is disabled.
  */
 #define GST_DEBUG_CATEGORY_EXTERN(cat) extern GstDebugCategory *cat
+
 /**
  * GST_DEBUG_CATEGORY_STATIC:
  * @cat: the category
@@ -226,10 +446,7 @@ void               gst_debug_unset_threshold_for_name (const gchar *       name);
  * This macro expands to nothing if debugging is disabled.
  */
 #define GST_DEBUG_CATEGORY_STATIC(cat) static GstDebugCategory *cat = NULL
-/* do not use this function, use the macros below */
-GstDebugCategory *_gst_debug_category_new      (gchar *                name,
-                                                guint                  color,
-                                                gchar *                description);
+
 /**
  * GST_DEBUG_CATEGORY_INIT:
  * @cat: the category to initialize.
@@ -265,44 +482,415 @@ GstDebugCategory *_gst_debug_category_new        (gchar *                name,
  * </para>
  * </note>
  */
-#define GST_DEBUG_CATEGORY_INIT(cat,name,color,description) G_STMT_START{      \
-  if (cat == NULL)                                                             \
-    cat = _gst_debug_category_new (name,color,description);                    \
+#define GST_DEBUG_CATEGORY_INIT(cat,name,color,description) G_STMT_START{\
+  if (cat == NULL)                                                     \
+    cat = _gst_debug_category_new (name,color,description);            \
 }G_STMT_END
 
-void           gst_debug_category_free         (GstDebugCategory *     category);
-void           gst_debug_category_set_threshold (GstDebugCategory *    category,
-                                                GstDebugLevel          level);
-void           gst_debug_category_reset_threshold (GstDebugCategory *  category);
-GstDebugLevel  gst_debug_category_get_threshold (GstDebugCategory *    category);
-G_CONST_RETURN gchar *
-               gst_debug_category_get_name     (GstDebugCategory *     category);
-guint          gst_debug_category_get_color    (GstDebugCategory *     category);
-G_CONST_RETURN gchar *
-               gst_debug_category_get_description (GstDebugCategory *  category);
-GSList *       gst_debug_get_all_categories    (void);
-
-gchar *                gst_debug_construct_term_color  (guint colorinfo);
-
+/**
+ * GST_DEBUG_CATEGORY_GET:
+ * @cat: the category to initialize.
+ * @name: log category name
+ *
+ * Looks up an existing #GstDebugCategory by its @name and sets @cat. If the
+ * category is not found, but GST_CAT_DEFAULT is defined, that is assigned to
+ * @cat. Otherwise @cat will be NULL.
+ *
+ * |[
+ * GST_DEBUG_CATEGORY_STATIC (gst_myplugin_debug);
+ * #define GST_CAT_DEFAULT gst_myplugin_debug
+ * GST_DEBUG_CATEGORY_STATIC (GST_CAT_PERFORMANCE);
+ * ...
+ * GST_DEBUG_CATEGORY_INIT (gst_myplugin_debug, "myplugin", 0, "nice element");
+ * GST_DEBUG_CATEGORY_GET (GST_CAT_PERFORMANCE, "GST_PERFORMANCE");
+ * ]|
+ *
+ * Since: 0.10.24
+ */
+#ifdef GST_CAT_DEFAULT
+#define GST_DEBUG_CATEGORY_GET(cat,name)  G_STMT_START{\
+  cat = _gst_debug_get_category (name);                        \
+  if (!cat) {                                          \
+    cat = GST_CAT_DEFAULT;                             \
+  }                                                    \
+}G_STMT_END
+#else
+#define GST_DEBUG_CATEGORY_GET(cat,name)  G_STMT_START{\
+  cat = _gst_debug_get_category (name);                        \
+}G_STMT_END
+#endif
 
-extern GstDebugCategory *      GST_CAT_DEFAULT;
+/**
+ * GST_CAT_DEFAULT:
+ *
+ * Default gstreamer core debug log category. Please define your own.
+ */
+GST_EXPORT GstDebugCategory *  GST_CAT_DEFAULT;
 /* this symbol may not be used */
 extern gboolean                        __gst_debug_enabled;
+
+/* since 0.10.7, the min debug level, used for quickly discarding debug
+ * messages that fall under the threshold. */
+GST_EXPORT GstDebugLevel            __gst_debug_min;
+
+/**
+ * GST_CAT_LEVEL_LOG:
+ * @cat: category to use
+ * @level: the severity of the message
+ * @object: the #GObject the message belongs to or NULL if none
+ * @...: A printf-style message to output
+ *
+ * Outputs a debugging message. This is the most general macro for outputting
+ * debugging messages. You will probably want to use one of the ones described
+ * below.
+ */
+#if defined(GST_USING_PRINTF_EXTENSION) && defined(G_HAVE_GNUC_VARARGS)
+#define GST_CAT_LEVEL_LOG_obj(cat,level,object,str,args...) G_STMT_START{  \
+  if (G_UNLIKELY (level <= __gst_debug_min)) {                             \
+    const GstDebugTraceLocation loc = GST_DEBUG_TRACE_LOCATION();          \
+    gst_debug_log2 ((cat), (level), &loc, NULL, "%"GST_PTR_FORMAT" "str,   \
+        (object), ##args );                                                \
+  }                                                                        \
+}G_STMT_END
+#define GST_CAT_LEVEL_LOG_noobj(cat,level,object,str,args...) G_STMT_START{\
+  if (G_UNLIKELY (level <= __gst_debug_min)) {                             \
+    const GstDebugTraceLocation loc = GST_DEBUG_TRACE_LOCATION();          \
+    gst_debug_log2 ((cat), (level), &loc, NULL, (str), ##args );           \
+  }                                                                        \
+}G_STMT_END
+#else
+#  define GST_CAT_LEVEL_LOG_obj   GST_CAT_LEVEL_LOG
+#  define GST_CAT_LEVEL_LOG_noobj GST_CAT_LEVEL_LOG
+#endif
+
+
 #ifdef G_HAVE_ISO_VARARGS
-#define GST_CAT_LEVEL_LOG(cat,level,object,...) G_STMT_START{                  \
-  if (__gst_debug_enabled) {                           \
-    gst_debug_log ((cat), (level), __FILE__, GST_FUNCTION, __LINE__, (GObject *) (object), __VA_ARGS__); \
-  }                                                                            \
+#define GST_CAT_LEVEL_LOG(cat,level,object,...) G_STMT_START{          \
+  if (G_UNLIKELY (level <= __gst_debug_min)) { \
+       const GstDebugTraceLocation loc = GST_DEBUG_TRACE_LOCATION();   \
+    gst_debug_log2 ((cat), (level), &loc, (GObject *) (object),                \
+            __VA_ARGS__);                                                                                      \
+  }                                                                    \
 }G_STMT_END
 #else /* G_HAVE_GNUC_VARARGS */
-#define GST_CAT_LEVEL_LOG(cat,level,object,args...) G_STMT_START{                      \
-  if (__gst_debug_enabled) {                           \
-    gst_debug_log ((cat), (level), __FILE__, GST_FUNCTION, __LINE__, (GObject *) (object), ##args ); \
-  }                                                                            \
+#ifdef G_HAVE_GNUC_VARARGS
+#define GST_CAT_LEVEL_LOG(cat,level,object,args...) G_STMT_START{      \
+  if (G_UNLIKELY (level <= __gst_debug_min)) {                                         \
+    const GstDebugTraceLocation loc = GST_DEBUG_TRACE_LOCATION();      \
+    gst_debug_log2 ((cat), (level), &loc, (GObject *) (object),                \
+            ##args );                                                                                      \
+  }                                                                    \
 }G_STMT_END
+#else /* no variadic macros, use inline */
+static inline void
+GST_CAT_LEVEL_LOG_valist (GstDebugCategory * cat,
+    GstDebugLevel level, gpointer object, const char *format, va_list varargs)
+{
+  if (G_UNLIKELY (level <= __gst_debug_min)) {
+    gst_debug_log_valist (cat, level, "", "", 0, (GObject *) object, format,
+        varargs);
+  }
+}
+
+static inline void
+GST_CAT_LEVEL_LOG (GstDebugCategory * cat, GstDebugLevel level,
+    gpointer object, const char *format, ...)
+{
+  va_list varargs;
+
+  va_start (varargs, format);
+  GST_CAT_LEVEL_LOG_valist (cat, level, object, format, varargs);
+  va_end (varargs);
+}
+#endif
 #endif /* G_HAVE_ISO_VARARGS */
 
-#ifndef GST_DEBUG_ENABLE_DEPRECATED
+/* This one doesn't have varargs in the macro, so it's different than all the
+ * other macros and hence in a separate block right here. Docs chunks are
+ * with the other doc chunks below though. */
+#define __GST_CAT_MEMDUMP_LOG(cat,object,msg,data,length) G_STMT_START{       \
+  if (G_UNLIKELY (GST_LEVEL_MEMDUMP <= __gst_debug_min)) {                    \
+    _gst_debug_dump_mem ((cat), __FILE__, GST_FUNCTION, __LINE__,             \
+        (GObject *) (object), (msg), (data), (length));                       \
+  }                                                                           \
+}G_STMT_END
+
+#define GST_CAT_MEMDUMP_OBJECT(cat,obj,msg,data,length)  \
+    __GST_CAT_MEMDUMP_LOG(cat,obj,msg,data,length)
+#define GST_CAT_MEMDUMP(cat,msg,data,length)             \
+    __GST_CAT_MEMDUMP_LOG(cat,NULL,msg,data,length)
+#define GST_MEMDUMP_OBJECT(obj,msg,data,length)          \
+    __GST_CAT_MEMDUMP_LOG(GST_CAT_DEFAULT,obj,msg,data,length)
+#define GST_MEMDUMP(msg,data,length)                     \
+    __GST_CAT_MEMDUMP_LOG(GST_CAT_DEFAULT,NULL,msg,data,length)
+
+/**
+ * GST_CAT_ERROR_OBJECT:
+ * @cat: category to use
+ * @obj: the #GObject the message belongs to
+ * @...: printf-style message to output
+ *
+ * Output an error message belonging to the given object in the given category.
+ */
+/**
+ * GST_CAT_WARNING_OBJECT:
+ * @cat: category to use
+ * @obj: the #GObject the message belongs to
+ * @...: printf-style message to output
+ *
+ * Output a warning message belonging to the given object in the given category.
+ */
+/**
+ * GST_CAT_INFO_OBJECT:
+ * @cat: category to use
+ * @obj: the #GObject the message belongs to
+ * @...: printf-style message to output
+ *
+ * Output an informational message belonging to the given object in the given
+ * category.
+ */
+/**
+ * GST_CAT_DEBUG_OBJECT:
+ * @cat: category to use
+ * @obj: the #GObject the message belongs to
+ * @...: printf-style message to output
+ *
+ * Output an debugging message belonging to the given object in the given category.
+ */
+/**
+ * GST_CAT_LOG_OBJECT:
+ * @cat: category to use
+ * @obj: the #GObject the message belongs to
+ * @...: printf-style message to output
+ *
+ * Output an logging message belonging to the given object in the given category.
+ */
+/**
+ * GST_CAT_FIXME_OBJECT:
+ * @cat: category to use
+ * @obj: the #GObject the message belongs to
+ * @...: printf-style message to output
+ *
+ * Output a fixme message belonging to the given object in the given category.
+ *
+ * Since: 0.10.23
+ */
+/**
+ * GST_CAT_TRACE_OBJECT:
+ * @cat: category to use
+ * @obj: the #GObject the message belongs to
+ * @...: printf-style message to output
+ *
+ * Output a tracing message belonging to the given object in the given
+ * category.
+ *
+ * Since: 0.10.30
+ */
+/**
+ * GST_CAT_MEMDUMP_OBJECT:
+ * @cat: category to use
+ * @obj: the #GObject the message belongs to
+ * @msg: message string to log with the data
+ * @data: pointer to the data to output
+ * @length: length of the data to output
+ *
+ * Output a hexdump of @data relating to the given object in the given
+ * category.
+ *
+ * Since: 0.10.23
+ */
+
+
+/**
+ * GST_CAT_ERROR:
+ * @cat: category to use
+ * @...: printf-style message to output
+ *
+ * Output an error message in the given category.
+ */
+/**
+ * GST_CAT_WARNING:
+ * @cat: category to use
+ * @...: printf-style message to output
+ *
+ * Output an warning message in the given category.
+ */
+/**
+ * GST_CAT_INFO:
+ * @cat: category to use
+ * @...: printf-style message to output
+ *
+ * Output an informational message in the given category.
+ */
+/**
+ * GST_CAT_DEBUG:
+ * @cat: category to use
+ * @...: printf-style message to output
+ *
+ * Output an debugging message in the given category.
+ */
+/**
+ * GST_CAT_LOG:
+ * @cat: category to use
+ * @...: printf-style message to output
+ *
+ * Output an logging message in the given category.
+ */
+/**
+ * GST_CAT_FIXME:
+ * @cat: category to use
+ * @...: printf-style message to output
+ *
+ * Output an fixme message in the given category.
+ *
+ * Since: 0.10.23
+ */
+/**
+ * GST_CAT_TRACE:
+ * @cat: category to use
+ * @...: printf-style message to output
+ *
+ * Output a tracing message in the given category.
+ *
+ * Since: 0.10.30
+ */
+/**
+ * GST_CAT_MEMDUMP:
+ * @cat: category to use
+ * @msg: message string to log with the data
+ * @data: pointer to the data to output
+ * @length: length of the data to output
+ *
+ * Output a hexdump of @data in the given category.
+ *
+ * Since: 0.10.23
+ */
+
+
+/**
+ * GST_ERROR_OBJECT:
+ * @obj: the #GObject the message belongs to
+ * @...: printf-style message to output
+ *
+ * Output an error message belonging to the given object in the default category.
+ */
+/**
+ * GST_WARNING_OBJECT:
+ * @obj: the #GObject the message belongs to
+ * @...: printf-style message to output
+ *
+ * Output a warning message belonging to the given object in the default category.
+ */
+/**
+ * GST_INFO_OBJECT:
+ * @obj: the #GObject the message belongs to
+ * @...: printf-style message to output
+ *
+ * Output an informational message belonging to the given object in the default
+ * category.
+ */
+/**
+ * GST_DEBUG_OBJECT:
+ * @obj: the #GObject the message belongs to
+ * @...: printf-style message to output
+ *
+ * Output a debugging message belonging to the given object in the default
+ * category.
+ */
+/**
+ * GST_LOG_OBJECT:
+ * @obj: the #GObject the message belongs to
+ * @...: printf-style message to output
+ *
+ * Output a logging message belonging to the given object in the default category.
+ */
+/**
+ * GST_FIXME_OBJECT:
+ * @obj: the #GObject the message belongs to
+ * @...: printf-style message to output
+ *
+ * Output a fixme message belonging to the given object in the default category.
+ *
+ * Since: 0.10.23
+ */
+/**
+ * GST_TRACE_OBJECT:
+ * @obj: the #GObject the message belongs to
+ * @...: printf-style message to output
+ *
+ * Output a tracing message belonging to the given object in the default category.
+ *
+ * Since: 0.10.30
+ */
+/**
+ * GST_MEMDUMP_OBJECT:
+ * @obj: the #GObject the message belongs to
+ * @msg: message string to log with the data
+ * @data: pointer to the data to output
+ * @length: length of the data to output
+ *
+ * Output a logging message belonging to the given object in the default category.
+ *
+ * Since: 0.10.23
+ */
+
+
+/**
+ * GST_ERROR:
+ * @...: printf-style message to output
+ *
+ * Output an error message in the default category.
+ */
+/**
+ * GST_WARNING:
+ * @...: printf-style message to output
+ *
+ * Output a warning message in the default category.
+ */
+/**
+ * GST_INFO:
+ * @...: printf-style message to output
+ *
+ * Output an informational message in the default category.
+ */
+/**
+ * GST_DEBUG:
+ * @...: printf-style message to output
+ *
+ * Output a debugging message in the default category.
+ */
+/**
+ * GST_LOG:
+ * @...: printf-style message to output
+ *
+ * Output a logging message in the default category.
+ */
+/**
+ * GST_FIXME:
+ * @...: printf-style message to output
+ *
+ * Output a fixme message in the default category.
+ *
+ * Since: 0.10.23
+ */
+/**
+ * GST_TRACE:
+ * @...: printf-style message to output
+ *
+ * Output a tracing message in the default category.
+ *
+ * Since: 0.10.30
+ */
+/**
+ * GST_MEMDUMP:
+ * @msg: message string to log with the data
+ * @data: pointer to the data to output
+ * @length: length of the data to output
+ *
+ * Output a hexdump of @data.
+ *
+ * Since: 0.10.23
+ */
 
 #ifdef G_HAVE_ISO_VARARGS
 
@@ -311,215 +899,709 @@ extern gboolean                 __gst_debug_enabled;
 #define GST_CAT_INFO_OBJECT(cat,obj,...)       GST_CAT_LEVEL_LOG (cat, GST_LEVEL_INFO,    obj,  __VA_ARGS__)
 #define GST_CAT_DEBUG_OBJECT(cat,obj,...)      GST_CAT_LEVEL_LOG (cat, GST_LEVEL_DEBUG,   obj,  __VA_ARGS__)
 #define GST_CAT_LOG_OBJECT(cat,obj,...)                GST_CAT_LEVEL_LOG (cat, GST_LEVEL_LOG,     obj,  __VA_ARGS__)
+#define GST_CAT_FIXME_OBJECT(cat,obj,...)      GST_CAT_LEVEL_LOG (cat, GST_LEVEL_FIXME,   obj,  __VA_ARGS__)
+#define GST_CAT_TRACE_OBJECT(cat,obj,...)      GST_CAT_LEVEL_LOG (cat, GST_LEVEL_TRACE,   obj,  __VA_ARGS__)
 
 #define GST_CAT_ERROR(cat,...)                 GST_CAT_LEVEL_LOG (cat, GST_LEVEL_ERROR,   NULL, __VA_ARGS__)
 #define GST_CAT_WARNING(cat,...)               GST_CAT_LEVEL_LOG (cat, GST_LEVEL_WARNING, NULL, __VA_ARGS__)
 #define GST_CAT_INFO(cat,...)                  GST_CAT_LEVEL_LOG (cat, GST_LEVEL_INFO,    NULL, __VA_ARGS__)
 #define GST_CAT_DEBUG(cat,...)                 GST_CAT_LEVEL_LOG (cat, GST_LEVEL_DEBUG,   NULL, __VA_ARGS__)
 #define GST_CAT_LOG(cat,...)                   GST_CAT_LEVEL_LOG (cat, GST_LEVEL_LOG,     NULL, __VA_ARGS__)
+#define GST_CAT_FIXME(cat,...)                 GST_CAT_LEVEL_LOG (cat, GST_LEVEL_FIXME,   NULL, __VA_ARGS__)
+#define GST_CAT_TRACE(cat,...)         GST_CAT_LEVEL_LOG (cat, GST_LEVEL_TRACE,   NULL, __VA_ARGS__)
 
 #define GST_ERROR_OBJECT(obj,...)      GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_ERROR,   obj,  __VA_ARGS__)
 #define GST_WARNING_OBJECT(obj,...)    GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_WARNING, obj,  __VA_ARGS__)
 #define GST_INFO_OBJECT(obj,...)       GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_INFO,    obj,  __VA_ARGS__)
 #define GST_DEBUG_OBJECT(obj,...)      GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_DEBUG,   obj,  __VA_ARGS__)
 #define GST_LOG_OBJECT(obj,...)                GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_LOG,     obj,  __VA_ARGS__)
+#define GST_FIXME_OBJECT(obj,...)      GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_FIXME,   obj,  __VA_ARGS__)
+#define GST_TRACE_OBJECT(obj,...)      GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_TRACE,   obj,  __VA_ARGS__)
 
 #define GST_ERROR(...)                 GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_ERROR,   NULL, __VA_ARGS__)
 #define GST_WARNING(...)               GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_WARNING, NULL, __VA_ARGS__)
 #define GST_INFO(...)                  GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_INFO,    NULL, __VA_ARGS__)
 #define GST_DEBUG(...)                 GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_DEBUG,   NULL, __VA_ARGS__)
 #define GST_LOG(...)                   GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_LOG,     NULL, __VA_ARGS__)
+#define GST_FIXME(...)                 GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_FIXME,   NULL, __VA_ARGS__)
+#define GST_TRACE(...)         GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_TRACE,   NULL, __VA_ARGS__)
 
-#else /* G_HAVE_GNUC_VARARGS */
+#else
+#ifdef G_HAVE_GNUC_VARARGS
 
 #define GST_CAT_ERROR_OBJECT(cat,obj,args...)  GST_CAT_LEVEL_LOG (cat, GST_LEVEL_ERROR,   obj,  ##args )
 #define GST_CAT_WARNING_OBJECT(cat,obj,args...)        GST_CAT_LEVEL_LOG (cat, GST_LEVEL_WARNING, obj,  ##args )
 #define GST_CAT_INFO_OBJECT(cat,obj,args...)   GST_CAT_LEVEL_LOG (cat, GST_LEVEL_INFO,    obj,  ##args )
 #define GST_CAT_DEBUG_OBJECT(cat,obj,args...)  GST_CAT_LEVEL_LOG (cat, GST_LEVEL_DEBUG,   obj,  ##args )
 #define GST_CAT_LOG_OBJECT(cat,obj,args...)    GST_CAT_LEVEL_LOG (cat, GST_LEVEL_LOG,     obj,  ##args )
+#define GST_CAT_FIXME_OBJECT(cat,obj,args...)  GST_CAT_LEVEL_LOG (cat, GST_LEVEL_FIXME,   obj,  ##args )
+#define GST_CAT_TRACE_OBJECT(cat,obj,args...)  GST_CAT_LEVEL_LOG (cat, GST_LEVEL_TRACE,   obj,  ##args )
 
 #define GST_CAT_ERROR(cat,args...)             GST_CAT_LEVEL_LOG (cat, GST_LEVEL_ERROR,   NULL, ##args )
 #define GST_CAT_WARNING(cat,args...)           GST_CAT_LEVEL_LOG (cat, GST_LEVEL_WARNING, NULL, ##args )
 #define GST_CAT_INFO(cat,args...)              GST_CAT_LEVEL_LOG (cat, GST_LEVEL_INFO,    NULL, ##args )
 #define GST_CAT_DEBUG(cat,args...)             GST_CAT_LEVEL_LOG (cat, GST_LEVEL_DEBUG,   NULL, ##args )
 #define GST_CAT_LOG(cat,args...)               GST_CAT_LEVEL_LOG (cat, GST_LEVEL_LOG,     NULL, ##args )
+#define GST_CAT_FIXME(cat,args...)             GST_CAT_LEVEL_LOG (cat, GST_LEVEL_FIXME,   NULL, ##args )
+#define GST_CAT_TRACE(cat,args...)             GST_CAT_LEVEL_LOG (cat, GST_LEVEL_TRACE,   NULL, ##args )
 
 #define GST_ERROR_OBJECT(obj,args...)  GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_ERROR,   obj,  ##args )
 #define GST_WARNING_OBJECT(obj,args...)        GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_WARNING, obj,  ##args )
 #define GST_INFO_OBJECT(obj,args...)   GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_INFO,    obj,  ##args )
 #define GST_DEBUG_OBJECT(obj,args...)  GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_DEBUG,   obj,  ##args )
 #define GST_LOG_OBJECT(obj,args...)    GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_LOG,     obj,  ##args )
+#define GST_FIXME_OBJECT(obj,args...)  GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_FIXME,   obj,  ##args )
+#define GST_TRACE_OBJECT(obj,args...)  GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_TRACE,   obj,  ##args )
 
 #define GST_ERROR(args...)             GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_ERROR,   NULL, ##args )
 #define GST_WARNING(args...)           GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_WARNING, NULL, ##args )
 #define GST_INFO(args...)              GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_INFO,    NULL, ##args )
 #define GST_DEBUG(args...)             GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_DEBUG,   NULL, ##args )
 #define GST_LOG(args...)               GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_LOG,     NULL, ##args )
+#define GST_FIXME(args...)             GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_FIXME,   NULL, ##args )
+#define GST_TRACE(args...)             GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_TRACE,   NULL, ##args )
 
-#endif /* G_HAVE_ISO_VARARGS */
-
-#else /* GST_DEBUG_ENABLE_DEPRECATED */
-/* This is a workaround so the old debugging stuff of GStreamer 0.6 works.
-   This is undocumented and will go when 0.8 comes out. */
+#else
+/* no variadic macros, use inline */
+static inline void
+GST_CAT_ERROR_OBJECT (GstDebugCategory * cat, gpointer obj, const char *format,
+    ...)
+{
+  va_list varargs;
+
+  va_start (varargs, format);
+  GST_CAT_LEVEL_LOG_valist (cat, GST_LEVEL_ERROR, obj, format, varargs);
+  va_end (varargs);
+}
+
+static inline void
+GST_CAT_WARNING_OBJECT (GstDebugCategory * cat, gpointer obj,
+    const char *format, ...)
+{
+  va_list varargs;
+
+  va_start (varargs, format);
+  GST_CAT_LEVEL_LOG_valist (cat, GST_LEVEL_WARNING, obj, format, varargs);
+  va_end (varargs);
+}
+
+static inline void
+GST_CAT_INFO_OBJECT (GstDebugCategory * cat, gpointer obj, const char *format,
+    ...)
+{
+  va_list varargs;
+
+  va_start (varargs, format);
+  GST_CAT_LEVEL_LOG_valist (cat, GST_LEVEL_INFO, obj, format, varargs);
+  va_end (varargs);
+}
+
+static inline void
+GST_CAT_DEBUG_OBJECT (GstDebugCategory * cat, gpointer obj, const char *format,
+    ...)
+{
+  va_list varargs;
+
+  va_start (varargs, format);
+  GST_CAT_LEVEL_LOG_valist (cat, GST_LEVEL_DEBUG, obj, format, varargs);
+  va_end (varargs);
+}
+
+static inline void
+GST_CAT_LOG_OBJECT (GstDebugCategory * cat, gpointer obj, const char *format,
+    ...)
+{
+  va_list varargs;
+
+  va_start (varargs, format);
+  GST_CAT_LEVEL_LOG_valist (cat, GST_LEVEL_LOG, obj, format, varargs);
+  va_end (varargs);
+}
+
+static inline void
+GST_CAT_FIXME_OBJECT (GstDebugCategory * cat, gpointer obj, const char *format,
+    ...)
+{
+  va_list varargs;
+
+  va_start (varargs, format);
+  GST_CAT_LEVEL_LOG_valist (cat, GST_LEVEL_FIXME, obj, format, varargs);
+  va_end (varargs);
+}
+
+static inline void
+GST_CAT_TRACE_OBJECT (GstDebugCategory * cat, gpointer obj, const char *format,
+    ...)
+{
+  va_list varargs;
+
+  va_start (varargs, format);
+  GST_CAT_LEVEL_LOG_valist (cat, GST_LEVEL_TRACE, obj, format, varargs);
+  va_end (varargs);
+}
+
+static inline void
+GST_CAT_ERROR (GstDebugCategory * cat, const char *format, ...)
+{
+  va_list varargs;
+
+  va_start (varargs, format);
+  GST_CAT_LEVEL_LOG_valist (cat, GST_LEVEL_ERROR, NULL, format, varargs);
+  va_end (varargs);
+}
+
+static inline void
+GST_CAT_WARNING (GstDebugCategory * cat, const char *format, ...)
+{
+  va_list varargs;
+
+  va_start (varargs, format);
+  GST_CAT_LEVEL_LOG_valist (cat, GST_LEVEL_WARNING, NULL, format, varargs);
+  va_end (varargs);
+}
+
+static inline void
+GST_CAT_INFO (GstDebugCategory * cat, const char *format, ...)
+{
+  va_list varargs;
+
+  va_start (varargs, format);
+  GST_CAT_LEVEL_LOG_valist (cat, GST_LEVEL_INFO, NULL, format, varargs);
+  va_end (varargs);
+}
+
+static inline void
+GST_CAT_DEBUG (GstDebugCategory * cat, const char *format, ...)
+{
+  va_list varargs;
+
+  va_start (varargs, format);
+  GST_CAT_LEVEL_LOG_valist (cat, GST_LEVEL_DEBUG, NULL, format, varargs);
+  va_end (varargs);
+}
+
+static inline void
+GST_CAT_LOG (GstDebugCategory * cat, const char *format, ...)
+{
+  va_list varargs;
+
+  va_start (varargs, format);
+  GST_CAT_LEVEL_LOG_valist (cat, GST_LEVEL_LOG, NULL, format, varargs);
+  va_end (varargs);
+}
+
+static inline void
+GST_CAT_FIXME (GstDebugCategory * cat, const char *format, ...)
+{
+  va_list varargs;
+
+  va_start (varargs, format);
+  GST_CAT_LEVEL_LOG_valist (cat, GST_LEVEL_FIXME, NULL, format, varargs);
+  va_end (varargs);
+}
+
+static inline void
+GST_CAT_TRACE (GstDebugCategory * cat, const char *format, ...)
+{
+  va_list varargs;
+
+  va_start (varargs, format);
+  GST_CAT_LEVEL_LOG_valist (cat, GST_LEVEL_TRACE, NULL, format, varargs);
+  va_end (varargs);
+}
+
+static inline void
+GST_ERROR_OBJECT (gpointer obj, const char *format, ...)
+{
+  va_list varargs;
+
+  va_start (varargs, format);
+  GST_CAT_LEVEL_LOG_valist (GST_CAT_DEFAULT, GST_LEVEL_ERROR, obj, format,
+      varargs);
+  va_end (varargs);
+}
+
+static inline void
+GST_WARNING_OBJECT (gpointer obj, const char *format, ...)
+{
+  va_list varargs;
+
+  va_start (varargs, format);
+  GST_CAT_LEVEL_LOG_valist (GST_CAT_DEFAULT, GST_LEVEL_WARNING, obj, format,
+      varargs);
+  va_end (varargs);
+}
+
+static inline void
+GST_INFO_OBJECT (gpointer obj, const char *format, ...)
+{
+  va_list varargs;
+
+  va_start (varargs, format);
+  GST_CAT_LEVEL_LOG_valist (GST_CAT_DEFAULT, GST_LEVEL_INFO, obj, format,
+      varargs);
+  va_end (varargs);
+}
+
+static inline void
+GST_DEBUG_OBJECT (gpointer obj, const char *format, ...)
+{
+  va_list varargs;
+
+  va_start (varargs, format);
+  GST_CAT_LEVEL_LOG_valist (GST_CAT_DEFAULT, GST_LEVEL_DEBUG, obj, format,
+      varargs);
+  va_end (varargs);
+}
+
+static inline void
+GST_LOG_OBJECT (gpointer obj, const char *format, ...)
+{
+  va_list varargs;
+
+  va_start (varargs, format);
+  GST_CAT_LEVEL_LOG_valist (GST_CAT_DEFAULT, GST_LEVEL_LOG, obj, format,
+      varargs);
+  va_end (varargs);
+}
+
+static inline void
+GST_FIXME_OBJECT (gpointer obj, const char *format, ...)
+{
+  va_list varargs;
+
+  va_start (varargs, format);
+  GST_CAT_LEVEL_LOG_valist (GST_CAT_DEFAULT, GST_LEVEL_FIXME, obj, format,
+      varargs);
+  va_end (varargs);
+}
+
+static inline void
+GST_TRACE_OBJECT (gpointer obj, const char *format, ...)
+{
+  va_list varargs;
+
+  va_start (varargs, format);
+  GST_CAT_LEVEL_LOG_valist (GST_CAT_DEFAULT, GST_LEVEL_TRACE, obj, format,
+      varargs);
+  va_end (varargs);
+}
+
+static inline void
+GST_ERROR (const char *format, ...)
+{
+  va_list varargs;
+
+  va_start (varargs, format);
+  GST_CAT_LEVEL_LOG_valist (GST_CAT_DEFAULT, GST_LEVEL_ERROR, NULL, format,
+      varargs);
+  va_end (varargs);
+}
+
+static inline void
+GST_WARNING (const char *format, ...)
+{
+  va_list varargs;
+
+  va_start (varargs, format);
+  GST_CAT_LEVEL_LOG_valist (GST_CAT_DEFAULT, GST_LEVEL_WARNING, NULL, format,
+      varargs);
+  va_end (varargs);
+}
+
+static inline void
+GST_INFO (const char *format, ...)
+{
+  va_list varargs;
+
+  va_start (varargs, format);
+  GST_CAT_LEVEL_LOG_valist (GST_CAT_DEFAULT, GST_LEVEL_INFO, NULL, format,
+      varargs);
+  va_end (varargs);
+}
+
+static inline void
+GST_DEBUG (const char *format, ...)
+{
+  va_list varargs;
+
+  va_start (varargs, format);
+  GST_CAT_LEVEL_LOG_valist (GST_CAT_DEFAULT, GST_LEVEL_DEBUG, NULL, format,
+      varargs);
+  va_end (varargs);
+}
+
+static inline void
+GST_LOG (const char *format, ...)
+{
+  va_list varargs;
+
+  va_start (varargs, format);
+  GST_CAT_LEVEL_LOG_valist (GST_CAT_DEFAULT, GST_LEVEL_LOG, NULL,
+      format, varargs);
+  va_end (varargs);
+}
+
+static inline void
+GST_FIXME (const char *format, ...)
+{
+  va_list varargs;
+
+  va_start (varargs, format);
+  GST_CAT_LEVEL_LOG_valist (GST_CAT_DEFAULT, GST_LEVEL_FIXME, NULL, format,
+      varargs);
+  va_end (varargs);
+}
+
+static inline void
+GST_TRACE (const char *format, ...)
+{
+  va_list varargs;
+
+  va_start (varargs, format);
+  GST_CAT_LEVEL_LOG_valist (GST_CAT_DEFAULT, GST_LEVEL_TRACE, NULL, format,
+      varargs);
+  va_end (varargs);
+}
+#endif
+#endif
 
-#ifdef G_HAVE_ISO_VARARGS
-#  define GST_INFO(cat,...)                    GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_INFO,    NULL, __VA_ARGS__)
-#  define GST_DEBUG(cat,...)                   GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_DEBUG,   NULL, __VA_ARGS__)
-#  define GST_INFO_ELEMENT(cat,obj,...)                GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_INFO,    obj, __VA_ARGS__)
-#  define GST_DEBUG_ELEMENT(cat,obj,...)       GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_DEBUG,   obj, __VA_ARGS__)
-#  define GST_DEBUG_ENTER(...)                 GST_DEBUG ("entering: " __VA_ARGS__ )
-#  define GST_DEBUG_LEAVE(...)                 GST_DEBUG ("leaving: "  __VA_ARGS__ )
-#  define GST_INFO_ENTER(...)                  GST_INFO ("entering: " __VA_ARGS__ )
-#  define GST_INFO_LEAVE(...)                  GST_INFO ("leaving: "  __VA_ARGS__ )
-#else /* G_HAVE_GNUC_VARARGS */
-#  define GST_INFO(cat,args...)                        GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_INFO,    NULL, ##args )
-#  define GST_DEBUG(cat,args...)               GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_DEBUG,   NULL, ##args )
-#  define GST_INFO_ELEMENT(cat,obj,args...)    GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_INFO,    obj, ##args )
-#  define GST_DEBUG_ELEMENT(cat,obj,args...)   GST_CAT_LEVEL_LOG (GST_CAT_DEFAULT, GST_LEVEL_DEBUG,   obj, ##args )
-#  define GST_DEBUG_ENTER(args...)             GST_DEBUG ("entering: " ##args )
-#  define GST_DEBUG_LEAVE(args...)             GST_DEBUG ("leaving: "  ##args )
-#  define GST_INFO_ENTER(args...)              GST_INFO ("entering: " ##args )
-#  define GST_INFO_LEAVE(args...)              GST_INFO ("leaving: "  ##args )
-#endif /* G_HAVE_ISO_VARARGS */
 
-#endif /* !GST_DEBUG_ENABLE_DEPRECATED */
+/********** function pointer stuff **********/
 
+/**
+ * GST_DEBUG_REGISTER_FUNCPTR:
+ * @ptr: pointer to the function to register
+ *
+ * Register a pointer to a function with its name, so it can later be used by
+ * GST_DEBUG_FUNCPTR_NAME().
+ *
+ * Use this variant of #GST_DEBUG_FUNCPTR if you do not need to use @ptr.
+ *
+ * Since: 0.10.26
+ */
+#define GST_DEBUG_REGISTER_FUNCPTR(ptr) \
+  _gst_debug_register_funcptr((GstDebugFuncPtr)(ptr), #ptr)
+/**
+ * GST_DEBUG_FUNCPTR:
+ * @ptr: pointer to the function to register
+ *
+ * Register a pointer to a function with its name, so it can later be used by
+ * GST_DEBUG_FUNCPTR_NAME().
+ *
+ * Returns: the value passed to @ptr.
+ */
+#define GST_DEBUG_FUNCPTR(ptr) \
+  (_gst_debug_register_funcptr((GstDebugFuncPtr)(ptr), #ptr) , ptr)
 
-/********** function pointer stuff **********/
-void*          _gst_debug_register_funcptr     (void *                 ptr,
-                                                gchar *                ptrname);
-G_CONST_RETURN gchar*
-               _gst_debug_nameof_funcptr       (void *                 ptr);
+/**
+ * GST_DEBUG_FUNCPTR_NAME:
+ * @ptr: address of the function of which to look up the name
+ *
+ * Retrieves the name of the function, if it was previously registered with
+ * GST_DEBUG_FUNCPTR(). If not, it returns a description of the pointer.
+ *
+ * This macro returns a constant string which must not be modified or
+ * freed by the caller.
+ */
+#define GST_DEBUG_FUNCPTR_NAME(ptr) \
+  _gst_debug_nameof_funcptr((GstDebugFuncPtr)ptr)
 
-#define GST_DEBUG_FUNCPTR(ptr) (_gst_debug_register_funcptr((void *)(ptr), #ptr) , ptr)
-#define GST_DEBUG_FUNCPTR_NAME(ptr) _gst_debug_nameof_funcptr((void *)ptr)
 
 #else /* GST_DISABLE_GST_DEBUG */
 
-#ifdef __GNUC__
+
+#ifndef GST_INFO_C
+
+#if defined(__GNUC__) && __GNUC__ >= 3
 #  pragma GCC poison gst_debug_log
+#  pragma GCC poison gst_debug_log2
 #  pragma GCC poison gst_debug_log_valist
-#  pragma GCC poison gst_debug_log_default
 #  pragma GCC poison _gst_debug_category_new
 #endif
 
-#define _gst_debug_init()                              /* NOP */
+#define __gst_debug_min GST_LEVEL_NONE
 
-#define gst_debug_set_log_function(func,data)          /* NOP */
-#define gst_debug_reset_log_function(void)             /* NOP */
-#define gst_debug_set_default_threshold(level)         /* NOP */
+#define _gst_debug_init()                              G_STMT_START{ }G_STMT_END
+
+#define gst_debug_set_default_threshold(level)         G_STMT_START{ }G_STMT_END
 #define gst_debug_get_default_threshold()              (GST_LEVEL_NONE)
-#define gst_debug_category_set_threshold_for_name(name, level) /* NOP */
-#define gst_debug_category_unset_threshold_for_name(name) /* NOP */
-
-#define gst_debug_level_get_name(level)                        ("NONE")
-#define gst_debug_add_log_function(func,data)          (FALSE)
-#define gst_debug_remove_log_function(func)            (0)
-#define gst_debug_remove_log_function_by_data(data)    (0)
-#define gst_debug_set_active(active)                   /* NOP */
+
+#define gst_debug_level_get_name(level)                                ("NONE")
+#define gst_debug_message_get(message)                         ("")
+#define gst_debug_add_log_function(func,data)          G_STMT_START{ }G_STMT_END
+#define gst_debug_set_active(active)                   G_STMT_START{ }G_STMT_END
 #define gst_debug_is_active()                          (FALSE)
-#define gst_debug_set_colored(colored)                 /* NOP */
+#define gst_debug_set_colored(colored)                 G_STMT_START{ }G_STMT_END
 #define gst_debug_is_colored()                         (FALSE)
-#define gst_debug_set_default_threshold(level)         /* NOP */
+#define gst_debug_set_default_threshold(level)         G_STMT_START{ }G_STMT_END
 #define gst_debug_get_default_threshold()              (GST_LEVEL_NONE)
-#define gst_debug_set_threshold_for_name(name,level)   /* NOP */
-#define gst_debug_unset_threshold_for_name(name)       /* NOP */
-
-#define GST_DEBUG_CATEGORY(var)                                /* NOP */
-#define GST_DEBUG_CATEGORY_EXTERN(var)                 /* NOP */
-#define GST_DEBUG_CATEGORY_STATIC(var)                 /* NOP */
-#define GST_DEBUG_CATEGORY_INIT(var,name,color,desc)   /* NOP */
-#define gst_debug_category_free(category)              /* NOP */
-#define gst_debug_category_set_threshold(category,level) /* NOP */
-#define gst_debug_category_reset_threshold(category)   /* NOP */
+#define gst_debug_set_threshold_for_name(name,level)   G_STMT_START{ }G_STMT_END
+#define gst_debug_unset_threshold_for_name(name)       G_STMT_START{ }G_STMT_END
+
+/* we are using dummy function prototypes here to eat ';' as these macros are
+ * used outside of functions */
+#define GST_DEBUG_CATEGORY(var)                                void _gst_debug_dummy_##var (void)
+#define GST_DEBUG_CATEGORY_EXTERN(var)                 void _gst_debug_dummy_extern_##var (void)
+#define GST_DEBUG_CATEGORY_STATIC(var)                 void _gst_debug_dummy_static_##var (void)
+
+#define GST_DEBUG_CATEGORY_INIT(var,name,color,desc)   G_STMT_START{ }G_STMT_END
+#define GST_DEBUG_CATEGORY_GET(var,name)               G_STMT_START{ }G_STMT_END
+#define gst_debug_category_free(category)              G_STMT_START{ }G_STMT_END
+#define gst_debug_category_set_threshold(category,level) G_STMT_START{ }G_STMT_END
+#define gst_debug_category_reset_threshold(category)   G_STMT_START{ }G_STMT_END
 #define gst_debug_category_get_threshold(category)     (GST_LEVEL_NONE)
 #define gst_debug_category_get_name(cat)               ("")
 #define gst_debug_category_get_color(cat)              (0)
 #define gst_debug_category_get_description(cat)                ("")
 #define gst_debug_get_all_categories()                 (NULL)
 #define gst_debug_construct_term_color(colorinfo)      (g_strdup ("00"))
+#define gst_debug_construct_win_color(colorinfo)       (0)
+
+#endif /* !GST_INFO_C */
 
 #ifdef G_HAVE_ISO_VARARGS
 
-#define GST_CAT_LEVEL_LOG(cat,level,...)               /* NOP */
-
-#define GST_CAT_ERROR_OBJECT(...)                      /* NOP */
-#define GST_CAT_WARNING_OBJECT(...)                    /* NOP */
-#define GST_CAT_INFO_OBJECT(...)                       /* NOP */
-#define GST_CAT_DEBUG_OBJECT(...)                      /* NOP */
-#define GST_CAT_LOG_OBJECT(...)                                /* NOP */
-
-#define GST_CAT_ERROR(...)                             /* NOP */
-#define GST_CAT_WARNING(...)                           /* NOP */
-#define GST_CAT_INFO(...)                              /* NOP */
-#define GST_CAT_DEBUG(...)                             /* NOP */
-#define GST_CAT_LOG(...)                               /* NOP */
-
-#define GST_ERROR_OBJECT(...)                          /* NOP */
-#define GST_WARNING_OBJECT(...)                                /* NOP */
-#define GST_INFO_OBJECT(...)                           /* NOP */
-#define GST_DEBUG_OBJECT(...)                          /* NOP */
-#define GST_LOG_OBJECT(...)                            /* NOP */
-
-#define GST_ERROR(...)                                 /* NOP */
-#define GST_WARNING(...)                               /* NOP */
-#define GST_INFO(...)                                  /* NOP */
-#define GST_DEBUG(...)                                 /* NOP */
-#define GST_LOG(...)                                   /* NOP */
-
-#ifdef GST_DEBUG_ENABLE_DEPRECATED
-#define GST_INFO_ELEMENT(cat,obj,...) /* NOP */
-#define GST_DEBUG_ELEMENT(cat,obj,...) /* NOP */
-#define GST_DEBUG_ENTER(...) /* NOP */
-#define GST_DEBUG_LEAVE(...) /* NOP */
-#define GST_INFO_ENTER(...) /* NOP */
-#define GST_INFO_LEAVE(...) /* NOP */
-#endif /* GST_DEBUG_ENABLE_DEPRECATED */
+#define GST_CAT_LEVEL_LOG(cat,level,...)               G_STMT_START{ }G_STMT_END
+
+#define GST_CAT_ERROR_OBJECT(...)                      G_STMT_START{ }G_STMT_END
+#define GST_CAT_WARNING_OBJECT(...)                    G_STMT_START{ }G_STMT_END
+#define GST_CAT_INFO_OBJECT(...)                       G_STMT_START{ }G_STMT_END
+#define GST_CAT_DEBUG_OBJECT(...)                      G_STMT_START{ }G_STMT_END
+#define GST_CAT_LOG_OBJECT(...)                                G_STMT_START{ }G_STMT_END
+#define GST_CAT_FIXME_OBJECT(...)                      G_STMT_START{ }G_STMT_END
+#define GST_CAT_TRACE_OBJECT(...)                      G_STMT_START{ }G_STMT_END
+
+#define GST_CAT_ERROR(...)                             G_STMT_START{ }G_STMT_END
+#define GST_CAT_WARNING(...)                           G_STMT_START{ }G_STMT_END
+#define GST_CAT_INFO(...)                              G_STMT_START{ }G_STMT_END
+#define GST_CAT_DEBUG(...)                             G_STMT_START{ }G_STMT_END
+#define GST_CAT_LOG(...)                               G_STMT_START{ }G_STMT_END
+#define GST_CAT_FIXME(...)                             G_STMT_START{ }G_STMT_END
+#define GST_CAT_TRACE(...)                             G_STMT_START{ }G_STMT_END
+
+#define GST_ERROR_OBJECT(...)                          G_STMT_START{ }G_STMT_END
+#define GST_WARNING_OBJECT(...)                                G_STMT_START{ }G_STMT_END
+#define GST_INFO_OBJECT(...)                           G_STMT_START{ }G_STMT_END
+#define GST_DEBUG_OBJECT(...)                          G_STMT_START{ }G_STMT_END
+#define GST_LOG_OBJECT(...)                            G_STMT_START{ }G_STMT_END
+#define GST_FIXME_OBJECT(...)                          G_STMT_START{ }G_STMT_END
+#define GST_TRACE_OBJECT(...)                          G_STMT_START{ }G_STMT_END
+
+#define GST_ERROR(...)                                 G_STMT_START{ }G_STMT_END
+#define GST_WARNING(...)                               G_STMT_START{ }G_STMT_END
+#define GST_INFO(...)                                  G_STMT_START{ }G_STMT_END
+#define GST_DEBUG(...)                                 G_STMT_START{ }G_STMT_END
+#define GST_LOG(...)                                   G_STMT_START{ }G_STMT_END
+#define GST_FIXME(...)                                 G_STMT_START{ }G_STMT_END
+#define GST_TRACE(...)                                 G_STMT_START{ }G_STMT_END
 
 #else /* !G_HAVE_ISO_VARARGS */
-
-#define GST_CAT_LEVEL_LOG(cat,level,args...)           /* NOP */
-
-#define GST_CAT_ERROR_OBJECT(args...)                  /* NOP */
-#define GST_CAT_WARNING_OBJECT(args...)                        /* NOP */
-#define GST_CAT_INFO_OBJECT(args...)                   /* NOP */
-#define GST_CAT_DEBUG_OBJECT(args...)                  /* NOP */
-#define GST_CAT_LOG_OBJECT(args...)                    /* NOP */
-
-#define GST_CAT_ERROR(args...)                         /* NOP */
-#define GST_CAT_WARNING(args...)                       /* NOP */
-#define GST_CAT_INFO(args...)                          /* NOP */
-#define GST_CAT_DEBUG(args...)                         /* NOP */
-#define GST_CAT_LOG(args...)                           /* NOP */
-
-#define GST_ERROR_OBJECT(args...)                      /* NOP */
-#define GST_WARNING_OBJECT(args...)                    /* NOP */
-#define GST_INFO_OBJECT(args...)                       /* NOP */
-#define GST_DEBUG_OBJECT(args...)                      /* NOP */
-#define GST_LOG_OBJECT(args...)                                /* NOP */
-
-#define GST_ERROR(args...)                             /* NOP */
-#define GST_WARNING(args...)                           /* NOP */
-#define GST_INFO(args...)                              /* NOP */
-#define GST_DEBUG(args...)                             /* NOP */
-#define GST_LOG(args...)                               /* NOP */
-
-#ifdef GST_DEBUG_ENABLE_DEPRECATED
-#define GST_INFO_ELEMENT(cat,obj,args...) /* NOP */
-#define GST_DEBUG_ELEMENT(cat,obj,args...) /* NOP */
-#define GST_DEBUG_ENTER(args...) /* NOP */
-#define GST_DEBUG_LEAVE(args...) /* NOP */
-#define GST_INFO_ENTER(args...) /* NOP */
-#define GST_INFO_LEAVE(args...) /* NOP */
-#endif /* GST_DEBUG_ENABLE_DEPRECATED */
-
+#ifdef G_HAVE_GNUC_VARARGS
+
+#define GST_CAT_LEVEL_LOG(cat,level,args...)           G_STMT_START{ }G_STMT_END
+
+#define GST_CAT_ERROR_OBJECT(args...)                  G_STMT_START{ }G_STMT_END
+#define GST_CAT_WARNING_OBJECT(args...)                        G_STMT_START{ }G_STMT_END
+#define GST_CAT_INFO_OBJECT(args...)                   G_STMT_START{ }G_STMT_END
+#define GST_CAT_DEBUG_OBJECT(args...)                  G_STMT_START{ }G_STMT_END
+#define GST_CAT_LOG_OBJECT(args...)                    G_STMT_START{ }G_STMT_END
+#define GST_CAT_FIXME_OBJECT(args...)                  G_STMT_START{ }G_STMT_END
+#define GST_CAT_TRACE_OBJECT(args...)                  G_STMT_START{ }G_STMT_END
+
+#define GST_CAT_ERROR(args...)                         G_STMT_START{ }G_STMT_END
+#define GST_CAT_WARNING(args...)                       G_STMT_START{ }G_STMT_END
+#define GST_CAT_INFO(args...)                          G_STMT_START{ }G_STMT_END
+#define GST_CAT_DEBUG(args...)                         G_STMT_START{ }G_STMT_END
+#define GST_CAT_LOG(args...)                           G_STMT_START{ }G_STMT_END
+#define GST_CAT_FIXME(args...)                         G_STMT_START{ }G_STMT_END
+#define GST_CAT_TRACE(args...)                         G_STMT_START{ }G_STMT_END
+
+#define GST_ERROR_OBJECT(args...)                      G_STMT_START{ }G_STMT_END
+#define GST_WARNING_OBJECT(args...)                    G_STMT_START{ }G_STMT_END
+#define GST_INFO_OBJECT(args...)                       G_STMT_START{ }G_STMT_END
+#define GST_DEBUG_OBJECT(args...)                      G_STMT_START{ }G_STMT_END
+#define GST_LOG_OBJECT(args...)                                G_STMT_START{ }G_STMT_END
+#define GST_FIXME_OBJECT(args...)                      G_STMT_START{ }G_STMT_END
+#define GST_TRACE_OBJECT(args...)                      G_STMT_START{ }G_STMT_END
+
+#define GST_ERROR(args...)                             G_STMT_START{ }G_STMT_END
+#define GST_WARNING(args...)                           G_STMT_START{ }G_STMT_END
+#define GST_INFO(args...)                              G_STMT_START{ }G_STMT_END
+#define GST_DEBUG(args...)                             G_STMT_START{ }G_STMT_END
+#define GST_LOG(args...)                               G_STMT_START{ }G_STMT_END
+#define GST_FIXME(args...)                             G_STMT_START{ }G_STMT_END
+#define GST_TRACE(args...)                             G_STMT_START{ }G_STMT_END
+
+#else /* !G_HAVE_GNUC_VARARGS */
+static inline void
+GST_CAT_LEVEL_LOG_valist (GstDebugCategory * cat,
+    GstDebugLevel level, gpointer object, const char *format, va_list varargs)
+{
+}
+
+static inline void
+GST_CAT_ERROR_OBJECT (GstDebugCategory * cat, gpointer obj, const char *format,
+    ...)
+{
+}
+
+static inline void
+GST_CAT_WARNING_OBJECT (GstDebugCategory * cat, gpointer obj,
+    const char *format, ...)
+{
+}
+
+static inline void
+GST_CAT_INFO_OBJECT (GstDebugCategory * cat, gpointer obj, const char *format,
+    ...)
+{
+}
+
+static inline void
+GST_CAT_DEBUG_OBJECT (GstDebugCategory * cat, gpointer obj, const char *format,
+    ...)
+{
+}
+
+static inline void
+GST_CAT_LOG_OBJECT (GstDebugCategory * cat, gpointer obj, const char *format,
+    ...)
+{
+}
+
+static inline void
+GST_CAT_FIXME_OBJECT (GstDebugCategory * cat, gpointer obj, const char *format,
+    ...)
+{
+}
+
+static inline void
+GST_CAT_TRACE_OBJECT (GstDebugCategory * cat, gpointer obj, const char *format,
+    ...)
+{
+}
+
+static inline void
+GST_CAT_ERROR (GstDebugCategory * cat, const char *format, ...)
+{
+}
+
+static inline void
+GST_CAT_WARNING (GstDebugCategory * cat, const char *format, ...)
+{
+}
+
+static inline void
+GST_CAT_INFO (GstDebugCategory * cat, const char *format, ...)
+{
+}
+
+static inline void
+GST_CAT_DEBUG (GstDebugCategory * cat, const char *format, ...)
+{
+}
+
+static inline void
+GST_CAT_LOG (GstDebugCategory * cat, const char *format, ...)
+{
+}
+
+static inline void
+GST_CAT_FIXME (GstDebugCategory * cat, const char *format, ...)
+{
+}
+
+static inline void
+GST_CAT_TRACE (GstDebugCategory * cat, const char *format, ...)
+{
+}
+
+static inline void
+GST_ERROR_OBJECT (gpointer obj, const char *format, ...)
+{
+}
+
+static inline void
+GST_WARNING_OBJECT (gpointer obj, const char *format, ...)
+{
+}
+
+static inline void
+GST_INFO_OBJECT (gpointer obj, const char *format, ...)
+{
+}
+
+static inline void
+GST_DEBUG_OBJECT (gpointer obj, const char *format, ...)
+{
+}
+
+static inline void
+GST_LOG_OBJECT (gpointer obj, const char *format, ...)
+{
+}
+
+static inline void
+GST_FIXME_OBJECT (gpointer obj, const char *format, ...)
+{
+}
+
+static inline void
+GST_TRACE_OBJECT (gpointer obj, const char *format, ...)
+{
+}
+
+static inline void
+GST_ERROR (const char *format, ...)
+{
+}
+
+static inline void
+GST_WARNING (const char *format, ...)
+{
+}
+
+static inline void
+GST_INFO (const char *format, ...)
+{
+}
+
+static inline void
+GST_DEBUG (const char *format, ...)
+{
+}
+
+static inline void
+GST_LOG (const char *format, ...)
+{
+}
+
+static inline void
+GST_FIXME (const char *format, ...)
+{
+}
+
+static inline void
+GST_TRACE (const char *format, ...)
+{
+}
+
+#endif /* G_HAVE_GNUC_VARARGS */
 #endif /* G_HAVE_ISO_VARARGS */
 
+#define GST_DEBUG_REGISTER_FUNCPTR(ptr) G_STMT_START{ }G_STMT_END
 #define GST_DEBUG_FUNCPTR(ptr) (ptr)
 #define GST_DEBUG_FUNCPTR_NAME(ptr) (g_strdup_printf ("%p", ptr))
 
+#define GST_CAT_MEMDUMP_OBJECT(cat,obj,msg,data,length) G_STMT_START{ }G_STMT_END
+#define GST_CAT_MEMDUMP(cat,msg,data,length)            G_STMT_START{ }G_STMT_END
+#define GST_MEMDUMP_OBJECT(obj,msg,data,length)         G_STMT_START{ }G_STMT_END
+#define GST_MEMDUMP(msg,data,length)                    G_STMT_START{ }G_STMT_END
+
 #endif /* GST_DISABLE_GST_DEBUG */
 
+
 void gst_debug_print_stack_trace (void);
 
 G_END_DECLS