diff --git a/gst/gstquery.c b/gst/gstquery.c
index 2c6783ed81f70b8d6032e674c127b48df6f1855d..1d7f5f99b4e6a354e538ac3456d70e8941c5fb57 100644 (file)
--- a/gst/gstquery.c
+++ b/gst/gstquery.c
* 2000 Wim Taymans <wim.taymans@chello.be>
* 2005 Wim Taymans <wim@fluendo.com>
*
- * gstquery.c: GstQueryType registration
+ * gstquery.c: GstQueryType registration and Query parsing/creation
*
* This library is free software; you can redistribute it and/or
* modify it under the terms of the GNU Library General Public
* Free Software Foundation, Inc., 59 Temple Place - Suite 330,
* Boston, MA 02111-1307, USA.
*/
+
/**
* SECTION:gstquery
- * @short_description: Dynamically register new query types and parse results
+ * @short_description: Dynamically register new query types. Provide functions
+ * to create queries, and to set and parse values in them.
* @see_also: #GstPad, #GstElement
*
- * GstQuery functions are used to register a new query types to the gstreamer core.
- * Query types can be used to perform queries on pads and elements.
+ * GstQuery functions are used to register new query types to the gstreamer
+ * core and use them.
+ * Queries can be performed on pads (gst_pad_query()) and elements
+ * (gst_element_query()). Please note that some queries might need a running
+ * pipeline to work.
+ *
+ * Queries can be created using the gst_query_new_*() functions.
+ * Query values can be set using gst_query_set_*(), and parsed using
+ * gst_query_parse_*() helpers.
+ *
+ * The following example shows how to query the duration of a pipeline:
+ *
+ * <example>
+ * <title>Query duration on a pipeline</title>
+ * <programlisting>
+ * GstQuery *query;
+ * gboolean res;
+ * query = gst_query_new_duration (GST_FORMAT_TIME);
+ * res = gst_element_query (pipeline, query);
+ * if (res) {
+ * gint64 duration;
+ * gst_query_parse_duration (query, NULL, &duration);
+ * g_print ("duration = %"GST_TIME_FORMAT, GST_TIME_ARGS (duration));
+ * }
+ * else {
+ * g_print ("duration query failed...");
+ * }
+ * gst_query_unref (query);
+ * </programlisting>
+ * </example>
*
- * Query answer can be parsed using gst_query_parse_xxx() helpers.
+ * Last reviewed on 2006-02-14 (0.10.4)
*/
-#include <string.h>
#include "gst_private.h"
+#include "gstinfo.h"
#include "gstquery.h"
+#include "gstvalue.h"
#include "gstenumtypes.h"
+#include "gstquark.h"
+#include "gsturi.h"
GST_DEBUG_CATEGORY_STATIC (gst_query_debug);
#define GST_CAT_DEFAULT gst_query_debug
-static void gst_query_init (GTypeInstance * instance, gpointer g_class);
-static void gst_query_class_init (gpointer g_class, gpointer class_data);
static void gst_query_finalize (GstQuery * query);
static GstQuery *_gst_query_copy (GstQuery * query);
-
static GStaticMutex mutex = G_STATIC_MUTEX_INIT;
static GList *_gst_queries = NULL;
static GHashTable *_nick_to_query = NULL;
static GHashTable *_query_type_to_nick = NULL;
static guint32 _n_values = 1; /* we start from 1 because 0 reserved for NONE */
+static GstMiniObjectClass *parent_class = NULL;
+
static GstQueryTypeDefinition standard_definitions[] = {
- {GST_QUERY_POSITION, "position", "Current position and total duration"},
- {GST_QUERY_LATENCY, "latency", "Latency"},
- {GST_QUERY_JITTER, "jitter", "Jitter"},
- {GST_QUERY_RATE, "rate", "Configured rate 1000000 = 1"},
- {GST_QUERY_SEEKING, "seeking", "Seeking capabilities and parameters"},
- {GST_QUERY_SEGMENT, "segment", "currently configured segment"},
- {GST_QUERY_CONVERT, "convert", "Converting between formats"},
- {GST_QUERY_FORMATS, "formats", "Supported formats for conversion"},
- {0, NULL, NULL}
+ {GST_QUERY_POSITION, "position", "Current position", 0},
+ {GST_QUERY_DURATION, "duration", "Total duration", 0},
+ {GST_QUERY_LATENCY, "latency", "Latency", 0},
+ {GST_QUERY_JITTER, "jitter", "Jitter", 0},
+ {GST_QUERY_RATE, "rate", "Configured rate 1000000 = 1", 0},
+ {GST_QUERY_SEEKING, "seeking", "Seeking capabilities and parameters", 0},
+ {GST_QUERY_SEGMENT, "segment", "currently configured segment", 0},
+ {GST_QUERY_CONVERT, "convert", "Converting between formats", 0},
+ {GST_QUERY_FORMATS, "formats", "Supported formats for conversion", 0},
+ {GST_QUERY_BUFFERING, "buffering", "Buffering status", 0},
+ {GST_QUERY_CUSTOM, "custom", "Custom query", 0},
+ {GST_QUERY_URI, "uri", "URI of the source or sink", 0},
+ {GST_QUERY_BUFFERS, "buffers", "Minimum buffer requirements", 0},
+ {GST_QUERY_NONE, NULL, NULL, 0}
};
void
}
while (standards->nick) {
- g_hash_table_insert (_nick_to_query, standards->nick, standards);
+ standards->quark = g_quark_from_static_string (standards->nick);
+ g_hash_table_insert (_nick_to_query, (gpointer) standards->nick, standards);
g_hash_table_insert (_query_type_to_nick,
GINT_TO_POINTER (standards->value), standards);
}
g_static_mutex_unlock (&mutex);
- gst_query_get_type ();
+ g_type_class_ref (gst_query_get_type ());
}
-GType
-gst_query_get_type (void)
+/**
+ * gst_query_type_get_name:
+ * @query: the query type
+ *
+ * Get a printable name for the given query type. Do not modify or free.
+ *
+ * Returns: a reference to the static name of the query.
+ */
+const gchar *
+gst_query_type_get_name (GstQueryType query)
{
- static GType _gst_query_type;
+ const GstQueryTypeDefinition *def;
- if (G_UNLIKELY (_gst_query_type == 0)) {
- static const GTypeInfo query_info = {
- sizeof (GstQueryClass),
- NULL,
- NULL,
- gst_query_class_init,
- NULL,
- NULL,
- sizeof (GstQuery),
- 0,
- gst_query_init,
- NULL
- };
+ def = gst_query_type_get_details (query);
- _gst_query_type = g_type_register_static (GST_TYPE_MINI_OBJECT,
- "GstQuery", &query_info, 0);
- }
- return _gst_query_type;
+ return def->nick;
+}
+
+/**
+ * gst_query_type_to_quark:
+ * @query: the query type
+ *
+ * Get the unique quark for the given query type.
+ *
+ * Returns: the quark associated with the query type
+ */
+GQuark
+gst_query_type_to_quark (GstQueryType query)
+{
+ const GstQueryTypeDefinition *def;
+
+ def = gst_query_type_get_details (query);
+
+ return def->quark;
}
+G_DEFINE_TYPE (GstQuery, gst_query, GST_TYPE_MINI_OBJECT);
+
static void
-gst_query_class_init (gpointer g_class, gpointer class_data)
+gst_query_class_init (GstQueryClass * klass)
{
- GstQueryClass *query_class = GST_QUERY_CLASS (g_class);
+ parent_class = g_type_class_peek_parent (klass);
- query_class->mini_object_class.copy =
- (GstMiniObjectCopyFunction) _gst_query_copy;
- query_class->mini_object_class.finalize =
+ klass->mini_object_class.copy = (GstMiniObjectCopyFunction) _gst_query_copy;
+ klass->mini_object_class.finalize =
(GstMiniObjectFinalizeFunction) gst_query_finalize;
}
+static void
+gst_query_init (GstQuery * query)
+{
+}
+
static void
gst_query_finalize (GstQuery * query)
{
gst_structure_set_parent_refcount (query->structure, NULL);
gst_structure_free (query->structure);
}
-}
-
-static void
-gst_query_init (GTypeInstance * instance, gpointer g_class)
-{
+/* GST_MINI_OBJECT_CLASS (parent_class)->finalize (GST_MINI_OBJECT (query)); */
}
static GstQuery *
* @description: The description of the new query
*
* Create a new GstQueryType based on the nick or return an
- * allrady registered query with that nick
+ * already registered query with that nick
*
* Returns: A new GstQueryType or an already registered query
* with the same nick.
GstQueryTypeDefinition *query;
GstQueryType lookup;
- g_return_val_if_fail (nick != NULL, 0);
- g_return_val_if_fail (description != NULL, 0);
+ g_return_val_if_fail (nick != NULL, GST_QUERY_NONE);
+ g_return_val_if_fail (description != NULL, GST_QUERY_NONE);
lookup = gst_query_type_get_by_nick (nick);
if (lookup != GST_QUERY_NONE)
return lookup;
- query = g_new0 (GstQueryTypeDefinition, 1);
- query->value = _n_values;
+ query = g_slice_new (GstQueryTypeDefinition);
+ query->value = (GstQueryType) _n_values;
query->nick = g_strdup (nick);
query->description = g_strdup (description);
+ query->quark = g_quark_from_static_string (query->nick);
g_static_mutex_lock (&mutex);
- g_hash_table_insert (_nick_to_query, query->nick, query);
+ g_hash_table_insert (_nick_to_query, (gpointer) query->nick, query);
g_hash_table_insert (_query_type_to_nick, GINT_TO_POINTER (query->value),
query);
_gst_queries = g_list_append (_gst_queries, query);
* gst_query_type_get_by_nick:
* @nick: The nick of the query
*
- * Return the query registered with the given nick.
+ * Get the query type registered with @nick.
*
- * Returns: The query with @nick or GST_QUERY_NONE
+ * Returns: The query registered with @nick or #GST_QUERY_NONE
* if the query was not registered.
*/
GstQueryType
{
GstQueryTypeDefinition *query;
- g_return_val_if_fail (nick != NULL, 0);
+ g_return_val_if_fail (nick != NULL, GST_QUERY_NONE);
g_static_mutex_lock (&mutex);
query = g_hash_table_lookup (_nick_to_query, nick);
/**
* gst_query_types_contains:
* @types: The query array to search
- * @type: the querytype to find
+ * @type: the #GstQueryType to find
*
- * See if the given query is inside the query array.
+ * See if the given #GstQueryType is inside the @types query types array.
*
- * Returns: TRUE if the query is found inside the array
+ * Returns: TRUE if the type is found inside the array
*/
gboolean
gst_query_types_contains (const GstQueryType * types, GstQueryType type)
/**
* gst_query_type_get_details:
- * @type: The query to get details of
+ * @type: a #GstQueryType
*
- * Get details about the given query.
+ * Get details about the given #GstQueryType.
*
- * Returns: The #GstQueryTypeDefinition for @query or NULL on failure.
+ * Returns: The #GstQueryTypeDefinition for @type or NULL on failure.
*/
const GstQueryTypeDefinition *
gst_query_type_get_details (GstQueryType type)
/**
* gst_query_type_iterate_definitions:
*
- * Get an Iterator of all the registered query types. The querytype
- * definition is read only.
+ * Get a #GstIterator of all the registered query types. The definitions
+ * iterated over are read only.
+ *
+ * Free-function: gst_iterator_free
*
- * Returns: A #GstIterator of #GstQueryTypeDefinition.
+ * Returns: (transfer full): a #GstIterator of #GstQueryTypeDefinition.
*/
GstIterator *
gst_query_type_iterate_definitions (void)
GstIterator *result;
g_static_mutex_lock (&mutex);
- result = gst_iterator_new_list (g_static_mutex_get_mutex (&mutex),
- &_n_values, &_gst_queries, NULL, NULL, NULL);
+ /* FIXME: register a boxed type for GstQueryTypeDefinition */
+ result = gst_iterator_new_list (G_TYPE_POINTER,
+ g_static_mutex_get_mutex (&mutex), &_n_values, &_gst_queries,
+ NULL, NULL, NULL);
g_static_mutex_unlock (&mutex);
return result;
query = (GstQuery *) gst_mini_object_new (GST_TYPE_QUERY);
- GST_DEBUG ("creating new query %p %d", query, type);
+ GST_DEBUG ("creating new query %p %s", query, gst_query_type_get_name (type));
query->type = type;
* @format: the default #GstFormat for the new query
*
* Constructs a new query stream position query object. Use gst_query_unref()
- * when done with it.
+ * when done with it. A position query is used to query the current position
+ * of playback in the streams, in some format.
+ *
+ * Free-function: gst_query_unref
*
- * Returns: A new #GstQuery
+ * Returns: (transfer full): a new #GstQuery
*/
GstQuery *
gst_query_new_position (GstFormat format)
GstQuery *query;
GstStructure *structure;
- structure = gst_structure_new ("GstQueryPosition",
- "format", GST_TYPE_FORMAT, format,
- "cur", G_TYPE_INT64, (gint64) - 1,
- "end", G_TYPE_INT64, (gint64) - 1, NULL);
+ structure = gst_structure_id_new (GST_QUARK (QUERY_POSITION),
+ GST_QUARK (FORMAT), GST_TYPE_FORMAT, format,
+ GST_QUARK (CURRENT), G_TYPE_INT64, G_GINT64_CONSTANT (-1), NULL);
+
query = gst_query_new (GST_QUERY_POSITION, structure);
return query;
/**
* gst_query_set_position:
- * @query: the query to fill in
+ * @query: a #GstQuery with query type GST_QUERY_POSITION
* @format: the requested #GstFormat
- * @cur: the current position
- * @end: the end position
+ * @cur: the position to set
*
- * Answer a position query by setting the requested values.
+ * Answer a position query by setting the requested value in the given format.
*/
void
-gst_query_set_position (GstQuery * query, GstFormat format,
- gint64 cur, gint64 end)
+gst_query_set_position (GstQuery * query, GstFormat format, gint64 cur)
{
- GstStructure *structure;
-
g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_POSITION);
- structure = gst_query_get_structure (query);
- gst_structure_set (structure,
- "format", GST_TYPE_FORMAT, format,
- "cur", G_TYPE_INT64, cur, "end", G_TYPE_INT64, end, NULL);
+ gst_structure_id_set (query->structure,
+ GST_QUARK (FORMAT), GST_TYPE_FORMAT, format,
+ GST_QUARK (CURRENT), G_TYPE_INT64, cur, NULL);
}
/**
* gst_query_parse_position:
- * @query: the query to parse
- * @format: the storage for the #GstFormat of the position values
- * @cur: the storage for the current position
- * @end: the storage for the end position
+ * @query: a #GstQuery
+ * @format: (out) (allow-none): the storage for the #GstFormat of the
+ * position values (may be NULL)
+ * @cur: (out) (allow-none): the storage for the current position (may be NULL)
*
- * Parse a position query answer.
+ * Parse a position query, writing the format into @format, and the position
+ * into @cur, if the respective parameters are non-NULL.
*/
void
-gst_query_parse_position (GstQuery * query, GstFormat * format,
- gint64 * cur, gint64 * end)
+gst_query_parse_position (GstQuery * query, GstFormat * format, gint64 * cur)
{
GstStructure *structure;
g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_POSITION);
- structure = gst_query_get_structure (query);
+ structure = query->structure;
if (format)
- *format = g_value_get_enum (gst_structure_get_value (structure, "format"));
+ *format =
+ (GstFormat) g_value_get_enum (gst_structure_id_get_value (structure,
+ GST_QUARK (FORMAT)));
if (cur)
- *cur = g_value_get_int64 (gst_structure_get_value (structure, "cur"));
- if (end)
- *end = g_value_get_int64 (gst_structure_get_value (structure, "end"));
+ *cur = g_value_get_int64 (gst_structure_id_get_value (structure,
+ GST_QUARK (CURRENT)));
+}
+
+
+/**
+ * gst_query_new_duration:
+ * @format: the #GstFormat for this duration query
+ *
+ * Constructs a new stream duration query object to query in the given format.
+ * Use gst_query_unref() when done with it. A duration query will give the
+ * total length of the stream.
+ *
+ * Free-function: gst_query_unref
+ *
+ * Returns: (transfer full): a new #GstQuery
+ */
+GstQuery *
+gst_query_new_duration (GstFormat format)
+{
+ GstQuery *query;
+ GstStructure *structure;
+
+ structure = gst_structure_id_new (GST_QUARK (QUERY_DURATION),
+ GST_QUARK (FORMAT), GST_TYPE_FORMAT, format,
+ GST_QUARK (DURATION), G_TYPE_INT64, G_GINT64_CONSTANT (-1), NULL);
+
+ query = gst_query_new (GST_QUERY_DURATION, structure);
+
+ return query;
+}
+
+/**
+ * gst_query_set_duration:
+ * @query: a #GstQuery
+ * @format: the #GstFormat for the duration
+ * @duration: the duration of the stream
+ *
+ * Answer a duration query by setting the requested value in the given format.
+ */
+void
+gst_query_set_duration (GstQuery * query, GstFormat format, gint64 duration)
+{
+ g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_DURATION);
+
+ gst_structure_id_set (query->structure,
+ GST_QUARK (FORMAT), GST_TYPE_FORMAT, format,
+ GST_QUARK (DURATION), G_TYPE_INT64, duration, NULL);
+}
+
+/**
+ * gst_query_parse_duration:
+ * @query: a #GstQuery
+ * @format: (out) (allow-none): the storage for the #GstFormat of the duration
+ * value, or NULL.
+ * @duration: (out) (allow-none): the storage for the total duration, or NULL.
+ *
+ * Parse a duration query answer. Write the format of the duration into @format,
+ * and the value into @duration, if the respective variables are non-NULL.
+ */
+void
+gst_query_parse_duration (GstQuery * query, GstFormat * format,
+ gint64 * duration)
+{
+ GstStructure *structure;
+
+ g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_DURATION);
+
+ structure = query->structure;
+ if (format)
+ *format =
+ (GstFormat) g_value_get_enum (gst_structure_id_get_value (structure,
+ GST_QUARK (FORMAT)));
+ if (duration)
+ *duration = g_value_get_int64 (gst_structure_id_get_value (structure,
+ GST_QUARK (DURATION)));
+}
+
+/**
+ * gst_query_new_latency:
+ *
+ * Constructs a new latency query object.
+ * Use gst_query_unref() when done with it. A latency query is usually performed
+ * by sinks to compensate for additional latency introduced by elements in the
+ * pipeline.
+ *
+ * Free-function: gst_query_unref
+ *
+ * Returns: (transfer full): a #GstQuery
+ *
+ * Since: 0.10.12
+ */
+GstQuery *
+gst_query_new_latency (void)
+{
+ GstQuery *query;
+ GstStructure *structure;
+
+ structure = gst_structure_id_new (GST_QUARK (QUERY_LATENCY),
+ GST_QUARK (LIVE), G_TYPE_BOOLEAN, FALSE,
+ GST_QUARK (MIN_LATENCY), G_TYPE_UINT64, G_GUINT64_CONSTANT (0),
+ GST_QUARK (MAX_LATENCY), G_TYPE_UINT64, G_GUINT64_CONSTANT (-1), NULL);
+
+ query = gst_query_new (GST_QUERY_LATENCY, structure);
+
+ return query;
+}
+
+/**
+ * gst_query_set_latency:
+ * @query: a #GstQuery
+ * @live: if there is a live element upstream
+ * @min_latency: the minimal latency of the live element
+ * @max_latency: the maximal latency of the live element
+ *
+ * Answer a latency query by setting the requested values in the given format.
+ *
+ * Since: 0.10.12
+ */
+void
+gst_query_set_latency (GstQuery * query, gboolean live,
+ GstClockTime min_latency, GstClockTime max_latency)
+{
+ g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_LATENCY);
+
+ gst_structure_id_set (query->structure,
+ GST_QUARK (LIVE), G_TYPE_BOOLEAN, live,
+ GST_QUARK (MIN_LATENCY), G_TYPE_UINT64, min_latency,
+ GST_QUARK (MAX_LATENCY), G_TYPE_UINT64, max_latency, NULL);
+}
+
+/**
+ * gst_query_parse_latency:
+ * @query: a #GstQuery
+ * @live: (out) (allow-none): storage for live or NULL
+ * @min_latency: (out) (allow-none): the storage for the min latency or NULL
+ * @max_latency: (out) (allow-none): the storage for the max latency or NULL
+ *
+ * Parse a latency query answer.
+ *
+ * Since: 0.10.12
+ */
+void
+gst_query_parse_latency (GstQuery * query, gboolean * live,
+ GstClockTime * min_latency, GstClockTime * max_latency)
+{
+ GstStructure *structure;
+
+ g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_LATENCY);
+
+ structure = query->structure;
+ if (live)
+ *live =
+ g_value_get_boolean (gst_structure_id_get_value (structure,
+ GST_QUARK (LIVE)));
+ if (min_latency)
+ *min_latency = g_value_get_uint64 (gst_structure_id_get_value (structure,
+ GST_QUARK (MIN_LATENCY)));
+ if (max_latency)
+ *max_latency = g_value_get_uint64 (gst_structure_id_get_value (structure,
+ GST_QUARK (MAX_LATENCY)));
}
/**
* gst_query_new_convert:
- * @src_fmt: the source #GstFormat for the new query
+ * @src_format: the source #GstFormat for the new query
* @value: the value to convert
- * @dest_fmt: the target #GstFormat
+ * @dest_format: the target #GstFormat
*
- * Constructs a new query convert object. Use gst_query_unref()
- * when done with it.
+ * Constructs a new convert query object. Use gst_query_unref()
+ * when done with it. A convert query is used to ask for a conversion between
+ * one format and another.
*
- * Returns: A new #GstQuery
+ * Free-function: gst_query_unref
+ *
+ * Returns: (transfer full): a #GstQuery
*/
GstQuery *
-gst_query_new_convert (GstFormat src_fmt, gint64 value, GstFormat dest_fmt)
+gst_query_new_convert (GstFormat src_format, gint64 value,
+ GstFormat dest_format)
{
GstQuery *query;
GstStructure *structure;
- g_return_val_if_fail (value >= 0, NULL);
+ structure = gst_structure_id_new (GST_QUARK (QUERY_CONVERT),
+ GST_QUARK (SRC_FORMAT), GST_TYPE_FORMAT, src_format,
+ GST_QUARK (SRC_VALUE), G_TYPE_INT64, value,
+ GST_QUARK (DEST_FORMAT), GST_TYPE_FORMAT, dest_format,
+ GST_QUARK (DEST_VALUE), G_TYPE_INT64, G_GINT64_CONSTANT (-1), NULL);
- structure = gst_structure_new ("GstQueryConvert",
- "src_format", GST_TYPE_FORMAT, src_fmt,
- "src_value", G_TYPE_INT64, value,
- "dest_format", GST_TYPE_FORMAT, dest_fmt,
- "dest_value", G_TYPE_INT64, (gint64) - 1, NULL);
query = gst_query_new (GST_QUERY_CONVERT, structure);
return query;
/**
* gst_query_set_convert:
- * @query: the query to fill in
+ * @query: a #GstQuery
* @src_format: the source #GstFormat
* @src_value: the source value
* @dest_format: the destination #GstFormat
gst_query_set_convert (GstQuery * query, GstFormat src_format, gint64 src_value,
GstFormat dest_format, gint64 dest_value)
{
- GstStructure *structure;
-
g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_CONVERT);
- structure = gst_query_get_structure (query);
- gst_structure_set (structure,
- "src_format", GST_TYPE_FORMAT, src_format,
- "src_value", G_TYPE_INT64, src_value,
- "dest_format", GST_TYPE_FORMAT, dest_format,
- "dest_value", G_TYPE_INT64, dest_value, NULL);
+ gst_structure_id_set (query->structure,
+ GST_QUARK (SRC_FORMAT), GST_TYPE_FORMAT, src_format,
+ GST_QUARK (SRC_VALUE), G_TYPE_INT64, src_value,
+ GST_QUARK (DEST_FORMAT), GST_TYPE_FORMAT, dest_format,
+ GST_QUARK (DEST_VALUE), G_TYPE_INT64, dest_value, NULL);
}
/**
* gst_query_parse_convert:
- * @query: the query to parse
- * @src_format: the storage for the #GstFormat of the source value
- * @src_value: the storage for the source value
- * @dest_format: the storage for the #GstFormat of the destination value
- * @dest_value: the storage for the destination value
+ * @query: a #GstQuery
+ * @src_format: (out) (allow-none): the storage for the #GstFormat of the
+ * source value, or NULL
+ * @src_value: (out) (allow-none): the storage for the source value, or NULL
+ * @dest_format: (out) (allow-none): the storage for the #GstFormat of the
+ * destination value, or NULL
+ * @dest_value: (out) (allow-none): the storage for the destination value,
+ * or NULL
*
- * Parse a convert query answer.
+ * Parse a convert query answer. Any of @src_format, @src_value, @dest_format,
+ * and @dest_value may be NULL, in which case that value is omitted.
*/
void
gst_query_parse_convert (GstQuery * query, GstFormat * src_format,
g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_CONVERT);
- structure = gst_query_get_structure (query);
+ structure = query->structure;
if (src_format)
*src_format =
- g_value_get_enum (gst_structure_get_value (structure, "src_format"));
+ (GstFormat) g_value_get_enum (gst_structure_id_get_value (structure,
+ GST_QUARK (SRC_FORMAT)));
if (src_value)
- *src_value =
- g_value_get_int64 (gst_structure_get_value (structure, "src_value"));
+ *src_value = g_value_get_int64 (gst_structure_id_get_value (structure,
+ GST_QUARK (SRC_VALUE)));
if (dest_format)
*dest_format =
- g_value_get_enum (gst_structure_get_value (structure, "dest_format"));
+ (GstFormat) g_value_get_enum (gst_structure_id_get_value (structure,
+ GST_QUARK (DEST_FORMAT)));
if (dest_value)
- *dest_value =
- g_value_get_int64 (gst_structure_get_value (structure, "dest_value"));
+ *dest_value = g_value_get_int64 (gst_structure_id_get_value (structure,
+ GST_QUARK (DEST_VALUE)));
}
/**
* gst_query_new_segment:
* @format: the #GstFormat for the new query
*
- * Constructs a new query segment object. Use gst_query_unref()
- * when done with it.
+ * Constructs a new segment query object. Use gst_query_unref()
+ * when done with it. A segment query is used to discover information about the
+ * currently configured segment for playback.
+ *
+ * Free-function: gst_query_unref
*
- * Returns: A new #GstQuery
+ * Returns: (transfer full): a new #GstQuery
*/
GstQuery *
gst_query_new_segment (GstFormat format)
GstQuery *query;
GstStructure *structure;
- structure = gst_structure_new ("GstQuerySegment",
- "format", GST_TYPE_FORMAT, format, NULL);
+ structure = gst_structure_id_new (GST_QUARK (QUERY_SEGMENT),
+ GST_QUARK (RATE), G_TYPE_DOUBLE, (gdouble) 0.0,
+ GST_QUARK (FORMAT), GST_TYPE_FORMAT, format,
+ GST_QUARK (START_VALUE), G_TYPE_INT64, G_GINT64_CONSTANT (-1),
+ GST_QUARK (STOP_VALUE), G_TYPE_INT64, G_GINT64_CONSTANT (-1), NULL);
+
query = gst_query_new (GST_QUERY_SEGMENT, structure);
return query;
/**
* gst_query_set_segment:
- * @query: the query to fill in
+ * @query: a #GstQuery
* @rate: the rate of the segment
- * @format: the #GstFormat of the segment values
+ * @format: the #GstFormat of the segment values (@start_value and @stop_value)
* @start_value: the start value
* @stop_value: the stop value
- * @base: the base value
*
- * Answer a segment query by setting the requested values.
+ * Answer a segment query by setting the requested values. The normal
+ * playback segment of a pipeline is 0 to duration at the default rate of
+ * 1.0. If a seek was performed on the pipeline to play a different
+ * segment, this query will return the range specified in the last seek.
+ *
+ * @start_value and @stop_value will respectively contain the configured
+ * playback range start and stop values expressed in @format.
+ * The values are always between 0 and the duration of the media and
+ * @start_value <= @stop_value. @rate will contain the playback rate. For
+ * negative rates, playback will actually happen from @stop_value to
+ * @start_value.
*/
void
gst_query_set_segment (GstQuery * query, gdouble rate, GstFormat format,
- gint64 start_value, gint64 stop_value, gint64 base)
+ gint64 start_value, gint64 stop_value)
{
- GstStructure *structure;
-
g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_SEGMENT);
- structure = gst_query_get_structure (query);
- gst_structure_set (structure,
- "rate", G_TYPE_DOUBLE, rate,
- "format", GST_TYPE_FORMAT, format,
- "start_value", G_TYPE_INT64, start_value,
- "stop_value", G_TYPE_INT64, stop_value, "base", G_TYPE_INT64, base, NULL);
+ gst_structure_id_set (query->structure,
+ GST_QUARK (RATE), G_TYPE_DOUBLE, rate,
+ GST_QUARK (FORMAT), GST_TYPE_FORMAT, format,
+ GST_QUARK (START_VALUE), G_TYPE_INT64, start_value,
+ GST_QUARK (STOP_VALUE), G_TYPE_INT64, stop_value, NULL);
}
/**
* gst_query_parse_segment:
- * @query: the query to parse
- * @rate: the storage for the rate of the segment
- * @format: the storage for the #GstFormat of the values
- * @start_value: the storage for the start value
- * @stop_value: the storage for the stop value
- * @base: the storage for the base value
+ * @query: a #GstQuery
+ * @rate: (out) (allow-none): the storage for the rate of the segment, or NULL
+ * @format: (out) (allow-none): the storage for the #GstFormat of the values,
+ * or NULL
+ * @start_value: (out) (allow-none): the storage for the start value, or NULL
+ * @stop_value: (out) (allow-none): the storage for the stop value, or NULL
*
- * Parse a segment query answer.
+ * Parse a segment query answer. Any of @rate, @format, @start_value, and
+ * @stop_value may be NULL, which will cause this value to be omitted.
+ *
+ * See gst_query_set_segment() for an explanation of the function arguments.
*/
void
gst_query_parse_segment (GstQuery * query, gdouble * rate, GstFormat * format,
- gint64 * start_value, gint64 * stop_value, gint64 * base)
+ gint64 * start_value, gint64 * stop_value)
{
GstStructure *structure;
g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_SEGMENT);
- structure = gst_query_get_structure (query);
+ structure = query->structure;
if (rate)
- *rate = g_value_get_double (gst_structure_get_value (structure, "rate"));
+ *rate = g_value_get_double (gst_structure_id_get_value (structure,
+ GST_QUARK (RATE)));
if (format)
- *format = g_value_get_enum (gst_structure_get_value (structure, "format"));
+ *format =
+ (GstFormat) g_value_get_enum (gst_structure_id_get_value (structure,
+ GST_QUARK (FORMAT)));
if (start_value)
- *start_value =
- g_value_get_int64 (gst_structure_get_value (structure, "start_value"));
+ *start_value = g_value_get_int64 (gst_structure_id_get_value (structure,
+ GST_QUARK (START_VALUE)));
if (stop_value)
- *stop_value =
- g_value_get_int64 (gst_structure_get_value (structure, "stop_value"));
- if (base)
- *base = g_value_get_int64 (gst_structure_get_value (structure, "base"));
+ *stop_value = g_value_get_int64 (gst_structure_id_get_value (structure,
+ GST_QUARK (STOP_VALUE)));
}
/**
* Constructs a new custom application query object. Use gst_query_unref()
* when done with it.
*
- * Returns: A new #GstQuery
+ * Free-function: gst_query_unref
+ *
+ * Returns: (transfer full): a new #GstQuery
*/
GstQuery *
gst_query_new_application (GstQueryType type, GstStructure * structure)
/**
* gst_query_get_structure:
- * @query: the query to parse
+ * @query: a #GstQuery
*
* Get the structure of a query.
*
- * Returns: The #GstStructure of the query. The structure is still owned
- * by the query and will therefore be freed when the query is unreffed.
+ * Returns: (transfer none): the #GstStructure of the query. The structure is
+ * still owned by the query and will therefore be freed when the query
+ * is unreffed.
*/
GstStructure *
gst_query_get_structure (GstQuery * query)
return query->structure;
}
+
+/**
+ * gst_query_new_seeking:
+ * @format: the default #GstFormat for the new query
+ *
+ * Constructs a new query object for querying seeking properties of
+ * the stream.
+ *
+ * Free-function: gst_query_unref
+ *
+ * Returns: (transfer full): a new #GstQuery
+ */
+GstQuery *
+gst_query_new_seeking (GstFormat format)
+{
+ GstQuery *query;
+ GstStructure *structure;
+
+ structure = gst_structure_id_new (GST_QUARK (QUERY_SEEKING),
+ GST_QUARK (FORMAT), GST_TYPE_FORMAT, format,
+ GST_QUARK (SEEKABLE), G_TYPE_BOOLEAN, FALSE,
+ GST_QUARK (SEGMENT_START), G_TYPE_INT64, G_GINT64_CONSTANT (-1),
+ GST_QUARK (SEGMENT_END), G_TYPE_INT64, G_GINT64_CONSTANT (-1), NULL);
+
+ query = gst_query_new (GST_QUERY_SEEKING, structure);
+
+ return query;
+}
+
+/**
+ * gst_query_set_seeking:
+ * @query: a #GstQuery
+ * @format: the format to set for the @segment_start and @segment_end values
+ * @seekable: the seekable flag to set
+ * @segment_start: the segment_start to set
+ * @segment_end: the segment_end to set
+ *
+ * Set the seeking query result fields in @query.
+ */
+void
+gst_query_set_seeking (GstQuery * query, GstFormat format,
+ gboolean seekable, gint64 segment_start, gint64 segment_end)
+{
+ g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_SEEKING);
+
+ gst_structure_id_set (query->structure,
+ GST_QUARK (FORMAT), GST_TYPE_FORMAT, format,
+ GST_QUARK (SEEKABLE), G_TYPE_BOOLEAN, seekable,
+ GST_QUARK (SEGMENT_START), G_TYPE_INT64, segment_start,
+ GST_QUARK (SEGMENT_END), G_TYPE_INT64, segment_end, NULL);
+}
+
+/**
+ * gst_query_parse_seeking:
+ * @query: a GST_QUERY_SEEKING type query #GstQuery
+ * @format: (out) (allow-none): the format to set for the @segment_start
+ * and @segment_end values, or NULL
+ * @seekable: (out) (allow-none): the seekable flag to set, or NULL
+ * @segment_start: (out) (allow-none): the segment_start to set, or NULL
+ * @segment_end: (out) (allow-none): the segment_end to set, or NULL
+ *
+ * Parse a seeking query, writing the format into @format, and
+ * other results into the passed parameters, if the respective parameters
+ * are non-NULL
+ */
+void
+gst_query_parse_seeking (GstQuery * query, GstFormat * format,
+ gboolean * seekable, gint64 * segment_start, gint64 * segment_end)
+{
+ GstStructure *structure;
+
+ g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_SEEKING);
+
+ structure = query->structure;
+ if (format)
+ *format =
+ (GstFormat) g_value_get_enum (gst_structure_id_get_value (structure,
+ GST_QUARK (FORMAT)));
+ if (seekable)
+ *seekable = g_value_get_boolean (gst_structure_id_get_value (structure,
+ GST_QUARK (SEEKABLE)));
+ if (segment_start)
+ *segment_start = g_value_get_int64 (gst_structure_id_get_value (structure,
+ GST_QUARK (SEGMENT_START)));
+ if (segment_end)
+ *segment_end = g_value_get_int64 (gst_structure_id_get_value (structure,
+ GST_QUARK (SEGMENT_END)));
+}
+
+/**
+ * gst_query_new_formats:
+ *
+ * Constructs a new query object for querying formats of
+ * the stream.
+ *
+ * Free-function: gst_query_unref
+ *
+ * Returns: (transfer full): a new #GstQuery
+ *
+ * Since: 0.10.4
+ */
+GstQuery *
+gst_query_new_formats (void)
+{
+ GstQuery *query;
+ GstStructure *structure;
+
+ structure = gst_structure_id_empty_new (GST_QUARK (QUERY_FORMATS));
+ query = gst_query_new (GST_QUERY_FORMATS, structure);
+
+ return query;
+}
+
+static void
+gst_query_list_add_format (GValue * list, GstFormat format)
+{
+ GValue item = { 0, };
+
+ g_value_init (&item, GST_TYPE_FORMAT);
+ g_value_set_enum (&item, format);
+ gst_value_list_append_value (list, &item);
+ g_value_unset (&item);
+}
+
+/**
+ * gst_query_set_formats:
+ * @query: a #GstQuery
+ * @n_formats: the number of formats to set.
+ * @...: A number of @GstFormats equal to @n_formats.
+ *
+ * Set the formats query result fields in @query. The number of formats passed
+ * must be equal to @n_formats.
+ */
+void
+gst_query_set_formats (GstQuery * query, gint n_formats, ...)
+{
+ va_list ap;
+ GValue list = { 0, };
+ gint i;
+
+ g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_FORMATS);
+
+ g_value_init (&list, GST_TYPE_LIST);
+
+ va_start (ap, n_formats);
+ for (i = 0; i < n_formats; i++) {
+ gst_query_list_add_format (&list, va_arg (ap, GstFormat));
+ }
+ va_end (ap);
+
+ gst_structure_set_value (query->structure, "formats", &list);
+
+ g_value_unset (&list);
+
+}
+
+/**
+ * gst_query_set_formatsv:
+ * @query: a #GstQuery
+ * @n_formats: the number of formats to set.
+ * @formats: (in) (array length=n_formats): an array containing @n_formats
+ * @GstFormat values.
+ *
+ * Set the formats query result fields in @query. The number of formats passed
+ * in the @formats array must be equal to @n_formats.
+ *
+ * Since: 0.10.4
+ */
+void
+gst_query_set_formatsv (GstQuery * query, gint n_formats,
+ const GstFormat * formats)
+{
+ GValue list = { 0, };
+ gint i;
+
+ g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_FORMATS);
+
+ g_value_init (&list, GST_TYPE_LIST);
+ for (i = 0; i < n_formats; i++) {
+ gst_query_list_add_format (&list, formats[i]);
+ }
+ gst_structure_set_value (query->structure, "formats", &list);
+
+ g_value_unset (&list);
+}
+
+/**
+ * gst_query_parse_formats_length:
+ * @query: a #GstQuery
+ * @n_formats: (out): the number of formats in this query.
+ *
+ * Parse the number of formats in the formats @query.
+ *
+ * Since: 0.10.4
+ */
+void
+gst_query_parse_formats_length (GstQuery * query, guint * n_formats)
+{
+ g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_FORMATS);
+
+ if (n_formats) {
+ const GValue *list;
+
+ list = gst_structure_get_value (query->structure, "formats");
+ if (list == NULL)
+ *n_formats = 0;
+ else
+ *n_formats = gst_value_list_get_size (list);
+ }
+}
+
+/**
+ * gst_query_parse_formats_nth:
+ * @query: a #GstQuery
+ * @nth: (out): the nth format to retrieve.
+ * @format: (out): a pointer to store the nth format
+ *
+ * Parse the format query and retrieve the @nth format from it into
+ * @format. If the list contains less elements than @nth, @format will be
+ * set to GST_FORMAT_UNDEFINED.
+ *
+ * Since: 0.10.4
+ */
+void
+gst_query_parse_formats_nth (GstQuery * query, guint nth, GstFormat * format)
+{
+ g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_FORMATS);
+
+ if (format) {
+ const GValue *list;
+
+ list = gst_structure_get_value (query->structure, "formats");
+ if (list == NULL) {
+ *format = GST_FORMAT_UNDEFINED;
+ } else {
+ if (nth < gst_value_list_get_size (list)) {
+ *format =
+ (GstFormat) g_value_get_enum (gst_value_list_get_value (list, nth));
+ } else
+ *format = GST_FORMAT_UNDEFINED;
+ }
+ }
+}
+
+/**
+ * gst_query_new_buffering
+ * @format: the default #GstFormat for the new query
+ *
+ * Constructs a new query object for querying the buffering status of
+ * a stream.
+ *
+ * Free-function: gst_query_new
+ *
+ * Returns: (transfer full): a new #GstQuery
+ *
+ * Since: 0.10.20
+ */
+GstQuery *
+gst_query_new_buffering (GstFormat format)
+{
+ GstQuery *query;
+ GstStructure *structure;
+
+ /* by default, we configure the answer as no buffering with a 100% buffering
+ * progress */
+ structure = gst_structure_id_new (GST_QUARK (QUERY_BUFFERING),
+ GST_QUARK (BUSY), G_TYPE_BOOLEAN, FALSE,
+ GST_QUARK (BUFFER_PERCENT), G_TYPE_INT, 100,
+ GST_QUARK (BUFFERING_MODE), GST_TYPE_BUFFERING_MODE, GST_BUFFERING_STREAM,
+ GST_QUARK (AVG_IN_RATE), G_TYPE_INT, -1,
+ GST_QUARK (AVG_OUT_RATE), G_TYPE_INT, -1,
+ GST_QUARK (BUFFERING_LEFT), G_TYPE_INT64, G_GINT64_CONSTANT (0),
+ GST_QUARK (ESTIMATED_TOTAL), G_TYPE_INT64, G_GINT64_CONSTANT (-1),
+ GST_QUARK (FORMAT), GST_TYPE_FORMAT, format,
+ GST_QUARK (START_VALUE), G_TYPE_INT64, G_GINT64_CONSTANT (-1),
+ GST_QUARK (STOP_VALUE), G_TYPE_INT64, G_GINT64_CONSTANT (-1), NULL);
+
+ query = gst_query_new (GST_QUERY_BUFFERING, structure);
+
+ return query;
+}
+
+/**
+ * gst_query_set_buffering_percent
+ * @query: A valid #GstQuery of type GST_QUERY_BUFFERING.
+ * @busy: if buffering is busy
+ * @percent: a buffering percent
+ *
+ * Set the percentage of buffered data. This is a value between 0 and 100.
+ * The @busy indicator is %TRUE when the buffering is in progress.
+ *
+ * Since: 0.10.20
+ */
+void
+gst_query_set_buffering_percent (GstQuery * query, gboolean busy, gint percent)
+{
+ g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_BUFFERING);
+ g_return_if_fail (percent >= 0 && percent <= 100);
+
+ gst_structure_id_set (query->structure,
+ GST_QUARK (BUSY), G_TYPE_BOOLEAN, busy,
+ GST_QUARK (BUFFER_PERCENT), G_TYPE_INT, percent, NULL);
+}
+
+/**
+ * gst_query_parse_buffering_percent
+ * @query: A valid #GstQuery of type GST_QUERY_BUFFERING.
+ * @busy: (out) (allow-none): if buffering is busy, or NULL
+ * @percent: (out) (allow-none): a buffering percent, or NULL
+ *
+ * Get the percentage of buffered data. This is a value between 0 and 100.
+ * The @busy indicator is %TRUE when the buffering is in progress.
+ *
+ * Since: 0.10.20
+ */
+void
+gst_query_parse_buffering_percent (GstQuery * query, gboolean * busy,
+ gint * percent)
+{
+ g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_BUFFERING);
+
+ if (busy)
+ *busy = g_value_get_boolean (gst_structure_id_get_value (query->structure,
+ GST_QUARK (BUSY)));
+ if (percent)
+ *percent = g_value_get_int (gst_structure_id_get_value (query->structure,
+ GST_QUARK (BUFFER_PERCENT)));
+}
+
+/**
+ * gst_query_set_buffering_stats:
+ * @query: A valid #GstQuery of type GST_QUERY_BUFFERING.
+ * @mode: a buffering mode
+ * @avg_in: the average input rate
+ * @avg_out: the average output rate
+ * @buffering_left: amount of buffering time left
+ *
+ * Configures the buffering stats values in @query.
+ *
+ * Since: 0.10.20
+ */
+void
+gst_query_set_buffering_stats (GstQuery * query, GstBufferingMode mode,
+ gint avg_in, gint avg_out, gint64 buffering_left)
+{
+ g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_BUFFERING);
+
+ gst_structure_id_set (query->structure,
+ GST_QUARK (BUFFERING_MODE), GST_TYPE_BUFFERING_MODE, mode,
+ GST_QUARK (AVG_IN_RATE), G_TYPE_INT, avg_in,
+ GST_QUARK (AVG_OUT_RATE), G_TYPE_INT, avg_out,
+ GST_QUARK (BUFFERING_LEFT), G_TYPE_INT64, buffering_left, NULL);
+}
+
+/**
+ * gst_query_parse_buffering_stats:
+ * @query: A valid #GstQuery of type GST_QUERY_BUFFERING.
+ * @mode: (out) (allow-none): a buffering mode, or NULL
+ * @avg_in: (out) (allow-none): the average input rate, or NULL
+ * @avg_out: (out) (allow-none): the average output rat, or NULLe
+ * @buffering_left: (out) (allow-none): amount of buffering time left, or NULL
+ *
+ * Extracts the buffering stats values from @query.
+ *
+ * Since: 0.10.20
+ */
+void
+gst_query_parse_buffering_stats (GstQuery * query,
+ GstBufferingMode * mode, gint * avg_in, gint * avg_out,
+ gint64 * buffering_left)
+{
+ g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_BUFFERING);
+
+ if (mode)
+ *mode = (GstBufferingMode)
+ g_value_get_enum (gst_structure_id_get_value (query->structure,
+ GST_QUARK (BUFFERING_MODE)));
+ if (avg_in)
+ *avg_in = g_value_get_int (gst_structure_id_get_value (query->structure,
+ GST_QUARK (AVG_IN_RATE)));
+ if (avg_out)
+ *avg_out = g_value_get_int (gst_structure_id_get_value (query->structure,
+ GST_QUARK (AVG_OUT_RATE)));
+ if (buffering_left)
+ *buffering_left =
+ g_value_get_int64 (gst_structure_id_get_value (query->structure,
+ GST_QUARK (BUFFERING_LEFT)));
+}
+
+
+/**
+ * gst_query_set_buffering_range:
+ * @query: a #GstQuery
+ * @format: the format to set for the @start and @stop values
+ * @start: the start to set
+ * @stop: the stop to set
+ * @estimated_total: estimated total amount of download time
+ *
+ * Set the available query result fields in @query.
+ *
+ * Since: 0.10.20
+ */
+void
+gst_query_set_buffering_range (GstQuery * query, GstFormat format,
+ gint64 start, gint64 stop, gint64 estimated_total)
+{
+ g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_BUFFERING);
+
+ gst_structure_id_set (query->structure,
+ GST_QUARK (FORMAT), GST_TYPE_FORMAT, format,
+ GST_QUARK (START_VALUE), G_TYPE_INT64, start,
+ GST_QUARK (STOP_VALUE), G_TYPE_INT64, stop,
+ GST_QUARK (ESTIMATED_TOTAL), G_TYPE_INT64, estimated_total, NULL);
+}
+
+/**
+ * gst_query_parse_buffering_range:
+ * @query: a GST_QUERY_BUFFERING type query #GstQuery
+ * @format: (out) (allow-none): the format to set for the @segment_start
+ * and @segment_end values, or NULL
+ * @start: (out) (allow-none): the start to set, or NULL
+ * @stop: (out) (allow-none): the stop to set, or NULL
+ * @estimated_total: (out) (allow-none): estimated total amount of download
+ * time, or NULL
+ *
+ * Parse an available query, writing the format into @format, and
+ * other results into the passed parameters, if the respective parameters
+ * are non-NULL
+ *
+ * Since: 0.10.20
+ */
+void
+gst_query_parse_buffering_range (GstQuery * query, GstFormat * format,
+ gint64 * start, gint64 * stop, gint64 * estimated_total)
+{
+ GstStructure *structure;
+
+ g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_BUFFERING);
+
+ structure = query->structure;
+ if (format)
+ *format =
+ (GstFormat) g_value_get_enum (gst_structure_id_get_value (structure,
+ GST_QUARK (FORMAT)));
+ if (start)
+ *start = g_value_get_int64 (gst_structure_id_get_value (structure,
+ GST_QUARK (START_VALUE)));
+ if (stop)
+ *stop = g_value_get_int64 (gst_structure_id_get_value (structure,
+ GST_QUARK (STOP_VALUE)));
+ if (estimated_total)
+ *estimated_total =
+ g_value_get_int64 (gst_structure_id_get_value (structure,
+ GST_QUARK (ESTIMATED_TOTAL)));
+}
+
+/**
+ * gst_query_add_buffering_range
+ * @query: a GST_QUERY_BUFFERING type query #GstQuery
+ * @start: start position of the range
+ * @stop: stop position of the range
+ *
+ * Set the buffering-ranges array field in @query. The current last
+ * start position of the array should be inferior to @start.
+ *
+ * Returns: a #gboolean indicating if the range was added or not.
+ *
+ * Since: 0.10.31
+ */
+gboolean
+gst_query_add_buffering_range (GstQuery * query, gint64 start, gint64 stop)
+{
+ GValueArray *array;
+ GValue *last_array_value;
+ const GValue *value;
+ GValue range_value = { 0 };
+
+ g_return_val_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_BUFFERING, FALSE);
+
+ if (G_UNLIKELY (start >= stop))
+ return FALSE;
+
+ value =
+ gst_structure_id_get_value (query->structure,
+ GST_QUARK (BUFFERING_RANGES));
+ if (value) {
+ array = (GValueArray *) g_value_get_boxed (value);
+ last_array_value = g_value_array_get_nth (array, array->n_values - 1);
+ if (G_UNLIKELY (start <= gst_value_get_int64_range_min (last_array_value)))
+ return FALSE;
+ } else {
+ GValue new_array_val = { 0, };
+
+ array = g_value_array_new (0);
+
+ g_value_init (&new_array_val, G_TYPE_VALUE_ARRAY);
+ g_value_take_boxed (&new_array_val, array);
+
+ /* set the value array only once, so we then modify (append to) the
+ * existing value array owned by the GstStructure / the field's GValue */
+ gst_structure_id_take_value (query->structure, GST_QUARK (BUFFERING_RANGES),
+ &new_array_val);
+ }
+
+ g_value_init (&range_value, GST_TYPE_INT64_RANGE);
+ gst_value_set_int64_range (&range_value, start, stop);
+ g_value_array_append (array, &range_value);
+ /* skip the g_value_unset(&range_value) here, we know it's not needed */
+
+ return TRUE;
+}
+
+/**
+ * gst_query_get_n_buffering_ranges
+ * @query: a GST_QUERY_BUFFERING type query #GstQuery
+ *
+ * Retrieve the number of values currently stored in the
+ * buffered-ranges array of the query's structure.
+ *
+ * Returns: the range array size as a #guint.
+ *
+ * Since: 0.10.31
+ */
+guint
+gst_query_get_n_buffering_ranges (GstQuery * query)
+{
+ GValueArray *array;
+ const GValue *value;
+ guint size = 0;
+
+ g_return_val_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_BUFFERING, 0);
+
+ value =
+ gst_structure_id_get_value (query->structure,
+ GST_QUARK (BUFFERING_RANGES));
+ if (value) {
+ array = (GValueArray *) g_value_get_boxed (value);
+ size = array->n_values;
+ }
+ return size;
+}
+
+
+/**
+ * gst_query_parse_nth_buffering_range
+ * @query: a GST_QUERY_BUFFERING type query #GstQuery
+ * @index: position in the buffered-ranges array to read
+ * @start: (out) (allow-none): the start position to set, or NULL
+ * @stop: (out) (allow-none): the stop position to set, or NULL
+ *
+ * Parse an available query and get the start and stop values stored
+ * at the @index of the buffered ranges array.
+ *
+ * Returns: a #gboolean indicating if the parsing succeeded.
+ *
+ * Since: 0.10.31
+ */
+gboolean
+gst_query_parse_nth_buffering_range (GstQuery * query, guint index,
+ gint64 * start, gint64 * stop)
+{
+ const GValue *value;
+ GValueArray *ranges;
+ GValue *range_value;
+ gboolean ret = FALSE;
+
+ g_return_val_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_BUFFERING, ret);
+
+ value =
+ gst_structure_id_get_value (query->structure,
+ GST_QUARK (BUFFERING_RANGES));
+ ranges = (GValueArray *) g_value_get_boxed (value);
+ range_value = g_value_array_get_nth (ranges, index);
+ if (range_value) {
+ if (start)
+ *start = gst_value_get_int64_range_min (range_value);
+ if (stop)
+ *stop = gst_value_get_int64_range_max (range_value);
+ ret = TRUE;
+ }
+
+ return ret;
+}
+
+
+/**
+ * gst_query_new_uri:
+ *
+ * Constructs a new query URI query object. Use gst_query_unref()
+ * when done with it. An URI query is used to query the current URI
+ * that is used by the source or sink.
+ *
+ * Free-function: gst_query_unref
+ *
+ * Returns: (transfer full): a new #GstQuery
+ *
+ * Since: 0.10.22
+ */
+GstQuery *
+gst_query_new_uri (void)
+{
+ GstQuery *query;
+ GstStructure *structure;
+
+ structure = gst_structure_id_new (GST_QUARK (QUERY_URI),
+ GST_QUARK (URI), G_TYPE_STRING, NULL, NULL);
+
+ query = gst_query_new (GST_QUERY_URI, structure);
+
+ return query;
+}
+
+/**
+ * gst_query_set_uri:
+ * @query: a #GstQuery with query type GST_QUERY_URI
+ * @uri: the URI to set
+ *
+ * Answer a URI query by setting the requested URI.
+ *
+ * Since: 0.10.22
+ */
+void
+gst_query_set_uri (GstQuery * query, const gchar * uri)
+{
+ g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_URI);
+ g_return_if_fail (gst_uri_is_valid (uri));
+
+ gst_structure_id_set (query->structure, GST_QUARK (URI), G_TYPE_STRING, uri,
+ NULL);
+}
+
+/**
+ * gst_query_parse_uri:
+ * @query: a #GstQuery
+ * @uri: (out callee-allocates) (allow-none): the storage for the current URI
+ * (may be NULL)
+ *
+ * Parse an URI query, writing the URI into @uri as a newly
+ * allocated string, if the respective parameters are non-NULL.
+ * Free the string with g_free() after usage.
+ *
+ * Since: 0.10.22
+ */
+void
+gst_query_parse_uri (GstQuery * query, gchar ** uri)
+{
+ g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_URI);
+
+ if (uri)
+ *uri = g_value_dup_string (gst_structure_id_get_value (query->structure,
+ GST_QUARK (URI)));
+}
+
+/**
+ * gst_query_new_buffers:
+ * @caps: the #GstCaps for the buffers that are going to be allocated
+ *
+ * Constructs a new buffer requirements query object to query buffer
+ * requirements for a particular caps. Use gst_query_unref() when done
+ * with it.
+ *
+ * Returns: A #GstQuery
+ */
+GstQuery *
+gst_query_new_buffers (GstCaps * caps)
+{
+ GstQuery *query;
+ GstStructure *structure;
+
+ /* XXX could add size here, for linear (non YUV/RGB) buffers? But I'm not
+ * entirely sure what is the use-case for that.. it should be easy enough
+ * to add more optional reply fields later
+ */
+ structure = gst_structure_id_new (GST_QUARK (QUERY_BUFFERS),
+ GST_QUARK (CAPS), GST_TYPE_CAPS, caps,
+ GST_QUARK (COUNT), G_TYPE_INT, -1,
+ GST_QUARK (WIDTH), G_TYPE_INT, -1,
+ GST_QUARK (HEIGHT), G_TYPE_INT, -1, NULL);
+
+ query = gst_query_new (GST_QUERY_BUFFERS, structure);
+
+ return query;
+}
+
+/**
+ * gst_query_set_buffers_count:
+ * @count: minimum number of buffers required
+ *
+ * Answer a buffers query by setting the minimum number of buffers required.
+ * If there is no minimum buffer count requirement, don't set this field in
+ * the query.
+ */
+void
+gst_query_set_buffers_count (GstQuery * query, gint count)
+{
+ GstStructure *structure;
+
+ g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_BUFFERS);
+
+ structure = gst_query_get_structure (query);
+ gst_structure_id_set (structure, GST_QUARK (COUNT), G_TYPE_INT, count, NULL);
+}
+
+/**
+ * gst_query_set_buffers_dimensions:
+ * @width: minimum buffer width
+ * @height: minimum buffer height
+ *
+ * Answer a buffers query by setting the minimum buffer dimensions required.
+ * If there is no minimum buffer dimensions (beyond the width/height specified
+ * in the #GstCaps), don't set this field in the query.
+ */
+void
+gst_query_set_buffers_dimensions (GstQuery * query, gint width, gint height)
+{
+ GstStructure *structure;
+
+ g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_BUFFERS);
+
+ structure = gst_query_get_structure (query);
+ gst_structure_id_set (structure,
+ GST_QUARK (WIDTH), G_TYPE_INT, width,
+ GST_QUARK (HEIGHT), G_TYPE_INT, height, NULL);
+}
+
+/**
+ * gst_query_parse_buffers_caps:
+ * @query: a #GstQuery
+ * @caps: the storage for the #GstCaps pointer, or NULL
+ *
+ * Parse a buffers query.
+ */
+void
+gst_query_parse_buffers_caps (GstQuery * query, const GstCaps ** caps)
+{
+ GstStructure *structure;
+
+ g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_BUFFERS);
+
+ structure = gst_query_get_structure (query);
+ if (caps)
+ *caps = gst_value_get_caps (gst_structure_id_get_value (structure,
+ GST_QUARK (CAPS)));
+}
+
+/**
+ * gst_query_parse_buffers_count:
+ * @query: a #GstQuery
+ * @count: the storage for minimum number of buffers, or NULL
+ *
+ * Parse a buffers query answer to see the minimum number of buffers
+ * required. A returned value of -1 means there is no minimum requirement
+ */
+void
+gst_query_parse_buffers_count (GstQuery * query, gint * count)
+{
+ GstStructure *structure;
+
+ g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_BUFFERS);
+
+ structure = gst_query_get_structure (query);
+ if (count)
+ *count = g_value_get_int (gst_structure_id_get_value (structure,
+ GST_QUARK (COUNT)));
+}
+
+/**
+ * gst_query_parse_buffers_dimensions:
+ * @query: a #GstQuery
+ * @width: the storage for minimum width, or NULL
+ * @height: the storage for minimum height, or NULL
+ *
+ * Parse a buffers query answer to see the minimum buffer dimensions required.
+ * A returned value of -1 for either dimension means there is no minimum
+ * requirement in that axis
+ */
+void
+gst_query_parse_buffers_dimensions (GstQuery * query, gint * width,
+ gint * height)
+{
+ GstStructure *structure;
+
+ g_return_if_fail (GST_QUERY_TYPE (query) == GST_QUERY_BUFFERS);
+
+ structure = gst_query_get_structure (query);
+ if (width)
+ *width = g_value_get_int (gst_structure_id_get_value (structure,
+ GST_QUARK (WIDTH)));
+ if (height)
+ *height = g_value_get_int (gst_structure_id_get_value (structure,
+ GST_QUARK (HEIGHT)));
+}