]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/gstreamer0-10.git/blobdiff - gst/gststructure.c
gststructure: clarify _get docs about the returned reference
[glsdk/gstreamer0-10.git] / gst / gststructure.c
index 4cadad955675487dc1d5b5bf5637b36079227a23..23c54b35f533d823d52fdf3d9e55596b175fb933 100644 (file)
@@ -27,8 +27,9 @@
  * A #GstStructure is a collection of key/value pairs. The keys are expressed
  * as GQuarks and the values can be of any GType.
  *
- * In addition to the key/value pairs, a #GstStructure also has a name.
- * 
+ * In addition to the key/value pairs, a #GstStructure also has a name. The name
+ * starts with a letter and can be folled by letters, numbers and any of "/-_.:".
+ *
  * #GstStructure is used by various GStreamer subsystems to store information
  * in a flexible and extensible way. A #GstStructure does not have a refcount
  * because it usually is part of a higher level object such as #GstCaps. It
@@ -38,7 +39,7 @@
  * A #GstStructure can be created with gst_structure_empty_new() or
  * gst_structure_new(), which both take a name and an optional set of
  * key/value pairs along with the types of the values.
- * 
+ *
  * Field values can be changed with gst_structure_set_value() or
  * gst_structure_set().
  *
  * Fields can be removed with gst_structure_remove_field() or
  * gst_structure_remove_fields().
  *
- * Last reviewed on 2005-11-09 (0.9.4)
+ * Strings in structures must be ASCII or UTF-8 encoded. Other encodings are
+ * not allowed. Strings must not be empty either, but may be NULL.
+ *
+ * Last reviewed on 2009-06-08 (0.10.23)
  */
 
 #ifdef HAVE_CONFIG_H
@@ -58,6 +62,7 @@
 #include <string.h>
 
 #include "gst_private.h"
+#include "gstquark.h"
 #include <gst/gst.h>
 #include <gobject/gvaluecollector.h>
 
@@ -76,6 +81,9 @@ struct _GstStructureField
     (!(structure)->parent_refcount || \
      g_atomic_int_get ((structure)->parent_refcount) == 1)
 
+#define IS_TAGLIST(structure) \
+    (structure->name == GST_QUARK (TAGLIST))
+
 static void gst_structure_set_field (GstStructure * structure,
     GstStructureField * field);
 static GstStructureField *gst_structure_get_field (const GstStructure *
@@ -112,11 +120,12 @@ gst_structure_id_empty_new_with_size (GQuark quark, guint prealloc)
 {
   GstStructure *structure;
 
-  structure = g_new0 (GstStructure, 1);
+  structure = g_slice_new (GstStructure);
   structure->type = gst_structure_get_type ();
   structure->name = quark;
+  structure->parent_refcount = NULL;
   structure->fields =
-      g_array_sized_new (FALSE, TRUE, sizeof (GstStructureField), prealloc);
+      g_array_sized_new (FALSE, FALSE, sizeof (GstStructureField), prealloc);
 
   return structure;
 }
@@ -127,7 +136,9 @@ gst_structure_id_empty_new_with_size (GQuark quark, guint prealloc)
  *
  * Creates a new, empty #GstStructure with the given name as a GQuark.
  *
- * Returns: a new, empty #GstStructure
+ * Free-function: gst_structure_free
+ *
+ * Returns: (transfer full): a new, empty #GstStructure
  */
 GstStructure *
 gst_structure_id_empty_new (GQuark quark)
@@ -137,18 +148,52 @@ gst_structure_id_empty_new (GQuark quark)
   return gst_structure_id_empty_new_with_size (quark, 0);
 }
 
+#ifndef G_DISABLE_CHECKS
+static gboolean
+gst_structure_validate_name (const gchar * name)
+{
+  const gchar *s;
+
+  g_return_val_if_fail (name != NULL, FALSE);
+
+  /* FIXME 0.11: use g_ascii_isalpha() */
+  if (G_UNLIKELY (!g_ascii_isalnum (*name))) {
+    GST_WARNING ("Invalid character '%c' at offset 0 in structure name: %s",
+        *name, name);
+    return FALSE;
+  }
+
+  /* FIXME 0.11: don't allow spaces */
+  /* FIXME: test name string more */
+  s = &name[1];
+  while (*s && (g_ascii_isalnum (*s) || strchr ("/-_.:+ ", *s) != NULL))
+    s++;
+  if (G_UNLIKELY (*s != '\0')) {
+    GST_WARNING ("Invalid character '%c' at offset %" G_GUINTPTR_FORMAT " in"
+        " structure name: %s", *s, ((guintptr) s - (guintptr) name), name);
+    return FALSE;
+  }
+
+  return TRUE;
+}
+#endif
+
 /**
  * gst_structure_empty_new:
  * @name: name of new structure
  *
- * Creates a new, empty #GstStructure with the given name.
+ * Creates a new, empty #GstStructure with the given @name.
+ *
+ * See gst_structure_set_name() for constraints on the @name parameter.
  *
- * Returns: a new, empty #GstStructure
+ * Free-function: gst_structure_free
+ *
+ * Returns: (transfer full): a new, empty #GstStructure
  */
 GstStructure *
 gst_structure_empty_new (const gchar * name)
 {
-  g_return_val_if_fail (name != NULL, NULL);
+  g_return_val_if_fail (gst_structure_validate_name (name), NULL);
 
   return gst_structure_id_empty_new_with_size (g_quark_from_string (name), 0);
 }
@@ -164,7 +209,9 @@ gst_structure_empty_new (const gchar * name)
  * Variable arguments should be passed as field name, field type,
  * and value.  Last variable argument should be NULL.
  *
- * Returns: a new #GstStructure
+ * Free-function: gst_structure_free
+ *
+ * Returns: (transfer full): a new #GstStructure
  */
 GstStructure *
 gst_structure_new (const gchar * name, const gchar * firstfield, ...)
@@ -172,12 +219,8 @@ gst_structure_new (const gchar * name, const gchar * firstfield, ...)
   GstStructure *structure;
   va_list varargs;
 
-  g_return_val_if_fail (name != NULL, NULL);
-
   va_start (varargs, firstfield);
-
   structure = gst_structure_new_valist (name, firstfield, varargs);
-
   va_end (varargs);
 
   return structure;
@@ -189,11 +232,15 @@ gst_structure_new (const gchar * name, const gchar * firstfield, ...)
  * @firstfield: name of first field to set
  * @varargs: variable argument list
  *
- * Creates a new #GstStructure with the given name.  Structure fields
+ * Creates a new #GstStructure with the given @name.  Structure fields
  * are set according to the varargs in a manner similar to
- * @gst_structure_new.
+ * gst_structure_new().
+ *
+ * See gst_structure_set_name() for constraints on the @name parameter.
  *
- * Returns: a new #GstStructure
+ * Free-function: gst_structure_free
+ *
+ * Returns: (transfer full): a new #GstStructure
  */
 GstStructure *
 gst_structure_new_valist (const gchar * name,
@@ -201,10 +248,10 @@ gst_structure_new_valist (const gchar * name,
 {
   GstStructure *structure;
 
-  g_return_val_if_fail (name != NULL, NULL);
-
   structure = gst_structure_empty_new (name);
-  gst_structure_set_valist (structure, firstfield, varargs);
+
+  if (structure)
+    gst_structure_set_valist (structure, firstfield, varargs);
 
   return structure;
 }
@@ -212,7 +259,7 @@ gst_structure_new_valist (const gchar * name,
 /**
  * gst_structure_set_parent_refcount:
  * @structure: a #GstStructure
- * @refcount: a pointer to the parent's refcount
+ * @refcount: (in): a pointer to the parent's refcount
  *
  * Sets the parent_refcount field of #GstStructure. This field is used to
  * determine whether a structure is mutable or not. This function should only be
@@ -220,7 +267,7 @@ gst_structure_new_valist (const gchar * name,
  * the MT Refcounting section of the design documents.
  */
 void
-gst_structure_set_parent_refcount (GstStructure * structure, int *refcount)
+gst_structure_set_parent_refcount (GstStructure * structure, gint * refcount)
 {
   g_return_if_fail (structure != NULL);
 
@@ -240,22 +287,23 @@ gst_structure_set_parent_refcount (GstStructure * structure, int *refcount)
  *
  * Duplicates a #GstStructure and all its fields and values.
  *
- * Returns: a new #GstStructure.
+ * Free-function: gst_structure_free
+ *
+ * Returns: (transfer none): a new #GstStructure.
  */
 GstStructure *
 gst_structure_copy (const GstStructure * structure)
 {
   GstStructure *new_structure;
   GstStructureField *field;
-  guint i;
+  guint i, len;
 
   g_return_val_if_fail (structure != NULL, NULL);
 
-  new_structure =
-      gst_structure_id_empty_new_with_size (structure->name,
-      structure->fields->len);
+  len = structure->fields->len;
+  new_structure = gst_structure_id_empty_new_with_size (structure->name, len);
 
-  for (i = 0; i < structure->fields->len; i++) {
+  for (i = 0; i < len; i++) {
     GstStructureField new_field = { 0 };
 
     field = GST_STRUCTURE_FIELD (structure, i);
@@ -270,7 +318,7 @@ gst_structure_copy (const GstStructure * structure)
 
 /**
  * gst_structure_free:
- * @structure: the #GstStructure to free
+ * @structure: (in) (transfer full): the #GstStructure to free
  *
  * Frees a #GstStructure and all its fields and values. The structure must not
  * have a parent when this function is called.
@@ -279,12 +327,13 @@ void
 gst_structure_free (GstStructure * structure)
 {
   GstStructureField *field;
-  guint i;
+  guint i, len;
 
   g_return_if_fail (structure != NULL);
   g_return_if_fail (structure->parent_refcount == NULL);
 
-  for (i = 0; i < structure->fields->len; i++) {
+  len = structure->fields->len;
+  for (i = 0; i < len; i++) {
     field = GST_STRUCTURE_FIELD (structure, i);
 
     if (G_IS_VALUE (&field->value)) {
@@ -295,7 +344,7 @@ gst_structure_free (GstStructure * structure)
 #ifdef USE_POISONING
   memset (structure, 0xff, sizeof (GstStructure));
 #endif
-  g_free (structure);
+  g_slice_free (GstStructure, structure);
 }
 
 /**
@@ -331,6 +380,9 @@ gst_structure_has_name (const GstStructure * structure, const gchar * name)
   g_return_val_if_fail (structure != NULL, FALSE);
   g_return_val_if_fail (name != NULL, FALSE);
 
+  /* getting the string is cheap and comparing short strings is too
+   * should be faster than getting the quark for name and comparing the quarks
+   */
   structure_name = g_quark_to_string (structure->name);
 
   return (structure_name && strcmp (structure_name, name) == 0);
@@ -357,19 +409,32 @@ gst_structure_get_name_id (const GstStructure * structure)
  * @structure: a #GstStructure
  * @name: the new name of the structure
  *
- * Sets the name of the structure to the given name.  The string
- * provided is copied before being used.
+ * Sets the name of the structure to the given @name.  The string
+ * provided is copied before being used. It must not be empty, start with a
+ * letter and can be followed by letters, numbers and any of "/-_.:".
  */
 void
 gst_structure_set_name (GstStructure * structure, const gchar * name)
 {
   g_return_if_fail (structure != NULL);
-  g_return_if_fail (name != NULL);
   g_return_if_fail (IS_MUTABLE (structure));
+  g_return_if_fail (gst_structure_validate_name (name));
 
   structure->name = g_quark_from_string (name);
 }
 
+static inline void
+gst_structure_id_set_value_internal (GstStructure * structure, GQuark field,
+    const GValue * value)
+{
+  GstStructureField gsfield = { 0, {0,} };
+
+  gsfield.name = field;
+  gst_value_init_and_copy (&gsfield.value, value);
+
+  gst_structure_set_field (structure, &gsfield);
+}
+
 /**
  * gst_structure_id_set_value:
  * @structure: a #GstStructure
@@ -384,30 +449,12 @@ void
 gst_structure_id_set_value (GstStructure * structure,
     GQuark field, const GValue * value)
 {
-  GstStructureField gsfield = { 0, {0,} };
 
   g_return_if_fail (structure != NULL);
   g_return_if_fail (G_IS_VALUE (value));
   g_return_if_fail (IS_MUTABLE (structure));
 
-  /* if someones disables GST_DEBUG output, they probably do it for
-   * performance reasons, so skip the UTF-8 check here as well then */
-#ifndef GST_DISABLE_GST_DEBUG
-  if (G_VALUE_HOLDS_STRING (value)) {
-    const gchar *s;
-
-    s = g_value_get_string (value);
-    if (s != NULL && !g_utf8_validate (s, -1, NULL)) {
-      g_warning ("Trying to set string field '%s' on structure, but string is "
-          "not valid UTF-8. Please file a bug.", g_quark_to_string (field));
-    }
-  }
-#endif
-
-  gsfield.name = field;
-  gst_value_init_and_copy (&gsfield.value, value);
-
-  gst_structure_set_field (structure, &gsfield);
+  gst_structure_id_set_value_internal (structure, field, value);
 }
 
 /**
@@ -429,8 +476,104 @@ gst_structure_set_value (GstStructure * structure,
   g_return_if_fail (G_IS_VALUE (value));
   g_return_if_fail (IS_MUTABLE (structure));
 
-  gst_structure_id_set_value (structure, g_quark_from_string (fieldname),
-      value);
+  gst_structure_id_set_value_internal (structure,
+      g_quark_from_string (fieldname), value);
+}
+
+static inline void
+gst_structure_id_take_value_internal (GstStructure * structure, GQuark field,
+    GValue * value)
+{
+  GstStructureField gsfield = { 0, {0,} };
+
+  gsfield.name = field;
+  gsfield.value = *value;
+
+  gst_structure_set_field (structure, &gsfield);
+
+  /* we took ownership */
+#ifdef USE_POISONING
+  memset (value, 0, sizeof (GValue));
+#else
+  value->g_type = G_TYPE_INVALID;
+#endif
+}
+
+/**
+ * gst_structure_id_take_value:
+ * @structure: a #GstStructure
+ * @field: a #GQuark representing a field
+ * @value: (transfer full): the new value of the field
+ *
+ * Sets the field with the given GQuark @field to @value.  If the field
+ * does not exist, it is created.  If the field exists, the previous
+ * value is replaced and freed.
+ *
+ * Since: 0.10.31
+ */
+void
+gst_structure_id_take_value (GstStructure * structure, GQuark field,
+    GValue * value)
+{
+  g_return_if_fail (structure != NULL);
+  g_return_if_fail (G_IS_VALUE (value));
+  g_return_if_fail (IS_MUTABLE (structure));
+
+  gst_structure_id_take_value_internal (structure, field, value);
+}
+
+/**
+ * gst_structure_take_value:
+ * @structure: a #GstStructure
+ * @fieldname: the name of the field to set
+ * @value: (transfer full): the new value of the field
+ *
+ * Sets the field with the given name @field to @value.  If the field
+ * does not exist, it is created.  If the field exists, the previous
+ * value is replaced and freed. The function will take ownership of @value.
+ *
+ * Since: 0.10.31
+ */
+void
+gst_structure_take_value (GstStructure * structure, const gchar * fieldname,
+    GValue * value)
+{
+  g_return_if_fail (structure != NULL);
+  g_return_if_fail (fieldname != NULL);
+  g_return_if_fail (G_IS_VALUE (value));
+  g_return_if_fail (IS_MUTABLE (structure));
+
+  gst_structure_id_take_value_internal (structure,
+      g_quark_from_string (fieldname), value);
+}
+
+static void
+gst_structure_set_valist_internal (GstStructure * structure,
+    const gchar * fieldname, va_list varargs)
+{
+  gchar *err = NULL;
+  GType type;
+
+  while (fieldname) {
+    GstStructureField field = { 0 };
+
+    field.name = g_quark_from_string (fieldname);
+
+    type = va_arg (varargs, GType);
+
+    if (G_UNLIKELY (type == G_TYPE_DATE)) {
+      g_warning ("Don't use G_TYPE_DATE, use GST_TYPE_DATE instead\n");
+      type = GST_TYPE_DATE;
+    }
+    G_VALUE_COLLECT_INIT (&field.value, type, varargs, 0, &err);
+    if (G_UNLIKELY (err)) {
+      g_critical ("%s", err);
+      return;
+    }
+    gst_structure_set_field (structure, &field);
+
+    fieldname = va_arg (varargs, gchar *);
+  }
 }
 
 /**
@@ -449,11 +592,10 @@ gst_structure_set (GstStructure * structure, const gchar * field, ...)
   va_list varargs;
 
   g_return_if_fail (structure != NULL);
+  g_return_if_fail (IS_MUTABLE (structure) || field == NULL);
 
   va_start (varargs, field);
-
-  gst_structure_set_valist (structure, field, varargs);
-
+  gst_structure_set_valist_internal (structure, field, varargs);
   va_end (varargs);
 }
 
@@ -469,33 +611,43 @@ void
 gst_structure_set_valist (GstStructure * structure,
     const gchar * fieldname, va_list varargs)
 {
-  gchar *err = NULL;
-  GType type;
-
   g_return_if_fail (structure != NULL);
   g_return_if_fail (IS_MUTABLE (structure));
 
+  gst_structure_set_valist_internal (structure, fieldname, varargs);
+}
+
+static void
+gst_structure_id_set_valist_internal (GstStructure * structure,
+    GQuark fieldname, va_list varargs)
+{
+  gchar *err = NULL;
+  GType type;
+
   while (fieldname) {
     GstStructureField field = { 0 };
 
-    field.name = g_quark_from_string (fieldname);
+    field.name = fieldname;
 
     type = va_arg (varargs, GType);
 
-    if (type == G_TYPE_DATE) {
+    if (G_UNLIKELY (type == G_TYPE_DATE)) {
       g_warning ("Don't use G_TYPE_DATE, use GST_TYPE_DATE instead\n");
       type = GST_TYPE_DATE;
     }
-
+#ifndef G_VALUE_COLLECT_INIT
     g_value_init (&field.value, type);
     G_VALUE_COLLECT (&field.value, varargs, 0, &err);
-    if (err) {
+#else
+    G_VALUE_COLLECT_INIT (&field.value, type, varargs, 0, &err);
+#endif
+    if (G_UNLIKELY (err)) {
       g_critical ("%s", err);
       return;
     }
     gst_structure_set_field (structure, &field);
 
-    fieldname = va_arg (varargs, gchar *);
+    fieldname = va_arg (varargs, GQuark);
   }
 }
 
@@ -521,7 +673,7 @@ gst_structure_id_set (GstStructure * structure, GQuark field, ...)
   g_return_if_fail (structure != NULL);
 
   va_start (varargs, field);
-  gst_structure_id_set_valist (structure, field, varargs);
+  gst_structure_id_set_valist_internal (structure, field, varargs);
   va_end (varargs);
 }
 
@@ -539,36 +691,55 @@ void
 gst_structure_id_set_valist (GstStructure * structure,
     GQuark fieldname, va_list varargs)
 {
-  gchar *err = NULL;
-  GType type;
-
   g_return_if_fail (structure != NULL);
   g_return_if_fail (IS_MUTABLE (structure));
 
-  while (fieldname) {
-    GstStructureField field = { 0 };
+  gst_structure_id_set_valist_internal (structure, fieldname, varargs);
+}
 
-    field.name = fieldname;
+/**
+ * gst_structure_id_new:
+ * @name_quark: name of new structure
+ * @field_quark: the GQuark for the name of the field to set
+ * @...: variable arguments
+ *
+ * Creates a new #GstStructure with the given name as a GQuark, followed by
+ * fieldname quark, GType, argument(s) "triplets" in the same format as
+ * gst_structure_id_set(). Basically a convenience wrapper around
+ * gst_structure_id_empty_new() and gst_structure_id_set().
+ *
+ * The last variable argument must be NULL (or 0).
+ *
+ * Free-function: gst_structure_free
+ *
+ * Returns: (transfer full): a new #GstStructure
+ *
+ * Since: 0.10.24
+ */
+GstStructure *
+gst_structure_id_new (GQuark name_quark, GQuark field_quark, ...)
+{
+  GstStructure *s;
+  va_list varargs;
 
-    type = va_arg (varargs, GType);
+  g_return_val_if_fail (name_quark != 0, NULL);
+  g_return_val_if_fail (field_quark != 0, NULL);
 
-    if (type == G_TYPE_DATE) {
-      g_warning ("Don't use G_TYPE_DATE, use GST_TYPE_DATE instead\n");
-      type = GST_TYPE_DATE;
-    }
+  s = gst_structure_id_empty_new (name_quark);
 
-    g_value_init (&field.value, type);
-    G_VALUE_COLLECT (&field.value, varargs, 0, &err);
-    if (err) {
-      g_critical ("%s", err);
-      return;
-    }
-    gst_structure_set_field (structure, &field);
+  va_start (varargs, field_quark);
+  gst_structure_id_set_valist_internal (s, field_quark, varargs);
+  va_end (varargs);
 
-    fieldname = va_arg (varargs, GQuark);
-  }
+  return s;
 }
 
+#if GST_VERSION_NANO == 1
+#define GIT_G_WARNING g_warning
+#else
+#define GIT_G_WARNING GST_WARNING
+#endif
+
 /* If the structure currently contains a field with the same name, it is
  * replaced with the provided field. Otherwise, the field is added to the
  * structure. The field's value is not deeply copied.
@@ -577,12 +748,60 @@ static void
 gst_structure_set_field (GstStructure * structure, GstStructureField * field)
 {
   GstStructureField *f;
-  guint i;
+  guint i, len = structure->fields->len;
+
+  if (G_UNLIKELY (G_VALUE_HOLDS_STRING (&field->value))) {
+    const gchar *s;
+
+    s = g_value_get_string (&field->value);
+    /* only check for NULL strings in taglists, as they are allowed in message
+     * structs, e.g. error message debug strings */
+    if (G_UNLIKELY (IS_TAGLIST (structure) && (s == NULL || *s == '\0'))) {
+      if (s == NULL) {
+        GIT_G_WARNING ("Trying to set NULL string on field '%s' on taglist. "
+            "Please file a bug.", g_quark_to_string (field->name));
+        g_value_unset (&field->value);
+        return;
+      } else {
+        /* empty strings never make sense */
+        GIT_G_WARNING ("Trying to set empty string on taglist field '%s'. "
+            "Please file a bug.", g_quark_to_string (field->name));
+        g_value_unset (&field->value);
+        return;
+      }
+    } else if (G_UNLIKELY (s != NULL && !g_utf8_validate (s, -1, NULL))) {
+      g_warning ("Trying to set string on %s field '%s', but string is not "
+          "valid UTF-8. Please file a bug.",
+          IS_TAGLIST (structure) ? "taglist" : "structure",
+          g_quark_to_string (field->name));
+      g_value_unset (&field->value);
+      return;
+    }
+  } else if (G_UNLIKELY (GST_VALUE_HOLDS_DATE (&field->value))) {
+    const GDate *d;
+
+    d = gst_value_get_date (&field->value);
+    /* only check for NULL GDates in taglists, as they might make sense
+     * in other, generic structs */
+    if (G_UNLIKELY ((IS_TAGLIST (structure) && d == NULL))) {
+      GIT_G_WARNING ("Trying to set NULL GDate on field '%s' on taglist. "
+          "Please file a bug.", g_quark_to_string (field->name));
+      g_value_unset (&field->value);
+      return;
+    } else if (G_UNLIKELY (d != NULL && !g_date_valid (d))) {
+      g_warning
+          ("Trying to set invalid GDate on %s field '%s'. Please file a bug.",
+          IS_TAGLIST (structure) ? "taglist" : "structure",
+          g_quark_to_string (field->name));
+      g_value_unset (&field->value);
+      return;
+    }
+  }
 
-  for (i = 0; i < structure->fields->len; i++) {
+  for (i = 0; i < len; i++) {
     f = GST_STRUCTURE_FIELD (structure, i);
 
-    if (f->name == field->name) {
+    if (G_UNLIKELY (f->name == field->name)) {
       g_value_unset (&f->value);
       memcpy (f, field, sizeof (GstStructureField));
       return;
@@ -598,14 +817,14 @@ static GstStructureField *
 gst_structure_id_get_field (const GstStructure * structure, GQuark field_id)
 {
   GstStructureField *field;
-  guint i;
+  guint i, len;
 
-  g_return_val_if_fail (structure != NULL, NULL);
+  len = structure->fields->len;
 
-  for (i = 0; i < structure->fields->len; i++) {
+  for (i = 0; i < len; i++) {
     field = GST_STRUCTURE_FIELD (structure, i);
 
-    if (field->name == field_id)
+    if (G_UNLIKELY (field->name == field_id))
       return field;
   }
 
@@ -687,15 +906,16 @@ gst_structure_remove_field (GstStructure * structure, const gchar * fieldname)
 {
   GstStructureField *field;
   GQuark id;
-  guint i;
+  guint i, len;
 
   g_return_if_fail (structure != NULL);
   g_return_if_fail (fieldname != NULL);
   g_return_if_fail (IS_MUTABLE (structure));
 
   id = g_quark_from_string (fieldname);
+  len = structure->fields->len;
 
-  for (i = 0; i < structure->fields->len; i++) {
+  for (i = 0; i < len; i++) {
     field = GST_STRUCTURE_FIELD (structure, i);
 
     if (field->name == id) {
@@ -728,9 +948,7 @@ gst_structure_remove_fields (GstStructure * structure,
   /* mutability checked in remove_field */
 
   va_start (varargs, fieldname);
-
   gst_structure_remove_fields_valist (structure, fieldname, varargs);
-
   va_end (varargs);
 }
 
@@ -851,8 +1069,8 @@ gst_structure_nth_field_name (const GstStructure * structure, guint index)
 /**
  * gst_structure_foreach:
  * @structure: a #GstStructure
- * @func: a function to call for each field
- * @user_data: private data
+ * @func: (scope call): a function to call for each field
+ * @user_data: (closure): private data
  *
  * Calls the provided function once for each field in the #GstStructure. The
  * function must not modify the fields. Also see gst_structure_map_in_place().
@@ -864,18 +1082,20 @@ gboolean
 gst_structure_foreach (const GstStructure * structure,
     GstStructureForeachFunc func, gpointer user_data)
 {
-  guint i;
+  guint i, len;
   GstStructureField *field;
   gboolean ret;
 
   g_return_val_if_fail (structure != NULL, FALSE);
   g_return_val_if_fail (func != NULL, FALSE);
 
-  for (i = 0; i < structure->fields->len; i++) {
+  len = structure->fields->len;
+
+  for (i = 0; i < len; i++) {
     field = GST_STRUCTURE_FIELD (structure, i);
 
     ret = func (field->name, &field->value, user_data);
-    if (!ret)
+    if (G_UNLIKELY (!ret))
       return FALSE;
   }
 
@@ -885,12 +1105,12 @@ gst_structure_foreach (const GstStructure * structure,
 /**
  * gst_structure_map_in_place:
  * @structure: a #GstStructure
- * @func: a function to call for each field
- * @user_data: private data
+ * @func: (scope call): a function to call for each field
+ * @user_data: (closure): private data
  *
  * Calls the provided function once for each field in the #GstStructure. In
- * contrast to gst_structure_foreach(), the function may modify the fields. The
- * structure must be mutable.
+ * contrast to gst_structure_foreach(), the function may modify but not delete the
+ * fields. The structure must be mutable.
  *
  * Returns: TRUE if the supplied function returns TRUE For each of the fields,
  * FALSE otherwise.
@@ -899,15 +1119,16 @@ gboolean
 gst_structure_map_in_place (GstStructure * structure,
     GstStructureMapFunc func, gpointer user_data)
 {
-  guint i;
+  guint i, len;
   GstStructureField *field;
   gboolean ret;
 
   g_return_val_if_fail (structure != NULL, FALSE);
   g_return_val_if_fail (IS_MUTABLE (structure), FALSE);
   g_return_val_if_fail (func != NULL, FALSE);
+  len = structure->fields->len;
 
-  for (i = 0; i < structure->fields->len; i++) {
+  for (i = 0; i < len; i++) {
     field = GST_STRUCTURE_FIELD (structure, i);
 
     ret = func (field->name, &field->value, user_data);
@@ -918,6 +1139,30 @@ gst_structure_map_in_place (GstStructure * structure,
   return TRUE;
 }
 
+/**
+ * gst_structure_id_has_field:
+ * @structure: a #GstStructure
+ * @field: #GQuark of the field name
+ *
+ * Check if @structure contains a field named @field.
+ *
+ * Returns: TRUE if the structure contains a field with the given name
+ *
+ * Since: 0.10.26
+ */
+gboolean
+gst_structure_id_has_field (const GstStructure * structure, GQuark field)
+{
+  GstStructureField *f;
+
+  g_return_val_if_fail (structure != NULL, FALSE);
+  g_return_val_if_fail (field != 0, FALSE);
+
+  f = gst_structure_id_get_field (structure, field);
+
+  return (f != NULL);
+}
+
 /**
  * gst_structure_has_field:
  * @structure: a #GstStructure
@@ -931,14 +1176,39 @@ gboolean
 gst_structure_has_field (const GstStructure * structure,
     const gchar * fieldname)
 {
-  GstStructureField *field;
+  g_return_val_if_fail (structure != NULL, FALSE);
+  g_return_val_if_fail (fieldname != NULL, FALSE);
 
-  g_return_val_if_fail (structure != NULL, 0);
-  g_return_val_if_fail (fieldname != NULL, 0);
+  return gst_structure_id_has_field (structure,
+      g_quark_from_string (fieldname));
+}
 
-  field = gst_structure_get_field (structure, fieldname);
+/**
+ * gst_structure_id_has_field_typed:
+ * @structure: a #GstStructure
+ * @field: #GQuark of the field name
+ * @type: the type of a value
+ *
+ * Check if @structure contains a field named @field and with GType @type.
+ *
+ * Returns: TRUE if the structure contains a field with the given name and type
+ *
+ * Since: 0.10.26
+ */
+gboolean
+gst_structure_id_has_field_typed (const GstStructure * structure,
+    GQuark field, GType type)
+{
+  GstStructureField *f;
+
+  g_return_val_if_fail (structure != NULL, FALSE);
+  g_return_val_if_fail (field != 0, FALSE);
+
+  f = gst_structure_id_get_field (structure, field);
+  if (f == NULL)
+    return FALSE;
 
-  return (field != NULL);
+  return (G_VALUE_TYPE (&f->value) == type);
 }
 
 /**
@@ -955,26 +1225,20 @@ gboolean
 gst_structure_has_field_typed (const GstStructure * structure,
     const gchar * fieldname, GType type)
 {
-  GstStructureField *field;
-
-  g_return_val_if_fail (structure != NULL, 0);
-  g_return_val_if_fail (fieldname != NULL, 0);
-
-  field = gst_structure_get_field (structure, fieldname);
-  if (field == NULL)
-    return FALSE;
+  g_return_val_if_fail (structure != NULL, FALSE);
+  g_return_val_if_fail (fieldname != NULL, FALSE);
 
-  return (G_VALUE_TYPE (&field->value) == type);
+  return gst_structure_id_has_field_typed (structure,
+      g_quark_from_string (fieldname), type);
 }
 
-
 /* utility functions */
 
 /**
  * gst_structure_get_boolean:
  * @structure: a #GstStructure
  * @fieldname: the name of a field
- * @value: a pointer to a #gboolean to set
+ * @value: (out): a pointer to a #gboolean to set
  *
  * Sets the boolean pointed to by @value corresponding to the value of the
  * given field.  Caller is responsible for making sure the field exists
@@ -1000,7 +1264,7 @@ gst_structure_get_boolean (const GstStructure * structure,
   if (!G_VALUE_HOLDS_BOOLEAN (&field->value))
     return FALSE;
 
-  *value = g_value_get_boolean (&field->value);
+  *value = gst_g_value_get_boolean_unchecked (&field->value);
 
   return TRUE;
 }
@@ -1009,15 +1273,15 @@ gst_structure_get_boolean (const GstStructure * structure,
  * gst_structure_get_int:
  * @structure: a #GstStructure
  * @fieldname: the name of a field
- * @value: a pointer to an int to set
+ * @value: (out): a pointer to an int to set
  *
  * Sets the int pointed to by @value corresponding to the value of the
  * given field.  Caller is responsible for making sure the field exists
  * and has the correct type.
  *
- * Returns: TRUE if the value could be set correctly. If there was no field
+ * Returns: %TRUE if the value could be set correctly. If there was no field
  * with @fieldname or the existing field did not contain an int, this function
- * returns FALSE.
+ * returns %FALSE.
  */
 gboolean
 gst_structure_get_int (const GstStructure * structure,
@@ -1036,28 +1300,30 @@ gst_structure_get_int (const GstStructure * structure,
   if (!G_VALUE_HOLDS_INT (&field->value))
     return FALSE;
 
-  *value = g_value_get_int (&field->value);
+  *value = gst_g_value_get_int_unchecked (&field->value);
 
   return TRUE;
 }
 
 /**
- * gst_structure_get_fourcc:
+ * gst_structure_get_uint:
  * @structure: a #GstStructure
  * @fieldname: the name of a field
- * @value: a pointer to a #GstFourcc to set
+ * @value: (out): a pointer to a uint to set
  *
- * Sets the #GstFourcc pointed to by @value corresponding to the value of the
+ * Sets the uint pointed to by @value corresponding to the value of the
  * given field.  Caller is responsible for making sure the field exists
  * and has the correct type.
  *
- * Returns: TRUE if the value could be set correctly. If there was no field
- * with @fieldname or the existing field did not contain a fourcc, this function
- * returns FALSE.
+ * Returns: %TRUE if the value could be set correctly. If there was no field
+ * with @fieldname or the existing field did not contain a uint, this function
+ * returns %FALSE.
+ *
+ * Since: 0.10.15
  */
 gboolean
-gst_structure_get_fourcc (const GstStructure * structure,
-    const gchar * fieldname, guint32 * value)
+gst_structure_get_uint (const GstStructure * structure,
+    const gchar * fieldname, guint * value)
 {
   GstStructureField *field;
 
@@ -1069,10 +1335,46 @@ gst_structure_get_fourcc (const GstStructure * structure,
 
   if (field == NULL)
     return FALSE;
-  if (!GST_VALUE_HOLDS_FOURCC (&field->value))
+  if (!G_VALUE_HOLDS_UINT (&field->value))
     return FALSE;
 
-  *value = gst_value_get_fourcc (&field->value);
+  *value = gst_g_value_get_uint_unchecked (&field->value);
+
+  return TRUE;
+}
+
+/**
+ * gst_structure_get_fourcc:
+ * @structure: a #GstStructure
+ * @fieldname: the name of a field
+ * @value: (out): a pointer to a 32bit unsigned int to set
+ *
+ * Sets the Fourcc pointed to by @value corresponding to the value of the
+ * given field.  Caller is responsible for making sure the field exists
+ * and has the correct type.
+ *
+ * Returns: TRUE if the value could be set correctly. If there was no field
+ * with @fieldname or the existing field did not contain a fourcc, this function
+ * returns FALSE.
+ */
+gboolean
+gst_structure_get_fourcc (const GstStructure * structure,
+    const gchar * fieldname, guint32 * value)
+{
+  GstStructureField *field;
+
+  g_return_val_if_fail (structure != NULL, FALSE);
+  g_return_val_if_fail (fieldname != NULL, FALSE);
+  g_return_val_if_fail (value != NULL, FALSE);
+
+  field = gst_structure_get_field (structure, fieldname);
+
+  if (field == NULL)
+    return FALSE;
+  if (!GST_VALUE_HOLDS_FOURCC (&field->value))
+    return FALSE;
+
+  *value = gst_value_get_fourcc (&field->value);
 
   return TRUE;
 }
@@ -1081,12 +1383,17 @@ gst_structure_get_fourcc (const GstStructure * structure,
  * gst_structure_get_date:
  * @structure: a #GstStructure
  * @fieldname: the name of a field
- * @value: a pointer to a #GDate to set
+ * @value: (out callee-allocates): a pointer to a #GDate to set
  *
  * Sets the date pointed to by @value corresponding to the date of the
  * given field.  Caller is responsible for making sure the field exists
  * and has the correct type.
  *
+ * On success @value will point to a newly-allocated copy of the date which
+ * should be freed with g_date_free() when no longer needed (note: this is
+ * inconsistent with e.g. gst_structure_get_string() which doesn't return a
+ * copy of the string).
+ *
  * Returns: TRUE if the value could be set correctly. If there was no field
  * with @fieldname or the existing field did not contain a data, this function
  * returns FALSE.
@@ -1108,6 +1415,51 @@ gst_structure_get_date (const GstStructure * structure, const gchar * fieldname,
   if (!GST_VALUE_HOLDS_DATE (&field->value))
     return FALSE;
 
+  /* FIXME: 0.11 g_value_dup_boxed() -> g_value_get_boxed() */
+  *value = g_value_dup_boxed (&field->value);
+
+  return TRUE;
+}
+
+/**
+ * gst_structure_get_date_time:
+ * @structure: a #GstStructure
+ * @fieldname: the name of a field
+ * @value: (out callee-allocates): a pointer to a #GstDateTime to set
+ *
+ * Sets the datetime pointed to by @value corresponding to the datetime of the
+ * given field. Caller is responsible for making sure the field exists
+ * and has the correct type.
+ *
+ * On success @value will point to a reference of the datetime which
+ * should be unreffed with gst_date_time_unref() when no longer needed
+ * (note: this is inconsistent with e.g. gst_structure_get_string()
+ * which doesn't return a copy of the string).
+ *
+ * Returns: TRUE if the value could be set correctly. If there was no field
+ * with @fieldname or the existing field did not contain a data, this function
+ * returns FALSE.
+ *
+ * Since: 0.10.31
+ */
+gboolean
+gst_structure_get_date_time (const GstStructure * structure,
+    const gchar * fieldname, GstDateTime ** value)
+{
+  GstStructureField *field;
+
+  g_return_val_if_fail (structure != NULL, FALSE);
+  g_return_val_if_fail (fieldname != NULL, FALSE);
+  g_return_val_if_fail (value != NULL, FALSE);
+
+  field = gst_structure_get_field (structure, fieldname);
+
+  if (field == NULL)
+    return FALSE;
+  if (!GST_VALUE_HOLDS_DATE_TIME (&field->value))
+    return FALSE;
+
+  /* FIXME: 0.11 g_value_dup_boxed() -> g_value_get_boxed() */
   *value = g_value_dup_boxed (&field->value);
 
   return TRUE;
@@ -1117,14 +1469,14 @@ gst_structure_get_date (const GstStructure * structure, const gchar * fieldname,
  * gst_structure_get_clock_time:
  * @structure: a #GstStructure
  * @fieldname: the name of a field
- * @value: a pointer to a #GstClockTime to set
+ * @value: (out): a pointer to a #GstClockTime to set
  *
  * Sets the clock time pointed to by @value corresponding to the clock time
  * of the given field.  Caller is responsible for making sure the field exists
  * and has the correct type.
  *
  * Returns: TRUE if the value could be set correctly. If there was no field
- * with @fieldname or the existing field did not contain a #GstClockTime, this 
+ * with @fieldname or the existing field did not contain a #GstClockTime, this
  * function returns FALSE.
  */
 gboolean
@@ -1144,7 +1496,7 @@ gst_structure_get_clock_time (const GstStructure * structure,
   if (!G_VALUE_HOLDS_UINT64 (&field->value))
     return FALSE;
 
-  *value = g_value_get_uint64 (&field->value);
+  *value = gst_g_value_get_uint64_unchecked (&field->value);
 
   return TRUE;
 }
@@ -1153,14 +1505,14 @@ gst_structure_get_clock_time (const GstStructure * structure,
  * gst_structure_get_double:
  * @structure: a #GstStructure
  * @fieldname: the name of a field
- * @value: a pointer to a #GstFourcc to set
+ * @value: (out): a pointer to a gdouble to set
  *
  * Sets the double pointed to by @value corresponding to the value of the
  * given field.  Caller is responsible for making sure the field exists
  * and has the correct type.
  *
  * Returns: TRUE if the value could be set correctly. If there was no field
- * with @fieldname or the existing field did not contain a double, this 
+ * with @fieldname or the existing field did not contain a double, this
  * function returns FALSE.
  */
 gboolean
@@ -1180,7 +1532,7 @@ gst_structure_get_double (const GstStructure * structure,
   if (!G_VALUE_HOLDS_DOUBLE (&field->value))
     return FALSE;
 
-  *value = g_value_get_double (&field->value);
+  *value = gst_g_value_get_double_unchecked (&field->value);
 
   return TRUE;
 }
@@ -1216,7 +1568,7 @@ gst_structure_get_string (const GstStructure * structure,
   if (!G_VALUE_HOLDS_STRING (&field->value))
     return NULL;
 
-  return g_value_get_string (&field->value);
+  return gst_g_value_get_string_unchecked (&field->value);
 }
 
 /**
@@ -1224,7 +1576,7 @@ gst_structure_get_string (const GstStructure * structure,
  * @structure: a #GstStructure
  * @fieldname: the name of a field
  * @enumtype: the enum type of a field
- * @value: a pointer to an int to set
+ * @value: (out): a pointer to an int to set
  *
  * Sets the int pointed to by @value corresponding to the value of the
  * given field.  Caller is responsible for making sure the field exists,
@@ -1249,8 +1601,6 @@ gst_structure_get_enum (const GstStructure * structure,
 
   if (field == NULL)
     return FALSE;
-  if (!G_VALUE_HOLDS_ENUM (&field->value))
-    return FALSE;
   if (!G_TYPE_CHECK_VALUE_TYPE (&field->value, enumtype))
     return FALSE;
 
@@ -1263,15 +1613,15 @@ gst_structure_get_enum (const GstStructure * structure,
  * gst_structure_get_fraction:
  * @structure: a #GstStructure
  * @fieldname: the name of a field
- * @value_numerator: a pointer to an int to set
- * @value_denominator: a pointer to an int to set
+ * @value_numerator: (out): a pointer to an int to set
+ * @value_denominator: (out): a pointer to an int to set
  *
- * Sets the integers pointed to by @value_numerator and @value_denominator 
- * corresponding to the value of the given field.  Caller is responsible 
+ * Sets the integers pointed to by @value_numerator and @value_denominator
+ * corresponding to the value of the given field.  Caller is responsible
  * for making sure the field exists and has the correct type.
  *
  * Returns: TRUE if the values could be set correctly. If there was no field
- * with @fieldname or the existing field did not contain a GstFraction, this 
+ * with @fieldname or the existing field did not contain a GstFraction, this
  * function returns FALSE.
  */
 gboolean
@@ -1300,7 +1650,7 @@ gst_structure_get_fraction (const GstStructure * structure,
 
 typedef struct _GstStructureAbbreviation
 {
-  char *type_name;
+  const gchar *type_name;
   GType type;
 }
 GstStructureAbbreviation;
@@ -1311,15 +1661,20 @@ static GstStructureAbbreviation *
 gst_structure_get_abbrs (gint * n_abbrs)
 {
   static GstStructureAbbreviation *abbrs = NULL;
-  static gint num = 0;
+  static volatile gsize num = 0;
 
-  if (abbrs == NULL) {
+  if (g_once_init_enter (&num)) {
     /* dynamically generate the array */
+    gsize _num;
     GstStructureAbbreviation dyn_abbrs[] = {
       {"int", G_TYPE_INT}
       ,
       {"i", G_TYPE_INT}
       ,
+      {"uint", G_TYPE_UINT}
+      ,
+      {"u", G_TYPE_UINT}
+      ,
       {"float", G_TYPE_FLOAT}
       ,
       {"f", G_TYPE_FLOAT}
@@ -1347,11 +1702,18 @@ gst_structure_get_abbrs (gint * n_abbrs)
       {"str", G_TYPE_STRING}
       ,
       {"s", G_TYPE_STRING}
+      ,
+      {"structure", GST_TYPE_STRUCTURE}
+      ,
+      {"date", GST_TYPE_DATE}
+      ,
+      {"datetime", GST_TYPE_DATE_TIME}
     };
-    num = G_N_ELEMENTS (dyn_abbrs);
+    _num = G_N_ELEMENTS (dyn_abbrs);
     /* permanently allocate and copy the array now */
-    abbrs = g_new0 (GstStructureAbbreviation, num);
-    memcpy (abbrs, dyn_abbrs, sizeof (GstStructureAbbreviation) * num);
+    abbrs = g_new0 (GstStructureAbbreviation, _num);
+    memcpy (abbrs, dyn_abbrs, sizeof (GstStructureAbbreviation) * _num);
+    g_once_init_leave (&num, _num);
   }
   *n_abbrs = num;
 
@@ -1417,6 +1779,8 @@ gst_structure_value_get_generic_type (GValue * val)
     }
   } else if (G_VALUE_TYPE (val) == GST_TYPE_INT_RANGE) {
     return G_TYPE_INT;
+  } else if (G_VALUE_TYPE (val) == GST_TYPE_INT64_RANGE) {
+    return G_TYPE_INT64;
   } else if (G_VALUE_TYPE (val) == GST_TYPE_DOUBLE_RANGE) {
     return G_TYPE_DOUBLE;
   } else if (G_VALUE_TYPE (val) == GST_TYPE_FRACTION_RANGE) {
@@ -1425,9 +1789,39 @@ gst_structure_value_get_generic_type (GValue * val)
   return G_VALUE_TYPE (val);
 }
 
-#define GST_ASCII_IS_STRING(c) (g_ascii_isalnum((c)) || ((c) == '_') || \
-      ((c) == '-') || ((c) == '+') || ((c) == '/') || ((c) == ':') || \
-      ((c) == '.'))
+gboolean
+priv_gst_structure_append_to_gstring (const GstStructure * structure,
+    GString * s)
+{
+  GstStructureField *field;
+  guint i, len;
+
+  g_return_val_if_fail (s != NULL, FALSE);
+
+  g_string_append (s, g_quark_to_string (structure->name));
+  len = structure->fields->len;
+  for (i = 0; i < len; i++) {
+    char *t;
+    GType type;
+
+    field = GST_STRUCTURE_FIELD (structure, i);
+
+    t = gst_value_serialize (&field->value);
+    type = gst_structure_value_get_generic_type (&field->value);
+
+    g_string_append_len (s, ", ", 2);
+    /* FIXME: do we need to escape fieldnames? */
+    g_string_append (s, g_quark_to_string (field->name));
+    g_string_append_len (s, "=(", 2);
+    g_string_append (s, gst_structure_to_abbr (type));
+    g_string_append_c (s, ')');
+    g_string_append (s, t == NULL ? "NULL" : t);
+    g_free (t);
+  }
+
+  g_string_append_c (s, ';');
+  return TRUE;
+}
 
 /**
  * gst_structure_to_string:
@@ -1435,15 +1829,21 @@ gst_structure_value_get_generic_type (GValue * val)
  *
  * Converts @structure to a human-readable string representation.
  *
- * Returns: a pointer to string allocated by g_malloc(). g_free() after
- * usage.
+ * For debugging purposes its easier to do something like this:
+ * |[
+ * GST_LOG ("structure is %" GST_PTR_FORMAT, structure);
+ * ]|
+ * This prints the structure in human readble form.
+ *
+ * Free-function: g_free
+ *
+ * Returns: (transfer full)L a pointer to string allocated by g_malloc().
+ *     g_free() after usage.
  */
 gchar *
 gst_structure_to_string (const GstStructure * structure)
 {
-  GstStructureField *field;
   GString *s;
-  guint i;
 
   /* NOTE:  This function is potentially called by the debug system,
    * so any calls to gst_log() (and GST_DEBUG(), GST_LOG(), etc.)
@@ -1453,22 +1853,10 @@ gst_structure_to_string (const GstStructure * structure)
 
   g_return_val_if_fail (structure != NULL, NULL);
 
-  s = g_string_new ("");
-  /* FIXME this string may need to be escaped */
-  g_string_append_printf (s, "%s", g_quark_to_string (structure->name));
-  for (i = 0; i < structure->fields->len; i++) {
-    char *t;
-    GType type;
-
-    field = GST_STRUCTURE_FIELD (structure, i);
-
-    t = gst_value_serialize (&field->value);
-    type = gst_structure_value_get_generic_type (&field->value);
-
-    g_string_append_printf (s, ", %s=(%s)%s", g_quark_to_string (field->name),
-        gst_structure_to_abbr (type), GST_STR_NULL (t));
-    g_free (t);
-  }
+  /* we estimate a minimum size based on the number of fields in order to
+   * avoid unnecessary reallocs within GString */
+  s = g_string_sized_new (STRUCTURE_ESTIMATED_STRING_LEN (structure));
+  priv_gst_structure_append_to_gstring (structure, s);
   return g_string_free (s, FALSE);
 }
 
@@ -1480,7 +1868,8 @@ gst_structure_to_string (const GstStructure * structure)
  * THIS FUNCTION MODIFIES THE STRING AND DETECTS INSIDE A NONTERMINATED STRING
  */
 static gboolean
-gst_structure_parse_string (gchar * s, gchar ** end, gchar ** next)
+gst_structure_parse_string (gchar * s, gchar ** end, gchar ** next,
+    gboolean unescape)
 {
   gchar *w;
 
@@ -1496,21 +1885,32 @@ gst_structure_parse_string (gchar * s, gchar ** end, gchar ** next)
     return ret;
   }
 
-  w = s;
-  s++;
-  while (*s != '"') {
-    if (*s == 0)
-      return FALSE;
-
-    if (*s == '\\') {
+  if (unescape) {
+    w = s;
+    s++;
+    while (*s != '"') {
+      if (G_UNLIKELY (*s == 0))
+        return FALSE;
+      if (G_UNLIKELY (*s == '\\'))
+        s++;
+      *w = *s;
+      w++;
       s++;
     }
-
-    *w = *s;
-    w++;
     s++;
+  } else {
+    /* Find the closing quotes */
+    s++;
+    while (*s != '"') {
+      if (G_UNLIKELY (*s == 0))
+        return FALSE;
+      if (G_UNLIKELY (*s == '\\'))
+        s++;
+      s++;
+    }
+    s++;
+    w = s;
   }
-  s++;
 
   *end = w;
   *next = s;
@@ -1527,7 +1927,6 @@ gst_structure_parse_range (gchar * s, gchar ** after, GValue * value,
   GType range_type;
   gboolean ret;
 
-
   if (*s != '[')
     return FALSE;
   s++;
@@ -1563,13 +1962,19 @@ gst_structure_parse_range (gchar * s, gchar ** after, GValue * value,
   if (G_VALUE_TYPE (&value1) == G_TYPE_DOUBLE) {
     range_type = GST_TYPE_DOUBLE_RANGE;
     g_value_init (value, range_type);
-    gst_value_set_double_range (value, g_value_get_double (&value1),
-        g_value_get_double (&value2));
+    gst_value_set_double_range (value,
+        gst_g_value_get_double_unchecked (&value1),
+        gst_g_value_get_double_unchecked (&value2));
   } else if (G_VALUE_TYPE (&value1) == G_TYPE_INT) {
     range_type = GST_TYPE_INT_RANGE;
     g_value_init (value, range_type);
-    gst_value_set_int_range (value, g_value_get_int (&value1),
-        g_value_get_int (&value2));
+    gst_value_set_int_range (value, gst_g_value_get_int_unchecked (&value1),
+        gst_g_value_get_int_unchecked (&value2));
+  } else if (G_VALUE_TYPE (&value1) == G_TYPE_INT64) {
+    range_type = GST_TYPE_INT64_RANGE;
+    g_value_init (value, range_type);
+    gst_value_set_int64_range (value, gst_g_value_get_int64_unchecked (&value1),
+        gst_g_value_get_int64_unchecked (&value2));
   } else if (G_VALUE_TYPE (&value1) == GST_TYPE_FRACTION) {
     range_type = GST_TYPE_FRACTION_RANGE;
     g_value_init (value, range_type);
@@ -1658,7 +2063,7 @@ gst_structure_parse_simple_string (gchar * str, gchar ** end)
 {
   char *s = str;
 
-  while (GST_ASCII_IS_STRING (*s)) {
+  while (G_LIKELY (GST_ASCII_IS_STRING (*s))) {
     s++;
   }
 
@@ -1681,24 +2086,32 @@ gst_structure_parse_field (gchar * str,
   while (g_ascii_isspace (*s) || (s[0] == '\\' && g_ascii_isspace (s[1])))
     s++;
   name = s;
-  if (!gst_structure_parse_simple_string (s, &name_end))
+  if (G_UNLIKELY (!gst_structure_parse_simple_string (s, &name_end))) {
+    GST_WARNING ("failed to parse simple string, str=%s", str);
     return FALSE;
+  }
 
   s = name_end;
   while (g_ascii_isspace (*s) || (s[0] == '\\' && g_ascii_isspace (s[1])))
     s++;
 
-  if (*s != '=')
+  if (G_UNLIKELY (*s != '=')) {
+    GST_WARNING ("missing assignment operator in the field, str=%s", str);
     return FALSE;
+  }
   s++;
 
   c = *name_end;
-  *name_end = 0;
+  *name_end = '\0';
   field->name = g_quark_from_string (name);
+  GST_DEBUG ("trying field name '%s'", name);
   *name_end = c;
 
-  if (!gst_structure_parse_value (s, &s, &field->value, G_TYPE_INVALID))
+  if (G_UNLIKELY (!gst_structure_parse_value (s, &s, &field->value,
+              G_TYPE_INVALID))) {
+    GST_WARNING ("failed to parse value %s", str);
     return FALSE;
+  }
 
   *after = s;
   return TRUE;
@@ -1717,7 +2130,6 @@ gst_structure_parse_value (gchar * str,
   int ret = 0;
   GType type = default_type;
 
-
   s = str;
   while (g_ascii_isspace (*s))
     s++;
@@ -1725,18 +2137,16 @@ gst_structure_parse_value (gchar * str,
   /* check if there's a (type_name) 'cast' */
   type_name = NULL;
   if (*s == '(') {
-    type = G_TYPE_INVALID;
-
     s++;
     while (g_ascii_isspace (*s))
       s++;
     type_name = s;
-    if (!gst_structure_parse_simple_string (s, &type_end))
+    if (G_UNLIKELY (!gst_structure_parse_simple_string (s, &type_end)))
       return FALSE;
     s = type_end;
     while (g_ascii_isspace (*s))
       s++;
-    if (*s != ')')
+    if (G_UNLIKELY (*s != ')'))
       return FALSE;
     s++;
     while (g_ascii_isspace (*s))
@@ -1745,10 +2155,13 @@ gst_structure_parse_value (gchar * str,
     c = *type_end;
     *type_end = 0;
     type = gst_structure_gtype_from_abbr (type_name);
+    GST_DEBUG ("trying type name '%s'", type_name);
     *type_end = c;
 
-    if (type == G_TYPE_INVALID)
+    if (G_UNLIKELY (type == G_TYPE_INVALID)) {
+      GST_WARNING ("invalid type");
       return FALSE;
+    }
   }
 
   while (g_ascii_isspace (*s))
@@ -1761,17 +2174,21 @@ gst_structure_parse_value (gchar * str,
     ret = gst_structure_parse_array (s, &s, value, type);
   } else {
     value_s = s;
-    if (!gst_structure_parse_string (s, &value_end, &s))
-      return FALSE;
 
-    c = *value_end;
-    *value_end = 0;
-    if (type == G_TYPE_INVALID) {
+    if (G_UNLIKELY (type == G_TYPE_INVALID)) {
       GType try_types[] =
-          { G_TYPE_INT, G_TYPE_DOUBLE, GST_TYPE_FRACTION, G_TYPE_STRING };
+          { G_TYPE_INT, G_TYPE_DOUBLE, GST_TYPE_FRACTION, G_TYPE_BOOLEAN,
+        G_TYPE_STRING
+      };
       int i;
 
-      for (i = 0; i < 4; i++) {
+      if (G_UNLIKELY (!gst_structure_parse_string (s, &value_end, &s, TRUE)))
+        return FALSE;
+      /* Set NULL terminator for deserialization */
+      c = *value_end;
+      *value_end = '\0';
+
+      for (i = 0; i < G_N_ELEMENTS (try_types); i++) {
         g_value_init (value, try_types[i]);
         ret = gst_value_deserialize (value, value_s);
         if (ret)
@@ -1781,7 +2198,16 @@ gst_structure_parse_value (gchar * str,
     } else {
       g_value_init (value, type);
 
+      if (G_UNLIKELY (!gst_structure_parse_string (s, &value_end, &s,
+                  (type != G_TYPE_STRING))))
+        return FALSE;
+      /* Set NULL terminator for deserialization */
+      c = *value_end;
+      *value_end = '\0';
+
       ret = gst_value_deserialize (value, value_s);
+      if (G_UNLIKELY (!ret))
+        g_value_unset (value);
     }
     *value_end = c;
   }
@@ -1794,14 +2220,16 @@ gst_structure_parse_value (gchar * str,
 /**
  * gst_structure_from_string:
  * @string: a string representation of a #GstStructure.
- * @end: pointer to store the end of the string in.
+ * @end: (out) (allow-none): pointer to store the end of the string in.
  *
  * Creates a #GstStructure from a string representation.
  * If end is not NULL, a pointer to the place inside the given string
  * where parsing ended will be returned.
  *
- * Returns: a new #GstStructure or NULL when the string could not
- * be parsed. Free after usage.
+ * Free-function: gst_structure_free
+ *
+ * Returns: (transfer full): a new #GstStructure or NULL when the string could
+ *     not be parsed. Free with gst_structure_free() after use.
  */
 GstStructure *
 gst_structure_from_string (const gchar * string, gchar ** end)
@@ -1812,46 +2240,67 @@ gst_structure_from_string (const gchar * string, gchar ** end)
   char *r;
   char save;
   GstStructure *structure = NULL;
-  GstStructureField field = { 0 };
+  GstStructureField field;
 
   g_return_val_if_fail (string != NULL, NULL);
 
   copy = g_strdup (string);
   r = copy;
 
-  name = r;
-  if (!gst_structure_parse_string (r, &w, &r))
-    goto error;
-
-  while (g_ascii_isspace (*r) || (r[0] == '\\' && g_ascii_isspace (r[1])))
+  /* skip spaces (FIXME: _isspace treats tabs and newlines as space!) */
+  while (*r && (g_ascii_isspace (*r) || (r[0] == '\\'
+              && g_ascii_isspace (r[1]))))
     r++;
-  if (*r != 0 && *r != ';' && *r != ',')
+
+  name = r;
+  if (G_UNLIKELY (!gst_structure_parse_string (r, &w, &r, TRUE))) {
+    GST_WARNING ("Failed to parse structure string '%s'", string);
     goto error;
+  }
 
   save = *w;
-  *w = 0;
+  *w = '\0';
   structure = gst_structure_empty_new (name);
   *w = save;
 
-  while (*r && (*r != ';')) {
-    if (*r != ',')
+  if (G_UNLIKELY (structure == NULL))
+    goto error;
+
+  do {
+    while (*r && (g_ascii_isspace (*r) || (r[0] == '\\'
+                && g_ascii_isspace (r[1]))))
+      r++;
+    if (*r == ';') {
+      /* end of structure, get the next char and finish */
+      r++;
+      break;
+    }
+    if (*r == '\0') {
+      /* accept \0 as end delimiter */
+      break;
+    }
+    if (G_UNLIKELY (*r != ',')) {
+      GST_WARNING ("Failed to find delimiter, r=%s", r);
       goto error;
+    }
     r++;
     while (*r && (g_ascii_isspace (*r) || (r[0] == '\\'
                 && g_ascii_isspace (r[1]))))
       r++;
 
     memset (&field, 0, sizeof (field));
-    if (!gst_structure_parse_field (r, &r, &field))
+    if (G_UNLIKELY (!gst_structure_parse_field (r, &r, &field))) {
+      GST_WARNING ("Failed to parse field, r=%s", r);
       goto error;
+    }
     gst_structure_set_field (structure, &field);
-    while (*r && (g_ascii_isspace (*r) || (r[0] == '\\'
-                && g_ascii_isspace (r[1]))))
-      r++;
-  }
+  } while (TRUE);
 
   if (end)
     *end = (char *) string + (r - copy);
+  else if (*r)
+    g_warning ("gst_structure_from_string did not consume whole string,"
+        " but caller did not provide end pointer (\"%s\")", string);
 
   g_free (copy);
   return structure;
@@ -1930,7 +2379,7 @@ gst_structure_fixate_field_nearest_int (GstStructure * structure,
     for (i = 0; i < n; i++) {
       list_value = gst_value_list_get_value (value, i);
       if (G_VALUE_TYPE (list_value) == G_TYPE_INT) {
-        int x = g_value_get_int (list_value);
+        int x = gst_g_value_get_int_unchecked (list_value);
 
         if (best_index == -1 || (ABS (target - x) < ABS (target - best))) {
           best_index = i;
@@ -1994,7 +2443,7 @@ gst_structure_fixate_field_nearest_double (GstStructure * structure,
     for (i = 0; i < n; i++) {
       list_value = gst_value_list_get_value (value, i);
       if (G_VALUE_TYPE (list_value) == G_TYPE_DOUBLE) {
-        double x = g_value_get_double (list_value);
+        double x = gst_g_value_get_double_unchecked (list_value);
 
         if (best_index == -1 || (ABS (target - x) < ABS (target - best))) {
           best_index = i;
@@ -2048,7 +2497,7 @@ gst_structure_fixate_field_boolean (GstStructure * structure,
     for (i = 0; i < n; i++) {
       list_value = gst_value_list_get_value (value, i);
       if (G_VALUE_TYPE (list_value) == G_TYPE_BOOLEAN) {
-        gboolean x = g_value_get_boolean (list_value);
+        gboolean x = gst_g_value_get_boolean_unchecked (list_value);
 
         if (best_index == -1 || x == target) {
           best_index = i;
@@ -2066,6 +2515,61 @@ gst_structure_fixate_field_boolean (GstStructure * structure,
   return FALSE;
 }
 
+/**
+ * gst_structure_fixate_field_string:
+ * @structure: a #GstStructure
+ * @field_name: a field in @structure
+ * @target: the target value of the fixation
+ *
+ * Fixates a #GstStructure by changing the given @field_name field to the given
+ * @target string if that field is not fixed yet.
+ *
+ * Returns: TRUE if the structure could be fixated
+ *
+ * Since: 0.10.30
+ */
+gboolean
+gst_structure_fixate_field_string (GstStructure * structure,
+    const gchar * field_name, const gchar * target)
+{
+  const GValue *value;
+
+  g_return_val_if_fail (gst_structure_has_field (structure, field_name), FALSE);
+  g_return_val_if_fail (IS_MUTABLE (structure), FALSE);
+
+  value = gst_structure_get_value (structure, field_name);
+
+  if (G_VALUE_TYPE (value) == G_TYPE_STRING) {
+    /* already fixed */
+    return FALSE;
+  } else if (G_VALUE_TYPE (value) == GST_TYPE_LIST) {
+    const GValue *list_value;
+    int i, n;
+    const gchar *best = NULL;
+    int best_index = -1;
+
+    n = gst_value_list_get_size (value);
+    for (i = 0; i < n; i++) {
+      list_value = gst_value_list_get_value (value, i);
+      if (G_VALUE_TYPE (list_value) == G_TYPE_STRING) {
+        const gchar *x = g_value_get_string (list_value);
+
+        if (best_index == -1 || g_str_equal (x, target)) {
+          best_index = i;
+          best = x;
+        }
+      }
+    }
+    if (best_index != -1) {
+      gst_structure_set (structure, field_name, G_TYPE_STRING, best, NULL);
+      return TRUE;
+    }
+    return FALSE;
+  }
+
+  return FALSE;
+}
+
 /**
  * gst_structure_fixate_field_nearest_fraction:
  * @structure: a #GstStructure
@@ -2074,7 +2578,7 @@ gst_structure_fixate_field_boolean (GstStructure * structure,
  * @target_denominator: The denominator of the target value of the fixation
  *
  * Fixates a #GstStructure by changing the given field to the nearest
- * fraction to @target_numerator/@target_denominator that is a subset 
+ * fraction to @target_numerator/@target_denominator that is a subset
  * of the existing field.
  *
  * Returns: TRUE if the structure could be fixated
@@ -2115,46 +2619,555 @@ gst_structure_fixate_field_nearest_fraction (GstStructure * structure,
     const GValue *list_value;
     int i, n;
     const GValue *best = NULL;
-    GValue best_diff = { 0 };
-    GValue cur_diff = { 0 };
-    GValue target = { 0 };
-    gboolean res = FALSE;
+    gdouble target;
+    gdouble cur_diff;
+    gdouble best_diff = G_MAXDOUBLE;
 
-    g_value_init (&best_diff, GST_TYPE_FRACTION);
-    g_value_init (&cur_diff, GST_TYPE_FRACTION);
-    g_value_init (&target, GST_TYPE_FRACTION);
+    target = (gdouble) target_numerator / (gdouble) target_denominator;
 
-    gst_value_set_fraction (&target, target_numerator, target_denominator);
+    GST_DEBUG ("target %g, best %g", target, best_diff);
+
+    best = NULL;
 
     n = gst_value_list_get_size (value);
     for (i = 0; i < n; i++) {
       list_value = gst_value_list_get_value (value, i);
       if (G_VALUE_TYPE (list_value) == GST_TYPE_FRACTION) {
-        if (best == NULL) {
+        gint num, denom;
+        gdouble list_double;
+
+        num = gst_value_get_fraction_numerator (list_value);
+        denom = gst_value_get_fraction_denominator (list_value);
+
+        list_double = ((gdouble) num / (gdouble) denom);
+        cur_diff = target - list_double;
+
+        GST_DEBUG ("curr diff %g, list %g", cur_diff, list_double);
+
+        if (cur_diff < 0)
+          cur_diff = -cur_diff;
+
+        if (!best || cur_diff < best_diff) {
+          GST_DEBUG ("new best %g", list_double);
           best = list_value;
-          gst_value_set_fraction (&best_diff, 0, 1);
-        } else {
-          if (gst_value_compare (list_value, &target) == GST_VALUE_LESS_THAN)
-            gst_value_fraction_subtract (&cur_diff, &target, list_value);
-          else
-            gst_value_fraction_subtract (&cur_diff, list_value, &target);
-
-          if (gst_value_compare (&cur_diff, &best_diff) == GST_VALUE_LESS_THAN) {
-            best = list_value;
-            g_value_copy (&cur_diff, &best_diff);
-          }
+          best_diff = cur_diff;
         }
       }
     }
     if (best != NULL) {
       gst_structure_set_value (structure, field_name, best);
-      res = TRUE;
+      return TRUE;
     }
-    g_value_unset (&best_diff);
-    g_value_unset (&cur_diff);
-    g_value_unset (&target);
-    return res;
   }
 
   return FALSE;
 }
+
+/* our very own version of G_VALUE_LCOPY that allows NULL return locations
+ * (useful for message parsing functions where the return location is user
+ * supplied and the user may pass NULL if the value isn't of interest) */
+#define GST_VALUE_LCOPY(value, var_args, flags, __error, fieldname)           \
+G_STMT_START {                                                                \
+  const GValue *_value = (value);                                             \
+  guint _flags = (flags);                                                     \
+  GType _value_type = G_VALUE_TYPE (_value);                                  \
+  GTypeValueTable *_vtable = g_type_value_table_peek (_value_type);           \
+  gchar *_lcopy_format = _vtable->lcopy_format;                               \
+  GTypeCValue _cvalues[G_VALUE_COLLECT_FORMAT_MAX_LENGTH] = { { 0, }, };      \
+  guint _n_values = 0;                                                        \
+                                                                              \
+  while (*_lcopy_format != '\0') {                                            \
+    g_assert (*_lcopy_format == G_VALUE_COLLECT_POINTER);                     \
+    _cvalues[_n_values++].v_pointer = va_arg ((var_args), gpointer);          \
+    _lcopy_format++;                                                          \
+  }                                                                           \
+  if (_n_values == 2 && !!_cvalues[0].v_pointer != !!_cvalues[1].v_pointer) { \
+    *(__error) = g_strdup_printf ("either all or none of the return "         \
+        "locations for field '%s' need to be NULL", fieldname);               \
+  } else if (_cvalues[0].v_pointer != NULL) {                                 \
+    *(__error) = _vtable->lcopy_value (_value, _n_values, _cvalues, _flags);  \
+  }                                                                           \
+} G_STMT_END
+
+/**
+ * gst_structure_get_valist:
+ * @structure: a #GstStructure
+ * @first_fieldname: the name of the first field to read
+ * @args: variable arguments
+ *
+ * Parses the variable arguments and reads fields from @structure accordingly.
+ * valist-variant of gst_structure_get(). Look at the documentation of
+ * gst_structure_get() for more details.
+ *
+ * Returns: TRUE, or FALSE if there was a problem reading any of the fields
+ *
+ * Since: 0.10.24
+ */
+gboolean
+gst_structure_get_valist (const GstStructure * structure,
+    const char *first_fieldname, va_list args)
+{
+  const char *field_name;
+  GType expected_type = G_TYPE_INVALID;
+
+  g_return_val_if_fail (GST_IS_STRUCTURE (structure), FALSE);
+  g_return_val_if_fail (first_fieldname != NULL, FALSE);
+
+  field_name = first_fieldname;
+  while (field_name) {
+    const GValue *val = NULL;
+    gchar *err = NULL;
+
+    expected_type = va_arg (args, GType);
+
+    val = gst_structure_get_value (structure, field_name);
+
+    if (val == NULL)
+      goto no_such_field;
+
+    if (G_VALUE_TYPE (val) != expected_type)
+      goto wrong_type;
+
+    GST_VALUE_LCOPY (val, args, 0, &err, field_name);
+    if (err) {
+      g_warning ("%s: %s", G_STRFUNC, err);
+      g_free (err);
+      return FALSE;
+    }
+
+    field_name = va_arg (args, const gchar *);
+  }
+
+  return TRUE;
+
+/* ERRORS */
+no_such_field:
+  {
+    GST_WARNING ("Expected field '%s' in structure: %" GST_PTR_FORMAT,
+        field_name, structure);
+    return FALSE;
+  }
+wrong_type:
+  {
+    GST_WARNING ("Expected field '%s' in structure to be of type '%s', but "
+        "field was of type '%s': %" GST_PTR_FORMAT, field_name,
+        GST_STR_NULL (g_type_name (expected_type)),
+        G_VALUE_TYPE_NAME (gst_structure_get_value (structure, field_name)),
+        structure);
+    return FALSE;
+  }
+}
+
+/**
+ * gst_structure_id_get_valist:
+ * @structure: a #GstStructure
+ * @first_field_id: the quark of the first field to read
+ * @args: variable arguments
+ *
+ * Parses the variable arguments and reads fields from @structure accordingly.
+ * valist-variant of gst_structure_id_get(). Look at the documentation of
+ * gst_structure_id_get() for more details.
+ *
+ * Returns: TRUE, or FALSE if there was a problem reading any of the fields
+ *
+ * Since: 0.10.24
+ */
+gboolean
+gst_structure_id_get_valist (const GstStructure * structure,
+    GQuark first_field_id, va_list args)
+{
+  GQuark field_id;
+  GType expected_type = G_TYPE_INVALID;
+
+  g_return_val_if_fail (GST_IS_STRUCTURE (structure), FALSE);
+  g_return_val_if_fail (first_field_id != 0, FALSE);
+
+  field_id = first_field_id;
+  while (field_id) {
+    const GValue *val = NULL;
+    gchar *err = NULL;
+
+    expected_type = va_arg (args, GType);
+
+    val = gst_structure_id_get_value (structure, field_id);
+
+    if (val == NULL)
+      goto no_such_field;
+
+    if (G_VALUE_TYPE (val) != expected_type)
+      goto wrong_type;
+
+    GST_VALUE_LCOPY (val, args, 0, &err, g_quark_to_string (field_id));
+    if (err) {
+      g_warning ("%s: %s", G_STRFUNC, err);
+      g_free (err);
+      return FALSE;
+    }
+
+    field_id = va_arg (args, GQuark);
+  }
+
+  return TRUE;
+
+/* ERRORS */
+no_such_field:
+  {
+    GST_WARNING ("Expected field '%s' in structure: %" GST_PTR_FORMAT,
+        GST_STR_NULL (g_quark_to_string (field_id)), structure);
+    return FALSE;
+  }
+wrong_type:
+  {
+    GST_WARNING ("Expected field '%s' in structure to be of type '%s', but "
+        "field was of type '%s': %" GST_PTR_FORMAT,
+        g_quark_to_string (field_id),
+        GST_STR_NULL (g_type_name (expected_type)),
+        G_VALUE_TYPE_NAME (gst_structure_id_get_value (structure, field_id)),
+        structure);
+    return FALSE;
+  }
+}
+
+/**
+ * gst_structure_get:
+ * @structure: a #GstStructure
+ * @first_fieldname: the name of the first field to read
+ * @...: variable arguments
+ *
+ * Parses the variable arguments and reads fields from @structure accordingly.
+ * Variable arguments should be in the form field name, field type
+ * (as a GType), pointer(s) to a variable(s) to hold the return value(s).
+ * The last variable argument should be NULL.
+ *
+ * For refcounted (mini)objects you will receive a new reference which
+ * you must release with a suitable _unref() when no longer needed. For
+ * strings and boxed types you will receive a copy which you will need to
+ * release with either g_free() or the suitable function for the boxed type.
+ *
+ * Returns: FALSE if there was a problem reading any of the fields (e.g.
+ *     because the field requested did not exist, or was of a type other
+ *     than the type specified), otherwise TRUE.
+ *
+ * Since: 0.10.24
+ */
+gboolean
+gst_structure_get (const GstStructure * structure, const char *first_fieldname,
+    ...)
+{
+  gboolean ret;
+  va_list args;
+
+  g_return_val_if_fail (GST_IS_STRUCTURE (structure), FALSE);
+  g_return_val_if_fail (first_fieldname != NULL, FALSE);
+
+  va_start (args, first_fieldname);
+  ret = gst_structure_get_valist (structure, first_fieldname, args);
+  va_end (args);
+
+  return ret;
+}
+
+/**
+ * gst_structure_id_get:
+ * @structure: a #GstStructure
+ * @first_field_id: the quark of the first field to read
+ * @...: variable arguments
+ *
+ * Parses the variable arguments and reads fields from @structure accordingly.
+ * Variable arguments should be in the form field id quark, field type
+ * (as a GType), pointer(s) to a variable(s) to hold the return value(s).
+ * The last variable argument should be NULL (technically it should be a
+ * 0 quark, but we require NULL so compilers that support it can check for
+ * the NULL terminator and warn if it's not there).
+ *
+ * This function is just like gst_structure_get() only that it is slightly
+ * more efficient since it saves the string-to-quark lookup in the global
+ * quark hashtable.
+ *
+ * For refcounted (mini)objects you will receive a new reference which
+ * you must release with a suitable _unref() when no longer needed. For
+ * strings and boxed types you will receive a copy which you will need to
+ * release with either g_free() or the suitable function for the boxed type.
+ *
+ * Returns: FALSE if there was a problem reading any of the fields (e.g.
+ *     because the field requested did not exist, or was of a type other
+ *     than the type specified), otherwise TRUE.
+ *
+ * Since: 0.10.24
+ */
+gboolean
+gst_structure_id_get (const GstStructure * structure, GQuark first_field_id,
+    ...)
+{
+  gboolean ret;
+  va_list args;
+
+  g_return_val_if_fail (GST_IS_STRUCTURE (structure), FALSE);
+  g_return_val_if_fail (first_field_id != 0, FALSE);
+
+  va_start (args, first_field_id);
+  ret = gst_structure_id_get_valist (structure, first_field_id, args);
+  va_end (args);
+
+  return ret;
+}
+
+static gboolean
+gst_structure_is_equal_foreach (GQuark field_id, const GValue * val2,
+    gpointer data)
+{
+  const GstStructure *struct1 = (const GstStructure *) data;
+  const GValue *val1 = gst_structure_id_get_value (struct1, field_id);
+
+  if (G_UNLIKELY (val1 == NULL))
+    return FALSE;
+  if (gst_value_compare (val1, val2) == GST_VALUE_EQUAL) {
+    return TRUE;
+  }
+
+  return FALSE;
+}
+
+/**
+ * gst_structure_is_equal:
+ * @structure1: a #GstStructure.
+ * @structure2: a #GstStructure.
+ *
+ * Tests if the two #GstStructure are equal.
+ *
+ * Returns: TRUE if the two structures have the same name and field.
+ *
+ * Since: 0.10.36
+ **/
+gboolean
+gst_structure_is_equal (const GstStructure * structure1,
+    const GstStructure * structure2)
+{
+  g_return_val_if_fail (GST_IS_STRUCTURE (structure1), FALSE);
+  g_return_val_if_fail (GST_IS_STRUCTURE (structure2), FALSE);
+
+  if (G_UNLIKELY (structure1 == structure2))
+    return TRUE;
+
+  if (structure1->name != structure2->name) {
+    return FALSE;
+  }
+  if (structure1->fields->len != structure2->fields->len) {
+    return FALSE;
+  }
+
+  return gst_structure_foreach (structure1, gst_structure_is_equal_foreach,
+      (gpointer) structure2);
+}
+
+
+typedef struct
+{
+  GstStructure *dest;
+  const GstStructure *intersect;
+}
+IntersectData;
+
+static gboolean
+gst_structure_intersect_field1 (GQuark id, const GValue * val1, gpointer data)
+{
+  IntersectData *idata = (IntersectData *) data;
+  const GValue *val2 = gst_structure_id_get_value (idata->intersect, id);
+
+  if (G_UNLIKELY (val2 == NULL)) {
+    gst_structure_id_set_value (idata->dest, id, val1);
+  } else {
+    GValue dest_value = { 0 };
+    if (gst_value_intersect (&dest_value, val1, val2)) {
+      gst_structure_id_set_value (idata->dest, id, &dest_value);
+      g_value_unset (&dest_value);
+    } else {
+      return FALSE;
+    }
+  }
+  return TRUE;
+}
+
+static gboolean
+gst_structure_intersect_field2 (GQuark id, const GValue * val1, gpointer data)
+{
+  IntersectData *idata = (IntersectData *) data;
+  const GValue *val2 = gst_structure_id_get_value (idata->intersect, id);
+
+  if (G_UNLIKELY (val2 == NULL)) {
+    gst_structure_id_set_value (idata->dest, id, val1);
+  }
+  return TRUE;
+}
+
+/**
+ * gst_structure_intersect:
+ * @struct1: a #GstStructure
+ * @struct2: a #GstStructure
+ *
+ * Interesects @struct1 and @struct2 and returns the intersection.
+ *
+ * Returns: Intersection of @struct1 and @struct2
+ *
+ * Since: 0.10.36
+ */
+GstStructure *
+gst_structure_intersect (const GstStructure * struct1,
+    const GstStructure * struct2)
+{
+  IntersectData data;
+
+  g_assert (struct1 != NULL);
+  g_assert (struct2 != NULL);
+
+  if (G_UNLIKELY (struct1->name != struct2->name))
+    return NULL;
+
+  /* copy fields from struct1 which we have not in struct2 to target
+   * intersect if we have the field in both */
+  data.dest = gst_structure_id_empty_new (struct1->name);
+  data.intersect = struct2;
+  if (G_UNLIKELY (!gst_structure_foreach ((GstStructure *) struct1,
+              gst_structure_intersect_field1, &data)))
+    goto error;
+
+  /* copy fields from struct2 which we have not in struct1 to target */
+  data.intersect = struct1;
+  if (G_UNLIKELY (!gst_structure_foreach ((GstStructure *) struct2,
+              gst_structure_intersect_field2, &data)))
+    goto error;
+
+  return data.dest;
+
+error:
+  gst_structure_free (data.dest);
+  return NULL;
+}
+
+static gboolean
+gst_caps_structure_can_intersect_field (GQuark id, const GValue * val1,
+    gpointer data)
+{
+  GstStructure *other = (GstStructure *) data;
+  const GValue *val2 = gst_structure_id_get_value (other, id);
+
+  if (G_LIKELY (val2)) {
+    if (!gst_value_can_intersect (val1, val2)) {
+      return FALSE;
+    } else {
+      gint eq = gst_value_compare (val1, val2);
+
+      if (eq == GST_VALUE_UNORDERED) {
+        /* we need to try interseting */
+        if (!gst_value_intersect (NULL, val1, val2)) {
+          return FALSE;
+        }
+      } else if (eq != GST_VALUE_EQUAL) {
+        return FALSE;
+      }
+    }
+  }
+  return TRUE;
+}
+
+/**
+ * gst_structure_can_intersect:
+ * @struct1: a #GstStructure
+ * @struct2: a #GstStructure
+ *
+ * Tries intersecting @struct1 and @struct2 and reports whether the result
+ * would not be empty.
+ *
+ * Returns: %TRUE if intersection would not be empty
+ *
+ * Since: 0.10.36
+ */
+gboolean
+gst_structure_can_intersect (const GstStructure * struct1,
+    const GstStructure * struct2)
+{
+  g_return_val_if_fail (GST_IS_STRUCTURE (struct1), FALSE);
+  g_return_val_if_fail (GST_IS_STRUCTURE (struct2), FALSE);
+
+  if (G_UNLIKELY (struct1->name != struct2->name))
+    return FALSE;
+
+  /* tries to intersect if we have the field in both */
+  return gst_structure_foreach ((GstStructure *) struct1,
+      gst_caps_structure_can_intersect_field, (gpointer) struct2);
+}
+
+static gboolean
+gst_caps_structure_is_subset_field (GQuark field_id, const GValue * value,
+    gpointer user_data)
+{
+  GstStructure *superset = user_data;
+  const GValue *other;
+  int comparison;
+
+  if (!(other = gst_structure_id_get_value (superset, field_id)))
+    /* field is missing in the superset => is subset */
+    return TRUE;
+
+  comparison = gst_value_compare (other, value);
+
+  /* equal values are subset */
+  if (comparison == GST_VALUE_EQUAL)
+    return TRUE;
+
+  /* ordered, but unequal, values are not */
+  if (comparison != GST_VALUE_UNORDERED)
+    return FALSE;
+
+  /*
+   * 1 - [1,2] = empty
+   * -> !subset
+   *
+   * [1,2] - 1 = 2
+   *  -> 1 - [1,2] = empty
+   *  -> subset
+   *
+   * [1,3] - [1,2] = 3
+   * -> [1,2] - [1,3] = empty
+   * -> subset
+   *
+   * {1,2} - {1,3} = 2
+   * -> {1,3} - {1,2} = 3
+   * -> !subset
+   *
+   *  First caps subtraction needs to return a non-empty set, second
+   *  subtractions needs to give en empty set.
+   *  Both substractions are switched below, as it's faster that way.
+   */
+  if (!gst_value_subtract (NULL, value, other)) {
+    if (gst_value_subtract (NULL, other, value)) {
+      return TRUE;
+    }
+  }
+  return FALSE;
+}
+
+/**
+ * gst_structure_is_subset:
+ * @subset: a #GstStructure
+ * @superset: a potentially greater #GstStructure
+ *
+ * Checks if @subset is a subset of @superset, i.e. has the same
+ * structure name and for all fields that are existing in @superset,
+ * @subset has a value that is a subset of the value in @superset.
+ *
+ * Returns: %TRUE if @subset is a subset of @superset
+ *
+ * Since: 0.10.36
+ */
+gboolean
+gst_structure_is_subset (const GstStructure * subset,
+    const GstStructure * superset)
+{
+  if ((superset->name != subset->name) ||
+      (gst_structure_n_fields (superset) > gst_structure_n_fields (subset)))
+    return FALSE;
+
+  return gst_structure_foreach ((GstStructure *) subset,
+      gst_caps_structure_is_subset_field, (gpointer) superset);
+}