diff --git a/gst/gststructure.c b/gst/gststructure.c
index 8a3aa6f7c50169623d4956d7c574655a5eccb1d6..23c54b35f533d823d52fdf3d9e55596b175fb933 100644 (file)
--- a/gst/gststructure.c
+++ b/gst/gststructure.c
*
* In addition to the key/value pairs, a #GstStructure also has a name. The name
* starts with a letter and can be folled by letters, numbers and any of "/-_.:".
- *
+ *
* #GstStructure is used by various GStreamer subsystems to store information
* in a flexible and extensible way. A #GstStructure does not have a refcount
* because it usually is part of a higher level object such as #GstCaps. It
* A #GstStructure can be created with gst_structure_empty_new() or
* gst_structure_new(), which both take a name and an optional set of
* key/value pairs along with the types of the values.
- *
+ *
* Field values can be changed with gst_structure_set_value() or
* gst_structure_set().
*
*
* Creates a new, empty #GstStructure with the given name as a GQuark.
*
- * Returns: a new, empty #GstStructure
+ * Free-function: gst_structure_free
+ *
+ * Returns: (transfer full): a new, empty #GstStructure
*/
GstStructure *
gst_structure_id_empty_new (GQuark quark)
while (*s && (g_ascii_isalnum (*s) || strchr ("/-_.:+ ", *s) != NULL))
s++;
if (G_UNLIKELY (*s != '\0')) {
- GST_WARNING ("Invalid character '%c' at offset %lu in structure name: %s",
- *s, ((gulong) s - (gulong) name), name);
+ GST_WARNING ("Invalid character '%c' at offset %" G_GUINTPTR_FORMAT " in"
+ " structure name: %s", *s, ((guintptr) s - (guintptr) name), name);
return FALSE;
}
*
* See gst_structure_set_name() for constraints on the @name parameter.
*
- * Returns: a new, empty #GstStructure
+ * Free-function: gst_structure_free
+ *
+ * Returns: (transfer full): a new, empty #GstStructure
*/
GstStructure *
gst_structure_empty_new (const gchar * name)
* Variable arguments should be passed as field name, field type,
* and value. Last variable argument should be NULL.
*
- * Returns: a new #GstStructure
+ * Free-function: gst_structure_free
+ *
+ * Returns: (transfer full): a new #GstStructure
*/
GstStructure *
gst_structure_new (const gchar * name, const gchar * firstfield, ...)
GstStructure *structure;
va_list varargs;
- g_return_val_if_fail (name != NULL, NULL);
-
va_start (varargs, firstfield);
structure = gst_structure_new_valist (name, firstfield, varargs);
va_end (varargs);
*
* See gst_structure_set_name() for constraints on the @name parameter.
*
- * Returns: a new #GstStructure
+ * Free-function: gst_structure_free
+ *
+ * Returns: (transfer full): a new #GstStructure
*/
GstStructure *
gst_structure_new_valist (const gchar * name,
{
GstStructure *structure;
- g_return_val_if_fail (name != NULL, NULL);
-
structure = gst_structure_empty_new (name);
if (structure)
/**
* gst_structure_set_parent_refcount:
* @structure: a #GstStructure
- * @refcount: a pointer to the parent's refcount
+ * @refcount: (in): a pointer to the parent's refcount
*
* Sets the parent_refcount field of #GstStructure. This field is used to
* determine whether a structure is mutable or not. This function should only be
*
* Duplicates a #GstStructure and all its fields and values.
*
- * Returns: a new #GstStructure.
+ * Free-function: gst_structure_free
+ *
+ * Returns: (transfer none): a new #GstStructure.
*/
GstStructure *
gst_structure_copy (const GstStructure * structure)
/**
* gst_structure_free:
- * @structure: the #GstStructure to free
+ * @structure: (in) (transfer full): the #GstStructure to free
*
* Frees a #GstStructure and all its fields and values. The structure must not
* have a parent when this function is called.
structure->name = g_quark_from_string (name);
}
+static inline void
+gst_structure_id_set_value_internal (GstStructure * structure, GQuark field,
+ const GValue * value)
+{
+ GstStructureField gsfield = { 0, {0,} };
+
+ gsfield.name = field;
+ gst_value_init_and_copy (&gsfield.value, value);
+
+ gst_structure_set_field (structure, &gsfield);
+}
+
/**
* gst_structure_id_set_value:
* @structure: a #GstStructure
gst_structure_id_set_value (GstStructure * structure,
GQuark field, const GValue * value)
{
- GstStructureField gsfield = { 0, {0,} };
g_return_if_fail (structure != NULL);
g_return_if_fail (G_IS_VALUE (value));
g_return_if_fail (IS_MUTABLE (structure));
- gsfield.name = field;
- gst_value_init_and_copy (&gsfield.value, value);
-
- gst_structure_set_field (structure, &gsfield);
+ gst_structure_id_set_value_internal (structure, field, value);
}
/**
g_return_if_fail (G_IS_VALUE (value));
g_return_if_fail (IS_MUTABLE (structure));
- gst_structure_id_set_value (structure, g_quark_from_string (fieldname),
- value);
+ gst_structure_id_set_value_internal (structure,
+ g_quark_from_string (fieldname), value);
+}
+
+static inline void
+gst_structure_id_take_value_internal (GstStructure * structure, GQuark field,
+ GValue * value)
+{
+ GstStructureField gsfield = { 0, {0,} };
+
+ gsfield.name = field;
+ gsfield.value = *value;
+
+ gst_structure_set_field (structure, &gsfield);
+
+ /* we took ownership */
+#ifdef USE_POISONING
+ memset (value, 0, sizeof (GValue));
+#else
+ value->g_type = G_TYPE_INVALID;
+#endif
+}
+
+/**
+ * gst_structure_id_take_value:
+ * @structure: a #GstStructure
+ * @field: a #GQuark representing a field
+ * @value: (transfer full): the new value of the field
+ *
+ * Sets the field with the given GQuark @field to @value. If the field
+ * does not exist, it is created. If the field exists, the previous
+ * value is replaced and freed.
+ *
+ * Since: 0.10.31
+ */
+void
+gst_structure_id_take_value (GstStructure * structure, GQuark field,
+ GValue * value)
+{
+ g_return_if_fail (structure != NULL);
+ g_return_if_fail (G_IS_VALUE (value));
+ g_return_if_fail (IS_MUTABLE (structure));
+
+ gst_structure_id_take_value_internal (structure, field, value);
+}
+
+/**
+ * gst_structure_take_value:
+ * @structure: a #GstStructure
+ * @fieldname: the name of the field to set
+ * @value: (transfer full): the new value of the field
+ *
+ * Sets the field with the given name @field to @value. If the field
+ * does not exist, it is created. If the field exists, the previous
+ * value is replaced and freed. The function will take ownership of @value.
+ *
+ * Since: 0.10.31
+ */
+void
+gst_structure_take_value (GstStructure * structure, const gchar * fieldname,
+ GValue * value)
+{
+ g_return_if_fail (structure != NULL);
+ g_return_if_fail (fieldname != NULL);
+ g_return_if_fail (G_IS_VALUE (value));
+ g_return_if_fail (IS_MUTABLE (structure));
+
+ gst_structure_id_take_value_internal (structure,
+ g_quark_from_string (fieldname), value);
+}
+
+static void
+gst_structure_set_valist_internal (GstStructure * structure,
+ const gchar * fieldname, va_list varargs)
+{
+ gchar *err = NULL;
+ GType type;
+
+ while (fieldname) {
+ GstStructureField field = { 0 };
+
+ field.name = g_quark_from_string (fieldname);
+
+ type = va_arg (varargs, GType);
+
+ if (G_UNLIKELY (type == G_TYPE_DATE)) {
+ g_warning ("Don't use G_TYPE_DATE, use GST_TYPE_DATE instead\n");
+ type = GST_TYPE_DATE;
+ }
+ G_VALUE_COLLECT_INIT (&field.value, type, varargs, 0, &err);
+ if (G_UNLIKELY (err)) {
+ g_critical ("%s", err);
+ return;
+ }
+ gst_structure_set_field (structure, &field);
+
+ fieldname = va_arg (varargs, gchar *);
+ }
}
/**
va_list varargs;
g_return_if_fail (structure != NULL);
+ g_return_if_fail (IS_MUTABLE (structure) || field == NULL);
va_start (varargs, field);
- gst_structure_set_valist (structure, field, varargs);
+ gst_structure_set_valist_internal (structure, field, varargs);
va_end (varargs);
}
gst_structure_set_valist (GstStructure * structure,
const gchar * fieldname, va_list varargs)
{
- gchar *err = NULL;
- GType type;
-
g_return_if_fail (structure != NULL);
g_return_if_fail (IS_MUTABLE (structure));
+ gst_structure_set_valist_internal (structure, fieldname, varargs);
+}
+
+static void
+gst_structure_id_set_valist_internal (GstStructure * structure,
+ GQuark fieldname, va_list varargs)
+{
+ gchar *err = NULL;
+ GType type;
+
while (fieldname) {
GstStructureField field = { 0 };
- field.name = g_quark_from_string (fieldname);
+ field.name = fieldname;
type = va_arg (varargs, GType);
g_warning ("Don't use G_TYPE_DATE, use GST_TYPE_DATE instead\n");
type = GST_TYPE_DATE;
}
-#if GLIB_CHECK_VERSION(2,23,3)
- G_VALUE_COLLECT_INIT (&field.value, type, varargs, 0, &err);
-#else
+#ifndef G_VALUE_COLLECT_INIT
g_value_init (&field.value, type);
G_VALUE_COLLECT (&field.value, varargs, 0, &err);
+#else
+ G_VALUE_COLLECT_INIT (&field.value, type, varargs, 0, &err);
#endif
if (G_UNLIKELY (err)) {
g_critical ("%s", err);
}
gst_structure_set_field (structure, &field);
- fieldname = va_arg (varargs, gchar *);
+ fieldname = va_arg (varargs, GQuark);
}
}
g_return_if_fail (structure != NULL);
va_start (varargs, field);
- gst_structure_id_set_valist (structure, field, varargs);
+ gst_structure_id_set_valist_internal (structure, field, varargs);
va_end (varargs);
}
gst_structure_id_set_valist (GstStructure * structure,
GQuark fieldname, va_list varargs)
{
- gchar *err = NULL;
- GType type;
-
g_return_if_fail (structure != NULL);
g_return_if_fail (IS_MUTABLE (structure));
- while (fieldname) {
- GstStructureField field = { 0 };
-
- field.name = fieldname;
-
- type = va_arg (varargs, GType);
-
- if (G_UNLIKELY (type == G_TYPE_DATE)) {
- g_warning ("Don't use G_TYPE_DATE, use GST_TYPE_DATE instead\n");
- type = GST_TYPE_DATE;
- }
-#ifndef G_VALUE_COLLECT_INIT
- g_value_init (&field.value, type);
- G_VALUE_COLLECT (&field.value, varargs, 0, &err);
-#else
- G_VALUE_COLLECT_INIT (&field.value, type, varargs, 0, &err);
-#endif
- if (G_UNLIKELY (err)) {
- g_critical ("%s", err);
- return;
- }
- gst_structure_set_field (structure, &field);
-
- fieldname = va_arg (varargs, GQuark);
- }
+ gst_structure_id_set_valist_internal (structure, fieldname, varargs);
}
/**
*
* The last variable argument must be NULL (or 0).
*
- * Returns: a new #GstStructure
+ * Free-function: gst_structure_free
+ *
+ * Returns: (transfer full): a new #GstStructure
*
* Since: 0.10.24
*/
s = gst_structure_id_empty_new (name_quark);
va_start (varargs, field_quark);
- gst_structure_id_set_valist (s, field_quark, varargs);
+ gst_structure_id_set_valist_internal (s, field_quark, varargs);
va_end (varargs);
return s;
g_value_unset (&field->value);
return;
}
+ } else if (G_UNLIKELY (GST_VALUE_HOLDS_DATE (&field->value))) {
+ const GDate *d;
+
+ d = gst_value_get_date (&field->value);
+ /* only check for NULL GDates in taglists, as they might make sense
+ * in other, generic structs */
+ if (G_UNLIKELY ((IS_TAGLIST (structure) && d == NULL))) {
+ GIT_G_WARNING ("Trying to set NULL GDate on field '%s' on taglist. "
+ "Please file a bug.", g_quark_to_string (field->name));
+ g_value_unset (&field->value);
+ return;
+ } else if (G_UNLIKELY (d != NULL && !g_date_valid (d))) {
+ g_warning
+ ("Trying to set invalid GDate on %s field '%s'. Please file a bug.",
+ IS_TAGLIST (structure) ? "taglist" : "structure",
+ g_quark_to_string (field->name));
+ g_value_unset (&field->value);
+ return;
+ }
}
for (i = 0; i < len; i++) {
/**
* gst_structure_foreach:
* @structure: a #GstStructure
- * @func: a function to call for each field
- * @user_data: private data
+ * @func: (scope call): a function to call for each field
+ * @user_data: (closure): private data
*
* Calls the provided function once for each field in the #GstStructure. The
* function must not modify the fields. Also see gst_structure_map_in_place().
/**
* gst_structure_map_in_place:
* @structure: a #GstStructure
- * @func: a function to call for each field
- * @user_data: private data
+ * @func: (scope call): a function to call for each field
+ * @user_data: (closure): private data
*
* Calls the provided function once for each field in the #GstStructure. In
* contrast to gst_structure_foreach(), the function may modify but not delete the
* gst_structure_get_boolean:
* @structure: a #GstStructure
* @fieldname: the name of a field
- * @value: a pointer to a #gboolean to set
+ * @value: (out): a pointer to a #gboolean to set
*
* Sets the boolean pointed to by @value corresponding to the value of the
* given field. Caller is responsible for making sure the field exists
* gst_structure_get_int:
* @structure: a #GstStructure
* @fieldname: the name of a field
- * @value: a pointer to an int to set
+ * @value: (out): a pointer to an int to set
*
* Sets the int pointed to by @value corresponding to the value of the
* given field. Caller is responsible for making sure the field exists
* gst_structure_get_uint:
* @structure: a #GstStructure
* @fieldname: the name of a field
- * @value: a pointer to a uint to set
+ * @value: (out): a pointer to a uint to set
*
* Sets the uint pointed to by @value corresponding to the value of the
* given field. Caller is responsible for making sure the field exists
* gst_structure_get_fourcc:
* @structure: a #GstStructure
* @fieldname: the name of a field
- * @value: a pointer to a 32bit unsigned int to set
+ * @value: (out): a pointer to a 32bit unsigned int to set
*
* Sets the Fourcc pointed to by @value corresponding to the value of the
* given field. Caller is responsible for making sure the field exists
* gst_structure_get_date:
* @structure: a #GstStructure
* @fieldname: the name of a field
- * @value: a pointer to a #GDate to set
+ * @value: (out callee-allocates): a pointer to a #GDate to set
*
* Sets the date pointed to by @value corresponding to the date of the
* given field. Caller is responsible for making sure the field exists
@@ -1309,18 +1421,62 @@ gst_structure_get_date (const GstStructure * structure, const gchar * fieldname,
return TRUE;
}
+/**
+ * gst_structure_get_date_time:
+ * @structure: a #GstStructure
+ * @fieldname: the name of a field
+ * @value: (out callee-allocates): a pointer to a #GstDateTime to set
+ *
+ * Sets the datetime pointed to by @value corresponding to the datetime of the
+ * given field. Caller is responsible for making sure the field exists
+ * and has the correct type.
+ *
+ * On success @value will point to a reference of the datetime which
+ * should be unreffed with gst_date_time_unref() when no longer needed
+ * (note: this is inconsistent with e.g. gst_structure_get_string()
+ * which doesn't return a copy of the string).
+ *
+ * Returns: TRUE if the value could be set correctly. If there was no field
+ * with @fieldname or the existing field did not contain a data, this function
+ * returns FALSE.
+ *
+ * Since: 0.10.31
+ */
+gboolean
+gst_structure_get_date_time (const GstStructure * structure,
+ const gchar * fieldname, GstDateTime ** value)
+{
+ GstStructureField *field;
+
+ g_return_val_if_fail (structure != NULL, FALSE);
+ g_return_val_if_fail (fieldname != NULL, FALSE);
+ g_return_val_if_fail (value != NULL, FALSE);
+
+ field = gst_structure_get_field (structure, fieldname);
+
+ if (field == NULL)
+ return FALSE;
+ if (!GST_VALUE_HOLDS_DATE_TIME (&field->value))
+ return FALSE;
+
+ /* FIXME: 0.11 g_value_dup_boxed() -> g_value_get_boxed() */
+ *value = g_value_dup_boxed (&field->value);
+
+ return TRUE;
+}
+
/**
* gst_structure_get_clock_time:
* @structure: a #GstStructure
* @fieldname: the name of a field
- * @value: a pointer to a #GstClockTime to set
+ * @value: (out): a pointer to a #GstClockTime to set
*
* Sets the clock time pointed to by @value corresponding to the clock time
* of the given field. Caller is responsible for making sure the field exists
* and has the correct type.
*
* Returns: TRUE if the value could be set correctly. If there was no field
- * with @fieldname or the existing field did not contain a #GstClockTime, this
+ * with @fieldname or the existing field did not contain a #GstClockTime, this
* function returns FALSE.
*/
gboolean
* gst_structure_get_double:
* @structure: a #GstStructure
* @fieldname: the name of a field
- * @value: a pointer to a gdouble to set
+ * @value: (out): a pointer to a gdouble to set
*
* Sets the double pointed to by @value corresponding to the value of the
* given field. Caller is responsible for making sure the field exists
* and has the correct type.
*
* Returns: TRUE if the value could be set correctly. If there was no field
- * with @fieldname or the existing field did not contain a double, this
+ * with @fieldname or the existing field did not contain a double, this
* function returns FALSE.
*/
gboolean
* @structure: a #GstStructure
* @fieldname: the name of a field
* @enumtype: the enum type of a field
- * @value: a pointer to an int to set
+ * @value: (out): a pointer to an int to set
*
* Sets the int pointed to by @value corresponding to the value of the
* given field. Caller is responsible for making sure the field exists,
* gst_structure_get_fraction:
* @structure: a #GstStructure
* @fieldname: the name of a field
- * @value_numerator: a pointer to an int to set
- * @value_denominator: a pointer to an int to set
+ * @value_numerator: (out): a pointer to an int to set
+ * @value_denominator: (out): a pointer to an int to set
*
- * Sets the integers pointed to by @value_numerator and @value_denominator
- * corresponding to the value of the given field. Caller is responsible
+ * Sets the integers pointed to by @value_numerator and @value_denominator
+ * corresponding to the value of the given field. Caller is responsible
* for making sure the field exists and has the correct type.
*
* Returns: TRUE if the values could be set correctly. If there was no field
- * with @fieldname or the existing field did not contain a GstFraction, this
+ * with @fieldname or the existing field did not contain a GstFraction, this
* function returns FALSE.
*/
gboolean
{"s", G_TYPE_STRING}
,
{"structure", GST_TYPE_STRUCTURE}
+ ,
+ {"date", GST_TYPE_DATE}
+ ,
+ {"datetime", GST_TYPE_DATE_TIME}
};
_num = G_N_ELEMENTS (dyn_abbrs);
/* permanently allocate and copy the array now */
}
} else if (G_VALUE_TYPE (val) == GST_TYPE_INT_RANGE) {
return G_TYPE_INT;
+ } else if (G_VALUE_TYPE (val) == GST_TYPE_INT64_RANGE) {
+ return G_TYPE_INT64;
} else if (G_VALUE_TYPE (val) == GST_TYPE_DOUBLE_RANGE) {
return G_TYPE_DOUBLE;
} else if (G_VALUE_TYPE (val) == GST_TYPE_FRACTION_RANGE) {
* ]|
* This prints the structure in human readble form.
*
- * Returns: a pointer to string allocated by g_malloc(). g_free() after
- * usage.
+ * Free-function: g_free
+ *
+ * Returns: (transfer full)L a pointer to string allocated by g_malloc().
+ * g_free() after usage.
*/
gchar *
gst_structure_to_string (const GstStructure * structure)
g_value_init (value, range_type);
gst_value_set_int_range (value, gst_g_value_get_int_unchecked (&value1),
gst_g_value_get_int_unchecked (&value2));
+ } else if (G_VALUE_TYPE (&value1) == G_TYPE_INT64) {
+ range_type = GST_TYPE_INT64_RANGE;
+ g_value_init (value, range_type);
+ gst_value_set_int64_range (value, gst_g_value_get_int64_unchecked (&value1),
+ gst_g_value_get_int64_unchecked (&value2));
} else if (G_VALUE_TYPE (&value1) == GST_TYPE_FRACTION) {
range_type = GST_TYPE_FRACTION_RANGE;
g_value_init (value, range_type);
/**
* gst_structure_from_string:
* @string: a string representation of a #GstStructure.
- * @end: pointer to store the end of the string in.
+ * @end: (out) (allow-none): pointer to store the end of the string in.
*
* Creates a #GstStructure from a string representation.
* If end is not NULL, a pointer to the place inside the given string
* where parsing ended will be returned.
*
- * Returns: a new #GstStructure or NULL when the string could not
- * be parsed. Free with gst_structure_free() after use.
+ * Free-function: gst_structure_free
+ *
+ * Returns: (transfer full): a new #GstStructure or NULL when the string could
+ * not be parsed. Free with gst_structure_free() after use.
*/
GstStructure *
gst_structure_from_string (const gchar * string, gchar ** end)
* @target_denominator: The denominator of the target value of the fixation
*
* Fixates a #GstStructure by changing the given field to the nearest
- * fraction to @target_numerator/@target_denominator that is a subset
+ * fraction to @target_numerator/@target_denominator that is a subset
* of the existing field.
*
* Returns: TRUE if the structure could be fixated
* Since: 0.10.24
*/
gboolean
-gst_structure_get_valist (GstStructure * structure,
+gst_structure_get_valist (const GstStructure * structure,
const char *first_fieldname, va_list args)
{
const char *field_name;
* Since: 0.10.24
*/
gboolean
-gst_structure_id_get_valist (GstStructure * structure, GQuark first_field_id,
- va_list args)
+gst_structure_id_get_valist (const GstStructure * structure,
+ GQuark first_field_id, va_list args)
{
GQuark field_id;
GType expected_type = G_TYPE_INVALID;
* (as a GType), pointer(s) to a variable(s) to hold the return value(s).
* The last variable argument should be NULL.
*
- * For refcounted (mini)objects you will acquire your own reference which
+ * For refcounted (mini)objects you will receive a new reference which
* you must release with a suitable _unref() when no longer needed. For
- * strings and boxed types you will acquire a copy which you will need to
- * release with either g_free() or the suiteable function for the boxed type.
+ * strings and boxed types you will receive a copy which you will need to
+ * release with either g_free() or the suitable function for the boxed type.
*
* Returns: FALSE if there was a problem reading any of the fields (e.g.
* because the field requested did not exist, or was of a type other
* Since: 0.10.24
*/
gboolean
-gst_structure_get (GstStructure * structure, const char *first_fieldname, ...)
+gst_structure_get (const GstStructure * structure, const char *first_fieldname,
+ ...)
{
gboolean ret;
va_list args;
@@ -2712,10 +2884,10 @@ gst_structure_get (GstStructure * structure, const char *first_fieldname, ...)
* more efficient since it saves the string-to-quark lookup in the global
* quark hashtable.
*
- * For refcounted (mini)objects you will acquire your own reference which
+ * For refcounted (mini)objects you will receive a new reference which
* you must release with a suitable _unref() when no longer needed. For
- * strings and boxed types you will acquire a copy which you will need to
- * release with either g_free() or the suiteable function for the boxed type.
+ * strings and boxed types you will receive a copy which you will need to
+ * release with either g_free() or the suitable function for the boxed type.
*
* Returns: FALSE if there was a problem reading any of the fields (e.g.
* because the field requested did not exist, or was of a type other
@@ -2724,7 +2896,8 @@ gst_structure_get (GstStructure * structure, const char *first_fieldname, ...)
* Since: 0.10.24
*/
gboolean
-gst_structure_id_get (GstStructure * structure, GQuark first_field_id, ...)
+gst_structure_id_get (const GstStructure * structure, GQuark first_field_id,
+ ...)
{
gboolean ret;
va_list args;
return ret;
}
+
+static gboolean
+gst_structure_is_equal_foreach (GQuark field_id, const GValue * val2,
+ gpointer data)
+{
+ const GstStructure *struct1 = (const GstStructure *) data;
+ const GValue *val1 = gst_structure_id_get_value (struct1, field_id);
+
+ if (G_UNLIKELY (val1 == NULL))
+ return FALSE;
+ if (gst_value_compare (val1, val2) == GST_VALUE_EQUAL) {
+ return TRUE;
+ }
+
+ return FALSE;
+}
+
+/**
+ * gst_structure_is_equal:
+ * @structure1: a #GstStructure.
+ * @structure2: a #GstStructure.
+ *
+ * Tests if the two #GstStructure are equal.
+ *
+ * Returns: TRUE if the two structures have the same name and field.
+ *
+ * Since: 0.10.36
+ **/
+gboolean
+gst_structure_is_equal (const GstStructure * structure1,
+ const GstStructure * structure2)
+{
+ g_return_val_if_fail (GST_IS_STRUCTURE (structure1), FALSE);
+ g_return_val_if_fail (GST_IS_STRUCTURE (structure2), FALSE);
+
+ if (G_UNLIKELY (structure1 == structure2))
+ return TRUE;
+
+ if (structure1->name != structure2->name) {
+ return FALSE;
+ }
+ if (structure1->fields->len != structure2->fields->len) {
+ return FALSE;
+ }
+
+ return gst_structure_foreach (structure1, gst_structure_is_equal_foreach,
+ (gpointer) structure2);
+}
+
+
+typedef struct
+{
+ GstStructure *dest;
+ const GstStructure *intersect;
+}
+IntersectData;
+
+static gboolean
+gst_structure_intersect_field1 (GQuark id, const GValue * val1, gpointer data)
+{
+ IntersectData *idata = (IntersectData *) data;
+ const GValue *val2 = gst_structure_id_get_value (idata->intersect, id);
+
+ if (G_UNLIKELY (val2 == NULL)) {
+ gst_structure_id_set_value (idata->dest, id, val1);
+ } else {
+ GValue dest_value = { 0 };
+ if (gst_value_intersect (&dest_value, val1, val2)) {
+ gst_structure_id_set_value (idata->dest, id, &dest_value);
+ g_value_unset (&dest_value);
+ } else {
+ return FALSE;
+ }
+ }
+ return TRUE;
+}
+
+static gboolean
+gst_structure_intersect_field2 (GQuark id, const GValue * val1, gpointer data)
+{
+ IntersectData *idata = (IntersectData *) data;
+ const GValue *val2 = gst_structure_id_get_value (idata->intersect, id);
+
+ if (G_UNLIKELY (val2 == NULL)) {
+ gst_structure_id_set_value (idata->dest, id, val1);
+ }
+ return TRUE;
+}
+
+/**
+ * gst_structure_intersect:
+ * @struct1: a #GstStructure
+ * @struct2: a #GstStructure
+ *
+ * Interesects @struct1 and @struct2 and returns the intersection.
+ *
+ * Returns: Intersection of @struct1 and @struct2
+ *
+ * Since: 0.10.36
+ */
+GstStructure *
+gst_structure_intersect (const GstStructure * struct1,
+ const GstStructure * struct2)
+{
+ IntersectData data;
+
+ g_assert (struct1 != NULL);
+ g_assert (struct2 != NULL);
+
+ if (G_UNLIKELY (struct1->name != struct2->name))
+ return NULL;
+
+ /* copy fields from struct1 which we have not in struct2 to target
+ * intersect if we have the field in both */
+ data.dest = gst_structure_id_empty_new (struct1->name);
+ data.intersect = struct2;
+ if (G_UNLIKELY (!gst_structure_foreach ((GstStructure *) struct1,
+ gst_structure_intersect_field1, &data)))
+ goto error;
+
+ /* copy fields from struct2 which we have not in struct1 to target */
+ data.intersect = struct1;
+ if (G_UNLIKELY (!gst_structure_foreach ((GstStructure *) struct2,
+ gst_structure_intersect_field2, &data)))
+ goto error;
+
+ return data.dest;
+
+error:
+ gst_structure_free (data.dest);
+ return NULL;
+}
+
+static gboolean
+gst_caps_structure_can_intersect_field (GQuark id, const GValue * val1,
+ gpointer data)
+{
+ GstStructure *other = (GstStructure *) data;
+ const GValue *val2 = gst_structure_id_get_value (other, id);
+
+ if (G_LIKELY (val2)) {
+ if (!gst_value_can_intersect (val1, val2)) {
+ return FALSE;
+ } else {
+ gint eq = gst_value_compare (val1, val2);
+
+ if (eq == GST_VALUE_UNORDERED) {
+ /* we need to try interseting */
+ if (!gst_value_intersect (NULL, val1, val2)) {
+ return FALSE;
+ }
+ } else if (eq != GST_VALUE_EQUAL) {
+ return FALSE;
+ }
+ }
+ }
+ return TRUE;
+}
+
+/**
+ * gst_structure_can_intersect:
+ * @struct1: a #GstStructure
+ * @struct2: a #GstStructure
+ *
+ * Tries intersecting @struct1 and @struct2 and reports whether the result
+ * would not be empty.
+ *
+ * Returns: %TRUE if intersection would not be empty
+ *
+ * Since: 0.10.36
+ */
+gboolean
+gst_structure_can_intersect (const GstStructure * struct1,
+ const GstStructure * struct2)
+{
+ g_return_val_if_fail (GST_IS_STRUCTURE (struct1), FALSE);
+ g_return_val_if_fail (GST_IS_STRUCTURE (struct2), FALSE);
+
+ if (G_UNLIKELY (struct1->name != struct2->name))
+ return FALSE;
+
+ /* tries to intersect if we have the field in both */
+ return gst_structure_foreach ((GstStructure *) struct1,
+ gst_caps_structure_can_intersect_field, (gpointer) struct2);
+}
+
+static gboolean
+gst_caps_structure_is_subset_field (GQuark field_id, const GValue * value,
+ gpointer user_data)
+{
+ GstStructure *superset = user_data;
+ const GValue *other;
+ int comparison;
+
+ if (!(other = gst_structure_id_get_value (superset, field_id)))
+ /* field is missing in the superset => is subset */
+ return TRUE;
+
+ comparison = gst_value_compare (other, value);
+
+ /* equal values are subset */
+ if (comparison == GST_VALUE_EQUAL)
+ return TRUE;
+
+ /* ordered, but unequal, values are not */
+ if (comparison != GST_VALUE_UNORDERED)
+ return FALSE;
+
+ /*
+ * 1 - [1,2] = empty
+ * -> !subset
+ *
+ * [1,2] - 1 = 2
+ * -> 1 - [1,2] = empty
+ * -> subset
+ *
+ * [1,3] - [1,2] = 3
+ * -> [1,2] - [1,3] = empty
+ * -> subset
+ *
+ * {1,2} - {1,3} = 2
+ * -> {1,3} - {1,2} = 3
+ * -> !subset
+ *
+ * First caps subtraction needs to return a non-empty set, second
+ * subtractions needs to give en empty set.
+ * Both substractions are switched below, as it's faster that way.
+ */
+ if (!gst_value_subtract (NULL, value, other)) {
+ if (gst_value_subtract (NULL, other, value)) {
+ return TRUE;
+ }
+ }
+ return FALSE;
+}
+
+/**
+ * gst_structure_is_subset:
+ * @subset: a #GstStructure
+ * @superset: a potentially greater #GstStructure
+ *
+ * Checks if @subset is a subset of @superset, i.e. has the same
+ * structure name and for all fields that are existing in @superset,
+ * @subset has a value that is a subset of the value in @superset.
+ *
+ * Returns: %TRUE if @subset is a subset of @superset
+ *
+ * Since: 0.10.36
+ */
+gboolean
+gst_structure_is_subset (const GstStructure * subset,
+ const GstStructure * superset)
+{
+ if ((superset->name != subset->name) ||
+ (gst_structure_n_fields (superset) > gst_structure_n_fields (subset)))
+ return FALSE;
+
+ return gst_structure_foreach ((GstStructure *) subset,
+ gst_caps_structure_is_subset_field, (gpointer) superset);
+}