]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/gstreamer0-10.git/blobdiff - gst/gstsystemclock.c
g_thread_create() is deprecated in GLib master, use g_thread_try_new() instead
[glsdk/gstreamer0-10.git] / gst / gstsystemclock.c
index 6b31bab0d1b8e2f76ac72d0525d50f5caf075895..2c71489cfa2bbd20b19847e900bebc10c56b8d23 100644 (file)
@@ -44,6 +44,7 @@
 #include "gstenumtypes.h"
 #include "gstpoll.h"
 #include "gstutils.h"
+#include "glib-compat-private.h"
 
 #include <errno.h>
 
 #  define WIN32_LEAN_AND_MEAN   /* prevents from including too many things */
 #  include <windows.h>          /* QueryPerformance* stuff */
 #  undef WIN32_LEAN_AND_MEAN
+#  define EWOULDBLOCK EAGAIN    /* This is just to placate gcc */
 #endif /* G_OS_WIN32 */
 
+#define GET_ENTRY_STATUS(e)          ((GstClockReturn) g_atomic_int_get(&GST_CLOCK_ENTRY_STATUS(e)))
+#define SET_ENTRY_STATUS(e,val)      (g_atomic_int_set(&GST_CLOCK_ENTRY_STATUS(e),(val)))
+#define CAS_ENTRY_STATUS(e,old,val)  (G_ATOMIC_INT_COMPARE_AND_EXCHANGE(\
+                                       (&GST_CLOCK_ENTRY_STATUS(e)), (old), (val)))
+
 /* Define this to get some extra debug about jitter from each clock_wait */
 #undef WAIT_DEBUGGING
 
@@ -142,7 +149,8 @@ gst_system_clock_class_init (GstSystemClockClass * klass)
   g_object_class_install_property (gobject_class, PROP_CLOCK_TYPE,
       g_param_spec_enum ("clock-type", "Clock type",
           "The type of underlying clock implementation used",
-          GST_TYPE_CLOCK_TYPE, DEFAULT_CLOCK_TYPE, G_PARAM_READWRITE));
+          GST_TYPE_CLOCK_TYPE, DEFAULT_CLOCK_TYPE,
+          G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
 
   gstclock_class->get_internal_time = gst_system_clock_get_internal_time;
   gstclock_class->get_resolution = gst_system_clock_get_resolution;
@@ -196,7 +204,7 @@ gst_system_clock_dispose (GObject * object)
     GstClockEntry *entry = (GstClockEntry *) entries->data;
 
     GST_CAT_DEBUG (GST_CAT_CLOCK, "unscheduling entry %p", entry);
-    entry->status = GST_CLOCK_UNSCHEDULED;
+    SET_ENTRY_STATUS (entry, GST_CLOCK_UNSCHEDULED);
   }
   GST_CLOCK_BROADCAST (clock);
   gst_system_clock_add_wakeup (sysclock);
@@ -229,7 +237,7 @@ gst_system_clock_set_property (GObject * object, guint prop_id,
 
   switch (prop_id) {
     case PROP_CLOCK_TYPE:
-      sysclock->priv->clock_type = g_value_get_enum (value);
+      sysclock->priv->clock_type = (GstClockType) g_value_get_enum (value);
       GST_CAT_DEBUG (GST_CAT_CLOCK, "clock-type set to %d",
           sysclock->priv->clock_type);
       break;
@@ -262,7 +270,7 @@ gst_system_clock_get_property (GObject * object, guint prop_id, GValue * value,
  * clock will be increased so you need to unref the clock after
  * usage.
  *
- * Returns: the default clock.
+ * Returns: (transfer full): the default clock.
  *
  * MT safe.
  */
@@ -320,9 +328,16 @@ gst_system_clock_add_wakeup (GstSystemClock * sysclock)
   if (sysclock->priv->wakeup_count == 0) {
     GST_CAT_DEBUG (GST_CAT_CLOCK, "writing control");
     while (!gst_poll_write_control (sysclock->priv->timer)) {
-      g_warning
-          ("gstsystemclock: write control failed in wakeup_async, trying again : %d:%s\n",
-          errno, g_strerror (errno));
+      if (errno == EAGAIN || errno == EWOULDBLOCK || errno == EINTR) {
+        g_warning
+            ("gstsystemclock: write control failed in wakeup_async, trying again: %d:%s\n",
+            errno, g_strerror (errno));
+      } else {
+        g_critical
+            ("gstsystemclock: write control failed in wakeup_async: %d:%s\n",
+            errno, g_strerror (errno));
+        return;
+      }
     }
   }
   sysclock->priv->wakeup_count++;
@@ -386,11 +401,7 @@ gst_system_clock_async_thread (GstClock * clock)
 
     /* pick the next entry */
     entry = clock->entries->data;
-    /* if it was unscheduled, just move on to the next entry */
-    if (entry->status == GST_CLOCK_UNSCHEDULED) {
-      GST_CAT_DEBUG (GST_CAT_CLOCK, "entry %p was unscheduled", entry);
-      goto next_entry;
-    }
+    GST_OBJECT_UNLOCK (clock);
 
     requested = entry->time;
 
@@ -399,6 +410,8 @@ gst_system_clock_async_thread (GstClock * clock)
         gst_system_clock_id_wait_jitter_unlocked (clock, (GstClockID) entry,
         NULL, FALSE);
 
+    GST_OBJECT_LOCK (clock);
+
     switch (res) {
       case GST_CLOCK_UNSCHEDULED:
         /* entry was unscheduled, move to the next */
@@ -441,7 +454,7 @@ gst_system_clock_async_thread (GstClock * clock)
         /* we set the entry back to the OK state. This is needed so that the
          * _unschedule() code can see if an entry is currently being waited
          * on (when its state is BUSY). */
-        entry->status = GST_CLOCK_OK;
+        SET_ENTRY_STATUS (entry, GST_CLOCK_OK);
         continue;
       default:
         GST_CAT_DEBUG (GST_CAT_CLOCK,
@@ -548,18 +561,16 @@ gst_system_clock_get_resolution (GstClock * clock)
 
 /* synchronously wait on the given GstClockEntry.
  *
- * We do this by blocking on the global clock GCond variable with
- * the requested time as a timeout. This allows us to unblock the
- * entry by signaling the GCond variable.
+ * We do this by blocking on the global GstPoll timer with
+ * the requested timeout. This allows us to unblock the
+ * entry by writing on the control fd.
  *
- * Note that signaling the global GCond unlocks all waiting entries. So
+ * Note that writing the global GstPoll unlocks all waiting entries. So
  * we need to check if an unlocked entry has changed when it unlocks.
  *
  * Entries that arrive too late are simply not waited on and a
  * GST_CLOCK_EARLY result is returned.
  *
- * should be called with LOCK held.
- *
  * MT safe.
  */
 static GstClockReturn
@@ -567,78 +578,95 @@ gst_system_clock_id_wait_jitter_unlocked (GstClock * clock,
     GstClockEntry * entry, GstClockTimeDiff * jitter, gboolean restart)
 {
   GstSystemClock *sysclock = GST_SYSTEM_CLOCK_CAST (clock);
-  GstClockTime entryt, real, now;
+  GstClockTime entryt, now;
   GstClockTimeDiff diff;
+  GstClockReturn status;
+
+  if (G_UNLIKELY (GET_ENTRY_STATUS (entry) == GST_CLOCK_UNSCHEDULED))
+    return GST_CLOCK_UNSCHEDULED;
 
   /* need to call the overridden method because we want to sync against the time
    * of the clock, whatever the subclass uses as a clock. */
-  real = GST_CLOCK_GET_CLASS (clock)->get_internal_time (clock);
-  now = gst_clock_adjust_unlocked (clock, real);
+  now = gst_clock_get_time (clock);
 
   /* get the time of the entry */
   entryt = GST_CLOCK_ENTRY_TIME (entry);
 
-  if (jitter) {
-    *jitter = GST_CLOCK_DIFF (entryt, now);
-  }
   /* the diff of the entry with the clock is the amount of time we have to
    * wait */
-  diff = entryt - now;
+  diff = GST_CLOCK_DIFF (now, entryt);
+  if (G_LIKELY (jitter))
+    *jitter = -diff;
 
   GST_CAT_DEBUG (GST_CAT_CLOCK, "entry %p"
       " time %" GST_TIME_FORMAT
       " now %" GST_TIME_FORMAT
-      " real %" GST_TIME_FORMAT
       " diff (time-now) %" G_GINT64_FORMAT,
-      entry,
-      GST_TIME_ARGS (entryt), GST_TIME_ARGS (now), GST_TIME_ARGS (real), diff);
+      entry, GST_TIME_ARGS (entryt), GST_TIME_ARGS (now), diff);
 
-  if (diff > 0) {
+  if (G_LIKELY (diff > 0)) {
 #ifdef WAIT_DEBUGGING
     GstClockTime final;
 #endif
 
-    while (entry->status != GST_CLOCK_UNSCHEDULED) {
+    while (TRUE) {
       gint pollret;
 
-      /* mark the entry as busy */
-      entry->status = GST_CLOCK_BUSY;
-      GST_OBJECT_UNLOCK (clock);
+      do {
+        status = GET_ENTRY_STATUS (entry);
 
-      /* now wait on the entry, it either times out or the fd is written. */
+        /* stop when we are unscheduled */
+        if (G_UNLIKELY (status == GST_CLOCK_UNSCHEDULED))
+          goto done;
+
+        /* mark the entry as busy but watch out for intermediate unscheduled
+         * statuses */
+      } while (G_UNLIKELY (!CAS_ENTRY_STATUS (entry, status, GST_CLOCK_BUSY)));
+
+      /* now wait on the entry, it either times out or the fd is written. The
+       * status of the entry is only BUSY around the poll. */
       pollret = gst_poll_wait (sysclock->priv->timer, diff);
 
-      /* another thread can read the fd before we get the lock */
-      GST_OBJECT_LOCK (clock);
-      if (entry->status == GST_CLOCK_UNSCHEDULED) {
-        GST_CAT_DEBUG (GST_CAT_CLOCK, "entry %p unlocked", entry);
-        gst_system_clock_remove_wakeup (sysclock);
+      /* get the new status, mark as DONE. We do this so that the unschedule
+       * function knows when we left the poll and doesn't need to wakeup the
+       * poll anymore. */
+      do {
+        status = GET_ENTRY_STATUS (entry);
+        /* we were unscheduled, exit immediately */
+        if (G_UNLIKELY (status == GST_CLOCK_UNSCHEDULED))
+          break;
+      } while (G_UNLIKELY (!CAS_ENTRY_STATUS (entry, status, GST_CLOCK_DONE)));
+
+      GST_CAT_DEBUG (GST_CAT_CLOCK, "entry %p unlocked, status %d, ret %d",
+          entry, status, pollret);
+
+      if (G_UNLIKELY (status == GST_CLOCK_UNSCHEDULED)) {
+        /* try to clean up The unschedule function managed to set the status to
+         * unscheduled. We now take the lock and mark the entry as unscheduled.
+         * This makes sure that the unschedule function doesn't perform a
+         * wakeup anymore. If the unschedule function has a change to perform
+         * the wakeup before us, we clean up here */
+        GST_OBJECT_LOCK (sysclock);
+        entry->unscheduled = TRUE;
+        if (entry->woken_up) {
+          gst_system_clock_remove_wakeup (sysclock);
+        }
+        GST_OBJECT_UNLOCK (sysclock);
+        goto done;
       } else {
-        if (pollret != 0) {
+        if (G_UNLIKELY (pollret != 0)) {
           /* some other id got unlocked */
           if (!restart) {
             /* this can happen if the entry got unlocked because of an async
              * entry was added to the head of the async queue. */
             GST_CAT_DEBUG (GST_CAT_CLOCK, "wakeup waiting for entry %p", entry);
-            break;
+            goto done;
           }
 
-          /* mark ourselves as EARLY, we release the lock and we could be
-           * unscheduled ourselves but we don't want the unscheduling thread
-           * to write on the control socket (it does that when an entry has a
-           * BUSY status). */
-          entry->status = GST_CLOCK_EARLY;
-
           /* wait till all the entries got woken up */
+          GST_OBJECT_LOCK (sysclock);
           gst_system_clock_wait_wakeup (sysclock);
-
-          /* we released the lock in the wait, recheck our status, we don't need
-           * to remove the wakeup count because we marked the entry as EARLY
-           * before releasing the object lock. */
-          if (entry->status == GST_CLOCK_UNSCHEDULED) {
-            GST_CAT_DEBUG (GST_CAT_CLOCK, "entry %p got unscheduled", entry);
-            break;
-          }
+          GST_OBJECT_UNLOCK (sysclock);
 
           GST_CAT_DEBUG (GST_CAT_CLOCK, "entry %p needs to be restarted",
               entry);
@@ -649,13 +677,13 @@ gst_system_clock_id_wait_jitter_unlocked (GstClock * clock,
 
         /* reschedule if gst_poll_wait returned early or we have to reschedule after
          * an unlock*/
-        real = GST_CLOCK_GET_CLASS (clock)->get_internal_time (clock);
-        now = gst_clock_adjust_unlocked (clock, real);
-        diff = entryt - now;
+        now = gst_clock_get_time (clock);
+        diff = GST_CLOCK_DIFF (now, entryt);
 
         if (diff <= 0) {
           /* timeout, this is fine, we can report success now */
-          entry->status = GST_CLOCK_OK;
+          status = GST_CLOCK_OK;
+          SET_ENTRY_STATUS (entry, status);
 
           GST_CAT_DEBUG (GST_CAT_CLOCK,
               "entry %p finished, diff %" G_GINT64_FORMAT, entry, diff);
@@ -670,42 +698,31 @@ gst_system_clock_id_wait_jitter_unlocked (GstClock * clock,
               (final - target),
               ((double) (GstClockTimeDiff) (final - target)) / GST_SECOND);
 #endif
-          break;
+          goto done;
         } else {
           GST_CAT_DEBUG (GST_CAT_CLOCK,
               "entry %p restart, diff %" G_GINT64_FORMAT, entry, diff);
         }
       }
     }
-  } else if (diff == 0) {
-    entry->status = GST_CLOCK_OK;
   } else {
-    entry->status = GST_CLOCK_EARLY;
+    /* we are right on time or too late */
+    if (G_UNLIKELY (diff == 0))
+      status = GST_CLOCK_OK;
+    else
+      status = GST_CLOCK_EARLY;
+
+    SET_ENTRY_STATUS (entry, status);
   }
-  return entry->status;
+done:
+  return status;
 }
 
 static GstClockReturn
 gst_system_clock_id_wait_jitter (GstClock * clock, GstClockEntry * entry,
     GstClockTimeDiff * jitter)
 {
-  GstClockReturn ret;
-
-  GST_OBJECT_LOCK (clock);
-  if (G_UNLIKELY (entry->status == GST_CLOCK_UNSCHEDULED))
-    goto was_unscheduled;
-
-  ret = gst_system_clock_id_wait_jitter_unlocked (clock, entry, jitter, TRUE);
-  GST_OBJECT_UNLOCK (clock);
-
-  return ret;
-
-  /* ERRORS */
-was_unscheduled:
-  {
-    GST_OBJECT_UNLOCK (clock);
-    return GST_CLOCK_UNSCHEDULED;
-  }
+  return gst_system_clock_id_wait_jitter_unlocked (clock, entry, jitter, TRUE);
 }
 
 /* Start the async clock thread. Must be called with the object lock
@@ -718,8 +735,14 @@ gst_system_clock_start_async (GstSystemClock * clock)
   if (G_LIKELY (clock->thread != NULL))
     return TRUE;                /* Thread already running. Nothing to do */
 
+#if !GLIB_CHECK_VERSION (2, 31, 0)
   clock->thread = g_thread_create ((GThreadFunc) gst_system_clock_async_thread,
       clock, TRUE, &error);
+#else
+  clock->thread = g_thread_try_new ("GstSystemClock",
+      (GThreadFunc) gst_system_clock_async_thread, clock, &error);
+#endif
+
   if (G_UNLIKELY (error))
     goto no_thread;
 
@@ -759,7 +782,7 @@ gst_system_clock_id_wait_async (GstClock * clock, GstClockEntry * entry)
   if (G_UNLIKELY (!gst_system_clock_start_async (sysclock)))
     goto thread_error;
 
-  if (G_UNLIKELY (entry->status == GST_CLOCK_UNSCHEDULED))
+  if (G_UNLIKELY (GET_ENTRY_STATUS (entry) == GST_CLOCK_UNSCHEDULED))
     goto was_unscheduled;
 
   if (clock->entries)
@@ -777,14 +800,20 @@ gst_system_clock_id_wait_async (GstClock * clock, GstClockEntry * entry)
    * front, else the thread is just waiting for another entry and
    * will get to this entry automatically. */
   if (clock->entries->data == entry) {
-    GST_CAT_DEBUG (GST_CAT_CLOCK, "async entry added to head");
+    GST_CAT_DEBUG (GST_CAT_CLOCK, "async entry added to head %p", head);
     if (head == NULL) {
       /* the list was empty before, signal the cond so that the async thread can
        * start taking a look at the queue */
       GST_CAT_DEBUG (GST_CAT_CLOCK, "first entry, sending signal");
       GST_CLOCK_BROADCAST (clock);
     } else {
-      if (head->status == GST_CLOCK_BUSY) {
+      GstClockReturn status;
+
+      status = GET_ENTRY_STATUS (head);
+      GST_CAT_DEBUG (GST_CAT_CLOCK, "head entry %p status %d", head, status);
+
+      if (status == GST_CLOCK_BUSY) {
+        GST_CAT_DEBUG (GST_CAT_CLOCK, "head entry is busy");
         /* the async thread was waiting for an entry, unlock the wait so that it
          * looks at the new head entry instead, we only need to do this once */
         if (!sysclock->priv->async_wakeup) {
@@ -824,21 +853,29 @@ static void
 gst_system_clock_id_unschedule (GstClock * clock, GstClockEntry * entry)
 {
   GstSystemClock *sysclock;
+  GstClockReturn status;
 
   sysclock = GST_SYSTEM_CLOCK_CAST (clock);
 
   GST_CAT_DEBUG (GST_CAT_CLOCK, "unscheduling entry %p", entry);
 
   GST_OBJECT_LOCK (clock);
-  if (entry->status == GST_CLOCK_BUSY) {
+  /* change the entry status to unscheduled */
+  do {
+    status = GET_ENTRY_STATUS (entry);
+  } while (G_UNLIKELY (!CAS_ENTRY_STATUS (entry, status,
+              GST_CLOCK_UNSCHEDULED)));
+
+  if (G_LIKELY (status == GST_CLOCK_BUSY)) {
     /* the entry was being busy, wake up all entries so that they recheck their
      * status. We cannot wake up just one entry because allocating such a
      * datastructure for each entry would be too heavy and unlocking an entry
      * is usually done when shutting down or some other exceptional case. */
     GST_CAT_DEBUG (GST_CAT_CLOCK, "entry was BUSY, doing wakeup");
-    gst_system_clock_add_wakeup (sysclock);
+    if (!entry->unscheduled && !entry->woken_up) {
+      gst_system_clock_add_wakeup (sysclock);
+      entry->woken_up = TRUE;
+    }
   }
-  /* when it leaves the poll, it'll detect the unscheduled */
-  entry->status = GST_CLOCK_UNSCHEDULED;
   GST_OBJECT_UNLOCK (clock);
 }