]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/gstreamer0-10.git/blobdiff - libs/gst/check/gstcheck.c
DEBIAN: Debianization
[glsdk/gstreamer0-10.git] / libs / gst / check / gstcheck.c
index a18ad57ee552ec930278fe20059c5d74b2daeb46..c4370a3ae9101431fef23f7d471b338842d83079 100644 (file)
@@ -2,7 +2,8 @@
  *
  * Common code for GStreamer unittests
  *
- * Copyright (C) <2004> Thomas Vander Stichele <thomas at apestaart dot org>
+ * Copyright (C) 2004,2006 Thomas Vander Stichele <thomas at apestaart dot org>
+ * Copyright (C) 2008 Thijs Vermeir <thijsvermeir@gmail.com>
  *
  * This library is free software; you can redistribute it and/or
  * modify it under the terms of the GNU Library General Public
@@ -43,12 +44,17 @@ GMutex *mutex;
 GCond *start_cond;              /* used to notify main thread of thread startups */
 GCond *sync_cond;               /* used to synchronize all threads and main thread */
 
+GList *buffers = NULL;
+GMutex *check_mutex = NULL;
+GCond *check_cond = NULL;
+
+/* FIXME 0.11: shouldn't _gst_check_debug be static? Not used anywhere */
 gboolean _gst_check_debug = FALSE;
 gboolean _gst_check_raised_critical = FALSE;
 gboolean _gst_check_raised_warning = FALSE;
 gboolean _gst_check_expecting_log = FALSE;
 
-void gst_check_log_message_func
+static void gst_check_log_message_func
     (const gchar * log_domain, GLogLevelFlags log_level,
     const gchar * message, gpointer user_data)
 {
@@ -57,7 +63,7 @@ void gst_check_log_message_func
   }
 }
 
-void gst_check_log_critical_func
+static void gst_check_log_critical_func
     (const gchar * log_domain, GLogLevelFlags log_level,
     const gchar * message, gpointer user_data)
 {
@@ -76,6 +82,35 @@ void gst_check_log_critical_func
     _gst_check_raised_warning = TRUE;
 }
 
+static gint
+sort_plugins (GstPlugin * a, GstPlugin * b)
+{
+  int ret;
+
+  ret = strcmp (gst_plugin_get_source (a), gst_plugin_get_source (b));
+  if (ret == 0)
+    ret = strcmp (gst_plugin_get_name (a), gst_plugin_get_name (b));
+  return ret;
+}
+
+static void
+print_plugins (void)
+{
+  GList *plugins, *l;
+
+  plugins = gst_default_registry_get_plugin_list ();
+  plugins = g_list_sort (plugins, (GCompareFunc) sort_plugins);
+  for (l = plugins; l != NULL; l = l->next) {
+    GstPlugin *plugin = GST_PLUGIN (l->data);
+
+    if (strcmp (gst_plugin_get_source (plugin), "BLACKLIST") != 0) {
+      GST_LOG ("%20s@%s", gst_plugin_get_name (plugin),
+          GST_STR_NULL (gst_plugin_get_filename (plugin)));
+    }
+  }
+  gst_plugin_list_free (plugins);
+}
+
 /* initialize GStreamer testing */
 void
 gst_check_init (int *argc, char **argv[])
@@ -95,6 +130,10 @@ gst_check_init (int *argc, char **argv[])
       gst_check_log_critical_func, NULL);
   g_log_set_handler ("GLib-GObject", G_LOG_LEVEL_CRITICAL | G_LOG_LEVEL_WARNING,
       gst_check_log_critical_func, NULL);
+  g_log_set_handler ("Gst-Phonon", G_LOG_LEVEL_CRITICAL | G_LOG_LEVEL_WARNING,
+      gst_check_log_critical_func, NULL);
+
+  print_plugins ();
 
   check_cond = g_cond_new ();
   check_mutex = g_mutex_new ();
@@ -108,7 +147,10 @@ gst_check_message_error (GstMessage * message, GstMessageType type,
   GError *error;
   gchar *debug;
 
-  fail_unless_equals_int (GST_MESSAGE_TYPE (message), type);
+  fail_unless (GST_MESSAGE_TYPE (message) == type,
+      "message is of type %s instead of expected type %s",
+      gst_message_type_get_name (GST_MESSAGE_TYPE (message)),
+      gst_message_type_get_name (type));
   gst_message_parse_error (message, &error, &debug);
   fail_unless_equals_int (error->domain, domain);
   fail_unless_equals_int (error->code, code);
@@ -139,7 +181,7 @@ gst_check_setup_element (const gchar * factory)
   GST_DEBUG ("setup_element");
 
   element = gst_element_factory_make (factory, factory);
-  fail_if (element == NULL, "Could not create a %s", factory);
+  fail_if (element == NULL, "Could not create a '%s' element", factory);
   ASSERT_OBJECT_REFCOUNT (element, factory, 1);
   return element;
 }
@@ -159,22 +201,34 @@ gst_check_teardown_element (GstElement * element)
  */
 GstPad *
 gst_check_setup_src_pad (GstElement * element,
-    GstStaticPadTemplate * template, GstCaps * caps)
+    GstStaticPadTemplate * tmpl, GstCaps * caps)
+{
+  GstPad *srcpad;
+
+  srcpad = gst_check_setup_src_pad_by_name (element, tmpl, "sink");
+  if (caps)
+    fail_unless (gst_pad_set_caps (srcpad, caps), "could not set caps on pad");
+  return srcpad;
+}
+
+GstPad *
+gst_check_setup_src_pad_by_name (GstElement * element,
+    GstStaticPadTemplate * tmpl, const gchar * name)
 {
   GstPad *srcpad, *sinkpad;
 
   /* sending pad */
-  srcpad = gst_pad_new_from_static_template (template, "src");
+  srcpad = gst_pad_new_from_static_template (tmpl, "src");
   GST_DEBUG_OBJECT (element, "setting up sending pad %p", srcpad);
   fail_if (srcpad == NULL, "Could not create a srcpad");
   ASSERT_OBJECT_REFCOUNT (srcpad, "srcpad", 1);
 
-  sinkpad = gst_element_get_pad (element, "sink");
+  sinkpad = gst_element_get_static_pad (element, name);
+  if (sinkpad == NULL)
+    sinkpad = gst_element_get_request_pad (element, name);
   fail_if (sinkpad == NULL, "Could not get sink pad from %s",
       GST_ELEMENT_NAME (element));
   ASSERT_OBJECT_REFCOUNT (sinkpad, "sinkpad", 2);
-  if (caps)
-    fail_unless (gst_pad_set_caps (srcpad, caps));
   fail_unless (gst_pad_link (srcpad, sinkpad) == GST_PAD_LINK_OK,
       "Could not link source and %s sink pads", GST_ELEMENT_NAME (element));
   gst_object_unref (sinkpad);   /* because we got it higher up */
@@ -184,49 +238,77 @@ gst_check_setup_src_pad (GstElement * element,
 }
 
 void
-gst_check_teardown_src_pad (GstElement * element)
+gst_check_teardown_pad_by_name (GstElement * element, const gchar * name)
 {
-  GstPad *srcpad, *sinkpad;
+  GstPad *pad_peer, *pad_element;
 
   /* clean up floating src pad */
-  sinkpad = gst_element_get_pad (element, "sink");
-  ASSERT_OBJECT_REFCOUNT (sinkpad, "sinkpad", 2);
-  srcpad = gst_pad_get_peer (sinkpad);
-
-  gst_pad_unlink (srcpad, sinkpad);
-
-  /* caps could have been set, make sure they get unset */
-  gst_pad_set_caps (srcpad, NULL);
+  pad_element = gst_element_get_static_pad (element, name);
+  /* We don't check the refcount here since there *might* be
+   * a pad cache holding an extra reference on pad_element.
+   * To get to a state where no pad cache will exist,
+   * we first unlink that pad. */
+  pad_peer = gst_pad_get_peer (pad_element);
+
+  if (pad_peer) {
+    if (gst_pad_get_direction (pad_element) == GST_PAD_SINK)
+      gst_pad_unlink (pad_peer, pad_element);
+    else
+      gst_pad_unlink (pad_element, pad_peer);
+
+    /* caps could have been set, make sure they get unset */
+    gst_pad_set_caps (pad_peer, NULL);
+  }
 
   /* pad refs held by both creator and this function (through _get) */
-  ASSERT_OBJECT_REFCOUNT (sinkpad, "element sinkpad", 2);
-  gst_object_unref (sinkpad);
+  ASSERT_OBJECT_REFCOUNT (pad_element, "element pad_element", 2);
+  gst_object_unref (pad_element);
   /* one more ref is held by element itself */
 
-  /* pad refs held by both creator and this function (through _get_peer) */
-  ASSERT_OBJECT_REFCOUNT (srcpad, "check srcpad", 2);
-  gst_object_unref (srcpad);
-  gst_object_unref (srcpad);
+  if (pad_peer) {
+    /* pad refs held by both creator and this function (through _get_peer) */
+    ASSERT_OBJECT_REFCOUNT (pad_peer, "check pad_peer", 2);
+    gst_object_unref (pad_peer);
+    gst_object_unref (pad_peer);
+  }
+}
+
+void
+gst_check_teardown_src_pad (GstElement * element)
+{
+  gst_check_teardown_pad_by_name (element, "sink");
 }
 
 /* FIXME: set_caps isn't that useful; might want to check if fixed,
  * then use set_use_fixed or somesuch */
 GstPad *
-gst_check_setup_sink_pad (GstElement * element, GstStaticPadTemplate * template,
+gst_check_setup_sink_pad (GstElement * element, GstStaticPadTemplate * tmpl,
     GstCaps * caps)
+{
+  GstPad *sinkpad;
+
+  sinkpad = gst_check_setup_sink_pad_by_name (element, tmpl, "src");
+  if (caps)
+    fail_unless (gst_pad_set_caps (sinkpad, caps), "Could not set pad caps");
+  return sinkpad;
+}
+
+GstPad *
+gst_check_setup_sink_pad_by_name (GstElement * element,
+    GstStaticPadTemplate * tmpl, const gchar * name)
 {
   GstPad *srcpad, *sinkpad;
 
   /* receiving pad */
-  sinkpad = gst_pad_new_from_static_template (template, "sink");
+  sinkpad = gst_pad_new_from_static_template (tmpl, "sink");
   GST_DEBUG_OBJECT (element, "setting up receiving pad %p", sinkpad);
   fail_if (sinkpad == NULL, "Could not create a sinkpad");
 
-  srcpad = gst_element_get_pad (element, "src");
+  srcpad = gst_element_get_static_pad (element, name);
+  if (srcpad == NULL)
+    srcpad = gst_element_get_request_pad (element, name);
   fail_if (srcpad == NULL, "Could not get source pad from %s",
       GST_ELEMENT_NAME (element));
-  if (caps)
-    fail_unless (gst_pad_set_caps (sinkpad, caps));
   gst_pad_set_chain_function (sinkpad, gst_check_chain_func);
 
   GST_DEBUG_OBJECT (element, "Linking element src pad and receiving sink pad");
@@ -242,22 +324,204 @@ gst_check_setup_sink_pad (GstElement * element, GstStaticPadTemplate * template,
 void
 gst_check_teardown_sink_pad (GstElement * element)
 {
-  GstPad *srcpad, *sinkpad;
+  gst_check_teardown_pad_by_name (element, "src");
+}
 
-  /* clean up floating sink pad */
-  srcpad = gst_element_get_pad (element, "src");
-  sinkpad = gst_pad_get_peer (srcpad);
-  gst_pad_unlink (srcpad, sinkpad);
+/**
+ * gst_check_drop_buffers:
+ *
+ * Unref and remove all buffers that are in the global @buffers GList,
+ * emptying the list.
+ *
+ * Since: 0.10.18
+ */
+void
+gst_check_drop_buffers (void)
+{
+  while (buffers != NULL) {
+    gst_buffer_unref (GST_BUFFER (buffers->data));
+    buffers = g_list_delete_link (buffers, buffers);
+  }
+}
 
-  /* pad refs held by both creator and this function (through _get_pad) */
-  ASSERT_OBJECT_REFCOUNT (srcpad, "element srcpad", 2);
-  gst_object_unref (srcpad);
-  /* one more ref is held by element itself */
+/**
+ * gst_check_caps_equal:
+ * @caps1: first caps to compare
+ * @caps2: second caps to compare
+ *
+ * Compare two caps with gst_caps_is_equal and fail unless they are
+ * equal.
+ *
+ * Since: 0.10.18
+ */
+void
+gst_check_caps_equal (GstCaps * caps1, GstCaps * caps2)
+{
+  gchar *name1 = gst_caps_to_string (caps1);
+  gchar *name2 = gst_caps_to_string (caps2);
+
+  fail_unless (gst_caps_is_equal (caps1, caps2),
+      "caps ('%s') is not equal to caps ('%s')", name1, name2);
+  g_free (name1);
+  g_free (name2);
+}
+
+/**
+ * gst_check_element_push_buffer_list:
+ * @element_name: name of the element that needs to be created
+ * @buffer_in: a list of buffers that needs to be puched to the element
+ * @buffer_out: a list of buffers that we expect from the element
+ * @last_flow_return: the last buffer push needs to give this GstFlowReturn
+ *
+ * Create an @element with the factory with the name and push the buffers in
+ * @buffer_in to this element. The element should create the buffers equal to
+ * the buffers in @buffer_out. We only check the caps, size and the data of the
+ * buffers. This function unrefs the buffers in the two lists.
+ * The last_flow_return parameter indicates the expected flow return value from
+ * pushing the final buffer in the list.
+ * This can be used to set up a test which pushes some buffers and then an
+ * invalid buffer, when the final buffer is expected to fail, for example.
+ * 
+ * Since: 0.10.18
+ */
+/* FIXME 0.11: rename this function now that there's GstBufferList? */
+void
+gst_check_element_push_buffer_list (const gchar * element_name,
+    GList * buffer_in, GList * buffer_out, GstFlowReturn last_flow_return)
+{
+  GstCaps *sink_caps;
+  GstCaps *src_caps = NULL;
+  GstElement *element;
+  GstPad *pad_peer;
+  GstPad *sink_pad = NULL;
+  GstPad *src_pad;
+  GstBuffer *buffer;
+
+  /* check that there are no buffers waiting */
+  gst_check_drop_buffers ();
+  /* create the element */
+  element = gst_check_setup_element (element_name);
+  fail_if (element == NULL, "failed to create the element '%s'", element_name);
+  fail_unless (GST_IS_ELEMENT (element), "the element is no element");
+  /* create the src pad */
+  buffer = GST_BUFFER (buffer_in->data);
+
+  fail_unless (GST_IS_BUFFER (buffer), "There should be a buffer in buffer_in");
+  src_caps = GST_BUFFER_CAPS (buffer);
+  src_pad = gst_pad_new (NULL, GST_PAD_SRC);
+  gst_pad_set_caps (src_pad, src_caps);
+  pad_peer = gst_element_get_static_pad (element, "sink");
+  fail_if (pad_peer == NULL);
+  fail_unless (gst_pad_link (src_pad, pad_peer) == GST_PAD_LINK_OK,
+      "Could not link source and %s sink pads", GST_ELEMENT_NAME (element));
+  gst_object_unref (pad_peer);
+  /* activate the pad */
+  gst_pad_set_active (src_pad, TRUE);
+  GST_DEBUG ("src pad activated");
+  /* don't create the sink_pad if there is no buffer_out list */
+  if (buffer_out != NULL) {
+    gchar *temp;
+
+    GST_DEBUG ("buffer out detected, creating the sink pad");
+    /* get the sink caps */
+    sink_caps = GST_BUFFER_CAPS (GST_BUFFER (buffer_out->data));
+    fail_unless (GST_IS_CAPS (sink_caps), "buffer out don't have caps");
+    temp = gst_caps_to_string (sink_caps);
+
+    GST_DEBUG ("sink caps requested by buffer out: '%s'", temp);
+    g_free (temp);
+    fail_unless (gst_caps_is_fixed (sink_caps), "we need fixed caps");
+    /* get the sink pad */
+    sink_pad = gst_pad_new (NULL, GST_PAD_SINK);
+    fail_unless (GST_IS_PAD (sink_pad));
+    gst_pad_set_caps (sink_pad, sink_caps);
+    /* get the peer pad */
+    pad_peer = gst_element_get_static_pad (element, "src");
+    fail_unless (gst_pad_link (pad_peer, sink_pad) == GST_PAD_LINK_OK,
+        "Could not link sink and %s source pads", GST_ELEMENT_NAME (element));
+    gst_object_unref (pad_peer);
+    /* configure the sink pad */
+    gst_pad_set_chain_function (sink_pad, gst_check_chain_func);
+    gst_pad_set_active (sink_pad, TRUE);
+  }
+  fail_unless (gst_element_set_state (element,
+          GST_STATE_PLAYING) == GST_STATE_CHANGE_SUCCESS,
+      "could not set to playing");
+  /* push all the buffers in the buffer_in list */
+  fail_unless (g_list_length (buffer_in) > 0, "the buffer_in list is empty");
+  while (buffer_in != NULL) {
+    GstBuffer *next_buffer = GST_BUFFER (buffer_in->data);
+
+    fail_unless (GST_IS_BUFFER (next_buffer),
+        "data in buffer_in should be a buffer");
+    /* remove the buffer from the list */
+    buffer_in = g_list_remove (buffer_in, next_buffer);
+    if (buffer_in == NULL) {
+      fail_unless (gst_pad_push (src_pad, next_buffer) == last_flow_return,
+          "we expect something else from the last buffer");
+    } else {
+      fail_unless (gst_pad_push (src_pad, next_buffer) == GST_FLOW_OK,
+          "Failed to push buffer in");
+    }
+  }
+  fail_unless (gst_element_set_state (element,
+          GST_STATE_NULL) == GST_STATE_CHANGE_SUCCESS, "could not set to null");
+  /* check that there is a buffer out */
+  fail_unless_equals_int (g_list_length (buffers), g_list_length (buffer_out));
+  while (buffers != NULL) {
+    GstBuffer *new = GST_BUFFER (buffers->data);
+    GstBuffer *orig = GST_BUFFER (buffer_out->data);
+
+    GST_LOG ("orig buffer: size %u, caps %" GST_PTR_FORMAT,
+        GST_BUFFER_SIZE (orig), GST_BUFFER_CAPS (orig));
+    GST_LOG ("new  buffer: size %u, caps %" GST_PTR_FORMAT,
+        GST_BUFFER_SIZE (new), GST_BUFFER_CAPS (new));
+    GST_MEMDUMP ("orig buffer", GST_BUFFER_DATA (orig), GST_BUFFER_SIZE (orig));
+    GST_MEMDUMP ("new  buffer", GST_BUFFER_DATA (new), GST_BUFFER_SIZE (new));
+
+    /* remove the buffers */
+    buffers = g_list_remove (buffers, new);
+    buffer_out = g_list_remove (buffer_out, orig);
+    fail_unless (GST_BUFFER_SIZE (orig) == GST_BUFFER_SIZE (new),
+        "size of the buffers are not the same");
+    fail_unless (memcmp (GST_BUFFER_DATA (orig), GST_BUFFER_DATA (new),
+            GST_BUFFER_SIZE (new)) == 0, "data is not the same");
+    gst_check_caps_equal (GST_BUFFER_CAPS (orig), GST_BUFFER_CAPS (new));
+    gst_buffer_unref (new);
+    gst_buffer_unref (orig);
+  }
+  /* teardown the element and pads */
+  gst_pad_set_active (src_pad, FALSE);
+  gst_check_teardown_src_pad (element);
+  gst_pad_set_active (sink_pad, FALSE);
+  gst_check_teardown_sink_pad (element);
+  gst_check_teardown_element (element);
+}
+
+/**
+ * gst_check_element_push_buffer:
+ * @element_name: name of the element that needs to be created
+ * @buffer_in: push this buffer to the element
+ * @buffer_out: compare the result with this buffer
+ *
+ * Create an @element with the factory with the name and push the
+ * @buffer_in to this element. The element should create one buffer
+ * and this will be compared with @buffer_out. We only check the caps
+ * and the data of the buffers. This function unrefs the buffers.
+ * 
+ * Since: 0.10.18
+ */
+void
+gst_check_element_push_buffer (const gchar * element_name,
+    GstBuffer * buffer_in, GstBuffer * buffer_out)
+{
+  GList *in = NULL;
+  GList *out = NULL;
+
+  in = g_list_append (in, buffer_in);
+  out = g_list_append (out, buffer_out);
 
-  /* pad refs held by both creator and this function (through _get_peer) */
-  ASSERT_OBJECT_REFCOUNT (sinkpad, "check sinkpad", 2);
-  gst_object_unref (sinkpad);
-  gst_object_unref (sinkpad);
+  gst_check_element_push_buffer_list (element_name, in, out, GST_FLOW_OK);
 }
 
 void
@@ -276,19 +540,78 @@ gst_check_abi_list (GstCheckABIStruct list[], gboolean have_abi_sizes)
     }
     fail_unless (ok, "failed ABI check");
   } else {
-    if (g_getenv ("GST_ABI")) {
+    const gchar *fn;
+
+    if ((fn = g_getenv ("GST_ABI"))) {
+      GError *err = NULL;
+      GString *s;
       gint i;
 
-      g_print ("\nGstCheckABIStruct list[] = {\n");
+      s = g_string_new ("\nGstCheckABIStruct list[] = {\n");
       for (i = 0; list[i].name; i++) {
-        g_print ("  {\"%s\", sizeof (%s), %d},\n", list[i].name, list[i].name,
-            list[i].size);
+        g_string_append_printf (s, "  {\"%s\", sizeof (%s), %d},\n",
+            list[i].name, list[i].name, list[i].size);
+      }
+      g_string_append (s, "  {NULL, 0, 0}\n");
+      g_string_append (s, "};\n");
+      if (!g_file_set_contents (fn, s->str, s->len, &err)) {
+        g_print ("%s", s->str);
+        g_printerr ("\nFailed to write ABI information: %s\n", err->message);
+      } else {
+        g_print ("\nWrote ABI information to '%s'.\n", fn);
       }
-      g_print ("  {NULL, 0, 0}\n");
-      g_print ("};\n");
+      g_string_free (s, TRUE);
     } else {
       g_print ("No structure size list was generated for this architecture.\n");
       g_print ("Run with GST_ABI environment variable set to output header.\n");
     }
   }
 }
+
+gint
+gst_check_run_suite (Suite * suite, const gchar * name, const gchar * fname)
+{
+  SRunner *sr;
+  gchar *xmlfilename = NULL;
+  gint nf;
+
+  sr = srunner_create (suite);
+
+  if (g_getenv ("GST_CHECK_XML")) {
+    /* how lucky we are to have __FILE__ end in .c */
+    xmlfilename = g_strdup_printf ("%sheck.xml", fname);
+
+    srunner_set_xml (sr, xmlfilename);
+  }
+
+  srunner_run_all (sr, CK_NORMAL);
+  nf = srunner_ntests_failed (sr);
+  g_free (xmlfilename);
+  srunner_free (sr);
+  return nf;
+}
+
+gboolean
+_gst_check_run_test_func (const gchar * func_name)
+{
+  const gchar *gst_checks;
+  gboolean res = FALSE;
+  gchar **funcs, **f;
+
+  gst_checks = g_getenv ("GST_CHECKS");
+
+  /* no filter specified => run all checks */
+  if (gst_checks == NULL || *gst_checks == '\0')
+    return TRUE;
+
+  /* only run specified functions */
+  funcs = g_strsplit (gst_checks, ",", -1);
+  for (f = funcs; f != NULL && *f != NULL; ++f) {
+    if (g_pattern_match_simple (*f, func_name)) {
+      res = TRUE;
+      break;
+    }
+  }
+  g_strfreev (funcs);
+  return res;
+}