index f25bf3294a5fb07c14c31c8ba6b59cf703c51a72..c4370a3ae9101431fef23f7d471b338842d83079 100644 (file)
* Common code for GStreamer unittests
*
* Copyright (C) 2004,2006 Thomas Vander Stichele <thomas at apestaart dot org>
+ * Copyright (C) 2008 Thijs Vermeir <thijsvermeir@gmail.com>
*
* This library is free software; you can redistribute it and/or
* modify it under the terms of the GNU Library General Public
GMutex *check_mutex = NULL;
GCond *check_cond = NULL;
+/* FIXME 0.11: shouldn't _gst_check_debug be static? Not used anywhere */
gboolean _gst_check_debug = FALSE;
gboolean _gst_check_raised_critical = FALSE;
gboolean _gst_check_raised_warning = FALSE;
gboolean _gst_check_expecting_log = FALSE;
-void gst_check_log_message_func
+static void gst_check_log_message_func
(const gchar * log_domain, GLogLevelFlags log_level,
const gchar * message, gpointer user_data)
{
}
}
-void gst_check_log_critical_func
+static void gst_check_log_critical_func
(const gchar * log_domain, GLogLevelFlags log_level,
const gchar * message, gpointer user_data)
{
_gst_check_raised_warning = TRUE;
}
+static gint
+sort_plugins (GstPlugin * a, GstPlugin * b)
+{
+ int ret;
+
+ ret = strcmp (gst_plugin_get_source (a), gst_plugin_get_source (b));
+ if (ret == 0)
+ ret = strcmp (gst_plugin_get_name (a), gst_plugin_get_name (b));
+ return ret;
+}
+
+static void
+print_plugins (void)
+{
+ GList *plugins, *l;
+
+ plugins = gst_default_registry_get_plugin_list ();
+ plugins = g_list_sort (plugins, (GCompareFunc) sort_plugins);
+ for (l = plugins; l != NULL; l = l->next) {
+ GstPlugin *plugin = GST_PLUGIN (l->data);
+
+ if (strcmp (gst_plugin_get_source (plugin), "BLACKLIST") != 0) {
+ GST_LOG ("%20s@%s", gst_plugin_get_name (plugin),
+ GST_STR_NULL (gst_plugin_get_filename (plugin)));
+ }
+ }
+ gst_plugin_list_free (plugins);
+}
+
/* initialize GStreamer testing */
void
gst_check_init (int *argc, char **argv[])
g_log_set_handler ("Gst-Phonon", G_LOG_LEVEL_CRITICAL | G_LOG_LEVEL_WARNING,
gst_check_log_critical_func, NULL);
+ print_plugins ();
+
check_cond = g_cond_new ();
check_mutex = g_mutex_new ();
}
GST_DEBUG ("setup_element");
element = gst_element_factory_make (factory, factory);
- fail_if (element == NULL, "Could not create a %s", factory);
+ fail_if (element == NULL, "Could not create a '%s' element", factory);
ASSERT_OBJECT_REFCOUNT (element, factory, 1);
return element;
}
*/
GstPad *
gst_check_setup_src_pad (GstElement * element,
- GstStaticPadTemplate * template, GstCaps * caps)
+ GstStaticPadTemplate * tmpl, GstCaps * caps)
+{
+ GstPad *srcpad;
+
+ srcpad = gst_check_setup_src_pad_by_name (element, tmpl, "sink");
+ if (caps)
+ fail_unless (gst_pad_set_caps (srcpad, caps), "could not set caps on pad");
+ return srcpad;
+}
+
+GstPad *
+gst_check_setup_src_pad_by_name (GstElement * element,
+ GstStaticPadTemplate * tmpl, const gchar * name)
{
GstPad *srcpad, *sinkpad;
/* sending pad */
- srcpad = gst_pad_new_from_static_template (template, "src");
+ srcpad = gst_pad_new_from_static_template (tmpl, "src");
GST_DEBUG_OBJECT (element, "setting up sending pad %p", srcpad);
fail_if (srcpad == NULL, "Could not create a srcpad");
ASSERT_OBJECT_REFCOUNT (srcpad, "srcpad", 1);
- sinkpad = gst_element_get_pad (element, "sink");
+ sinkpad = gst_element_get_static_pad (element, name);
+ if (sinkpad == NULL)
+ sinkpad = gst_element_get_request_pad (element, name);
fail_if (sinkpad == NULL, "Could not get sink pad from %s",
GST_ELEMENT_NAME (element));
ASSERT_OBJECT_REFCOUNT (sinkpad, "sinkpad", 2);
- if (caps)
- fail_unless (gst_pad_set_caps (srcpad, caps), "could not set caps on pad");
fail_unless (gst_pad_link (srcpad, sinkpad) == GST_PAD_LINK_OK,
"Could not link source and %s sink pads", GST_ELEMENT_NAME (element));
gst_object_unref (sinkpad); /* because we got it higher up */
}
void
-gst_check_teardown_src_pad (GstElement * element)
+gst_check_teardown_pad_by_name (GstElement * element, const gchar * name)
{
- GstPad *srcpad, *sinkpad;
+ GstPad *pad_peer, *pad_element;
/* clean up floating src pad */
- sinkpad = gst_element_get_pad (element, "sink");
- ASSERT_OBJECT_REFCOUNT (sinkpad, "sinkpad", 2);
- srcpad = gst_pad_get_peer (sinkpad);
-
- gst_pad_unlink (srcpad, sinkpad);
-
- /* caps could have been set, make sure they get unset */
- gst_pad_set_caps (srcpad, NULL);
+ pad_element = gst_element_get_static_pad (element, name);
+ /* We don't check the refcount here since there *might* be
+ * a pad cache holding an extra reference on pad_element.
+ * To get to a state where no pad cache will exist,
+ * we first unlink that pad. */
+ pad_peer = gst_pad_get_peer (pad_element);
+
+ if (pad_peer) {
+ if (gst_pad_get_direction (pad_element) == GST_PAD_SINK)
+ gst_pad_unlink (pad_peer, pad_element);
+ else
+ gst_pad_unlink (pad_element, pad_peer);
+
+ /* caps could have been set, make sure they get unset */
+ gst_pad_set_caps (pad_peer, NULL);
+ }
/* pad refs held by both creator and this function (through _get) */
- ASSERT_OBJECT_REFCOUNT (sinkpad, "element sinkpad", 2);
- gst_object_unref (sinkpad);
+ ASSERT_OBJECT_REFCOUNT (pad_element, "element pad_element", 2);
+ gst_object_unref (pad_element);
/* one more ref is held by element itself */
- /* pad refs held by both creator and this function (through _get_peer) */
- ASSERT_OBJECT_REFCOUNT (srcpad, "check srcpad", 2);
- gst_object_unref (srcpad);
- gst_object_unref (srcpad);
+ if (pad_peer) {
+ /* pad refs held by both creator and this function (through _get_peer) */
+ ASSERT_OBJECT_REFCOUNT (pad_peer, "check pad_peer", 2);
+ gst_object_unref (pad_peer);
+ gst_object_unref (pad_peer);
+ }
+}
+
+void
+gst_check_teardown_src_pad (GstElement * element)
+{
+ gst_check_teardown_pad_by_name (element, "sink");
}
/* FIXME: set_caps isn't that useful; might want to check if fixed,
* then use set_use_fixed or somesuch */
GstPad *
-gst_check_setup_sink_pad (GstElement * element, GstStaticPadTemplate * template,
+gst_check_setup_sink_pad (GstElement * element, GstStaticPadTemplate * tmpl,
GstCaps * caps)
+{
+ GstPad *sinkpad;
+
+ sinkpad = gst_check_setup_sink_pad_by_name (element, tmpl, "src");
+ if (caps)
+ fail_unless (gst_pad_set_caps (sinkpad, caps), "Could not set pad caps");
+ return sinkpad;
+}
+
+GstPad *
+gst_check_setup_sink_pad_by_name (GstElement * element,
+ GstStaticPadTemplate * tmpl, const gchar * name)
{
GstPad *srcpad, *sinkpad;
/* receiving pad */
- sinkpad = gst_pad_new_from_static_template (template, "sink");
+ sinkpad = gst_pad_new_from_static_template (tmpl, "sink");
GST_DEBUG_OBJECT (element, "setting up receiving pad %p", sinkpad);
fail_if (sinkpad == NULL, "Could not create a sinkpad");
- srcpad = gst_element_get_pad (element, "src");
+ srcpad = gst_element_get_static_pad (element, name);
+ if (srcpad == NULL)
+ srcpad = gst_element_get_request_pad (element, name);
fail_if (srcpad == NULL, "Could not get source pad from %s",
GST_ELEMENT_NAME (element));
- if (caps)
- fail_unless (gst_pad_set_caps (sinkpad, caps), "Could not set pad caps");
gst_pad_set_chain_function (sinkpad, gst_check_chain_func);
GST_DEBUG_OBJECT (element, "Linking element src pad and receiving sink pad");
@@ -251,23 +324,204 @@ gst_check_setup_sink_pad (GstElement * element, GstStaticPadTemplate * template,
void
gst_check_teardown_sink_pad (GstElement * element)
{
- GstPad *srcpad, *sinkpad;
+ gst_check_teardown_pad_by_name (element, "src");
+}
- /* clean up floating sink pad */
- srcpad = gst_element_get_pad (element, "src");
- sinkpad = gst_pad_get_peer (srcpad);
+/**
+ * gst_check_drop_buffers:
+ *
+ * Unref and remove all buffers that are in the global @buffers GList,
+ * emptying the list.
+ *
+ * Since: 0.10.18
+ */
+void
+gst_check_drop_buffers (void)
+{
+ while (buffers != NULL) {
+ gst_buffer_unref (GST_BUFFER (buffers->data));
+ buffers = g_list_delete_link (buffers, buffers);
+ }
+}
+
+/**
+ * gst_check_caps_equal:
+ * @caps1: first caps to compare
+ * @caps2: second caps to compare
+ *
+ * Compare two caps with gst_caps_is_equal and fail unless they are
+ * equal.
+ *
+ * Since: 0.10.18
+ */
+void
+gst_check_caps_equal (GstCaps * caps1, GstCaps * caps2)
+{
+ gchar *name1 = gst_caps_to_string (caps1);
+ gchar *name2 = gst_caps_to_string (caps2);
- gst_pad_unlink (srcpad, sinkpad);
+ fail_unless (gst_caps_is_equal (caps1, caps2),
+ "caps ('%s') is not equal to caps ('%s')", name1, name2);
+ g_free (name1);
+ g_free (name2);
+}
- /* pad refs held by both creator and this function (through _get_pad) */
- ASSERT_OBJECT_REFCOUNT (srcpad, "element srcpad", 2);
- gst_object_unref (srcpad);
- /* one more ref is held by element itself */
+/**
+ * gst_check_element_push_buffer_list:
+ * @element_name: name of the element that needs to be created
+ * @buffer_in: a list of buffers that needs to be puched to the element
+ * @buffer_out: a list of buffers that we expect from the element
+ * @last_flow_return: the last buffer push needs to give this GstFlowReturn
+ *
+ * Create an @element with the factory with the name and push the buffers in
+ * @buffer_in to this element. The element should create the buffers equal to
+ * the buffers in @buffer_out. We only check the caps, size and the data of the
+ * buffers. This function unrefs the buffers in the two lists.
+ * The last_flow_return parameter indicates the expected flow return value from
+ * pushing the final buffer in the list.
+ * This can be used to set up a test which pushes some buffers and then an
+ * invalid buffer, when the final buffer is expected to fail, for example.
+ *
+ * Since: 0.10.18
+ */
+/* FIXME 0.11: rename this function now that there's GstBufferList? */
+void
+gst_check_element_push_buffer_list (const gchar * element_name,
+ GList * buffer_in, GList * buffer_out, GstFlowReturn last_flow_return)
+{
+ GstCaps *sink_caps;
+ GstCaps *src_caps = NULL;
+ GstElement *element;
+ GstPad *pad_peer;
+ GstPad *sink_pad = NULL;
+ GstPad *src_pad;
+ GstBuffer *buffer;
+
+ /* check that there are no buffers waiting */
+ gst_check_drop_buffers ();
+ /* create the element */
+ element = gst_check_setup_element (element_name);
+ fail_if (element == NULL, "failed to create the element '%s'", element_name);
+ fail_unless (GST_IS_ELEMENT (element), "the element is no element");
+ /* create the src pad */
+ buffer = GST_BUFFER (buffer_in->data);
+
+ fail_unless (GST_IS_BUFFER (buffer), "There should be a buffer in buffer_in");
+ src_caps = GST_BUFFER_CAPS (buffer);
+ src_pad = gst_pad_new (NULL, GST_PAD_SRC);
+ gst_pad_set_caps (src_pad, src_caps);
+ pad_peer = gst_element_get_static_pad (element, "sink");
+ fail_if (pad_peer == NULL);
+ fail_unless (gst_pad_link (src_pad, pad_peer) == GST_PAD_LINK_OK,
+ "Could not link source and %s sink pads", GST_ELEMENT_NAME (element));
+ gst_object_unref (pad_peer);
+ /* activate the pad */
+ gst_pad_set_active (src_pad, TRUE);
+ GST_DEBUG ("src pad activated");
+ /* don't create the sink_pad if there is no buffer_out list */
+ if (buffer_out != NULL) {
+ gchar *temp;
+
+ GST_DEBUG ("buffer out detected, creating the sink pad");
+ /* get the sink caps */
+ sink_caps = GST_BUFFER_CAPS (GST_BUFFER (buffer_out->data));
+ fail_unless (GST_IS_CAPS (sink_caps), "buffer out don't have caps");
+ temp = gst_caps_to_string (sink_caps);
+
+ GST_DEBUG ("sink caps requested by buffer out: '%s'", temp);
+ g_free (temp);
+ fail_unless (gst_caps_is_fixed (sink_caps), "we need fixed caps");
+ /* get the sink pad */
+ sink_pad = gst_pad_new (NULL, GST_PAD_SINK);
+ fail_unless (GST_IS_PAD (sink_pad));
+ gst_pad_set_caps (sink_pad, sink_caps);
+ /* get the peer pad */
+ pad_peer = gst_element_get_static_pad (element, "src");
+ fail_unless (gst_pad_link (pad_peer, sink_pad) == GST_PAD_LINK_OK,
+ "Could not link sink and %s source pads", GST_ELEMENT_NAME (element));
+ gst_object_unref (pad_peer);
+ /* configure the sink pad */
+ gst_pad_set_chain_function (sink_pad, gst_check_chain_func);
+ gst_pad_set_active (sink_pad, TRUE);
+ }
+ fail_unless (gst_element_set_state (element,
+ GST_STATE_PLAYING) == GST_STATE_CHANGE_SUCCESS,
+ "could not set to playing");
+ /* push all the buffers in the buffer_in list */
+ fail_unless (g_list_length (buffer_in) > 0, "the buffer_in list is empty");
+ while (buffer_in != NULL) {
+ GstBuffer *next_buffer = GST_BUFFER (buffer_in->data);
+
+ fail_unless (GST_IS_BUFFER (next_buffer),
+ "data in buffer_in should be a buffer");
+ /* remove the buffer from the list */
+ buffer_in = g_list_remove (buffer_in, next_buffer);
+ if (buffer_in == NULL) {
+ fail_unless (gst_pad_push (src_pad, next_buffer) == last_flow_return,
+ "we expect something else from the last buffer");
+ } else {
+ fail_unless (gst_pad_push (src_pad, next_buffer) == GST_FLOW_OK,
+ "Failed to push buffer in");
+ }
+ }
+ fail_unless (gst_element_set_state (element,
+ GST_STATE_NULL) == GST_STATE_CHANGE_SUCCESS, "could not set to null");
+ /* check that there is a buffer out */
+ fail_unless_equals_int (g_list_length (buffers), g_list_length (buffer_out));
+ while (buffers != NULL) {
+ GstBuffer *new = GST_BUFFER (buffers->data);
+ GstBuffer *orig = GST_BUFFER (buffer_out->data);
+
+ GST_LOG ("orig buffer: size %u, caps %" GST_PTR_FORMAT,
+ GST_BUFFER_SIZE (orig), GST_BUFFER_CAPS (orig));
+ GST_LOG ("new buffer: size %u, caps %" GST_PTR_FORMAT,
+ GST_BUFFER_SIZE (new), GST_BUFFER_CAPS (new));
+ GST_MEMDUMP ("orig buffer", GST_BUFFER_DATA (orig), GST_BUFFER_SIZE (orig));
+ GST_MEMDUMP ("new buffer", GST_BUFFER_DATA (new), GST_BUFFER_SIZE (new));
+
+ /* remove the buffers */
+ buffers = g_list_remove (buffers, new);
+ buffer_out = g_list_remove (buffer_out, orig);
+ fail_unless (GST_BUFFER_SIZE (orig) == GST_BUFFER_SIZE (new),
+ "size of the buffers are not the same");
+ fail_unless (memcmp (GST_BUFFER_DATA (orig), GST_BUFFER_DATA (new),
+ GST_BUFFER_SIZE (new)) == 0, "data is not the same");
+ gst_check_caps_equal (GST_BUFFER_CAPS (orig), GST_BUFFER_CAPS (new));
+ gst_buffer_unref (new);
+ gst_buffer_unref (orig);
+ }
+ /* teardown the element and pads */
+ gst_pad_set_active (src_pad, FALSE);
+ gst_check_teardown_src_pad (element);
+ gst_pad_set_active (sink_pad, FALSE);
+ gst_check_teardown_sink_pad (element);
+ gst_check_teardown_element (element);
+}
+
+/**
+ * gst_check_element_push_buffer:
+ * @element_name: name of the element that needs to be created
+ * @buffer_in: push this buffer to the element
+ * @buffer_out: compare the result with this buffer
+ *
+ * Create an @element with the factory with the name and push the
+ * @buffer_in to this element. The element should create one buffer
+ * and this will be compared with @buffer_out. We only check the caps
+ * and the data of the buffers. This function unrefs the buffers.
+ *
+ * Since: 0.10.18
+ */
+void
+gst_check_element_push_buffer (const gchar * element_name,
+ GstBuffer * buffer_in, GstBuffer * buffer_out)
+{
+ GList *in = NULL;
+ GList *out = NULL;
+
+ in = g_list_append (in, buffer_in);
+ out = g_list_append (out, buffer_out);
- /* pad refs held by both creator and this function (through _get_peer) */
- ASSERT_OBJECT_REFCOUNT (sinkpad, "check sinkpad", 2);
- gst_object_unref (sinkpad);
- gst_object_unref (sinkpad);
+ gst_check_element_push_buffer_list (element_name, in, out, GST_FLOW_OK);
}
void
gint
gst_check_run_suite (Suite * suite, const gchar * name, const gchar * fname)
{
+ SRunner *sr;
+ gchar *xmlfilename = NULL;
gint nf;
- SRunner *sr = srunner_create (suite);
+ sr = srunner_create (suite);
if (g_getenv ("GST_CHECK_XML")) {
/* how lucky we are to have __FILE__ end in .c */
- gchar *xmlfilename = g_strdup_printf ("%sheck.xml", fname);
+ xmlfilename = g_strdup_printf ("%sheck.xml", fname);
srunner_set_xml (sr, xmlfilename);
}
srunner_run_all (sr, CK_NORMAL);
nf = srunner_ntests_failed (sr);
+ g_free (xmlfilename);
srunner_free (sr);
return nf;
}
/* only run specified functions */
funcs = g_strsplit (gst_checks, ",", -1);
for (f = funcs; f != NULL && *f != NULL; ++f) {
- if (strcmp (*f, func_name) == 0) {
+ if (g_pattern_match_simple (*f, func_name)) {
res = TRUE;
break;
}