index 0627a48b3b0a2b498e324660acefec0d91ae0666..e77c007bce3783f370ff579e4aa31b4e23dfc7f6 100644 (file)
* Common code for GStreamer unittests
*
* Copyright (C) <2004> Thomas Vander Stichele <thomas at apestaart dot org>
+ * Copyright (C) <2008> Thijs Vermeir <thijsvermeir@gmail.com>
*
* This library is free software; you can redistribute it and/or
* modify it under the terms of the GNU Library General Public
#include <signal.h>
#include <string.h>
#include <stdlib.h>
+#include <math.h>
-#include <check.h>
+#include <gst/check/internal-check.h>
#include <gst/gst.h>
+G_BEGIN_DECLS
+
GST_DEBUG_CATEGORY_EXTERN (check_debug);
#define GST_CAT_DEFAULT check_debug
*/
extern gboolean _gst_check_threads_running;
extern gboolean _gst_check_raised_critical;
+extern gboolean _gst_check_raised_warning;
extern gboolean _gst_check_expecting_log;
/* global variables used in test methods */
-GList * buffers;
-
-void gst_check_init (int *argc, char **argv[]);
+extern GList * buffers;
-GstFlowReturn gst_check_chain_func (GstPad *pad, GstBuffer *buffer);
+extern GMutex *check_mutex;
+extern GCond *check_cond;
-void gst_check_message_error (GstMessage *message, GstMessageType type, GQuark domain, gint code);
+typedef struct
+{
+ const char *name;
+ int size;
+ int abi_size;
+}
+GstCheckABIStruct;
-GstElement * gst_check_setup_element (const gchar *factory);
-void gst_check_teardown_element (GstElement *element);
-GstPad * gst_check_setup_src_pad (GstElement *element,
- GstStaticPadTemplate *template, GstCaps *caps);
-void gst_check_teardown_src_pad (GstElement *element);
-GstPad * gst_check_setup_sink_pad (GstElement *element,
- GstStaticPadTemplate *template, GstCaps *caps);
-void gst_check_teardown_sink_pad (GstElement *element);
+void gst_check_init (int *argc, char **argv[]);
+GstFlowReturn gst_check_chain_func (GstPad * pad, GstBuffer * buffer);
+
+void gst_check_message_error (GstMessage * message, GstMessageType type,
+ GQuark domain, gint code);
+
+GstElement *gst_check_setup_element (const gchar * factory);
+void gst_check_teardown_element (GstElement * element);
+GstPad *gst_check_setup_src_pad (GstElement * element,
+ GstStaticPadTemplate * tmpl, GstCaps * caps);
+GstPad * gst_check_setup_src_pad_by_name (GstElement * element,
+ GstStaticPadTemplate * tmpl, const gchar *name);
+GstPad * gst_check_setup_sink_pad_by_name (GstElement * element,
+ GstStaticPadTemplate * tmpl, const gchar *name);
+void gst_check_teardown_pad_by_name (GstElement * element, const gchar *name);
+void gst_check_teardown_src_pad (GstElement * element);
+void gst_check_drop_buffers (void);
+void gst_check_caps_equal (GstCaps * caps1, GstCaps * caps2);
+void gst_check_element_push_buffer_list (const gchar * element_name,
+ GList * buffer_in, GList * buffer_out, GstFlowReturn last_flow_return);
+void gst_check_element_push_buffer (const gchar * element_name,
+ GstBuffer * buffer_in, GstBuffer * buffer_out);
+GstPad *gst_check_setup_sink_pad (GstElement * element,
+ GstStaticPadTemplate * tmpl, GstCaps * caps);
+void gst_check_teardown_sink_pad (GstElement * element);
+void gst_check_abi_list (GstCheckABIStruct list[], gboolean have_abi_sizes);
+gint gst_check_run_suite (Suite * suite, const gchar * name,
+ const gchar * fname);
#define fail_unless_message_error(msg, domain, code) \
gst_check_message_error (msg, GST_MESSAGE_ERROR, \
GST_ ## domain ## _ERROR, GST_ ## domain ## _ERROR_ ## code)
+#define assert_message_error(m, d, c) fail_unless_message_error(m, d, c)
-/***
- * wrappers for START_TEST and END_TEST
+/**
+ * GST_START_TEST:
+ * @__testname: test function name
+ *
+ * wrapper for checks START_TEST
+ */
+/**
+ * GST_END_TEST:
+ *
+ * wrapper for checks END_TEST
*/
#define GST_START_TEST(__testname) \
-static void __testname (void)\
+static void __testname (int __i__)\
{\
GST_DEBUG ("test start"); \
tcase_fn_start (""# __testname, __FILE__, __LINE__);
-#define GST_END_TEST END_TEST
+#define GST_END_TEST GST_LOG ("cleaning up tasks"); \
+ gst_task_cleanup_all (); \
+ END_TEST
/* additional fail macros */
+/**
+ * fail_unless_equals_int:
+ * @a: a #gint value or expression
+ * @b: a #gint value or expression
+ *
+ * This macro checks that @a and @b are equal and aborts if this is not the
+ * case, printing both expressions and the values they evaluated to. This
+ * macro is for use in unit tests.
+ */
#define fail_unless_equals_int(a, b) \
G_STMT_START { \
int first = a; \
fail_unless(first == second, \
"'" #a "' (%d) is not equal to '" #b"' (%d)", first, second); \
} G_STMT_END;
+/**
+ * assert_equals_int:
+ * @a: a #gint value or expression
+ * @b: a #gint value or expression
+ *
+ * This macro checks that @a and @b are equal and aborts if this is not the
+ * case, printing both expressions and the values they evaluated to. This
+ * macro is for use in unit tests.
+ */
+#define assert_equals_int(a, b) fail_unless_equals_int(a, b)
+
+/**
+ * fail_unless_equals_int64:
+ * @a: a #gint64 value or expression
+ * @b: a #gint64 value or expression
+ *
+ * This macro checks that @a and @b are equal and aborts if this is not the
+ * case, printing both expressions and the values they evaluated to. This
+ * macro is for use in unit tests.
+ */
+#define fail_unless_equals_int64(a, b) \
+G_STMT_START { \
+ gint64 first = a; \
+ gint64 second = b; \
+ fail_unless(first == second, \
+ "'" #a "' (%" G_GINT64_FORMAT") is not equal to '" #b"' (%" \
+ G_GINT64_FORMAT")", first, second); \
+} G_STMT_END;
+/**
+ * assert_equals_int64:
+ * @a: a #gint64 value or expression
+ * @b: a #gint64 value or expression
+ *
+ * This macro checks that @a and @b are equal and aborts if this is not the
+ * case, printing both expressions and the values they evaluated to. This
+ * macro is for use in unit tests.
+ */
+#define assert_equals_int64(a, b) fail_unless_equals_int64(a, b)
-#define fail_unless_equals_string(a, b) \
+/**
+ * fail_unless_equals_uint64:
+ * @a: a #guint64 value or expression
+ * @b: a #guint64 value or expression
+ *
+ * This macro checks that @a and @b are equal and aborts if this is not the
+ * case, printing both expressions and the values they evaluated to. This
+ * macro is for use in unit tests.
+ */
+#define fail_unless_equals_uint64(a, b) \
G_STMT_START { \
- gchar * first = a; \
- gchar * second = b; \
- fail_unless(strcmp (first, second) == 0, \
- "'" #a "' (%s) is not equal to '" #b"' (%s)", first, second); \
+ guint64 first = a; \
+ guint64 second = b; \
+ fail_unless(first == second, \
+ "'" #a "' (%" G_GUINT64_FORMAT ") is not equal to '" #b"' (%" \
+ G_GUINT64_FORMAT ")", first, second); \
} G_STMT_END;
+/**
+ * assert_equals_uint64:
+ * @a: a #guint64 value or expression
+ * @b: a #guint64 value or expression
+ *
+ * This macro checks that @a and @b are equal and aborts if this is not the
+ * case, printing both expressions and the values they evaluated to. This
+ * macro is for use in unit tests.
+ */
+#define assert_equals_uint64(a, b) fail_unless_equals_uint64(a, b)
+
+/**
+ * fail_unless_equals_string:
+ * @a: a string literal or expression
+ * @b: a string literal or expression
+ *
+ * This macro checks that @a and @b are equal (as per strcmp) and aborts if
+ * this is not the case, printing both expressions and the values they
+ * evaluated to. This macro is for use in unit tests.
+ */
+#define fail_unless_equals_string(a, b) \
+G_STMT_START { \
+ const gchar * first = a; \
+ const gchar * second = b; \
+ fail_unless(g_strcmp0 (first, second) == 0, \
+ "'" #a "' (%s) is not equal to '" #b"' (%s)", first, second); \
+} G_STMT_END;
+/**
+ * assert_equals_string:
+ * @a: a string literal or expression
+ * @b: a string literal or expression
+ *
+ * This macro checks that @a and @b are equal (as per strcmp) and aborts if
+ * this is not the case, printing both expressions and the values they
+ * evaluated to. This macro is for use in unit tests.
+ */
+#define assert_equals_string(a, b) fail_unless_equals_string(a, b)
+
+/**
+ * fail_unless_equals_float:
+ * @a: a #gdouble or #gfloat value or expression
+ * @b: a #gdouble or #gfloat value or expression
+ *
+ * This macro checks that @a and @b are (almost) equal and aborts if this
+ * is not the case, printing both expressions and the values they evaluated
+ * to. This macro is for use in unit tests.
+ *
+ * Since: 0.10.14
+ */
+#define fail_unless_equals_float(a, b) \
+G_STMT_START { \
+ double first = a; \
+ double second = b; \
+ /* This will only work for 'normal' values and values around 0, \
+ * which should be good enough for our purposes here */ \
+ fail_unless(fabs (first - second) < 0.0000001, \
+ "'" #a "' (%g) is not equal to '" #b "' (%g)", first, second);\
+} G_STMT_END;
+
+/**
+ * assert_equals_float:
+ * @a: a #gdouble or #gfloat value or expression
+ * @b: a #gdouble or #gfloat value or expression
+ *
+ * This macro checks that @a and @b are (almost) equal and aborts if this
+ * is not the case, printing both expressions and the values they evaluated
+ * to. This macro is for use in unit tests.
+ *
+ * Since: 0.10.14
+ */
+#define assert_equals_float(a, b) fail_unless_equals_float(a, b)
/***
MAIN_START_THREAD_FUNCTIONS(count, function, data); \
MAIN_SYNCHRONIZE();
+#if GLIB_CHECK_VERSION (2, 31, 0)
+#define g_thread_create gst_g_thread_create
+static inline GThread *
+gst_g_thread_create (GThreadFunc func, gpointer data, gboolean joinable,
+ GError **error)
+{
+ g_assert (joinable);
+ return g_thread_try_new ("gst-check", func, data, error);
+}
+#endif
+
#define MAIN_INIT() \
G_STMT_START { \
_gst_check_threads_running = TRUE; \
\
- mutex = g_mutex_new (); \
- start_cond = g_cond_new (); \
- sync_cond = g_cond_new (); \
+ if (mutex == NULL) { \
+ mutex = g_mutex_new (); \
+ start_cond = g_cond_new (); \
+ sync_cond = g_cond_new (); \
+ } \
} G_STMT_END;
#define MAIN_START_THREAD_FUNCTIONS(count, function, data) \
#define MAIN_START_THREAD_FUNCTION(i, function, data) \
G_STMT_START { \
GThread *thread = NULL; \
- g_message ("MAIN: creating thread %d\n", i); \
+ GST_DEBUG ("MAIN: creating thread %d", i); \
g_mutex_lock (mutex); \
thread = g_thread_create ((GThreadFunc) function, data, \
TRUE, NULL); \
/* wait for thread to signal us that it's ready */ \
- g_message ("MAIN: waiting for thread %d\n", i); \
+ GST_DEBUG ("MAIN: waiting for thread %d", i); \
g_cond_wait (start_cond, mutex); \
g_mutex_unlock (mutex); \
\
#define MAIN_SYNCHRONIZE() \
G_STMT_START { \
- g_message ("MAIN: synchronizing\n"); \
+ GST_DEBUG ("MAIN: synchronizing"); \
g_cond_broadcast (sync_cond); \
- g_message ("MAIN: synchronized\n"); \
+ GST_DEBUG ("MAIN: synchronized"); \
} G_STMT_END;
#define MAIN_STOP_THREADS() \
_gst_check_threads_running = FALSE; \
\
/* join all threads */ \
- g_message ("MAIN: joining\n"); \
+ GST_DEBUG ("MAIN: joining"); \
g_list_foreach (thread_list, (GFunc) g_thread_join, NULL); \
- g_message ("MAIN: joined\n"); \
+ g_list_free (thread_list); \
+ thread_list = NULL; \
+ GST_DEBUG ("MAIN: joined"); \
} G_STMT_END;
#define THREAD_START() \
#define THREAD_STARTED() \
G_STMT_START { \
/* signal main thread that we started */ \
- g_message ("THREAD %p: started\n", g_thread_self ()); \
+ GST_DEBUG ("THREAD %p: started", g_thread_self ()); \
g_mutex_lock (mutex); \
g_cond_signal (start_cond); \
} G_STMT_END;
#define THREAD_SYNCHRONIZE() \
G_STMT_START { \
/* synchronize everyone */ \
- g_message ("THREAD %p: syncing\n", g_thread_self ()); \
+ GST_DEBUG ("THREAD %p: syncing", g_thread_self ()); \
g_cond_wait (sync_cond, mutex); \
- g_message ("THREAD %p: synced\n", g_thread_self ()); \
+ GST_DEBUG ("THREAD %p: synced", g_thread_self ()); \
g_mutex_unlock (mutex); \
} G_STMT_END;
_gst_check_raised_critical = FALSE; \
code; \
_fail_unless (_gst_check_raised_critical, __FILE__, __LINE__, \
- "Expected g_critical, got nothing: '"#code"'"); \
+ "Expected g_critical, got nothing", NULL); \
_gst_check_expecting_log = FALSE; \
} G_STMT_END
+#define ASSERT_WARNING(code) \
+G_STMT_START { \
+ _gst_check_expecting_log = TRUE; \
+ _gst_check_raised_warning = FALSE; \
+ code; \
+ _fail_unless (_gst_check_raised_warning, __FILE__, __LINE__, \
+ "Expected g_warning, got nothing", NULL); \
+ _gst_check_expecting_log = FALSE; \
+} G_STMT_END
+
+
#define ASSERT_OBJECT_REFCOUNT(object, name, value) \
G_STMT_START { \
int rc; \
rc = GST_OBJECT_REFCOUNT_VALUE (object); \
fail_unless (rc == value, \
- "%s refcount is %d instead of %d", name, rc, value); \
+ "%s (%p) refcount is %d instead of %d", \
+ name, object, rc, value); \
} G_STMT_END
+#define ASSERT_OBJECT_REFCOUNT_BETWEEN(object, name, lower, upper) \
+G_STMT_START { \
+ int rc = GST_OBJECT_REFCOUNT_VALUE (object); \
+ int lo = lower; \
+ int hi = upper; \
+ \
+ fail_unless (rc >= lo, \
+ "%s (%p) refcount %d is smaller than %d", \
+ name, object, rc, lo); \
+ fail_unless (rc <= hi, \
+ "%s (%p) refcount %d is bigger than %d", \
+ name, object, rc, hi); \
+} G_STMT_END
+
+
#define ASSERT_CAPS_REFCOUNT(caps, name, value) \
ASSERT_MINI_OBJECT_REFCOUNT(caps, name, value)
name " refcount is %d instead of %d", rc, value);\
} G_STMT_END
+#define ASSERT_SET_STATE(element, state, ret) \
+fail_unless (gst_element_set_state (element, \
+ state) == ret, \
+ "could not change state to " #state);
-#endif /* __GST_CHECK_H__ */
+#define GST_CHECK_MAIN(name) \
+int main (int argc, char **argv) \
+{ \
+ Suite *s; \
+ gst_check_init (&argc, &argv); \
+ s = name ## _suite (); \
+ return gst_check_run_suite (s, # name, __FILE__); \
+}
+
+/* Hack to allow run-time selection of unit tests to run via the
+ * GST_CHECKS environment variable (test function names, comma-separated) */
+
+gboolean _gst_check_run_test_func (const gchar * func_name);
+
+static inline void
+__gst_tcase_add_test (TCase * tc, TFun tf, const char * fname, int signal,
+ int allowed_exit_value, int start, int end)
+{
+ if (_gst_check_run_test_func (fname)) {
+ _tcase_add_test (tc, tf, fname, signal, allowed_exit_value, start, end);
+ }
+}
+#define _tcase_add_test __gst_tcase_add_test
+
+G_END_DECLS
+
+#endif /* __GST_CHECK_H__ */