index 68f7810d58a42571167ef24cb6230b0cbef0414d..e77c007bce3783f370ff579e4aa31b4e23dfc7f6 100644 (file)
#include <stdlib.h>
#include <math.h>
-#include <check.h>
+#include <gst/check/internal-check.h>
#include <gst/gst.h>
typedef struct
{
- char *name;
+ const char *name;
int size;
int abi_size;
}
GstElement *gst_check_setup_element (const gchar * factory);
void gst_check_teardown_element (GstElement * element);
GstPad *gst_check_setup_src_pad (GstElement * element,
- GstStaticPadTemplate * template, GstCaps * caps);
+ GstStaticPadTemplate * tmpl, GstCaps * caps);
GstPad * gst_check_setup_src_pad_by_name (GstElement * element,
- GstStaticPadTemplate * template, gchar *name);
+ GstStaticPadTemplate * tmpl, const gchar *name);
GstPad * gst_check_setup_sink_pad_by_name (GstElement * element,
- GstStaticPadTemplate * template, gchar *name);
-void gst_check_teardown_pad_by_name (GstElement * element, gchar *name);
+ GstStaticPadTemplate * tmpl, const gchar *name);
+void gst_check_teardown_pad_by_name (GstElement * element, const gchar *name);
void gst_check_teardown_src_pad (GstElement * element);
-void gst_check_drop_buffers ();
+void gst_check_drop_buffers (void);
void gst_check_caps_equal (GstCaps * caps1, GstCaps * caps2);
void gst_check_element_push_buffer_list (const gchar * element_name,
GList * buffer_in, GList * buffer_out, GstFlowReturn last_flow_return);
void gst_check_element_push_buffer (const gchar * element_name,
GstBuffer * buffer_in, GstBuffer * buffer_out);
GstPad *gst_check_setup_sink_pad (GstElement * element,
- GstStaticPadTemplate * template, GstCaps * caps);
+ GstStaticPadTemplate * tmpl, GstCaps * caps);
void gst_check_teardown_sink_pad (GstElement * element);
void gst_check_abi_list (GstCheckABIStruct list[], gboolean have_abi_sizes);
gint gst_check_run_suite (Suite * suite, const gchar * name,
*
* wrapper for checks END_TEST
*/
-#if CHECK_MAJOR_VERSION > 0 || \
- (CHECK_MAJOR_VERSION == 0 && CHECK_MINOR_VERSION > 9) || \
- (CHECK_MAJOR_VERSION == 0 && CHECK_MINOR_VERSION == 9 && CHECK_MICRO_VERSION > 3)
#define GST_START_TEST(__testname) \
static void __testname (int __i__)\
{\
GST_DEBUG ("test start"); \
tcase_fn_start (""# __testname, __FILE__, __LINE__);
-#define GST_END_TEST END_TEST
-#else
-#define GST_START_TEST(__testname) \
-static void __testname ()\
-{\
- GST_DEBUG ("test start"); \
- tcase_fn_start (""# __testname, __FILE__, __LINE__);
-
-#define GST_END_TEST END_TEST
-#endif
-
+#define GST_END_TEST GST_LOG ("cleaning up tasks"); \
+ gst_task_cleanup_all (); \
+ END_TEST
/* additional fail macros */
/**
*/
#define assert_equals_int(a, b) fail_unless_equals_int(a, b)
+/**
+ * fail_unless_equals_int64:
+ * @a: a #gint64 value or expression
+ * @b: a #gint64 value or expression
+ *
+ * This macro checks that @a and @b are equal and aborts if this is not the
+ * case, printing both expressions and the values they evaluated to. This
+ * macro is for use in unit tests.
+ */
+#define fail_unless_equals_int64(a, b) \
+G_STMT_START { \
+ gint64 first = a; \
+ gint64 second = b; \
+ fail_unless(first == second, \
+ "'" #a "' (%" G_GINT64_FORMAT") is not equal to '" #b"' (%" \
+ G_GINT64_FORMAT")", first, second); \
+} G_STMT_END;
+/**
+ * assert_equals_int64:
+ * @a: a #gint64 value or expression
+ * @b: a #gint64 value or expression
+ *
+ * This macro checks that @a and @b are equal and aborts if this is not the
+ * case, printing both expressions and the values they evaluated to. This
+ * macro is for use in unit tests.
+ */
+#define assert_equals_int64(a, b) fail_unless_equals_int64(a, b)
+
/**
* fail_unless_equals_uint64:
* @a: a #guint64 value or expression
G_STMT_START { \
const gchar * first = a; \
const gchar * second = b; \
- fail_unless(strcmp (first, second) == 0, \
+ fail_unless(g_strcmp0 (first, second) == 0, \
"'" #a "' (%s) is not equal to '" #b"' (%s)", first, second); \
} G_STMT_END;
/**
MAIN_START_THREAD_FUNCTIONS(count, function, data); \
MAIN_SYNCHRONIZE();
+#if GLIB_CHECK_VERSION (2, 31, 0)
+#define g_thread_create gst_g_thread_create
+static inline GThread *
+gst_g_thread_create (GThreadFunc func, gpointer data, gboolean joinable,
+ GError **error)
+{
+ g_assert (joinable);
+ return g_thread_try_new ("gst-check", func, data, error);
+}
+#endif
+
#define MAIN_INIT() \
G_STMT_START { \
_gst_check_threads_running = TRUE; \
\
- mutex = g_mutex_new (); \
- start_cond = g_cond_new (); \
- sync_cond = g_cond_new (); \
+ if (mutex == NULL) { \
+ mutex = g_mutex_new (); \
+ start_cond = g_cond_new (); \
+ sync_cond = g_cond_new (); \
+ } \
} G_STMT_END;
#define MAIN_START_THREAD_FUNCTIONS(count, function, data) \
/* join all threads */ \
GST_DEBUG ("MAIN: joining"); \
g_list_foreach (thread_list, (GFunc) g_thread_join, NULL); \
+ g_list_free (thread_list); \
+ thread_list = NULL; \
GST_DEBUG ("MAIN: joined"); \
} G_STMT_END;
#define GST_CHECK_MAIN(name) \
int main (int argc, char **argv) \
{ \
- Suite *s = name ## _suite (); \
+ Suite *s; \
gst_check_init (&argc, &argv); \
+ s = name ## _suite (); \
return gst_check_run_suite (s, # name, __FILE__); \
}
gboolean _gst_check_run_test_func (const gchar * func_name);
-#if CHECK_MAJOR_VERSION > 0 || \
- (CHECK_MAJOR_VERSION == 0 && CHECK_MINOR_VERSION > 9) || \
- (CHECK_MAJOR_VERSION == 0 && CHECK_MINOR_VERSION == 9 && CHECK_MICRO_VERSION > 3)
static inline void
__gst_tcase_add_test (TCase * tc, TFun tf, const char * fname, int signal,
- int start, int end)
-{
- if (_gst_check_run_test_func (fname)) {
- _tcase_add_test (tc, tf, fname, signal, start, end);
- }
-}
-#else
-static inline void
-__gst_tcase_add_test (TCase * tc, TFun tf, const char * fname, int signal)
+ int allowed_exit_value, int start, int end)
{
if (_gst_check_run_test_func (fname)) {
- _tcase_add_test (tc, tf, fname, signal);
+ _tcase_add_test (tc, tf, fname, signal, allowed_exit_value, start, end);
}
}
-#endif
#define _tcase_add_test __gst_tcase_add_test