index 2fdbc5fc74c1444c27cc879147cc593da08b0ce8..7c39492beaf0d7ead988a8b2a6e050a142a0f8ed 100644 (file)
gst_dp_crc (const guint8 * buffer, register guint length)
{
static gboolean initialized = FALSE;
- static guint16 crc_register, crc_table[256];
+ static guint16 crc_table[256];
+ guint16 crc_register;
unsigned long i, j, k;
if (!initialized) {
{
int i;
int n = 8; /* number of bytes per line */
- gchar *line = g_malloc (3 * n);
+ gchar *line = g_malloc (3 * n + 1);
GST_LOG ("dumping byte array of length %d", length);
for (i = 0; i < length; ++i) {
*
* Initialize GStreamer Data Protocol library.
*
- * Should be called before using these functions; either from source linking
- * to this source file or from plugin_init.
+ * Should be called before using these functions from source linking
+ * to this source file.
*/
void
gst_dp_init (void)
*
* Creates a GDP header from the given buffer.
*
- * Returns: %TRUE if the header was successfully created
+ * Returns: %TRUE if the header was successfully created.
*/
gboolean
guint16 flags_mask;
g_return_val_if_fail (GST_IS_BUFFER (buffer), FALSE);
- g_return_val_if_fail (GST_BUFFER_REFCOUNT_VALUE (buffer) > 0, FALSE);
g_return_val_if_fail (header, FALSE);
*length = GST_DP_HEADER_LENGTH;
h[0] = (guint8) GST_DP_VERSION_MAJOR;
h[1] = (guint8) GST_DP_VERSION_MINOR;
h[2] = (guint8) flags;
- h[3] = GST_DP_PAYLOAD_BUFFER;
+ h[3] = 0; /* padding byte */
+ GST_WRITE_UINT16_BE (h + 4, GST_DP_PAYLOAD_BUFFER);
/* buffer properties */
- GST_WRITE_UINT32_BE (h + 4, GST_BUFFER_SIZE (buffer));
- GST_WRITE_UINT64_BE (h + 8, GST_BUFFER_TIMESTAMP (buffer));
- GST_WRITE_UINT64_BE (h + 16, GST_BUFFER_DURATION (buffer));
- GST_WRITE_UINT64_BE (h + 24, GST_BUFFER_OFFSET (buffer));
- GST_WRITE_UINT64_BE (h + 32, GST_BUFFER_OFFSET_END (buffer));
+ GST_WRITE_UINT32_BE (h + 6, GST_BUFFER_SIZE (buffer));
+ GST_WRITE_UINT64_BE (h + 10, GST_BUFFER_TIMESTAMP (buffer));
+ GST_WRITE_UINT64_BE (h + 18, GST_BUFFER_DURATION (buffer));
+ GST_WRITE_UINT64_BE (h + 26, GST_BUFFER_OFFSET (buffer));
+ GST_WRITE_UINT64_BE (h + 34, GST_BUFFER_OFFSET_END (buffer));
/* data flags */
- /* we only copy KEY_UNIT and IN_CAPS flags */
- flags_mask = GST_DATA_FLAG_SHIFT (GST_BUFFER_KEY_UNIT) |
- GST_DATA_FLAG_SHIFT (GST_BUFFER_IN_CAPS);
+ /* we only copy KEY_UNIT,DELTA_UNIT and IN_CAPS flags */
+ flags_mask = GST_BUFFER_FLAG_PREROLL | GST_BUFFER_FLAG_IN_CAPS |
+ GST_BUFFER_FLAG_DELTA_UNIT;
- GST_WRITE_UINT16_BE (h + 40, GST_BUFFER_FLAGS (buffer) & flags_mask);
+ GST_WRITE_UINT16_BE (h + 42, GST_BUFFER_FLAGS (buffer) & flags_mask);
/* ABI padding */
- GST_WRITE_UINT16_BE (h + 42, (guint64) 0);
GST_WRITE_UINT32_BE (h + 44, (guint64) 0);
GST_WRITE_UINT64_BE (h + 48, (guint64) 0);
crc = 0;
if (flags & GST_DP_HEADER_FLAG_CRC_HEADER) {
/* we don't crc the last four bytes of the header since they are crc's */
- crc = gst_dp_crc (h, 56);
+ crc = gst_dp_crc (h, 58);
}
- GST_WRITE_UINT16_BE (h + 56, crc);
+ GST_WRITE_UINT16_BE (h + 58, crc);
crc = 0;
if (flags & GST_DP_HEADER_FLAG_CRC_PAYLOAD) {
crc = gst_dp_crc (GST_BUFFER_DATA (buffer), GST_BUFFER_SIZE (buffer));
}
- GST_WRITE_UINT16_BE (h + 58, crc);
+ GST_WRITE_UINT16_BE (h + 60, crc);
GST_LOG ("created header from buffer:");
gst_dp_dump_byte_array (h, GST_DP_HEADER_LENGTH);
*
* Creates a GDP packet from the given caps.
*
- * Returns: %TRUE if the packet was successfully created
+ * Returns: %TRUE if the packet was successfully created.
*/
gboolean
gst_dp_packet_from_caps (const GstCaps * caps, GstDPHeaderFlag flags,
{
guint8 *h;
guint16 crc;
- gchar *string;
+ guchar *string;
/* FIXME: GST_IS_CAPS doesn't work
g_return_val_if_fail (GST_IS_CAPS (caps), FALSE); */
*length = GST_DP_HEADER_LENGTH;
h = g_malloc (GST_DP_HEADER_LENGTH);
- string = gst_caps_to_string (caps);
+ string = (guchar *) gst_caps_to_string (caps);
/* version, flags, type */
h[0] = (guint8) GST_DP_VERSION_MAJOR;
h[1] = (guint8) GST_DP_VERSION_MINOR;
h[2] = (guint8) flags;
- h[3] = GST_DP_PAYLOAD_CAPS;
+ h[3] = 0; /* padding bytes */
+ GST_WRITE_UINT16_BE (h + 4, GST_DP_PAYLOAD_CAPS);
/* buffer properties */
- GST_WRITE_UINT32_BE (h + 4, strlen (string) + 1); /* include trailing 0 */
- GST_WRITE_UINT64_BE (h + 8, (guint64) 0);
- GST_WRITE_UINT64_BE (h + 16, (guint64) 0);
- GST_WRITE_UINT64_BE (h + 24, (guint64) 0);
- GST_WRITE_UINT64_BE (h + 32, (guint64) 0);
+ GST_WRITE_UINT32_BE (h + 8, strlen ((gchar *) string) + 1); /* include trailing 0 */
+ GST_WRITE_UINT64_BE (h + 10, (guint64) 0);
+ GST_WRITE_UINT64_BE (h + 18, (guint64) 0);
+ GST_WRITE_UINT64_BE (h + 26, (guint64) 0);
+ GST_WRITE_UINT64_BE (h + 34, (guint64) 0);
/* ABI padding */
- GST_WRITE_UINT64_BE (h + 40, (guint64) 0);
- GST_WRITE_UINT64_BE (h + 48, (guint64) 0);
+ GST_WRITE_UINT64_BE (h + 42, (guint64) 0);
+ GST_WRITE_UINT64_BE (h + 50, (guint64) 0);
/* CRC */
crc = 0;
if (flags & GST_DP_HEADER_FLAG_CRC_HEADER) {
- crc = gst_dp_crc (h, 56);
+ crc = gst_dp_crc (h, 58);
}
- GST_WRITE_UINT16_BE (h + 56, crc);
+ GST_WRITE_UINT16_BE (h + 58, crc);
crc = 0;
if (flags & GST_DP_HEADER_FLAG_CRC_PAYLOAD) {
- crc = gst_dp_crc (string, strlen (string) + 1);
+ crc = gst_dp_crc (string, strlen ((gchar *) string) + 1);
}
- GST_WRITE_UINT16_BE (h + 58, crc);
+ GST_WRITE_UINT16_BE (h + 60, crc);
GST_LOG ("created header from caps:");
gst_dp_dump_byte_array (h, GST_DP_HEADER_LENGTH);
*
* Creates a GDP packet from the given event.
*
- * Returns: %TRUE if the packet was successfully created
+ * Returns: %TRUE if the packet was successfully created.
*/
gboolean
gst_dp_packet_from_event (const GstEvent * event, GstDPHeaderFlag flags,
g_free (h);
return FALSE;
case GST_EVENT_EOS:
- case GST_EVENT_FLUSH:
- case GST_EVENT_EMPTY:
- case GST_EVENT_DISCONTINUOUS:
- GST_WRITE_UINT64_BE (h + 8, GST_EVENT_TIMESTAMP (event));
+ case GST_EVENT_FLUSH_START:
+ case GST_EVENT_FLUSH_STOP:
+ case GST_EVENT_NEWSEGMENT:
pl_length = 0;
*payload = NULL;
break;
case GST_EVENT_SEEK:
- pl_length = 4 + 8 + 4;
- *payload = g_malloc0 (pl_length);
- GST_WRITE_UINT32_BE (*payload, (guint32) GST_EVENT_SEEK_TYPE (event));
- GST_WRITE_UINT64_BE (*payload + 4,
- (guint64) GST_EVENT_SEEK_OFFSET (event));
- GST_WRITE_UINT32_BE (*payload + 12,
- (guint32) GST_EVENT_SEEK_ACCURACY (event));
- break;
- case GST_EVENT_SEEK_SEGMENT:
- pl_length = 4 + 8 + 8 + 4;
+ {
+ gdouble rate;
+ GstFormat format;
+ GstSeekFlags flags;
+ GstSeekType cur_type, stop_type;
+ gint64 cur, stop;
+
+ gst_event_parse_seek ((GstEvent *) event, &rate, &format, &flags,
+ &cur_type, &cur, &stop_type, &stop);
+
+ pl_length = 4 + 4 + 4 + 8 + 4 + 8;
*payload = g_malloc0 (pl_length);
- GST_WRITE_UINT32_BE (*payload, (guint32) GST_EVENT_SEEK_TYPE (event));
- GST_WRITE_UINT64_BE (*payload + 4,
- (guint64) GST_EVENT_SEEK_OFFSET (event));
- GST_WRITE_UINT64_BE (*payload + 12,
- (guint64) GST_EVENT_SEEK_ENDOFFSET (event));
- GST_WRITE_UINT32_BE (*payload + 20,
- (guint32) GST_EVENT_SEEK_ACCURACY (event));
+ /* FIXME write rate */
+ GST_WRITE_UINT32_BE (*payload, (guint32) format);
+ GST_WRITE_UINT32_BE (*payload + 4, (guint32) flags);
+ GST_WRITE_UINT32_BE (*payload + 8, (guint32) cur_type);
+ GST_WRITE_UINT64_BE (*payload + 12, (guint64) cur);
+ GST_WRITE_UINT32_BE (*payload + 20, (guint32) stop_type);
+ GST_WRITE_UINT64_BE (*payload + 24, (guint64) stop);
break;
+ }
case GST_EVENT_QOS:
- case GST_EVENT_SEGMENT_DONE:
- case GST_EVENT_SIZE:
- case GST_EVENT_RATE:
- case GST_EVENT_FILLER:
- case GST_EVENT_TS_OFFSET:
- case GST_EVENT_INTERRUPT:
case GST_EVENT_NAVIGATION:
case GST_EVENT_TAG:
g_warning ("Unhandled event type %d, ignoring", GST_EVENT_TYPE (event));
h[0] = (guint8) GST_DP_VERSION_MAJOR;
h[1] = (guint8) GST_DP_VERSION_MINOR;
h[2] = (guint8) flags;
- h[3] = GST_DP_PAYLOAD_EVENT_NONE + GST_EVENT_TYPE (event);
+ h[3] = 0; /* padding byte */
+ GST_WRITE_UINT16_BE (h + 4,
+ GST_DP_PAYLOAD_EVENT_NONE + GST_EVENT_TYPE (event));
/* length */
- GST_WRITE_UINT32_BE (h + 4, (guint32) pl_length);
+ GST_WRITE_UINT32_BE (h + 6, (guint32) pl_length);
/* timestamp */
- GST_WRITE_UINT64_BE (h + 8, GST_EVENT_TIMESTAMP (event));
+ GST_WRITE_UINT64_BE (h + 10, GST_EVENT_TIMESTAMP (event));
/* ABI padding */
- GST_WRITE_UINT64_BE (h + 40, (guint64) 0);
- GST_WRITE_UINT64_BE (h + 48, (guint64) 0);
+ GST_WRITE_UINT64_BE (h + 42, (guint64) 0);
+ GST_WRITE_UINT64_BE (h + 50, (guint64) 0);
/* CRC */
crc = 0;
if (flags & GST_DP_HEADER_FLAG_CRC_HEADER) {
- crc = gst_dp_crc (h, 56);
+ crc = gst_dp_crc (h, 58);
}
- GST_WRITE_UINT16_BE (h + 56, crc);
+ GST_WRITE_UINT16_BE (h + 58, crc);
crc = 0;
/* events can have a NULL payload */
if (*payload && flags & GST_DP_HEADER_FLAG_CRC_PAYLOAD) {
- crc = gst_dp_crc (*payload, strlen (*payload) + 1);
+ crc = gst_dp_crc (*payload, strlen ((gchar *) * payload) + 1);
}
- GST_WRITE_UINT16_BE (h + 58, crc);
+ GST_WRITE_UINT16_BE (h + 60, crc);
GST_LOG ("created header from event:");
gst_dp_dump_byte_array (h, GST_DP_HEADER_LENGTH);
* Use this function if you want to pre-allocate a buffer based on the
* packet header to read the packet payload in to.
*
- * Returns: %TRUE if the buffer was successfully created
+ * Returns: %TRUE if the buffer was successfully created.
*/
GstBuffer *
gst_dp_buffer_from_header (guint header_length, const guint8 * header)
GstBuffer *buffer;
g_return_val_if_fail (GST_DP_HEADER_PAYLOAD_TYPE (header) ==
- GST_DP_PAYLOAD_BUFFER, FALSE);
+ GST_DP_PAYLOAD_BUFFER, NULL);
buffer =
gst_buffer_new_and_alloc ((guint) GST_DP_HEADER_PAYLOAD_LENGTH (header));
GST_BUFFER_TIMESTAMP (buffer) = GST_DP_HEADER_TIMESTAMP (header);
*
* Creates a newly allocated #GstCaps from the given packet.
*
- * Returns: %TRUE if the caps was successfully created
+ * Returns: %TRUE if the caps was successfully created.
*/
GstCaps *
gst_dp_caps_from_packet (guint header_length, const guint8 * header,
GstCaps *caps;
const gchar *string;
- g_return_val_if_fail (header, FALSE);
- g_return_val_if_fail (payload, FALSE);
+ g_return_val_if_fail (header, NULL);
+ g_return_val_if_fail (payload, NULL);
g_return_val_if_fail (GST_DP_HEADER_PAYLOAD_TYPE (header) ==
- GST_DP_PAYLOAD_CAPS, FALSE);
+ GST_DP_PAYLOAD_CAPS, NULL);
- string = payload;
+ string = (gchar *) payload;
caps = gst_caps_from_string (string);
return caps;
}
*
* Creates a newly allocated #GstEvent from the given packet.
*
- * Returns: %TRUE if the event was successfully created
+ * Returns: %TRUE if the event was successfully created.
*/
GstEvent *
gst_dp_event_from_packet (guint header_length, const guint8 * header,
GstEvent *event = NULL;
GstEventType type;
- g_return_val_if_fail (header, FALSE);
+ g_return_val_if_fail (header, NULL);
/* payload can be NULL, e.g. for an EOS event */
type = GST_DP_HEADER_PAYLOAD_TYPE (header) - GST_DP_PAYLOAD_EVENT_NONE;
g_warning ("Unknown event, ignoring");
return FALSE;
case GST_EVENT_EOS:
- case GST_EVENT_FLUSH:
- case GST_EVENT_EMPTY:
- case GST_EVENT_DISCONTINUOUS:
- event = gst_event_new (type);
+ case GST_EVENT_FLUSH_START:
+ case GST_EVENT_FLUSH_STOP:
+ case GST_EVENT_NEWSEGMENT:
+ event = gst_event_new_custom (type, NULL);
GST_EVENT_TIMESTAMP (event) = GST_DP_HEADER_TIMESTAMP (header);
break;
case GST_EVENT_SEEK:
{
- GstSeekType type;
- gint64 offset;
- GstSeekAccuracy accuracy;
-
- type = (GstSeekType) GST_READ_UINT32_BE (payload);
- offset = (gint64) GST_READ_UINT64_BE (payload + 4);
- accuracy = (GstSeekAccuracy) GST_READ_UINT32_BE (payload + 12);
- event = gst_event_new_seek (type, offset);
- GST_EVENT_TIMESTAMP (event) = GST_DP_HEADER_TIMESTAMP (header);
- GST_EVENT_SEEK_ACCURACY (event) = accuracy;
- break;
- }
- case GST_EVENT_SEEK_SEGMENT:
- {
- GstSeekType type;
- gint64 offset, endoffset;
- GstSeekAccuracy accuracy;
-
- type = (GstSeekType) GST_READ_UINT32_BE (payload);
- offset = (gint64) GST_READ_UINT64_BE (payload + 4);
- endoffset = (gint64) GST_READ_UINT64_BE (payload + 12);
- accuracy = (GstSeekAccuracy) GST_READ_UINT32_BE (payload + 20);
- event = gst_event_new_segment_seek (type, offset, endoffset);
+ gdouble rate;
+ GstFormat format;
+ GstSeekFlags flags;
+ GstSeekType cur_type, stop_type;
+ gint64 cur, stop;
+
+ /* FIXME, read rate */
+ rate = 1.0;
+ format = (GstFormat) GST_READ_UINT32_BE (payload);
+ flags = (GstSeekFlags) GST_READ_UINT32_BE (payload + 4);
+ cur_type = (GstSeekType) GST_READ_UINT32_BE (payload + 8);
+ cur = (gint64) GST_READ_UINT64_BE (payload + 12);
+ stop_type = (GstSeekType) GST_READ_UINT32_BE (payload + 20);
+ stop = (gint64) GST_READ_UINT64_BE (payload + 24);
+
+ event = gst_event_new_seek (rate, format, flags, cur_type, cur,
+ stop_type, stop);
GST_EVENT_TIMESTAMP (event) = GST_DP_HEADER_TIMESTAMP (header);
- GST_EVENT_SEEK_ACCURACY (event) = accuracy;
break;
}
case GST_EVENT_QOS:
- case GST_EVENT_SEGMENT_DONE:
- case GST_EVENT_SIZE:
- case GST_EVENT_RATE:
- case GST_EVENT_FILLER:
- case GST_EVENT_TS_OFFSET:
- case GST_EVENT_INTERRUPT:
case GST_EVENT_NAVIGATION:
case GST_EVENT_TAG:
g_warning ("Unhandled event type %d, ignoring", GST_EVENT_TYPE (event));
*
* Validates the given packet header by checking the CRC checksum.
*
- * Returns: %TRUE if the CRC matches, or no CRC checksum is present
+ * Returns: %TRUE if the CRC matches, or no CRC checksum is present.
*/
gboolean
gst_dp_validate_header (guint header_length, const guint8 * header)
* Validates the given packet payload using the given packet header
* by checking the CRC checksum.
*
- * Returns: %TRUE if the CRC matches, or no CRC checksum is present
+ * Returns: %TRUE if the CRC matches, or no CRC checksum is present.
*/
gboolean
gst_dp_validate_payload (guint header_length, const guint8 * header,
*
* Validates the given packet by checking version information and checksums.
*
- * Returns: %TRUE if the packet validates
+ * Returns: %TRUE if the packet validates.
*/
gboolean
gst_dp_validate_packet (guint header_length, const guint8 * header,
return TRUE;
}
-
-/*** PLUGIN STUFF ***/
-static gboolean
-plugin_init (GstPlugin * plugin)
-{
- gst_dp_init ();
-
- return TRUE;
-}
-
-GST_PLUGIN_DEFINE (GST_VERSION_MAJOR,
- GST_VERSION_MINOR,
- "gstdataprotocol",
- "a data protocol to serialize buffers, caps and events",
- plugin_init, VERSION, GST_LICENSE, GST_PACKAGE, GST_ORIGIN)