index babefbd3c4e9a2567fe783c41c99a940b85dd9b4..b57d377d6939ee1551461b2cf71d4e8b0d088743 100644 (file)
/* GStreamer
* Copyright (C) <1999> Erik Walthinsen <omega@cse.ogi.edu>
- * Copyright (C) <2004> Thomas Vander Stichele <thomas at apestaart dot org>
+ * Copyright (C) 2004,2006 Thomas Vander Stichele <thomas at apestaart dot org>
*
* dataprotocol.c: Functions implementing the GStreamer Data Protocol
*
* Boston, MA 02111-1307, USA.
*/
+/**
+ * SECTION:gstdataprotocol
+ * @short_description: Serialization of caps, buffers and events.
+ * @see_also: #GstCaps, #GstEvent, #GstBuffer
+ *
+ * This helper library provides serialization of GstBuffer, GstCaps and
+ * GstEvent structures.
+ *
+ * This serialization is useful when GStreamer needs to interface with
+ * the outside world to transport data between distinct GStreamer pipelines.
+ * The connections with the outside world generally don't have mechanisms
+ * to transport properties of these structures.
+ *
+ * For example, transporting buffers across named pipes or network connections
+ * doesn't maintain the buffer size and separation.
+ *
+ * This data protocol assumes a reliable connection-oriented transport, such as
+ * TCP, a pipe, or a file. The protocol does not serialize the caps for
+ * each buffer; instead, it transport the caps only when they change in the
+ * stream. This implies that there will always be a caps packet before any
+ * buffer packets.
+ *
+ * The versioning of the protocol is independent of GStreamer's version.
+ * The major number gets incremented, and the minor reset, for incompatible
+ * changes. The minor number gets incremented for compatible changes that
+ * allow clients who do not completely understand the newer protocol version
+ * to still decode what they do understand.
+ *
+ * Version 0.2 serializes only a small subset of all events, with a custom
+ * payload for each type. Also, all GDP streams start with the initial caps
+ * packet.
+ *
+ * Version 1.0 serializes all events by taking the string representation of
+ * the event as the payload. In addition, GDP streams can now start with
+ * events as well, as required by the new data stream model in GStreamer 0.10.
+ *
+ * Converting buffers, caps and events to GDP buffers is done using a
+ * #GstDPPacketizer object and invoking its packetizer functions.
+ * For backwards-compatibility reasons, the old 0.2 methods are still
+ * available but deprecated.
+ *
+ * For reference, this image shows the byte layout of the GDP header:
+ *
+ * <inlinegraphic format="PNG" fileref="gdp-header.png"></inlinegraphic>
+ */
+
#ifdef HAVE_CONFIG_H
#include "config.h"
#endif
#include "dp-private.h"
/* debug category */
-GST_DEBUG_CATEGORY (data_protocol_debug);
+GST_DEBUG_CATEGORY_STATIC (data_protocol_debug);
#define GST_CAT_DEFAULT data_protocol_debug
+/* helper macros */
+
+/* write first 6 bytes of header */
+#define GST_DP_INIT_HEADER(h, version, flags, type) \
+G_STMT_START { \
+ gint maj = 0, min = 0; \
+ switch (version) { \
+ case GST_DP_VERSION_0_2: maj = 0; min = 2; break; \
+ case GST_DP_VERSION_1_0: maj = 1; min = 0; break; \
+ } \
+ h[0] = (guint8) maj; \
+ h[1] = (guint8) min; \
+ h[2] = (guint8) flags; \
+ h[3] = 0; /* padding byte */ \
+ GST_WRITE_UINT16_BE (h + 4, type); \
+} G_STMT_END
+
+#define GST_DP_SET_CRC(h, flags, payload, length); \
+G_STMT_START { \
+ guint16 crc = 0; \
+ if (flags & GST_DP_HEADER_FLAG_CRC_HEADER) \
+ /* we don't crc the last four bytes since they are crc's */ \
+ crc = gst_dp_crc (h, 58); \
+ GST_WRITE_UINT16_BE (h + 58, crc); \
+ \
+ crc = 0; \
+ if (length && (flags & GST_DP_HEADER_FLAG_CRC_PAYLOAD)) \
+ crc = gst_dp_crc (payload, length); \
+ GST_WRITE_UINT16_BE (h + 60, crc); \
+} G_STMT_END
+
/* calculate a CCITT 16 bit CRC check value for a given byte array */
/*
* this code snippet is adapted from a web page I found
#define POLY 0x1021
#define CRC_INIT 0xFFFF
-static guint16
-gst_dp_crc (const guint8 * buffer, register guint length)
+/*** HELPER FUNCTIONS ***/
+
+static gboolean
+gst_dp_header_from_buffer_any (const GstBuffer * buffer, GstDPHeaderFlag flags,
+ guint * length, guint8 ** header, GstDPVersion version)
{
- static gboolean initialized = FALSE;
- static guint16 crc_table[256];
- guint16 crc_register;
- unsigned long i, j, k;
-
- if (!initialized) {
- for (i = 0; i < 256; i++) {
- j = i << 8;
- for (k = 8; k--;) {
- j = j & 0x8000 ? (j << 1) ^ POLY : j << 1;
- }
-
- crc_table[i] = (guint16) j;
- }
- initialized = TRUE;
- }
+ guint8 *h;
+ guint16 flags_mask;
+
+ g_return_val_if_fail (GST_IS_BUFFER (buffer), FALSE);
+ g_return_val_if_fail (length, FALSE);
+ g_return_val_if_fail (header, FALSE);
+
+ *length = GST_DP_HEADER_LENGTH;
+ h = g_malloc0 (GST_DP_HEADER_LENGTH);
+
+ /* version, flags, type */
+ GST_DP_INIT_HEADER (h, version, flags, GST_DP_PAYLOAD_BUFFER);
+
+ /* buffer properties */
+ GST_WRITE_UINT32_BE (h + 6, GST_BUFFER_SIZE (buffer));
+ GST_WRITE_UINT64_BE (h + 10, GST_BUFFER_TIMESTAMP (buffer));
+ GST_WRITE_UINT64_BE (h + 18, GST_BUFFER_DURATION (buffer));
+ GST_WRITE_UINT64_BE (h + 26, GST_BUFFER_OFFSET (buffer));
+ GST_WRITE_UINT64_BE (h + 34, GST_BUFFER_OFFSET_END (buffer));
+
+ /* data flags; eats two bytes from the ABI area */
+ /* we copy everything but the read-only flags */
+ flags_mask = GST_BUFFER_FLAG_PREROLL | GST_BUFFER_FLAG_DISCONT |
+ GST_BUFFER_FLAG_IN_CAPS | GST_BUFFER_FLAG_GAP |
+ GST_BUFFER_FLAG_DELTA_UNIT;
+
+ GST_WRITE_UINT16_BE (h + 42, GST_BUFFER_FLAGS (buffer) & flags_mask);
+
+ GST_DP_SET_CRC (h, flags, GST_BUFFER_DATA (buffer), GST_BUFFER_SIZE (buffer));
+
+ GST_LOG ("created header from buffer:");
+ gst_dp_dump_byte_array (h, GST_DP_HEADER_LENGTH);
+ *header = h;
+ return TRUE;
+}
+
+static gboolean
+gst_dp_packet_from_caps_any (const GstCaps * caps, GstDPHeaderFlag flags,
+ guint * length, guint8 ** header, guint8 ** payload, GstDPVersion version)
+{
+ guint8 *h;
+ guchar *string;
+ guint payload_length;
+
+ g_return_val_if_fail (GST_IS_CAPS (caps), FALSE);
+ g_return_val_if_fail (length, FALSE);
+ g_return_val_if_fail (header, FALSE);
+ g_return_val_if_fail (payload, FALSE);
+
+ *length = GST_DP_HEADER_LENGTH;
+ h = g_malloc0 (GST_DP_HEADER_LENGTH);
+
+ string = (guchar *) gst_caps_to_string (caps);
+ payload_length = strlen ((gchar *) string) + 1; /* include trailing 0 */
+
+ /* version, flags, type */
+ GST_DP_INIT_HEADER (h, version, flags, GST_DP_PAYLOAD_CAPS);
+
+ /* buffer properties */
+ GST_WRITE_UINT32_BE (h + 6, payload_length);
+ GST_WRITE_UINT64_BE (h + 10, (guint64) 0);
+ GST_WRITE_UINT64_BE (h + 18, (guint64) 0);
+ GST_WRITE_UINT64_BE (h + 26, (guint64) 0);
+ GST_WRITE_UINT64_BE (h + 34, (guint64) 0);
+
+ GST_DP_SET_CRC (h, flags, string, payload_length);
+
+ GST_LOG ("created header from caps:");
+ gst_dp_dump_byte_array (h, GST_DP_HEADER_LENGTH);
+ *header = h;
+ *payload = string;
+ return TRUE;
+}
+
+
+/*** PUBLIC FUNCTIONS ***/
+
+static const guint16 gst_dp_crc_table[256] = {
+ 0x0000, 0x1021, 0x2042, 0x3063, 0x4084, 0x50a5, 0x60c6, 0x70e7,
+ 0x8108, 0x9129, 0xa14a, 0xb16b, 0xc18c, 0xd1ad, 0xe1ce, 0xf1ef,
+ 0x1231, 0x0210, 0x3273, 0x2252, 0x52b5, 0x4294, 0x72f7, 0x62d6,
+ 0x9339, 0x8318, 0xb37b, 0xa35a, 0xd3bd, 0xc39c, 0xf3ff, 0xe3de,
+ 0x2462, 0x3443, 0x0420, 0x1401, 0x64e6, 0x74c7, 0x44a4, 0x5485,
+ 0xa56a, 0xb54b, 0x8528, 0x9509, 0xe5ee, 0xf5cf, 0xc5ac, 0xd58d,
+ 0x3653, 0x2672, 0x1611, 0x0630, 0x76d7, 0x66f6, 0x5695, 0x46b4,
+ 0xb75b, 0xa77a, 0x9719, 0x8738, 0xf7df, 0xe7fe, 0xd79d, 0xc7bc,
+ 0x48c4, 0x58e5, 0x6886, 0x78a7, 0x0840, 0x1861, 0x2802, 0x3823,
+ 0xc9cc, 0xd9ed, 0xe98e, 0xf9af, 0x8948, 0x9969, 0xa90a, 0xb92b,
+ 0x5af5, 0x4ad4, 0x7ab7, 0x6a96, 0x1a71, 0x0a50, 0x3a33, 0x2a12,
+ 0xdbfd, 0xcbdc, 0xfbbf, 0xeb9e, 0x9b79, 0x8b58, 0xbb3b, 0xab1a,
+ 0x6ca6, 0x7c87, 0x4ce4, 0x5cc5, 0x2c22, 0x3c03, 0x0c60, 0x1c41,
+ 0xedae, 0xfd8f, 0xcdec, 0xddcd, 0xad2a, 0xbd0b, 0x8d68, 0x9d49,
+ 0x7e97, 0x6eb6, 0x5ed5, 0x4ef4, 0x3e13, 0x2e32, 0x1e51, 0x0e70,
+ 0xff9f, 0xefbe, 0xdfdd, 0xcffc, 0xbf1b, 0xaf3a, 0x9f59, 0x8f78,
+ 0x9188, 0x81a9, 0xb1ca, 0xa1eb, 0xd10c, 0xc12d, 0xf14e, 0xe16f,
+ 0x1080, 0x00a1, 0x30c2, 0x20e3, 0x5004, 0x4025, 0x7046, 0x6067,
+ 0x83b9, 0x9398, 0xa3fb, 0xb3da, 0xc33d, 0xd31c, 0xe37f, 0xf35e,
+ 0x02b1, 0x1290, 0x22f3, 0x32d2, 0x4235, 0x5214, 0x6277, 0x7256,
+ 0xb5ea, 0xa5cb, 0x95a8, 0x8589, 0xf56e, 0xe54f, 0xd52c, 0xc50d,
+ 0x34e2, 0x24c3, 0x14a0, 0x0481, 0x7466, 0x6447, 0x5424, 0x4405,
+ 0xa7db, 0xb7fa, 0x8799, 0x97b8, 0xe75f, 0xf77e, 0xc71d, 0xd73c,
+ 0x26d3, 0x36f2, 0x0691, 0x16b0, 0x6657, 0x7676, 0x4615, 0x5634,
+ 0xd94c, 0xc96d, 0xf90e, 0xe92f, 0x99c8, 0x89e9, 0xb98a, 0xa9ab,
+ 0x5844, 0x4865, 0x7806, 0x6827, 0x18c0, 0x08e1, 0x3882, 0x28a3,
+ 0xcb7d, 0xdb5c, 0xeb3f, 0xfb1e, 0x8bf9, 0x9bd8, 0xabbb, 0xbb9a,
+ 0x4a75, 0x5a54, 0x6a37, 0x7a16, 0x0af1, 0x1ad0, 0x2ab3, 0x3a92,
+ 0xfd2e, 0xed0f, 0xdd6c, 0xcd4d, 0xbdaa, 0xad8b, 0x9de8, 0x8dc9,
+ 0x7c26, 0x6c07, 0x5c64, 0x4c45, 0x3ca2, 0x2c83, 0x1ce0, 0x0cc1,
+ 0xef1f, 0xff3e, 0xcf5d, 0xdf7c, 0xaf9b, 0xbfba, 0x8fd9, 0x9ff8,
+ 0x6e17, 0x7e36, 0x4e55, 0x5e74, 0x2e93, 0x3eb2, 0x0ed1, 0x1ef0
+};
+
+/**
+ * gst_dp_crc:
+ * @buffer: array of bytes
+ * @length: the length of @buffer
+ *
+ * Calculate a CRC for the given buffer over the given number of bytes.
+ * This is only provided for verification purposes; typical GDP users
+ * will not need this function.
+ *
+ * Returns: a two-byte CRC checksum.
+ */
+guint16
+gst_dp_crc (const guint8 * buffer, guint length)
+{
+ guint16 crc_register = CRC_INIT;
- crc_register = CRC_INIT; /* always init register */
+ g_return_val_if_fail (buffer != NULL || length == 0, 0);
/* calc CRC */
for (; length--;) {
crc_register = (guint16) ((crc_register << 8) ^
- crc_table[((crc_register >> 8) & 0x00ff) ^ *buffer++]);
+ gst_dp_crc_table[((crc_register >> 8) & 0x00ff) ^ *buffer++]);
}
return (0xffff ^ crc_register);
}
{
int i;
int n = 8; /* number of bytes per line */
- gchar *line = g_malloc (3 * n + 1);
+ gchar *line = g_malloc0 (3 * n + 1);
GST_LOG ("dumping byte array of length %d", length);
for (i = 0; i < length; ++i) {
g_free (line);
}
+GType
+gst_dp_version_get_type (void)
+{
+ static gsize gst_dp_version_type = 0;
+ static const GEnumValue gst_dp_version[] = {
+ {GST_DP_VERSION_0_2, "GST_DP_VERSION_0_2", "0.2"},
+ {GST_DP_VERSION_1_0, "GST_DP_VERSION_1_0", "1.0"},
+ {0, NULL, NULL},
+ };
+
+ if (g_once_init_enter (&gst_dp_version_type)) {
+ GType tmp = g_enum_register_static ("GstDPVersion", gst_dp_version);
+ g_once_init_leave (&gst_dp_version_type, tmp);
+ }
+
+ return (GType) gst_dp_version_type;
+};
+
/**
* gst_dp_init:
*
_gst_dp_initialized = TRUE;
+ g_type_class_ref (gst_dp_version_get_type ());
+
GST_DEBUG_CATEGORY_INIT (data_protocol_debug, "gdp", 0,
"GStreamer Data Protocol");
}
-/*** PUBLIC FUNCTIONS ***/
-
/**
* gst_dp_header_payload_length:
* @header: the byte header of the packet array
*
+ * Get the length of the payload described by @header.
+ *
* Returns: the length of the payload this header describes.
*/
guint32
gst_dp_header_payload_length (const guint8 * header)
{
+ g_return_val_if_fail (header != NULL, 0);
+
return GST_DP_HEADER_PAYLOAD_LENGTH (header);
}
* gst_dp_header_payload_type:
* @header: the byte header of the packet array
*
+ * Get the type of the payload described by @header.
+ *
* Returns: the #GstDPPayloadType the payload this header describes.
*/
GstDPPayloadType
gst_dp_header_payload_type (const guint8 * header)
{
+ g_return_val_if_fail (header != NULL, GST_DP_PAYLOAD_NONE);
+
return GST_DP_HEADER_PAYLOAD_TYPE (header);
}
+/*** PACKETIZER FUNCTIONS ***/
+
/**
* gst_dp_header_from_buffer:
* @buffer: a #GstBuffer to create a header for
- * @flags: the #GDPHeaderFlags to create the header with
+ * @flags: the #GstDPHeaderFlag to create the header with
* @length: a guint pointer to store the header length in
* @header: a guint8 * pointer to store a newly allocated header byte array in
*
* Creates a GDP header from the given buffer.
*
+ * Deprecated: use a #GstDPPacketizer
+ *
* Returns: %TRUE if the header was successfully created.
*/
-
+#ifndef GST_REMOVE_DEPRECATED
+#ifdef GST_DISABLE_DEPRECATED
+gboolean
+gst_dp_header_from_buffer (const GstBuffer * buffer, GstDPHeaderFlag flags,
+ guint * length, guint8 ** header);
+#endif
gboolean
gst_dp_header_from_buffer (const GstBuffer * buffer, GstDPHeaderFlag flags,
guint * length, guint8 ** header)
{
- guint8 *h;
- guint16 crc;
- guint16 flags_mask;
-
- g_return_val_if_fail (GST_IS_BUFFER (buffer), FALSE);
- g_return_val_if_fail (header, FALSE);
-
- *length = GST_DP_HEADER_LENGTH;
- h = g_malloc (GST_DP_HEADER_LENGTH);
-
- /* version, flags, type */
- h[0] = (guint8) GST_DP_VERSION_MAJOR;
- h[1] = (guint8) GST_DP_VERSION_MINOR;
- h[2] = (guint8) flags;
- h[3] = GST_DP_PAYLOAD_BUFFER;
-
- /* buffer properties */
- GST_WRITE_UINT32_BE (h + 4, GST_BUFFER_SIZE (buffer));
- GST_WRITE_UINT64_BE (h + 8, GST_BUFFER_TIMESTAMP (buffer));
- GST_WRITE_UINT64_BE (h + 16, GST_BUFFER_DURATION (buffer));
- GST_WRITE_UINT64_BE (h + 24, GST_BUFFER_OFFSET (buffer));
- GST_WRITE_UINT64_BE (h + 32, GST_BUFFER_OFFSET_END (buffer));
-
- /* data flags */
- /* we only copy KEY_UNIT,DELTA_UNIT and IN_CAPS flags */
- flags_mask = GST_BUFFER_FLAG_PREROLL | GST_BUFFER_FLAG_IN_CAPS |
- GST_BUFFER_FLAG_DELTA_UNIT;
-
- GST_WRITE_UINT16_BE (h + 40, GST_BUFFER_FLAGS (buffer) & flags_mask);
-
- /* ABI padding */
- GST_WRITE_UINT16_BE (h + 42, (guint64) 0);
- GST_WRITE_UINT32_BE (h + 44, (guint64) 0);
- GST_WRITE_UINT64_BE (h + 48, (guint64) 0);
-
- /* CRC */
- crc = 0;
- if (flags & GST_DP_HEADER_FLAG_CRC_HEADER) {
- /* we don't crc the last four bytes of the header since they are crc's */
- crc = gst_dp_crc (h, 56);
- }
- GST_WRITE_UINT16_BE (h + 56, crc);
-
- crc = 0;
- if (flags & GST_DP_HEADER_FLAG_CRC_PAYLOAD) {
- crc = gst_dp_crc (GST_BUFFER_DATA (buffer), GST_BUFFER_SIZE (buffer));
- }
- GST_WRITE_UINT16_BE (h + 58, crc);
+ return gst_dp_header_from_buffer_any (buffer, flags, length, header,
+ GST_DP_VERSION_0_2);
+}
+#endif
- GST_LOG ("created header from buffer:");
- gst_dp_dump_byte_array (h, GST_DP_HEADER_LENGTH);
- *header = h;
- return TRUE;
+static gboolean
+gst_dp_header_from_buffer_1_0 (const GstBuffer * buffer, GstDPHeaderFlag flags,
+ guint * length, guint8 ** header)
+{
+ return gst_dp_header_from_buffer_any (buffer, flags, length, header,
+ GST_DP_VERSION_1_0);
}
- /**
+/**
* gst_dp_packet_from_caps:
* @caps: a #GstCaps to create a packet for
- * @flags: the #GDPHeaderFlags to create the header with
+ * @flags: the #GstDPHeaderFlag to create the header with
* @length: a guint pointer to store the header length in
* @header: a guint8 pointer to store a newly allocated header byte array in
* @payload: a guint8 pointer to store a newly allocated payload byte array in
*
* Creates a GDP packet from the given caps.
*
+ * Deprecated: use a #GstDPPacketizer
+ *
* Returns: %TRUE if the packet was successfully created.
*/
+#ifndef GST_REMOVE_DEPRECATED
+#ifdef GST_DISABLE_DEPRECATED
+gboolean
+gst_dp_packet_from_caps (const GstCaps * caps, GstDPHeaderFlag flags,
+ guint * length, guint8 ** header, guint8 ** payload);
+#endif
gboolean
gst_dp_packet_from_caps (const GstCaps * caps, GstDPHeaderFlag flags,
guint * length, guint8 ** header, guint8 ** payload)
{
- guint8 *h;
- guint16 crc;
- guchar *string;
-
- /* FIXME: GST_IS_CAPS doesn't work
- g_return_val_if_fail (GST_IS_CAPS (caps), FALSE); */
- g_return_val_if_fail (caps, FALSE);
- g_return_val_if_fail (header, FALSE);
- g_return_val_if_fail (payload, FALSE);
-
- *length = GST_DP_HEADER_LENGTH;
- h = g_malloc (GST_DP_HEADER_LENGTH);
-
- string = (guchar *) gst_caps_to_string (caps);
-
- /* version, flags, type */
- h[0] = (guint8) GST_DP_VERSION_MAJOR;
- h[1] = (guint8) GST_DP_VERSION_MINOR;
- h[2] = (guint8) flags;
- h[3] = GST_DP_PAYLOAD_CAPS;
-
- /* buffer properties */
- GST_WRITE_UINT32_BE (h + 4, strlen ((gchar *) string) + 1); /* include trailing 0 */
- GST_WRITE_UINT64_BE (h + 8, (guint64) 0);
- GST_WRITE_UINT64_BE (h + 16, (guint64) 0);
- GST_WRITE_UINT64_BE (h + 24, (guint64) 0);
- GST_WRITE_UINT64_BE (h + 32, (guint64) 0);
-
- /* ABI padding */
- GST_WRITE_UINT64_BE (h + 40, (guint64) 0);
- GST_WRITE_UINT64_BE (h + 48, (guint64) 0);
-
- /* CRC */
- crc = 0;
- if (flags & GST_DP_HEADER_FLAG_CRC_HEADER) {
- crc = gst_dp_crc (h, 56);
- }
- GST_WRITE_UINT16_BE (h + 56, crc);
-
- crc = 0;
- if (flags & GST_DP_HEADER_FLAG_CRC_PAYLOAD) {
- crc = gst_dp_crc (string, strlen ((gchar *) string) + 1);
- }
- GST_WRITE_UINT16_BE (h + 58, crc);
+ return gst_dp_packet_from_caps_any (caps, flags, length, header, payload,
+ GST_DP_VERSION_0_2);
+}
+#endif
- GST_LOG ("created header from caps:");
- gst_dp_dump_byte_array (h, GST_DP_HEADER_LENGTH);
- *header = h;
- *payload = string;
- return TRUE;
+static gboolean
+gst_dp_packet_from_caps_1_0 (const GstCaps * caps, GstDPHeaderFlag flags,
+ guint * length, guint8 ** header, guint8 ** payload)
+{
+ return gst_dp_packet_from_caps_any (caps, flags, length, header, payload,
+ GST_DP_VERSION_1_0);
}
/**
* gst_dp_packet_from_event:
* @event: a #GstEvent to create a packet for
- * @flags: the #GDPHeaderFlags to create the header with
+ * @flags: the #GstDPHeaderFlag to create the header with
* @length: a guint pointer to store the header length in
* @header: a guint8 pointer to store a newly allocated header byte array in
* @payload: a guint8 pointer to store a newly allocated payload byte array in
*
* Creates a GDP packet from the given event.
*
+ * Deprecated: use a #GstDPPacketizer
+ *
* Returns: %TRUE if the packet was successfully created.
*/
+#ifndef GST_REMOVE_DEPRECATED
+#ifdef GST_DISABLE_DEPRECATED
+gboolean
+gst_dp_packet_from_event (const GstEvent * event, GstDPHeaderFlag flags,
+ guint * length, guint8 ** header, guint8 ** payload);
+#endif
gboolean
gst_dp_packet_from_event (const GstEvent * event, GstDPHeaderFlag flags,
guint * length, guint8 ** header, guint8 ** payload)
{
guint8 *h;
- guint16 crc;
guint pl_length; /* length of payload */
- g_return_val_if_fail (event, FALSE);
g_return_val_if_fail (GST_IS_EVENT (event), FALSE);
+ g_return_val_if_fail (length, FALSE);
g_return_val_if_fail (header, FALSE);
g_return_val_if_fail (payload, FALSE);
- *length = GST_DP_HEADER_LENGTH;
- h = g_malloc0 (GST_DP_HEADER_LENGTH);
-
/* first construct payload, since we need the length */
switch (GST_EVENT_TYPE (event)) {
case GST_EVENT_UNKNOWN:
- g_warning ("Unknown event, ignoring");
- *length = 0;
- g_free (h);
+ GST_WARNING ("Unknown event, ignoring");
return FALSE;
case GST_EVENT_EOS:
case GST_EVENT_FLUSH_START:
case GST_EVENT_FLUSH_STOP:
case GST_EVENT_NEWSEGMENT:
- GST_WRITE_UINT64_BE (h + 8, GST_EVENT_TIMESTAMP (event));
pl_length = 0;
*payload = NULL;
break;
case GST_EVENT_SEEK:
- pl_length = 4 + 8 + 8 + 4;
+ {
+ gdouble rate;
+ GstFormat format;
+ GstSeekFlags flags;
+ GstSeekType cur_type, stop_type;
+ gint64 cur, stop;
+
+ gst_event_parse_seek ((GstEvent *) event, &rate, &format, &flags,
+ &cur_type, &cur, &stop_type, &stop);
+
+ pl_length = 4 + 4 + 4 + 8 + 4 + 8;
*payload = g_malloc0 (pl_length);
- /*
- GST_WRITE_UINT32_BE (*payload, (guint32) GST_EVENT_SEEK_TYPE (event));
- GST_WRITE_UINT64_BE (*payload + 4,
- (guint64) GST_EVENT_SEEK_OFFSET (event));
- GST_WRITE_UINT64_BE (*payload + 12,
- (guint64) GST_EVENT_SEEK_ENDOFFSET (event));
- GST_WRITE_UINT32_BE (*payload + 20,
- (guint32) GST_EVENT_SEEK_ACCURACY (event));
- */
+ /* FIXME write rate */
+ GST_WRITE_UINT32_BE (*payload, (guint32) format);
+ GST_WRITE_UINT32_BE (*payload + 4, (guint32) flags);
+ GST_WRITE_UINT32_BE (*payload + 8, (guint32) cur_type);
+ GST_WRITE_UINT64_BE (*payload + 12, (guint64) cur);
+ GST_WRITE_UINT32_BE (*payload + 20, (guint32) stop_type);
+ GST_WRITE_UINT64_BE (*payload + 24, (guint64) stop);
break;
+ }
case GST_EVENT_QOS:
case GST_EVENT_NAVIGATION:
case GST_EVENT_TAG:
- g_warning ("Unhandled event type %d, ignoring", GST_EVENT_TYPE (event));
+ GST_WARNING ("Unhandled event type %d, ignoring", GST_EVENT_TYPE (event));
return FALSE;
default:
- g_warning ("Unknown event type %d, ignoring", GST_EVENT_TYPE (event));
- *length = 0;
- g_free (h);
+ GST_WARNING ("Unknown event type %d, ignoring", GST_EVENT_TYPE (event));
return FALSE;
}
+ /* now we can create and fill the header */
+ h = g_malloc0 (GST_DP_HEADER_LENGTH);
+ *length = GST_DP_HEADER_LENGTH;
+
/* version, flags, type */
- h[0] = (guint8) GST_DP_VERSION_MAJOR;
- h[1] = (guint8) GST_DP_VERSION_MINOR;
- h[2] = (guint8) flags;
- h[3] = GST_DP_PAYLOAD_EVENT_NONE + GST_EVENT_TYPE (event);
+ GST_DP_INIT_HEADER (h, GST_DP_VERSION_0_2, flags,
+ GST_DP_PAYLOAD_EVENT_NONE + GST_EVENT_TYPE (event));
/* length */
- GST_WRITE_UINT32_BE (h + 4, (guint32) pl_length);
+ GST_WRITE_UINT32_BE (h + 6, (guint32) pl_length);
/* timestamp */
- GST_WRITE_UINT64_BE (h + 8, GST_EVENT_TIMESTAMP (event));
+ GST_WRITE_UINT64_BE (h + 10, GST_EVENT_TIMESTAMP (event));
- /* ABI padding */
- GST_WRITE_UINT64_BE (h + 40, (guint64) 0);
- GST_WRITE_UINT64_BE (h + 48, (guint64) 0);
+ GST_DP_SET_CRC (h, flags, *payload, pl_length);
- /* CRC */
- crc = 0;
- if (flags & GST_DP_HEADER_FLAG_CRC_HEADER) {
- crc = gst_dp_crc (h, 56);
- }
- GST_WRITE_UINT16_BE (h + 56, crc);
+ GST_LOG ("created header from event:");
+ gst_dp_dump_byte_array (h, GST_DP_HEADER_LENGTH);
+
+ *header = h;
+ return TRUE;
+}
+#endif
+
+static gboolean
+gst_dp_packet_from_event_1_0 (const GstEvent * event, GstDPHeaderFlag flags,
+ guint * length, guint8 ** header, guint8 ** payload)
+{
+ guint8 *h;
+ guint32 pl_length; /* length of payload */
+ guchar *string = NULL;
+
+ g_return_val_if_fail (GST_IS_EVENT (event), FALSE);
+ g_return_val_if_fail (length, FALSE);
+ g_return_val_if_fail (header, FALSE);
+ g_return_val_if_fail (payload, FALSE);
- crc = 0;
- /* events can have a NULL payload */
- if (*payload && flags & GST_DP_HEADER_FLAG_CRC_PAYLOAD) {
- crc = gst_dp_crc (*payload, strlen ((gchar *) * payload) + 1);
+ *length = GST_DP_HEADER_LENGTH;
+ h = g_malloc0 (GST_DP_HEADER_LENGTH);
+
+ if (event->structure) {
+ string = (guchar *) gst_structure_to_string (event->structure);
+ GST_LOG ("event %p has structure, string %s", event, string);
+ pl_length = strlen ((gchar *) string) + 1; /* include trailing 0 */
+ } else {
+ GST_LOG ("event %p has no structure", event);
+ pl_length = 0;
}
- GST_WRITE_UINT16_BE (h + 58, crc);
+
+ /* version, flags, type */
+ GST_DP_INIT_HEADER (h, GST_DP_VERSION_1_0, flags,
+ GST_DP_PAYLOAD_EVENT_NONE + GST_EVENT_TYPE (event));
+
+ /* length */
+ GST_WRITE_UINT32_BE (h + 6, pl_length);
+ /* timestamp */
+ GST_WRITE_UINT64_BE (h + 10, GST_EVENT_TIMESTAMP (event));
+
+ GST_DP_SET_CRC (h, flags, string, pl_length);
GST_LOG ("created header from event:");
gst_dp_dump_byte_array (h, GST_DP_HEADER_LENGTH);
*header = h;
+ *payload = string;
return TRUE;
}
+/*** DEPACKETIZING FUNCTIONS ***/
/**
* gst_dp_buffer_from_header:
* Use this function if you want to pre-allocate a buffer based on the
* packet header to read the packet payload in to.
*
- * Returns: %TRUE if the buffer was successfully created.
+ * This function does not check the header passed to it, use
+ * gst_dp_validate_header() first if the header data is unchecked.
+ *
+ * Returns: A #GstBuffer if the buffer was successfully created, or NULL.
*/
GstBuffer *
gst_dp_buffer_from_header (guint header_length, const guint8 * header)
{
GstBuffer *buffer;
+ g_return_val_if_fail (header != NULL, NULL);
+ g_return_val_if_fail (header_length >= GST_DP_HEADER_LENGTH, NULL);
g_return_val_if_fail (GST_DP_HEADER_PAYLOAD_TYPE (header) ==
- GST_DP_PAYLOAD_BUFFER, FALSE);
+ GST_DP_PAYLOAD_BUFFER, NULL);
+
buffer =
gst_buffer_new_and_alloc ((guint) GST_DP_HEADER_PAYLOAD_LENGTH (header));
+
GST_BUFFER_TIMESTAMP (buffer) = GST_DP_HEADER_TIMESTAMP (header);
GST_BUFFER_DURATION (buffer) = GST_DP_HEADER_DURATION (header);
GST_BUFFER_OFFSET (buffer) = GST_DP_HEADER_OFFSET (header);
*
* Creates a newly allocated #GstCaps from the given packet.
*
- * Returns: %TRUE if the caps was successfully created.
+ * This function does not check the arguments passed to it, use
+ * gst_dp_validate_packet() first if the header and payload data are
+ * unchecked.
+ *
+ * Returns: A #GstCaps containing the caps represented in the packet,
+ * or NULL if the packet could not be converted.
*/
GstCaps *
gst_dp_caps_from_packet (guint header_length, const guint8 * header,
const guint8 * payload)
{
GstCaps *caps;
- const gchar *string;
+ gchar *string;
- g_return_val_if_fail (header, FALSE);
- g_return_val_if_fail (payload, FALSE);
+ g_return_val_if_fail (header, NULL);
+ g_return_val_if_fail (header_length >= GST_DP_HEADER_LENGTH, NULL);
g_return_val_if_fail (GST_DP_HEADER_PAYLOAD_TYPE (header) ==
- GST_DP_PAYLOAD_CAPS, FALSE);
+ GST_DP_PAYLOAD_CAPS, NULL);
+ g_return_val_if_fail (payload, NULL);
- string = (gchar *) payload;
+ /* 0 sized payload length will work create NULL string */
+ string = g_strndup ((gchar *) payload, GST_DP_HEADER_PAYLOAD_LENGTH (header));
caps = gst_caps_from_string (string);
+ g_free (string);
+
return caps;
}
-/**
- * gst_dp_event_from_packet:
- * @header_length: the length of the packet header
- * @header: the byte array of the packet header
- * @payload: the byte array of the packet payload
- *
- * Creates a newly allocated #GstEvent from the given packet.
- *
- * Returns: %TRUE if the event was successfully created.
- */
-GstEvent *
-gst_dp_event_from_packet (guint header_length, const guint8 * header,
+static GstEvent *
+gst_dp_event_from_packet_0_2 (guint header_length, const guint8 * header,
const guint8 * payload)
{
GstEvent *event = NULL;
GstEventType type;
- g_return_val_if_fail (header, FALSE);
- /* payload can be NULL, e.g. for an EOS event */
-
type = GST_DP_HEADER_PAYLOAD_TYPE (header) - GST_DP_PAYLOAD_EVENT_NONE;
switch (type) {
case GST_EVENT_UNKNOWN:
- g_warning ("Unknown event, ignoring");
- return FALSE;
+ GST_WARNING ("Unknown event, ignoring");
+ return NULL;
case GST_EVENT_EOS:
case GST_EVENT_FLUSH_START:
case GST_EVENT_FLUSH_STOP:
break;
case GST_EVENT_SEEK:
{
- /*
- GstSeekType type;
- gint64 offset, endoffset;
- GstSeekAccuracy accuracy;
-
- type = (GstSeekType) GST_READ_UINT32_BE (payload);
- offset = (gint64) GST_READ_UINT64_BE (payload + 4);
- endoffset = (gint64) GST_READ_UINT64_BE (payload + 12);
- accuracy = (GstSeekAccuracy) GST_READ_UINT32_BE (payload + 20);
- event = gst_event_new_segment_seek (type, offset, endoffset);
- GST_EVENT_TIMESTAMP (event) = GST_DP_HEADER_TIMESTAMP (header);
- GST_EVENT_SEEK_ACCURACY (event) = accuracy;
- */
+ gdouble rate;
+ GstFormat format;
+ GstSeekFlags flags;
+ GstSeekType cur_type, stop_type;
+ gint64 cur, stop;
+
+ g_return_val_if_fail (payload != NULL, NULL);
+
+ /* FIXME, read rate */
+ rate = 1.0;
+ format = (GstFormat) GST_READ_UINT32_BE (payload);
+ flags = (GstSeekFlags) GST_READ_UINT32_BE (payload + 4);
+ cur_type = (GstSeekType) GST_READ_UINT32_BE (payload + 8);
+ cur = (gint64) GST_READ_UINT64_BE (payload + 12);
+ stop_type = (GstSeekType) GST_READ_UINT32_BE (payload + 20);
+ stop = (gint64) GST_READ_UINT64_BE (payload + 24);
+
+ event = gst_event_new_seek (rate, format, flags, cur_type, cur,
+ stop_type, stop);
+ GST_EVENT_TIMESTAMP (event) = GST_DP_HEADER_TIMESTAMP (header);
break;
}
case GST_EVENT_QOS:
case GST_EVENT_NAVIGATION:
case GST_EVENT_TAG:
- g_warning ("Unhandled event type %d, ignoring", GST_EVENT_TYPE (event));
- return FALSE;
+ GST_WARNING ("Unhandled event type %d, ignoring", type);
+ return NULL;
default:
- g_warning ("Unknown event type %d, ignoring", GST_EVENT_TYPE (event));
- return FALSE;
+ GST_WARNING ("Unknown event type %d, ignoring", type);
+ return NULL;
}
return event;
}
+static GstEvent *
+gst_dp_event_from_packet_1_0 (guint header_length, const guint8 * header,
+ const guint8 * payload)
+{
+ GstEvent *event = NULL;
+ GstEventType type;
+ gchar *string = NULL;
+ GstStructure *s = NULL;
+
+ type = GST_DP_HEADER_PAYLOAD_TYPE (header) - GST_DP_PAYLOAD_EVENT_NONE;
+ if (payload) {
+ string =
+ g_strndup ((gchar *) payload, GST_DP_HEADER_PAYLOAD_LENGTH (header));
+ s = gst_structure_from_string (string, NULL);
+ g_free (string);
+ }
+ event = gst_event_new_custom (type, s);
+ return event;
+}
+
+
+/**
+ * gst_dp_event_from_packet:
+ * @header_length: the length of the packet header
+ * @header: the byte array of the packet header
+ * @payload: the byte array of the packet payload
+ *
+ * Creates a newly allocated #GstEvent from the given packet.
+ *
+ * This function does not check the arguments passed to it, use
+ * gst_dp_validate_packet() first if the header and payload data are
+ * unchecked.
+ *
+ * Returns: A #GstEvent if the event was successfully created,
+ * or NULL if an event could not be read from the payload.
+ */
+GstEvent *
+gst_dp_event_from_packet (guint header_length, const guint8 * header,
+ const guint8 * payload)
+{
+ guint8 major, minor;
+
+ g_return_val_if_fail (header, NULL);
+ g_return_val_if_fail (header_length >= GST_DP_HEADER_LENGTH, NULL);
+
+ major = GST_DP_HEADER_MAJOR_VERSION (header);
+ minor = GST_DP_HEADER_MINOR_VERSION (header);
+
+ if (major == 0 && minor == 2)
+ return gst_dp_event_from_packet_0_2 (header_length, header, payload);
+ else if (major == 1 && minor == 0)
+ return gst_dp_event_from_packet_1_0 (header_length, header, payload);
+ else {
+ GST_ERROR ("Unknown GDP version %d.%d", major, minor);
+ return NULL;
+ }
+}
+
/**
* gst_dp_validate_header:
* @header_length: the length of the packet header
{
guint16 crc_read, crc_calculated;
+ g_return_val_if_fail (header != NULL, FALSE);
+ g_return_val_if_fail (header_length >= GST_DP_HEADER_LENGTH, FALSE);
+
if (!(GST_DP_HEADER_FLAGS (header) & GST_DP_HEADER_FLAG_CRC_HEADER))
return TRUE;
+
crc_read = GST_DP_HEADER_CRC_HEADER (header);
- /* don't included the last two crc fields for the crc check */
+
+ /* don't include the last two crc fields for the crc check */
crc_calculated = gst_dp_crc (header, header_length - 4);
- if (crc_read != crc_calculated) {
+ if (crc_read != crc_calculated)
+ goto crc_error;
+
+ GST_LOG ("header crc validation: %02x", crc_read);
+ return TRUE;
+
+ /* ERRORS */
+crc_error:
+ {
GST_WARNING ("header crc mismatch: read %02x, calculated %02x", crc_read,
crc_calculated);
return FALSE;
}
- GST_LOG ("header crc validation: %02x", crc_read);
- return TRUE;
}
/**
{
guint16 crc_read, crc_calculated;
+ g_return_val_if_fail (header != NULL, FALSE);
+ g_return_val_if_fail (header_length >= GST_DP_HEADER_LENGTH, FALSE);
+
if (!(GST_DP_HEADER_FLAGS (header) & GST_DP_HEADER_FLAG_CRC_PAYLOAD))
return TRUE;
+
crc_read = GST_DP_HEADER_CRC_PAYLOAD (header);
crc_calculated = gst_dp_crc (payload, GST_DP_HEADER_PAYLOAD_LENGTH (header));
- if (crc_read != crc_calculated) {
+ if (crc_read != crc_calculated)
+ goto crc_error;
+
+ GST_LOG ("payload crc validation: %02x", crc_read);
+ return TRUE;
+
+ /* ERRORS */
+crc_error:
+ {
GST_WARNING ("payload crc mismatch: read %02x, calculated %02x", crc_read,
crc_calculated);
return FALSE;
}
- GST_LOG ("payload crc validation: %02x", crc_read);
- return TRUE;
}
/**
return TRUE;
}
+
+/**
+ * gst_dp_packetizer_new:
+ * @version: the #GstDPVersion of the protocol to packetize for.
+ *
+ * Creates a new packetizer.
+ *
+ * Returns: a newly allocated #GstDPPacketizer
+ */
+GstDPPacketizer *
+gst_dp_packetizer_new (GstDPVersion version)
+{
+ GstDPPacketizer *ret;
+
+ ret = g_malloc0 (sizeof (GstDPPacketizer));
+ ret->version = version;
+
+ switch (version) {
+#ifndef GST_REMOVE_DEPRECATED
+ case GST_DP_VERSION_0_2:
+ ret->header_from_buffer = gst_dp_header_from_buffer;
+ ret->packet_from_caps = gst_dp_packet_from_caps;
+ ret->packet_from_event = gst_dp_packet_from_event;
+ break;
+#endif
+ case GST_DP_VERSION_1_0:
+ ret->header_from_buffer = gst_dp_header_from_buffer_1_0;
+ ret->packet_from_caps = gst_dp_packet_from_caps_1_0;
+ ret->packet_from_event = gst_dp_packet_from_event_1_0;
+ break;
+ default:
+ g_free (ret);
+ ret = NULL;
+ break;
+ }
+
+ return ret;
+}
+
+/**
+ * gst_dp_packetizer_free:
+ * @packetizer: the #GstDPPacketizer to free.
+ *
+ * Free the given packetizer.
+ */
+void
+gst_dp_packetizer_free (GstDPPacketizer * packetizer)
+{
+ g_free (packetizer);
+}