index 9b59d1ddde4fab72d255340508e814cca5519881..244023627fec85466547075a95af6864a94b672a 100644 (file)
/* other defines */
#define DEFAULT_BUFFER_SIZE 4096
#define QUEUE_IS_USING_TEMP_FILE(queue) ((queue)->temp_location_set || (queue)->temp_template != NULL)
-#define QUEUE_IS_USING_RING_BUFFER(queue) ((queue)->use_ring_buffer) /* for consistency with the above macro */
+#define QUEUE_IS_USING_RING_BUFFER(queue) ((queue)->ring_buffer_max_size != 0) /* for consistency with the above macro */
#define QUEUE_IS_USING_QUEUE(queue) (!QUEUE_IS_USING_TEMP_FILE(queue) && !QUEUE_IS_USING_RING_BUFFER (queue))
#define QUEUE_MAX_BYTES(queue) MIN((queue)->max_level.bytes, (queue)->ring_buffer_max_size)
queue->max_level.time, \
(guint64) (!QUEUE_IS_USING_QUEUE(queue) ? \
queue->current->writing_pos - queue->current->max_reading_pos : \
- queue->queue->length))
+ queue->queue.length))
#define GST_QUEUE2_MUTEX_LOCK(q) G_STMT_START { \
g_mutex_lock (q->qlock); \
guint prop_id, GValue * value, GParamSpec * pspec);
static GstFlowReturn gst_queue2_chain (GstPad * pad, GstBuffer * buffer);
+static GstFlowReturn gst_queue2_chain_list (GstPad * pad,
+ GstBufferList * buffer_list);
static GstFlowReturn gst_queue2_bufferalloc (GstPad * pad, guint64 offset,
guint size, GstCaps * caps, GstBuffer ** buf);
static GstFlowReturn gst_queue2_push_one (GstQueue2 * queue);
static void update_cur_level (GstQueue2 * queue, GstQueue2Range * range);
+typedef enum
+{
+ GST_QUEUE2_ITEM_TYPE_UNKNOWN = 0,
+ GST_QUEUE2_ITEM_TYPE_BUFFER,
+ GST_QUEUE2_ITEM_TYPE_BUFFER_LIST,
+ GST_QUEUE2_ITEM_TYPE_EVENT
+} GstQueue2ItemType;
/* static guint gst_queue2_signals[LAST_SIGNAL] = { 0 }; */
GObjectClass *gobject_class = G_OBJECT_CLASS (klass);
GstElementClass *gstelement_class = GST_ELEMENT_CLASS (klass);
- parent_class = g_type_class_peek_parent (klass);
-
gobject_class->set_property = gst_queue2_set_property;
gobject_class->get_property = gst_queue2_get_property;
G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
g_object_class_install_property (gobject_class, PROP_LOW_PERCENT,
g_param_spec_int ("low-percent", "Low percent",
- "Low threshold for buffering to start", 0, 100, DEFAULT_LOW_PERCENT,
+ "Low threshold for buffering to start. Only used if use-buffering is True",
+ 0, 100, DEFAULT_LOW_PERCENT,
G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
g_object_class_install_property (gobject_class, PROP_HIGH_PERCENT,
g_param_spec_int ("high-percent", "High percent",
- "High threshold for buffering to finish", 0, 100,
- DEFAULT_HIGH_PERCENT, G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
+ "High threshold for buffering to finish. Only used if use-buffering is True",
+ 0, 100, DEFAULT_HIGH_PERCENT,
+ G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
g_object_class_install_property (gobject_class, PROP_TEMP_TEMPLATE,
g_param_spec_string ("temp-template", "Temporary File Template",
* The maximum size of the ring buffer in bytes. If set to 0, the ring
* buffer is disabled. Default 0.
*
- * Since: 0.10.30
+ * Since: 0.10.31
*/
g_object_class_install_property (gobject_class, PROP_RING_BUFFER_MAX_SIZE,
g_param_spec_uint64 ("ring-buffer-max-size",
"Max. ring buffer size (bytes)",
- "Max. amount of data in the ring buffer (bytes, 0 = disabled",
- 0, G_MAXUINT, DEFAULT_RING_BUFFER_MAX_SIZE,
+ "Max. amount of data in the ring buffer (bytes, 0 = disabled)",
+ 0, G_MAXUINT64, DEFAULT_RING_BUFFER_MAX_SIZE,
G_PARAM_READWRITE | G_PARAM_STATIC_STRINGS));
/* set several parent class virtual functions */
gst_pad_set_chain_function (queue->sinkpad,
GST_DEBUG_FUNCPTR (gst_queue2_chain));
+ gst_pad_set_chain_list_function (queue->sinkpad,
+ GST_DEBUG_FUNCPTR (gst_queue2_chain_list));
gst_pad_set_activatepush_function (queue->sinkpad,
GST_DEBUG_FUNCPTR (gst_queue2_sink_activate_push));
gst_pad_set_event_function (queue->sinkpad,
gst_segment_init (&queue->sink_segment, GST_FORMAT_TIME);
gst_segment_init (&queue->src_segment, GST_FORMAT_TIME);
+ queue->sinktime = GST_CLOCK_TIME_NONE;
+ queue->srctime = GST_CLOCK_TIME_NONE;
+ queue->sink_tainted = TRUE;
+ queue->src_tainted = TRUE;
+
queue->srcresult = GST_FLOW_WRONG_STATE;
queue->sinkresult = GST_FLOW_WRONG_STATE;
queue->is_eos = FALSE;
queue->item_add = g_cond_new ();
queue->waiting_del = FALSE;
queue->item_del = g_cond_new ();
- queue->queue = g_queue_new ();
+ g_queue_init (&queue->queue);
queue->buffering_percent = 100;
queue->temp_location_set = FALSE;
queue->temp_remove = DEFAULT_TEMP_REMOVE;
- queue->use_ring_buffer = FALSE;
queue->ring_buffer = NULL;
queue->ring_buffer_max_size = DEFAULT_RING_BUFFER_MAX_SIZE;
GST_DEBUG_OBJECT (queue, "finalizing queue");
- while (!g_queue_is_empty (queue->queue)) {
- GstMiniObject *data = g_queue_pop_head (queue->queue);
+ while (!g_queue_is_empty (&queue->queue)) {
+ GstMiniObject *data = g_queue_pop_head (&queue->queue);
gst_mini_object_unref (data);
}
- g_queue_free (queue->queue);
+ g_queue_clear (&queue->queue);
g_mutex_free (queue->qlock);
g_cond_free (queue->item_add);
g_cond_free (queue->item_del);
GstPad *otherpad;
GstCaps *result;
- queue = GST_QUEUE2 (GST_PAD_PARENT (pad));
+ queue = GST_QUEUE2 (gst_pad_get_parent (pad));
+ if (G_UNLIKELY (queue == NULL))
+ return gst_caps_new_any ();
otherpad = (pad == queue->srcpad ? queue->sinkpad : queue->srcpad);
result = gst_pad_peer_get_caps (otherpad);
if (result == NULL)
result = gst_caps_new_any ();
+ gst_object_unref (queue);
+
return result;
}
static void
update_time_level (GstQueue2 * queue)
{
- gint64 sink_time, src_time;
-
- sink_time =
- gst_segment_to_running_time (&queue->sink_segment, GST_FORMAT_TIME,
- queue->sink_segment.last_stop);
+ if (queue->sink_tainted) {
+ queue->sinktime =
+ gst_segment_to_running_time (&queue->sink_segment, GST_FORMAT_TIME,
+ queue->sink_segment.last_stop);
+ queue->sink_tainted = FALSE;
+ }
- src_time = gst_segment_to_running_time (&queue->src_segment, GST_FORMAT_TIME,
- queue->src_segment.last_stop);
+ if (queue->src_tainted) {
+ queue->srctime =
+ gst_segment_to_running_time (&queue->src_segment, GST_FORMAT_TIME,
+ queue->src_segment.last_stop);
+ queue->src_tainted = FALSE;
+ }
GST_DEBUG_OBJECT (queue, "sink %" GST_TIME_FORMAT ", src %" GST_TIME_FORMAT,
- GST_TIME_ARGS (sink_time), GST_TIME_ARGS (src_time));
+ GST_TIME_ARGS (queue->sinktime), GST_TIME_ARGS (queue->srctime));
- if (sink_time >= src_time)
- queue->cur_level.time = sink_time - src_time;
+ if (queue->sinktime != GST_CLOCK_TIME_NONE
+ && queue->srctime != GST_CLOCK_TIME_NONE
+ && queue->sinktime >= queue->srctime)
+ queue->cur_level.time = queue->sinktime - queue->srctime;
else
queue->cur_level.time = 0;
}
/* take a NEWSEGMENT event and apply the values to segment, updating the time
* level of queue. */
static void
-apply_segment (GstQueue2 * queue, GstEvent * event, GstSegment * segment)
+apply_segment (GstQueue2 * queue, GstEvent * event, GstSegment * segment,
+ gboolean is_sink)
{
gboolean update;
GstFormat format;
GST_DEBUG_OBJECT (queue,
"configured NEWSEGMENT %" GST_SEGMENT_FORMAT, segment);
+ if (is_sink)
+ queue->sink_tainted = TRUE;
+ else
+ queue->src_tainted = TRUE;
+
/* segment can update the time level of the queue */
update_time_level (queue);
}
/* take a buffer and update segment, updating the time level of the queue. */
static void
-apply_buffer (GstQueue2 * queue, GstBuffer * buffer, GstSegment * segment)
+apply_buffer (GstQueue2 * queue, GstBuffer * buffer, GstSegment * segment,
+ gboolean is_sink)
{
GstClockTime duration, timestamp;
timestamp = GST_BUFFER_TIMESTAMP (buffer);
duration = GST_BUFFER_DURATION (buffer);
- /* if no timestamp is set, assume it's continuous with the previous
+ /* if no timestamp is set, assume it's continuous with the previous
* time */
if (timestamp == GST_CLOCK_TIME_NONE)
timestamp = segment->last_stop;
gst_segment_set_last_stop (segment, GST_FORMAT_TIME, timestamp);
+ if (is_sink)
+ queue->sink_tainted = TRUE;
+ else
+ queue->src_tainted = TRUE;
+
+ /* calc diff with other end */
+ update_time_level (queue);
+}
+
+static GstBufferListItem
+buffer_list_apply_time (GstBuffer ** buf, guint group, guint idx, gpointer data)
+{
+ GstClockTime *timestamp = data;
+
+ GST_TRACE ("buffer %u in group %u has ts %" GST_TIME_FORMAT
+ " duration %" GST_TIME_FORMAT, idx, group,
+ GST_TIME_ARGS (GST_BUFFER_TIMESTAMP (*buf)),
+ GST_TIME_ARGS (GST_BUFFER_DURATION (*buf)));
+
+ if (GST_BUFFER_TIMESTAMP_IS_VALID (*buf))
+ *timestamp = GST_BUFFER_TIMESTAMP (*buf);
+
+ if (GST_BUFFER_DURATION_IS_VALID (*buf))
+ *timestamp += GST_BUFFER_DURATION (*buf);
+
+ GST_TRACE ("ts now %" GST_TIME_FORMAT, GST_TIME_ARGS (*timestamp));
+ return GST_BUFFER_LIST_CONTINUE;
+}
+
+/* take a buffer list and update segment, updating the time level of the queue */
+static void
+apply_buffer_list (GstQueue2 * queue, GstBufferList * buffer_list,
+ GstSegment * segment, gboolean is_sink)
+{
+ GstClockTime timestamp;
+
+ /* if no timestamp is set, assume it's continuous with the previous time */
+ timestamp = segment->last_stop;
+
+ gst_buffer_list_foreach (buffer_list, buffer_list_apply_time, ×tamp);
+
+ GST_DEBUG_OBJECT (queue, "last_stop updated to %" GST_TIME_FORMAT,
+ GST_TIME_ARGS (timestamp));
+
+ gst_segment_set_last_stop (segment, GST_FORMAT_TIME, timestamp);
+
+ if (is_sink)
+ queue->sink_tainted = TRUE;
+ else
+ queue->src_tainted = TRUE;
+
/* calc diff with other end */
update_time_level (queue);
}
gint64 percent;
gboolean post = FALSE;
- if (!queue->use_buffering || queue->high_percent <= 0)
+ if (queue->high_percent <= 0)
return;
#define GET_PERCENT(format,alt_max) ((queue->max_level.format) > 0 ? (queue->cur_level.format) * 100 / ((alt_max) > 0 ? MIN ((alt_max), (queue->max_level.format)) : (queue->max_level.format)) : 0)
queue->bytes_in = 0;
queue->bytes_out = 0;
queue->byte_in_rate = 0.0;
+ queue->byte_in_period = 0;
queue->byte_out_rate = 0.0;
queue->last_in_elapsed = 0.0;
queue->last_out_elapsed = 0.0;
/* Tuning for rate estimation. We use a large window for the input rate because
* it should be stable when connected to a network. The output rate is less
* stable (the elements preroll, queues behind a demuxer fill, ...) and should
- * therefore adapt more quickly. */
-#define AVG_IN(avg,val) ((avg) * 15.0 + (val)) / 16.0
+ * therefore adapt more quickly.
+ * However, initial input rate may be subject to a burst, and should therefore
+ * initially also adapt more quickly to changes, and only later on give higher
+ * weight to previous values. */
+#define AVG_IN(avg,val,w1,w2) ((avg) * (w1) + (val) * (w2)) / ((w1) + (w2))
#define AVG_OUT(avg,val) ((avg) * 3.0 + (val)) / 4.0
static void
period = elapsed - queue->last_in_elapsed;
GST_DEBUG_OBJECT (queue,
- "rates: period %f, in %" G_GUINT64_FORMAT, period, queue->bytes_in);
+ "rates: period %f, in %" G_GUINT64_FORMAT ", global period %f",
+ period, queue->bytes_in, queue->byte_in_period);
byte_in_rate = queue->bytes_in / period;
if (queue->byte_in_rate == 0.0)
queue->byte_in_rate = byte_in_rate;
else
- queue->byte_in_rate = AVG_IN (queue->byte_in_rate, byte_in_rate);
+ queue->byte_in_rate = AVG_IN (queue->byte_in_rate, byte_in_rate,
+ (double) queue->byte_in_period, period);
+
+ /* another data point, cap at 16 for long time running average */
+ if (queue->byte_in_period < 16 * RATE_INTERVAL)
+ queue->byte_in_period += period;
/* reset the values to calculate rate over the next interval */
queue->last_in_elapsed = elapsed;
GstEvent *event;
gboolean res;
+ GST_QUEUE2_MUTEX_UNLOCK (queue);
+
GST_DEBUG_OBJECT (queue, "Seeking to %" G_GUINT64_FORMAT, offset);
event =
GST_SEEK_FLAG_FLUSH | GST_SEEK_FLAG_ACCURATE, GST_SEEK_TYPE_SET, offset,
GST_SEEK_TYPE_NONE, -1);
- GST_QUEUE2_MUTEX_UNLOCK (queue);
res = gst_pad_push_event (queue->sinkpad, event);
GST_QUEUE2_MUTEX_LOCK (queue);
} else {
GST_INFO_OBJECT (queue, "not found in any range");
/* we don't have the range, see how far away we are, FIXME, find a good
- * threshold based on the incomming rate. */
+ * threshold based on the incoming rate. */
if (!queue->is_eos && queue->current) {
if (QUEUE_IS_USING_RING_BUFFER (queue)) {
if (offset < queue->current->offset || offset >
} else {
GST_DEBUG_OBJECT (queue,
"EOS hit and we don't have any requested data");
+ gst_buffer_unref (buf);
return GST_FLOW_UNEXPECTED;
}
}
/* set range reading_pos to actual reading position for this read */
queue->current->reading_pos = rpos;
- /* congfigure how much and from where to read */
+ /* configure how much and from where to read */
if (QUEUE_IS_USING_RING_BUFFER (queue)) {
file_offset =
(queue->current->rb_offset + (rpos -
out_flushing:
{
GST_DEBUG_OBJECT (queue, "we are flushing");
+ gst_buffer_unref (buf);
return GST_FLOW_WRONG_STATE;
}
read_error:
gst_queue2_flush_temp_file (queue);
init_ranges (queue);
} else {
- while (!g_queue_is_empty (queue->queue)) {
- GstMiniObject *data = g_queue_pop_head (queue->queue);
+ while (!g_queue_is_empty (&queue->queue)) {
+ GstMiniObject *data = g_queue_pop_head (&queue->queue);
/* Then lose another reference because we are supposed to destroy that
data when flushing */
GST_QUEUE2_CLEAR_LEVEL (queue->cur_level);
gst_segment_init (&queue->sink_segment, GST_FORMAT_TIME);
gst_segment_init (&queue->src_segment, GST_FORMAT_TIME);
+ queue->sinktime = queue->srctime = GST_CLOCK_TIME_NONE;
+ queue->sink_tainted = queue->src_tainted = TRUE;
if (queue->starting_segment != NULL)
gst_event_unref (queue->starting_segment);
queue->starting_segment = NULL;
{
guint8 *data, *ring_buffer;
guint size, rb_size;
- guint64 writing_pos, new_writing_pos, max_reading_pos;
- gint64 space;
+ guint64 writing_pos, new_writing_pos;
GstQueue2Range *range, *prev, *next;
if (QUEUE_IS_USING_RING_BUFFER (queue))
writing_pos = queue->current->rb_writing_pos;
else
writing_pos = queue->current->writing_pos;
- max_reading_pos = queue->current->max_reading_pos;
ring_buffer = queue->ring_buffer;
rb_size = queue->ring_buffer_max_size;
guint to_write;
if (QUEUE_IS_USING_RING_BUFFER (queue)) {
+ gint64 space;
+
/* calculate the space in the ring buffer not used by data from
* the current range */
while (QUEUE_MAX_BYTES (queue) <= queue->cur_level.bytes) {
}
}
} else {
- space = to_write = size;
+ to_write = size;
new_writing_pos = writing_pos + to_write;
}
update_cur_level (queue, queue->current);
/* update the buffering status */
- update_buffering (queue);
+ if (queue->use_buffering)
+ update_buffering (queue);
GST_INFO_OBJECT (queue, "cur_level.bytes %u (max %" G_GUINT64_FORMAT ")",
queue->cur_level.bytes, QUEUE_MAX_BYTES (queue));
}
}
+static GstBufferListItem
+buffer_list_create_write (GstBuffer ** buf, guint group, guint idx, gpointer q)
+{
+ GstQueue2 *queue = q;
+
+ GST_TRACE_OBJECT (queue, "writing buffer %u in group %u of size %u bytes",
+ idx, group, GST_BUFFER_SIZE (*buf));
+
+ if (!gst_queue2_create_write (queue, *buf)) {
+ GST_INFO_OBJECT (queue, "create_write() returned FALSE, bailing out");
+ return GST_BUFFER_LIST_END;
+ }
+
+ return GST_BUFFER_LIST_CONTINUE;
+}
+
+static GstBufferListItem
+buffer_list_calc_size (GstBuffer ** buf, guint group, guint idx, gpointer data)
+{
+ guint *p_size = data;
+ guint buf_size;
+
+ buf_size = GST_BUFFER_SIZE (*buf);
+ GST_TRACE ("buffer %u in group %u has size %u", idx, group, buf_size);
+ *p_size += buf_size;
+
+ return GST_BUFFER_LIST_CONTINUE;
+}
+
/* enqueue an item an update the level stats */
static void
-gst_queue2_locked_enqueue (GstQueue2 * queue, gpointer item)
+gst_queue2_locked_enqueue (GstQueue2 * queue, gpointer item,
+ GstQueue2ItemType item_type)
{
- if (GST_IS_BUFFER (item)) {
+ if (item_type == GST_QUEUE2_ITEM_TYPE_BUFFER) {
GstBuffer *buffer;
guint size;
queue->bytes_in += size;
/* apply new buffer to segment stats */
- apply_buffer (queue, buffer, &queue->sink_segment);
+ apply_buffer (queue, buffer, &queue->sink_segment, TRUE);
/* update the byterate stats */
update_in_rates (queue);
/* FIXME - check return value? */
gst_queue2_create_write (queue, buffer);
}
- } else if (GST_IS_EVENT (item)) {
+ } else if (item_type == GST_QUEUE2_ITEM_TYPE_BUFFER_LIST) {
+ GstBufferList *buffer_list;
+ guint size = 0;
+
+ buffer_list = GST_BUFFER_LIST_CAST (item);
+
+ gst_buffer_list_foreach (buffer_list, buffer_list_calc_size, &size);
+ GST_LOG_OBJECT (queue, "total size of buffer list: %u bytes", size);
+
+ /* add buffer to the statistics */
+ if (QUEUE_IS_USING_QUEUE (queue)) {
+ queue->cur_level.buffers++;
+ queue->cur_level.bytes += size;
+ }
+ queue->bytes_in += size;
+
+ /* apply new buffer to segment stats */
+ apply_buffer_list (queue, buffer_list, &queue->sink_segment, TRUE);
+
+ /* update the byterate stats */
+ update_in_rates (queue);
+
+ if (!QUEUE_IS_USING_QUEUE (queue)) {
+ gst_buffer_list_foreach (buffer_list, buffer_list_create_write, queue);
+ }
+ } else if (item_type == GST_QUEUE2_ITEM_TYPE_EVENT) {
GstEvent *event;
event = GST_EVENT_CAST (item);
queue->is_eos = TRUE;
break;
case GST_EVENT_NEWSEGMENT:
- apply_segment (queue, event, &queue->sink_segment);
+ apply_segment (queue, event, &queue->sink_segment, TRUE);
/* This is our first new segment, we hold it
* as we can't save it on the temp file */
if (!QUEUE_IS_USING_QUEUE (queue)) {
if (item) {
/* update the buffering status */
- update_buffering (queue);
+ if (queue->use_buffering)
+ update_buffering (queue);
if (QUEUE_IS_USING_QUEUE (queue)) {
- g_queue_push_tail (queue->queue, item);
+ g_queue_push_tail (&queue->queue, item);
} else {
gst_mini_object_unref (GST_MINI_OBJECT_CAST (item));
}
/* dequeue an item from the queue and update level stats */
static GstMiniObject *
-gst_queue2_locked_dequeue (GstQueue2 * queue)
+gst_queue2_locked_dequeue (GstQueue2 * queue, GstQueue2ItemType * item_type)
{
GstMiniObject *item;
if (!QUEUE_IS_USING_QUEUE (queue))
item = gst_queue2_read_item_from_file (queue);
else
- item = g_queue_pop_head (queue->queue);
+ item = g_queue_pop_head (&queue->queue);
if (item == NULL)
goto no_item;
buffer = GST_BUFFER_CAST (item);
size = GST_BUFFER_SIZE (buffer);
+ *item_type = GST_QUEUE2_ITEM_TYPE_BUFFER;
GST_CAT_LOG_OBJECT (queue_dataflow, queue,
"retrieved buffer %p from queue", buffer);
}
queue->bytes_out += size;
- apply_buffer (queue, buffer, &queue->src_segment);
+ apply_buffer (queue, buffer, &queue->src_segment, FALSE);
/* update the byterate stats */
update_out_rates (queue);
/* update the buffering */
- update_buffering (queue);
+ if (queue->use_buffering)
+ update_buffering (queue);
} else if (GST_IS_EVENT (item)) {
GstEvent *event = GST_EVENT_CAST (item);
+ *item_type = GST_QUEUE2_ITEM_TYPE_EVENT;
+
GST_CAT_LOG_OBJECT (queue_dataflow, queue,
"retrieved event %p from queue", event);
GST_QUEUE2_CLEAR_LEVEL (queue->cur_level);
break;
case GST_EVENT_NEWSEGMENT:
- apply_segment (queue, event, &queue->src_segment);
+ apply_segment (queue, event, &queue->src_segment, FALSE);
break;
default:
break;
}
+ } else if (GST_IS_BUFFER_LIST (item)) {
+ GstBufferList *buffer_list;
+ guint size = 0;
+
+ buffer_list = GST_BUFFER_LIST_CAST (item);
+ gst_buffer_list_foreach (buffer_list, buffer_list_calc_size, &size);
+ *item_type = GST_QUEUE2_ITEM_TYPE_BUFFER_LIST;
+
+ GST_CAT_LOG_OBJECT (queue_dataflow, queue,
+ "retrieved buffer list %p from queue", buffer_list);
+
+ if (QUEUE_IS_USING_QUEUE (queue)) {
+ queue->cur_level.buffers--;
+ queue->cur_level.bytes -= size;
+ }
+ queue->bytes_out += size;
+
+ apply_buffer_list (queue, buffer_list, &queue->src_segment, FALSE);
+ /* update the byterate stats */
+ update_out_rates (queue);
+ /* update the buffering */
+ if (queue->use_buffering)
+ update_buffering (queue);
+
} else {
g_warning
("Unexpected item %p dequeued from queue %s (refcounting problem?)",
item, GST_OBJECT_NAME (queue));
item = NULL;
+ *item_type = GST_QUEUE2_ITEM_TYPE_UNKNOWN;
}
GST_QUEUE2_SIGNAL_DEL (queue);
/* refuse more events on EOS */
if (queue->is_eos)
goto out_eos;
- gst_queue2_locked_enqueue (queue, event);
+ gst_queue2_locked_enqueue (queue, event, GST_QUEUE2_ITEM_TYPE_EVENT);
GST_QUEUE2_MUTEX_UNLOCK (queue);
} else {
/* non-serialized events are passed upstream. */
if (!QUEUE_IS_USING_QUEUE (queue) && queue->current) {
return queue->current->writing_pos <= queue->current->max_reading_pos;
} else {
- if (queue->queue->length == 0)
+ if (queue->queue.length == 0)
return TRUE;
}
}
static GstFlowReturn
-gst_queue2_chain (GstPad * pad, GstBuffer * buffer)
+gst_queue2_chain_buffer_or_buffer_list (GstQueue2 * queue,
+ GstMiniObject * item, GstQueue2ItemType item_type)
{
- GstQueue2 *queue;
-
- queue = GST_QUEUE2 (GST_OBJECT_PARENT (pad));
-
- GST_CAT_LOG_OBJECT (queue_dataflow, queue,
- "received buffer %p of size %d, time %" GST_TIME_FORMAT ", duration %"
- GST_TIME_FORMAT, buffer, GST_BUFFER_SIZE (buffer),
- GST_TIME_ARGS (GST_BUFFER_TIMESTAMP (buffer)),
- GST_TIME_ARGS (GST_BUFFER_DURATION (buffer)));
-
/* we have to lock the queue since we span threads */
GST_QUEUE2_MUTEX_LOCK_CHECK (queue, queue->sinkresult, out_flushing);
/* when we received EOS, we refuse more data */
goto out_flushing;
/* put buffer in queue now */
- gst_queue2_locked_enqueue (queue, buffer);
+ gst_queue2_locked_enqueue (queue, item, item_type);
GST_QUEUE2_MUTEX_UNLOCK (queue);
return GST_FLOW_OK;
GST_CAT_LOG_OBJECT (queue_dataflow, queue,
"exit because task paused, reason: %s", gst_flow_get_name (ret));
GST_QUEUE2_MUTEX_UNLOCK (queue);
- gst_buffer_unref (buffer);
+ gst_mini_object_unref (item);
return ret;
}
{
GST_CAT_LOG_OBJECT (queue_dataflow, queue, "exit because we received EOS");
GST_QUEUE2_MUTEX_UNLOCK (queue);
- gst_buffer_unref (buffer);
+ gst_mini_object_unref (item);
return GST_FLOW_UNEXPECTED;
}
GST_CAT_LOG_OBJECT (queue_dataflow, queue,
"exit because we received UNEXPECTED");
GST_QUEUE2_MUTEX_UNLOCK (queue);
- gst_buffer_unref (buffer);
+ gst_mini_object_unref (item);
return GST_FLOW_UNEXPECTED;
}
}
+static GstFlowReturn
+gst_queue2_chain (GstPad * pad, GstBuffer * buffer)
+{
+ GstQueue2 *queue;
+
+ queue = GST_QUEUE2 (GST_OBJECT_PARENT (pad));
+
+ GST_CAT_LOG_OBJECT (queue_dataflow, queue,
+ "received buffer %p of size %d, time %" GST_TIME_FORMAT ", duration %"
+ GST_TIME_FORMAT, buffer, GST_BUFFER_SIZE (buffer),
+ GST_TIME_ARGS (GST_BUFFER_TIMESTAMP (buffer)),
+ GST_TIME_ARGS (GST_BUFFER_DURATION (buffer)));
+
+ return gst_queue2_chain_buffer_or_buffer_list (queue,
+ GST_MINI_OBJECT_CAST (buffer), GST_QUEUE2_ITEM_TYPE_BUFFER);
+}
+
+static GstFlowReturn
+gst_queue2_chain_list (GstPad * pad, GstBufferList * buffer_list)
+{
+ GstQueue2 *queue;
+
+ queue = GST_QUEUE2 (GST_OBJECT_PARENT (pad));
+
+ GST_CAT_LOG_OBJECT (queue_dataflow, queue,
+ "received buffer list %p", buffer_list);
+
+ return gst_queue2_chain_buffer_or_buffer_list (queue,
+ GST_MINI_OBJECT_CAST (buffer_list), GST_QUEUE2_ITEM_TYPE_BUFFER_LIST);
+}
+
+static GstMiniObject *
+gst_queue2_dequeue_on_unexpected (GstQueue2 * queue,
+ GstQueue2ItemType * item_type)
+{
+ GstMiniObject *data;
+
+ GST_CAT_LOG_OBJECT (queue_dataflow, queue, "got UNEXPECTED from downstream");
+
+ /* stop pushing buffers, we dequeue all items until we see an item that we
+ * can push again, which is EOS or NEWSEGMENT. If there is nothing in the
+ * queue we can push, we set a flag to make the sinkpad refuse more
+ * buffers with an UNEXPECTED return value until we receive something
+ * pushable again or we get flushed. */
+ while ((data = gst_queue2_locked_dequeue (queue, item_type))) {
+ if (*item_type == GST_QUEUE2_ITEM_TYPE_BUFFER) {
+ GST_CAT_LOG_OBJECT (queue_dataflow, queue,
+ "dropping UNEXPECTED buffer %p", data);
+ gst_buffer_unref (GST_BUFFER_CAST (data));
+ } else if (*item_type == GST_QUEUE2_ITEM_TYPE_EVENT) {
+ GstEvent *event = GST_EVENT_CAST (data);
+ GstEventType type = GST_EVENT_TYPE (event);
+
+ if (type == GST_EVENT_EOS || type == GST_EVENT_NEWSEGMENT) {
+ /* we found a pushable item in the queue, push it out */
+ GST_CAT_LOG_OBJECT (queue_dataflow, queue,
+ "pushing pushable event %s after UNEXPECTED",
+ GST_EVENT_TYPE_NAME (event));
+ return data;
+ }
+ GST_CAT_LOG_OBJECT (queue_dataflow, queue,
+ "dropping UNEXPECTED event %p", event);
+ gst_event_unref (event);
+ } else if (*item_type == GST_QUEUE2_ITEM_TYPE_BUFFER_LIST) {
+ GST_CAT_LOG_OBJECT (queue_dataflow, queue,
+ "dropping UNEXPECTED buffer list %p", data);
+ gst_buffer_list_unref (GST_BUFFER_LIST_CAST (data));
+ }
+ }
+ /* no more items in the queue. Set the unexpected flag so that upstream
+ * make us refuse any more buffers on the sinkpad. Since we will still
+ * accept EOS and NEWSEGMENT we return _FLOW_OK to the caller so that the
+ * task function does not shut down. */
+ queue->unexpected = TRUE;
+ return NULL;
+}
+
/* dequeue an item from the queue an push it downstream. This functions returns
* the result of the push. */
static GstFlowReturn
{
GstFlowReturn result = GST_FLOW_OK;
GstMiniObject *data;
+ GstQueue2ItemType item_type;
- data = gst_queue2_locked_dequeue (queue);
+ data = gst_queue2_locked_dequeue (queue, &item_type);
if (data == NULL)
goto no_item;
next:
- if (GST_IS_BUFFER (data)) {
+ GST_QUEUE2_MUTEX_UNLOCK (queue);
+
+ if (item_type == GST_QUEUE2_ITEM_TYPE_BUFFER) {
GstBuffer *buffer;
GstCaps *caps;
buffer = GST_BUFFER_CAST (data);
caps = GST_BUFFER_CAPS (buffer);
- GST_QUEUE2_MUTEX_UNLOCK (queue);
-
/* set caps before pushing the buffer so that core does not try to do
* something fancy to check if this is possible. */
if (caps && caps != GST_PAD_CAPS (queue->srcpad))
/* need to check for srcresult here as well */
GST_QUEUE2_MUTEX_LOCK_CHECK (queue, queue->srcresult, out_flushing);
if (result == GST_FLOW_UNEXPECTED) {
- GST_CAT_LOG_OBJECT (queue_dataflow, queue,
- "got UNEXPECTED from downstream");
- /* stop pushing buffers, we dequeue all items until we see an item that we
- * can push again, which is EOS or NEWSEGMENT. If there is nothing in the
- * queue we can push, we set a flag to make the sinkpad refuse more
- * buffers with an UNEXPECTED return value until we receive something
- * pushable again or we get flushed. */
- while ((data = gst_queue2_locked_dequeue (queue))) {
- if (GST_IS_BUFFER (data)) {
- GST_CAT_LOG_OBJECT (queue_dataflow, queue,
- "dropping UNEXPECTED buffer %p", data);
- gst_buffer_unref (GST_BUFFER_CAST (data));
- } else if (GST_IS_EVENT (data)) {
- GstEvent *event = GST_EVENT_CAST (data);
- GstEventType type = GST_EVENT_TYPE (event);
-
- if (type == GST_EVENT_EOS || type == GST_EVENT_NEWSEGMENT) {
- /* we found a pushable item in the queue, push it out */
- GST_CAT_LOG_OBJECT (queue_dataflow, queue,
- "pushing pushable event %s after UNEXPECTED",
- GST_EVENT_TYPE_NAME (event));
- goto next;
- }
- GST_CAT_LOG_OBJECT (queue_dataflow, queue,
- "dropping UNEXPECTED event %p", event);
- gst_event_unref (event);
- }
- }
- /* no more items in the queue. Set the unexpected flag so that upstream
- * make us refuse any more buffers on the sinkpad. Since we will still
- * accept EOS and NEWSEGMENT we return _FLOW_OK to the caller so that the
- * task function does not shut down. */
- queue->unexpected = TRUE;
+ data = gst_queue2_dequeue_on_unexpected (queue, &item_type);
+ if (data != NULL)
+ goto next;
+ /* Since we will still accept EOS and NEWSEGMENT we return _FLOW_OK
+ * to the caller so that the task function does not shut down */
result = GST_FLOW_OK;
}
- } else if (GST_IS_EVENT (data)) {
+ } else if (item_type == GST_QUEUE2_ITEM_TYPE_EVENT) {
GstEvent *event = GST_EVENT_CAST (data);
GstEventType type = GST_EVENT_TYPE (event);
- GST_QUEUE2_MUTEX_UNLOCK (queue);
-
gst_pad_push_event (queue->srcpad, event);
- GST_QUEUE2_MUTEX_LOCK_CHECK (queue, queue->srcresult, out_flushing);
/* if we're EOS, return UNEXPECTED so that the task pauses. */
if (type == GST_EVENT_EOS) {
GST_CAT_LOG_OBJECT (queue_dataflow, queue,
"pushed EOS event %p, return UNEXPECTED", event);
result = GST_FLOW_UNEXPECTED;
}
+
+ GST_QUEUE2_MUTEX_LOCK_CHECK (queue, queue->srcresult, out_flushing);
+ } else if (item_type == GST_QUEUE2_ITEM_TYPE_BUFFER_LIST) {
+ GstBufferList *buffer_list;
+ GstBuffer *first_buf;
+ GstCaps *caps;
+
+ buffer_list = GST_BUFFER_LIST_CAST (data);
+
+ first_buf = gst_buffer_list_get (buffer_list, 0, 0);
+ caps = (first_buf != NULL) ? GST_BUFFER_CAPS (first_buf) : NULL;
+
+ /* set caps before pushing the buffer so that core does not try to do
+ * something fancy to check if this is possible. */
+ if (caps && caps != GST_PAD_CAPS (queue->srcpad))
+ gst_pad_set_caps (queue->srcpad, caps);
+
+ result = gst_pad_push_list (queue->srcpad, buffer_list);
+
+ /* need to check for srcresult here as well */
+ GST_QUEUE2_MUTEX_LOCK_CHECK (queue, queue->srcresult, out_flushing);
+ if (result == GST_FLOW_UNEXPECTED) {
+ data = gst_queue2_dequeue_on_unexpected (queue, &item_type);
+ if (data != NULL)
+ goto next;
+ /* Since we will still accept EOS and NEWSEGMENT we return _FLOW_OK
+ * to the caller so that the task function does not shut down */
+ result = GST_FLOW_OK;
+ }
}
return result;
}
}
-/* called repeadedly with @pad as the source pad. This function should push out
+/* called repeatedly with @pad as the source pad. This function should push out
* data to the peer element. */
static void
gst_queue2_loop (GstPad * pad)
GstFlowReturn ret = queue->srcresult;
gst_pad_pause_task (queue->srcpad);
+ GST_QUEUE2_MUTEX_UNLOCK (queue);
GST_CAT_LOG_OBJECT (queue_dataflow, queue,
"pause task, reason: %s", gst_flow_get_name (queue->srcresult));
- GST_QUEUE2_MUTEX_UNLOCK (queue);
/* let app know about us giving up if upstream is not expected to do so */
/* UNEXPECTED is already taken care of elsewhere */
if (eos && (ret == GST_FLOW_NOT_LINKED || ret < GST_FLOW_UNEXPECTED)) {
gst_queue2_handle_src_event (GstPad * pad, GstEvent * event)
{
gboolean res = TRUE;
- GstQueue2 *queue = GST_QUEUE2 (GST_PAD_PARENT (pad));
+ GstQueue2 *queue = GST_QUEUE2 (gst_pad_get_parent (pad));
+ if (G_UNLIKELY (queue == NULL)) {
+ gst_event_unref (event);
+ return FALSE;
+ }
#ifndef GST_DISABLE_GST_DEBUG
GST_CAT_DEBUG_OBJECT (queue_dataflow, queue, "got event %p (%s)",
event, GST_EVENT_TYPE_NAME (event));
break;
}
+ gst_object_unref (queue);
return res;
}
{
GstQueue2 *queue;
- queue = GST_QUEUE2 (GST_PAD_PARENT (pad));
+ queue = GST_QUEUE2 (gst_pad_get_parent (pad));
+ if (G_UNLIKELY (queue == NULL))
+ return FALSE;
switch (GST_QUERY_TYPE (query)) {
case GST_QUERY_POSITION:
break;
}
+ gst_object_unref (queue);
return TRUE;
/* ERRORS */
peer_failed:
{
GST_DEBUG_OBJECT (queue, "failed peer query");
+ gst_object_unref (queue);
return FALSE;
}
}
return gst_queue2_handle_src_query (GST_QUEUE2_CAST (element)->srcpad, query);
}
+static void
+gst_queue2_update_upstream_size (GstQueue2 * queue)
+{
+ GstFormat fmt = GST_FORMAT_BYTES;
+ gint64 upstream_size = -1;
+
+ if (gst_pad_query_peer_duration (queue->sinkpad, &fmt, &upstream_size)) {
+ GST_INFO_OBJECT (queue, "upstream size: %" G_GINT64_FORMAT, upstream_size);
+ queue->upstream_size = upstream_size;
+ }
+}
+
static GstFlowReturn
gst_queue2_get_range (GstPad * pad, guint64 offset, guint length,
GstBuffer ** buffer)
queue = GST_QUEUE2_CAST (gst_pad_get_parent (pad));
- GST_QUEUE2_MUTEX_LOCK_CHECK (queue, queue->srcresult, out_flushing);
length = (length == -1) ? DEFAULT_BUFFER_SIZE : length;
+ GST_QUEUE2_MUTEX_LOCK_CHECK (queue, queue->srcresult, out_flushing);
offset = (offset == -1) ? queue->current->reading_pos : offset;
GST_DEBUG_OBJECT (queue,
"Getting range: offset %" G_GUINT64_FORMAT ", length %u", offset, length);
+
+ /* catch any reads beyond the size of the file here to make sure queue2
+ * doesn't send seek events beyond the size of the file upstream, since
+ * that would confuse elements such as souphttpsrc and/or http servers.
+ * Demuxers often just loop until EOS at the end of the file to figure out
+ * when they've read all the end-headers or index chunks. */
+ if (G_UNLIKELY (offset >= queue->upstream_size)) {
+ gst_queue2_update_upstream_size (queue);
+ if (queue->upstream_size > 0 && offset >= queue->upstream_size)
+ goto out_unexpected;
+ }
+
+ if (G_UNLIKELY (offset + length > queue->upstream_size)) {
+ gst_queue2_update_upstream_size (queue);
+ if (queue->upstream_size > 0 && offset + length >= queue->upstream_size) {
+ length = queue->upstream_size - offset;
+ GST_DEBUG_OBJECT (queue, "adjusting length downto %d", length);
+ }
+ }
+
/* FIXME - function will block when the range is not yet available */
ret = gst_queue2_create_read (queue, offset, length, buffer);
GST_QUEUE2_MUTEX_UNLOCK (queue);
GST_DEBUG_OBJECT (queue, "we are flushing");
GST_QUEUE2_MUTEX_UNLOCK (queue);
+ gst_object_unref (queue);
return ret;
}
+out_unexpected:
+ {
+ GST_DEBUG_OBJECT (queue, "read beyond end of file");
+ GST_QUEUE2_MUTEX_UNLOCK (queue);
+ gst_object_unref (queue);
+ return GST_FLOW_UNEXPECTED;
+ }
}
static gboolean
result = gst_queue2_open_temp_location_file (queue);
} else if (!queue->ring_buffer) {
queue->ring_buffer = g_malloc (queue->ring_buffer_max_size);
- result = !!queue->ring_buffer;
+ result = ! !queue->ring_buffer;
} else {
result = TRUE;
}
queue->sinkresult = GST_FLOW_OK;
queue->is_eos = FALSE;
queue->unexpected = FALSE;
- GST_QUEUE2_MUTEX_UNLOCK (queue);
+ queue->upstream_size = 0;
} else {
- GST_QUEUE2_MUTEX_LOCK (queue);
GST_DEBUG_OBJECT (queue, "no temp file, cannot activate pull mode");
/* this is not allowed, we cannot operate in pull mode without a temp
* file. */
queue->srcresult = GST_FLOW_WRONG_STATE;
queue->sinkresult = GST_FLOW_WRONG_STATE;
result = FALSE;
- GST_QUEUE2_MUTEX_UNLOCK (queue);
}
+ GST_QUEUE2_MUTEX_UNLOCK (queue);
} else {
GST_QUEUE2_MUTEX_LOCK (queue);
GST_DEBUG_OBJECT (queue, "deactivating pull mode");
g_free (queue->ring_buffer);
queue->ring_buffer = NULL;
}
+ clean_ranges (queue);
}
if (queue->starting_segment != NULL) {
gst_event_unref (queue->starting_segment);
break;
case PROP_RING_BUFFER_MAX_SIZE:
queue->ring_buffer_max_size = g_value_get_uint64 (value);
- queue->use_ring_buffer = !!queue->ring_buffer_max_size;
break;
default:
G_OBJECT_WARN_INVALID_PROPERTY_ID (object, prop_id, pspec);