index 483613f3f3a91e3eca0af1fbb5b19a9513b26c2e..80a985750519f58b940d63067064f517ece0c7f5 100644 (file)
}
}
+static GstMiniObject *
+gst_queue2_dequeue_on_unexpected (GstQueue2 * queue,
+ GstQueue2ItemType * item_type)
+{
+ GstMiniObject *data;
+
+ GST_CAT_LOG_OBJECT (queue_dataflow, queue, "got UNEXPECTED from downstream");
+
+ /* stop pushing buffers, we dequeue all items until we see an item that we
+ * can push again, which is EOS or NEWSEGMENT. If there is nothing in the
+ * queue we can push, we set a flag to make the sinkpad refuse more
+ * buffers with an UNEXPECTED return value until we receive something
+ * pushable again or we get flushed. */
+ while ((data = gst_queue2_locked_dequeue (queue, item_type))) {
+ if (*item_type == GST_QUEUE2_ITEM_TYPE_BUFFER) {
+ GST_CAT_LOG_OBJECT (queue_dataflow, queue,
+ "dropping UNEXPECTED buffer %p", data);
+ gst_buffer_unref (GST_BUFFER_CAST (data));
+ } else if (*item_type == GST_QUEUE2_ITEM_TYPE_EVENT) {
+ GstEvent *event = GST_EVENT_CAST (data);
+ GstEventType type = GST_EVENT_TYPE (event);
+
+ if (type == GST_EVENT_EOS || type == GST_EVENT_NEWSEGMENT) {
+ /* we found a pushable item in the queue, push it out */
+ GST_CAT_LOG_OBJECT (queue_dataflow, queue,
+ "pushing pushable event %s after UNEXPECTED",
+ GST_EVENT_TYPE_NAME (event));
+ return data;
+ }
+ GST_CAT_LOG_OBJECT (queue_dataflow, queue,
+ "dropping UNEXPECTED event %p", event);
+ gst_event_unref (event);
+ } else if (*item_type == GST_QUEUE2_ITEM_TYPE_BUFFER_LIST) {
+ GST_CAT_LOG_OBJECT (queue_dataflow, queue,
+ "dropping UNEXPECTED buffer list %p", data);
+ gst_buffer_list_unref (GST_BUFFER_LIST_CAST (data));
+ }
+ }
+ /* no more items in the queue. Set the unexpected flag so that upstream
+ * make us refuse any more buffers on the sinkpad. Since we will still
+ * accept EOS and NEWSEGMENT we return _FLOW_OK to the caller so that the
+ * task function does not shut down. */
+ queue->unexpected = TRUE;
+ return NULL;
+}
+
/* dequeue an item from the queue an push it downstream. This functions returns
* the result of the push. */
static GstFlowReturn
/* need to check for srcresult here as well */
GST_QUEUE2_MUTEX_LOCK_CHECK (queue, queue->srcresult, out_flushing);
if (result == GST_FLOW_UNEXPECTED) {
- GST_CAT_LOG_OBJECT (queue_dataflow, queue,
- "got UNEXPECTED from downstream");
- /* stop pushing buffers, we dequeue all items until we see an item that we
- * can push again, which is EOS or NEWSEGMENT. If there is nothing in the
- * queue we can push, we set a flag to make the sinkpad refuse more
- * buffers with an UNEXPECTED return value until we receive something
- * pushable again or we get flushed. */
- while ((data = gst_queue2_locked_dequeue (queue, &item_type))) {
- if (item_type == GST_QUEUE2_ITEM_TYPE_BUFFER) {
- GST_CAT_LOG_OBJECT (queue_dataflow, queue,
- "dropping UNEXPECTED buffer %p", data);
- gst_buffer_unref (GST_BUFFER_CAST (data));
- } else if (item_type == GST_QUEUE2_ITEM_TYPE_EVENT) {
- GstEvent *event = GST_EVENT_CAST (data);
- GstEventType type = GST_EVENT_TYPE (event);
-
- if (type == GST_EVENT_EOS || type == GST_EVENT_NEWSEGMENT) {
- /* we found a pushable item in the queue, push it out */
- GST_CAT_LOG_OBJECT (queue_dataflow, queue,
- "pushing pushable event %s after UNEXPECTED",
- GST_EVENT_TYPE_NAME (event));
- goto next;
- }
- GST_CAT_LOG_OBJECT (queue_dataflow, queue,
- "dropping UNEXPECTED event %p", event);
- gst_event_unref (event);
- }
- }
- /* no more items in the queue. Set the unexpected flag so that upstream
- * make us refuse any more buffers on the sinkpad. Since we will still
- * accept EOS and NEWSEGMENT we return _FLOW_OK to the caller so that the
- * task function does not shut down. */
- queue->unexpected = TRUE;
- result = GST_FLOW_OK;
+ data = gst_queue2_dequeue_on_unexpected (queue, &item_type);
+ if (data != NULL)
+ goto next;
}
} else if (item_type == GST_QUEUE2_ITEM_TYPE_EVENT) {
GstEvent *event = GST_EVENT_CAST (data);