diff --git a/scripts/gst-uninstalled b/scripts/gst-uninstalled
--- /dev/null
+++ b/scripts/gst-uninstalled
@@ -0,0 +1,173 @@
+#!/bin/bash -i
+#
+# this script is in git as gstreamer/scripts/gst-uninstalled
+#
+# It will set up the environment to use and develop gstreamer and projects
+# that use gstreamer with an uninstalled git checkout of gstreamer and the
+# plugin modules.
+#
+# It will set up LD_LIBRARY_PATH, DYLD_LIBRARY_PATH, PKG_CONFIG_PATH,
+# GST_PLUGIN_PATH, GST_PLUGIN_SYSTEM_PATH, GST_REGISTRY, MANPATH, PYTHONPATH
+# to prefer the uninstalled versions but also contain the installed ones.
+# The only exception to this is, that no system installed plugins will be
+# used but only the uninstalled ones.
+#
+# This script assumes that the relevant modules are checked out one by one
+# under a given tree specified below in MYGST.
+#
+# Symlink this script in a directory in your path (for example $HOME/bin). You
+# must name the symlink gst-something, where something is the subdirectory
+# of MYGST that contains your gstreamer module checkouts.
+#
+# e.g.:
+# - mkdir $HOME/gst/head
+# - ln -sf gst-uninstalled $HOME/bin/gst-head
+# - checkout copies of gstreamer modules in $HOME/gst/head
+# - gst-head
+
+# This script is run -i so that PS1 doesn't get cleared
+
+# Change this variable to the location of your gstreamer git checkouts
+MYGST=$HOME/gst
+
+#
+# Everything below this line shouldn't be edited!
+#
+
+# extract version from $0
+# if this script is called "gst-head" then version will be "head"
+VERSION=`echo $0 | sed s/.*gst-//g`
+
+# base path under which dirs are installed
+GST=$MYGST/$VERSION
+if test ! -e $GST; then
+ echo "$GST does not exist !"
+ exit
+fi
+
+# set up a bunch of paths
+PATH="\
+$GST/gstreamer/tools:\
+$GST/gst-plugins-base/tools:\
+$GST/gst-player/src:\
+$GST/gst-editor/src:\
+$GST/gstreamer-sharp/tools:\
+$GST/prefix/bin:\
+$PATH"
+
+# /some/path: makes the dynamic linker look in . too, so avoid this
+LD_LIBRARY_PATH=$GST/prefix/lib${LD_LIBRARY_PATH:+:$LD_LIBRARY_PATH}
+DYLD_LIBRARY_PATH=$GST/prefix/lib${DYLD_LIBRARY_PATH:+:$DYLD_LIBRARY_PATH}
+
+# GStreamer rtsp server library
+LD_LIBRARY_PATH=$GST/gst-rtsp-server/gst/rtsp-server/.libs:$LD_LIBRARY_PATH
+DYLD_LIBRARY_PATH=$GST/gst-rtsp-server/gst/rtsp-server/.libs:$DYLD_LIBRARY_PATH
+
+# GStreamer ffmpeg libraries
+for path in libavformat libavutil libavcodec libpostproc libavdevice
+do
+ LD_LIBRARY_PATH=$GST/gst-ffmpeg/gst-libs/ext/ffmpeg/$path:$LD_LIBRARY_PATH
+ DYLD_LIBRARY_PATH=$GST/gst-ffmpeg/gst-libs/ext/ffmpeg/$path:$DYLD_LIBRARY_PATH
+done
+
+# GStreamer plugins base libraries
+for path in app audio cdda fft interfaces pbutils netbuffer riff rtp rtsp sdp tag utils video
+do
+ LD_LIBRARY_PATH=$GST/gst-plugins-base/gst-libs/gst/$path/.libs:$LD_LIBRARY_PATH
+ DYLD_LIBRARY_PATH=$GST/gst-plugins-base/gst-libs/gst/$path/.libs:$DYLD_LIBRARY_PATH
+done
+
+# GStreamer core libraries
+for path in base net check controller dataprotocol
+do
+ LD_LIBRARY_PATH=$GST/gstreamer/libs/gst/$path/.libs:$LD_LIBRARY_PATH
+ DYLD_LIBRARY_PATH=$GST/gstreamer/libs/gst/$path/.libs:$DYLD_LIBRARY_PATH
+done
+LD_LIBRARY_PATH=$GST/gstreamer/gst/.libs:$LD_LIBRARY_PATH
+DYLD_LIBRARY_PATH=$GST/gstreamer/gst/.libs:$DYLD_LIBRARY_PATH
+export LD_LIBRARY_PATH
+export DYLD_LIBRARY_PATH
+
+export PKG_CONFIG_PATH="\
+$GST/prefix/lib/pkgconfig\
+:$GST/gstreamer/pkgconfig\
+:$GST/gst-plugins-base/pkgconfig\
+:$GST/gst-plugins-good/pkgconfig\
+:$GST/gst-python/pkgconfig\
+:$GST/gst-rtsp-server/pkgconfig\
+:$GST/gstreamer-sharp/pkgconfig\
+${PKG_CONFIG_PATH:+:$PKG_CONFIG_PATH}"
+
+export GST_PLUGIN_PATH="\
+$GST/gstreamer/plugins\
+:$GST/gst-plugins-base/ext\
+:$GST/gst-plugins-base/gst\
+:$GST/gst-plugins-base/sys\
+:$GST/gst-plugins-good/ext\
+:$GST/gst-plugins-good/gst\
+:$GST/gst-plugins-good/sys\
+:$GST/gst-plugins-ugly/ext\
+:$GST/gst-plugins-ugly/gst\
+:$GST/gst-plugins-ugly/sys\
+:$GST/gst-plugins-bad/ext\
+:$GST/gst-plugins-bad/gst\
+:$GST/gst-plugins-bad/sys\
+:$GST/gst-ffmpeg/ext\
+:$GST/gnonlin/gnl\
+:$GST/gst-openmax\
+:$GST/gst-plugins-gl/gst\
+:$GST/plugins\
+${GST_PLUGIN_PATH:+:$GST_PLUGIN_PATH}"
+
+# don't use any system-installed plug-ins at all
+export GST_PLUGIN_SYSTEM_PATH=
+# set our registry somewhere else so we don't mess up the registry generated
+# by an installed copy
+rm -f $GST/gstreamer/registry.xml 2>/dev/null
+export GST_REGISTRY=$GST/gstreamer/registry.dat
+# Point at the uninstalled plugin scanner
+export GST_PLUGIN_SCANNER=$GST/gstreamer/libs/gst/helpers/gst-plugin-scanner
+
+# once MANPATH is set, it needs at least an "empty"component to keep pulling
+# in the system-configured man paths from man.config
+# this still doesn't make it work for the uninstalled case, since man goes
+# look for a man directory "nearby" instead of the directory I'm telling it to
+export MANPATH=$GST/gstreamer/tools:$GST/prefix/share/man:$MANPATH
+pythonver=`python -c "import sys; print sys.version[:3]"`
+export PYTHONPATH=$GST/gst-python:$GST/prefix/lib/python$pythonver/site-packages${PYTHONPATH:+:$PYTHONPATH}
+
+# totem-pl-parser
+export PKG_CONFIG_PATH=$GST/totem-pl-parser:$PKG_CONFIG_PATH
+export LD_LIBRARY_PATH=$GST/totem-pl-parser/plparse/.libs:$LD_LIBRARY_PATH
+export DYLD_LIBRARY_PATH=$GST/totem-pl-parser/plparse/.libs:$DYLD_LIBRARY_PATH
+
+# totem
+export PATH=$GST/totem/src:$PATH
+
+# gstreamer-sharp
+export MONO_PATH=$GST/gstreamer-sharp/gstreamer-sharp:$MONO_PATH
+export LD_LIBRARY_PATH=$GST/gstreamer-sharp/gstreamer-sharp/glue/.libs:$LD_LIBRARY_PATH
+export DYLD_LIBRARY_PATH=$GST/gstreamer-sharp/gstreamer-sharp/glue/.libs:$DYLD_LIBRARY_PATH
+
+# gst-qa-system
+export PYTHONPATH=$GST/gst-qa-system:$PYTHONPATH
+export PATH=$GST/gst-qa-system/bin:$PATH
+
+# if we got a command, run it, else start a shell
+if test ! -z "$1";
+then
+ $@
+ exit $?
+fi
+
+# set up prompt to help us remember we're in a subshell, cd to
+# the gstreamer base dir and start $SHELL
+cd $GST
+shell=$SHELL
+if test "x$SHELL" == "x/bin/bash"
+then
+ # debian/ubuntu resets our PS1. bastards.
+ shell="$SHELL --noprofile"
+fi
+PS1="[gst-$VERSION] $PS1" $shell
+