diff --git a/win32/common/config.h b/win32/common/config.h
index 634d4833d0833f08bbabfe25c96631175f4c00fb..52cb678bab0cb02e305f4dcdfb33848c2f06ce8a 100644 (file)
--- a/win32/common/config.h
+++ b/win32/common/config.h
-/* config.h.in. Generated from configure.ac by autoheader. */
-/* This copy of config.h.in is specifically for win32 Visual Studio builds */
+/* Autogenerated config.h created for win32 Visual Studio builds */
+
+/* PREFIX -- specifically added for Windows for easier moving */
+#define PREFIX "C:\\gstreamer"
+
+/* Define if building universal (internal helper macro) */
+#undef AC_APPLE_UNIVERSAL_BUILD
+
+/* poll doesn't work on devices */
+#undef BROKEN_POLL
+
+/* Buffer alignment to use */
+#undef BUFFER_ALIGNMENT
+
+/* Buffer alignment by malloc default */
+#define BUFFER_ALIGNMENT_MALLOC 1
+
+/* Buffer alignment by pagesize */
+#undef BUFFER_ALIGNMENT_PAGESIZE
/* Define to 1 if translation of program messages to the user's native
language is requested. */
#undef ENABLE_NLS
+/* Subunit protocol result output */
+#undef ENABLE_SUBUNIT
+
/* gettext package name */
#define GETTEXT_PACKAGE "gstreamer-0.10"
-/* PREFIX - specifically added for Windows for easier moving */
-#define PREFIX "C:\\gstreamer"
+/* data dir */
+#define GST_DATADIR PREFIX "\\share"
-/* Location of registry */
-#define GST_CACHE_DIR PREFIX "\\var\\cache"
+/* Define if option parsing is disabled */
+#undef GST_DISABLE_OPTION_PARSING
+
+/* Define if pipeline parsing code is disabled */
+#undef GST_DISABLE_PARSE
+
+/* Extra platform specific plugin suffix */
+#undef GST_EXTRA_MODULE_SUFFIX
/* macro to use to show function name */
-#define GST_FUNCTION "(function)"
+#undef GST_FUNCTION
/* Defined if gcov is enabled to force a rebuild due to config.h changing */
#undef GST_GCOV_ENABLED
+/* Defined when registry scanning through fork is unsafe */
+#undef GST_HAVE_UNSAFE_FORK
+
/* Default errorlevel to use */
#define GST_LEVEL_DEFAULT GST_LEVEL_ERROR
/* GStreamer license */
#define GST_LICENSE "LGPL"
+/* library major.minor version */
+#define GST_MAJORMINOR "0.10"
+
+/* package name in plugins */
+#define GST_PACKAGE_NAME "GStreamer source release"
+
/* package origin */
#define GST_PACKAGE_ORIGIN "Unknown package origin"
-/* package name in plugins */
-#define GST_PACKAGE_NAME "GStreamer CVS/prerelease"
+/* GStreamer package release date/time for plugins as YYYY-MM-DD */
+#define GST_PACKAGE_RELEASE_DATETIME "2011-01-21"
-/* Define the version */
-#define GST_VERSION "0.10.1.1"
+/* location of the installed gst-plugin-scanner */
+#define GST_PLUGIN_SCANNER_INSTALLED LIBDIR "\\gst-plugin-scanner"
-/* Define the MAJOR.MINOR version */
-#define GST_MAJORMINOR "0.10"
+/* Define to 1 if you have the MacOS X function CFLocaleCopyCurrent in the
+ CoreFoundation framework. */
+#undef HAVE_CFLOCALECOPYCURRENT
-/* Define host CPU */
-#define HOST_CPU "i686"
+/* Define to 1 if you have the MacOS X function CFPreferencesCopyAppValue in
+ the CoreFoundation framework. */
+#undef HAVE_CFPREFERENCESCOPYAPPVALUE
+
+/* Define to 1 if you have the `clock_gettime' function. */
+#undef HAVE_CLOCK_GETTIME
/* Define if the host CPU is an Alpha */
#undef HAVE_CPU_ALPHA
/* Define if the host CPU is an ARM */
#undef HAVE_CPU_ARM
+/* Define if the host CPU is a CRIS */
+#undef HAVE_CPU_CRIS
+
+/* Define if the host CPU is a CRISv32 */
+#undef HAVE_CPU_CRISV32
+
/* Define if the host CPU is a HPPA */
#undef HAVE_CPU_HPPA
/* Define if the host CPU is an x86 */
-#undef HAVE_CPU_I386
+#define HAVE_CPU_I386 1
/* Define if the host CPU is a IA64 */
#undef HAVE_CPU_IA64
/* Define if the host CPU is a PowerPC */
#undef HAVE_CPU_PPC
+/* Define if the host CPU is a 64 bit PowerPC */
+#undef HAVE_CPU_PPC64
+
/* Define if the host CPU is a S390 */
#undef HAVE_CPU_S390
/* Define if the GNU gettext() function is already present or preinstalled. */
#undef HAVE_GETTEXT
-/* Define if you have the iconv() function. */
+/* Have GMP library */
+#undef HAVE_GMP
+
+/* Define to 1 if you have the `gmtime_r' function. */
+#undef HAVE_GMTIME_R
+
+/* Have GSL library */
+#undef HAVE_GSL
+
+/* Define if you have the iconv() function and it works. */
#undef HAVE_ICONV
/* Define to 1 if you have the <inttypes.h> header file. */
#undef HAVE_INTTYPES_H
+/* Define to 1 if you have the `nsl' library (-lnsl). */
+#undef HAVE_LIBNSL
+
+/* Define to 1 if you have the `resolv' library (-lresolv). */
+#undef HAVE_LIBRESOLV
+
+/* Define to 1 if you have the `socket' library (-lsocket). */
+#undef HAVE_LIBSOCKET
+
/* Define if libxml2 is available */
#define HAVE_LIBXML2 1
+/* Define to 1 if you have the `localtime_r' function. */
+#undef HAVE_LOCALTIME_R
+
/* Define to 1 if you have the <memory.h> header file. */
#undef HAVE_MEMORY_H
/* Define to 1 if you have a working `mmap' system call. */
#undef HAVE_MMAP
+/* Have a monotonic clock */
+#undef HAVE_MONOTONIC_CLOCK
+
+/* Defined if compiling for OSX */
+#undef HAVE_OSX
+
+/* Define to 1 if you have the `poll' function. */
+#undef HAVE_POLL
+
+/* Define to 1 if you have the `posix_memalign' function. */
+#undef HAVE_POSIX_MEMALIGN
+
+/* Have posix timers */
+#undef HAVE_POSIX_TIMERS
+
+/* Define to 1 if you have the `ppoll' function. */
+#undef HAVE_PPOLL
+
/* defined if the compiler implements __PRETTY_FUNCTION__ */
#undef HAVE_PRETTY_FUNCTION
-/* Defined if we have register_printf_function () */
+/* Defined if we have printf specifier extensions available */
#undef HAVE_PRINTF_EXTENSION
/* Define to 1 if you have the <process.h> header file. */
#define HAVE_PROCESS_H 1
+/* Define to 1 if you have the `pselect' function. */
+#undef HAVE_PSELECT
+
+/* Define to 1 if you have the <pthread.h> header file. */
+#undef HAVE_PTHREAD_H
+
/* Define if RDTSC is available */
#undef HAVE_RDTSC
+/* Define to 1 if you have the `register_printf_function' function. */
+#undef HAVE_REGISTER_PRINTF_FUNCTION
+
+/* Define to 1 if you have the `register_printf_specifier' function. */
+#undef HAVE_REGISTER_PRINTF_SPECIFIER
+
/* Define to 1 if you have the `sigaction' function. */
#undef HAVE_SIGACTION
/* Define to 1 if you have the <stdint.h> header file. */
#undef HAVE_STDINT_H
+/* Define to 1 if you have the <stdio_ext.h> header file. */
+#undef HAVE_STDIO_EXT_H
+
/* Define to 1 if you have the <stdlib.h> header file. */
#define HAVE_STDLIB_H 1
/* Define to 1 if you have the <string.h> header file. */
#define HAVE_STRING_H 1
+/* Define to 1 if you have the <sys/param.h> header file. */
+#undef HAVE_SYS_PARAM_H
+
+/* Define to 1 if you have the <sys/prctl.h> header file. */
+#undef HAVE_SYS_PRCTL_H
+
/* Define to 1 if you have the <sys/socket.h> header file. */
#undef HAVE_SYS_SOCKET_H
/* Define to 1 if you have the <sys/stat.h> header file. */
#define HAVE_SYS_STAT_H 1
+/* Define to 1 if you have the <sys/times.h> header file. */
+#undef HAVE_SYS_TIMES_H
+
+/* Define to 1 if you have the <sys/time.h> header file. */
+#undef HAVE_SYS_TIME_H
+
/* Define to 1 if you have the <sys/types.h> header file. */
#define HAVE_SYS_TYPES_H 1
+/* Define to 1 if you have the <sys/utsname.h> header file. */
+#undef HAVE_SYS_UTSNAME_H
+
+/* Define to 1 if you have the <sys/wait.h> header file. */
+#undef HAVE_SYS_WAIT_H
+
+/* Have tm_gmtoff field in struct tm */
+#undef HAVE_TM_GMTOFF
+
/* Define to 1 if you have the <ucontext.h> header file. */
#undef HAVE_UCONTEXT_H
+/* Have __uint128_t type */
+#undef HAVE_UINT128_T
+
/* defined if unaligned memory access works correctly */
#undef HAVE_UNALIGNED_ACCESS
/* Define if valgrind should be used */
#undef HAVE_VALGRIND
+/* Define to 1 if you have the <valgrind/valgrind.h> header file. */
+#undef HAVE_VALGRIND_VALGRIND_H
+
/* Defined if compiling for Windows */
#define HAVE_WIN32 1
+/* Define to 1 if you have the <winsock2.h> header file. */
+#define HAVE_WINSOCK2_H 1
+
+/* the host CPU */
+#define HOST_CPU "i686"
+
/* library dir */
#ifdef _DEBUG
# define LIBDIR PREFIX "\\debug\\lib"
/* gettext locale dir */
#define LOCALEDIR PREFIX "\\share\\locale"
+/* Define to the sub-directory in which libtool stores uninstalled libraries.
+ */
+#undef LT_OBJDIR
+
+/* Define if you have no native inet_aton() function. */
+#undef NO_INET_ATON
+
+/* Define to 1 if your C compiler doesn't accept -c and -o together. */
+#undef NO_MINUS_C_MINUS_O
+
/* Name of package */
#define PACKAGE "gstreamer"
/* Define to the address where bug reports for this package should be sent. */
-#undef PACKAGE_BUGREPORT
+#define PACKAGE_BUGREPORT "http://bugzilla.gnome.org/enter_bug.cgi?product=GStreamer"
/* Define to the full name of this package. */
-#undef PACKAGE_NAME
+#define PACKAGE_NAME "GStreamer"
/* Define to the full name and version of this package. */
-#undef PACKAGE_STRING
+#define PACKAGE_STRING "GStreamer 0.10.32"
/* Define to the one symbol short name of this package. */
-#undef PACKAGE_TARNAME
+#define PACKAGE_TARNAME "gstreamer"
+
+/* Define to the home page for this package. */
+#undef PACKAGE_URL
/* Define to the version of this package. */
-#undef PACKAGE_VERSION
+#define PACKAGE_VERSION "0.10.32"
-/* Define the plugin directory */
+/* directory where plugins are located */
#ifdef _DEBUG
# define PLUGINDIR PREFIX "\\debug\\lib\\gstreamer-0.10"
#else
# define PLUGINDIR PREFIX "\\lib\\gstreamer-0.10"
#endif
+/* The size of `char', as computed by sizeof. */
+#undef SIZEOF_CHAR
+
+/* The size of `int', as computed by sizeof. */
+#undef SIZEOF_INT
+
+/* The size of `long', as computed by sizeof. */
+#undef SIZEOF_LONG
+
+/* The size of `short', as computed by sizeof. */
+#undef SIZEOF_SHORT
+
+/* The size of `void*', as computed by sizeof. */
+#undef SIZEOF_VOIDP
+
/* Define to 1 if you have the ANSI C header files. */
#undef STDC_HEADERS
#undef USE_POISONING
/* Version number of package */
-#define VERSION "0.10.1.1"
-
-/* Define to 1 if your processor stores words with the most significant byte
- first (like Motorola and SPARC, unlike Intel and VAX). */
-#undef WORDS_BIGENDIAN
+#define VERSION "0.10.32"
+
+/* Define WORDS_BIGENDIAN to 1 if your processor stores words with the most
+ significant byte first (like Motorola and SPARC, unlike Intel). */
+#if defined AC_APPLE_UNIVERSAL_BUILD
+# if defined __BIG_ENDIAN__
+# define WORDS_BIGENDIAN 1
+# endif
+#else
+# ifndef WORDS_BIGENDIAN
+# undef WORDS_BIGENDIAN
+# endif
+#endif
/* Number of bits in a file offset, on hosts where this is settable. */
#undef _FILE_OFFSET_BITS
/* Define for large files, on AIX-style hosts. */
#undef _LARGE_FILES
-/* Define to `__inline__' or `__inline' if that's what the C compiler
- calls it, or to nothing if 'inline' is not supported under any name. */
-/* #undef inline */
+/* We need at least WinXP SP2 for __stat64 */
+#undef __MSVCRT_VERSION__