summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 467035c)
raw | patch | inline | side by side (parent: 467035c)
author | Thomas Vander Stichele <thomas@apestaart.org> | |
Sun, 23 Dec 2001 00:07:59 +0000 (00:07 +0000) | ||
committer | Thomas Vander Stichele <thomas@apestaart.org> | |
Sun, 23 Dec 2001 00:07:59 +0000 (00:07 +0000) |
Original commit message from CVS:
moving bytestream in the same way as in gst-plugins since ac3parse needs it
moving bytestream in the same way as in gst-plugins since ac3parse needs it
libs/gst/Makefile.am | [new file with mode: 0644] | patch | blob |
libs/gst/bytestream/Makefile.am | [new file with mode: 0644] | patch | blob |
libs/gst/bytestream/bstest.c | [new file with mode: 0644] | patch | blob |
libs/gst/bytestream/bytestream.c | [new file with mode: 0644] | patch | blob |
libs/gst/bytestream/bytestream.h | [new file with mode: 0644] | patch | blob |
diff --git a/libs/gst/Makefile.am b/libs/gst/Makefile.am
--- /dev/null
+++ b/libs/gst/Makefile.am
@@ -0,0 +1,3 @@
+SUBDIRS = bytestream
+
+DIST_SUBDIRS = bytestream
diff --git a/libs/gst/bytestream/Makefile.am b/libs/gst/bytestream/Makefile.am
--- /dev/null
@@ -0,0 +1,15 @@
+libdir = $(libdir)/gst
+
+lib_LTLIBRARIES = libgstbytestream.la libgstbstest.la
+
+libgstbytestream_la_SOURCES = bytestream.c
+libgstbstest_la_SOURCES = bstest.c
+
+libgstbytestreamincludedir = $(includedir)/gst/bytestream
+libgstbytestreaminclude_HEADERS = bytestream.h
+
+libgstbytestream_la_LIBADD = $(GST_LIBS)
+libgstbytestream_la_CFLAGS = $(GST_CFLAGS)
+
+libgstbstest_la_LIBADD = $(GST_LIBS)
+libgstbstest_la_CFLAGS = $(GST_CFLAGS)
diff --git a/libs/gst/bytestream/bstest.c b/libs/gst/bytestream/bstest.c
--- /dev/null
@@ -0,0 +1,294 @@
+/* GStreamer
+ * Copyright (C) 1999,2000 Erik Walthinsen <omega@cse.ogi.edu>
+ * 2000 Wim Taymans <wtay@chello.be>
+ *
+ * gstidentity.c:
+ *
+ * This library is free software; you can redistribute it and/or
+ * modify it under the terms of the GNU Library General Public
+ * License as published by the Free Software Foundation; either
+ * version 2 of the License, or (at your option) any later version.
+ *
+ * This library is distributed in the hope that it will be useful,
+ * but WITHOUT ANY WARRANTY; without even the implied warranty of
+ * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU
+ * Library General Public License for more details.
+ *
+ * You should have received a copy of the GNU Library General Public
+ * License along with this library; if not, write to the
+ * Free Software Foundation, Inc., 59 Temple Place - Suite 330,
+ * Boston, MA 02111-1307, USA.
+ */
+
+#include <gst/gst.h>
+#include "gstbytestream.h"
+
+#define GST_TYPE_IDENTITY \
+ (gst_identity_get_type())
+#define GST_IDENTITY(obj) \
+ (G_TYPE_CHECK_INSTANCE_CAST((obj),GST_TYPE_IDENTITY,GstIdentity))
+#define GST_IDENTITY_CLASS(klass) \
+ (G_TYPE_CHECK_CLASS_CAST((klass),GST_TYPE_IDENTITY,GstIdentityClass))
+#define GST_IS_IDENTITY(obj) \
+ (G_TYPE_CHECK_INSTANCE_TYPE((obj),GST_TYPE_IDENTITY))
+#define GST_IS_IDENTITY_CLASS(obj) \
+ (G_TYPE_CHECK_CLASS_TYPE((klass),GST_TYPE_IDENTITY))
+
+typedef struct _GstIdentity GstIdentity;
+typedef struct _GstIdentityClass GstIdentityClass;
+
+struct _GstIdentity {
+ GstElement element;
+
+ GstPad *sinkpad;
+ GstPad *srcpad;
+
+ GstByteStream *bs;
+ gint byte_size;
+ gint count;
+};
+
+struct _GstIdentityClass {
+ GstElementClass parent_class;
+};
+
+GType gst_identity_get_type(void);
+
+
+GstElementDetails gst_identity_details = {
+ "ByteStreamTest",
+ "Filter",
+ "Test for the GstByteStream code",
+ VERSION,
+ "Erik Walthinsen <omega@temple-baptist.com>",
+ "(C) 2001",
+};
+
+
+/* Identity signals and args */
+enum {
+ /* FILL ME */
+ LAST_SIGNAL
+};
+
+enum {
+ ARG_0,
+ ARG_BYTE_SIZE,
+ ARG_COUNT,
+};
+
+
+static void gst_identity_class_init (GstIdentityClass *klass);
+static void gst_identity_init (GstIdentity *identity);
+
+static void gst_identity_set_property (GObject *object, guint prop_id, const GValue *value, GParamSpec *pspec);
+static void gst_identity_get_property (GObject *object, guint prop_id, GValue *value, GParamSpec *pspec);
+
+static void gst_identity_loop (GstElement *element);
+
+static GstElementClass *parent_class = NULL;
+// static guint gst_identity_signals[LAST_SIGNAL] = { 0 };
+
+GType
+gst_identity_get_type (void)
+{
+ static GType identity_type = 0;
+
+ if (!identity_type) {
+ static const GTypeInfo identity_info = {
+ sizeof(GstIdentityClass), NULL,
+ NULL,
+ (GClassInitFunc)gst_identity_class_init,
+ NULL,
+ NULL,
+ sizeof(GstIdentity),
+ 0,
+ (GInstanceInitFunc)gst_identity_init,
+ };
+ identity_type = g_type_register_static (GST_TYPE_ELEMENT, "GstBSTest", &identity_info, 0);
+ }
+ return identity_type;
+}
+
+static void
+gst_identity_class_init (GstIdentityClass *klass)
+{
+ GObjectClass *gobject_class;
+
+ gobject_class = (GObjectClass*)klass;
+
+ parent_class = g_type_class_ref (GST_TYPE_ELEMENT);
+
+ g_object_class_install_property (G_OBJECT_CLASS (klass), ARG_BYTE_SIZE,
+ g_param_spec_uint ("byte_size", "byte_size", "byte_size",
+ 0, G_MAXUINT, 0, G_PARAM_READWRITE));
+ g_object_class_install_property (G_OBJECT_CLASS (klass), ARG_COUNT,
+ g_param_spec_uint ("count", "count", "count",
+ 0, G_MAXUINT, 0, G_PARAM_READWRITE));
+
+ gobject_class->set_property = GST_DEBUG_FUNCPTR (gst_identity_set_property);
+ gobject_class->get_property = GST_DEBUG_FUNCPTR (gst_identity_get_property);
+}
+
+static GstPadNegotiateReturn
+gst_identity_negotiate_src (GstPad *pad, GstCaps **caps, gpointer *data)
+{
+ GstIdentity *identity;
+
+ identity = GST_IDENTITY (gst_pad_get_parent (pad));
+
+ return gst_pad_negotiate_proxy (pad, identity->sinkpad, caps);
+}
+
+static GstPadNegotiateReturn
+gst_identity_negotiate_sink (GstPad *pad, GstCaps **caps, gpointer *data)
+{
+ GstIdentity *identity;
+
+ identity = GST_IDENTITY (gst_pad_get_parent (pad));
+
+ return gst_pad_negotiate_proxy (pad, identity->srcpad, caps);
+}
+
+static void
+gst_identity_init (GstIdentity *identity)
+{
+ identity->sinkpad = gst_pad_new ("sink", GST_PAD_SINK);
+ gst_element_add_pad (GST_ELEMENT (identity), identity->sinkpad);
+ gst_pad_set_negotiate_function (identity->sinkpad, gst_identity_negotiate_sink);
+
+ identity->srcpad = gst_pad_new ("src", GST_PAD_SRC);
+ gst_element_add_pad (GST_ELEMENT (identity), identity->srcpad);
+ gst_pad_set_negotiate_function (identity->srcpad, gst_identity_negotiate_src);
+
+ gst_element_set_loop_function (GST_ELEMENT (identity), gst_identity_loop);
+
+ identity->byte_size = 384;
+ identity->count = 5;
+
+ identity->bs = gst_bytestream_new(identity->sinkpad);
+}
+
+static void
+gst_identity_loop (GstElement *element)
+{
+ GstIdentity *identity;
+ GstBuffer *buf;
+ int i;
+
+ g_return_if_fail (element != NULL);
+ g_return_if_fail (GST_IS_IDENTITY (element));
+
+ identity = GST_IDENTITY (element);
+
+/* THIS IS THE BUFFER BASED ONE
+ do {
+// g_print("\n");
+
+ for (i=0;i<identity->count;i++) {
+// g_print("bstest: getting a buffer of %d bytes\n",identity->byte_size);
+ buf = gst_bytestream_read(identity->bs,identity->byte_size);
+ if (!buf) g_print("BUFFER IS BOGUS\n");
+// g_print("pushing the buffer, %d bytes at %d\n",GST_BUFFER_SIZE(buf),GST_BUFFER_OFFSET(buf));
+ gst_pad_push(identity->srcpad,buf);
+// g_print("\n");
+ gst_bytestream_print_status(identity->bs);
+// g_print("\n\n");
+ }
+
+ exit(1);
+ } while (!GST_ELEMENT_IS_COTHREAD_STOPPING(element));
+*/
+
+/* THIS IS THE BYTE BASED ONE*/
+ do {
+ for (i=0;i<identity->count;i++) {
+ buf = gst_buffer_new();
+ // note that this is dangerous, as it does *NOT* refcount the data, it can go away!!!
+ GST_BUFFER_DATA(buf) = gst_bytestream_peek_bytes(identity->bs,identity->byte_size);
+ GST_BUFFER_SIZE(buf) = identity->byte_size;
+ GST_BUFFER_FLAG_SET(buf,GST_BUFFER_DONTFREE);
+ gst_pad_push(identity->srcpad,buf);
+ gst_bytestream_flush(identity->bs,identity->byte_size);
+ }
+
+ exit(1);
+ } while (!GST_ELEMENT_IS_COTHREAD_STOPPING(element));
+/**/
+}
+
+static void
+gst_identity_set_property (GObject *object, guint prop_id, const GValue *value, GParamSpec *pspec)
+{
+ GstIdentity *identity;
+
+ /* it's not null if we got it, but it might not be ours */
+ g_return_if_fail (GST_IS_IDENTITY (object));
+
+ identity = GST_IDENTITY (object);
+
+ switch (prop_id) {
+ case ARG_BYTE_SIZE:
+ identity->byte_size = g_value_get_uint (value);
+ break;
+ case ARG_COUNT:
+ identity->count = g_value_get_uint (value);
+ break;
+ default:
+ G_OBJECT_WARN_INVALID_PROPERTY_ID (object, prop_id, pspec);
+ break;
+ }
+}
+
+static void gst_identity_get_property(GObject *object, guint prop_id, GValue *value, GParamSpec *pspec) {
+ GstIdentity *identity;
+
+ /* it's not null if we got it, but it might not be ours */
+ g_return_if_fail (GST_IS_IDENTITY (object));
+
+ identity = GST_IDENTITY (object);
+
+ switch (prop_id) {
+ case ARG_BYTE_SIZE:
+ g_value_set_uint (value, identity->byte_size);
+ break;
+ case ARG_COUNT:
+ g_value_set_uint (value, identity->count);
+ break;
+ default:
+ G_OBJECT_WARN_INVALID_PROPERTY_ID (object, prop_id, pspec);
+ break;
+ }
+}
+
+static gboolean
+plugin_init (GModule *module, GstPlugin *plugin)
+{
+ GstElementFactory *factory;
+
+ // we need gstbytestream
+ if (!gst_library_load ("gstbytestream")) {
+ g_print("can't load bytestream\n");
+ return FALSE;
+ }
+
+ /* We need to create an ElementFactory for each element we provide.
+ * This consists of the name of the element, the GType identifier,
+ * and a pointer to the details structure at the top of the file.
+ */
+ factory = gst_elementfactory_new("gstbstest", GST_TYPE_IDENTITY, &gst_identity_details);
+ g_return_val_if_fail(factory != NULL, FALSE);
+
+ /* The very last thing is to register the elementfactory with the plugin. */
+ gst_plugin_add_feature (plugin, GST_PLUGIN_FEATURE (factory));
+
+ return TRUE;
+}
+
+GstPluginDesc plugin_desc = {
+ GST_VERSION_MAJOR,
+ GST_VERSION_MINOR,
+ "gstbstest",
+ plugin_init
+};
+
diff --git a/libs/gst/bytestream/bytestream.c b/libs/gst/bytestream/bytestream.c
--- /dev/null
@@ -0,0 +1,455 @@
+/* GStreamer
+ * Copyright (C) 2001 Erik Walthinsen <omega@temple-baptist.com>
+ *
+ * gstbytestream.c: adds a convenient bytestream based API to a pad.
+ *
+ * This library is free software; you can redistribute it and/or
+ * modify it under the terms of the GNU Library General Public
+ * License as published by the Free Software Foundation; either
+ * version 2 of the License, or (at your option) any later version.
+ *
+ * This library is distributed in the hope that it will be useful,
+ * but WITHOUT ANY WARRANTY; without even the implied warranty of
+ * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU
+ * Library General Public License for more details.
+ *
+ * You should have received a copy of the GNU Library General Public
+ * License along with this library; if not, write to the
+ * Free Software Foundation, Inc., 59 Temple Place - Suite 330,
+ * Boston, MA 02111-1307, USA.
+ */
+
+#include <stdio.h>
+#include <string.h>
+#include <stdlib.h>
+
+#include <gst/gstinfo.h>
+#include "gstbytestream.h"
+
+//#define BS_DEBUG
+
+#ifdef BS_DEBUG
+# define bs_print(format,args...) GST_DEBUG (GST_CAT_BUFFER, format, ## args)
+# define bs_status(bs) gst_bytestream_print_status(bs)
+#else
+# define bs_print(format,args...)
+# define bs_status(bs)
+#endif
+
+guint8 *gst_bytestream_assemble (GstByteStream * bs, guint32 len);
+
+/**
+ * gst_bytestream_new:
+ * @pad: the pad to attach the bytestream to
+ *
+ * creates a bytestream from the given pad
+ *
+ * Returns: a new #GstByteStream object
+ */
+GstByteStream *
+gst_bytestream_new (GstPad * pad)
+{
+ GstByteStream *bs = g_new (GstByteStream, 1);
+
+ bs->pad = pad;
+ bs->event = NULL;
+ bs->buflist = NULL;
+ bs->headbufavail = 0;
+ bs->listavail = 0;
+ bs->assembled = NULL;
+
+ return bs;
+}
+
+void
+gst_bytestream_destroy (GstByteStream * bs)
+{
+ GSList *walk;
+
+ if (bs->event)
+ gst_event_free (bs->event);
+
+ walk = bs->buflist;
+ while (walk) {
+ gst_buffer_unref (GST_BUFFER (walk->data));
+ walk = g_slist_next (walk);
+ }
+ g_slist_free (bs->buflist);
+ if (bs->assembled)
+ g_free (bs->assembled);
+ g_free (bs);
+}
+
+// HOW THIS WORKS:
+//
+// The fundamental structure is a singly-linked list of buffers. The
+// buffer on the front is the oldest, and thus the first to read data
+// from. The number of bytes left to be read in this buffer is stored
+// in bs->headbufavail. The number of bytes available in the entire
+// list (including the head buffer) is in bs->listavail.
+//
+// When a request is made for data (peek), _fill_bytes is called with
+// the number of bytes needed, but only if the listavail indicates
+// that there aren't already enough. This calls _get_next_buf until
+// the listavail is sufficient to satisfy the demand.
+//
+// _get_next_buf pulls a buffer from the pad the bytestream is attached
+// to, and shoves it in the list. There are actually two things it can
+// do. If there's already a buffer in the list, and the _is_span_fast()
+// test returns true, it will merge it with that last buffer. Otherwise
+// it will simply tack it onto the end of the list.
+//
+// The _peek itself first checks the simple case of the request fitting
+// within the head buffer, and if so creates a subbuffer and returns.
+// Otherwise, it creates a new buffer and allocates space for the request
+// and calls _assemble to fill it. We know we have to copy because this
+// case only happens when the _merge wasn't feasible during _get_next_buf.
+//
+// The _flush method repeatedly inspects the head buffer and flushes as
+// much data from it as it needs to, up to the size of the buffer. If
+// the flush decimates the buffer, it's stripped, unref'd, and removed.
+
+
+// get the next buffer
+// if the buffer can be merged with the head buffer, do so
+// else add it onto the head of the
+static gboolean
+gst_bytestream_get_next_buf (GstByteStream * bs)
+{
+ GstBuffer *nextbuf, *lastbuf;
+ GSList *end;
+
+ g_assert (!bs->event);
+
+ bs_print ("get_next_buf: pulling buffer\n");
+ nextbuf = gst_pad_pull (bs->pad);
+
+ if (GST_IS_EVENT (nextbuf))
+ {
+ bs->event = GST_EVENT (nextbuf);
+ return FALSE;
+ }
+
+ if (!nextbuf)
+ return FALSE;
+
+ bs_print ("get_next_buf: got buffer of %d bytes\n", GST_BUFFER_SIZE (nextbuf));
+
+ // first see if there are any buffers in the list at all
+ if (bs->buflist) {
+ bs_print ("gst_next_buf: there is at least one buffer in the list\n");
+ // now find the end of the list
+ end = g_slist_last (bs->buflist);
+ // get the buffer that's there
+ lastbuf = GST_BUFFER (end->data);
+
+ // see if we can marge cheaply
+ if (gst_buffer_is_span_fast (lastbuf, nextbuf)) {
+ bs_print ("get_next_buf: merging new buffer with last buf on list\n");
+ // it is, let's merge them (this is really an append, but...)
+ end->data = gst_buffer_merge (lastbuf, nextbuf);
+ // add to the length of the list
+ bs->listavail += GST_BUFFER_SIZE (nextbuf);
+
+ // have to check to see if we merged with the head buffer
+ if (end == bs->buflist) {
+ bs->headbufavail += GST_BUFFER_SIZE (nextbuf);
+ }
+
+ gst_buffer_unref (lastbuf);
+ gst_buffer_unref (nextbuf);
+
+ // if we can't, we just append this buffer
+ }
+ else {
+ bs_print ("get_next_buf: adding new buffer to the end of the list\n");
+ end = g_slist_append (end, nextbuf);
+ // also need to increment length of list and buffer count
+ bs->listavail += GST_BUFFER_SIZE (nextbuf);
+ }
+
+ // if there are no buffers in the list
+ }
+ else {
+ bs_print ("get_next_buf: buflist is empty, adding new buffer to list\n");
+ // put this on the end of the list
+ bs->buflist = g_slist_append (bs->buflist, nextbuf);
+ // and increment the number of bytes in the list
+ bs->listavail = GST_BUFFER_SIZE (nextbuf);
+ // set the head buffer avail to the size
+ bs->headbufavail = GST_BUFFER_SIZE (nextbuf);
+ }
+
+ return TRUE;
+}
+
+static gboolean
+gst_bytestream_fill_bytes (GstByteStream * bs, guint32 len)
+{
+ // as long as we don't have enough, we get more buffers
+ while (bs->listavail < len) {
+ bs_print ("fill_bytes: there are %d bytes in the list, we need %d\n", bs->listavail, len);
+ if (!gst_bytestream_get_next_buf (bs))
+ return FALSE;
+ }
+
+ return TRUE;
+}
+
+
+GstBuffer *
+gst_bytestream_peek (GstByteStream * bs, guint32 len)
+{
+ GstBuffer *headbuf, *retbuf = NULL;
+
+ g_return_val_if_fail (bs != NULL, NULL);
+ g_return_val_if_fail (len > 0, NULL);
+
+ bs_print ("peek: asking for %d bytes\n", len);
+
+ // make sure we have enough
+ bs_print ("peek: there are %d bytes in the list\n", bs->listavail);
+ if (len > bs->listavail) {
+ if (!gst_bytestream_fill_bytes (bs, len))
+ return NULL;
+ bs_print ("peek: there are now %d bytes in the list\n", bs->listavail);
+ }
+ bs_status (bs);
+
+ // extract the head buffer
+ headbuf = GST_BUFFER (bs->buflist->data);
+
+ // if the requested bytes are in the current buffer
+ bs_print ("peek: headbufavail is %d\n", bs->headbufavail);
+ if (len <= bs->headbufavail) {
+ bs_print ("peek: there are enough bytes in headbuf (need %d, have %d)\n", len, bs->headbufavail);
+ // create a sub-buffer of the headbuf
+ retbuf = gst_buffer_create_sub (headbuf, GST_BUFFER_SIZE (headbuf) - bs->headbufavail, len);
+
+ // otherwise we need to figure out how to assemble one
+ }
+ else {
+ bs_print ("peek: current buffer is not big enough for len %d\n", len);
+
+ retbuf = gst_buffer_new ();
+ GST_BUFFER_SIZE (retbuf) = len;
+ GST_BUFFER_DATA (retbuf) = gst_bytestream_assemble (bs, len);
+ if (GST_BUFFER_OFFSET (headbuf) != -1)
+ GST_BUFFER_OFFSET (retbuf) = GST_BUFFER_OFFSET (headbuf) + (GST_BUFFER_SIZE (headbuf) - bs->headbufavail);
+ }
+
+ return retbuf;
+}
+
+guint8 *
+gst_bytestream_peek_bytes (GstByteStream * bs, guint32 len)
+{
+ GstBuffer *headbuf;
+ guint8 *data = NULL;
+
+ g_return_val_if_fail (bs != NULL, NULL);
+ g_return_val_if_fail (len > 0, NULL);
+
+ bs_print ("peek_bytes: asking for %d bytes\n", len);
+ if (bs->assembled) {
+ g_free (bs->assembled);
+ bs->assembled = NULL;
+ }
+
+ // make sure we have enough
+ bs_print ("peek_bytes: there are %d bytes in the list\n", bs->listavail);
+ if (len > bs->listavail) {
+ if (!gst_bytestream_fill_bytes (bs, len))
+ return NULL;
+ bs_print ("peek_bytes: there are now %d bytes in the list\n", bs->listavail);
+ }
+ bs_status (bs);
+
+ // extract the head buffer
+ headbuf = GST_BUFFER (bs->buflist->data);
+
+ // if the requested bytes are in the current buffer
+ bs_print ("peek_bytes: headbufavail is %d\n", bs->headbufavail);
+ if (len <= bs->headbufavail) {
+ bs_print ("peek_bytes: there are enough bytes in headbuf (need %d, have %d)\n", len, bs->headbufavail);
+ // create a sub-buffer of the headbuf
+ data = GST_BUFFER_DATA (headbuf) + (GST_BUFFER_SIZE (headbuf) - bs->headbufavail);
+
+ // otherwise we need to figure out how to assemble one
+ }
+ else {
+ bs_print ("peek_bytes: current buffer is not big enough for len %d\n", len);
+
+ data = gst_bytestream_assemble (bs, len);
+ bs->assembled = data;
+ bs->assembled_len = len;
+ }
+
+ return data;
+}
+
+guint8 *
+gst_bytestream_assemble (GstByteStream * bs, guint32 len)
+{
+ guint8 *data = g_malloc (len);
+ GSList *walk;
+ guint32 copied = 0;
+ GstBuffer *buf;
+
+ // copy the data from the curbuf
+ buf = GST_BUFFER (bs->buflist->data);
+ bs_print ("assemble: copying %d bytes from curbuf at %d to *data\n", bs->headbufavail,
+ GST_BUFFER_SIZE (buf) - bs->headbufavail);
+ memcpy (data, GST_BUFFER_DATA (buf) + GST_BUFFER_SIZE (buf) - bs->headbufavail, bs->headbufavail);
+ copied += bs->headbufavail;
+
+ // asumption is made that the buffers all exist in the list
+ walk = g_slist_next (bs->buflist);
+ while (copied < len) {
+ buf = GST_BUFFER (walk->data);
+ if (GST_BUFFER_SIZE (buf) < (len - copied)) {
+ bs_print ("assemble: copying %d bytes from buf to output offset %d\n", GST_BUFFER_SIZE (buf), copied);
+ memcpy (data + copied, GST_BUFFER_DATA (buf), GST_BUFFER_SIZE (buf));
+ copied += GST_BUFFER_SIZE (buf);
+ }
+ else {
+ bs_print ("assemble: copying %d bytes from buf to output offset %d\n", len - copied, copied);
+ memcpy (data + copied, GST_BUFFER_DATA (buf), len - copied);
+ copied = len;
+ }
+ walk = g_slist_next (walk);
+ }
+
+ return data;
+}
+
+gboolean
+gst_bytestream_flush (GstByteStream * bs, guint32 len)
+{
+ bs_print ("flush: flushing %d bytes\n", len);
+
+ // make sure we have enough
+ bs_print ("flush: there are %d bytes in the list\n", bs->listavail);
+ if (len > bs->listavail) {
+ if (!gst_bytestream_fill_bytes (bs, len))
+ return FALSE;
+ bs_print ("flush: there are now %d bytes in the list\n", bs->listavail);
+ }
+
+ gst_bytestream_flush_fast (bs, len);
+
+ return TRUE;
+}
+
+void
+gst_bytestream_flush_fast (GstByteStream * bs, guint32 len)
+{
+ GstBuffer *headbuf;
+
+ g_assert (len <= bs->listavail);
+
+ if (bs->assembled) {
+ g_free (bs->assembled);
+ bs->assembled = NULL;
+ }
+
+ // repeat until we've flushed enough data
+ while (len > 0) {
+ headbuf = GST_BUFFER (bs->buflist->data);
+
+ bs_print ("flush: analyzing buffer that's %d bytes long, offset %d\n", GST_BUFFER_SIZE (headbuf),
+ GST_BUFFER_OFFSET (headbuf));
+
+ // if there's enough to complete the flush
+ if (bs->headbufavail > len) {
+ // just trim it off
+ bs_print ("flush: trimming %d bytes off end of headbuf\n", len);
+ bs->headbufavail -= len;
+ bs->listavail -= len;
+ len = 0;
+
+ // otherwise we have to trim the whole buffer
+ }
+ else {
+ bs_print ("flush: removing head buffer completely\n");
+ // remove it from the list
+ bs->buflist = g_slist_delete_link (bs->buflist, bs->buflist);
+ // trim it from the avail size
+ bs->listavail -= bs->headbufavail;
+ // record that we've trimmed this many bytes
+ len -= bs->headbufavail;
+ // unref it
+ gst_buffer_unref (headbuf);
+
+ // record the new headbufavail
+ if (bs->buflist) {
+ bs->headbufavail = GST_BUFFER_SIZE (GST_BUFFER (bs->buflist->data));
+ bs_print ("flush: next headbuf is %d bytes\n", bs->headbufavail);
+ }
+ else {
+ bs_print ("flush: no more bytes at all\n");
+ }
+ }
+
+ bs_print ("flush: bottom of while(), len is now %d\n", len);
+ }
+}
+
+GstBuffer *
+gst_bytestream_read (GstByteStream * bs, guint32 len)
+{
+ GstBuffer *buf = gst_bytestream_peek (bs, len);
+ if (!buf)
+ return NULL;
+
+ gst_bytestream_flush_fast (bs, len);
+
+ return buf;
+}
+
+
+/**
+ * gst_bytestream_get_status
+ * @bs: a bytestream
+ * @avail_out: total number of bytes buffered
+ * @event_out: an event
+ *
+ * When an event occurs, the bytestream will return NULL. You must
+ * retrieve the event using this API before reading more bytes from
+ * the stream.
+ *
+ * It is possible for the bytestream to return NULL due to running
+ * out of buffers, however, this indicates a bug because an EOS
+ * event should have been sent.
+ */
+void
+gst_bytestream_get_status (GstByteStream *bs,
+ guint32 *avail_out,
+ GstEvent **event_out)
+{
+ if (avail_out)
+ *avail_out = bs->listavail;
+
+ if (event_out)
+ {
+ *event_out = bs->event;
+ bs->event = NULL;
+ }
+}
+
+void
+gst_bytestream_print_status (GstByteStream * bs)
+{
+ GSList *walk;
+ GstBuffer *buf;
+
+ bs_print ("STATUS: head buffer has %d bytes available\n", bs->headbufavail);
+ bs_print ("STATUS: list has %d bytes available\n", bs->listavail);
+ walk = bs->buflist;
+ while (walk) {
+ buf = GST_BUFFER (walk->data);
+ walk = g_slist_next (walk);
+
+ bs_print ("STATUS: buffer starts at %d and is %d bytes long\n", GST_BUFFER_OFFSET (buf), GST_BUFFER_SIZE (buf));
+ }
+}
diff --git a/libs/gst/bytestream/bytestream.h b/libs/gst/bytestream/bytestream.h
--- /dev/null
@@ -0,0 +1,57 @@
+/* GStreamer
+ * Copyright (C) 2001 Erik Walthinsen <omega@temple-baptist.com>
+ *
+ * This library is free software; you can redistribute it and/or
+ * modify it under the terms of the GNU Library General Public
+ * License as published by the Free Software Foundation; either
+ * version 2 of the License, or (at your option) any later version.
+ *
+ * This library is distributed in the hope that it will be useful,
+ * but WITHOUT ANY WARRANTY; without even the implied warranty of
+ * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU
+ * Library General Public License for more details.
+ *
+ * You should have received a copy of the GNU Library General Public
+ * License along with this library; if not, write to the
+ * Free Software Foundation, Inc., 59 Temple Place - Suite 330,
+ * Boston, MA 02111-1307, USA.
+ */
+
+#ifndef __GST_BYTESTREAM_H__
+#define __GST_BYTESTREAM_H__
+
+#include <gst/gst.h>
+
+#ifdef __cplusplus
+extern "C" {
+#endif /* __cplusplus */
+
+typedef struct _GstByteStream GstByteStream;
+
+struct _GstByteStream {
+ GstPad *pad;
+
+ GstEvent * event;
+
+ GSList *buflist;
+ guint32 headbufavail;
+ guint32 listavail;
+
+ // we keep state of assembled pieces
+ guint8 *assembled;
+ guint32 assembled_len;
+};
+
+GstByteStream* gst_bytestream_new (GstPad *pad);
+void gst_bytestream_destroy (GstByteStream *bs);
+
+GstBuffer* gst_bytestream_read (GstByteStream *bs, guint32 len);
+GstBuffer* gst_bytestream_peek (GstByteStream *bs, guint32 len);
+guint8* gst_bytestream_peek_bytes (GstByteStream *bs, guint32 len);
+gboolean gst_bytestream_flush (GstByteStream *bs, guint32 len);
+void gst_bytestream_flush_fast (GstByteStream * bs, guint32 len);
+void gst_bytestream_get_status (GstByteStream *bs, guint32 *avail_out, GstEvent **event_out);
+
+void gst_bytestream_print_status (GstByteStream *bs);
+
+#endif /* __GST_BYTESTREAM_H__ */