summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 6c40c75)
raw | patch | inline | side by side (parent: 6c40c75)
author | Tim-Philipp Müller <tim@centricular.net> | |
Thu, 6 Apr 2006 15:46:04 +0000 (15:46 +0000) | ||
committer | Tim-Philipp Müller <tim@centricular.net> | |
Thu, 6 Apr 2006 15:46:04 +0000 (15:46 +0000) |
Original commit message from CVS:
* gst/gstpad.c:
Typo fixes in docs.
* gst/gstpad.c:
Typo fixes in docs.
ChangeLog | patch | blob | history | |
gst/gstpad.c | patch | blob | history |
diff --git a/ChangeLog b/ChangeLog
index b3be0977a8a202c194ddb5510c5649783849a5c7..955db0d2e75402d6bf54dedef18d084fb000dc8d 100644 (file)
--- a/ChangeLog
+++ b/ChangeLog
+2006-04-06 Tim-Philipp Müller <tim at centricular dot net>
+
+ * gst/gstpad.c:
+ Typo fixes in docs.
+
2006-04-06 Michael Smith <msmith@fluendo.com>
* gst/gstpad.c: (gst_pad_set_property):
diff --git a/gst/gstpad.c b/gst/gstpad.c
index c78992ecac9fcce6d1eefc46f0ff1cd76ef42a02..4788b063132b07cea12243ebccec47c76e23e39b 100644 (file)
--- a/gst/gstpad.c
+++ b/gst/gstpad.c
*
* Sets the given setcaps function for the pad. The setcaps function
* will be called whenever a buffer with a new media type is pushed or
- * pulled from the pad. The pad/element needs to update it's internal
+ * pulled from the pad. The pad/element needs to update its internal
* structures to process the new media type. If this new type is not
* acceptable, the setcaps function should return FALSE.
*/
* @pad: a #GstPad to get the capabilities of.
*
* Gets the capabilities this pad can produce or consume.
- * Note that this method doesn't necessarily returns the caps set by
+ * Note that this method doesn't necessarily return the caps set by
* gst_pad_set_caps() - use #GST_PAD_CAPS for that instead.
* gst_pad_get_caps returns all possible caps a pad can operate with, using
* the pad's get_caps function;