summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: d03ae79)
raw | patch | inline | side by side (parent: d03ae79)
author | Thomas Vander Stichele <thomas@apestaart.org> | |
Mon, 23 Sep 2002 05:26:44 +0000 (05:26 +0000) | ||
committer | Thomas Vander Stichele <thomas@apestaart.org> | |
Mon, 23 Sep 2002 05:26:44 +0000 (05:26 +0000) |
Original commit message from CVS:
yay for cookies
yay for cookies
README | patch | blob | history |
index 99fd6aceb4e2cf239287bcb3815fbad24ae4f934..12c0836526578112db2c0534da363d7d1ca5c655 100644 (file)
--- a/README
+++ b/README
+WHAT IT IS
+----------
This is GStreamer, a framework for streaming media. The
fundamental design comes from the video pipeline at Oregon Graduate
Institute, as well as some ideas from DirectMedia. It's based on plug-ins
to release binary codecs for Linux, until such time as they get a clue and
release the source.
+COMPILING FROM SOURCE
+---------------------
+- check output of ./configure --help to see if any options apply to you
+- run
+ ./configure
+ make
-Developer note: When building from CVS sources, you will need to run
-autogen.sh to generate the build system files.
+ to build GStreamer.
+- if you want to install it (not required), run
+ make install
+- You should create a registry for things to work.
+ If you ran make install in the previous step, run
+ gst-register
+ as root.
+
+ If you didn't install, run
+ tools/gst-register
+ as a normal user.
+
+- try out a simple test:
+ gst-launch fakesrc num_buffers=5 ! fakesink
+ (If you didn't install GStreamer, again prefix gst-launch with tools/)
+
+ If it outputs a bunch of messages from fakesrc and fakesink, everything is
+ ok.
+
+- After this, you're ready to install gst-plugins, which will provide the
+ functionality you're probably looking for by now, so go on and read
+ that README.
+
+COMPILING FROM CVS
+------------------
+When building from CVS sources, you will need to run autogen.sh to generate
+the build system files.
GStreamer is cutting-edge stuff. To be a CVS developer, you need
-cutting-edge tools.
+what used to be considered cutting-edge tools.
ATM, most of us have at least these versions :
* autoconf 2.52 (NOT 2.52d)
* automake 1.5
-* libtool 1.4
+* libtool 1.4 (NOT Gentoo's genetic failure 1.4.2)
* pkg-config 0.8.0
autogen.sh will check for these versions and complain if you don't have
-them.
+them. You can also specify specific versions of automake and autoconf with
+--with-automake and --with-autoconf
Check autogen.sh options by running autogen.sh --help
prefix has been added to autogen.sh but will be passed on to configure because
some build scripts like that.
+When you have done this once, you can use autoregen.sh to re-autogen with
+the last passed options as a handy shortcut. Use it.
+
+After the autogen.sh stage, you can follow the directions listed in
+"COMPILING FROM SOURCE"