summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 9a5109b)
raw | patch | inline | side by side (parent: 9a5109b)
author | Sebastian Dröge <sebastian.droege@collabora.co.uk> | |
Fri, 28 Oct 2011 07:18:55 +0000 (09:18 +0200) | ||
committer | Sebastian Dröge <sebastian.droege@collabora.co.uk> | |
Fri, 28 Oct 2011 07:36:06 +0000 (09:36 +0200) |
This handles muxing of sparse/subtitle streams and has
lots of cleanup. Still missing is special support for
live streams but this can be added later without breaking
API/ABI.
Based on the version from the videomixer plugin.
https://bugzilla.gnome.org/show_bug.cgi?id=415754
lots of cleanup. Still missing is special support for
live streams but this can be added later without breaking
API/ABI.
Based on the version from the videomixer plugin.
https://bugzilla.gnome.org/show_bug.cgi?id=415754
libs/gst/base/Makefile.am | patch | blob | history | |
libs/gst/base/gstcollectpads2.c | [new file with mode: 0644] | patch | blob |
libs/gst/base/gstcollectpads2.h | [new file with mode: 0644] | patch | blob |
index f6fa3efa7f34f432f10325abb7e5a81f4b34a193..4c8bccfec03c02c42299d5bb271416d58b917869 100644 (file)
gstbytereader.c \
gstbytewriter.c \
gstcollectpads.c \
+ gstcollectpads2.c \
gstpushsrc.c \
gsttypefindhelper.c \
gstdataqueue.c
gstbytereader.h \
gstbytewriter.h \
gstcollectpads.h \
+ gstcollectpads2.h \
gstpushsrc.h \
gsttypefindhelper.h \
gstdataqueue.h
diff --git a/libs/gst/base/gstcollectpads2.c b/libs/gst/base/gstcollectpads2.c
--- /dev/null
@@ -0,0 +1,1975 @@
+/* GStreamer
+ * Copyright (C) 2005 Wim Taymans <wim@fluendo.com>
+ * Copyright (C) 2008 Mark Nauwelaerts <mnauw@users.sourceforge.net>
+ * Copyright (C) 2010 Sebastian Dröge <sebastian.droege@collabora.co.uk>
+ *
+ * gstcollectpads2.c:
+ *
+ * This library is free software; you can redistribute it and/or
+ * modify it under the terms of the GNU Library General Public
+ * License as published by the Free Software Foundation; either
+ * version 2 of the License, or (at your option) any later version.
+ *
+ * This library is distributed in the hope that it will be useful,
+ * but WITHOUT ANY WARRANTY; without even the implied warranty of
+ * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU
+ * Library General Public License for more details.
+ *
+ * You should have received a copy of the GNU Library General Public
+ * License along with this library; if not, write to the
+ * Free Software Foundation, Inc., 59 Temple Place - Suite 330,
+ * Boston, MA 02111-1307, USA.
+ */
+/**
+ * SECTION:gstcollectpads2
+ * @short_description: manages a set of pads that operate in collect mode
+ * @see_also:
+ *
+ * Manages a set of pads that operate in collect mode. This means that control
+ * is given to the manager of this object when all pads have data.
+ * <itemizedlist>
+ * <listitem><para>
+ * Collectpads are created with gst_collect_pads2_new(). A callback should then
+ * be installed with gst_collect_pads2_set_function ().
+ * </para></listitem>
+ * <listitem><para>
+ * Pads are added to the collection with gst_collect_pads2_add_pad()/
+ * gst_collect_pads2_remove_pad(). The pad
+ * has to be a sinkpad. The chain and event functions of the pad are
+ * overridden. The element_private of the pad is used to store
+ * private information for the collectpads.
+ * </para></listitem>
+ * <listitem><para>
+ * For each pad, data is queued in the _chain function or by
+ * performing a pull_range.
+ * </para></listitem>
+ * <listitem><para>
+ * When data is queued on all pads in waiting mode, the callback function is called.
+ * </para></listitem>
+ * <listitem><para>
+ * Data can be dequeued from the pad with the gst_collect_pads2_pop() method.
+ * One can peek at the data with the gst_collect_pads2_peek() function.
+ * These functions will return NULL if the pad received an EOS event. When all
+ * pads return NULL from a gst_collect_pads2_peek(), the element can emit an EOS
+ * event itself.
+ * </para></listitem>
+ * <listitem><para>
+ * Data can also be dequeued in byte units using the gst_collect_pads2_available(),
+ * gst_collect_pads2_read() and gst_collect_pads2_flush() calls.
+ * </para></listitem>
+ * <listitem><para>
+ * Elements should call gst_collect_pads2_start() and gst_collect_pads2_stop() in
+ * their state change functions to start and stop the processing of the collectpads.
+ * The gst_collect_pads2_stop() call should be called before calling the parent
+ * element state change function in the PAUSED_TO_READY state change to ensure
+ * no pad is blocked and the element can finish streaming.
+ * </para></listitem>
+ * <listitem><para>
+ * gst_collect_pads2_collect() and gst_collect_pads2_collect_range() can be used by
+ * elements that start a #GstTask to drive the collect_pads2. This feature is however
+ * not yet implemented.
+ * </para></listitem>
+ * <listitem><para>
+ * gst_collect_pads2_set_waiting() sets a pad to waiting or non-waiting mode.
+ * CollectPads element is not waiting for data to be collected on non-waiting pads.
+ * Thus these pads may but need not have data when the callback is called.
+ * All pads are in waiting mode by default.
+ * </para></listitem>
+ * </itemizedlist>
+ *
+ * Last reviewed on 2008-03-14 (0.10.17)
+ *
+ * Since: 0.10.36
+ */
+
+#include "gstcollectpads2.h"
+
+GST_DEBUG_CATEGORY_STATIC (collect_pads2_debug);
+#define GST_CAT_DEFAULT collect_pads2_debug
+
+GST_BOILERPLATE (GstCollectPads2, gst_collect_pads2, GstObject,
+ GST_TYPE_OBJECT);
+
+static void gst_collect_pads2_clear (GstCollectPads2 * pads,
+ GstCollectData2 * data);
+static GstFlowReturn gst_collect_pads2_chain (GstPad * pad, GstBuffer * buffer);
+static gboolean gst_collect_pads2_event (GstPad * pad, GstEvent * event);
+static void gst_collect_pads2_finalize (GObject * object);
+static GstFlowReturn gst_collect_pads2_default_collected (GstCollectPads2 *
+ pads, gpointer user_data);
+static gint gst_collect_pads2_default_compare_func (GstCollectPads2 * pads,
+ GstCollectData2 * data1, GstClockTime timestamp1, GstCollectData2 * data2,
+ GstClockTime timestamp2, gpointer user_data);
+static gboolean gst_collect_pads2_recalculate_full (GstCollectPads2 * pads);
+static void ref_data (GstCollectData2 * data);
+static void unref_data (GstCollectData2 * data);
+
+/* Some properties are protected by LOCK, others by STREAM_LOCK
+ * However, manipulating either of these partitions may require
+ * to signal/wake a _WAIT, so use a separate (sort of) event to prevent races
+ * Alternative implementations are possible, e.g. some low-level re-implementing
+ * of the 2 above locks to drop both of them atomically when going into _WAIT.
+ */
+#define GST_COLLECT_PADS2_GET_EVT_COND(pads) (((GstCollectPads2 *)pads)->evt_cond)
+#define GST_COLLECT_PADS2_GET_EVT_LOCK(pads) (((GstCollectPads2 *)pads)->evt_lock)
+#define GST_COLLECT_PADS2_EVT_WAIT(pads, cookie) G_STMT_START { \
+ g_mutex_lock (GST_COLLECT_PADS2_GET_EVT_LOCK (pads)); \
+ /* should work unless a lot of event'ing and thread starvation */\
+ while (cookie == ((GstCollectPads2 *) pads)->evt_cookie) \
+ g_cond_wait (GST_COLLECT_PADS2_GET_EVT_COND (pads), \
+ GST_COLLECT_PADS2_GET_EVT_LOCK (pads)); \
+ cookie = ((GstCollectPads2 *) pads)->evt_cookie; \
+ g_mutex_unlock (GST_COLLECT_PADS2_GET_EVT_LOCK (pads)); \
+} G_STMT_END
+#define GST_COLLECT_PADS2_EVT_WAIT_TIMED(pads, cookie, timeout) G_STMT_START { \
+ GTimeVal __tv; \
+ \
+ g_get_current_time (&tv); \
+ g_time_val_add (&tv, timeout); \
+ \
+ g_mutex_lock (GST_COLLECT_PADS2_GET_EVT_LOCK (pads)); \
+ /* should work unless a lot of event'ing and thread starvation */\
+ while (cookie == ((GstCollectPads2 *) pads)->evt_cookie) \
+ g_cond_timed_wait (GST_COLLECT_PADS2_GET_EVT_COND (pads), \
+ GST_COLLECT_PADS2_GET_EVT_LOCK (pads), &tv); \
+ cookie = ((GstCollectPads2 *) pads)->evt_cookie; \
+ g_mutex_unlock (GST_COLLECT_PADS2_GET_EVT_LOCK (pads)); \
+} G_STMT_END
+#define GST_COLLECT_PADS2_EVT_BROADCAST(pads) G_STMT_START { \
+ g_mutex_lock (GST_COLLECT_PADS2_GET_EVT_LOCK (pads)); \
+ /* never mind wrap-around */ \
+ ++(((GstCollectPads2 *) pads)->evt_cookie); \
+ g_cond_broadcast (GST_COLLECT_PADS2_GET_EVT_COND (pads)); \
+ g_mutex_unlock (GST_COLLECT_PADS2_GET_EVT_LOCK (pads)); \
+} G_STMT_END
+#define GST_COLLECT_PADS2_EVT_INIT(cookie) G_STMT_START { \
+ g_mutex_lock (GST_COLLECT_PADS2_GET_EVT_LOCK (pads)); \
+ cookie = ((GstCollectPads2 *) pads)->evt_cookie; \
+ g_mutex_unlock (GST_COLLECT_PADS2_GET_EVT_LOCK (pads)); \
+} G_STMT_END
+
+static void
+gst_collect_pads2_base_init (gpointer g_class)
+{
+ /* Do nothing here */
+}
+
+static void
+gst_collect_pads2_class_init (GstCollectPads2Class * klass)
+{
+ GObjectClass *gobject_class = (GObjectClass *) klass;
+
+ GST_DEBUG_CATEGORY_INIT (collect_pads2_debug, "collectpads2", 0,
+ "GstCollectPads2");
+
+ gobject_class->finalize = GST_DEBUG_FUNCPTR (gst_collect_pads2_finalize);
+}
+
+static void
+gst_collect_pads2_init (GstCollectPads2 * pads, GstCollectPads2Class * g_class)
+{
+ pads->data = NULL;
+ pads->cookie = 0;
+ pads->numpads = 0;
+ pads->queuedpads = 0;
+ pads->eospads = 0;
+ pads->started = FALSE;
+
+ g_static_rec_mutex_init (&pads->stream_lock);
+
+ pads->func = gst_collect_pads2_default_collected;
+ pads->user_data = NULL;
+ pads->event_func = NULL;
+ pads->event_user_data = NULL;
+
+ pads->prepare_buffer_func = NULL;
+ pads->prepare_buffer_user_data = NULL;
+
+ /* members for default muxing */
+ pads->buffer_func = NULL;
+ pads->buffer_user_data = NULL;
+ pads->compare_func = gst_collect_pads2_default_compare_func;
+ pads->compare_user_data = NULL;
+ pads->earliest_data = NULL;
+ pads->earliest_time = GST_CLOCK_TIME_NONE;
+
+ /* members to manage the pad list */
+ pads->pad_cookie = 0;
+ pads->pad_list = NULL;
+
+ /* members for event */
+ pads->evt_lock = g_mutex_new ();
+ pads->evt_cond = g_cond_new ();
+ pads->evt_cookie = 0;
+}
+
+static void
+gst_collect_pads2_finalize (GObject * object)
+{
+ GstCollectPads2 *pads = GST_COLLECT_PADS2 (object);
+
+ GST_DEBUG_OBJECT (object, "finalize");
+
+ g_static_rec_mutex_free (&pads->stream_lock);
+
+ g_cond_free (pads->evt_cond);
+ g_mutex_free (pads->evt_lock);
+
+ /* Remove pads and free pads list */
+ g_slist_foreach (pads->pad_list, (GFunc) unref_data, NULL);
+ g_slist_foreach (pads->data, (GFunc) unref_data, NULL);
+ g_slist_free (pads->data);
+ g_slist_free (pads->pad_list);
+
+ G_OBJECT_CLASS (parent_class)->finalize (object);
+}
+
+/**
+ * gst_collect_pads2_new:
+ *
+ * Create a new instance of #GstCollectsPads.
+ *
+ * Returns: a new #GstCollectPads2, or NULL in case of an error.
+ *
+ * MT safe.
+ *
+ * Since: 0.10.36
+ */
+GstCollectPads2 *
+gst_collect_pads2_new (void)
+{
+ GstCollectPads2 *newcoll;
+
+ newcoll = g_object_new (GST_TYPE_COLLECT_PADS2, NULL);
+
+ return newcoll;
+}
+
+/**
+ * gst_collect_pads2_set_prepare_buffer_function:
+ * @pads: the collectpads to use
+ * @func: the function to set
+ * @user_data: user data passed to the function
+ *
+ * Set the callback function and user data that will be called
+ * for every buffer that arrives.
+ *
+ * MT safe.
+ *
+ * Since: 0.10.36
+ */
+void
+gst_collect_pads2_set_prepare_buffer_function (GstCollectPads2 * pads,
+ GstCollectPads2BufferFunction func, gpointer user_data)
+{
+ g_return_if_fail (pads != NULL);
+ g_return_if_fail (GST_IS_COLLECT_PADS2 (pads));
+
+ GST_OBJECT_LOCK (pads);
+ pads->prepare_buffer_func = func;
+ pads->prepare_buffer_user_data = user_data;
+ GST_OBJECT_UNLOCK (pads);
+}
+
+/* Must be called with GstObject lock! */
+static void
+gst_collect_pads2_set_buffer_function_locked (GstCollectPads2 * pads,
+ GstCollectPads2BufferFunction func, gpointer user_data)
+{
+ pads->buffer_func = func;
+ pads->buffer_user_data = user_data;
+}
+
+/**
+ * gst_collect_pads2_set_buffer_function:
+ * @pads: the collectpads to use
+ * @func: the function to set
+ * @user_data: user data passed to the function
+ *
+ * Set the callback function and user data that will be called with
+ * the oldest buffer when all pads have been collected.
+ *
+ * MT safe.
+ *
+ * Since: 0.10.36
+ */
+void
+gst_collect_pads2_set_buffer_function (GstCollectPads2 * pads,
+ GstCollectPads2BufferFunction func, gpointer user_data)
+{
+ g_return_if_fail (pads != NULL);
+ g_return_if_fail (GST_IS_COLLECT_PADS2 (pads));
+
+ GST_OBJECT_LOCK (pads);
+ gst_collect_pads2_set_buffer_function_locked (pads, func, user_data);
+ GST_OBJECT_UNLOCK (pads);
+}
+
+/**
+ * gst_collect_pads2_set_compare_function:
+ * @pads: the pads to use
+ * @func: the function to set
+ * @user_data: user data passed to the function
+ *
+ * Set the timestamp comparison function.
+ *
+ * MT safe.
+ *
+ * Since: 0.10.36
+ */
+/* NOTE allowing to change comparison seems not advisable;
+no known use-case, and collaboration with default algorithm is unpredictable.
+If custom compairing/operation is needed, just use a collect function of
+your own */
+void
+gst_collect_pads2_set_compare_function (GstCollectPads2 * pads,
+ GstCollectPads2CompareFunction func, gpointer user_data)
+{
+ g_return_if_fail (pads != NULL);
+ g_return_if_fail (GST_IS_COLLECT_PADS2 (pads));
+
+ GST_OBJECT_LOCK (pads);
+ pads->compare_func = func;
+ pads->compare_user_data = user_data;
+ GST_OBJECT_UNLOCK (pads);
+}
+
+/**
+ * gst_collect_pads2_set_function:
+ * @pads: the collectspads to use
+ * @func: the function to set
+ * @user_data: user data passed to the function
+ *
+ * CollectPads provides a default collection algorithm that will determine
+ * the oldest buffer available on all of its pads, and then delegate
+ * to a configured callback.
+ * However, if circumstances are more complicated and/or more control
+ * is desired, this sets a callback that will be invoked instead when
+ * all the pads added to the collection have buffers queued.
+ * Evidently, this callback is not compatible with
+ * gst_collect_pads2_set_buffer_function() callback.
+ * If this callback is set, the former will be unset.
+ *
+ * MT safe.
+ *
+ * Since: 0.10.36
+ */
+void
+gst_collect_pads2_set_function (GstCollectPads2 * pads,
+ GstCollectPads2Function func, gpointer user_data)
+{
+ g_return_if_fail (pads != NULL);
+ g_return_if_fail (GST_IS_COLLECT_PADS2 (pads));
+
+ GST_OBJECT_LOCK (pads);
+ pads->func = func;
+ pads->user_data = user_data;
+ gst_collect_pads2_set_buffer_function_locked (pads, NULL, NULL);
+ GST_OBJECT_UNLOCK (pads);
+}
+
+static void
+ref_data (GstCollectData2 * data)
+{
+ g_assert (data != NULL);
+
+ g_atomic_int_inc (&(data->refcount));
+}
+
+static void
+unref_data (GstCollectData2 * data)
+{
+ g_assert (data != NULL);
+ g_assert (data->refcount > 0);
+
+ if (!g_atomic_int_dec_and_test (&(data->refcount)))
+ return;
+
+ if (data->destroy_notify)
+ data->destroy_notify (data);
+
+ g_object_unref (data->pad);
+ if (data->buffer) {
+ gst_buffer_unref (data->buffer);
+ }
+ g_free (data);
+}
+
+/**
+ * gst_collect_pads2_set_event_function:
+ * @pads: the collectspads to use
+ * @func: the function to set
+ * @user_data: user data passed to the function
+ *
+ * Set the event callback function and user data that will be called after
+ * collectpads has processed and event originating from one of the collected
+ * pads. If the event being processed is a serialized one, this callback is
+ * called with @pads STREAM_LOCK held, otherwise not. As this lock should be
+ * held when calling a number of CollectPads functions, it should be acquired
+ * if so (unusually) needed.
+ *
+ * MT safe.
+ *
+ * Since: 0.10.36
+ */
+void
+gst_collect_pads2_set_event_function (GstCollectPads2 * pads,
+ GstCollectPads2EventFunction func, gpointer user_data)
+{
+ g_return_if_fail (pads != NULL);
+ g_return_if_fail (GST_IS_COLLECT_PADS2 (pads));
+
+ GST_OBJECT_LOCK (pads);
+ pads->event_func = func;
+ pads->event_user_data = user_data;
+ GST_OBJECT_UNLOCK (pads);
+}
+
+/**
+ * gst_collect_pads2_add_pad:
+ * @pads: the collectspads to use
+ * @pad: the pad to add
+ * @size: the size of the returned #GstCollectData2 structure
+ *
+ * Add a pad to the collection of collect pads. The pad has to be
+ * a sinkpad. The refcount of the pad is incremented. Use
+ * gst_collect_pads2_remove_pad() to remove the pad from the collection
+ * again.
+ *
+ * You specify a size for the returned #GstCollectData2 structure
+ * so that you can use it to store additional information.
+ *
+ * The pad will be automatically activated in push mode when @pads is
+ * started.
+ *
+ * This function calls gst_collect_pads2_add_pad() passing a value of NULL
+ * for destroy_notify and TRUE for locked.
+ *
+ * Returns: a new #GstCollectData2 to identify the new pad. Or NULL
+ * if wrong parameters are supplied.
+ *
+ * MT safe.
+ *
+ * Since: 0.10.36
+ */
+GstCollectData2 *
+gst_collect_pads2_add_pad (GstCollectPads2 * pads, GstPad * pad, guint size)
+{
+ return gst_collect_pads2_add_pad_full (pads, pad, size, NULL, TRUE);
+}
+
+/**
+ * gst_collect_pads2_add_pad_full:
+ * @pads: the collectspads to use
+ * @pad: the pad to add
+ * @size: the size of the returned #GstCollectData2 structure
+ * @destroy_notify: function to be called before the returned #GstCollectData2
+ * structure is freed
+ * @lock: whether to lock this pad in usual waiting state
+ *
+ * Add a pad to the collection of collect pads. The pad has to be
+ * a sinkpad. The refcount of the pad is incremented. Use
+ * gst_collect_pads2_remove_pad() to remove the pad from the collection
+ * again.
+ *
+ * You specify a size for the returned #GstCollectData2 structure
+ * so that you can use it to store additional information.
+ *
+ * You can also specify a #GstCollectData2DestroyNotify that will be called
+ * just before the #GstCollectData2 structure is freed. It is passed the
+ * pointer to the structure and should free any custom memory and resources
+ * allocated for it.
+ *
+ * Keeping a pad locked in waiting state is only relevant when using
+ * the default collection algorithm (providing the oldest buffer).
+ * It ensures a buffer must be available on this pad for a collection
+ * to take place. This is of typical use to a muxer element where
+ * non-subtitle streams should always be in waiting state,
+ * e.g. to assure that caps information is available on all these streams
+ * when initial headers have to be written.
+ *
+ * The pad will be automatically activated in push mode when @pads is
+ * started.
+ *
+ * Since: 0.10.36
+ *
+ * Returns: a new #GstCollectData2 to identify the new pad. Or NULL
+ * if wrong parameters are supplied.
+ *
+ * MT safe.
+ */
+GstCollectData2 *
+gst_collect_pads2_add_pad_full (GstCollectPads2 * pads, GstPad * pad,
+ guint size, GstCollectData2DestroyNotify destroy_notify, gboolean lock)
+{
+ GstCollectData2 *data;
+
+ g_return_val_if_fail (pads != NULL, NULL);
+ g_return_val_if_fail (GST_IS_COLLECT_PADS2 (pads), NULL);
+ g_return_val_if_fail (pad != NULL, NULL);
+ g_return_val_if_fail (GST_PAD_IS_SINK (pad), NULL);
+ g_return_val_if_fail (size >= sizeof (GstCollectData2), NULL);
+
+ GST_DEBUG_OBJECT (pads, "adding pad %s:%s", GST_DEBUG_PAD_NAME (pad));
+
+ data = g_malloc0 (size);
+ data->collect = pads;
+ data->pad = gst_object_ref (pad);
+ data->buffer = NULL;
+ data->pos = 0;
+ gst_segment_init (&data->segment, GST_FORMAT_UNDEFINED);
+ data->state = GST_COLLECT_PADS2_STATE_WAITING;
+ data->state |= lock ? GST_COLLECT_PADS2_STATE_LOCKED : 0;
+ data->refcount = 1;
+ data->destroy_notify = destroy_notify;
+
+ GST_OBJECT_LOCK (pads);
+ GST_OBJECT_LOCK (pad);
+ gst_pad_set_element_private (pad, data);
+ GST_OBJECT_UNLOCK (pad);
+ pads->pad_list = g_slist_append (pads->pad_list, data);
+ gst_pad_set_chain_function (pad, GST_DEBUG_FUNCPTR (gst_collect_pads2_chain));
+ gst_pad_set_event_function (pad, GST_DEBUG_FUNCPTR (gst_collect_pads2_event));
+ /* backward compat, also add to data if stopped, so that the element already
+ * has this in the public data list before going PAUSED (typically)
+ * this can only be done when we are stopped because we don't take the
+ * STREAM_LOCK to protect the pads->data list. */
+ if (!pads->started) {
+ pads->data = g_slist_append (pads->data, data);
+ ref_data (data);
+ }
+ /* activate the pad when needed */
+ if (pads->started)
+ gst_pad_set_active (pad, TRUE);
+ pads->pad_cookie++;
+ GST_OBJECT_UNLOCK (pads);
+
+ return data;
+}
+
+static gint
+find_pad (GstCollectData2 * data, GstPad * pad)
+{
+ if (data->pad == pad)
+ return 0;
+ return 1;
+}
+
+/**
+ * gst_collect_pads2_remove_pad:
+ * @pads: the collectspads to use
+ * @pad: the pad to remove
+ *
+ * Remove a pad from the collection of collect pads. This function will also
+ * free the #GstCollectData2 and all the resources that were allocated with
+ * gst_collect_pads2_add_pad().
+ *
+ * The pad will be deactivated automatically when @pads is stopped.
+ *
+ * Returns: %TRUE if the pad could be removed.
+ *
+ * MT safe.
+ *
+ * Since: 0.10.36
+ */
+gboolean
+gst_collect_pads2_remove_pad (GstCollectPads2 * pads, GstPad * pad)
+{
+ GstCollectData2 *data;
+ GSList *list;
+
+ g_return_val_if_fail (pads != NULL, FALSE);
+ g_return_val_if_fail (GST_IS_COLLECT_PADS2 (pads), FALSE);
+ g_return_val_if_fail (pad != NULL, FALSE);
+ g_return_val_if_fail (GST_IS_PAD (pad), FALSE);
+
+ GST_DEBUG_OBJECT (pads, "removing pad %s:%s", GST_DEBUG_PAD_NAME (pad));
+
+ GST_OBJECT_LOCK (pads);
+ list = g_slist_find_custom (pads->pad_list, pad, (GCompareFunc) find_pad);
+ if (!list)
+ goto unknown_pad;
+
+ data = (GstCollectData2 *) list->data;
+
+ GST_DEBUG_OBJECT (pads, "found pad %s:%s at %p", GST_DEBUG_PAD_NAME (pad),
+ data);
+
+ /* clear the stuff we configured */
+ gst_pad_set_chain_function (pad, NULL);
+ gst_pad_set_event_function (pad, NULL);
+ GST_OBJECT_LOCK (pad);
+ gst_pad_set_element_private (pad, NULL);
+ GST_OBJECT_UNLOCK (pad);
+
+ /* backward compat, also remove from data if stopped, note that this function
+ * can only be called when we are stopped because we don't take the
+ * STREAM_LOCK to protect the pads->data list. */
+ if (!pads->started) {
+ GSList *dlist;
+
+ dlist = g_slist_find_custom (pads->data, pad, (GCompareFunc) find_pad);
+ if (dlist) {
+ GstCollectData2 *pdata = dlist->data;
+
+ pads->data = g_slist_delete_link (pads->data, dlist);
+ unref_data (pdata);
+ }
+ }
+ /* remove from the pad list */
+ pads->pad_list = g_slist_delete_link (pads->pad_list, list);
+ pads->pad_cookie++;
+
+ /* signal waiters because something changed */
+ GST_COLLECT_PADS2_EVT_BROADCAST (pads);
+
+ /* deactivate the pad when needed */
+ if (!pads->started)
+ gst_pad_set_active (pad, FALSE);
+
+ /* clean and free the collect data */
+ unref_data (data);
+
+ GST_OBJECT_UNLOCK (pads);
+
+ return TRUE;
+
+unknown_pad:
+ {
+ GST_WARNING_OBJECT (pads, "cannot remove unknown pad %s:%s",
+ GST_DEBUG_PAD_NAME (pad));
+ GST_OBJECT_UNLOCK (pads);
+ return FALSE;
+ }
+}
+
+/**
+ * gst_collect_pads2_is_active:
+ * @pads: the collectspads to use
+ * @pad: the pad to check
+ *
+ * Check if a pad is active.
+ *
+ * This function is currently not implemented.
+ *
+ * Returns: %TRUE if the pad is active.
+ *
+ * MT safe.
+ *
+ * Since: 0.10.36
+ */
+gboolean
+gst_collect_pads2_is_active (GstCollectPads2 * pads, GstPad * pad)
+{
+ g_return_val_if_fail (pads != NULL, FALSE);
+ g_return_val_if_fail (GST_IS_COLLECT_PADS2 (pads), FALSE);
+ g_return_val_if_fail (pad != NULL, FALSE);
+ g_return_val_if_fail (GST_IS_PAD (pad), FALSE);
+
+ g_warning ("gst_collect_pads2_is_active() is not implemented");
+
+ return FALSE;
+}
+
+/**
+ * gst_collect_pads2_collect:
+ * @pads: the collectspads to use
+ *
+ * Collect data on all pads. This function is usually called
+ * from a #GstTask function in an element.
+ *
+ * This function is currently not implemented.
+ *
+ * Returns: #GstFlowReturn of the operation.
+ *
+ * MT safe.
+ *
+ * Since: 0.10.36
+ */
+GstFlowReturn
+gst_collect_pads2_collect (GstCollectPads2 * pads)
+{
+ g_return_val_if_fail (pads != NULL, GST_FLOW_ERROR);
+ g_return_val_if_fail (GST_IS_COLLECT_PADS2 (pads), GST_FLOW_ERROR);
+
+ g_warning ("gst_collect_pads2_collect() is not implemented");
+
+ return GST_FLOW_NOT_SUPPORTED;
+}
+
+/**
+ * gst_collect_pads2_collect_range:
+ * @pads: the collectspads to use
+ * @offset: the offset to collect
+ * @length: the length to collect
+ *
+ * Collect data with @offset and @length on all pads. This function
+ * is typically called in the getrange function of an element.
+ *
+ * This function is currently not implemented.
+ *
+ * Returns: #GstFlowReturn of the operation.
+ *
+ * MT safe.
+ *
+ * Since: 0.10.36
+ */
+GstFlowReturn
+gst_collect_pads2_collect_range (GstCollectPads2 * pads, guint64 offset,
+ guint length)
+{
+ g_return_val_if_fail (pads != NULL, GST_FLOW_ERROR);
+ g_return_val_if_fail (GST_IS_COLLECT_PADS2 (pads), GST_FLOW_ERROR);
+
+ g_warning ("gst_collect_pads2_collect_range() is not implemented");
+
+ return GST_FLOW_NOT_SUPPORTED;
+}
+
+/*
+ * Must be called with STREAM_LOCK.
+ */
+static void
+gst_collect_pads2_set_flushing_unlocked (GstCollectPads2 * pads,
+ gboolean flushing)
+{
+ GSList *walk = NULL;
+
+ /* Update the pads flushing flag */
+ for (walk = pads->data; walk; walk = g_slist_next (walk)) {
+ GstCollectData2 *cdata = walk->data;
+
+ if (GST_IS_PAD (cdata->pad)) {
+ GST_OBJECT_LOCK (cdata->pad);
+ if (flushing)
+ GST_PAD_SET_FLUSHING (cdata->pad);
+ else
+ GST_PAD_UNSET_FLUSHING (cdata->pad);
+ if (flushing)
+ GST_COLLECT_PADS2_STATE_SET (cdata, GST_COLLECT_PADS2_STATE_FLUSHING);
+ else
+ GST_COLLECT_PADS2_STATE_UNSET (cdata, GST_COLLECT_PADS2_STATE_FLUSHING);
+ gst_collect_pads2_clear (pads, cdata);
+ GST_OBJECT_UNLOCK (cdata->pad);
+ }
+ }
+
+ /* inform _chain of changes */
+ GST_COLLECT_PADS2_EVT_BROADCAST (pads);
+}
+
+/**
+ * gst_collect_pads2_set_flushing:
+ * @pads: the collectspads to use
+ * @flushing: desired state of the pads
+ *
+ * Change the flushing state of all the pads in the collection. No pad
+ * is able to accept anymore data when @flushing is %TRUE. Calling this
+ * function with @flushing %FALSE makes @pads accept data again.
+ * Caller must ensure that downstream streaming (thread) is not blocked,
+ * e.g. by sending a FLUSH_START downstream.
+ *
+ * MT safe.
+ *
+ *
+ * Since: 0.10.36
+ */
+void
+gst_collect_pads2_set_flushing (GstCollectPads2 * pads, gboolean flushing)
+{
+ g_return_if_fail (pads != NULL);
+ g_return_if_fail (GST_IS_COLLECT_PADS2 (pads));
+
+ /* NOTE since this eventually calls _pop, some (STREAM_)LOCK is needed here */
+ GST_COLLECT_PADS2_STREAM_LOCK (pads);
+ gst_collect_pads2_set_flushing_unlocked (pads, flushing);
+ GST_COLLECT_PADS2_STREAM_UNLOCK (pads);
+}
+
+/**
+ * gst_collect_pads2_start:
+ * @pads: the collectspads to use
+ *
+ * Starts the processing of data in the collect_pads2.
+ *
+ * MT safe.
+ *
+ * Since: 0.10.36
+ */
+void
+gst_collect_pads2_start (GstCollectPads2 * pads)
+{
+ GSList *collected;
+
+ g_return_if_fail (pads != NULL);
+ g_return_if_fail (GST_IS_COLLECT_PADS2 (pads));
+
+ GST_DEBUG_OBJECT (pads, "starting collect pads");
+
+ /* make sure stop and collect cannot be called anymore */
+ GST_COLLECT_PADS2_STREAM_LOCK (pads);
+
+ /* make pads streamable */
+ GST_OBJECT_LOCK (pads);
+
+ /* loop over the master pad list and reset the segment */
+ collected = pads->pad_list;
+ for (; collected; collected = g_slist_next (collected)) {
+ GstCollectData2 *data;
+
+ data = collected->data;
+ gst_segment_init (&data->segment, GST_FORMAT_UNDEFINED);
+ }
+
+ gst_collect_pads2_set_flushing_unlocked (pads, FALSE);
+
+ /* Start collect pads */
+ pads->started = TRUE;
+ GST_OBJECT_UNLOCK (pads);
+ GST_COLLECT_PADS2_STREAM_UNLOCK (pads);
+}
+
+/**
+ * gst_collect_pads2_stop:
+ * @pads: the collectspads to use
+ *
+ * Stops the processing of data in the collect_pads2. this function
+ * will also unblock any blocking operations.
+ *
+ * MT safe.
+ *
+ * Since: 0.10.36
+ */
+void
+gst_collect_pads2_stop (GstCollectPads2 * pads)
+{
+ GSList *collected;
+
+ g_return_if_fail (pads != NULL);
+ g_return_if_fail (GST_IS_COLLECT_PADS2 (pads));
+
+ GST_DEBUG_OBJECT (pads, "stopping collect pads");
+
+ /* make sure collect and start cannot be called anymore */
+ GST_COLLECT_PADS2_STREAM_LOCK (pads);
+
+ /* make pads not accept data anymore */
+ GST_OBJECT_LOCK (pads);
+ gst_collect_pads2_set_flushing_unlocked (pads, TRUE);
+
+ /* Stop collect pads */
+ pads->started = FALSE;
+ pads->eospads = 0;
+ pads->queuedpads = 0;
+
+ /* loop over the master pad list and flush buffers */
+ collected = pads->pad_list;
+ for (; collected; collected = g_slist_next (collected)) {
+ GstCollectData2 *data;
+ GstBuffer **buffer_p;
+
+ data = collected->data;
+ if (data->buffer) {
+ buffer_p = &data->buffer;
+ gst_buffer_replace (buffer_p, NULL);
+ data->pos = 0;
+ }
+ GST_COLLECT_PADS2_STATE_UNSET (data, GST_COLLECT_PADS2_STATE_EOS);
+ }
+
+ if (pads->earliest_data)
+ unref_data (pads->earliest_data);
+ pads->earliest_data = NULL;
+ pads->earliest_time = GST_CLOCK_TIME_NONE;
+
+ GST_OBJECT_UNLOCK (pads);
+ /* Wake them up so they can end the chain functions. */
+ GST_COLLECT_PADS2_EVT_BROADCAST (pads);
+
+ GST_COLLECT_PADS2_STREAM_UNLOCK (pads);
+}
+
+/**
+ * gst_collect_pads2_peek:
+ * @pads: the collectspads to peek
+ * @data: the data to use
+ *
+ * Peek at the buffer currently queued in @data. This function
+ * should be called with the @pads STREAM_LOCK held, such as in the callback
+ * handler.
+ *
+ * Returns: The buffer in @data or NULL if no buffer is queued.
+ * should unref the buffer after usage.
+ *
+ * MT safe.
+ *
+ * Since: 0.10.36
+ */
+GstBuffer *
+gst_collect_pads2_peek (GstCollectPads2 * pads, GstCollectData2 * data)
+{
+ GstBuffer *result;
+
+ g_return_val_if_fail (pads != NULL, NULL);
+ g_return_val_if_fail (GST_IS_COLLECT_PADS2 (pads), NULL);
+ g_return_val_if_fail (data != NULL, NULL);
+
+ if ((result = data->buffer))
+ gst_buffer_ref (result);
+
+ GST_DEBUG_OBJECT (pads, "Peeking at pad %s:%s: buffer=%p",
+ GST_DEBUG_PAD_NAME (data->pad), result);
+
+ return result;
+}
+
+/**
+ * gst_collect_pads2_pop:
+ * @pads: the collectspads to pop
+ * @data: the data to use
+ *
+ * Pop the buffer currently queued in @data. This function
+ * should be called with the @pads STREAM_LOCK held, such as in the callback
+ * handler.
+ *
+ * Returns: The buffer in @data or NULL if no buffer was queued.
+ * You should unref the buffer after usage.
+ *
+ * MT safe.
+ *
+ * Since: 0.10.36
+ */
+GstBuffer *
+gst_collect_pads2_pop (GstCollectPads2 * pads, GstCollectData2 * data)
+{
+ GstBuffer *result;
+
+ g_return_val_if_fail (pads != NULL, NULL);
+ g_return_val_if_fail (GST_IS_COLLECT_PADS2 (pads), NULL);
+ g_return_val_if_fail (data != NULL, NULL);
+
+ if ((result = data->buffer)) {
+ data->buffer = NULL;
+ data->pos = 0;
+ /* one less pad with queued data now */
+ if (GST_COLLECT_PADS2_STATE_IS_SET (data, GST_COLLECT_PADS2_STATE_WAITING))
+ pads->queuedpads--;
+ }
+
+ GST_COLLECT_PADS2_EVT_BROADCAST (pads);
+
+ GST_DEBUG_OBJECT (pads, "Pop buffer on pad %s:%s: buffer=%p",
+ GST_DEBUG_PAD_NAME (data->pad), result);
+
+ return result;
+}
+
+/* pop and unref the currently queued buffer, should be called with STREAM_LOCK
+ * held */
+static void
+gst_collect_pads2_clear (GstCollectPads2 * pads, GstCollectData2 * data)
+{
+ GstBuffer *buf;
+
+ if ((buf = gst_collect_pads2_pop (pads, data)))
+ gst_buffer_unref (buf);
+}
+
+/**
+ * gst_collect_pads2_available:
+ * @pads: the collectspads to query
+ *
+ * Query how much bytes can be read from each queued buffer. This means
+ * that the result of this call is the maximum number of bytes that can
+ * be read from each of the pads.
+ *
+ * This function should be called with @pads STREAM_LOCK held, such as
+ * in the callback.
+ *
+ * Returns: The maximum number of bytes queued on all pads. This function
+ * returns 0 if a pad has no queued buffer.
+ *
+ * MT safe.
+ *
+ * Since: 0.10.36
+ */
+/* we might pre-calculate this in some struct field,
+ * but would then have to maintain this in _chain and particularly _pop, etc,
+ * even if element is never interested in this information */
+guint
+gst_collect_pads2_available (GstCollectPads2 * pads)
+{
+ GSList *collected;
+ guint result = G_MAXUINT;
+
+ g_return_val_if_fail (pads != NULL, 0);
+ g_return_val_if_fail (GST_IS_COLLECT_PADS2 (pads), 0);
+
+ collected = pads->data;
+ for (; collected; collected = g_slist_next (collected)) {
+ GstCollectData2 *pdata;
+ GstBuffer *buffer;
+ gint size;
+
+ pdata = (GstCollectData2 *) collected->data;
+
+ /* ignore pad with EOS */
+ if (G_UNLIKELY (GST_COLLECT_PADS2_STATE_IS_SET (pdata,
+ GST_COLLECT_PADS2_STATE_EOS))) {
+ GST_DEBUG_OBJECT (pads, "pad %p is EOS", pdata);
+ continue;
+ }
+
+ /* an empty buffer without EOS is weird when we get here.. */
+ if (G_UNLIKELY ((buffer = pdata->buffer) == NULL)) {
+ GST_WARNING_OBJECT (pads, "pad %p has no buffer", pdata);
+ goto not_filled;
+ }
+
+ /* this is the size left of the buffer */
+ size = GST_BUFFER_SIZE (buffer) - pdata->pos;
+ GST_DEBUG_OBJECT (pads, "pad %p has %d bytes left", pdata, size);
+
+ /* need to return the min of all available data */
+ if (size < result)
+ result = size;
+ }
+ /* nothing changed, all must be EOS then, return 0 */
+ if (G_UNLIKELY (result == G_MAXUINT))
+ result = 0;
+
+ return result;
+
+not_filled:
+ {
+ return 0;
+ }
+}
+
+/**
+ * gst_collect_pads2_read:
+ * @pads: the collectspads to query
+ * @data: the data to use
+ * @bytes: a pointer to a byte array
+ * @size: the number of bytes to read
+ *
+ * Get a pointer in @bytes where @size bytes can be read from the
+ * given pad data.
+ *
+ * This function should be called with @pads STREAM_LOCK held, such as
+ * in the callback.
+ *
+ * Returns: The number of bytes available for consumption in the
+ * memory pointed to by @bytes. This can be less than @size and
+ * is 0 if the pad is end-of-stream.
+ *
+ * MT safe.
+ *
+ * Since: 0.10.36
+ */
+guint
+gst_collect_pads2_read (GstCollectPads2 * pads, GstCollectData2 * data,
+ guint8 ** bytes, guint size)
+{
+ guint readsize;
+ GstBuffer *buffer;
+
+ g_return_val_if_fail (pads != NULL, 0);
+ g_return_val_if_fail (GST_IS_COLLECT_PADS2 (pads), 0);
+ g_return_val_if_fail (data != NULL, 0);
+ g_return_val_if_fail (bytes != NULL, 0);
+
+ /* no buffer, must be EOS */
+ if ((buffer = data->buffer) == NULL)
+ return 0;
+
+ readsize = MIN (size, GST_BUFFER_SIZE (buffer) - data->pos);
+
+ *bytes = GST_BUFFER_DATA (buffer) + data->pos;
+
+ return readsize;
+}
+
+/**
+ * gst_collect_pads2_flush:
+ * @pads: the collectspads to query
+ * @data: the data to use
+ * @size: the number of bytes to flush
+ *
+ * Flush @size bytes from the pad @data.
+ *
+ * This function should be called with @pads STREAM_LOCK held, such as
+ * in the callback.
+ *
+ * Returns: The number of bytes flushed This can be less than @size and
+ * is 0 if the pad was end-of-stream.
+ *
+ * MT safe.
+ *
+ * Since: 0.10.36
+ */
+guint
+gst_collect_pads2_flush (GstCollectPads2 * pads, GstCollectData2 * data,
+ guint size)
+{
+ guint flushsize;
+ GstBuffer *buffer;
+
+ g_return_val_if_fail (pads != NULL, 0);
+ g_return_val_if_fail (GST_IS_COLLECT_PADS2 (pads), 0);
+ g_return_val_if_fail (data != NULL, 0);
+
+ /* no buffer, must be EOS */
+ if ((buffer = data->buffer) == NULL)
+ return 0;
+
+ /* this is what we can flush at max */
+ flushsize = MIN (size, GST_BUFFER_SIZE (buffer) - data->pos);
+
+ data->pos += size;
+
+ if (data->pos >= GST_BUFFER_SIZE (buffer))
+ /* _clear will also reset data->pos to 0 */
+ gst_collect_pads2_clear (pads, data);
+
+ return flushsize;
+}
+
+/**
+ * gst_collect_pads2_read_buffer:
+ * @pads: the collectspads to query
+ * @data: the data to use
+ * @size: the number of bytes to read
+ *
+ * Get a subbuffer of @size bytes from the given pad @data.
+ *
+ * This function should be called with @pads STREAM_LOCK held, such as in the
+ * callback.
+ *
+ * Since: 0.10.36
+ *
+ * Returns: A sub buffer. The size of the buffer can be less that requested.
+ * A return of NULL signals that the pad is end-of-stream.
+ * Unref the buffer after use.
+ *
+ * MT safe.
+ */
+GstBuffer *
+gst_collect_pads2_read_buffer (GstCollectPads2 * pads, GstCollectData2 * data,
+ guint size)
+{
+ guint readsize;
+ GstBuffer *buffer;
+
+ g_return_val_if_fail (pads != NULL, NULL);
+ g_return_val_if_fail (GST_IS_COLLECT_PADS2 (pads), NULL);
+ g_return_val_if_fail (data != NULL, NULL);
+
+ /* no buffer, must be EOS */
+ if ((buffer = data->buffer) == NULL)
+ return NULL;
+
+ readsize = MIN (size, GST_BUFFER_SIZE (buffer) - data->pos);
+
+ return gst_buffer_create_sub (buffer, data->pos, readsize);
+}
+
+/**
+ * gst_collect_pads2_take_buffer:
+ * @pads: the collectspads to query
+ * @data: the data to use
+ * @size: the number of bytes to read
+ *
+ * Get a subbuffer of @size bytes from the given pad @data. Flushes the amount
+ * of read bytes.
+ *
+ * This function should be called with @pads STREAM_LOCK held, such as in the
+ * callback.
+ *
+ * Since: 0.10.36
+ *
+ * Returns: A sub buffer. The size of the buffer can be less that requested.
+ * A return of NULL signals that the pad is end-of-stream.
+ * Unref the buffer after use.
+ *
+ * MT safe.
+ */
+GstBuffer *
+gst_collect_pads2_take_buffer (GstCollectPads2 * pads, GstCollectData2 * data,
+ guint size)
+{
+ GstBuffer *buffer = gst_collect_pads2_read_buffer (pads, data, size);
+
+ if (buffer) {
+ gst_collect_pads2_flush (pads, data, GST_BUFFER_SIZE (buffer));
+ }
+ return buffer;
+}
+
+/**
+ * gst_collect_pads2_set_waiting:
+ * @pads: the collectspads
+ * @data: the data to use
+ * @waiting: boolean indicating whether this pad should operate
+ * in waiting or non-waiting mode
+ *
+ * Sets a pad to waiting or non-waiting mode, if at least this pad
+ * has not been created with locked waiting state,
+ * in which case nothing happens.
+ *
+ * This function should be called with @pads STREAM_LOCK held, such as
+ * in the callback.
+ *
+ * MT safe.
+ *
+ * Since: 0.10.36
+ */
+void
+gst_collect_pads2_set_waiting (GstCollectPads2 * pads, GstCollectData2 * data,
+ gboolean waiting)
+{
+ g_return_if_fail (pads != NULL);
+ g_return_if_fail (GST_IS_COLLECT_PADS2 (pads));
+ g_return_if_fail (data != NULL);
+
+ GST_DEBUG_OBJECT (pads, "Setting pad %s to waiting %d, locked %d",
+ GST_PAD_NAME (data->pad), waiting,
+ GST_COLLECT_PADS2_STATE_IS_SET (data, GST_COLLECT_PADS2_STATE_LOCKED));
+
+ /* Do something only on a change and if not locked */
+ if (!GST_COLLECT_PADS2_STATE_IS_SET (data, GST_COLLECT_PADS2_STATE_LOCKED) &&
+ (GST_COLLECT_PADS2_STATE_IS_SET (data, GST_COLLECT_PADS2_STATE_WAITING) !=
+ ! !waiting)) {
+ /* Set waiting state for this pad */
+ if (waiting)
+ GST_COLLECT_PADS2_STATE_SET (data, GST_COLLECT_PADS2_STATE_WAITING);
+ else
+ GST_COLLECT_PADS2_STATE_UNSET (data, GST_COLLECT_PADS2_STATE_WAITING);
+ /* Update number of queued pads if needed */
+ if (!data->buffer &&
+ !GST_COLLECT_PADS2_STATE_IS_SET (data, GST_COLLECT_PADS2_STATE_EOS)) {
+ if (waiting)
+ pads->queuedpads--;
+ else
+ pads->queuedpads++;
+ }
+
+ /* signal waiters because something changed */
+ GST_COLLECT_PADS2_EVT_BROADCAST (pads);
+ }
+}
+
+/* see if pads were added or removed and update our stats. Any pad
+ * added after releasing the LOCK will get collected in the next
+ * round.
+ *
+ * We can do a quick check by checking the cookies, that get changed
+ * whenever the pad list is updated.
+ *
+ * Must be called with STREAM_LOCK.
+ */
+static void
+gst_collect_pads2_check_pads (GstCollectPads2 * pads)
+{
+ /* the master list and cookie are protected with LOCK */
+ GST_OBJECT_LOCK (pads);
+ if (G_UNLIKELY (pads->pad_cookie != pads->cookie)) {
+ GSList *collected;
+
+ /* clear list and stats */
+ g_slist_foreach (pads->data, (GFunc) unref_data, NULL);
+ g_slist_free (pads->data);
+ pads->data = NULL;
+ pads->numpads = 0;
+ pads->queuedpads = 0;
+ pads->eospads = 0;
+ if (pads->earliest_data)
+ unref_data (pads->earliest_data);
+ pads->earliest_data = NULL;
+ pads->earliest_time = GST_CLOCK_TIME_NONE;
+
+ /* loop over the master pad list */
+ collected = pads->pad_list;
+ for (; collected; collected = g_slist_next (collected)) {
+ GstCollectData2 *data;
+
+ /* update the stats */
+ pads->numpads++;
+ data = collected->data;
+ if (GST_COLLECT_PADS2_STATE_IS_SET (data, GST_COLLECT_PADS2_STATE_EOS))
+ pads->eospads++;
+ else if (data->buffer || !GST_COLLECT_PADS2_STATE_IS_SET (data,
+ GST_COLLECT_PADS2_STATE_WAITING))
+ pads->queuedpads++;
+
+ /* add to the list of pads to collect */
+ ref_data (data);
+ /* preserve order of adding/requesting pads */
+ pads->data = g_slist_append (pads->data, data);
+ }
+ /* and update the cookie */
+ pads->cookie = pads->pad_cookie;
+ }
+ GST_OBJECT_UNLOCK (pads);
+}
+
+/* checks if all the pads are collected and call the collectfunction
+ *
+ * Should be called with STREAM_LOCK.
+ *
+ * Returns: The #GstFlowReturn of collection.
+ */
+static GstFlowReturn
+gst_collect_pads2_check_collected (GstCollectPads2 * pads)
+{
+ GstFlowReturn flow_ret = GST_FLOW_OK;
+ GstCollectPads2Function func;
+ gpointer user_data;
+
+ g_return_val_if_fail (GST_IS_COLLECT_PADS2 (pads), GST_FLOW_ERROR);
+
+ GST_OBJECT_LOCK (pads);
+ func = pads->func;
+ user_data = pads->user_data;
+ GST_OBJECT_UNLOCK (pads);
+
+ g_return_val_if_fail (pads->func != NULL, GST_FLOW_NOT_SUPPORTED);
+
+ /* check for new pads, update stats etc.. */
+ gst_collect_pads2_check_pads (pads);
+
+ if (G_UNLIKELY (pads->eospads == pads->numpads)) {
+ /* If all our pads are EOS just collect once to let the element
+ * do its final EOS handling. */
+ GST_DEBUG_OBJECT (pads, "All active pads (%d) are EOS, calling %s",
+ pads->numpads, GST_DEBUG_FUNCPTR_NAME (func));
+
+ flow_ret = func (pads, user_data);
+ } else {
+ gboolean collected = FALSE;
+
+ /* We call the collected function as long as our condition matches. */
+ while (((pads->queuedpads + pads->eospads) >= pads->numpads)) {
+ GST_DEBUG_OBJECT (pads, "All active pads (%d + %d >= %d) have data, "
+ "calling %s", pads->queuedpads, pads->eospads, pads->numpads,
+ GST_DEBUG_FUNCPTR_NAME (func));
+
+ flow_ret = func (pads, user_data);
+ collected = TRUE;
+
+ /* break on error */
+ if (flow_ret != GST_FLOW_OK)
+ break;
+ /* Don't keep looping after telling the element EOS or flushing */
+ if (pads->queuedpads == 0)
+ break;
+ }
+ if (!collected)
+ GST_DEBUG_OBJECT (pads, "Not all active pads (%d) have data, continuing",
+ pads->numpads);
+ }
+ return flow_ret;
+}
+
+
+/* General overview:
+ * - only pad with a buffer can determine earliest_data (and earliest_time)
+ * - only segment info determines (non-)waiting state
+ * - ? perhaps use _stream_time for comparison
+ * (which muxers might have use as well ?)
+ */
+
+/*
+ * Function to recalculate the waiting state of all pads.
+ *
+ * Must be called with STREAM_LOCK.
+ *
+ * Returns TRUE if a pad was set to waiting
+ * (from non-waiting state).
+ */
+static gboolean
+gst_collect_pads2_recalculate_waiting (GstCollectPads2 * pads)
+{
+ GSList *collected;
+ gboolean result = FALSE;
+
+ /* If earliest time is not known, there is nothing to do. */
+ if (pads->earliest_data == NULL)
+ return FALSE;
+
+ for (collected = pads->data; collected; collected = g_slist_next (collected)) {
+ GstCollectData2 *data = (GstCollectData2 *) collected->data;
+ int cmp_res;
+
+ /* check if pad has a segment */
+ if (data->segment.format == GST_FORMAT_UNDEFINED)
+ continue;
+
+ /* check segment format */
+ if (data->segment.format != GST_FORMAT_TIME) {
+ GST_ERROR_OBJECT (pads, "GstCollectPads2 can handle only time segments.");
+ continue;
+ }
+
+ /* check if the waiting state should be changed */
+ cmp_res = pads->compare_func (pads, data, data->segment.start,
+ pads->earliest_data, pads->earliest_time, pads->compare_user_data);
+ if (cmp_res > 0)
+ /* stop waiting */
+ gst_collect_pads2_set_waiting (pads, data, FALSE);
+ else {
+ if (!GST_COLLECT_PADS2_STATE_IS_SET (data,
+ GST_COLLECT_PADS2_STATE_WAITING)) {
+ /* start waiting */
+ gst_collect_pads2_set_waiting (pads, data, TRUE);
+ result = TRUE;
+ }
+ }
+ }
+
+ return result;
+}
+
+/**
+ * gst_collect_pads2_find_best_pad:
+ * @pads: the collectpads to use
+ * @data: returns the collectdata for earliest data
+ * @time: returns the earliest available buffertime
+ *
+ * Find the oldest/best pad, i.e. pad holding the oldest buffer and
+ * and return the corresponding #GstCollectData2 and buffertime.
+ *
+ * This function should be called with STREAM_LOCK held,
+ * such as in the callback.
+ *
+ * Since: 0.10.36
+ */
+static void
+gst_collect_pads2_find_best_pad (GstCollectPads2 * pads,
+ GstCollectData2 ** data, GstClockTime * time)
+{
+ GSList *collected;
+ GstCollectData2 *best = NULL;
+ GstClockTime best_time = GST_CLOCK_TIME_NONE;
+
+ g_return_if_fail (data != NULL);
+ g_return_if_fail (time != NULL);
+
+ for (collected = pads->data; collected; collected = g_slist_next (collected)) {
+ GstBuffer *buffer;
+ GstCollectData2 *data = (GstCollectData2 *) collected->data;
+ GstClockTime timestamp;
+
+ buffer = gst_collect_pads2_peek (pads, data);
+ /* if we have a buffer check if it is better then the current best one */
+ if (buffer != NULL) {
+ timestamp = GST_BUFFER_TIMESTAMP (buffer);
+ gst_buffer_unref (buffer);
+ if (best == NULL || pads->compare_func (pads, data, timestamp,
+ best, best_time, pads->compare_user_data) < 0) {
+ best = data;
+ best_time = timestamp;
+ }
+ }
+ }
+
+ /* set earliest time */
+ *data = best;
+ *time = best_time;
+
+ GST_DEBUG_OBJECT (pads, "best pad %s, best time %" GST_TIME_FORMAT,
+ best ? GST_PAD_NAME (((GstCollectData2 *) best)->pad) : "(nil)",
+ GST_TIME_ARGS (best_time));
+}
+
+/*
+ * Function to recalculate earliest_data and earliest_timestamp. This also calls
+ * gst_collect_pads2_recalculate_waiting
+ *
+ * Must be called with STREAM_LOCK.
+ */
+static gboolean
+gst_collect_pads2_recalculate_full (GstCollectPads2 * pads)
+{
+ if (pads->earliest_data)
+ unref_data (pads->earliest_data);
+ gst_collect_pads2_find_best_pad (pads, &pads->earliest_data,
+ &pads->earliest_time);
+ if (pads->earliest_data)
+ ref_data (pads->earliest_data);
+ return gst_collect_pads2_recalculate_waiting (pads);
+}
+
+/*
+ * Default collect callback triggered when #GstCollectPads2 gathered all data.
+ *
+ * Called with STREAM_LOCK.
+ */
+static GstFlowReturn
+gst_collect_pads2_default_collected (GstCollectPads2 * pads, gpointer user_data)
+{
+ GstCollectData2 *best = NULL;
+ GstBuffer *buffer;
+ GstFlowReturn ret = GST_FLOW_OK;
+ GstCollectPads2BufferFunction func;
+ gpointer buffer_user_data;
+
+ g_return_val_if_fail (GST_IS_COLLECT_PADS2 (pads), GST_FLOW_ERROR);
+
+ GST_OBJECT_LOCK (pads);
+ func = pads->buffer_func;
+ buffer_user_data = pads->buffer_user_data;
+ GST_OBJECT_UNLOCK (pads);
+
+ g_return_val_if_fail (func != NULL, GST_FLOW_NOT_SUPPORTED);
+
+ /* Find the oldest pad at all cost */
+ if (gst_collect_pads2_recalculate_full (pads)) {
+ /* waiting was switched on,
+ * so give another thread a chance to deliver a possibly
+ * older buffer; don't charge on yet with the current oldest */
+ ret = GST_FLOW_OK;
+ }
+
+ best = pads->earliest_data;
+
+ /* No data collected means EOS. */
+ if (G_UNLIKELY (best == NULL)) {
+ ret = func (pads, best, NULL, buffer_user_data);
+ if (ret == GST_FLOW_OK)
+ ret = GST_FLOW_UNEXPECTED;
+ goto done;
+ }
+
+ /* make sure that the pad we take a buffer from is waiting;
+ * otherwise popping a buffer will seem not to have happened
+ * and collectpads can get into a busy loop */
+ gst_collect_pads2_set_waiting (pads, best, TRUE);
+
+ /* Send buffer */
+ buffer = gst_collect_pads2_pop (pads, best);
+ ret = func (pads, best, buffer, buffer_user_data);
+
+done:
+ return ret;
+}
+
+/*
+ * Default timestamp compare function.
+ */
+static gint
+gst_collect_pads2_default_compare_func (GstCollectPads2 * pads,
+ GstCollectData2 * data1, GstClockTime timestamp1,
+ GstCollectData2 * data2, GstClockTime timestamp2, gpointer user_data)
+{
+
+ GST_LOG_OBJECT (pads, "comparing %" GST_TIME_FORMAT
+ " and %" GST_TIME_FORMAT, GST_TIME_ARGS (timestamp1),
+ GST_TIME_ARGS (timestamp2));
+ /* non-valid timestamps go first as they are probably headers or so */
+ if (G_UNLIKELY (!GST_CLOCK_TIME_IS_VALID (timestamp1)))
+ return GST_CLOCK_TIME_IS_VALID (timestamp2) ? -1 : 0;
+
+ if (G_UNLIKELY (!GST_CLOCK_TIME_IS_VALID (timestamp2)))
+ return 1;
+
+ /* compare timestamp */
+ if (timestamp1 < timestamp2)
+ return -1;
+
+ if (timestamp1 > timestamp2)
+ return 1;
+
+ return 0;
+}
+
+static gboolean
+gst_collect_pads2_event (GstPad * pad, GstEvent * event)
+{
+ gboolean res = FALSE, need_unlock = FALSE;
+ GstCollectData2 *data;
+ GstCollectPads2 *pads;
+ GstCollectPads2EventFunction event_func;
+ GstCollectPads2BufferFunction buffer_func;
+ gpointer event_user_data;
+
+ /* some magic to get the managing collect_pads2 */
+ GST_OBJECT_LOCK (pad);
+ data = (GstCollectData2 *) gst_pad_get_element_private (pad);
+ if (G_UNLIKELY (data == NULL))
+ goto pad_removed;
+ ref_data (data);
+ GST_OBJECT_UNLOCK (pad);
+
+ res = FALSE;
+
+ pads = data->collect;
+
+ GST_DEBUG ("Got %s event on pad %s:%s", GST_EVENT_TYPE_NAME (event),
+ GST_DEBUG_PAD_NAME (data->pad));
+
+ GST_OBJECT_LOCK (pads);
+ event_func = pads->event_func;
+ event_user_data = pads->event_user_data;
+ buffer_func = pads->buffer_func;
+ GST_OBJECT_UNLOCK (pads);
+
+ switch (GST_EVENT_TYPE (event)) {
+ case GST_EVENT_FLUSH_START:
+ {
+ /* forward event to unblock check_collected */
+ if (event_func)
+ res = event_func (pads, data, event, event_user_data);
+ if (!res)
+ res = gst_pad_event_default (pad, event);
+
+ /* now unblock the chain function.
+ * no cond per pad, so they all unblock,
+ * non-flushing block again */
+ GST_COLLECT_PADS2_STREAM_LOCK (pads);
+ GST_COLLECT_PADS2_STATE_SET (data, GST_COLLECT_PADS2_STATE_FLUSHING);
+ gst_collect_pads2_clear (pads, data);
+
+ /* cater for possible default muxing functionality */
+ if (buffer_func) {
+ /* restore to initial state */
+ gst_collect_pads2_set_waiting (pads, data, TRUE);
+ /* if the current pad is affected, reset state, recalculate later */
+ if (pads->earliest_data == data) {
+ unref_data (data);
+ pads->earliest_data = NULL;
+ pads->earliest_time = GST_CLOCK_TIME_NONE;
+ }
+ }
+
+ GST_COLLECT_PADS2_STREAM_UNLOCK (pads);
+
+ /* event already cleaned up by forwarding */
+ res = TRUE;
+ goto done;
+ }
+ case GST_EVENT_FLUSH_STOP:
+ {
+ /* flush the 1 buffer queue */
+ GST_COLLECT_PADS2_STREAM_LOCK (pads);
+ GST_COLLECT_PADS2_STATE_UNSET (data, GST_COLLECT_PADS2_STATE_FLUSHING);
+ gst_collect_pads2_clear (pads, data);
+ /* we need new segment info after the flush */
+ gst_segment_init (&data->segment, GST_FORMAT_UNDEFINED);
+ GST_COLLECT_PADS2_STATE_UNSET (data, GST_COLLECT_PADS2_STATE_NEW_SEGMENT);
+ /* if the pad was EOS, remove the EOS flag and
+ * decrement the number of eospads */
+ if (G_UNLIKELY (GST_COLLECT_PADS2_STATE_IS_SET (data,
+ GST_COLLECT_PADS2_STATE_EOS))) {
+ if (!GST_COLLECT_PADS2_STATE_IS_SET (data,
+ GST_COLLECT_PADS2_STATE_WAITING))
+ pads->queuedpads++;
+ pads->eospads--;
+ GST_COLLECT_PADS2_STATE_UNSET (data, GST_COLLECT_PADS2_STATE_EOS);
+ }
+ GST_COLLECT_PADS2_STREAM_UNLOCK (pads);
+
+ /* forward event */
+ goto forward_or_default;
+ }
+ case GST_EVENT_EOS:
+ {
+ GST_COLLECT_PADS2_STREAM_LOCK (pads);
+ /* if the pad was not EOS, make it EOS and so we
+ * have one more eospad */
+ if (G_LIKELY (!GST_COLLECT_PADS2_STATE_IS_SET (data,
+ GST_COLLECT_PADS2_STATE_EOS))) {
+ GST_COLLECT_PADS2_STATE_SET (data, GST_COLLECT_PADS2_STATE_EOS);
+ if (!GST_COLLECT_PADS2_STATE_IS_SET (data,
+ GST_COLLECT_PADS2_STATE_WAITING))
+ pads->queuedpads--;
+ pads->eospads++;
+ }
+ /* check if we need collecting anything, we ignore the result. */
+ gst_collect_pads2_check_collected (pads);
+ GST_COLLECT_PADS2_STREAM_UNLOCK (pads);
+
+ goto forward_or_eat;
+ }
+ case GST_EVENT_NEWSEGMENT:
+ {
+ gint64 start, stop, time;
+ gdouble rate, arate;
+ GstFormat format;
+ gboolean update;
+ gint cmp_res;
+
+ GST_COLLECT_PADS2_STREAM_LOCK (pads);
+
+ gst_event_parse_new_segment_full (event, &update, &rate, &arate, &format,
+ &start, &stop, &time);
+
+ GST_DEBUG_OBJECT (data->pad, "got newsegment, start %" GST_TIME_FORMAT
+ ", stop %" GST_TIME_FORMAT, GST_TIME_ARGS (start),
+ GST_TIME_ARGS (stop));
+
+ gst_segment_set_newsegment_full (&data->segment, update, rate, arate,
+ format, start, stop, time);
+
+ GST_COLLECT_PADS2_STATE_SET (data, GST_COLLECT_PADS2_STATE_NEW_SEGMENT);
+
+ /* default muxing functionality */
+ if (!buffer_func)
+ goto newsegment_done;
+
+ /* default collection can not handle other segment formats than time */
+ if (format != GST_FORMAT_TIME) {
+ GST_ERROR_OBJECT (pads, "GstCollectPads2 default collecting "
+ "can only handle time segments.");
+ goto newsegment_done;
+ }
+
+ /* If oldest time is not known, or current pad got newsegment;
+ * recalculate the state */
+ if (!pads->earliest_data || pads->earliest_data == data) {
+ gst_collect_pads2_recalculate_full (pads);
+ goto newsegment_done;
+ }
+
+ /* Check if the waiting state of the pad should change. */
+ cmp_res = pads->compare_func (pads, data, start, pads->earliest_data,
+ pads->earliest_time, pads->compare_user_data);
+
+ if (cmp_res > 0)
+ /* Stop waiting */
+ gst_collect_pads2_set_waiting (pads, data, FALSE);
+
+ newsegment_done:
+ GST_COLLECT_PADS2_STREAM_UNLOCK (pads);
+ /* we must not forward this event since multiple segments will be
+ * accumulated and this is certainly not what we want. */
+ goto forward_or_eat;
+ }
+ default:
+ /* forward other events */
+ goto forward_or_default;
+ }
+
+forward_or_default:
+ if (GST_EVENT_IS_SERIALIZED (event)) {
+ GST_COLLECT_PADS2_STREAM_LOCK (pads);
+ need_unlock = TRUE;
+ }
+ if (event_func)
+ res = event_func (pads, data, event, event_user_data);
+ if (!res)
+ res = gst_pad_event_default (pad, event);
+ if (need_unlock)
+ GST_COLLECT_PADS2_STREAM_UNLOCK (pads);
+ goto done;
+
+forward_or_eat:
+ if (GST_EVENT_IS_SERIALIZED (event)) {
+ GST_COLLECT_PADS2_STREAM_LOCK (pads);
+ need_unlock = TRUE;
+ }
+ if (event_func)
+ res = event_func (pads, data, event, event_user_data);
+ if (!res) {
+ gst_event_unref (event);
+ res = TRUE;
+ }
+ if (need_unlock)
+ GST_COLLECT_PADS2_STREAM_UNLOCK (pads);
+ goto done;
+
+done:
+ unref_data (data);
+ return res;
+
+ /* ERRORS */
+pad_removed:
+ {
+ GST_DEBUG ("%s got removed from collectpads", GST_OBJECT_NAME (pad));
+ GST_OBJECT_UNLOCK (pad);
+ return FALSE;
+ }
+}
+
+/* For each buffer we receive we check if our collected condition is reached
+ * and if so we call the collected function. When this is done we check if
+ * data has been unqueued. If data is still queued we wait holding the stream
+ * lock to make sure no EOS event can happen while we are ready to be
+ * collected
+ */
+static GstFlowReturn
+gst_collect_pads2_chain (GstPad * pad, GstBuffer * buffer)
+{
+ GstCollectData2 *data;
+ GstCollectPads2 *pads;
+ GstFlowReturn ret;
+ GstBuffer **buffer_p;
+ guint32 cookie;
+ GstCollectPads2BufferFunction prepare_buffer_func;
+ gpointer prepare_buffer_user_data;
+
+ GST_DEBUG ("Got buffer for pad %s:%s", GST_DEBUG_PAD_NAME (pad));
+
+ /* some magic to get the managing collect_pads2 */
+ GST_OBJECT_LOCK (pad);
+ data = (GstCollectData2 *) gst_pad_get_element_private (pad);
+ if (G_UNLIKELY (data == NULL))
+ goto no_data;
+ ref_data (data);
+ GST_OBJECT_UNLOCK (pad);
+
+ pads = data->collect;
+ GST_OBJECT_LOCK (pads);
+ prepare_buffer_func = pads->prepare_buffer_func;
+ prepare_buffer_user_data = pads->prepare_buffer_user_data;
+ GST_OBJECT_UNLOCK (pads);
+
+ GST_COLLECT_PADS2_STREAM_LOCK (pads);
+ /* if not started, bail out */
+ if (G_UNLIKELY (!pads->started))
+ goto not_started;
+ /* check if this pad is flushing */
+ if (G_UNLIKELY (GST_COLLECT_PADS2_STATE_IS_SET (data,
+ GST_COLLECT_PADS2_STATE_FLUSHING)))
+ goto flushing;
+ /* pad was EOS, we can refuse this data */
+ if (G_UNLIKELY (GST_COLLECT_PADS2_STATE_IS_SET (data,
+ GST_COLLECT_PADS2_STATE_EOS)))
+ goto unexpected;
+
+ GST_DEBUG_OBJECT (pads, "Queuing buffer %p for pad %s:%s", buffer,
+ GST_DEBUG_PAD_NAME (pad));
+
+ if (prepare_buffer_func) {
+ ret = prepare_buffer_func (pads, data, buffer, prepare_buffer_user_data);
+ if (ret == GST_COLLECT_PADS2_FLOW_DROP) {
+ GST_DEBUG_OBJECT (pads, "Dropping buffer as requested");
+ ret = GST_FLOW_OK;
+ goto unlock_done;
+ } else if (ret == GST_FLOW_UNEXPECTED) {
+ goto unexpected;
+ } else if (ret != GST_FLOW_OK) {
+ goto error;
+ }
+ }
+
+ /* One more pad has data queued */
+ if (GST_COLLECT_PADS2_STATE_IS_SET (data, GST_COLLECT_PADS2_STATE_WAITING))
+ pads->queuedpads++;
+ buffer_p = &data->buffer;
+ gst_buffer_replace (buffer_p, buffer);
+
+ /* update segment last position if in TIME */
+ if (G_LIKELY (data->segment.format == GST_FORMAT_TIME)) {
+ GstClockTime timestamp = GST_BUFFER_TIMESTAMP (buffer);
+
+ if (GST_CLOCK_TIME_IS_VALID (timestamp))
+ gst_segment_set_last_stop (&data->segment, GST_FORMAT_TIME, timestamp);
+ }
+
+ /* While we have data queued on this pad try to collect stuff */
+ do {
+ /* Check if our collected condition is matched and call the collected
+ * function if it is */
+ ret = gst_collect_pads2_check_collected (pads);
+ /* when an error occurs, we want to report this back to the caller ASAP
+ * without having to block if the buffer was not popped */
+ if (G_UNLIKELY (ret != GST_FLOW_OK))
+ goto error;
+
+ /* data was consumed, we can exit and accept new data */
+ if (data->buffer == NULL)
+ break;
+
+ /* Having the _INIT here means we don't care about any broadcast up to here
+ * (most of which occur with STREAM_LOCK held, so could not have happened
+ * anyway). We do care about e.g. a remove initiated broadcast as of this
+ * point. Putting it here also makes this thread ignores any evt it raised
+ * itself (as is a usual WAIT semantic).
+ */
+ GST_COLLECT_PADS2_EVT_INIT (cookie);
+
+ /* pad could be removed and re-added */
+ unref_data (data);
+ GST_OBJECT_LOCK (pad);
+ if (G_UNLIKELY ((data = gst_pad_get_element_private (pad)) == NULL))
+ goto pad_removed;
+ ref_data (data);
+ GST_OBJECT_UNLOCK (pad);
+
+ GST_DEBUG_OBJECT (pads, "Pad %s:%s has a buffer queued, waiting",
+ GST_DEBUG_PAD_NAME (pad));
+
+ /* wait to be collected, this must happen from another thread triggered
+ * by the _chain function of another pad. We release the lock so we
+ * can get stopped or flushed as well. We can however not get EOS
+ * because we still hold the STREAM_LOCK.
+ */
+ GST_COLLECT_PADS2_STREAM_UNLOCK (pads);
+ GST_COLLECT_PADS2_EVT_WAIT (pads, cookie);
+ GST_COLLECT_PADS2_STREAM_LOCK (pads);
+
+ GST_DEBUG_OBJECT (pads, "Pad %s:%s resuming", GST_DEBUG_PAD_NAME (pad));
+
+ /* after a signal, we could be stopped */
+ if (G_UNLIKELY (!pads->started))
+ goto not_started;
+ /* check if this pad is flushing */
+ if (G_UNLIKELY (GST_COLLECT_PADS2_STATE_IS_SET (data,
+ GST_COLLECT_PADS2_STATE_FLUSHING)))
+ goto flushing;
+ }
+ while (data->buffer != NULL);
+
+unlock_done:
+ GST_COLLECT_PADS2_STREAM_UNLOCK (pads);
+ unref_data (data);
+ gst_buffer_unref (buffer);
+ return ret;
+
+pad_removed:
+ {
+ GST_WARNING ("%s got removed from collectpads", GST_OBJECT_NAME (pad));
+ GST_OBJECT_UNLOCK (pad);
+ ret = GST_FLOW_NOT_LINKED;
+ goto unlock_done;
+ }
+ /* ERRORS */
+no_data:
+ {
+ GST_DEBUG ("%s got removed from collectpads", GST_OBJECT_NAME (pad));
+ GST_OBJECT_UNLOCK (pad);
+ gst_buffer_unref (buffer);
+ return GST_FLOW_NOT_LINKED;
+ }
+not_started:
+ {
+ GST_DEBUG ("not started");
+ gst_collect_pads2_clear (pads, data);
+ ret = GST_FLOW_WRONG_STATE;
+ goto unlock_done;
+ }
+flushing:
+ {
+ GST_DEBUG ("pad %s:%s is flushing", GST_DEBUG_PAD_NAME (pad));
+ gst_collect_pads2_clear (pads, data);
+ ret = GST_FLOW_WRONG_STATE;
+ goto unlock_done;
+ }
+unexpected:
+ {
+ /* we should not post an error for this, just inform upstream that
+ * we don't expect anything anymore */
+ GST_DEBUG ("pad %s:%s is eos", GST_DEBUG_PAD_NAME (pad));
+ ret = GST_FLOW_UNEXPECTED;
+ goto unlock_done;
+ }
+error:
+ {
+ /* we print the error, the element should post a reasonable error
+ * message for fatal errors */
+ GST_DEBUG ("collect failed, reason %d (%s)", ret, gst_flow_get_name (ret));
+ gst_collect_pads2_clear (pads, data);
+ goto unlock_done;
+ }
+}
diff --git a/libs/gst/base/gstcollectpads2.h b/libs/gst/base/gstcollectpads2.h
--- /dev/null
@@ -0,0 +1,362 @@
+/* GStreamer
+ * Copyright (C) 2005 Wim Taymans <wim@fluendo.com>
+ * Copyright (C) 2008 Mark Nauwelaerts <mnauw@users.sourceforge.net>
+ *
+ * gstcollectpads2.h:
+ *
+ * This library is free software; you can redistribute it and/or
+ * modify it under the terms of the GNU Library General Public
+ * License as published by the Free Software Foundation; either
+ * version 2 of the License, or (at your option) any later version.
+ *
+ * This library is distributed in the hope that it will be useful,
+ * but WITHOUT ANY WARRANTY; without even the implied warranty of
+ * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU
+ * Library General Public License for more details.
+ *
+ * You should have received a copy of the GNU Library General Public
+ * License along with this library; if not, write to the
+ * Free Software Foundation, Inc., 59 Temple Place - Suite 330,
+ * Boston, MA 02111-1307, USA.
+ */
+
+#ifndef __GST_COLLECT_PADS2_H__
+#define __GST_COLLECT_PADS2_H__
+
+#include <gst/gst.h>
+
+G_BEGIN_DECLS
+
+#define GST_TYPE_COLLECT_PADS2 (gst_collect_pads2_get_type())
+#define GST_COLLECT_PADS2(obj) (G_TYPE_CHECK_INSTANCE_CAST((obj),GST_TYPE_COLLECT_PADS2,GstCollectPads2))
+#define GST_COLLECT_PADS2_CLASS(klass) (G_TYPE_CHECK_CLASS_CAST((klass),GST_TYPE_COLLECT_PADS2,GstCollectPads2Class))
+#define GST_COLLECT_PADS2_GET_CLASS(obj) (G_TYPE_INSTANCE_GET_CLASS ((obj),GST_TYPE_COLLECT_PADS2,GstCollectPads2Class))
+#define GST_IS_COLLECT_PADS2(obj) (G_TYPE_CHECK_INSTANCE_TYPE((obj),GST_TYPE_COLLECT_PADS2))
+#define GST_IS_COLLECT_PADS2_CLASS(klass) (G_TYPE_CHECK_CLASS_TYPE((klass),GST_TYPE_COLLECT_PADS2))
+
+typedef struct _GstCollectData2 GstCollectData2;
+typedef struct _GstCollectPads2 GstCollectPads2;
+typedef struct _GstCollectPads2Class GstCollectPads2Class;
+
+/**
+ * GstCollectData2DestroyNotify:
+ * @data: the #GstCollectData2 that will be freed
+ *
+ * A function that will be called when the #GstCollectData2 will be freed.
+ * It is passed the pointer to the structure and should free any custom
+ * memory and resources allocated for it.
+ *
+ * Since: 0.10.36
+ */
+typedef void (*GstCollectData2DestroyNotify) (GstCollectData2 *data);
+
+/**
+ * GstCollectPads2StateFlags:
+ * @GST_COLLECT_PADS2_STATE_EOS: Set if collectdata's pad is EOS.
+ * @GST_COLLECT_PADS2_STATE_FLUSHING: Set if collectdata's pad is flushing.
+ * @GST_COLLECT_PADS2_STATE_NEW_SEGMENT: Set if collectdata's pad received a
+ * new_segment event.
+ * @GST_COLLECT_PADS2_STATE_WAITING: Set if collectdata's pad must be waited
+ * for when collecting.
+ * @GST_COLLECT_PADS2_STATE_LOCKED: Set collectdata's pad WAITING state must
+ * not be changed.
+ * #GstCollectPads2StateFlags indicate private state of a collectdata('s pad).
+ *
+ * Since: 0.10.36
+ */
+typedef enum {
+ GST_COLLECT_PADS2_STATE_EOS = 1 << 0,
+ GST_COLLECT_PADS2_STATE_FLUSHING = 1 << 1,
+ GST_COLLECT_PADS2_STATE_NEW_SEGMENT = 1 << 2,
+ GST_COLLECT_PADS2_STATE_WAITING = 1 << 3,
+ GST_COLLECT_PADS2_STATE_LOCKED = 1 << 4
+} GstCollectPads2StateFlags;
+
+/**
+ * GST_COLLECT_PADS2_STATE:
+ * @data: a #GstCollectData2.
+ *
+ * A flags word containing #GstCollectPads2StateFlags flags set
+ * on this collected pad.
+ *
+ * Since: 0.10.36
+ */
+#define GST_COLLECT_PADS2_STATE(data) (((GstCollectData2 *) data)->state)
+/**
+ * GST_COLLECT_PADS2_STATE_IS_SET:
+ * @data: a #GstCollectData2.
+ * @flag: the #GstCollectPads2StateFlags to check.
+ *
+ * Gives the status of a specific flag on a collected pad.
+ *
+ * Since: 0.10.36
+ */
+#define GST_COLLECT_PADS2_STATE_IS_SET(data,flag) !!(GST_COLLECT_PADS2_STATE (data) & flag)
+/**
+ * GST_COLLECT_PADS2_STATE_SET:
+ * @data: a #GstCollectData2.
+ * @flag: the #GstCollectPads2StateFlags to set.
+ *
+ * Sets a state flag on a collected pad.
+ *
+ * Since: 0.10.36
+ */
+#define GST_COLLECT_PADS2_STATE_SET(data,flag) (GST_COLLECT_PADS2_STATE (data) |= flag)
+/**
+ * GST_COLLECT_PADS2_STATE_UNSET:
+ * @data: a #GstCollectData2.
+ * @flag: the #GstCollectPads2StateFlags to clear.
+ *
+ * Clears a state flag on a collected pad.
+ *
+ * Since: 0.10.36
+ */
+#define GST_COLLECT_PADS2_STATE_UNSET(data,flag) (GST_COLLECT_PADS2_STATE (data) &= ~(flag))
+
+#define GST_COLLECT_PADS2_FLOW_DROP GST_FLOW_CUSTOM_SUCCESS
+
+/**
+ * GstCollectData2:
+ * @collect: owner #GstCollectPads2
+ * @pad: #GstPad managed by this data
+ * @buffer: currently queued buffer.
+ * @pos: position in the buffer
+ * @segment: last segment received.
+ *
+ * Structure used by the collect_pads2.
+ *
+ * Since: 0.10.36
+ */
+struct _GstCollectData2
+{
+ /* with STREAM_LOCK of @collect */
+ GstCollectPads2 *collect;
+ GstPad *pad;
+ GstBuffer *buffer;
+ guint pos;
+ GstSegment segment;
+
+ /*< private >*/
+ /* state: bitfield for easier extension;
+ * eos, flushing, new_segment, waiting */
+ guint state;
+
+ /* refcounting for struct, and destroy callback */
+ GstCollectData2DestroyNotify destroy_notify;
+ gint refcount;
+
+ gpointer _gst_reserved[GST_PADDING];
+};
+
+/**
+ * GstCollectPads2Function:
+ * @pads: the #GstCollectPads2 that trigered the callback
+ * @user_data: user data passed to gst_collect_pads2_set_function()
+ *
+ * A function that will be called when all pads have received data.
+ *
+ * Returns: #GST_FLOW_OK for success
+ *
+ * Since: 0.10.36
+ */
+typedef GstFlowReturn (*GstCollectPads2Function) (GstCollectPads2 *pads, gpointer user_data);
+
+/**
+ * GstCollectPads2BufferFunction:
+ * @pads: the #GstCollectPads2 that trigered the callback
+ * @data: the #GstCollectData2 of pad that has received the buffer
+ * @buffer: the #GstBuffer
+ * @user_data: user data passed to gst_collect_pads2_set_buffer_function()
+ *
+ * A function that will be called when a (considered oldest) buffer can be muxed.
+ * If all pads have reached EOS, this function is called with NULL @buffer
+ * and NULL @data.
+ *
+ * Returns: #GST_FLOW_OK for success
+ *
+ * Since: 0.10.36
+ */
+typedef GstFlowReturn (*GstCollectPads2BufferFunction) (GstCollectPads2 *pads, GstCollectData2 *data,
+ GstBuffer *buffer, gpointer user_data);
+
+/**
+ * GstCollectPads2CompareFunction:
+ * @pads: the #GstCollectPads that is comparing the timestamps
+ * @data1: the first #GstCollectData2
+ * @timestamp1: the first timestamp
+ * @data2: the second #GstCollectData2
+ * @timestamp2: the second timestamp
+ * @user_data: user data passed to gst_collect_pads2_set_compare_function()
+ *
+ * A function for comparing two timestamps of buffers or newsegments collected on one pad.
+ *
+ * Returns: Integer less than zero when first timestamp is deemed older than the second one.
+ * Zero if the timestamps are deemed equally old.
+ * Integer greate than zero when second timestamp is deemed older than the first one.
+ *
+ * Since: 0.10.36
+ */
+typedef gint (*GstCollectPads2CompareFunction) (GstCollectPads2 *pads,
+ GstCollectData2 * data1, GstClockTime timestamp1,
+ GstCollectData2 * data2, GstClockTime timestamp2,
+ gpointer user_data);
+
+/**
+ * GstCollectPads2EventFunction:
+ * @pads: the #GstCollectPads2 that trigered the callback
+ * @pad: the #GstPad that received an event
+ * @event: the #GstEvent received
+ * @user_data: user data passed to gst_collect_pads2_set_event_function()
+ *
+ * A function that will be called after collectpads has processed the event.
+ *
+ * Returns: %TRUE if the pad could handle the event
+ *
+ * Since: 0.10.36
+ */
+typedef gboolean (*GstCollectPads2EventFunction) (GstCollectPads2 *pads, GstCollectData2 * pad,
+ GstEvent * event, gpointer user_data);
+
+/**
+ * GST_COLLECT_PADS2_GET_STREAM_LOCK:
+ * @pads: a #GstCollectPads2
+ *
+ * Get the stream lock of @pads. The stream lock is used to coordinate and
+ * serialize execution among the various streams being collected, and in
+ * protecting the resources used to accomplish this.
+ *
+ * Since: 0.10.36
+ */
+#define GST_COLLECT_PADS2_GET_STREAM_LOCK(pads) (&((GstCollectPads2 *)pads)->stream_lock)
+/**
+ * GST_COLLECT_PADS2_STREAM_LOCK:
+ * @pads: a #GstCollectPads2
+ *
+ * Lock the stream lock of @pads.
+ *
+ * Since: 0.10.36
+ */
+#define GST_COLLECT_PADS2_STREAM_LOCK(pads) (g_static_rec_mutex_lock(GST_COLLECT_PADS2_GET_STREAM_LOCK (pads)))
+/**
+ * GST_COLLECT_PADS2_STREAM_UNLOCK:
+ * @pads: a #GstCollectPads2
+ *
+ * Unlock the stream lock of @pads.
+ *
+ * Since: 0.10.36
+ */
+#define GST_COLLECT_PADS2_STREAM_UNLOCK(pads) (g_static_rec_mutex_unlock(GST_COLLECT_PADS2_GET_STREAM_LOCK (pads)))
+
+/**
+ * GstCollectPads2:
+ * @data: #GList of #GstCollectData2 managed by this #GstCollectPads2.
+ *
+ * Collectpads object.
+ *
+ * Since: 0.10.36
+ */
+struct _GstCollectPads2 {
+ GstObject object;
+
+ /*< public >*/ /* with LOCK and/or STREAM_LOCK */
+ GSList *data; /* list of CollectData items */
+
+ /*< private >*/
+ GStaticRecMutex stream_lock; /* used to serialize collection among several streams */
+ /* with LOCK and/or STREAM_LOCK*/
+ gboolean started;
+
+ /* with STREAM_LOCK */
+ guint32 cookie; /* @data list cookie */
+ guint numpads; /* number of pads in @data */
+ guint queuedpads; /* number of pads with a buffer */
+ guint eospads; /* number of pads that are EOS */
+ GstClockTime earliest_time; /* Current earliest time */
+ GstCollectData2 *earliest_data; /* Pad data for current earliest time */
+
+ /* with LOCK */
+ GSList *pad_list; /* updated pad list */
+ guint32 pad_cookie; /* updated cookie */
+
+ GstCollectPads2Function func; /* function and user_data for callback */
+ gpointer user_data;
+ GstCollectPads2BufferFunction prepare_buffer_func; /* function and user_data for prepare buffer callback */
+ gpointer prepare_buffer_user_data;
+ GstCollectPads2BufferFunction buffer_func; /* function and user_data for buffer callback */
+ gpointer buffer_user_data;
+ GstCollectPads2CompareFunction compare_func;
+ gpointer compare_user_data;
+ GstCollectPads2EventFunction event_func; /* function and data for event callback */
+ gpointer event_user_data;
+
+ /* no other lock needed */
+ GMutex *evt_lock; /* these make up sort of poor man's event signaling */
+ GCond *evt_cond;
+ guint32 evt_cookie;
+
+ gpointer _gst_reserved[GST_PADDING + 0];
+
+};
+
+struct _GstCollectPads2Class {
+ GstObjectClass parent_class;
+
+ /*< private >*/
+ gpointer _gst_reserved[GST_PADDING];
+};
+
+GType gst_collect_pads2_get_type(void);
+
+/* creating the object */
+GstCollectPads2* gst_collect_pads2_new (void);
+
+/* set the callbacks */
+void gst_collect_pads2_set_function (GstCollectPads2 *pads, GstCollectPads2Function func,
+ gpointer user_data);
+void gst_collect_pads2_set_prepare_buffer_function (GstCollectPads2 *pads,
+ GstCollectPads2BufferFunction func, gpointer user_data);
+void gst_collect_pads2_set_buffer_function (GstCollectPads2 *pads,
+ GstCollectPads2BufferFunction func, gpointer user_data);
+void gst_collect_pads2_set_event_function (GstCollectPads2 *pads,
+ GstCollectPads2EventFunction func, gpointer user_data);
+void gst_collect_pads2_set_compare_function (GstCollectPads2 *pads,
+ GstCollectPads2CompareFunction func, gpointer user_data);
+
+/* pad management */
+GstCollectData2* gst_collect_pads2_add_pad (GstCollectPads2 *pads, GstPad *pad, guint size);
+GstCollectData2* gst_collect_pads2_add_pad_full (GstCollectPads2 *pads, GstPad *pad, guint size, GstCollectData2DestroyNotify destroy_notify,
+ gboolean lock);
+gboolean gst_collect_pads2_remove_pad (GstCollectPads2 *pads, GstPad *pad);
+gboolean gst_collect_pads2_is_active (GstCollectPads2 *pads, GstPad *pad);
+
+/* start/stop collection */
+GstFlowReturn gst_collect_pads2_collect (GstCollectPads2 *pads);
+GstFlowReturn gst_collect_pads2_collect_range (GstCollectPads2 *pads, guint64 offset, guint length);
+
+void gst_collect_pads2_start (GstCollectPads2 *pads);
+void gst_collect_pads2_stop (GstCollectPads2 *pads);
+void gst_collect_pads2_set_flushing (GstCollectPads2 *pads, gboolean flushing);
+
+/* get collected buffers */
+GstBuffer* gst_collect_pads2_peek (GstCollectPads2 *pads, GstCollectData2 *data);
+GstBuffer* gst_collect_pads2_pop (GstCollectPads2 *pads, GstCollectData2 *data);
+
+/* get collected bytes */
+guint gst_collect_pads2_available (GstCollectPads2 *pads);
+guint gst_collect_pads2_read (GstCollectPads2 *pads, GstCollectData2 *data,
+ guint8 **bytes, guint size);
+guint gst_collect_pads2_flush (GstCollectPads2 *pads, GstCollectData2 *data,
+ guint size);
+GstBuffer* gst_collect_pads2_read_buffer (GstCollectPads2 * pads, GstCollectData2 * data,
+ guint size);
+GstBuffer* gst_collect_pads2_take_buffer (GstCollectPads2 * pads, GstCollectData2 * data,
+ guint size);
+
+/* setting and unsetting waiting mode */
+void gst_collect_pads2_set_waiting (GstCollectPads2 *pads, GstCollectData2 *data,
+ gboolean waiting);
+
+
+G_END_DECLS
+
+#endif /* __GST_COLLECT_PADS22_H__ */