summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 8108494)
raw | patch | inline | side by side (parent: 8108494)
author | Jan Schmidt <thaytan@noraisin.net> | |
Mon, 5 Oct 2009 15:41:50 +0000 (16:41 +0100) | ||
committer | Jan Schmidt <thaytan@noraisin.net> | |
Tue, 6 Oct 2009 18:51:45 +0000 (19:51 +0100) |
Remove old cruft from the release script, and change some CVS
references to equivalent git commands
references to equivalent git commands
docs/random/release | patch | blob | history |
diff --git a/docs/random/release b/docs/random/release
index 473bbcf4948ae1b257b3160e50e71ea94adcf3fd..773cb7a2d16dc70a71f1c1bb81f98fd04b9411d8 100644 (file)
--- a/docs/random/release
+++ b/docs/random/release
- build packages to test
- release:
- - cvs commit in the tree
+ - 'git commit -a' in the tree
- tag tree
for example for 0.6.3 :
- cvs tag RELEASE-0_6_3
+ git tag -a RELEASE-0.6.3
- bump nano number in configure.ac, commit
- - if working in the "stable" release branch, update to this tag to freeze it:
- cvs up -r RELEASE-0_6_3
- sync source and packages to website
+ run /bin/data-put in www
- change versions in www/src/htdocs/entities.gst
gstreamer-devel@lists.sourceforge.net gstreamer-announce@lists.sourceforge.net kde-multimedia@kde.org gnome-multimedia@gnome.org
- Update freshmeat with new releases (get Uraeus to do it)
-Old release notes - superseded by the www/bin/new-release script.
-----------------------------------------------------------------
-
-TODO :
- - Decide on the next version number (major, minor or micro upgrade ?)
- - Get a fresh copy to do the necessary tests on
- - If this isn't on the stable branch (like for 0.6), then create a new branch;
- - with 0.3.3 as an example, tag is BRANCH-RELEASE-0_3_3
- cvs tag BRANCH-RELEASE-0_3_3-ROOT
- cvs tag -b BRANCH-RELEASE-0_3_3
- - update your local copy to the branch:
- cvs update -r BRANCH-RELEASE-0_3_3
- - Set the nano to 2 (in configure.ac, AS_VERSION)
- - If this is a release candidate for a new major version, override
- MAJOR/MINOR in configure.ac
- - Do all updates/patches/changes for the release tarball in this branch
- - Think of a good codename for the release
- - Check the bug lists:
- - The idea is to have all bugs for this milestone listed as fixed
- - Check all of the bug reports with this version as a milestone, and verify
- that these bugs are fixed, or reassign to a later milestone if not
- - Check later milestone bugs, and if any of them are fixed, reassign to
- this milestone
- - Check the list of bugs resolved with milestone HEAD, which should be
- assigned to an actual milestone
- - create a new $(version).xml file in www/src/htdocs/releases/$(module)
- and add that to cvs
- - Start updating the release notes on the www cvs tree
- - create the base xml file in www/htdocs/releases/$/module)/$(version).xml
- - grepping ChangeLog for contributors:
- grep "<.*>" ChangeLog | perl -i -p -e 's@\d*-\d*-\d*\s*(.*)\s*<.*$@$1@' | sort | uniq
- - use www/bin/bugzilla (module) (version) to get an xml list of the
- bugs fixed in this version, and add it to the release .xml
- - depending on how the API has changed update the libtool versioning
- in configure.ac, AS_LIBTOOL
- (Look at the libtool info page about versioning for guidelines)
- (if MAJOR/MINOR version has changed, however, you can reset all to 0)
- - FIXME: autotools have latest config.{guess,sub}
- This is needed in order to support newer platforms.
- On Debian install the autotools-dev package to get these.
- Someone please add some more useful info here on how to do this
- - while (IS_PRERELEASE)
- {
- - increase the nano number (starting with 2)
- - check out a fresh anonymous copy
- cvs -d:pserver:anonymous@cvs.gstreamer.sf.net:/cvsroot/gstreamer \
- co -rBRANCH-RELEASE-0_3_3 gstreamer
- - make distcheck, rpm build should pass, from a FRESH cvs tree
- - media tests should be done
- - source tarball should be installed and tested
- - rpms should be installed and tested
- - .2 tarball should be submitted to translation project
- - put up tarball for a day
- }
-
-
-Release Period
---------------
-When we're satisfied with the prereleases, it's time to make the final tarball.
-It's very important that the tarball we put out is fully checked, works as
-planned, and generally is generated only ONCE by someone with a relatively
-clean (and reference) system. We don't want to put out more than one tarball
-with the same name.
-
-TODO :
- - give the latest prerelease another good testing
- - proofread the release notes
- - run bugzilla with the correct module and milestone and include
- the output in the release notes
- bin/bugzilla gstreamer 0.7.5 >> src/htdocs/releases/gstreamer/0.7.5.xml
- then edit it
- - verify all new translations are in and po files are updated:
- run 'make download-po' to make sure translations in CVS are up-to-date,
- and then 'make update' in po/ (which will update the .pot template too and
- merge the changes into the .po files)
- - run win32-update from toplevel to copy new versions and enum files
- - copy www/htdocs/releases/$(module)/$(version) to RELEASE
- - copy the list of changes, bugs fixed, and API changes and add them to NEWS
- - update the ChangeLog to account for NEWS, RELEASE, and configure.ac,
- mentioning the release name
- - add === release (version) === to ChangeLog
- - update web site docs
- - release-specific docs should go in CVS
- - change docs/current symlink
- - remove the nano version number in configure.ac, AS_VERSION
- - cvs commit
- - tag tree
- for example for 0.6.3 :
- cvs tag RELEASE-0_6_3
- - run "make release", build rpms
- - install on gnome's ftp
- - for plugins docs: run "make update" in docs/plugins to update version info
- - for docs: run "make upload" from gstreamer/docs to get the new docs online
- - change www/src/htdocs/entities.gst with the new version numbers
- - change www/src/htdocs/bugs/bugs.xml and add a new milestone
- - possibly add new version and milestone to bugzilla
- - add a news item to the news.xml
-
-Post-Release Period
--------------------
-Time to bring the new version under the eyes of the public.
-
-TODO :
- - FIXME: should we md5 the tarballs?
- - upload to sourceforge
- upload.sourceforge.net/incoming
- administer the release
-
- - FIXME: announcements
- - gstreamer-{devel, announce} : a simple mail with RELEASE
- - freshmeat
- - linux-audio-dev (if it's a big release) : a simple mail with RELEASE
- - gnome lists (?)
- - lwn (if it's a big release)
- - send mail for translators with URL to .tar.bz2:
- translation@iro.umontreal.ca
- - Kick back, have a party, enjoy people coming in on IRC telling us how
- GStreamer rocks.
- - Later on, if necessary, merge back latest release branch to current dev
- branch (if patches to source were made)
-
- TWO WAYS:
- A)
- * get a diff between the branch root and the final release:
- cvs diff -r BRANCH-RELEASE-0_7_5-ROOT -r RELEASE-0_7_5 > patch
- * fix up this patch (remove RELEASE)
- * and apply it to the HEAD branch
- * update nano version to 1 in configure.ac
-
- B)
- * change to a HEAD branch, make sure it's updated
- * cvs diff -R -r RELEASE-0_3_4-30SECONDFRENCHMAN
- gives a list of differences between head and release tag,
- stuff with > is how it's in HEAD, < is in the rel branch
-
- * cvs update -j BRANCH-RELEASE-0_3_4
- merges the difference made in that branch to the current source
- this is what you want to use when merging back the branch
- resolve conflicts and commit
-
-Some various random comments that might or might not make sense :
-
-- Should work:
- * autoconf feature to allow building outside source dir
-
-- Package version policy
- - Use major.minor.micro versioning
- - Before 1.0.0, Update micro until code and API are fairly stable,
- then update minor.
- - After 1.0.0,
- Update major when code and api hit new level of stability or major features.
- Update minor on API changes.
- Update micro on API-compatible changes.
-
-NOTES ON STARTING A NEW STABLE SERIES
--------------------------------------
-- Given x.y.z being the last devel release, where y is an odd number
-- all API/ABI/renaming changes should be done
-- for every module:
- - get a completely fresh checkout
- - set GST_MAJORMINOR to x.(y + 1)
- - reset libtool versioning to 0, 0, 0
- - build every piece
- - grep for possible non-updates of MAJORMINOR:
- grep -r "0\.9" * | grep -v "0\.9\.6" | less -R
- change stuff:
- perl -i -p -e 's@0\.9(\.[^0-9])@0.10$1@g' (file) changes 0.9. -> 0.10.
- perl -i -p -e 's@0\.9([^.])@0.10$1@g' (file) changes 0.9 -> 0.10
-
-
-
-
-