summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: c33b50e)
raw | patch | inline | side by side (parent: c33b50e)
author | Sebastian Dröge <sebastian.droege@collabora.co.uk> | |
Wed, 7 Dec 2011 08:50:40 +0000 (09:50 +0100) | ||
committer | Sebastian Dröge <sebastian.droege@collabora.co.uk> | |
Wed, 7 Dec 2011 08:51:42 +0000 (09:51 +0100) |
Fixes bug #662199.
libs/gst/base/gstbasetransform.c | patch | blob | history |
index 5622a9b520d54ca732acf1c0d7a2ceee2414198e..25abdd860e603f495b26be215309fa1f92e5db2c 100644 (file)
/* get the caps that can be handled by @pad. We perform:
*
* - take the caps of peer of otherpad,
- * - filter against the padtemplate of otherpad,
+ * - filter against the padtemplate of otherpad,
* - calculate all transforms of remaining caps
* - filter against template of @pad
*
* This function can do renegotiation on the source pad
*
* The output buffer is always writable. outbuf can be equal to
- * inbuf, the caller should be prepared for this and perform
+ * inbuf, the caller should be prepared for this and perform
* appropriate refcounting.
*/
static GstFlowReturn
*/
peercaps =
gst_pad_peer_get_caps_reffed (GST_BASE_TRANSFORM_SINK_PAD (trans));
+
if (peercaps) {
GstCaps *intersect;
gst_caps_intersect_full (sink_suggest, peercaps,
GST_CAPS_INTERSECT_FIRST);
gst_caps_unref (peercaps);
+
+ /* If intersected caps is empty then just keep them empty. The
+ * code below will try to come up with possible caps if there
+ * are any */
gst_caps_unref (sink_suggest);
sink_suggest = intersect;
}
- if (!gst_caps_is_fixed (sink_suggest) || gst_caps_is_empty (sink_suggest)) {
- GST_DEBUG_OBJECT (trans, "Suggested caps is not fixed: %"
- GST_PTR_FORMAT, sink_suggest);
-
- if (gst_caps_is_empty (sink_suggest))
- goto not_supported;
+ /* If the suggested caps are not empty and not fixed, try to fixate them */
+ if (!gst_caps_is_fixed (sink_suggest)
+ && !gst_caps_is_empty (sink_suggest)) {
+ GST_DEBUG_OBJECT (trans,
+ "Suggested caps is not fixed: %" GST_PTR_FORMAT, sink_suggest);
/* try the alloc caps if it is still not fixed */
if (!gst_caps_is_fixed (sink_suggest)) {
sink_suggest);
}
+ /* Check if the suggested caps are compatible with our
+ * sinkpad template caps and if they're not (or were
+ * empty after intersecting with the peer caps above)
+ * we try to come up with any supported caps
+ */
if (sink_suggest) {
templ = gst_pad_get_pad_template_caps (pad);
/* first try to allocate an output buffer based on the currently negotiated
* format. While we call pad-alloc we could renegotiate the srcpad format or
- * have a new suggestion for upstream buffer-alloc.
+ * have a new suggestion for upstream buffer-alloc.
* In any case, outbuf will contain a buffer suitable for doing the configured
* transform after this function. */
ret = gst_base_transform_prepare_output_buffer (trans, inbuf, outbuf);
gst_base_transform_drop_delayed_events (trans);
trans->have_same_caps = FALSE;
- /* We can only reset the passthrough mode if the instance told us to
+ /* We can only reset the passthrough mode if the instance told us to
handle it in configure_caps */
if (bclass->passthrough_on_same_caps) {
gst_base_transform_set_passthrough (trans, FALSE);