registry: Support installed/uninstalled plugin-scanner helper
authorJan Schmidt <thaytan@noraisin.net>
Fri, 6 Feb 2009 09:49:34 +0000 (09:49 +0000)
committerJan Schmidt <thaytan@noraisin.net>
Tue, 6 Oct 2009 18:51:44 +0000 (19:51 +0100)
Add a simple version check when starting the plugin-scanner so we can
verify we're talking to one that talks the same language.
First try a plugin-scanner in the installed path, then try one via the
GST_PLUGIN_SCANNER env var if that doesn't work.
Update the uninstalled script.
Install the plugin-scanner to the libexec dir

configure.ac
docs/faq/gst-uninstalled
gst/gstpluginloader.c
libs/gst/helpers/Makefile.am

index 072b332b3c57c6f51e706ef5b5a522e842cec883..6f30757747d390829e4767100d15ed421c86eb50 100644 (file)
@@ -654,6 +654,11 @@ dnl LDFLAGS for plugins; includes GST_ALL_LDFLAGS
 GST_PLUGIN_LDFLAGS="-module -avoid-version -export-symbols-regex '^[_]*gst_plugin_desc\$\$' $GST_ALL_LDFLAGS"
 AC_SUBST(GST_PLUGIN_LDFLAGS, "$GST_PLUGIN_LDFLAGS")
 
+dnl plugin scanner locations
+AS_AC_EXPAND(GST_PLUGIN_SCANNER_INSTALLED,${libexecdir}/plugin-scanner)
+AC_DEFINE_UNQUOTED(GST_PLUGIN_SCANNER_INSTALLED,
+    "$GST_PLUGIN_SCANNER_INSTALLED", [location of the installed plugin-scanner])
+
 SHAVE_INIT([common],[enable])
 
 dnl things for our internal libcheck
index 8c56286a600378ff13cf95801e1b8d353567eb07..2c28b8cb3150e65b861750fd27e450d4716349fa 100755 (executable)
@@ -123,6 +123,8 @@ export GST_PLUGIN_SYSTEM_PATH=
 # by an installed copy
 rm -f $GST/gstreamer/registry.xml 2>/dev/null
 export GST_REGISTRY=$GST/gstreamer/registry.dat
+# Point at the uninstalled plugin scanner
+export GST_PLUGIN_SCANNER=$GST/gstreamer/libs/gst/helpers/plugin-scanner
 
 # once MANPATH is set, it needs at least an "empty"component to keep pulling
 # in the system-configured man paths from man.config
index 2679a0c6a8dd12a872eb2035bb497db46eac9d8e..8f9bffe04384a25596e30be2511a402498b79da2 100644 (file)
@@ -40,6 +40,9 @@
 #include <gst/gstpluginloader.h>
 #include <gst/gstregistrychunks.h>
 
+/* IMPORTANT: Bump the version number if the plugin loader protocol changes */
+static const guint32 loader_protocol_version = 1;
+
 #define GST_CAT_DEFAULT GST_CAT_PLUGIN_LOADING
 
 static GstPluginLoader *plugin_loader_new (GstRegistry * registry);
@@ -85,6 +88,8 @@ struct _GstPluginLoader
   gboolean rx_done;
   gboolean rx_got_sync;
 
+  guint32 got_version;
+
   /* Head and tail of the pending plugins list. List of
      PendingPluginEntry structs */
   GList *pending_plugins;
@@ -95,13 +100,13 @@ struct _GstPluginLoader
 #define PACKET_LOAD_PLUGIN 2
 #define PACKET_SYNC 3
 #define PACKET_PLUGIN_DETAILS 4
+#define PACKET_VERSION 5
 
 #define BUF_INIT_SIZE 512
 #define BUF_GROW_EXTRA 512
 #define HEADER_SIZE 8
 #define ALIGNMENT   (sizeof (void *))
 
-
 static gboolean gst_plugin_loader_spawn (GstPluginLoader * loader);
 static void put_packet (GstPluginLoader * loader, guint type, guint32 tag,
     const guint8 * payload, guint32 payload_len);
@@ -112,6 +117,7 @@ static gboolean plugin_loader_load_and_sync (GstPluginLoader * l,
 static void plugin_loader_create_blacklist_plugin (GstPluginLoader * l,
     PendingPluginEntry * entry);
 static void plugin_loader_cleanup_child (GstPluginLoader * loader);
+static gboolean plugin_loader_sync_with_child (GstPluginLoader * l);
 
 static GstPluginLoader *
 plugin_loader_new (GstRegistry * registry)
@@ -273,6 +279,19 @@ restart:
   return TRUE;
 }
 
+static gboolean
+plugin_loader_sync_with_child (GstPluginLoader * l)
+{
+  put_packet (l, PACKET_SYNC, 0, NULL, 0);
+
+  l->rx_got_sync = FALSE;
+  while (!l->rx_got_sync) {
+    if (!exchange_packets (l))
+      return FALSE;
+  }
+  return TRUE;
+}
+
 static gboolean
 plugin_loader_load_and_sync (GstPluginLoader * l, PendingPluginEntry * entry)
 {
@@ -284,15 +303,8 @@ plugin_loader_load_and_sync (GstPluginLoader * l, PendingPluginEntry * entry)
   len = strlen (entry->filename);
   put_packet (l, PACKET_LOAD_PLUGIN, entry->tag,
       (guint8 *) entry->filename, len + 1);
-  put_packet (l, PACKET_SYNC, 0, NULL, 0);
 
-  l->rx_got_sync = FALSE;
-  while (!l->rx_got_sync) {
-    if (!exchange_packets (l))
-      return FALSE;
-  }
-
-  return TRUE;
+  return plugin_loader_sync_with_child (l);
 }
 
 static void
@@ -320,23 +332,16 @@ plugin_loader_create_blacklist_plugin (GstPluginLoader * l,
 }
 
 static gboolean
-gst_plugin_loader_spawn (GstPluginLoader * loader)
+gst_plugin_loader_try_helper (GstPluginLoader * loader, gchar * location)
 {
-  if (loader->child_running)
-    return TRUE;
+  char *argv[] = { location, "-l", NULL };
 
-  {
-    /* FIXME: Find the plugin-scanner! */
-    char *helper_bin =
-        "/home/jan/devel/gstreamer/head/gstreamer/libs/gst/helpers/plugin-scanner";
-    char *argv[] = { helper_bin, "-l", NULL };
-
-    if (!g_spawn_async_with_pipes (NULL, argv, NULL,
-            G_SPAWN_DO_NOT_REAP_CHILD /* | G_SPAWN_STDERR_TO_DEV_NULL */ ,
-            NULL, NULL, &loader->child_pid, &loader->fd_w.fd, &loader->fd_r.fd,
-            NULL, NULL))
-      return FALSE;
-  }
+  GST_LOG ("Trying to spawn plugin-scanner helper at %s", location);
+  if (!g_spawn_async_with_pipes (NULL, argv, NULL,
+          G_SPAWN_DO_NOT_REAP_CHILD /* | G_SPAWN_STDERR_TO_DEV_NULL */ ,
+          NULL, NULL, &loader->child_pid, &loader->fd_w.fd, &loader->fd_r.fd,
+          NULL, NULL))
+    return FALSE;
 
   gst_poll_add_fd (loader->fdset, &loader->fd_w);
   gst_poll_add_fd (loader->fdset, &loader->fd_r);
@@ -345,11 +350,53 @@ gst_plugin_loader_spawn (GstPluginLoader * loader)
 
   loader->tx_buf_write = loader->tx_buf_read = 0;
 
+  loader->got_version = (guint32) (-1);
+  put_packet (loader, PACKET_VERSION, 0, NULL, 0);
+  if (!plugin_loader_sync_with_child (loader))
+    return FALSE;
+
+  GST_LOG ("Got VERSION %u from child. Ours is %u", loader->got_version,
+      loader_protocol_version);
+  if (loader->got_version != loader_protocol_version)
+    return FALSE;
+
   loader->child_running = TRUE;
 
   return TRUE;
 }
 
+static gboolean
+gst_plugin_loader_spawn (GstPluginLoader * loader)
+{
+  char *helper_bin;
+  gboolean res;
+
+  if (loader->child_running)
+    return TRUE;
+
+  /* Find the plugin-scanner, first try installed then by env-var */
+  helper_bin = g_strdup (GST_PLUGIN_SCANNER_INSTALLED);
+  res = gst_plugin_loader_try_helper (loader, helper_bin);
+  g_free (helper_bin);
+
+  if (!res) {
+    /* Try the GST_PLUGIN_SCANNER env var */
+    const gchar *env = g_getenv ("GST_PLUGIN_SCANNER");
+    if (env != NULL) {
+      GST_LOG ("Installed plugin scanner failed. "
+          "Trying GST_PLUGIN_SCANNER env var: %s", env);
+      helper_bin = g_strdup (env);
+      res = gst_plugin_loader_try_helper (loader, helper_bin);
+      g_free (helper_bin);
+    } else {
+      GST_LOG ("Installed plugin scanner failed and "
+          "GST_PLUGIN_SCANNER env var not set. No plugin-scanner available");
+    }
+  }
+
+  return loader->child_running;
+}
+
 static void
 plugin_loader_cleanup_child (GstPluginLoader * l)
 {
@@ -645,11 +692,26 @@ handle_rx_packet (GstPluginLoader * l,
     case PACKET_SYNC:
       if (l->is_child) {
         /* Respond with our reply - also a sync */
-        put_packet (l, PACKET_SYNC, 0, NULL, 0);
+        put_packet (l, PACKET_SYNC, tag, NULL, 0);
         GST_LOG ("Got SYNC in child - replying");
       } else
         l->rx_got_sync = TRUE;
       break;
+    case PACKET_VERSION:
+      if (l->is_child) {
+        /* Respond with our reply - a version packet, with the version */
+        guint32 val;
+        GST_WRITE_UINT32_BE (&val, loader_protocol_version);
+        put_packet (l, PACKET_VERSION, tag, (guint8 *) & val, sizeof (guint32));
+        GST_LOG ("Got VERSION in child - replying %u", loader_protocol_version);
+      } else {
+        if (payload_len == sizeof (loader_protocol_version)) {
+          l->got_version = GST_READ_UINT32_BE (payload);
+        } else {
+          res = FALSE;
+        }
+      }
+      break;
     default:
       return FALSE;             /* Invalid packet -> something is wrong */
   }
index 419762b50ad94b0765a518b4b6ca95b5aabfd454..b9ca33c234663ff2b9df3ab9d1a9d359a311622e 100644 (file)
@@ -1,6 +1,5 @@
-# helpers_PROGRAMS = plugin-scanner
-# FIXME: Subst helpersdir in configure.ac
-noinst_PROGRAMS = plugin-scanner
+helpers_PROGRAMS = plugin-scanner
+helpersdir=$(libexecdir)
 
 plugin_scanner_SOURCES = plugin-scanner.c
 plugin_scanner_CFLAGS = $(GST_OBJ_CFLAGS)