docs changes
authorThomas Vander Stichele <thomas@apestaart.org>
Tue, 11 Dec 2001 22:55:55 +0000 (22:55 +0000)
committerThomas Vander Stichele <thomas@apestaart.org>
Tue, 11 Dec 2001 22:55:55 +0000 (22:55 +0000)
Original commit message from CVS:
docs changes

ChangeLog
NEWS
README
TODO
autogen.sh

index ac64cbcfb7f77ad976462c60ed1b56f6d2d1ba8c..ca7a313446c0af547c6dba198b55027113443538 100644 (file)
--- a/ChangeLog
+++ b/ChangeLog
@@ -1,3 +1,7 @@
+2001-12-11 22:10  thomasvs
+
+       * lots of build fixes for 0.3.0 release
+
 2001-08-15 23:43  cael
 
        * gstplay/: ChangeLog, gstmediaplay.c, gstplay.c: Added hacky check
diff --git a/NEWS b/NEWS
index e69de29bb2d1d6434b8b29ae775ad8c2e48c5391..034f4067f2321ca82f5c3b4a47c154d23f99d9ea 100644 (file)
--- a/NEWS
+++ b/NEWS
@@ -0,0 +1,2 @@
+2001-12-12
+       * GStreamer 0.3.0 released, "Most Eventful Ever"
diff --git a/README b/README
index a0c2a20bf7420a07dd35305830be40e17a781d15..28b88f725831cc1590d9d38a9ad806faa8b3703f 100644 (file)
--- a/README
+++ b/README
@@ -10,26 +10,15 @@ release the source.
 Developer note:  When building from CVS sources, you will need to run
 autogen.sh to generate the build system files.
 
-Unfortunately, there is a bug in automake which causes it to use a large
-amount of memory when generating plugins/Makefile.in.  The following patch,
-which you may wish to apply to automake (version 1.4), fixes this problem.
-It is also fixed in versions of automake 1.4f and later.
-Alternatively, ensure that you have at least 512Mb of memory on your system,
-and be prepared to wait a little while when running automake (or autogen.sh).
+GStreamer is cutting-edge stuff.  To be a CVS developer, you need 
+cutting-edge tools.
 
-The autogen.sh script will automatically detect an unpatched automake and give
-a warning.  It will also generate a patched version of automake in the top
-build directory, which you can use by putting it in a directory in your $PATH
-ahead of the unpatched version of automake.
+ATM, most of use have at least these versions :
 
-@@ -2383,8 +2383,8 @@
-       # to all possible directories, and use it.  If DIST_SUBDIRS is
-       # defined, just use it.
-       local ($dist_subdir_name);
--      if (&variable_conditions ('SUBDIRS')
--          || &variable_defined ('DIST_SUBDIRS'))
-+      if (&variable_defined ('DIST_SUBDIRS')
-+          || &variable_conditions ('SUBDIRS'))
-       {
-           $dist_subdir_name = 'DIST_SUBDIRS';
-           if (! &variable_defined ('DIST_SUBDIRS'))
+* autoconf     2.52    (NOT 2.52d)
+* automake     1.5
+* libtool      1.4
+* pkg-config    0.8.0
+
+autogen.sh will check for these versions and complain if you don't have 
+them.  
diff --git a/TODO b/TODO
index 436d370fbd52ad3de98a9821c07f6a9dd85e2feb..e109cf190f8686c579d3855ed3cec12832efbfc5 100644 (file)
--- a/TODO
+++ b/TODO
@@ -8,11 +8,6 @@
 - deal with clocking issues
 - use real chaining where possible
 - factory aliases?
-
-* autoconf testing :
-
-- SDL : seems to be ok now, test
-- rtp : weird problem, can't get it to work with AC_CHECK_HEADER(S)
-- arts : rh72 has artsflowh. in /usr/include/kde/arts
-        there's no arts-config
-        so what do we do to find it ?
+- fix plugins :
+wtay : the proper fix is of course to fix the plugins and 
+implement the cleanup in the state change function..
index dbd780d7c76609df3927bb368ed0586c0d935a66..5db2e98bc3a9e487faa305501aa25cc5f712c421 100755 (executable)
@@ -96,7 +96,7 @@ fi
 version_check "autoconf" "ftp://ftp.gnu.org/pub/gnu/autoconf/" 2 52 || DIE=1
 version_check "automake" "ftp://ftp.gnu.org/pub/gnu/automake/" 1 5 || DIE=1
 version_check "libtool" "ftp://ftp.gnu.org/pub/gnu/libtool/" 1 4 0 || DIE=1
-version_check "pkg-config" "http://www.freedesktop.org/software/pkgconfig" 0 7 0 || DIE=1
+version_check "pkg-config" "http://www.freedesktop.org/software/pkgconfig" 0 8 0 || DIE=1
 
 if test "$DIE" -eq 1; then
        exit 1