]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/gstreamer0-10.git/history - ChangeLog
docs/design/: Many doc updates.
[glsdk/gstreamer0-10.git] / ChangeLog
2005-10-08 Wim Taymansdocs/design/: Many doc updates.
2005-10-08 Wim Taymansgst/gstevent.*: Fix event quark registration.
2005-10-08 Wim Taymansgst/base/gstbasesink.c: Better log message.
2005-10-08 Stefan Kostlots of new docs and doc fixes
2005-10-08 Thomas Vander Stichelegst/: Only ever load one plugin for a given plugin...
2005-10-08 Wim Taymansgst/base/gstbasesink.c: Prepare for doing QOS.
2005-10-08 Wim Taymanscheck/: Allow new clock message too.
2005-10-08 Wim Taymansgst/gstmessage.*: Also carry the clock in question.
2005-10-08 Wim Taymansgst/gstmessage.*: Clean up.
2005-10-08 Tim-Philipp Müllertools/gst-inspect.c: Can't pass NULL strings to g_print...
2005-10-08 Thomas Vander Sticheledocs/: add a chapter on running GStreamer.
2005-10-08 Wim Taymansgst/base/gstbasesink.*: Repost EOS message while going...
2005-10-08 Wim Taymanstools/gst-launch.c: Better message printout.
2005-10-08 Wim Taymansgst/: Make ChildProxy threadsafe and fix mem leaks.
2005-10-08 Thomas Vander Stichelegst/gst.c: debug the GST_PLUGIN_ env vars
2005-10-08 Wim TaymansAdded extra field to STATE_CHANGE message with the...
2005-10-08 Wim Taymansgst/: Small cleanups and doc updates.
2005-10-08 Thomas Vander Stichelegst/: log distributing clocks and base time
2005-10-07 Wim Taymansgst/base/gstbasesrc.*: Make the newsegment event custom...
2005-10-07 Wim Taymansgst/gstevent.*: New event for future idea.
2005-10-07 Andy Wingogst/gstelement.c (gst_element_post_message): Doc update.
2005-10-07 Andy Wingodocs/gst/gstreamer-sections.txt: Update.
2005-10-07 Andy Wingocheck/elements/fakesrc.c (test_no_preroll): New check...
2005-10-07 Wim Taymansgst/gstghostpad.c: Activating a ghostpad with no intern...
2005-10-07 Thomas Vander Stichelegst/gstobject.h: there's no point in wrapping FLAG_SET...
2005-10-07 Michael SmithPrint out feature and plugin count at the end when...
2005-10-07 Johan DahlinAdd a GType to GstIterator, update callsites and tests.
2005-10-06 Thomas Vander Stichelegst/gstpad.c: give events a chance to be handled by...
2005-10-06 Thomas Vander Stichelegst/gstevent.*: add string representations for event...
2005-10-06 Wim Taymansgst/elements/gstfilesink.c: Don't use NULL pointers.
2005-10-06 Thomas Vander Stichelegst/: widen the debug category in output to fit the...
2005-10-06 Thomas Vander Stichelegst/gstghostpad.c: add push activation of sink ghost...
2005-10-05 Thomas Vander Stichelegst/gstutils.c: fix a bug in the case where neither...
2005-10-05 Thomas Vander Stichelegst/gstpad.c: emit have-data before checking for peers...
2005-10-04 Wim Taymansgst/elements/: Protect last_message with lock.
2005-10-04 Edward Herveygst/gstformat.h: Added precision in the comments for...
2005-10-04 Tim-Philipp Müllertools/gst-launch.c: Don't try to run erroneous pipelines.
2005-10-04 Julien Mouttegst/gstbus.c: We don't need this header.
2005-10-03 Thomas Vander Sticheleback to head
2005-10-03 Thomas Vander Stichelerelease time
2005-10-02 Andy Wingogst/gstpad.c (gst_pad_activate_push): There is a race...
2005-10-02 Andy Wingochangelog
2005-10-02 Andy Wingogst/gstobject.h (GST_OBJECT_REFCOUNT_VALUE): Just use...
2005-10-02 Tim-Philipp Müllerconfigure.ac: Fix (unused) AM_CONDITIONAL tests.
2005-10-01 Tim-Philipp Müllergst/gstutils.c: Add assertion that makes sure src_val...
2005-09-30 Edward Herveygst/elements/gsttee.c: Let's not iterate pads we're...
2005-09-30 Wim Taymansgst/gstelement.c: Small tweak, element in ASYNC remains...
2005-09-30 Wim Taymansgst/base/gstbasesink.c: Only error is an error.
2005-09-29 Tim-Philipp Müllergst/base/gstbasesrc.c: Fix documentation typos. Add...
2005-09-29 David Schleefgst/gstplugin.c: Make some error messages more end...
2005-09-29 Thomas Vander Stichelecheck/: fix tests for the new warning
2005-09-29 Thomas Vander Stichelegst/gstobject.c: for 2.6 refcounting, make debug log...
2005-09-29 Andy Wingochangelog
2005-09-29 Edward Herveylibs/gst/controller/gstcontroller.c: Better if we actua...
2005-09-29 Wim Taymanscheck/gst/gstbin.c: Change for new bus API.
2005-09-29 Thomas Vander Stichelerename filter-caps to caps property
2005-09-29 Tim-Philipp Müllergst/gstvalue.c: More robust fraction string parsing.
2005-09-29 Tim-Philipp Müllergst/gstcaps.c: Thou shalt not free a structure and...
2005-09-29 Wim Taymanscheck/gst/gstbin.c: Oops.
2005-09-29 Wim Taymanscheck/gst/gstbin.c: Add bus to bin.
2005-09-29 Johan Dahlingst/gstmessage.c (gst_message_parse_state_changed)...
2005-09-29 Johan Dahlingst/gstmessage.c (gst_message_new_state_changed): Use
2005-09-28 Stefan Kostfixed umlauts in ChangeLog again
2005-09-28 Stefan Kostgst/gstinfo.c: don't do dummy g_strdup()s
2005-09-28 Wim Taymansgst/gstbus.*: Added async-message and sync-message...
2005-09-28 Stefan Kostadded another constructor for language bindings
2005-09-28 Thomas Vander Stichelecheck/gst/gstpipeline.c: add another check
2005-09-28 Wim Taymansgst/gstbin.c: Small doc fixes. get_clock -> provide_clock.
2005-09-28 Andy Wingogst/base/gstbasesrc.c (gst_base_src_unlock): Comment...
2005-09-28 Tim-Philipp Müllergst/elements/: Make element details static.
2005-09-28 Wim Taymansgst/gstbin.c: Some documentation updates.
2005-09-27 Stefan Kostadded two new functions to the docs documents all undoc...
2005-09-27 Thomas Vander Stichelegst/: remove now useless and leaky resurrection code...
2005-09-27 Wim Taymansdocs/design/part-TODO.txt: Update TODO.
2005-09-27 Andy Wingolibs/gst/dataprotocol/dataprotocol.c: Fix error-checkin...
2005-09-27 Wim Taymanscheck/gst/gstbin.c: Enable check that works now.
2005-09-27 Wim Taymansgst/: Leak fixes, the fold functions need to unref...
2005-09-27 Tim-Philipp Müllercheck/gst/gstbuffer.c: Plug leak in test case and fix...
2005-09-27 Tim-Philipp Müllergst/gstbuffer.c: Set READONLY flag on subbuffers, so...
2005-09-27 Wim Taymansgst/gstbin.c: use gst_object_has_ancestor().
2005-09-27 Tim-Philipp Müllergst/gsterror.h: Remove comment. GST_TYPE_G_ERROR is...
2005-09-26 Wim Taymanscheck/gst/gstbin.c: Added check that shows error in...
2005-09-26 Wim Taymansgst/gstbin.c: Make state change function use 3 queues...
2005-09-26 Tim-Philipp Müllerdocs/design/: Replace all _pull_region() with _pull_range()
2005-09-26 Andy Wingogst/gstvalue.c (_gst_value_initialize): Better fakeout.
2005-09-26 Andy Wingocheck/gst-libs/controller.c: Update for controller...
2005-09-26 Andy WingoRemove memchunk benchmark stuff, this is taken over...
2005-09-26 Thomas Vander Sticheleremove queryutils headers after moving the two used...
2005-09-26 Michael SmithCorrect syntax for debug option in gst-launch manpage
2005-09-26 Wim Taymansgst/base/gstbasesrc.c: Some more debugging info.
2005-09-25 Stefan Kostadded more docs
2005-09-25 Stefan Kostinlined the last two docs files removed the tmpl direct...
2005-09-25 Stefan Kostinlined two more docs factored gstpadtemplate out of...
2005-09-24 Tim-Philipp Müllercheck/gst/gstbin.c: Fix test case: we can't rely on...
2005-09-24 Wim TaymansVarious documentation updates.
2005-09-24 Thomas Vander Stichelegst/gstclock.h: Well, that's embarassing. Luckily...
2005-09-23 Thomas Vander Stichelecommon/gtk-doc.mak: don't fail on building XML, FC4...
2005-09-23 Tim-Philipp MüllerAdd blurb about how the bus goes into flushing mode...
2005-09-23 Thomas Vander Sticheleadd a method to get a GstClockTime out of a structure
2005-09-23 Tim-Philipp Müllercheck/gst/gstbin.c: Added test to check state change...
next