docs/design/: Update some docs.
[glsdk/gstreamer0-10.git] / ChangeLog
2007-08-24 Wim Taymansdocs/design/: Update some docs.
2007-08-24 Jan Schmidtgst/Makefile.am: Revert patch which uses $(gst_headers...
2007-08-24 Jan Schmidttests/check/gst/gstbin.c: Fix leaks in the new unit...
2007-08-23 Tim-Philipp Müllergst/gst.c: Don't use GST_INFO before the debug system...
2007-08-23 David Nečasgst/Makefile.am: Replace some non portable makefile...
2007-08-21 Stefan Kostcommon/gtk-doc-plugins.mak: Grrrrr. Don't remove the...
2007-08-20 Wim Taymanstools/gst-launch.1.in: Add colorspace to example pipeli...
2007-08-20 Tim-Philipp Müllerdocs/random/release: The release manager should run...
2007-08-17 Wim Taymanstools/gst-launch.c: Don´t try to do any state managemen...
2007-08-16 Wim Taymansgst/gstbin.c: Improve debugging.
2007-08-16 Wim Taymansgst/gstbin.c: Fix annoying bug in the sorted iterator...
2007-08-16 Wim Taymansgst/gstmessage.h: Add some more docs for the messages.
2007-08-14 Wim Taymansgst/gstbin.c: Move ASYNC_START message posting to where...
2007-08-14 Julien Mouttegst/gstindex.c: Fix index entry generation from vargs...
2007-08-14 Wim Taymansgst/gstbin.c: Always change the state of a NO_PREROLL...
2007-08-13 Stefan KostAdd more missing docs.
2007-08-12 Wim Taymansgst/gststructure.c: Add Since tag to docs.
2007-08-12 Wim TaymansAdd function to get uint from a structure.
2007-08-12 Wim Taymansgst/gstcaps.c: Fix proper check for simple caps.
2007-08-10 Stefan Kostdocs/: Remove cruft and do some cleanups.
2007-08-10 Michael Smithdocs/gst/gstreamer-sections.txt: Add gst_registry_add_p...
2007-08-10 Michael Smithgst/gstregistry.h: Add gst_registry_add_path, which...
2007-08-10 Tim-Philipp Müllerlibs/gst/controller/gstlfocontrolsource.c: Printf forma...
2007-08-09 Philippe Kalaflibs/gst/base/gstbasesink.c: Don't send an async_start...
2007-08-09 Thomas Vander Stichelepo/: Added Hungarian translation.
2007-08-09 Thomas Vander Stichelepo/: Updated translations.
2007-08-07 Jan Schmidtlibs/gst/controller/Makefile.am: Dist gstlfocontrolsour...
2007-08-07 Jan Schmidtdocs/libs/gstreamer-libs.types: Don't register the...
2007-08-07 Wim Taymansgst/gstbuffer.h: Remove comma from last element in...
2007-08-07 Wim Taymansdocs/design/part-TODO.txt: Add some more TODO items
2007-08-05 Stefan Kostpo/POTFILES.*: Update POTFILES. Fixes #461599.
2007-08-03 Sebastian Drögegst/gst.c: Fix confusing typo in debug output.
2007-08-03 Sebastian Drögelibs/gst/controller/: API: Add GstLFOControlSource...
2007-08-03 Jan Schmidtconfigure.ac: Back to CVS
2007-08-03 Jan SchmidtRelease 0.10.14
2007-08-02 Tim-Philipp Müllergst/gstelement.*: Make strings passed to gst_element_cl...
2007-08-02 Wim Taymansgst/gstbin.c: Don't forget about the fact that some...
2007-07-31 Jan Schmidtgst/gstregistry.c: When replacing an existing feature...
2007-07-31 Jan Schmidtgst/gstpluginfeature.c: Revert patch from #459466 until...
2007-07-26 Tim-Philipp MüllerAPI: add GST_TAG_LICENSE_URI and GST_TAG_COPYRIGHT_URI...
2007-07-26 Jan Schmidtdocs/libs/Makefile.am: Include our build-prefix libs...
2007-07-26 Steve Finkdocs/pwg/building-testapp.xml: Mention that GST_PLUGIN_...
2007-07-25 Steve Finktools/gst-inspect.1.in: Document --print-all and -...
2007-07-25 Wim Taymansdocs/gst/gstreamer-sections.txt: Add docs for new api...
2007-07-25 Wim Taymansgst/gstelementfactory.*: API: gst_element_factory_has_i...
2007-07-25 Stefan KostAnother conditional doc check.
2007-07-24 Stefan Kostgst/gstregistrybinary.c: Print error just once and...
2007-07-24 Stefan Kostlibs/gst/base/gsttypefindhelper.c: Cleanup the typefind...
2007-07-24 Edward Herveyplugins/elements/gstcapsfilter.c: Fix capsfilter for...
2007-07-24 Stefan Kostgst/gsttypefindfactory.c: Fix docs that recommened...
2007-07-23 Stefan Kosttools/gst-inspect.c: Also give media-type for typefinde...
2007-07-23 Stefan Kostgst/gstregistry.*: Speed up gst_registry_lookup_feature...
2007-07-23 Stefan Kostgst/gstpluginfeature.c: Avoid double memory usage for...
2007-07-22 Tim-Philipp Müllergst/gstpad.h: Small addition to GST_FLOW_IS_FATAL(...
2007-07-22 Tim-Philipp Müllerdocs/pwg/advanced-types.xml: Fix typo and duplicate...
2007-07-22 Sebastian Drögelibs/gst/controller/gstinterpolation.c: Also round...
2007-07-21 Jan Schmidtlibs/gst/controller/gstinterpolation.c: When linearly...
2007-07-20 Stefan Kosttools/gst-plot-timeline.py: Better log parsing (categor...
2007-07-20 Stefan Kostdocs/random/ensonic/: Save my thoughts.
2007-07-20 Stefan KostAdd libm check as we use in for plugins.
2007-07-18 Jan Schmidtgst/gstbin.c: Check that the state_cookie hasn't change...
2007-07-17 Stefan Kostgst/gstregistrybinary.c: Fix memory leak. Be less verbo...
2007-07-16 Jan Schmidttests/check/elements/.cvsignore: Add file to cvsignore...
2007-07-16 Jan Schmidttests/check/elements/multiqueue.c: Use a GStaticMutex...
2007-07-16 Jan Schmidttests/check/pipelines/stress.c: Make sure we set the...
2007-07-16 Jan Schmidttests/check/elements/tee.c: Make the tee stress-test...
2007-07-16 Stefan Kostgst/gst.c: Avoid reading registry twice on startup...
2007-07-13 Jan Schmidtpkgconfig/: Substitute the CFLAGS for libcheck into...
2007-07-13 Jan Schmidtconfigure.ac: Revert the pkg-config check for libcheck...
2007-07-12 Stefan Kostconfigure.ac: Use pkg-config to locate check.
2007-07-10 Stefan Kostgst/gsttaglist.c: Fix doc syntax.
2007-07-08 Tim-Philipp Müllergst/gststructure.c: When deserialising foo=bar without...
2007-07-06 Sebastian Drögelibs/gst/controller/: API: Refactor GstController into...
2007-07-05 Mark Nauwelaertsplugins/elements/gstmultiqueue.c: Implement non-default...
2007-07-05 Stefan Kostdocs/: Simplity --extra-dir as gtkdoc scans recursively.
2007-07-03 Wim Taymanstools/gst-launch.c: When we got an error, there is...
2007-07-03 Wim Taymansplugins/elements/gsttee.c: Be a lot smarter when decidi...
2007-07-01 Thomas Vander Stichelepo/: Updated translations.
2007-07-01 Thomas Vander Stichelepo/: Added new Finnish translation.
2007-06-28 Wim Taymansplugins/elements/gstmultiqueue.c: When figuring out...
2007-06-27 Jan SchmidtMention bug 430682 closed by previous commit.
2007-06-27 Stefan Kostgst/gstminiobject.c: Remove 3 do-nothing methods.
2007-06-27 Tim Angusplugins/elements/gstcapsfilter.c: Take a reference...
2007-06-27 Stefan Kostgst/: Remove empty instance_init() functions to save...
2007-06-27 Étienne Noreau-Hébertgst/gstghostpad.c: Add peer and direction in the XML...
2007-06-26 Stefan Kostconfigure.ac: Preserve useful information, thanks Tim.
2007-06-26 Jan Schmidtplugins/elements/gstmultiqueue.*: Take the multiqueue...
2007-06-26 Jan Schmidtdocs/random/release: Some updates to the release procedure.
2007-06-26 Stefan Kostgst/gstelementfactory.c: Microoptimization that saves...
2007-06-25 Stefan Kostdocs/plugins/: Update docs with caps info.
2007-06-23 Thomas Vander Stichelepo/it.po: Updated Italian translation.
2007-06-23 Thomas Vander Stichelepo/: Update Vietnamese translations.
2007-06-21 Tim-Philipp Müllerlibs/gst/base/gstbasesink.c: Remove unused signal enum.
2007-06-21 Jan SchmidtBeef up and include the docs for gst_type_register_stat...
2007-06-21 Wim Taymansplugins/elements/gstmultiqueue.c: Fix setting max-...
2007-06-21 Stefan KostSaving relocations for GTypeInfo and GstElementDetails...
2007-06-21 Tim-Philipp Müllerdocs/pwg/advanced-types.xml: Fix typo in iana.org URI.
2007-06-19 Andy Wingotests/check/pipelines/simple-launch-lines.c
2007-06-19 Andy Wingotests/check/pipelines/simple-launch-lines.c
2007-06-19 Wim Taymansplugins/elements/gstmultiqueue.c: Fix event leak.
next