gststructure: early out when we know a value cannot be a subset
[glsdk/gstreamer0-10.git] / autogen.sh
2011-03-22 Luis de Bethencourtautogen: wingo signed comment
2010-06-28 Tim-Philipp MüllerBump automake requirement to 1.10
2010-04-07 Tim-Philipp Müllerbuild: bump autoconf requirement to 2.60 for gobject...
2010-03-30 Tim-Philipp Müllerbuild: make autotools put its m4 files into m4/ instead...
2009-08-06 Tim-Philipp Müllerautogen.sh: older aclocals don't like -I. so use -I...
2009-08-06 Tim-Philipp Müllercheck: use private copy of check for libgstcheck
2009-06-26 Jan Schmidtautogen.sh: Use printf instead of 'echo -n'. Check...
2009-06-03 Tim-Philipp MüllerRevert "go back to allowing gettext 0.11.5, but don...
2009-06-03 Tim-Philipp MüllerRevert "only update submodule when it is not on a speci...
2009-06-02 Thomas Vander Stichelego back to allowing gettext 0.11.5, but don't mix with...
2009-06-02 Thomas Vander Sticheleonly update submodule when it is not on a specific...
2009-05-21 Tim-Philipp Müllerautogen.sh: can remove the -Wno-portability from here now
2009-05-12 Marc-Andre LureauRun libtoolize before aclocal
2009-01-30 Edward HerveyUse a symbolic link for the pre-commit client-side...
2009-01-22 Wim TaymansMerge branch 'master' of ssh://git.freedesktop.org...
2009-01-22 Edward HerveyInstall and use pre-commit indentation hook from common
2009-01-21 Edward Herveyautogen.sh : Use git submodule
2008-11-29 Sebastian DrögeRequire gettext 0.17 because older versions don't mix...
2008-01-10 Sebastian Drögeautogen.sh: Add -Wno-portability to the automake parame...
2006-07-24 Thomas Vander Sticheleremove --enable-docs
2006-06-16 Tim-Philipp Müllerautogen.sh: Add default for new --enable-plugin-docs...
2006-05-08 Edward Herveyautogen.sh: Darwin's libtoolize is in fact called glibt...
2006-01-20 Thomas Vander Sticheleautogen.sh: up required version of automake to 1.7
2005-10-12 Thomas Vander Sticheleautoconf for freebsd
2005-10-12 Thomas Vander Sticheleautoconf for freebsd
2005-10-12 Thomas Vander Sticheleautoconf for freebsd
2005-10-12 Thomas Vander Sticheleautoconf for freebsd
2005-10-12 Thomas Vander Sticheleautoconf for freebsd
2005-10-10 Andy Wingoautogen.sh (CONFIGURE_DEF_OPT): No more --plugin-buiddi...
2005-09-05 Thomas Vander Stichelemaintenance updates
2005-09-03 Thomas Vander Sticheleclean up docs build a little; have docdir be an overrid...
2005-04-10 Thomas Vander Sticheleignore already applied patch
2004-12-08 Thomas Vander Sticheleremove patch if autopoint fails
2004-06-24 David Schleefautogen.sh: Remove call to env, since the buildbot...
2004-06-04 David Schleefautogen.sh: Add a temporary 'env' to test buildbot...
2004-02-29 Thomas Vander Sticheleupdate libtool requirement for latest plugin symbol...
2004-02-22 Benjamin Otteautogen.sh: replace test -e with test -x for mkinstalld...
2004-02-13 Thomas Vander Sticheleup version of gettext
2004-02-12 Thomas Vander Sticheleuse long options
2004-02-12 Thomas Vander Stichelecopy libtool
2004-02-06 Thomas Vander Stichelecheck out common with right tag
2004-02-05 Thomas Vander Sticheleprint configure lien
2004-01-23 Thomas Vander Stichelefix doc build fix autogen
2004-01-13 Thomas Vander SticheleI'm too lazy to comment this
2004-01-13 Thomas Vander Stichelelax gettext requirment
2004-01-13 Thomas Vander Sticheleadding i18n tested with nl, seems to work fine
2003-08-23 David SchleefRemove running configure for cothreads, since it's...
2003-08-21 David SchleefAdd --enable-poisoning option, and make it default...
2003-08-17 David SchleefFind correct name for libtoolize
2003-08-06 David SchleefAutomake-1.5 chokes on gst/Makefile.am, so updating...
2003-07-29 David SchleefRemove lines that pull libs/ext/cothreads from CVS
2003-05-01 Brian CameronUse -f instead of -e since -e does not work in Solaris...
2003-05-01 Brian CameronFixed if-test in autogen.sh so it works on Solaris...
2003-04-13 David SchleefChange autoconf_2.52d_check to 2_52 to make bash happy
2003-04-13 Matthias FriedrichUsing bash is problematic on non-linux plattforms,...
2002-11-01 David I. Lehnrun libtoolize in autogen.sh.
2002-09-30 Thomas Vander Stichelesuggest sane values for autotool programs
2002-07-01 Thomas Vander Stichelefor better or worse, make distcheck now passes again
2002-05-27 Thomas Vander Sticheletogether with the recent commit in common, this little...
2002-04-28 Thomas Vander Stichelemake sure autogen.sh options get passed on to cothreads
2002-04-18 Thomas Vander Stichelemessy aclocals tuff
2002-03-02 Thomas Vander SticheleGood luck with this one ;) converted to using getopt...
2002-02-13 Thomas Vander Stichelesmall addition
2002-02-10 Thomas Vander Stichelesync with as-version small autogen fix
2002-02-10 Thomas Vander SticheleSome people might have stray acinclude.m4's lying aroun...
2002-02-09 Thomas Vander Sticheleremoving m4 dir
2002-02-09 Thomas Vander Stichelemore build cleanups (using as-version and as-libtool...
2002-02-07 Andy Wingofix the whole cothread thing
2002-02-06 Thomas Vander Sticheletaaz: it doesn't work thomas: ok, I'll fix it.
2002-02-06 Thomas Vander Sticheletaaz's yapping
2002-02-06 Thomas Vander Sticheledisabling cothreads build until it passes make distcheck
2002-02-06 Steve Bakeruse numerical comparisions for version check
2002-02-04 Richard BoultonRevert aclocal invocation to do cat m4/*.m4 > acinclude...
2002-02-04 Andy Wingocothreads stuff i forgot to commit last night
2002-01-30 Wrobell- use aclocal -I option instead of cat
2002-01-23 Andy Wingobuild system tweaks, and now the cothreads test code...
2002-01-12 David I. Lehnmake libtoolize run like the other tools
2002-01-07 Thomas Vander Stichelefix for libtool issue which has been fixed in cvs ...
2001-12-22 Andy Wingochanged -d configure option to --autogen-debug added...
2001-12-20 Andy Wingoremoved gstreamer.m4 (packages should use pkg.m4) guila...
2001-12-15 Thomas Vander Stichelethis is better for everyone involved
2001-12-15 Thomas Vander Sticheleautogen.sh uses m4 dir for acinclude.m4 see if this...
2001-12-14 Thomas Vander SticheleWe should fix build errors as they happen and not find...
2001-12-13 Michael MeeksAplied a patch from Michael Meeks to add libxml2 support.
2001-12-12 Andy Wingominor typographical change to autogen added --with...
2001-12-11 Thomas Vander Sticheledocs changes
2001-12-11 Thomas Vander Stichelecosmetic change
2001-12-10 Thomas Vander Sticheleautomake copies instead of link
2001-12-10 Thomas Vander Sticheleadded check for 2.52d, we don't want it
2001-12-10 Thomas Vander Stichelea little bit more output
2001-12-10 Thomas Vander SticheleI guess we need bash for lexicographical comparison
2001-12-10 Thomas Vander Stichelethis makes somewhat more sense
2001-12-10 Thomas Vander Stichelemore "" around variables
2001-12-10 Thomas Vander Sticheleadded better testing
2001-12-10 Thomas Vander Sticheleadded -d flag for autogen.sh debugging, tell me if...
2001-12-09 Thomas Vander Sticheledo lexical comparison on version parts
2001-12-09 Thomas Vander Stichelerestructured autotools tests please test !
2001-12-08 Thomas Vander Stichelechanged some things
2001-12-08 Andy Wingoremove support for autoconf2.13
2001-11-13 Thomas Vander Sticheleremoved that bit
next