configure: back to development
[glsdk/gstreamer0-10.git] / configure.ac
2010-02-12 Tim-Philipp Müllerconfigure: back to development
2010-02-10 Tim-Philipp MüllerRelease 0.10.26
2010-02-10 Tim-Philipp Müllerconfigure: define GST_PLUGIN_SCANNER_INSTALLED in win32...
2010-02-04 Tim-Philipp Müller0.10.25.3 pre-release
2010-01-27 Tim-Philipp Müller0.10.25.2 pre-release
2010-01-20 Sebastian Drögebuild: Define G_THREADS_MANDATORY everywhere
2010-01-06 Tim-Philipp Müllerconfigure: move SHAVE_INIT behind all checks
2009-12-19 Tim-Philipp Müllerconfigure: always call our check checks for the SUBUNIT...
2009-12-19 Руслан Ижбулатовcheck: update autotools and docs stuff for new check...
2009-12-01 Sebastian Drögeconfigure: Use new AG_GST_PLATFORM macro
2009-11-20 Sebastian Drögecheck: Only check for gmp/gsl if building of tests...
2009-11-18 Tim-Philipp Müllerplugin-scanner: rename plugin-scanner helper binary...
2009-10-12 Edward Herveyconfigure.ac: Detect broken poll()
2009-10-07 Jan Schmidtconfigure: Beef up the test for __uint128_t on GCC
2009-10-07 Tim-Philipp Müllerconfigure: bump GLib requirement to 2.18
2009-10-06 Jan Schmidtregistry: Support installed/uninstalled plugin-scanner...
2009-10-06 Jan SchmidtRemove checking for and mentions of fork where possible.
2009-10-06 Jan Schmidtregistry: Add registry helper phase 1
2009-10-06 Jan SchmidtBack to development -> 0.10.25.1
2009-10-05 Jan SchmidtRelease 0.10.25
2009-10-01 Jan Schmidt0.10.24.4 pre-release
2009-09-17 Jan Schmidt0.10.24.3 pre-release
2009-09-14 David SchleefFix out-of-tree build
2009-09-11 Jan Schmidt0.10.24.2 pre-release
2009-09-09 Sebastian Drögeutils: Use gcc's __uint128_t for 64bit unsigned integer...
2009-09-05 Sebastian Drögegst: Add gobject-introspection support
2009-08-14 Sebastian Drögeconfigure: Remove duplicated check for clock_gettime
2009-08-14 Sebastian Drögegstutils: Add special random unit test for 64 scaling...
2009-08-10 Tim-Philipp Müllerchecks: try to fix GstObject unit test on OSX
2009-08-06 Tim-Philipp Müllercheck: disable unit test support on win32 for now
2009-08-06 Tim-Philipp Müllercheck: use private copy of check for libgstcheck
2009-08-06 Tim-Philipp Müllerconfigure.ac: fix libxml2 check, which is only needed...
2009-08-06 Jan Schmidtback to development -> 0.10.24.1
2009-08-04 Jan SchmidtRelease 0.10.24
2009-07-30 Jan Schmidt0.10.24.5 pre-release
2009-07-24 Jan Schmidt0.10.23.4 pre-release
2009-07-20 Jan Schmidt0.10.23.3 pre-release
2009-07-14 Jan Schmidt0.10.23.2 pre-release
2009-06-07 Wim Taymanstests: conditionally compile the streams example
2009-06-04 Tim-Philipp Müllerconfigure: remove AC_C_INLINE and update win32 files...
2009-06-03 Tim-Philipp MüllerRevert "go back to allowing gettext 0.11.5, but don...
2009-06-02 Thomas Vander Stichelego back to allowing gettext 0.11.5, but don't mix with...
2009-06-01 Wim TaymansAdd frame stepping in PAUSED example
2009-05-19 Tim-Philipp Müllerconfigure: pass -Wno-portability to automake to suppres...
2009-05-12 Tim-Philipp Müllerconfigure: rename CVS -> git in a couple of places
2009-05-11 Tim-Philipp Müllerconfigure: bump the GLib requirement to GLib >= 2.16
2009-05-11 Tim-Philipp Müllerxmlregistry: remove the old xml registry
2009-05-11 Wim Taymanstests: add example app for stream-status
2009-05-11 Jan Schmidtinfo: Support new printf extensions in glibc 2.10
2009-05-11 Jan SchmidtBack to development -> 0.10.23.1
2009-05-10 Jan SchmidtRelease 0.10.23
2009-05-06 Jan Schmidt0.10.22.4 pre-release
2009-04-21 Jan Schmidt0.10.22.3 pre-release
2009-04-17 Tim-Philipp Müllerwin32: define __MSVCRT_VERSION__ when compiling with...
2009-04-17 Yaakov Selkowitzconfigure.ac: fork() during registry scanning is unsafe...
2009-04-15 Jan Schmidtrelease: Bump version to 0.10.22.2 for pre-release
2009-04-15 Stefan Kostgstdebug: show enabled/disabled in configure and fix...
2009-02-28 David SchleefBump glib requirement to 2.14
2009-02-25 Jan Schmidtbuild: Update shave init statement for changes in commo...
2009-02-23 David SchleefChange how win32/common/config.h is updated
2009-02-22 Jan SchmidtUse shave (git.lespiau.name/cgit/shave/) to simplify...
2009-01-23 Brian CameronFix linking failures on Solaris. Fixes bug #568481.
2009-01-22 Wim TaymansMerge branch 'master' of ssh://git.freedesktop.org...
2009-01-22 Jan SchmidtBack to development -> 0.10.22.1
2009-01-19 Jan SchmidtRelease 0.10.22
2009-01-09 Jan Schmidtconfigure.ac: pre-release 0.10.21.3
2008-12-04 Sebastian Drögeconfigure.ac: Apparently AC_CONFIG_MACRO_DIR breaks...
2008-12-04 Sebastian Drögeconfigure.ac: Set AC_CONFIG_MACRO_DIR to common/m4...
2008-11-29 Sebastian DrögeRequire gettext 0.17 because older versions don't mix...
2008-10-22 Jan Schmidtconfigure.ac: Fix a bug in the output of the configure...
2008-10-05 Jan Schmidtconfigure.ac: Back to development -> 0.10.21.1
2008-10-02 Jan SchmidtRelease 0.10.21
2008-09-28 Jan Schmidtconfigure.ac: 0.10.20.4 pre-release
2008-09-16 Jan SchmidtGah. Commit pre-release info that should have gone...
2008-09-15 Stefan Kostconfigure.ac: Do not probe availability of check unit...
2008-08-01 Stefan KostRevert 'accidential' change of the configure option...
2008-07-31 Sebastian DrögeRemove GST_DISABLE_(ENUMTYPES|INDEX|URI) everywhere.
2008-07-29 Michael SmithBuild the net library if we have winsock2.
2008-07-22 Michael Smithconfigure.ac: Remove AC_ISC_POSIX macro; it's broken...
2008-07-10 Michael Smithconfigure.ac: Don't require flex and bison if the parse...
2008-06-27 Stefan Kostconfigure.ac:
2008-06-20 Thomas Vander SticheleDon't assume that <valgrind/valgrind.h> exists just...
2008-06-20 Jan Schmidtconfigure.ac: Bump version number back to dev -> 0...
2008-06-18 Jan SchmidtRelease 0.10.20
2008-06-11 Jan Schmidtconfigure.ac: 0.10.19.3 pre-release
2008-06-11 David SchleefRename DATADIR to GST_DATADIR to avoid build problems
2008-06-05 Sebastian Drögeconfigure.ac: Explicitely link with -ldl if dladdr...
2008-06-05 Jan Schmidtconfigure.ac: 0.10.19.2 pre-release
2008-05-27 Stefan Kostconfigure.ac: Add DATADIR for storing presets.
2008-05-22 Sebastian Drögeconfigure.ac: After discussion on IRC use the binary...
2008-04-11 Julien MoutteMac OS X love...
2008-04-06 Damien Lespiauconfigure.ac: Actually build dlls when cross-compiling...
2008-04-03 Tim-Philipp Müllerconfigure.ac: Bump version to 0.10.19.1 after the unsch...
2008-04-03 Stefan Kostconfigure.ac: Revert part that belongs to the preset...
2008-04-03 Stefan Kostconfigure.ac: Add qoutes to the define. Fixes # 525961.
2008-04-01 Sebastian Drögeconfigure.ac: Require GLib 2.12.
2008-04-01 Jason Zhaoconfigure.ac: Add a configure switch to disable option...
2008-03-31 Stefan KostMacOS has plugins under .so or under .dylib. Add detect...
2008-03-21 Jan Schmidtconfigure.ac: Back to development - 0.10.18.1
2008-03-21 Jan SchmidtRelease 0.10.18
next