]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/gstreamer0-10.git/history - docs/faq/gst-uninstalled
plugin-scanner: rename plugin-scanner helper binary to gst-plugin-scanner
[glsdk/gstreamer0-10.git] / docs / faq / gst-uninstalled
2009-11-18 Tim-Philipp Müllerplugin-scanner: rename plugin-scanner helper binary...
2009-11-17 Tim-Philipp Müllergst-uninstalled: add paths for gst-qa-system
2009-10-07 Sebastian Drögegst-uninstalled: Extend environment variables to allow...
2009-10-06 Jan Schmidtregistry: Support installed/uninstalled plugin-scanner...
2009-08-06 Tim-Philipp Müllergst-uninstalled: rename uninstalled registry file to...
2009-08-06 Tim-Philipp Müllergst-uninstalled: refine search paths for uninstalled...
2009-03-19 Tim-Philipp Müllergst-uninstalled: add gst-rtsp-server bits and break...
2009-03-03 Tim-Philipp Müllergst-uninstalled: add bits for uninstalled checkouts...
2009-02-14 Tim-Philipp MüllerFAQ: update for git and miscellaneous small fixes and...
2009-01-06 Tim-Philipp Müllerdocs/faq/gst-uninstalled: Add libgstapp-0.10 from ...
2008-05-23 Suresh Kumar Pdocs/faq/gst-uninstalled: Also support ffmpeg in gst...
2008-04-11 Julien MoutteMac OS X love...
2008-02-08 Jan Schmidtconfigure.ac: Make DISABLE_DEPRECATED defined *only...
2008-01-03 Sebastian Drögedocs/faq/gst-uninstalled: Clarify the comments to make...
2007-11-21 Julien Mouttedocs/faq/gst-uninstalled: Yet another missing library...
2007-11-20 Julien Mouttedocs/faq/gst-uninstalled: Add another library to the...
2007-11-19 Julien Mouttedocs/faq/gst-uninstalled: Add new base libraries in...
2007-04-17 Thomas Vander SticheleMANPATH fix
2007-04-12 Thomas Vander Sticheledocs/faq/gst-uninstalled: don't get empty paths on...
2007-01-19 Edward Herveydocs/faq/gst-uninstalled: Add gst-plugins-base/gst...
2007-01-17 Edward Herveydocs/faq/gst-uninstalled: Add DYLD_LIBRARY_PATH declara...
2006-07-02 Thomas Vander Sticheledocs/faq/gst-uninstalled: don't put empty paths on...
2006-04-06 Thomas Vander Sticheleadd gnonlin
2006-04-03 Thomas Vander Sticheleupdate win32 common dir; update uninstalled script
2006-03-24 Michael Smithdocs/faq/gst-uninstalled: Set up LD_LIBRARY_PATH to...
2005-12-16 Thomas Vander Stichelegst/gst.c: make the registry cache file HOST_CPU-dependent
2005-11-08 Thomas Vander Stichelerevert part of the patch so that paths are correct
2005-11-07 Thomas Vander Sticheledocs/faq/gst-uninstalled: fix up PS1 for systems that...
2005-10-06 Thomas Vander Sticheledoh. use correct variable
2005-10-04 Thomas Vander Sticheleupdate uninstalled script
2005-09-05 Thomas Vander Sticheleadding -bad
2005-08-31 Thomas Vander Sticheledocs/faq/gst-uninstalled: add -good
2005-06-08 Thomas Vander Sticheleadd a 'plugins' dir to the PLUGIN_PATH in the uninstall...
2005-04-16 Thomas Vander Sticheleadd gst-plugins-base to pkgconfig path
2005-03-25 Thomas Vander Sticheledocs/faq/gst-uninstalled: add gst-plugins-base
2004-08-09 Thomas Vander Sticheledocs/faq/gst-uninstalled: fix PKG_CONFIG_PATH and PYTHO...
2004-06-18 Thomas Vander Stichelegst-python
2004-04-22 Thomas Vander Sticheledon't trash previous ones
2004-04-07 Thomas Vander Stichelemake sure we don't have a stray : in LD_LIBRARY_PATH
2004-03-17 Thomas Vander Sticheleadding monkeysaudio to uninstalled dirs
2004-02-16 Thomas Vander Sticheleadd comment
2004-02-16 Thomas Vander Stichelesmall update
2004-02-16 Thomas Vander Sticheleadding gst-uninstalled script