]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/gstreamer0-10.git/history - docs/gst/gstreamer-sections.txt
Remove GST_DISABLE_(ENUMTYPES|INDEX|URI) everywhere.
[glsdk/gstreamer0-10.git] / docs / gst / gstreamer-sections.txt
2008-07-31 Sebastian DrögeRemove GST_DISABLE_(ENUMTYPES|INDEX|URI) everywhere.
2008-07-29 Stefan Kostdocs/gst/gstreamer-sections.txt: Cleanup section-file.
2008-06-20 Sebastian DrögeAPI: Add GST_TAG_ATTACHMENT for generic file attachment...
2008-05-27 Stefan Kostconfigure.ac: Add DATADIR for storing presets.
2008-05-27 Tim-Philipp MüllerAPI: add gst_bin_find_unlinked_pad()
2008-05-24 Tim-Philipp MüllerAPI: gst_parse_launch_full()
2008-05-19 Tim-Philipp MüllerAPI: add gst_type_find_suggest_simple(), #533740.
2008-04-29 Wim TaymansAdd method to conveniently check the name of a custom...
2008-04-23 Stefan Kostdocs/gst/gstreamer-sections.txt: Move GParamSepc macros...
2008-04-15 Stefan KostAdd GST_PARAM_CONTROLLABLE and GST_PARAM_USER_SHIFT...
2008-04-10 José AlburquerqueAdd gst_pad_add_*_probe_full() functions with a notify...
2008-04-09 José AlburquerqueExpose gst_segment_copy() to make things easier for...
2008-04-08 Wim TaymansRename _avail -> _range
2008-04-08 Wim TaymansReorder the message docs and headers for clarity.
2008-03-27 Stefan KostExpose macro to docs and fix link to it.
2008-03-22 Sebastian DrögeAPI: Add GST_IS_PARAM_SPEC_MINI_OBJECT, GST_PARAM_SPEC_...
2008-03-21 Sebastian DrögeCall the version GST_MAGIC_BINARY_VERSION_STR to be...
2008-03-18 Ole André Vadla... Add new function gst_poll_fd_ignored() for improved...
2008-03-07 Ole André Vadla... Remove GstPollMode from the API, it does not make sense...
2008-02-29 Wim TaymansAdd INIT macro and _init method for initializing the...
2008-02-27 Wim Taymansconfigure.ac: Add checks for poll, ppoll and pselect.
2008-02-11 Siavash Safigst/gstindex.*: Add new function with option to dispose...
2008-02-01 Julien Mouttedocs/gst/gstreamer-sections.txt: Add GST_CHECK_VERSION...
2008-01-09 Tim-Philipp MüllerAPI: add gst_plugin_register_static() and deprecate
2007-12-11 Stefan KostChange GST_GET_TIMESTAMP into gst_util_get_timestamp...
2007-11-28 Stefan KostRename new API + ChangeLog surgery to remove old name...
2007-11-28 Stefan KostNow hide the different clock stuff behind a macro.
2007-11-28 Wim TaymansStart merging in the easy bits of #361155, the monotoni...
2007-11-26 Stefan KostDue to popular request remove preset interface again...
2007-11-20 Sebastian Drögedocs/gst/gstreamer-sections.txt: Add new gst_preset__ge...
2007-11-17 Stefan KostAdd the preset interface (Fixes #396779). Do some doc...
2007-10-24 Tim-Philipp MüllerAPI: add GST_TAG_ARTIST_SORTNAME
2007-10-22 Edgard Limadocs/gst/gstreamer-sections.txt: Fixed documentation...
2007-10-17 Stefan KostAllow dumping pipelines as dot graphs. Fixes #456573.
2007-10-16 Tim-Philipp MüllerAPI: add gst_bus_pop_filtered
2007-09-30 Sebastian Drögedocs/gst/gstreamer-sections.txt: Add M_PI and IMPORT_SY...
2007-09-25 Tim-Philipp MüllerAPI: add GST_TAG_COMPOSER, fixes #459809.
2007-09-11 Wim TaymansAdd function to perform a query on the peer of a pad.
2007-08-12 Wim TaymansAdd function to get uint from a structure.
2007-08-10 Michael Smithdocs/gst/gstreamer-sections.txt: Add gst_registry_add_p...
2007-07-26 Tim-Philipp MüllerAPI: add GST_TAG_LICENSE_URI and GST_TAG_COPYRIGHT_URI...
2007-07-25 Wim Taymansdocs/gst/gstreamer-sections.txt: Add docs for new api...
2007-06-21 Jan SchmidtBeef up and include the docs for gst_type_register_stat...
2007-06-06 Tim-Philipp MüllerAPI: add GstParamSpecFraction, so elements can have...
2007-05-22 Edward HerveyAdd a property for bins that handle the state change...
2007-04-27 Sebastian DrögeAPI: Add gst_uri_protocol_is_supported(), which checks...
2007-04-26 Tim-Philipp MüllerAPI: add gst_buffer_try_new_and_alloc() plus unit test...
2007-04-20 Stefan Kostdocs/gst/gstreamer-sections.txt: That was one byte...
2007-04-20 Stefan Kost2nd attempt to have a xml-less build as a joined effort...
2007-04-05 Wim TaymansImprove _adjust_unlocked() so that it overflows less.
2007-03-19 Wim Taymansdocs/gst/gstreamer-sections.txt: Add new element field...
2007-03-19 Wim TaymansAdd ASYNC_START and ASYNC_DONE messages to prepare...
2007-03-09 Wim TaymansAdd metadata copy functions. Fixes #393099.
2007-02-28 Wim Taymansdocs/gst/gstreamer-sections.txt: Add new stuff to docs.
2007-02-27 Wim TaymansAPI: gst_bus_timed_pop()
2007-02-21 Thomas Vander SticheleFix up documentation to link to the correct GstGError...
2007-02-21 Wim Taymansdocs/gst/gstreamer-sections.txt: Removed docs as well.
2007-02-15 Wim Taymansdocs/gst/gstreamer-sections.txt: Remove old unused...
2007-02-12 René StadlerAPI: add GST_TAG_REFERENCE_LEVEL (#403597).
2007-02-11 Stefan Kostdocs/libs/Makefile.am: Fix path to core docs.
2007-02-02 Wim Taymansdocs/gst/gstreamer-sections.txt: Add docs for new methods.
2007-01-29 Tim-Philipp MüllerAPI: add GST_ROUND_DOWN_* macros (#401781).
2007-01-15 Stefan Kostadd tag support for beat-per-minute
2007-01-11 Stefan Kostcommit binary registry (disabled by default, see #359653)
2007-01-08 Tim-Philipp MüllerAPI: add gst_update_registry() (#391296).
2006-11-06 Stefan Kostdocs/gst/gstreamer-sections.txt: add new API and fix...
2006-10-17 Tim-Philipp Müllerdocs/gst/gstreamer-sections.txt: Forgot this one, makes...
2006-10-09 Tim-Philipp MüllerAPI: add gst_tag_list_is_empty() (#360467).
2006-10-05 Tim-Philipp MüllerAdd GST_USING_PRINTF_EXTENSION to gstconfig.h so that...
2006-10-02 Edward Herveydocs/design/part-block.txt: Further explain the use...
2006-09-15 Wim TaymansAdded methods to create and parse BUFFERING messages.
2006-08-31 Edward HerveyRefactored *_new() functions.
2006-08-24 Stefan Kostimplement caps merging (fixes #352580)
2006-08-21 Stefan KostAPI: Add gst_caps_merge() and use it in basetransform...
2006-08-16 Jan SchmidtAdd internal helpers for pre-registering quarks from...
2006-08-14 Tim-Philipp MüllerAPI: add GST_TAG_EXTENDED_COMMENT (#350935).
2006-08-11 Wim Taymansdocs/gst/gstreamer-sections.txt: Add GstClockClass...
2006-08-11 Wim TaymansDoc updates.
2006-08-09 Tim-Philipp MüllerAPI: add GST_SEGMENT_FORMAT, which is a printf extensio...
2006-07-26 Jan Schmidtdocs/gst/gstreamer-sections.txt: Oops. Commit the docs...
2006-07-17 Wim TaymansAdd two functions to check and change the SIGSEGV behav...
2006-07-10 Stefan KostMore docs for configuration options, add docs to gtk...
2006-07-02 Thomas Vander Sticheledocs/faq/gst-uninstalled: don't put empty paths on...
2006-06-12 Wim Taymansdocs/gst/gstreamer-sections.txt: Fix docs.
2006-05-30 Thomas Vander Sticheledocs/: add declared symbols
2006-05-30 Tim-Philipp MüllerAPI: add GST_TAG_PREVIEW_IMAGE (#343341).
2006-05-23 Julien Mouttedocs/gst/gstreamer-sections.txt: Make new GST_FLOW_IS_S...
2006-05-19 Tim-Philipp MüllerAPI: add gst_element_seek_simple() (#342238).
2006-05-14 Tim-Philipp MüllerMinor docs fixes.
2006-03-24 Wim Taymansdocs/gst/gstreamer-sections.txt: Rearrange the order...
2006-03-23 Tim-Philipp MüllerAPI: add some new utility functions:
2006-03-13 Wim TaymansDocumentation updates.
2006-03-09 Tim-Philipp MüllerAdd new API: gst_pipeline_set_auto_flush_bus() and...
2006-03-09 Tim-Philipp MüllerAdd new API: gst_uri_has_protocol() (#333779).
2006-03-07 Wim TaymansSmall documentation fixes.
2006-02-14 Wim TaymansFix padtemplate docs, fixes #328805.
2006-02-14 Wim Taymansdocs/gst/gstreamer-sections.txt: Reworked query docs.
2006-02-13 Wim TaymansAdd new functions to docs.
2006-02-13 Tim-Philipp MüllerNew API: add GST_MESSAGE_TYPE_NAME and GST_QUERY_TYPE_N...
2006-02-02 Tim-Philipp MüllerAdd new API: gst_parse_bin_from_description() and gst_b...
next