]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/gstreamer0-10.git/history - examples
libs/gst/dataprotocol/: It's about time we bump the version number.
[glsdk/gstreamer0-10.git] / examples /
2005-09-05 Thomas Vander Stichelemaintenance updates
2005-09-02 Andy Wingogst/gstelement.h (GstState): Renamed from GstElementSta...
2005-08-29 Stefan Kostcheck/gst-libs/controller.c: more tests
2005-08-26 Jan SchmidtAdd metadata reading example that loops over a list...
2005-08-02 Stefan Kostadded controller code removed dparam pc files
2005-07-11 Ronald S. Bultjedocs/pwg/: Rewrite scheduling-chapter for scheduling...
2005-07-07 Thomas Vander Sticheleignore more
2005-07-06 Jan Schmidtexamples/: Update a couple of the examples to work...
2005-07-06 Ronald S. BultjeAdd a chapter on caps negotiation, simplify the origina...
2005-07-01 Ronald S. Bultjeexamples/pwg/Makefile.am: Fix buildbot again.
2005-07-01 Ronald S. Bultjedocs/pwg/building-testapp.xml: Add extra check.
2005-07-01 Ronald S. BultjeEnable building the PWG examples.
2005-06-29 Ronald S. BultjeAdd probe example.
2005-06-29 Ronald S. Bultjedocs/manual/: Update (until threads/scheduling) Applica...
2005-06-28 Andy Wingo*.c: Don't cast to GST_OBJECT when reffing or unreffing...
2005-06-17 Thomas Vander Sticheleignore more; fix README
2005-05-17 Thomas Vander Stichelesmall doc fixes
2005-03-07 Wim TaymansFirst THREADED backport attempt, focusing on adding...
2004-12-23 Ronald S. Bultjedocs/manual/advanced-dataaccess.xml: Add section on...
2004-12-19 Ronald S. Bultjedocs/manual/: Rewrites. Remove cothreads, go a bit...
2004-12-17 Thomas Vander Sticheleignore more
2004-12-15 Ronald S. Bultjedocs/manual/: Try 2. This time, include a short preface...
2004-12-15 Thomas Vander Stichelefix last example. Add example of adding code blocks...
2004-12-15 Thomas Vander SticheleMake it possible to extract example code from separate...
2004-10-13 David Schleefexamples/manual/Makefile.am: $< isn't portable in Makef...
2004-09-09 Thomas Vander Sticheleouch, this breaks our test bots heavily :)
2004-09-08 Thomas Vander Sticheleunbreak testsuite
2004-09-08 Thomas Vander Sticheledocs/: restructure so that common stuff is shown first
2004-09-08 Thomas Vander Sticheletwo more examples
2004-05-04 Thomas Vander Stichelereorganize C/LIB flags add gst_info to gstcompat.h
2004-05-03 Stéphane Loeuilletdisksink -> filesink
2004-04-20 David Schleefcommon/as-libtool.mak: Fine-tune DLL building.
2004-04-16 David Schleefdocs/gst/gstreamer-sections.txt: Remove deprecated...
2004-03-28 Benjamin Ottegst/gstbin.c: don't add decoupled elements to scheduler...
2004-03-15 Thomas Vander Sticheledon't mix tabs and spaces
2004-03-15 Johan DahlinRevert again, this time without post-commit reindent...
2004-03-15 Johan Dahlin*.h: Revert indentation changes.
2004-03-13 Thomas Vander Stichelegst-indent run on core
2004-01-30 Benjamin Otteparts of the patch submitted in bug #113913
2004-01-18 Colin Waltersexamples/retag/retag.c: Call gst_init before processing...
2004-01-12 Benjamin Otteupdate - this is huge, because it includes *.bb, *...
2003-12-22 David SchleefMerge CAPS branch
2003-12-19 Thomas Vander Sticheleminor cosmetic fixes
2003-12-04 Andy Wingoremove copyright field from plugin structs
2003-12-02 Thomas Vander Stichelefix docs build fix make distcheck
2003-12-02 Thomas Vander Sticheleremoving this broken example. holler if you need it.
2003-11-29 David SchleefRemove old autoplug code
2003-11-24 Benjamin Ottemerge in tagging
2003-10-31 Benjamin Otteupdate plugin initialization restructuring (see email...
2003-10-08 Andy Wingos/GstBuffer/GstData/ in the API where you can pass...
2003-09-11 Thomas Vander Sticheleignore
2003-07-29 Jan SchmidtFix installing plugin in wrong dir
2003-07-12 Ronald S. BultjePlugin details fixes
2003-07-10 Wim TaymansUpdated example app
2003-06-29 Benjamin OtteGST_DEBUG reorganization containing loads of stuff:
2003-06-09 Wim Taymansupdated example with correct code to add namespaces...
2003-05-18 David SchleefCall perl script using $(PERL_PATH)
2003-04-15 Benjamin Ottedestroyed gst_*_destroy in the examples - use gst_objec...
2003-02-25 Wim TaymansI'm too lazy to comment this
2003-02-23 Christian SchallerAdded cutter patch from Andrew Turner and sat default...
2003-02-12 Wim TaymansExample of how an app could read data from a pipeline...
2003-02-10 Wim Taymans- Add more --disable options
2003-01-10 David I. Lehnconnect -> link
2003-01-09 Thomas Vander Stichelecode cleanups and further deprecation fixes
2003-01-09 Thomas Vander Stichelefirst pass of connect->link gst-plugins and other stuff...
2002-11-29 Thomas Vander Stichelerandom cleanups and paranoia checks
2002-10-30 David I. Lehnuse G_{BEGIN,END}_DECLS
2002-09-15 Thomas Vander Sticheleanother example
2002-09-14 Thomas Vander Sticheletry again
2002-09-14 Thomas Vander Sticheleadd this
2002-09-14 Thomas Vander Sticheleadding automatic example extraction from manual
2002-09-08 Christian Schallercommitting many nice little memleaks fixes from Iain...
2002-07-25 Wim TaymansAdded an example state change function
2002-07-24 Wim Taymans- Added a little testapp for pad disable using two...
2002-07-11 Thomas Vander Stichelebetter problem checking
2002-05-30 Thomas Vander Stichelefixes bug 83427
2002-05-27 Andy Wingofixups in the prop view/controller compilation fixes...
2002-05-26 Wim TaymansSmall fixes, use some wierd hack to make the plugin...
2002-04-11 Andy Wingocommit to make gstreamer follow the gtk function/macro...
2002-04-07 Andy Wingonew parser that uses flex and bison
2002-03-30 Wim TaymansAdded some sanity checks
2002-03-24 Andy Wingofilter newlines out of GST_DEBUG statements to reflect...
2002-03-20 Andy Wingos/Gnome-Streamer/GStreamer/
2002-03-19 Andy Wingoremoval of //-style comments don't link plugins to...
2002-02-21 Andy Wingoadd two apis: gst_element_connect_elements_many (elem1...
2002-01-31 Martin EnlundUpdated to use gst-launch instead of gstreamer-launch...
2002-01-17 Wim Taymansautoplug doesn't depend on gnome anymore.
2002-01-17 Wim TaymansRemove the gnome dependency
2002-01-17 Thomas Vander SticheleI've removed autoplug from build and dist since it...
2002-01-14 Andy Wingofix doc build for glib2 remove template files from...
2002-01-12 David I. Lehns/filter/plugin/ add $(GST_LIBS) to all plugins move...
2002-01-11 Andy Wingorun a file, this is a quick hack
2002-01-11 Andy Wingosummary: fix xml in gstreamer 1) make clear distinction...
2002-01-06 Wim TaymansFix the helloworld example.
2002-01-06 Andy Wingoglobal s/disksrc/filesrc/, but edited by me
2002-01-05 Andy Wingofor i in `find . -name *.[ch]`; do perl -n -i -p -e...
2002-01-05 Andy Wingocompile fixen
2002-01-05 Andy Wingochanges to allow apps outside of gstreamer/ to use...
2001-12-22 Wim TaymansFixed the typefind function
2001-12-17 Wrobell- use GST_CFLAGS and GST_LIBS only
next