]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/gstreamer0-10.git/history - gst/Makefile.am
check/Makefile.am: look in the right place for elements, a lot more chance of success
[glsdk/gstreamer0-10.git] / gst / Makefile.am
2005-11-29 Thomas Vander Stichelecheck/Makefile.am: look in the right place for elements...
2005-11-28 Thomas Vander Stichelegst/Makefile.am: don't try and build net if we don...
2005-11-27 Thomas Vander Sticheleadd undefined for core
2005-11-27 Thomas Vander Sticheleupdate LDFLAGS use some more
2005-11-22 Edward HerveyRemoved GstURI , closes bug #321061
2005-11-21 Andy Wingogst/Makefile.am (gst_headers): Add glib-compat.h. noins...
2005-11-20 Wim TaymansAdded segment helper structure and methods. Not fully...
2005-11-16 Andy Wingogst/net/: New part of core to hold network elements...
2005-11-16 Michael Smithgst/Makefile.am: Don't link against VALGRIND_LIBS....
2005-10-17 Andy Wingogst/base/gstcollectpads.c (gst_collectpads_chain):...
2005-10-15 Thomas Vander Sticheleconfigure.ac: reorganize clean up document more remove...
2005-09-26 Thomas Vander Sticheleremove queryutils headers after moving the two used...
2005-09-25 Stefan Kostinlined two more docs factored gstpadtemplate out of...
2005-09-20 Stefan Kostmore docs inlined, splitted gstindex.{c,h}
2005-09-20 David Schleefdocs/gst/Makefile.am: Ignore a few more internal headers
2005-09-15 David Schleefgst/Makefile.am: Dist glib-compat.h
2005-09-15 David Schleefgst/Makefile.am: Oh yeah, libgstreamer.so needs to...
2005-09-15 David Schleefremove
2005-09-14 Michael SmithRest of the fix for 316155: don't confuse MinGW when...
2005-09-07 Stefan Kostrenamed gsttag -> gsttaglist, gsttaginterface -> gsttag...
2005-09-07 Stefan Kostgst/: splitted gsttypefind into gsttypefind, gsttypefin...
2005-08-22 Stefan Kostported gstchildproxy over from 0.8 ported gst-inspect...
2005-08-20 Thomas Vander Stichelework on builds without check
2005-08-20 Thomas Vander Stichelemove check stuff to its own library to be used by other...
2005-07-18 Wim TaymansRemoved plugable schedulers.
2005-07-18 Wim Taymansgst/: Remove old file.
2005-07-18 Wim Taymansgst/Makefile.am: No more cothreads.h
2005-06-29 Ronald S. BultjeRemove old probes, add new g-signal-based probes and...
2005-06-08 Andy Wingogst/gstutils.c: RPAD fixes all around.
2005-05-30 Wim Taymansgst/: Move elementfactory methods to separate .h file.
2005-05-19 Ronald S. Bultjegst/: Hi, I'm outdated. Please shoot me.
2005-05-16 David Schleefcheck/Makefile.am: remove GstData checks
2005-05-09 Andy Wingogst/gstiterator.h: Add some includes.
2005-05-08 Edward Herveygst/Makefile.am: Added gstqueryutils.h to the list...
2005-05-02 Thomas Vander Sticheleautomake 1.5 fixes
2005-05-02 Thomas Vander Stichelepossible fixes for automake-1.5
2005-04-24 David SchleefConvert everything from GstAtomicInt to g_atomic_int_...
2005-04-24 David Schleefgst/gstpad.c: Remove handling of filtered caps. Fix...
2005-04-23 David Schleefgst/Makefile.am: Remove as-libtool stuff. It's likely...
2005-03-28 Wim TaymansAdded state change code.
2005-03-26 David Schleefgst/Makefile.am: remove gstcpu.[ch]. The gst_cpu funct...
2005-03-21 Wim TaymansNext big merge.
2005-03-07 Wim TaymansFirst THREADED backport attempt, focusing on adding...
2004-05-09 Thomas Vander Sticheledon't break distcheck
2004-05-08 Thomas Vander Sticheleadd a dependency so it triggers a marshal code rebuild
2004-05-07 David SchleefChanges to handle compilers that don't have variadic...
2004-05-04 Thomas Vander Stichelereorganize C/LIB flags add gst_info to gstcompat.h
2004-05-03 Thomas Vander Sticheleremove gst_info remove gstlog.h, fold back to gstinfo...
2004-04-14 David Schleefgst/: Convert asm source into inline assembly.
2004-04-13 David Schleefconfigure.ac: Changes to remove POSIXisms (mmap in...
2004-04-05 Benjamin Otteadd support for detecting if GStreamer runs inside...
2004-03-26 David Schleefdocs/gst/gstreamer-sections.txt: More doc hacking.
2004-02-27 Thomas Vander Sticheleadding back RELEASE clean up disting of built files
2004-02-27 David Schleefconfigure.ac: We don't really need glib-2.3. Also...
2004-01-18 Thomas Vander Stichelechanging error signal add error codes and domains
2004-01-13 Thomas Vander Sticheledistcheck fixes
2004-01-13 Thomas Vander Sticheleadding i18n tested with nl, seems to work fine
2003-12-22 David Schleefrename gstcaps2.[ch] to gstcaps.[ch]
2003-12-22 David SchleefMerge CAPS branch
2003-12-09 David Schleefoops, didn't intend to do last checkin
2003-12-09 David SchleefChange GST_.*_PADDING to _gst_padding[GST_PADDING];
2003-12-01 David Schleefremove gstcaps2.h
2003-12-01 Jan SchmidtAdd gstcaps2.h for installation so gst-plugins builds.
2003-11-29 David SchleefRemove old autoplug code
2003-11-24 Benjamin Ottemerge in tagging
2003-11-14 Thomas Vander Sticheleput GST_CACHE_DIR in config.h
2003-11-03 David SchleefAdd GstStructure and GstValue
2003-10-28 Benjamin Ottemerge TYPEFIND branch. Major changes:
2003-10-01 Ronald S. BultjeNew typefind system: bytestream is now part of the...
2003-09-13 Ronald S. BultjeImplement generic interface stuff, with per-instance...
2003-06-29 Benjamin OtteGST_DEBUG reorganization containing loads of stuff:
2003-04-23 Thomas Vander Stichelemake the user registry location major-minor versioned...
2003-04-14 Wim TaymansUpdated makefile too..
2003-02-10 Wim Taymans- Add more --disable options
2003-01-16 Wim TaymansAdded infrastructure to register URI to element+propert...
2003-01-09 Thomas Vander Stichelecode cleanups and further deprecation fixes
2003-01-09 Thomas Vander Stichelefirst pass of connect->link gst-plugins and other stuff...
2003-01-06 Wim TaymansAnd now it's inlined again :)
2003-01-01 Wim Taymans- Added PAD_NEGOTIATING flag, remove PAD_EOS flag
2002-12-31 Wim Taymans- copy kernel headers (waiting for libatomic..)
2002-12-30 Wim Taymans- major API breakage (one of the last, I promise...)
2002-12-29 Wim Taymans- First pass at cleaning up the atomic mess
2002-12-12 Wim TaymansRenamed GstCache to GstIndex
2002-12-11 Thomas Vander Stichelenot used anymore
2002-12-08 Thomas Vander Stichelefix for parallel installability
2002-11-29 Wim TaymansMore forte compiler fixes, added a .h file to store...
2002-11-29 Wim TaymansIndex caches dir too, add caches to Makefile.am
2002-11-28 Christian Schallercommiting Leifs registry to /var/cache patch, works...
2002-11-27 Wim Taymans- Added first attempt at general caching mechanism...
2002-11-02 Wim TaymansAdded padprobe to makefile
2002-08-13 Thomas Vander Stichelefixing recursive make problem and nonscrdir builds
2002-07-31 Thomas Vander Stichelemake dist fix
2002-07-28 Thomas Vander Stichelethis triggers a regen of the autogenned source files
2002-07-28 Wim TaymansMake the formats dynamic so that plugins can register...
2002-07-24 Wim TaymansFixed the missing .h file and some reorg (not sure...
2002-07-24 Andy Wingoadd default bufferpool, clean up some code, add bufferp...
2002-07-08 Wim Taymans- Removed bufferpool code and move that to gstbuffer.c
2002-06-22 Thomas Vander Sticheleas promised, the header changes and some of wingo's...
2002-06-21 Wim TaymansAdded a runtime option to use a dummy threading impleme...
2002-06-16 David I. Lehnauto build some enum code.
next