]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/gstreamer0-10.git/history - gst/elements/gstidentity.c
gst-indent run on core
[glsdk/gstreamer0-10.git] / gst / elements / gstidentity.c
2004-03-13 Thomas Vander Stichelegst-indent run on core
2004-02-03 Benjamin Ottegst/: get rid of gstmarshal.h dependency. It's not...
2004-01-31 Thomas Vander Stichelesuffix errors with period.
2004-01-30 Benjamin Otteparts of the patch submitted in bug #113913
2004-01-29 Thomas Vander SticheleGST_ELEMENT_ERROR
2004-01-18 Thomas Vander Stichelechanging error signal add error codes and domains
2004-01-08 Benjamin Ottegst/gstutils.h: GST_PARENT_CALL and
2004-01-01 David SchleefNegotiation fixes
2003-12-22 David SchleefMerge CAPS branch
2003-11-13 David SchleefChange G_TYPE_POINTER to the appropriate type in g_sign...
2003-10-31 Benjamin Otteupdate plugin initialization restructuring (see email...
2003-10-08 Andy Wingos/GstBuffer/GstData/ in the API where you can pass...
2003-09-16 Thomas Vander Stichelereverting error patches before making a branch.
2003-09-14 Benjamin Otteimplement translatable error messages using gerror.
2003-06-29 Benjamin OtteGST_DEBUG reorganization containing loads of stuff:
2003-04-17 Wim Taymans- Added a property to perform caps negotiation in the...
2003-02-01 David SchleefConvert %lld and %llu in printf formats to G_G[U]INT64_...
2003-01-09 David I. Lehnmore connect -> link updates
2003-01-09 Thomas Vander Stichelecode cleanups and further deprecation fixes
2003-01-09 Thomas Vander Stichelefirst pass of connect->link gst-plugins and other stuff...
2003-01-08 Wim TaymansProvide intrastructure to not have to pass NULL buffers...
2002-12-15 Wim TaymansFix silent property
2002-09-29 Andy Wingoadding ::license field to core plugins
2002-09-10 Ronald S. BultjeThis changes an important part of the plugin API, gst_p...
2002-09-08 Christian Schallercommitting many nice little memleaks fixes from Iain...
2002-05-20 Andy Wingoadd gerror to gstplugin.c -- not fully propagated to...
2002-04-20 Andy Wingoa hack to work around intltool's brokenness a current...
2002-04-14 Steve BakerARG_ERROR_AFTER is an int
2002-04-03 Wim TaymansGST_DEBUG and _INFO should have no trailing \n
2002-03-31 Wim TaymansDocumentation updates
2002-02-19 Andy Wingochanges to spider: add padtemplates so the connect...
2002-02-17 Andy Wingocapsnego fixes in adder, speed, and identity
2002-02-17 Andy Wingoconvert identity to g_object_notify stuff i hate last...
2002-01-13 Wim TaymansLanded the new improved capsnegotiation system.
2002-01-01 Wim TaymansSome small cleanups. added a drop_probaility arg to...
2001-12-27 Wim TaymansAdded a property to make identity fail after N buffers
2001-12-22 Wim TaymansThis is an attempt at not segfaulting on errors but...
2001-08-13 Steve Bakersync with the current CVS glib API
2001-07-11 Wim TaymansSome cleanups in output of various test plugins.
2001-07-11 Wim TaymansAdded DEBUG_FUNCPTR to most plugins.
2001-07-11 Wim TaymansSome code cleanups.
2001-06-25 Erik WalthinsenMerged from GOBJECT1 to HEAD at 200106241
2001-05-27 Erik WalthinsenAdded some caps != NULL checks.
2001-04-20 Wim TaymansAdded caps proxying and bufferpool passing to identity...
2001-01-29 Wim TaymansThis is a megapatch with the following changes:
2001-01-14 Wim TaymansAdded an extra signal_cond to queue to make sure that...
2001-01-07 Wim TaymansAdded sleep time to identity
2000-12-29 Erik WalthinsenUpdated copyright notices.
2000-12-29 Erik WalthinsenReparented everything to GstElement, removing GstSrc...
2000-12-26 Erik WalthinsenMore massive changes to the scheduling system. Moved...
2000-12-23 Wim TaymansAdded handoff signals to fakesrc and fakesink
2000-12-22 Wim TaymansImplemented some test cases... they all fail :-(
2000-12-16 Erik WalthinsenWARNING: Don't grab this updated unless you're really...
2000-11-25 Wim TaymansCode Cleanups
2000-03-27 Wim TaymansDocumentation updates. All standard library objects...
2000-02-27 Wim TaymansThis is a rather large patch. Switched on -Wall compile...
2000-01-30 Erik Walthinseninitial checkin