]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/gstreamer0-10.git/history - gst/gstbin.c
gst/gstbin.c: Some documentation updates.
[glsdk/gstreamer0-10.git] / gst / gstbin.c
2005-09-28 Wim Taymansgst/gstbin.c: Some documentation updates.
2005-09-27 Thomas Vander Stichelegst/: remove now useless and leaky resurrection code...
2005-09-27 Wim Taymansdocs/design/part-TODO.txt: Update TODO.
2005-09-27 Wim Taymanscheck/gst/gstbin.c: Enable check that works now.
2005-09-27 Wim Taymansgst/gstbin.c: use gst_object_has_ancestor().
2005-09-26 Wim Taymansgst/gstbin.c: Make state change function use 3 queues...
2005-09-24 Wim TaymansVarious documentation updates.
2005-09-23 Tim-Philipp Müllercheck/gst/gstbin.c: Added test to check state change...
2005-09-22 Wim Taymansgst/gstbin.c: Some more debug info.
2005-09-20 Stefan Kostmore docs inlined, splitted gstindex.{c,h}
2005-09-02 Andy Wingogst/gstelement.h (GstState): Renamed from GstElementSta...
2005-08-25 Wim Taymansgst/gstbin.c: Be a bit more conservative about the...
2005-08-25 Jan SchmidtRevert unpopular change for GST_MESSAGE_SRC to GObject.
2005-08-24 Stefan Kostadded miissing classes and symbols (123 more to go...
2005-08-24 Jan Schmidtdocs/pwg/advanced-types.xml: Well done to Michael for...
2005-08-24 Jan SchmidtChange GST_MESSAGE_SRC to be a GObject rather than...
2005-08-23 Stefan Kostinlined more doc comments, added missing comments and...
2005-08-22 Stefan Kostported gstchildproxy over from 0.8 ported gst-inspect...
2005-08-21 Thomas Vander Stichelecheck/Makefile.am: clean up environment for when regist...
2005-08-17 Andy Wingogst/base/gstbasetransform.c: Debug changes.
2005-08-16 Wim Taymanscheck/gst/gstvalue.c: Added subtract checks.
2005-08-08 Ronald S. Bultjegst/gstbin.c: Use gst_element_post_message() instead.
2005-08-08 Ronald S. Bultjegst/gstbin.c: Make default message forwarding from...
2005-07-29 Wim Taymansdocs/design/part-gstghostpad.txt: Small update.
2005-07-28 Wim Taymanscheck/gst/gstbin.c: Added checks for hierarchy consiste...
2005-07-28 Wim Taymanscheck/gst/gstghostpad.c: Added some more tests for...
2005-07-18 Jan Schmidtgst/base/gstbasesrc.c: Send discont event from the...
2005-07-18 Wim TaymansRemoved plugable schedulers.
2005-07-16 Wim Taymansgst/base/gstbasesink.*: Store and use discont values...
2005-07-09 Thomas Vander Sticheledon't get src for all messages; only for eos
2005-07-09 Thomas Vander Stichelecheck/gst/gstbin.c: add more things to check
2005-07-09 Thomas Vander Stichelecheck/gst/gstbin.c: add test for state change message...
2005-07-06 Jan Schmidtexamples/: Update a couple of the examples to work...
2005-06-30 Wim Taymansgst/gstbin.c: Lame attempt at making the state change...
2005-06-28 Andy Wingo*.c: Don't cast to GST_OBJECT when reffing or unreffing...
2005-06-27 Wim Taymansgst/gstbin.c: Cleanup the get_state() function a little...
2005-06-27 Thomas Vander Stichelemore doc and whitespace fixes
2005-06-23 Wim TaymansAdded support for live sources and other elements that...
2005-06-08 Andy Wingogst/gstutils.c: RPAD fixes all around.
2005-05-25 Wim Taymansgst/: Fix state changes for non sinks. We now change...
2005-05-18 Ronald S. Bultjegst/gstbin.c: Fix clock settery in bins when adding...
2005-05-16 Andy Wingogst/gstbin.c (sink_iterator_filter): Err... um...
2005-05-14 Andy Wingogst/gstbin.c (gst_bin_iterate_sinks): Use sink_iterator...
2005-05-14 Andy Wingogst/gstbin.c (gst_bin_change_state): Fix state changes...
2005-05-12 Wim Taymansgst/: Identify sinks by their flag to avoid overly...
2005-05-12 Ronald S. Bultjegst/gstbin.c: Implement _query on a bin, similar to...
2005-05-12 Wim Taymansgst/gstbin.c: Same fix as Ronald's but without the...
2005-05-12 Ronald S. Bultjegst/gstbin.c: If a child is removed from a bin while...
2005-05-11 Andy Wingogst/elements/gstfakesink.c (gst_fakesink_render): Er...
2005-05-05 Wim Taymansgst/: Fix name lookup in GstBin.
2005-05-04 Andy WingoGCC 4 fixen.
2005-03-28 Wim TaymansAdded state change code.
2005-03-25 Ronald S. Bultjegst/gstbin.c: Add default event/set_manager handlers...
2005-03-21 Wim TaymansNext big merge.
2005-03-10 Wim TaymansDoc updates.
2005-03-09 Wim TaymansAdded GstBin test.
2005-03-09 Wim TaymansBump version number, we're now 0.9.0
2005-03-08 Wim TaymansDocs updates, clean up some headers.
2005-03-07 Wim TaymansFirst THREADED backport attempt, focusing on adding...
2005-01-31 Ronald S. Bultjegst/gstbin.c: Explicitely make an element release locks...
2005-01-31 Ronald S. Bultjegst/gstbin.c: Remove a piece of code that could never...
2005-01-31 Ronald S. Bultjedocs/pwg/advanced-types.xml: Fix description for buffer...
2004-12-21 Thomas Vander SticheleFix for #159852 - make iterate emission threadsafe
2004-11-22 Martin Sotogst/gstqueue.c (gst_queue_init, gst_queue_link_sink)
2004-11-02 Wim Taymansgst/: Aplied part of patch #157127: Cleanup of issues...
2004-10-13 Stefan Kostmore api documentation better error signaling and logging
2004-10-09 Ronald S. Bultjegst/gstbin.c: Add missing break.
2004-08-03 Wim Taymansgst/: Backported some debug logging from a reverted...
2004-07-29 Thomas Vander Stichelerevert state change changes as agreed so we can rework...
2004-07-28 Brian CameronCorrecting some debug messages so that they don't core...
2004-07-28 Wim Taymansgst/: Make sure that a bin state change tries to keep...
2004-07-21 Benjamin Ottegst/gstbin.c: make state changes work correctly and...
2004-07-12 Benjamin Ottegst/gstelement.c: virutalize gst_element_set_state...
2004-07-11 Andy Wingogst/gstbin.c (gst_bin_add_func): If we're adding an...
2004-07-11 Andy Wingogst/gstbin.c (gst_bin_foreach): New static function...
2004-07-09 Wim Taymansgst/: Since remove is virtual in GstBin we must not...
2004-07-09 Thomas Vander Sticheledebugging fixes
2004-07-09 Thomas Vander Stichelefixes 123774 - setting state on a bin should set state...
2004-07-09 Thomas Vander Sticheledebug
2004-07-04 Thomas Vander Stichelechain bin restore to parent method
2004-06-12 Steve LhommeSomehow a clean fix to the semi-private export
2004-06-12 Steve LhommeFix a bug to enable/disable DEBUG under MSVC
2004-05-18 Benjamin Ottegst/gstbin.c: don't
2004-05-11 Benjamin Ottegst/elements/gstfilesrc.c: compute mapsize correctly
2004-05-06 Benjamin Ottegst/elements/gstfilesrc.*: send NEW_MEDIA events correctly
2004-05-03 Benjamin Ottegst/gstbin.c: better debugging
2004-04-20 Benjamin Ottegst/autoplug/gstspider.c: improve debugging messages
2004-04-09 Benjamin Ottegst/: don't use memchunks for these objects, use malloc...
2004-03-28 Benjamin Ottegst/gstbin.c: don't add decoupled elements to scheduler...
2004-03-26 David Schleefdocs/gst/gstreamer-sections.txt: More doc hacking.
2004-03-15 Thomas Vander Sticheledon't mix tabs and spaces
2004-03-13 Thomas Vander Stichelegst-indent run on core
2004-03-09 Thomas Vander Stichelebetter debug info
2004-03-07 Andy Wingogst/gstbin.c (gst_bin_remove): Debugging fixes.
2004-03-04 Thomas Vander Stichelemake signals use dashes in the names
2004-02-24 Thomas Vander Sticheleadding error to gstbin.c
2004-02-20 Andy Wingogst/: Debugging tweaks.
2004-02-15 Julien Mouttegst/gstbin.c: Fix a big bug that was breaking pipelines...
2004-02-05 Andy Wingogst/gstpad.c (_gst_real_pad_fixate_accumulator): s...
2004-02-03 Benjamin Ottegst/: get rid of gstmarshal.h dependency. It's not...
next