ignore these test code
[glsdk/gstreamer0-10.git] / gst / gstelement.c
2003-09-11 Thomas Vander Sticheleignore these test code
2003-08-04 Ronald S. BultjeImplement simple seek API. This can later be extended...
2003-07-16 Andy Wingosome formatting and doc fixes, and make gstdebug output...
2003-06-29 Benjamin OtteGST_DEBUG reorganization containing loads of stuff:
2003-06-07 Thomas Vander Sticheledon't recursively call gst_bin_set_state on failure...
2003-06-07 Thomas Vander Stichelefix color for NULL from bright white to blue
2003-06-03 Wim Taymans- added GST_ELEMENT_ERROR flag to mark elements in...
2003-05-17 Thomas Vander Sticheleclock debug addition
2003-05-17 Benjamin Ottefix wrong debug message to print the right thing
2003-05-06 Benjamin Otteimplement proper refcounting of pad's templates and...
2003-05-02 Benjamin Ottemake gst-launch --gst-mask=-1 fakesrc ! fakesink work...
2003-04-26 Wim Taymans- remove some \n in GstThread debugging
2003-04-21 Benjamin Ottemake that error message more useful, it kept confusing me
2003-04-19 Wim TaymansGST_DEBUG/INFO doesn't need a \n at the end.
2003-04-18 Benjamin Ottemake EOS really recursive and not just one layer deep
2003-04-17 Wim Taymans- don't be rude but give informative message about...
2003-04-17 Benjamin OtteIt's absolute fun if you don't find this. If an element...
2003-04-13 Benjamin Ottesilence compiler warning
2003-04-12 Benjamin Ottesignal EOS on parent bins, when the last element playin...
2003-04-11 Benjamin Ottegeneral fixes:
2003-04-08 Benjamin Ottehuge modifications, hope i didn't break something:
2003-02-11 Wim Taymans- fix gst_element_unlink, only unlink pads that belong...
2003-02-10 Wim Taymans- Add more --disable options
2003-02-03 Wim TaymansOnly inform scheduler when the element changes scheduli...
2003-02-02 Wim Taymansgst_object_swap -> gst_object_replace as it's a better...
2003-01-23 Wim TaymansSome extra debug statement
2003-01-17 Wim Taymans- properly ref/unref scheduler and clock in gstelement
2003-01-11 Wim Taymans- return boolean in _interrupt to better inform element
2003-01-09 David I. Lehnmore connect -> link updates
2003-01-09 Thomas Vander Stichelecode cleanups and further deprecation fixes
2003-01-09 Thomas Vander Stichelefirst pass of connect->link gst-plugins and other stuff...
2003-01-01 Wim Taymans- Remove annoying \n from cothread INFO/DEBUG messages
2003-01-01 Wim Taymans- Added PAD_NEGOTIATING flag, remove PAD_EOS flag
2002-12-31 Wim TaymansIS_USABLE is only for PLAYING elements
2002-12-31 Wim TaymansNegotiation can happen even on disabled pads (in READY...
2002-12-31 Wim Taymans- Fix PAD_IS_USABLE on ghostpads
2002-12-31 Thomas Vander Stichelerevert usability test
2002-12-31 Thomas Vander Stichelesome more debug output
2002-12-30 Wim Taymans- major API breakage (one of the last, I promise...)
2002-12-27 Wim Taymans- disable pads when going to PAUSED, we want to make...
2002-12-19 Wim Taymans- Cleanups
2002-12-15 Wim TaymansImprove the optimal scheduler, mainly element remove...
2002-12-14 Wim TaymansDocumentation updates
2002-12-12 Wim TaymansRenamed GstCache to GstIndex
2002-12-11 Thomas Vander Stichelemerge from release branch
2002-12-07 Thomas Vander Stichelemove these to macros
2002-11-27 Wim Taymans- Added first attempt at general caching mechanism...
2002-11-20 Wim TaymansUse full object path string in default error/notify...
2002-11-19 Wim Taymans- an element also has a failed state change if the...
2002-11-02 Wim TaymansMoved deep notify to GstObject
2002-10-29 Thomas Vander Sticheleinstigated by alp. If this is wrong, let us know.
2002-10-02 Thomas Vander Stichelecode cleanup and API change (gst_caps_check_compatibili...
2002-10-01 Thomas Vander Stichelecode cleanup and more debug output
2002-09-13 Wim Taymans- some cleanups
2002-09-12 Wim Taymans- Make the return GList of gst_element_get_pad_list...
2002-09-08 Christian Schallercommitting many nice little memleaks fixes from Iain...
2002-09-02 Andy Wingodon't pass pointers to automatic variables
2002-08-30 Thomas Vander Stichelecode cleanups and doc fixes
2002-08-12 Thomas Vander Stichelefixes bug bugzilla.gnome.org/show_bug.cgi?id=90333...
2002-08-12 Thomas Vander Stichelefixes bug bugzilla.gnome.org/show_bug.cgi?id=90332
2002-07-30 Wim TaymansAdd default deep_notify and error signal callbacks...
2002-07-28 Wim Taymans- move the state_change signal emit to a better place...
2002-07-24 Wim Taymans- More element API docs.
2002-07-08 Wim Taymans- Removed bufferpool code and move that to gstbuffer.c
2002-07-05 Andy Wingoif you can't write to the registry (ie it is root-owned...
2002-06-12 Wim TaymansDocumentation updates
2002-06-08 Wim TaymansAdded element query
2002-06-05 Wim TaymansFix the case where one of the pads is a ghostpad.
2002-05-30 Wim TaymansCreated an overridable method for seeking on an element...
2002-05-27 Andy Wingofixups in the prop view/controller compilation fixes...
2002-05-26 Wim Taymans- The clock_wait now returns the difference between...
2002-05-26 Andy Wingoget rid of some debug printouts
2002-05-26 Andy Wingoimplemented threadsafe property set/get system as discu...
2002-05-25 Thomas Vander SticheleAPI cleanup: (s/g)et_sched -> _scheduler
2002-05-05 Andy Wingouse contents of GST_REGISTRY variable if --gst-registry...
2002-05-01 Wim TaymansSmall cleanups
2002-04-28 Wim TaymansAdded method for releasing request pads.
2002-04-23 Thomas Vander Sticheledoc fixes
2002-04-23 Thomas Vander Sticheleapi renaming
2002-04-23 Thomas Vander Sticheledoc changes
2002-04-23 Thomas Vander Stichelecode cleanup
2002-04-12 Andy Wingofeeble attempts to handle dynamic connections
2002-04-11 Andy Wingocommit to make gstreamer follow the gtk function/macro...
2002-04-07 Andy Wingonew parser that uses flex and bison
2002-04-03 Wim TaymansGST_DEBUG and _INFO should have no trailing \n
2002-03-31 Wim TaymansDocumentation updates
2002-03-30 Andy Wingoadd notify back to filesrc, it's needed for MVC applica...
2002-03-30 Wim Taymans- Remove the propsprivate header file
2002-03-24 Andy Wingofilter newlines out of GST_DEBUG statements to reflect...
2002-03-24 David I. Lehns/POINTER/OBJECT/ in g_signal_new for NEW_PAD and PAD_R...
2002-03-18 Andy Wingos/gst_element_install_std_props/gst_element_class_insta...
2002-03-18 Benjamin Ottebugfix for gst_element_request_pad_by_name returning...
2002-03-06 Andy Wingofix bug when requesting pads by name
2002-03-03 Andy Wingodocument gst_caps_debug change gst_caps_debug to accept...
2002-02-21 Andy Wingoadd two apis: gst_element_connect_elements_many (elem1...
2002-02-20 Andy Wingowarning fixes gst_object_set_name (name, NULL) uniquifi...
2002-02-19 Andy Wingochanges to spider: add padtemplates so the connect...
2002-02-18 Andy Wingomany fixes related to dynamic pipelines.
2002-02-17 Andy Wingosome object cleanup fixes
2002-02-06 Wim TaymansSmall cleanups
next