]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/gstreamer0-10.git/history - gst/gstelement.h
gstelement: add gst_element_class_add_pad_template_from_static
[glsdk/gstreamer0-10.git] / gst / gstelement.h
2011-11-28 Vincent Penquerc'hgstelement: add gst_element_class_add_pad_template_from...
2011-11-08 Tim-Philipp Müllerdocs: fix Since: markers for API added after 0.10.35
2011-08-15 Josep Torragststate: explicitly cast to the enum type
2011-06-18 Tim-Philipp MüllerBump git version after unplanned 0.10.35 release
2011-06-14 Javier JardónUse "const" instead G_CONST_RETURN
2011-06-09 Javier JardónUse "const" instead G_CONST_RETURN
2011-05-28 Stefan Kostdocs: xrefs more api around GstStateChange and GstState...
2011-05-14 Tim-Philipp Müllerdocs: fix up some Since markers and update for new...
2011-05-14 Sebastian Drögeelement: Add GstElement::state_changed vfunc
2011-05-03 Stefan Kostdocs: add two trivial doc blobs
2011-03-22 Thiago Santosgstelement: Fix typo in the docs
2011-01-05 Edward HerveyGstElement: Add a more flexible way to get request...
2010-12-07 Tim-Philipp Müllerdocs: gst: more gobject introspection annotations
2010-10-11 Wim Taymanselement: add IS_SOURCE flag
2010-09-06 Stefan Kostelement-details: allow for arbitrary element details
2010-06-15 Benjamin Gaignardelement: Improve gst_element_get_name() docs
2010-03-24 Benjamin OtteDeprecated gst_element_class_set_details()
2010-03-17 Mart Raudseppdocs: fix typo
2009-12-14 Stefan Kostdocs: add more docs around GstState and GstStateChange
2009-09-09 David SchleefFix typo in inline documentation
2009-08-28 Wim Taymanselement; whitespace fixes
2009-05-29 Wim Taymanselement: add start_time field an methods
2009-05-21 Wim Taymansdocs: update docs for stream_time->running_time
2009-05-14 Wim Taymanselement: add gst_element_lost_state_full()
2008-07-25 Thijs Vermeirgst/gstelement.h: Fix link in documentation.
2008-05-29 Sebastian Drögegst/gstelement.*: Deprecated gst_element_get_pad()...
2007-08-02 Tim-Philipp Müllergst/gstelement.*: Make strings passed to gst_element_cl...
2007-06-23 Thomas Vander Stichele80 line fix
2007-06-21 Stefan KostSaving relocations for GTypeInfo and GstElementDetails...
2007-03-19 Wim Taymansdocs/gst/gstreamer-sections.txt: Add new element field...
2007-02-28 Wim Taymansgst/gstelement.*: Improve docs a little. Added Since...
2007-02-21 Thomas Vander SticheleFix up documentation to link to the correct GstGError...
2007-01-09 Wim Taymansdocs/design/draft-latency.txt: Updates.
2006-10-16 Tim-Philipp Müllergst/gstelement.h: Add casts to the correct return type...
2006-10-13 Yves Lefebvregst/gstelement.h: Clarify _NO_PREROLL a bit more.
2006-10-08 Tim-Philipp Müllergst/gstelement.h: gcc versions prior to gcc 3.3 apparen...
2006-10-05 Tim-Philipp MüllerAdd GST_USING_PRINTF_EXTENSION to gstconfig.h so that...
2006-06-06 Thomas Vander Stichelewhitespace/width fixes
2005-11-29 Andy Wingogst/gstevent.h (struct _GstEvent): Only one pointer...
2005-11-22 Wim Taymansgst/base/gstbasesink.*: No need to store the clock...
2005-11-21 Andy Wingo*.*: Ran scripts/update-macros. Oh yes. gst/gstobject...
2005-11-19 Andy Wingogst/gstutils.h: gst/gstutils.c (g_static_rec_cond_wait)
2005-11-10 Wim TaymansFix docs, move some STATE macros to private.
2005-11-08 Wim Taymansgst/: Avoid excessive typechecking in macros.
2005-10-24 Michael SmithFix some minor documentation typos
2005-10-21 Wim TaymansAnd 2% more doc coverage.
2005-10-18 Wim Taymanscheck/: Small state change torture test.
2005-10-18 Wim Taymansgst/: Pending ABI changes.
2005-10-17 Stefan Kostadd new api entries hide internal macro
2005-10-15 Thomas Vander Stichelegst/gst.*: remove _gst_registry_auto_load, not used...
2005-10-12 Stefan Kostrenamed GST_FLAGS macros to GST_OBJECT_FLAGS moved...
2005-10-12 Wim TaymansUse GstClockTime in _get_state() instead of GTimeVal.
2005-10-10 Wim Taymanscheck/: Check fixes, use API as stated in design docs...
2005-10-10 Andy Wingogst/gstelement.c (gst_element_init, gst_element_finaliz...
2005-10-08 Wim Taymansgst/base/gstbasesink.c: Better log message.
2005-10-05 Thomas Vander Sticheledoc updates
2005-09-28 Wim Taymansgst/gstbin.c: Small doc fixes. get_clock -> provide_clock.
2005-09-27 Stefan Kostadded two new functions to the docs documents all undoc...
2005-09-27 Wim Taymansdocs/design/part-TODO.txt: Update TODO.
2005-09-27 Wim Taymanscheck/gst/gstbin.c: Enable check that works now.
2005-09-23 Thomas Vander Stichelefix docs
2005-09-23 Stefan Kostinlined 3 more biiiig doc files and added some missing...
2005-09-22 Wim Taymansgst/gstbin.c: Some more debug info.
2005-09-20 Stefan Kostmore docs inlined, splitted gstindex.{c,h}
2005-09-11 Thomas Vander Stichelevarious doc fixes
2005-09-07 Stefan Kostrenamed gsttag -> gsttaglist, gsttaginterface -> gsttag...
2005-09-02 Andy Wingogst/gstelement.h: Add magical pixie dust to make glib...
2005-09-02 Andy Wingogst/gstelement.h (GstState): Renamed from GstElementSta...
2005-08-24 Jan Schmidtdocs/pwg/advanced-types.xml: Well done to Michael for...
2005-08-20 Thomas Vander Stichelemake GST_ELEMENT_ERROR not do GST_ERROR_OBJECT - these...
2005-07-27 Wim TaymansSome docs updates
2005-07-20 Ronald S. BultjeGstElement::new-pad -> pad-added, GstElement::state...
2005-07-18 Wim TaymansRemoved plugable schedulers.
2005-07-16 Wim Taymansgst/base/gstbasesink.*: Store and use discont values...
2005-06-29 Thomas Vander Sticheledoc fixes
2005-06-27 Andy Wingogst/base/gsttypefindhelper.c (gst_type_find_helper...
2005-06-27 Thomas Vander Stichelemore doc and whitespace fixes
2005-06-25 Wim Taymansgst/: Keep track of current target state while performi...
2005-06-23 Wim TaymansAdded support for live sources and other elements that...
2005-06-08 Andy Wingogst/gstutils.c: RPAD fixes all around.
2005-05-30 Wim Taymansgst/: Move elementfactory methods to separate .h file.
2005-05-12 Wim Taymansgst/: Identify sinks by their flag to avoid overly...
2005-05-09 Wim TaymansRemove old query functions. Ported old code.
2005-04-12 Ronald S. BultjeUse libxml2 for registry parsing, use staticpadtemplate...
2005-03-21 Wim TaymansNext big merge.
2005-03-09 Wim TaymansAdded GstBin test.
2005-03-09 Wim TaymansBump version number, we're now 0.9.0
2005-03-08 Wim TaymansRemove threadsafe properties. Fix elements because...
2005-03-08 Wim TaymansDocs updates, clean up some headers.
2005-03-07 Wim TaymansFirst THREADED backport attempt, focusing on adding...
2005-01-24 Stefan Kostinstall style.css along with docs fixing incomplete...
2004-07-15 Benjamin Ottegst/gstelement.h: Don't GST_ERROR_OBJECT smpty strings...
2004-06-22 Benjamin Ottegst/gstelement.h: remove define that referenced a nonex...
2004-06-13 Steve Lhommerename GSTREAMER_EXPORT to GST_EXPORT
2004-06-12 Steve LhommeFix a bug to enable/disable DEBUG under MSVC
2004-05-10 Benjamin Ottegst/gstelement.*: add gst_element_no_more_pads and...
2004-03-30 David Schleefdocs/gst/Makefile.am: Disable a bunch of headers from...
2004-03-28 Martin Sotogst/gstelement.*: New function for setting element...
2004-03-15 Johan DahlinRevert again, this time without post-commit reindent...
2004-03-15 Johan Dahlin*.h: Revert indentation changes.
next