]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/gstreamer0-10.git/history - gst/gstpad.c
pad: Remove g_warning() if pad accepted caps that are not a subset of the pad caps
[glsdk/gstreamer0-10.git] / gst / gstpad.c
2011-11-24 Sebastian Drögepad: Remove g_warning() if pad accepted caps that are...
2011-10-20 Stefan Sauerpad: not only describe conditions in the docs, also...
2011-10-07 Robert SwainGST_PTR_FORMAT: Add GstBuffer ptr format and use in...
2011-09-19 Stas Sergeevpad: Set caps on pad before checking if the pad is...
2011-09-16 Tim-Philipp Müllerpad: add more debug logging for other chain function...
2011-09-16 Tim-Philipp Müllerpad: fix up printf format in debug message
2011-09-16 Vincent Penquerc'hpad: make some debug traces more useful
2011-09-09 Sebastian Drögepad: Only do the subset check in gst_pad_accept_caps...
2011-09-08 Sebastian DrögeRevert "pad: Use gst_pad_accept_caps() instead of manua...
2011-09-08 Sebastian Drögepad: Use gst_pad_accept_caps() instead of manually...
2011-09-08 Sebastian Drögepad: Print a g_warning() if pad accept caps that are...
2011-09-08 Sebastian DrögeRevert "pad: Check for subsets, not non-empty intersect...
2011-09-07 Piotr Fusikdocs, gst: typo fixes
2011-09-06 Sebastian Drögepad: Check for subsets, not non-empty intersections...
2011-08-26 Josep Torrapad: explicitly cast to the enum type
2011-06-18 Tim-Philipp MüllerBump git version after unplanned 0.10.35 release
2011-06-14 Javier JardónUse "const" instead G_CONST_RETURN
2011-06-09 Javier JardónUse "const" instead G_CONST_RETURN
2011-05-18 Stefan Kostdocs: add deprecation guards
2011-05-14 Sebastian Drögepad: Remove unnecessary FIXME
2011-04-19 Havard Graffpad: unlock before freeing the cache to avoid deadlock
2011-04-11 Robert Swainpad: Allow tracking of buffers in GST_SCHEDULING debug...
2011-03-16 Sebastian Drögepad: Document that pad blocks only make sense for sink...
2011-02-14 Wim Taymanspad: Check sinkpad for flushing
2010-12-26 Tim-Philipp MüllerRevert "micro-optim: if (x) is cheaper than if (x ...
2010-12-17 Edward Herveygst: documentation fixups and annotation
2010-12-07 Tim-Philipp Müllerdocs: gst: more gobject introspection annotations
2010-12-07 Tim-Philipp Müllerpad: register gst_pad_get_fixed_caps_func() with the...
2010-12-06 Mark Nauwelaertspad: add some debug to fast push path
2010-12-03 Edward Herveymicro-optim: if (x) is cheaper than if (x > 0) for...
2010-12-03 Wim Taymanspad: add push cache to bufferlists
2010-12-03 Wim Taymanspad: don't cache the peer chainfunc
2010-12-03 Wim Taymanspad: clear pad cache when installing probes
2010-12-03 Wim Taymanspad: explicitly inline some functions
2010-12-03 Wim Taymanspad: remove unused variable
2010-12-03 Wim Taymanspad: invalidate caches on flush and pad block
2010-12-03 Wim Taymanspad: don't unref NULL caps
2010-12-03 Wim Taymanspad: add invalidate function
2010-12-03 Wim Taymanspad: small cleanup
2010-12-03 Wim Taymanspad: improve pad push caching
2010-12-03 Wim Taymanspad: prototype of pad push cache
2010-12-03 Stefan Kostdocs: query doc improvements
2010-12-02 Sebastian Drögepad: Set the event source object if none is set yet...
2010-10-07 Tim-Philipp Müllerpads: use new g_object_notify_by_pspec() for caps notif...
2010-09-23 Stefan KostRevert "pad: use a nested lock to avoid reffing the...
2010-09-22 Stefan Kostpad: use a nested lock to avoid reffing the peer
2010-09-13 Thiago Santosgstpad: Fix flush-stop event handling
2010-09-13 Stefan Kostdocs: fix warnings pointed out by gtk-doc
2010-09-08 Stefan Kostpad: add a unchecked variant for pull
2010-08-05 Stefan Kostpad: log element:pad names with caps
2010-07-20 Edward Herveygstpad: Assume pads are compatible if we don't have...
2010-07-16 Edward HerveyGstPad: Do not call gst_pad_accept_caps() when caps...
2010-06-26 Tim-Philipp MüllerDon't include <libxml/parser.h> from public headers...
2010-06-25 Edward Herveypad: more documentation regarding the new flags
2010-06-25 Sebastian Drögegstxml: Deprecate GstXml and related functions
2010-06-23 Edward HerveyGstPad: Add new pad linking method with configurable...
2010-06-15 Edward HerveyRevert "GstPad: Add GST_PAD_NEGOTIABLE GstPadFlag"
2010-06-15 Edward HerveyRevert "gstpad: Return pad template in get_caps if...
2010-06-15 Edward HerveyRevert "pad: fix comment"
2010-06-14 Wim Taymanspad: fix comment
2010-06-14 Edward Herveygstpad: Return pad template in get_caps if pad is not...
2010-06-14 Edward HerveyGstPad: Add GST_PAD_NEGOTIABLE GstPadFlag
2010-06-13 Sebastian Drögepad: Fix iterator aggregation of all pads in the intern...
2010-06-01 Stefan Kostpads: Improve readability for gst_pad_fixate_caps()
2010-05-22 Stefan Kostdocs: xref function name
2010-05-17 Tim-Philipp Müllerpad: don't print WARNING debug statements for normal...
2010-05-06 Wim TaymansRevert "pad: don't check twice for changed caps per...
2010-05-06 Stefan Kostpad: don't check twice for changed caps per push
2010-05-05 Wim Taymansdocs: clarify the pull_range functions
2010-04-29 Benjamin Ottecaps: Do not allow fixating empty caps
2010-03-28 Sebastian Drögegst: Use GSlice instead of normal g_malloc in more...
2010-03-15 Wim Taymanspad: set a good name on the task of the pad
2010-03-11 Benjamin OtteFixes for -Wmissing-declarations -Wmissing-prototypes
2010-02-15 Tim-Philipp Müllerpad: don't print WARN debug statements for normal thing...
2010-01-19 Thijs Vermeirgstpad: directly set the caps when pushing buffer with...
2009-12-24 Wim Taymansavoid some more type checks
2009-12-23 Wim Taymanspad: Fix problem with destroy callback not being called
2009-12-01 Edward Herveygstpad: Only register debug funcptr once.
2009-11-25 Stefan Kostdocs: fix xrefs in docs
2009-11-05 Stefan Kostpad: rename new api from _refed to _reffed.
2009-10-28 Rob Clarkpad: make _fixate_caps() also truncate when needed
2009-10-28 Tim-Philipp MüllerRemove GST_DEBUG_FUNCPTR where they're pointless
2009-10-07 Tim-Philipp Müllerdocs: fix Since: tags in docs for newly-added API
2009-10-07 Stefan Kostpad: add variants of gst_pad_get_caps() that don't...
2009-10-06 Tim-Philipp Müllergst: remove more unnecessary cast when using g_signal_*()
2009-09-02 Wim Taymansstates: post structure change on sinkpads
2009-08-18 Sebastian Drögegstpad: Add some DISABLE_DEPRECATED markers in the...
2009-08-08 Edward Herveygst: Remove dead assignments
2009-08-06 Stefan Kostpad: use new _caps_can_intersect()
2009-08-06 Stefan Kostpad: use correct variable in test
2009-08-06 Wim Taymanspad: Add some more debugging
2009-06-30 Edward HerveySpread branch prediction macros.
2009-06-30 Edward HerveyUse local variables in for/while loops.
2009-06-29 Wim Taymansbufferlist: use faster gst_buffer_list_get()
2009-06-15 Wim Taymansdebug: add some more debug to element and pads
2009-05-28 Wim Taymanspad: add pad private structure
2009-05-25 Wim Taymanspad: keep task ref before releasing the lock
2009-05-22 Stefan Kostdocs: fix gtk-doc warnings
2009-05-22 Jan Schmidtdocs: Fix up some documentation warnings.
2009-05-20 Hannes Bistryloadsave: fix requestpad handling and serialisation...
next