]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/gstreamer0-10.git/history - gst/gstparse.c
gststructure: clarify _get docs about the returned reference
[glsdk/gstreamer0-10.git] / gst / gstparse.c
2011-11-12 Tim-Philipp Müllergst, controller: replace g_list_prepend + reverse with...
2011-10-08 Tim-Philipp Müllergstparse: prefix generated parser functions so they...
2011-09-07 Piotr Fusikdocs, gst: typo fixes
2011-08-26 Josep Torraparse: use GST_PARSE_FLAG_NONE instead of 0
2011-04-14 Sebastian Drögeparse: Add boxed type for GstParseContext for gobject...
2010-12-07 Tim-Philipp Müllerdocs: gst: more gobject introspection annotations
2010-10-16 Tim-Philipp Müllerdocs: add some gtk-doc Since: markers
2010-08-05 Stefan Kostdocs: more docs for gst_parse_launch and co
2010-03-11 Benjamin OtteFixes for -Wmissing-declarations -Wmissing-prototypes
2008-05-24 Tim-Philipp MüllerAPI: gst_parse_launch_full()
2008-05-22 Tim-Philipp Müllergst/: More guards against bad input; typo fix; some...
2007-12-28 Tim-Philipp Müllergst/: Bunch of gratuitous nano-optimisations.
2007-05-09 Peter Kjellerstedtgst/: Maintain API and ABI when --disable-parse is...
2007-04-18 Marc-Andre Lureaugst/parse/: Make the parser reentrant and recursively...
2006-07-21 Stefan Kostgst/gstparse.c: Also remove reentrance checks if flex...
2006-07-21 Stefan KostOriginal commit message from CVS:
2006-07-21 Wim Taymansgst/gstparse.c: Protect recursive calls to _parse with...
2006-07-20 Stefan Kostgst/gstparse.c: Do not hange on recursive uasge of...
2006-05-04 James AndrewarthaMake sure gstprivate.h and/or config.h are always inclu...
2005-10-20 Wim Taymansgst/: Another 1% more coverage.
2005-10-15 Thomas Vander Stichelevarious style fixes
2005-09-06 Stefan Kostcheck/pipelines/simple_launch_lines.c: test for pipe...
2004-04-21 Benjamin Ottegst/gstparse.c: Free the GString used in _gst_parse_esc...
2004-03-13 Thomas Vander Stichelegst-indent run on core
2003-06-29 Benjamin OtteGST_DEBUG reorganization containing loads of stuff:
2003-04-10 Benjamin Ottedocumentation
2003-04-08 Benjamin Otterewritten pipeline parsing lands. Have fun breaking it.
2003-02-02 Wim Taymans- implement FLOATING flag on caps/props
2003-01-09 Thomas Vander Stichelecode cleanups and further deprecation fixes
2003-01-09 Thomas Vander Stichelefirst pass of connect->link gst-plugins and other stuff...
2002-12-06 Wim TaymansAdded syntax to make filtered connections like: osssrc...
2002-08-31 Andy Wingoadd core elements to the registry pool plugin list...
2002-07-26 Wim TaymansOnly connect dynamic pads if with the right template...
2002-07-08 Wim Taymans- Removed unused locking from the cothreads
2002-06-12 Wim TaymansDocumentation updates
2002-05-01 Wim TaymansSmall cleanups
2002-04-14 Benjamin Ottewe don't use // in code we commit :)
2002-04-14 Wim TaymansThis is all a quick hack...
2002-04-14 Wim TaymansAdded more funky cases
2002-04-14 Wim TaymansMade dynamic pads work for sinkpads with no padtemplate
2002-04-13 Andy Wingoquote spaces in tokens passed to gst_parse_launchv...
2002-04-12 Andy Wingofeeble attempts to handle dynamic connections
2002-04-11 Andy Wingocommit to make gstreamer follow the gtk function/macro...
2002-04-07 Andy Wingonew parser that uses flex and bison
2002-03-24 Andy Wingofilter newlines out of GST_DEBUG statements to reflect...
2002-03-19 Andy Wingoremoval of //-style comments don't link plugins to...
2002-03-04 Andy Wingolet's not increment in GST_DEBUG code...
2002-02-20 Andy Wingowarning fixes gst_object_set_name (name, NULL) uniquifi...
2002-02-02 Wim TaymansMore pointless cleanups
2002-01-18 Andy Wingocleaning up duplicated code in gstbin.c added some...
2002-01-14 Andy Wingofix doc build for glib2 remove template files from...
2002-01-04 Andy Wingofinalize conversion to gst-register
2001-12-22 Wim TaymansThis is an attempt at not segfaulting on errors but...
2001-12-17 Wim TaymansAdded parallel pipeline syntex to the parser. ./gstream...
2001-12-15 Thomas Vander Stichelefix some of uraeus's commenting fixes can someone also...
2001-12-14 Christian Schalleraye ladie, no more ugly // comments here, even if Taaz...
2001-12-12 Wim TaymansSome code cleanups.
2001-12-09 Wim TaymansSet the pipeline to the paused state when doing dynimic...
2001-12-04 wrobell- some fixes to int2float making automake 1.5 happy...
2001-10-27 Steve Bakerreturn a negative error code instead of exiting on...
2001-10-17 Erik Walthinsenmerge from EVENTS1 on 20011016
2001-10-07 Steve Bakerremove ability to set dparams from -launch. this is...
2001-09-22 Steve Bakercrashes that only happen when debugging is on aren...
2001-09-17 Joshua N. Pritikinfix warnings
2001-09-14 Joshua N. Pritikin1. Add more warnings for the gst core only. Various...
2001-09-14 Steve Bakerno reason to lock
2001-09-12 Steve Bakeradded to -launch syntax: if an arg is prefixed with...
2001-08-13 Steve Bakersync with the current CVS glib API
2001-06-29 Richard BoultonAllow elements to be given custom names with [] syntax...
2001-06-25 Erik WalthinsenMerged from GOBJECT1 to HEAD at 200106241
2001-06-15 Wim TaymansChanged a stupid assert in request_pad.
2001-06-15 Steve Bakershould restore dynamic connection of pads (couldn't...
2001-06-10 Steve Bakercan now take comma delimited list of pads. eg gstreamer...
2001-06-09 Steve Bakerstore src and sink pads in slists to get ready for...
2001-06-09 Steve Bakerif a named pad doesn't exist, try creating a new pad...
2001-06-06 Wim TaymansChanged the maxcothreads to 16. connect to the new_ghos...
2001-06-04 Thomas Vander Sticheleadded an eos handler so that gstreamer-launch quits...
2001-05-20 Wim TaymansAdded the possibility to escape chars in gstparse....
2001-05-20 Thomas Vander Stichelereinstated exit(-1) when gstparse.c doesn't find the...
2001-05-03 Erik Walthinsenfixed spelling mistake in user-visible output
2001-05-03 Wim TaymansAdded dynamic pads to the command line parser. ./gstrea...
2001-03-06 Wim TaymansApplied Dominic Ludlam's patch to allow quoted args...
2001-03-03 Wim TaymansAdded a utility function in gstutils to set an object...
2001-01-29 Wim TaymansThis is a megapatch with the following changes:
2001-01-21 Wim TaymansDocs updates
2001-01-20 Erik WalthinsenGot ghostpads to work, even in -launch. Needs more...
2001-01-07 Erik Walthinsenmore leak fixes
2001-01-07 Erik Walthinsenturned -launch capabilities into gst_parse_launch()