2005-09-27 |
Wim Taymans | gst/: Leak fixes, the fold functions need to unref... |
blob | commitdiff | raw |
2005-09-23 |
Thomas Vander Stichele | various doc updates |
blob | commitdiff | raw | diff to current |
2005-09-21 |
Andy Wingo | check/gst/gstutils.c: New file. |
blob | commitdiff | raw | diff to current |
2005-09-21 |
Tim-Philipp Müller | gst/: Don't put functional code in g_return_if_fail... |
blob | commitdiff | raw | diff to current |
2005-09-13 |
Thomas Vander Stichele | gst/gstutils.c: Apparently people think it's better... |
blob | commitdiff | raw | diff to current |
2005-09-12 |
Thomas Vander Stichele | add a gst_element_set_state_async method that sets... |
blob | commitdiff | raw | diff to current |
2005-09-11 |
Thomas Vander Stichele | docs/gst/: rearrange gstvalue section |
blob | commitdiff | raw | diff to current |
2005-09-09 |
Thomas Vander Stichele | check/: adding a test for pipelines and state changes |
blob | commitdiff | raw | diff to current |
2005-09-02 |
Andy Wingo | gst/gstelement.h (GstState): Renamed from GstElementSta... |
blob | commitdiff | raw | diff to current |
2005-09-02 |
Thomas Vander Stichele | gst/: fix a bunch of unchecked return values |
blob | commitdiff | raw | diff to current |
2005-08-31 |
Thomas Vander Stichele | docs/faq/gst-uninstalled: add -good |
blob | commitdiff | raw | diff to current |
2005-08-31 |
Stefan Kost | inlined more docs, fixed double id-ref |
blob | commitdiff | raw | diff to current |
2005-08-30 |
Wim Taymans | gst/base/gstadapter.c: Flushing out 0 bytes is ok for... |
blob | commitdiff | raw | diff to current |
2005-08-29 |
Andy Wingo | gst/gstutils.c (gst_util_uint64_scale): New 3733t funct10n. |
blob | commitdiff | raw | diff to current |
2005-08-25 |
Stefan Kost | gst/gstbin.h: removed ';' from the end of macro defs |
blob | commitdiff | raw | diff to current |
2005-08-24 |
Stefan Kost | added miissing classes and symbols (123 more to go... |
blob | commitdiff | raw | diff to current |
2005-08-17 |
Andy Wingo | gst/base/gstbasetransform.c: Debug changes. |
blob | commitdiff | raw | diff to current |
2005-08-16 |
Ronald S. Bultje | gst/gstutils.*: Add two utility functions for tag handling. |
blob | commitdiff | raw | diff to current |
2005-07-21 |
Wim Taymans | docs/design/part-seeking.txt: Some small additions. |
blob | commitdiff | raw | diff to current |
2005-07-18 |
Wim Taymans | docs/design/: Some more docs in the works. |
blob | commitdiff | raw | diff to current |
2005-07-13 |
Andy Wingo | gst/base/gstbasesrc.c (gst_base_src_start): Post an... |
blob | commitdiff | raw | diff to current |
2005-07-12 |
Wim Taymans | gst/base/gstbasetransform.c: Added more debug info... |
blob | commitdiff | raw | diff to current |
2005-07-04 |
Edward Hervey | gst/gstutils.*: now returns the signal id for better... |
blob | commitdiff | raw | diff to current |
2005-06-30 |
Wim Taymans | gst/: Removed atomic operations, use existing LOCK. |
blob | commitdiff | raw | diff to current |
2005-06-29 |
Ronald S. Bultje | Remove old probes, add new g-signal-based probes and... |
blob | commitdiff | raw | diff to current |
2005-06-29 |
Edward Hervey | gst/: Moved gst_element_factory_can_[sink|src]_caps... |
blob | commitdiff | raw | diff to current |
2005-06-29 |
Thomas Vander Stichele | doc fixes |
blob | commitdiff | raw | diff to current |
2005-06-28 |
Andy Wingo | *.c: Don't cast to GST_OBJECT when reffing or unreffing... |
blob | commitdiff | raw | diff to current |
2005-06-08 |
Andy Wingo | gst/gstutils.c: RPAD fixes all around. |
blob | commitdiff | raw | diff to current |
2005-06-02 |
Jan Schmidt | gst/elements/gstcapsfilter.c: Free existing caps if... |
blob | commitdiff | raw | diff to current |
2005-05-25 |
Ronald S. Bultje | gst/base/gstbasesrc.c: Don't go in pull mode for non... |
blob | commitdiff | raw | diff to current |
2005-05-14 |
Andy Wingo | gst/gstpipeline.c (gst_pipeline_init): Drop ref on... |
blob | commitdiff | raw | diff to current |
2005-05-14 |
Andy Wingo | gst/gstutils.c (gst_element_link_pads): Instead of... |
blob | commitdiff | raw | diff to current |
2005-05-12 |
Ronald S. Bultje | gst/gstutils.c: No, an element is not a pad. |
blob | commitdiff | raw | diff to current |
2005-05-11 |
Wim Taymans | gst/: Fix refcounting in utils function. |
blob | commitdiff | raw | diff to current |
2005-05-09 |
Wim Taymans | Remove old query functions. Ported old code. |
blob | commitdiff | raw | diff to current |
2005-05-06 |
Wim Taymans | gst/: Fix gst_pad_peer_get_caps(), make it return NULL... |
blob | commitdiff | raw | diff to current |
2005-05-05 |
Wim Taymans | gst/: Fix name lookup in GstBin. |
blob | commitdiff | raw | diff to current |
2005-04-24 |
David Schleef | Convert everything from GstAtomicInt to g_atomic_int_... |
blob | commitdiff | raw | diff to current |
2005-04-24 |
David Schleef | gst/gstpad.c: Remove handling of filtered caps. Fix... |
blob | commitdiff | raw | diff to current |
2005-04-23 |
David Schleef | gst/elements/: New element that acts like an identity... |
blob | commitdiff | raw | diff to current |
2005-03-07 |
Wim Taymans | First THREADED backport attempt, focusing on adding... |
blob | commitdiff | raw | diff to current |
2004-11-02 |
Wim Taymans | gst/: Aplied part of patch #157127: Cleanup of issues... |
blob | commitdiff | raw | diff to current |
2004-03-22 |
Benjamin Otte | gst/gstutils.*: first argument of gst_util_dump_mem... |
blob | commitdiff | raw | diff to current |
2004-03-15 |
Thomas Vander Stichele | don't mix tabs and spaces |
blob | commitdiff | raw | diff to current |
2004-03-13 |
Thomas Vander Stichele | gst-indent run on core |
blob | commitdiff | raw | diff to current |
2004-02-11 |
David Schleef | docs/gst/tmpl/gstcaps.sgml: Fix stuff that mentions... |
blob | commitdiff | raw | diff to current |
2004-02-02 |
David Schleef | Change usage of isblah() to g_ascii_isblah() to be... |
blob | commitdiff | raw | diff to current |
2003-12-22 |
David Schleef | Merge CAPS branch |
blob | commitdiff | raw | diff to current |
2003-11-03 |
David Schleef | Add G_DISABLE_DEPRECATED and fix deprecated code |
blob | commitdiff | raw | diff to current |
2003-10-28 |
Benjamin Otte | merge TYPEFIND branch. Major changes: |
blob | commitdiff | raw | diff to current |
2003-08-05 |
Thomas Vander Stichele | cia check |
blob | commitdiff | raw | diff to current |
2003-06-29 |
Benjamin Otte | GST_DEBUG reorganization containing loads of stuff: |
blob | commitdiff | raw | diff to current |
2003-03-16 |
Christian Meyer | Fixed bug #108514. |
blob | commitdiff | raw | diff to current |
2003-02-21 |
Wim Taymans | dump_mem should be fast and correct now (finally) |
blob | commitdiff | raw | diff to current |
2003-02-10 |
Wim Taymans | - Add more --disable options |
blob | commitdiff | raw | diff to current |
2003-02-08 |
Wim Taymans | removed old code, g_object_get is the prefered method... |
blob | commitdiff | raw | diff to current |
2003-01-26 |
Wim Taymans | Faster _dump function |
blob | commitdiff | raw | diff to current |
2002-11-27 |
Wim Taymans | - Added first attempt at general caching mechanism... |
blob | commitdiff | raw | diff to current |
2002-07-08 |
Wim Taymans | - Removed bufferpool code and move that to gstbuffer.c |
blob | commitdiff | raw | diff to current |
2002-05-29 |
Wim Taymans | Error checking in pthread creation more info in gst_uti... |
blob | commitdiff | raw | diff to current |
2002-03-30 |
Wim Taymans | - Remove the propsprivate header file |
blob | commitdiff | raw | diff to current |
2002-03-24 |
Andy Wingo | filter newlines out of GST_DEBUG statements to reflect... |
blob | commitdiff | raw | diff to current |
2002-03-05 |
Benjamin Otte | warning: int format, GType arg (arg 3) |
blob | commitdiff | raw | diff to current |
2002-03-03 |
Steve Baker | added gst_util_set_value_from_string. |
blob | commitdiff | raw | diff to current |
2002-02-06 |
Andy Wingo | core is glib2 only now tried to convert to g_strdup_val... |
blob | commitdiff | raw | diff to current |
2002-01-01 |
Wim Taymans | API doc updates. |
blob | commitdiff | raw | diff to current |
2001-12-14 |
Christian Schaller | aye ladie, no more ugly // comments here, even if Taaz... |
blob | commitdiff | raw | diff to current |
2001-12-14 |
Michael Meeks | gst/gst.c (gst_main, gst_main_quit): upd. |
blob | commitdiff | raw | diff to current |
2001-12-04 |
wrobell | - some fixes to int2float making automake 1.5 happy... |
blob | commitdiff | raw | diff to current |
2001-10-21 |
Wim Taymans | API docs. revived _buffer_ref_by_count fast types for... |
blob | commitdiff | raw | diff to current |
2001-10-20 |
Erik Walthinsen | convert g_string_printfa to g_string_append_printf... |
blob | commitdiff | raw | diff to current |
2001-09-18 |
Joshua N. Pritikin | glib 1.2 fix minor formatting improvements add gst_prin... |
blob | commitdiff | raw | diff to current |
2001-09-17 |
Joshua N. Pritikin | fix warnings |
blob | commitdiff | raw | diff to current |
2001-09-14 |
Joshua N. Pritikin | 1. Add more warnings for the gst core only. Various... |
blob | commitdiff | raw | diff to current |
2001-07-04 |
Trivial commit,... | Added arg setting for UINT types. |
blob | commitdiff | raw | diff to current |
2001-06-25 |
Erik Walthinsen | Merged from GOBJECT1 to HEAD at 200106241 |
blob | commitdiff | raw | diff to current |
2001-04-27 |
Wim Taymans | Added enum parsing... |
blob | commitdiff | raw | diff to current |
2001-04-22 |
Wim Taymans | API docs updates. |
blob | commitdiff | raw | diff to current |
2001-03-21 |
Wim Taymans | API docs updates |
blob | commitdiff | raw | diff to current |
2001-03-06 |
Wim Taymans | Small fixes to pipeline and gstbin. |
blob | commitdiff | raw | diff to current |
2001-03-03 |
Wim Taymans | And the gst_utit_set_object_arg function too of course... |
blob | commitdiff | raw | diff to current |
2001-01-06 |
Erik Walthinsen | Cleaned up the docs a bit. |
blob | commitdiff | raw | diff to current |
2000-12-28 |
Erik Walthinsen | Updated copyright in all the libgst files. |
blob | commitdiff | raw | diff to current |
2000-12-25 |
Wim Taymans | Lots of editor changes: |
blob | commitdiff | raw | diff to current |
2000-12-15 |
Wim Taymans | Header cleanup: try to include as little as possible... |
blob | commitdiff | raw | diff to current |
2000-11-06 |
Wim Taymans | Added seeking to the avi decoder by implementing pull_r... |
blob | commitdiff | raw | diff to current |
2000-10-25 |
Wim Taymans | More Docs updates. |
blob | commitdiff | raw | diff to current |
2000-07-15 |
Wim Taymans | Fixed a bug in the riff parser with the allignment... |
blob | commitdiff | raw | diff to current |
2000-01-30 |
Erik Walthinsen | initial checkin |
blob | commitdiff | raw | diff to current |
|