]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/gstreamer0-10.git/history - libs/gst/base/gstbasesink.c
gst_private.h: make sure gst_private.h is included before glib.h
[glsdk/gstreamer0-10.git] / libs / gst / base / gstbasesink.c
2010-01-20 Tim-Philipp Müllergst_private.h: make sure gst_private.h is included...
2009-12-11 Wim Taymansbasesink: add some more debugging
2009-12-08 Sebastian Drögebasesink: Allow update NEWSEGMENT events after EOS
2009-12-01 Edward Herveybasesrc/basesink: Register debug funcptr only once.
2009-11-28 Wim Taymansbasesink: clip stepping boundaries
2009-11-27 Stefan Kostdocs: fix broken xrefs
2009-11-27 Stefan Kostdocs: fix broken xrefs
2009-11-19 Jan Schmidtbasesink: Clamp the base time correctly in position...
2009-11-18 Sebastian Drögebasesink: Handle the new sink-message event
2009-11-16 Wim Taymansbasesink: fix position reporting
2009-11-11 Jan Schmidtbasesink: Fix treating base_time as unsigned in positio...
2009-10-28 Tim-Philipp MüllerRemove GST_DEBUG_FUNCPTR where they're pointless
2009-10-09 Stefan Kostbasesink: lets keep -1 for segmenst as they are guint64...
2009-10-09 Stefan Kostbasesink: use GST_CLOCK_TIME_NONE and GST_CLOCK_TIME_IS...
2009-10-08 Edward Herveygst/base/basesink: Remove dead assignment.
2009-08-24 Wim Taymansbasesink: whitespace fixes
2009-08-08 Edward Herveybasesink: Remove dead assignments
2009-08-06 Wim Taymansbasesink: cleanups in position queries
2009-08-06 Stian Selnesbasesink: Query upstream for the position if conversion...
2009-07-06 Stefan Kostlogging: use perf category for dropped buffers
2009-06-29 Wim Taymansbufferlist: use faster gst_buffer_list_get()
2009-06-29 Ognyan Tonchevbasesink: take timestamp later
2009-06-25 Tim-Philipp Müllerbasesink: don't do things with side effects within...
2009-06-16 Branko Subasicbasesink: add support for buffer list
2009-06-12 Wim Taymansstepping: more stepping improvements
2009-06-12 Wim Taymansbasesink: post step-start
2009-06-09 Wim Taymansbasesink: update segment start/stop for clipping
2009-06-09 Wim Taymansbasesink: do proper clipping in stepping
2009-06-08 Wim Taymansstepping: do flushing steps correctly
2009-06-08 Jan Schmidtbasesink: Change awkward wording in a translateable...
2009-06-08 Wim Taymansbasesink: add non-flushing steps
2009-06-04 Wim Taymansbasesink: fix clipped start/stop after step
2009-06-04 Wim Taymansbasesink: use more correct segment methods
2009-06-03 Wim Taymansbasesink; handle EOS correctly.
2009-06-03 Wim Taymansbasesink: forget previous times when stepping
2009-06-02 Wim Taymansbasesink: fix regression in unit tests
2009-06-01 Wim Taymansbasesink: post a warning on excessive framedrops
2009-06-01 Wim Taymansbasesink: more stepping in reverse
2009-06-01 Wim Taymansbasesink: use start_time as the step start
2009-06-01 Wim Taymansbasesink: catch step cases in _wait_preroll()
2009-06-01 Wim Taymansbasesink: more stepping in reverse fixes
2009-06-01 Wim Taymansbasesink: small cleanups
2009-06-01 Wim Taymansframestep: implement backwards framestep
2009-06-01 Wim Taymansbasesink: add framestepping in time
2009-06-01 Wim Taymansbasesink: keep track of stepped time
2009-06-01 Wim Taymansbasesink: move stuff around, more stepping
2009-06-01 Wim Taymansbasesink: first stab at frame stepping in PAUSED
2009-04-04 Edward Herveybasesink: Remove dead assignments.
2009-04-04 Sebastian Drögegst: Use g_once_init* or G_DEFINE_TYPE
2009-04-03 Edward Herveybasesink : Remove unused variable.
2009-03-23 Tim-Philipp Müllerbasesink: fix once-per-second 'emergency rendering...
2009-03-05 Andy Wingobasesink: propagate UPSTREAM events in pull mode too
2009-02-26 Stefan Kostbasesink: move left over handling of the error case...
2009-02-23 Wim TaymansDon't forward LATENCY event when not ready
2009-02-03 Wim TaymansGstBaseSink: use new variable to schedule preroll
2009-02-03 Wim TaymansGstBaseSink: avoid calling preroll multiple times
2009-01-22 Wim TaymansMerge branch 'master' of ssh://git.freedesktop.org...
2009-01-22 Wim TaymansMerge branch 'master' of ssh://git.freedesktop.org...
2009-01-21 Wim TaymansUpdate the last_buffer exactly with the buffer that...
2009-01-09 Wim Taymanslibs/gst/base/gstbasesink.*: Fix documentation for...
2009-01-05 Wim Taymanslibs/gst/base/gstbasesink.c: Release the object lock...
2008-12-15 Wim Taymanslibs/gst/base/gstbasesink.c: Expose the render-delay...
2008-11-24 Stefan Kostlibs/gst/base/gstbasesink.c: Turn comment into gtk...
2008-11-20 Wim Taymanslibs/gst/base/gstbasesink.c: Changing the render delay...
2008-11-04 Wim TaymansCopy seqnums from events to messages so that they can...
2008-10-20 Wim Taymanslibs/gst/base/gstbasesink.c: Implement more seeking...
2008-10-17 Wim Taymanslibs/gst/base/gstbasesink.c: Query the total number...
2008-10-16 Wim TaymansAdd method to commit the state in subclasses.
2008-10-10 Wim Taymansgst/gstbin.c: The message src can be NULL, don't try...
2008-10-10 Wim Taymansdocs/design/part-negotiation.txt: Small doc update.
2008-10-08 Wim Taymanslibs/gst/base/gstbasesink.c: Forward LATENCY events...
2008-10-06 Wim Taymanslibs/gst/base/gstbasesink.c: Improve position reporting...
2008-08-19 Wim Taymanslibs/gst/base/gstbasesink.c: Improve position reporting...
2008-08-19 Jason Zhaolibs/gst/base/gstbasesink.c: When the subclass event...
2008-06-20 Wim TaymansAdd method to allow sinks to specify additional delay...
2008-06-20 Wim Taymanslibs/gst/base/gstbasesink.c: If we have not seen a...
2008-06-04 Wim Taymanslibs/gst/base/gstbasesink.c: Add some debug.
2008-05-30 Wim Taymanslibs/gst/base/gstbasesink.c: The reported position...
2008-05-29 Wim Taymanslibs/gst/base/gstbasesink.c: Fix position query range...
2008-05-22 Sjoerd Simonslibs/gst/base/gstbasesink.c: If nothing else can be...
2008-05-19 Wim TaymansExpose a method that was previously used internally...
2008-05-19 Wim Taymanslibs/gst/base/gstbasesink.c: Refactor adjusting the...
2008-05-07 Wim Taymanslibs/gst/base/gstadapter.c: Small code cleanup.
2008-04-25 Wim Taymanslibs/gst/base/gstbasesink.c: Rearrange the latency...
2008-04-17 Sebastian Drögegst/gstutils.*: API: Deprecate gst_atomic_int_set(...
2008-03-22 Sebastian DrögeDefine G_PARAM_STATIC_STRINGS if it's undefined (GLib...
2008-02-29 Wim Taymanslibs/gst/base/gstbasesink.c: Small doc update.
2008-02-05 Sebastian DrögeRevert previous changes to the behaviour of GstPadTempl...
2008-02-03 Sebastian DrögeDon't use base_init where not absolutely necessary...
2008-02-01 Wim Taymanslibs/gst/base/gstbasesink.c: Add fixme regarding EOS...
2007-12-13 Stefan Kostlibs/gst/base/: Replace gst_pad_get_parent by GST_OBJEC...
2007-12-11 Stefan KostChange GST_GET_TIMESTAMP into gst_util_get_timestamp...
2007-11-28 Stefan Kostlibs/gst/base/gstbasesink.c: Use new API to get elapsed...
2007-11-21 Wim Taymanslibs/gst/base/gstbasesink.c: Only send upstream events...
2007-11-09 Wim Taymanslibs/gst/base/gstbasesink.c: Don't hold the object...
2007-11-09 Wim Taymansgst/gstsegment.c: Also accumulate time correctly when...
2007-11-06 Wim Taymanslibs/gst/base/gstbasesink.c: Don't try to report a...
2007-10-30 Wim TaymansAdd a new last-buffer property that contains the last...
2007-10-25 Wim Taymanslibs/gst/base/gstbasesink.c: Reset last seen position...
2007-10-10 Wim Taymanslibs/gst/base/gstbasesink.*: Add function to wait for...
next