]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/gstreamer0-10.git/history - libs/gst/base/gstbasesrc.c
docs: fix Since: markers for API added after 0.10.35
[glsdk/gstreamer0-10.git] / libs / gst / base / gstbasesrc.c
2011-11-08 Tim-Philipp Müllerdocs: fix Since: markers for API added after 0.10.35
2011-10-18 Wim Taymansbasesrc: also update the stream time
2011-10-12 Wim Taymansbasesrc: properly adjust start time
2011-09-07 Piotr Fusikdocs, gst: typo fixes
2011-06-30 Mark Nauwelaertsbasesrc: do not sneakily mess with current offset when...
2011-06-18 Tim-Philipp MüllerBump git version after unplanned 0.10.35 release
2011-06-10 Tim-Philipp Müllerdocs: update for gst_base_src_set_dynamic_size
2011-06-08 Mark Nauwelaertsbasesrc: add dynamic size handling
2011-06-08 Mark NauwelaertsRevert "basesrc: Send an update NEWSEGMENT event downst...
2011-05-27 Sebastian Drögebasesrc: Send an update NEWSEGMENT event downstream...
2011-05-12 Vincent Penquerc'hbasesrc: do not set first buffer timestamp to 0 for...
2011-04-08 Havard Graffbasesrc: Make src query MT-safe
2011-04-08 Sebastian Drögebase: Unref events if the parent element disappeared
2011-04-08 Havard Graffbase: Make upstream events MT-safe
2011-04-07 Sebastian Drögebasesrc: Handle tag and custom downstream events the...
2011-04-07 Sebastian Drögebla
2011-04-07 Sebastian Drögebasesrc: Send syncronized custom downstream/both events...
2011-03-28 Arun Raghavanbasesrc: Return FALSE if we don't handle an event
2011-03-24 Stefan Kostdocs: cleanup and xref fixes
2011-03-24 Edward Herveybasesrc: Keep downstream caps order when fixating
2011-01-10 Wim Taymansbasesrc: make sure we wait and release the live lock
2011-01-02 Tim-Philipp Müllerbasesrc, basesink: add some FIXMEs for the type of...
2010-12-29 Wim Taymansbasesrc: fix deadlock
2010-12-17 Edward Herveybasesrc: Use an atomic integer instead of a lock for...
2010-12-07 Tim-Philipp Müllerdocs: libgstbase: more gobject introspection annotations
2010-10-11 Wim Taymansbasesrc: tag as a SOURCE element
2010-08-27 Sebastian Drögebase: Stop using GST_FLOW_IS_FATAL()
2010-08-06 Sebastian Drögebasesrc: Make sure the buffer metadata is writable...
2010-08-05 Stefan Kostdebug: logging improvements
2010-08-05 Stefan Kostbasesrc: log seek event details
2010-08-05 Stefan Kostbasesrc: avoid some caps manipulation
2010-07-16 Sebastian Drögebasesrc: Return values in stream time for the POSITION...
2010-06-13 Sebastian DrögeRemove some dead assignments
2010-05-06 Stefan Kostbasesrc: reflow to truncate caps just once
2010-05-04 Wim Taymansbasesrc: improve debugging
2010-04-30 Stefan Kostqueries: add more logging
2010-04-06 Jonas Holmbergbasesrc: fix gst_base_src_new_seamless_segment()
2010-03-18 Wim Taymansbasesrc: catch, parse and store QoS event values
2010-02-17 Edward Herveybasesrc: Don't use expensive cast checks in get_range.
2010-02-12 Sebastian Drögebasesrc: Make locking of the segment a bit more strict...
2010-02-12 Sebastian Drögebasesrc: Protect segment values from concurrent access...
2009-12-04 Jan Schmidtbasesrc: Shut down the pad task when the initial seek...
2009-12-01 Edward Herveybasesrc/basesink: Register debug funcptr only once.
2009-11-27 Stefan Kostdocs: fix broken xrefs
2009-11-21 Jan Schmidtbasesrc: Add gst_base_src_new_seamless_segment()
2009-11-05 Stefan Kostpad: rename new api from _refed to _reffed.
2009-10-28 Tim-Philipp MüllerRemove GST_DEBUG_FUNCPTR where they're pointless
2009-10-15 Wim Taymansbasesrc: fix race in PLAYING->PAUSED->PLAYING
2009-10-07 Stefan Kostpad: add variants of gst_pad_get_caps() that don't...
2009-09-01 Wim Taymansbasesrc: whitespace fixes
2009-08-24 Wim Taymansbasesrc: return result of _set_caps()
2009-07-24 Robin Stockerbasesrc: don't handle SEEKING queries for formats that...
2009-07-20 Wim Taymansbasesrc: make tag queuing threadsafe
2009-07-20 Edward Herveybasesrc: Serialize tags into the dataflow. Fixes #588745
2009-06-15 Wim Taymansbasesrc: add some more debug
2009-06-05 Mark Nauwelaertsbasesrc: reply to QUERY_SEEKING with original format...
2009-05-11 Wim Taymansbasesrc: don't ignore pad_start return value
2009-04-04 Edward Herveybasesrc: remove dead assignment.
2009-04-04 Sebastian Drögegst: Use g_once_init* or G_DEFINE_TYPE
2009-03-11 Edward Herveygstbasesrc: unsigned long is "%lu", not "%ul". Fixes...
2009-03-10 Stefan Kostlogging: some additional logging for tracing caps negot...
2009-02-23 Wim TaymansError out more specifically on empty caps
2009-01-29 Stefan KostAdd logging in failure case. Add more details to a...
2008-11-04 Wim TaymansCopy seqnums from events to messages so that they can...
2008-10-20 Wim Taymanslibs/gst/base/gstbasesrc.c: Update comment.
2008-10-19 Stefan Kostlibs/gst/base/gstbasesrc.c: (gst_base_src_default_do_seek);
2008-10-16 Wim Taymanslibs/gst/base/gstbasesrc.c: Update some docs.
2008-10-10 Wim Taymansdocs/design/part-negotiation.txt: Small doc update.
2008-08-21 Wim Taymanslibs/gst/base/gstbasesrc.c: Use the result from gst_pad...
2008-08-12 Stefan Kostlibs/gst/base/: Fix headings in docs and gtk-doc warnings.
2008-07-24 Thijs Vermeirlibs/gst/base/gstbasesrc.*: Don't cache the seekable...
2008-05-28 Bjarne Rosengrenlibs/gst/base/gstbasesrc.c: Make sending an EOS event...
2008-05-19 Tim-Philipp Müllerlibs/gst/base/gstbasesrc.c: Use right error code when...
2008-05-19 Wim Taymanslibs/gst/base/gstbasesrc.c: When the subclass did not...
2008-05-07 Ole André Vadla... libs/gst/base/gstbasesrc.c (gst_base_src_default_query...
2008-05-07 Wim Taymanslibs/gst/base/gstadapter.c: Small code cleanup.
2008-04-09 Wim Taymansdocs/design/part-buffering.txt: Fix some typos and...
2008-03-22 Sebastian DrögeDefine G_PARAM_STATIC_STRINGS if it's undefined (GLib...
2008-02-05 Sebastian DrögeRevert previous changes to the behaviour of GstPadTempl...
2008-02-03 Sebastian DrögeDon't use base_init where not absolutely necessary...
2008-01-09 Wim Taymanslibs/gst/base/gstbasesrc.c: The start segment for rever...
2008-01-07 Wim Taymanslibs/gst/base/gstbasesrc.c: Don't update the last_stop...
2007-12-19 Wim Taymanslibs/gst/base/gstbasesrc.c: Allow sending EOS to the...
2007-12-17 Wim Taymanslibs/gst/base/gstbasesrc.c: Make _wait_playing() not...
2007-12-13 Stefan Kostlibs/gst/base/: Replace gst_pad_get_parent by GST_OBJEC...
2007-11-06 Wim Taymanslibs/gst/base/gstbasesrc.c: Unify flushing code, remove...
2007-10-31 Stefan Kostlibs/gst/base/gstbasesrc.c: Its "Since:" and not "...
2007-10-05 Wim Taymanslibs/gst/base/gstbasesrc.c: Rework the locking of bases...
2007-10-02 Wim Taymanslibs/gst/base/gstbasesrc.c: Call unlock for live source...
2007-10-01 Wim Taymanslibs/gst/base/gstbasesrc.c: Also initialize the counter...
2007-09-19 Wim Taymanslibs/gst/base/gstbasesrc.c: Don't unref the event after...
2007-09-17 Jan SchmidtFix minor compilation warnings shown with Forte.
2007-09-13 Wim Taymanslibs/gst/base/gstbasesrc.c: Push OOB events downstream...
2007-09-13 Wim Taymanslibs/gst/base/gstbasesrc.c: Update docs.
2007-09-11 Wim Taymansdocs/design/part-live-source.txt: Add docs on how live...
2007-09-10 Wim Taymanslibs/gst/base/gstbasesrc.*: Add property to make the...
2007-08-28 Wim Taymanslibs/gst/base/gstbasesink.c: Improve debugging.
2007-06-15 Wim TaymansImprove debugging.
2007-05-03 Wim TaymansAPI: gst_base_src_query_latency(). Added method so...
2007-04-13 Jan SchmidtAllow basesrc derived classes to execute seeks in other...
next