]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/gstreamer0-10.git/history - libs/gst/base/gstbasetransform.c
DEBIAN: Debianization
[glsdk/gstreamer0-10.git] / libs / gst / base / gstbasetransform.c
2013-05-15 Nikhil Devshatwarhand revert f56c6e12255b37d75b1eb949e434fa8e3bb33f51
2013-05-15 Rob Clarkbasetransform: don't do unnecessary pad_alloc()
2011-12-19 Mark Nauwelaertsbasetransform: suggestion compatible with upstream...
2011-12-08 Sebastian Drögebasetransform: Fix code path to come up with possible...
2011-12-08 Sebastian Drögebasetransform: Fall back to upstream provided caps...
2011-12-08 Sebastian Drögebasetransform: Fall back to upstream provided caps...
2011-12-08 Sebastian Drögebasetransform: Refactor gst_base_transform_buffer_alloc...
2011-12-07 Sebastian Drögebasetransform: If suggested caps are not compatible...
2011-12-04 Tim-Philipp MüllerSuppress deprecation warnings in selected files, for...
2011-12-04 Tim-Philipp MüllerWork around deprecated thread API in glib master
2011-11-30 Sebastian Drögebasetransform: Always intersect the suggested sink...
2011-11-04 Sjoerd Simonsbasetransform: Only use the cached transform on strictl...
2011-10-28 Sjoerd Simonsbasetransform: Also fush the cache when changing the...
2011-10-28 Sjoerd Simonsbasetransform: Add debug output when returning a cached...
2011-10-27 Jan Schmidtbasetransform: Fix refcount leak
2011-10-20 Vincent Penquerc'hbasetransform: cache transformed caps where appropriate
2011-09-27 Vincent Penquerc'hbasetransform: send delayed events earlier
2011-09-21 Vincent Penquerc'hbasetransform: delay serialized events when src caps...
2011-09-08 Sebastian DrögeRevert "basetransform: Use check for subsets and not...
2011-09-07 Piotr Fusikdocs, gst: typo fixes
2011-09-07 Sebastian Drögebasetransform: If there's no peer we still have to...
2011-09-06 Sebastian Drögebasetransform: Use check for subsets and not non-empty...
2011-08-26 Sjoerd Simonsbasetransform: Use GstPadDirection in the query vfunc
2011-08-26 Sjoerd SimonsBaseTransform: Add a query vfunc
2011-06-18 Tim-Philipp MüllerBump git version after unplanned 0.10.35 release
2011-05-14 Sebastian Drögebasetransform: When trying to fixate the sink suggestio...
2011-05-14 Sebastian Drögebasetransform: In getcaps() prefer the caps order and...
2011-05-14 Sebastian Drögebasetransform: Prefer caps order given by the subclass...
2011-04-21 Thiago Santosbasetransform: fix negotiation regression
2011-04-19 Havard Graffbasetransform: don't unref trans until the function...
2011-04-13 Ole André Vadla... base: Fix pad callbacks so they handle when parent...
2011-04-08 Sebastian Drögebase: Unref events if the parent element disappeared
2011-04-08 Havard Graffbase: Make upstream events MT-safe
2011-03-24 Edward Herveybasetransform: Retain caps order when getting caps
2011-02-21 Thiago Santosbasetransform: Be smarter with pad allocs
2011-02-14 Thiago Santosbasetransform: Check for pad alloc caps when suggestion...
2010-12-16 Sebastian Drögebasetransform: Handle downstream giving a buffer with...
2010-12-07 Tim-Philipp Müllerdocs: libgstbase: more gobject introspection annotations
2010-10-29 Jonathan Matthewbasetransform: use input position for queries if we...
2010-10-29 Wim Taymansbasetransform: fix reverse negotiation
2010-10-10 Sebastian Drögebasetransform: Report the output position on POSITION...
2010-09-23 Havard Graffbasetransform: Make a WARNING into a DEBUG statement
2010-09-23 Wim Taymansbasetransform: avoid useless memcpy
2010-08-26 Wim Taymansbasetransform: recover from invalid downstream suggestions
2010-08-05 Stefan Kostdebug: logging improvements
2010-07-27 Rob Clarkbasetransform fix for upstream caps-renegotiation
2010-07-26 Thiago Santosbasetransform: Try suggesting caps on bad caps pad_alloc
2010-07-17 Sebastian Drögebasetransform: Allow the subclass to add new fields...
2010-07-16 Sebastian Drögebasetransform: Implement POSITION query
2010-06-14 Wim Taymansbasetransform: reevaluate proxy_alloc when reconfigured
2010-06-14 Wim Taymansbasetransform: add accept_caps vmethod
2010-06-14 Olivier Crêtebasetransform: Assume size is the same if no transform_...
2010-06-05 Stefan Kostbasetransform: avoid a caps-copy
2010-03-29 Thiago Santosbasetransform: Refactor caps suggestion on pad_alloc
2010-03-18 Robert Swainbasetransform: Implement QoS message posting
2010-03-16 Thiago Santosbasetransform: Accept non-fixed caps suggestions
2010-01-17 Sebastian Drögebasetransform: Only use suggested caps in buffer alloca...
2010-01-14 Sebastian Drögebasetransform: Handle buffers with NULL caps correctly
2009-11-05 Stefan Kostpad: rename new api from _refed to _reffed.
2009-10-28 Tim-Philipp MüllerRemove GST_DEBUG_FUNCPTR where they're pointless
2009-10-07 Stefan Kostpad: add variants of gst_pad_get_caps() that don't...
2009-08-28 Thijs VermeirCheck suggested caps for proxy alloc
2009-08-06 Stefan Kostbasetransform: use new _caps_can_intersect()
2009-08-06 Stefan Kostbasetransform: only check caps_is_fixed() if they changed
2009-08-06 Wim Taymansbasetransform: clarify _caps_is_equal()
2009-08-06 Wim Taymansbasetransform: refactor metadata modifications
2009-08-06 Wim Taymansbasetransform: enable optimisation
2009-08-06 Wim Taymansbasetransform: fix refcounting problem
2009-08-06 Kipp Cannonbasetransform: Improve debug output in gst_base_transfo...
2009-08-06 Sebastian Drögebasetransform: Don't unset GAP flag if working in passt...
2009-07-14 Stefan Kostbasetransform: take size once
2009-07-06 Stefan Kostbasetransform: make comment a FIXME comment
2009-04-15 Stefan Kostlogging: fix unused variable warning when disabling...
2009-04-04 Sebastian Drögegst: Use g_once_init* or G_DEFINE_TYPE
2009-04-03 Edward Herveybasetransform: move unused variable in the #if 0 block.
2009-04-03 Edward HerveyRemove unused variables detected by LLVM's Clang static...
2009-02-02 Thijs VermeirForce reconfigure of basetransform to recheck alloc...
2009-01-30 Wim TaymansRevert "Check suggested caps for proxy alloc"
2009-01-30 Wim TaymansRevert "Force reconfigure of basetransform to recheck...
2009-01-29 Stefan KostAdd logging in failure case. Add more details to a...
2009-01-29 Thijs VermeirCheck suggested caps for proxy alloc
2009-01-29 Thijs VermeirForce reconfigure of basetransform to recheck alloc...
2009-01-25 Thijs VermeirFix typo
2009-01-01 Stefan Kostgst/gstdebugutils.c: Add some ideas, how to make the...
2008-12-08 Wim Taymanslibs/gst/base/gstbasetransform.*: Add vmethod that...
2008-11-24 Wim Taymanslibs/gst/base/gstbasetransform.c: Revert quick accepcap...
2008-11-22 Wim Taymanslibs/gst/base/gstbasetransform.c: Rename a variable...
2008-11-21 Wim Taymanslibs/gst/base/gstbasetransform.c: Add beginnings of...
2008-10-27 Wim Taymanslibs/gst/base/gstbasetransform.c: If we have a fixate...
2008-10-24 Wim Taymanslibs/gst/base/gstbasetransform.c: Clear the output...
2008-10-21 Wim Taymanslibs/gst/base/gstbasetransform.c: Protect sink_alloc...
2008-10-20 Wim Taymanslibs/gst/base/gstbasesrc.c: Update comment.
2008-09-28 Jan SchmidtFix assertion in basetransform when the subclass choose...
2008-09-24 Wim Taymanslibs/gst/base/gstbasetransform.c: Take new caps ref...
2008-08-20 Wim TaymansImplement method for reconfiguring basetransform.
2008-08-18 Wim Taymanslibs/gst/base/gstbasetransform.c: If the element is...
2008-08-14 Wim Taymanslibs/gst/base/gstbasetransform.c: Go over the buffer_al...
2008-08-14 Wim Taymanslibs/gst/base/gstbasetransform.c: Don't overwrite the...
2008-08-12 Stefan Kostlibs/gst/base/: Fix headings in docs and gtk-doc warnings.
2008-08-11 Edward Herveylibs/gst/base/gstbasetransform.c: Fix a "may be used...
next