plugin-scanner: rename plugin-scanner helper binary to gst-plugin-scanner
[glsdk/gstreamer0-10.git] / libs / gst / check /
2009-10-12 Edward Herveylibs/gst/check: Make writing threadsafe. Backported...
2009-10-12 Edward Herveylibs/gst/check: Run gst-indent on libcheck.
2009-10-08 Edward Herveygst/check/consistencychecker: Check type of miniobject...
2009-09-30 Jan Schmidtlibgstcheck: Don't use character classes in sed expressions
2009-09-14 David SchleefFix out-of-tree build
2009-09-12 Sebastian Drögeintrospection: Build pkgconfig before all libraries...
2009-09-05 Sebastian Drögeintrospection: Strip Gst prefix from all types/functions
2009-09-05 Sebastian Drögeintrospection: Fix out-of-tree build
2009-09-05 Sebastian Drögeintrospection: Fix build if gir-repository is not installed
2009-09-05 Sebastian Drögecheck: Add gobject-introspection support
2009-08-10 Tim-Philipp Müllercheck: add some logging before calling gst_task_cleanup...
2009-08-08 Sebastian Drögecheck: Call gst_task_cleanup_all() in GST_END_TEST
2009-08-06 Tim-Philipp Müllercheck: add internal-check.h to BUILT_SOURCES in attempt...
2009-08-06 Tim-Philipp Müllercheck: fix symbol exporting
2009-08-06 Tim-Philipp Müllercheck: fix issues with 'make distcheck'
2009-08-06 Tim-Philipp Müllercheck: use private copy of check for libgstcheck
2009-08-06 Tim-Philipp Müllercheck: add internal copy of check-0.9.6
2009-07-28 Tim-Philipp Müllercheck: make new GstStreamConsistency structure private
2009-07-20 Edward Herveygstcheck: Add a stream consistency checking helper...
2009-04-02 Sebastian Drögegstcheck: Call gst_check_init() before creating the...
2009-03-19 Tim-Philipp Müllergstcheck: fix for check versions > 0.9.6
2009-02-04 Stefan Kostcheck: Don't assume gst_pad_get_peer returns non NULL...
2009-01-25 Thijs VermeirOnly free list of buffers once
2009-01-23 Jan SchmidtUpdate a bunch of gitignores to clean up my git status...
2008-12-10 Peter Kjellerstedtlibs/gst/check/gstcheck.h: Allow check tests to use
2008-12-09 Sebastian Drögelibs/gst/check/gstcheck.c: Revert accidentially commite...
2008-06-21 Thijs Vermeirdocs/libs/gstreamer-libs-sections.txt: Add new API...
2008-06-21 Thijs Vermeirlibs/gst/check/gstcheck.*: Also setup request pads...
2008-05-21 Wim TaymansDon't use gst_element_get_pad().
2008-04-28 Michael Smithlibs/gst/check/Makefile.am: Don't add an explicit link...
2008-04-10 Stefan Kostlibs/gst/check/gstcheck.c: Remove blank line between...
2008-03-24 Mark NauwelaertsSmall documentation fixes. Fixes #523978.
2008-03-22 Sebastian DrögeDefine G_PARAM_STATIC_STRINGS if it's undefined (GLib...
2008-02-29 Sebastian DrögeCorrect all relevant warnings found by the sparse seman...
2008-02-19 Jan Schmidtlibs/gst/check/gstcheck.*: Make the declaration in...
2008-02-01 Thijs VermeirAdd more functions for unit testing: gst_check_drop_buf...
2008-01-12 Jan Schmidtgst/gst.c: _gst_trace_on is already provided by gsttrac...
2007-12-20 Peter Kjellerstedtlibs/gst/check/gstcheck.h: Fix detection of the check...
2007-10-25 Jan SchmidtUse a custom export symbol regex for libgstcheck, as...
2007-10-16 Tim-Philipp Müllerlibs/gst/check/gstcheck.*: Allow runtime selection...
2007-08-13 Stefan KostAdd more missing docs.
2007-07-20 Stefan KostAdd libm check as we use in for plugins.
2007-06-14 Tim-Philipp Müllerlibs/gst/check/gstcheck.c: Intercept criticals and...
2007-06-14 Tim-Philipp MüllerUgly 'fix' for the controller unit test on the p5 bot...
2007-06-14 Tim-Philipp MüllerAPI: add fail_unless_equals_float() and assert_equals_f...
2007-01-16 Tim-Philipp Müllerlibs/gst/check/gstcheck.c: Actually write ABI structs...
2007-01-12 Tim-Philipp Müllerlibs/gst/check/: Add G_BEGIN_DECLS and G_END_DECLS...
2006-12-21 Stefan Kostlibs/gst/check/gstcheck.c: do not automatically (de...
2006-11-20 Sebastian Droegelibs/gst/check/gstcheck.h: Fix compilation and running...
2006-10-10 Wim Taymanslibs/gst/check/gstcheck.c: Activate/deactivate pads...
2006-09-28 Jan Schmidtconfigure.ac: Don't pull in gmodule-2.0.pc as a depende...
2006-08-17 Tim-Philipp MüllerMake gstcheck stuff show up in docs (still needs to...
2006-08-15 Tim-Philipp Müllerlibs/gst/check/gstcheck.h: Use const gchar * variables...
2006-08-15 Tim-Philipp Müllerlibs/gst/check/gstcheck.h: Fix ASSERT_CRITICAL and...
2006-07-21 Andy Wingolibs/gst/check/Makefile.am (libgstcheck_@GST_MAJORMINOR...
2006-07-02 Thomas Vander Stichelelibs/gst/check/gstcheck.c: if we get the wrong message...
2006-07-02 Thomas Vander Stichelelibs/gst/check/gstcheck.h: add some assert_ as alias...
2006-07-02 Thomas Vander Stichelemoap ignore
2006-07-01 Thomas Vander Sticheleconfigure.ac: set CFLAGS and friends to -O0 if gcov...
2006-07-01 Thomas Vander Stichelelibs/gst/check/gstcheck.*: create a macro and function...
2006-06-06 Thomas Vander Stichelecosmetics
2006-06-06 Thomas Vander Stichelelibs/gst/check/gstcheck.*: factor out the method from...
2006-06-02 Thomas Vander Stichelelibs/gst/check/gstcheck.c: make sure we unset caps
2006-06-02 Michael Smithlibs/gst/check/gstcheck.*: Add a cond/mutex to the...
2006-05-22 Thomas Vander Sticheledebugging changes
2006-05-10 Thomas Vander Stichelelibs/gst/check/gstcheck.h: add an assert for setting...
2005-11-29 Thomas Vander SticheleCVS surgery + support to move base, check, and net...
2005-11-27 Thomas Vander Sticheleupdate LDFLAGS use some more
2005-11-24 Thomas Vander Stichelecheck/gst/gstminiobject.c: don't use check calls from...
2005-11-16 Thomas Vander Stichelegst/gstpad.*: add gst_pad_new_from_static_template...
2005-10-15 Thomas Vander SticheleI'm too lazy to comment this
2005-09-15 David Schleefconfigure.ac: Add -no-undefined to GST_PLUGIN_LDFLAGS...
2005-09-09 Thomas Vander Stichelecheck/gst/gstpad.c: add tests for valid pad naming
2005-09-02 Andy Wingogst/gstelement.h (GstState): Renamed from GstElementSta...
2005-08-30 Stefan Kostdocs/gst/gstreamer-sections.txt: ultral33t func10ns...
2005-08-25 Thomas Vander Sticheleadd a uint64 checking method
2005-08-22 Thomas Vander Stichelecheck/gst/gstbin.c: since we don't know when preroll...
2005-08-21 Thomas Vander Stichelecheck/Makefile.am: clean up environment for when regist...
2005-08-21 Thomas Vander Stichelecheck/Makefile.am: don't valgrind the controller test...
2005-08-20 Thomas Vander Stichelecheck/Makefile.am: set GST_TOOLS_DIR
2005-08-20 Thomas Vander Stichelemove check stuff to its own library to be used by other...